]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/blob - fs/compat_binfmt_elf.c
ARM: OMAP5/DRA7: hwmod: add ADDR_TYPE_RT to bb2d address flags
[android-sdk/kernel-video.git] / fs / compat_binfmt_elf.c
1 /*
2  * 32-bit compatibility support for ELF format executables and core dumps.
3  *
4  * Copyright (C) 2007 Red Hat, Inc.  All rights reserved.
5  *
6  * This copyrighted material is made available to anyone wishing to use,
7  * modify, copy, or redistribute it subject to the terms and conditions
8  * of the GNU General Public License v.2.
9  *
10  * Red Hat Author: Roland McGrath.
11  *
12  * This file is used in a 64-bit kernel that wants to support 32-bit ELF.
13  * asm/elf.h is responsible for defining the compat_* and COMPAT_* macros
14  * used below, with definitions appropriate for 32-bit ABI compatibility.
15  *
16  * We use macros to rename the ABI types and machine-dependent
17  * functions used in binfmt_elf.c to compat versions.
18  */
20 #include <linux/elfcore-compat.h>
21 #include <linux/time.h>
23 /*
24  * Rename the basic ELF layout types to refer to the 32-bit class of files.
25  */
26 #undef  ELF_CLASS
27 #define ELF_CLASS       ELFCLASS32
29 #undef  elfhdr
30 #undef  elf_phdr
31 #undef  elf_shdr
32 #undef  elf_note
33 #undef  elf_addr_t
34 #define elfhdr          elf32_hdr
35 #define elf_phdr        elf32_phdr
36 #define elf_shdr        elf32_shdr
37 #define elf_note        elf32_note
38 #define elf_addr_t      Elf32_Addr
40 /*
41  * Some data types as stored in coredump.
42  */
43 #define user_long_t             compat_long_t
44 #define user_siginfo_t          compat_siginfo_t
45 #define copy_siginfo_to_user    copy_siginfo_to_user32
47 /*
48  * The machine-dependent core note format types are defined in elfcore-compat.h,
49  * which requires asm/elf.h to define compat_elf_gregset_t et al.
50  */
51 #define elf_prstatus    compat_elf_prstatus
52 #define elf_prpsinfo    compat_elf_prpsinfo
54 /*
55  * Compat version of cputime_to_compat_timeval, perhaps this
56  * should be an inline in <linux/compat.h>.
57  */
58 static void cputime_to_compat_timeval(const cputime_t cputime,
59                                       struct compat_timeval *value)
60 {
61         struct timeval tv;
62         cputime_to_timeval(cputime, &tv);
63         value->tv_sec = tv.tv_sec;
64         value->tv_usec = tv.tv_usec;
65 }
67 #undef cputime_to_timeval
68 #define cputime_to_timeval cputime_to_compat_timeval
71 /*
72  * To use this file, asm/elf.h must define compat_elf_check_arch.
73  * The other following macros can be defined if the compat versions
74  * differ from the native ones, or omitted when they match.
75  */
77 #undef  ELF_ARCH
78 #undef  elf_check_arch
79 #define elf_check_arch  compat_elf_check_arch
81 #ifdef  COMPAT_ELF_PLATFORM
82 #undef  ELF_PLATFORM
83 #define ELF_PLATFORM            COMPAT_ELF_PLATFORM
84 #endif
86 #ifdef  COMPAT_ELF_HWCAP
87 #undef  ELF_HWCAP
88 #define ELF_HWCAP               COMPAT_ELF_HWCAP
89 #endif
91 #ifdef  COMPAT_ARCH_DLINFO
92 #undef  ARCH_DLINFO
93 #define ARCH_DLINFO             COMPAT_ARCH_DLINFO
94 #endif
96 #ifdef  COMPAT_ELF_ET_DYN_BASE
97 #undef  ELF_ET_DYN_BASE
98 #define ELF_ET_DYN_BASE         COMPAT_ELF_ET_DYN_BASE
99 #endif
101 #ifdef COMPAT_ELF_EXEC_PAGESIZE
102 #undef  ELF_EXEC_PAGESIZE
103 #define ELF_EXEC_PAGESIZE       COMPAT_ELF_EXEC_PAGESIZE
104 #endif
106 #ifdef  COMPAT_ELF_PLAT_INIT
107 #undef  ELF_PLAT_INIT
108 #define ELF_PLAT_INIT           COMPAT_ELF_PLAT_INIT
109 #endif
111 #ifdef  COMPAT_SET_PERSONALITY
112 #undef  SET_PERSONALITY
113 #define SET_PERSONALITY         COMPAT_SET_PERSONALITY
114 #endif
116 #ifdef  compat_start_thread
117 #undef  start_thread
118 #define start_thread            compat_start_thread
119 #endif
121 #ifdef  compat_arch_setup_additional_pages
122 #undef  ARCH_HAS_SETUP_ADDITIONAL_PAGES
123 #define ARCH_HAS_SETUP_ADDITIONAL_PAGES 1
124 #undef  arch_setup_additional_pages
125 #define arch_setup_additional_pages compat_arch_setup_additional_pages
126 #endif
128 /*
129  * Rename a few of the symbols that binfmt_elf.c will define.
130  * These are all local so the names don't really matter, but it
131  * might make some debugging less confusing not to duplicate them.
132  */
133 #define elf_format              compat_elf_format
134 #define init_elf_binfmt         init_compat_elf_binfmt
135 #define exit_elf_binfmt         exit_compat_elf_binfmt
137 /*
138  * We share all the actual code with the native (64-bit) version.
139  */
140 #include "binfmt_elf.c"