1 /*
2 * linux/fs/file_table.c
3 *
4 * Copyright (C) 1991, 1992 Linus Torvalds
5 * Copyright (C) 1997 David S. Miller (davem@caip.rutgers.edu)
6 */
8 #include <linux/string.h>
9 #include <linux/slab.h>
10 #include <linux/file.h>
11 #include <linux/fdtable.h>
12 #include <linux/init.h>
13 #include <linux/module.h>
14 #include <linux/fs.h>
15 #include <linux/security.h>
16 #include <linux/eventpoll.h>
17 #include <linux/rcupdate.h>
18 #include <linux/mount.h>
19 #include <linux/capability.h>
20 #include <linux/cdev.h>
21 #include <linux/fsnotify.h>
22 #include <linux/sysctl.h>
23 #include <linux/lglock.h>
24 #include <linux/percpu_counter.h>
25 #include <linux/percpu.h>
26 #include <linux/hardirq.h>
27 #include <linux/task_work.h>
28 #include <linux/ima.h>
30 #include <linux/atomic.h>
32 #include "internal.h"
34 /* sysctl tunables... */
35 struct files_stat_struct files_stat = {
36 .max_files = NR_FILE
37 };
39 DEFINE_STATIC_LGLOCK(files_lglock);
41 /* SLAB cache for file structures */
42 static struct kmem_cache *filp_cachep __read_mostly;
44 static struct percpu_counter nr_files __cacheline_aligned_in_smp;
46 static void file_free_rcu(struct rcu_head *head)
47 {
48 struct file *f = container_of(head, struct file, f_u.fu_rcuhead);
50 put_cred(f->f_cred);
51 kmem_cache_free(filp_cachep, f);
52 }
54 static inline void file_free(struct file *f)
55 {
56 percpu_counter_dec(&nr_files);
57 file_check_state(f);
58 call_rcu(&f->f_u.fu_rcuhead, file_free_rcu);
59 }
61 /*
62 * Return the total number of open files in the system
63 */
64 static long get_nr_files(void)
65 {
66 return percpu_counter_read_positive(&nr_files);
67 }
69 /*
70 * Return the maximum number of open files in the system
71 */
72 unsigned long get_max_files(void)
73 {
74 return files_stat.max_files;
75 }
76 EXPORT_SYMBOL_GPL(get_max_files);
78 /*
79 * Handle nr_files sysctl
80 */
81 #if defined(CONFIG_SYSCTL) && defined(CONFIG_PROC_FS)
82 int proc_nr_files(ctl_table *table, int write,
83 void __user *buffer, size_t *lenp, loff_t *ppos)
84 {
85 files_stat.nr_files = get_nr_files();
86 return proc_doulongvec_minmax(table, write, buffer, lenp, ppos);
87 }
88 #else
89 int proc_nr_files(ctl_table *table, int write,
90 void __user *buffer, size_t *lenp, loff_t *ppos)
91 {
92 return -ENOSYS;
93 }
94 #endif
96 /* Find an unused file structure and return a pointer to it.
97 * Returns NULL, if there are no more free file structures or
98 * we run out of memory.
99 *
100 * Be very careful using this. You are responsible for
101 * getting write access to any mount that you might assign
102 * to this filp, if it is opened for write. If this is not
103 * done, you will imbalance int the mount's writer count
104 * and a warning at __fput() time.
105 */
106 struct file *get_empty_filp(void)
107 {
108 const struct cred *cred = current_cred();
109 static long old_max;
110 struct file * f;
112 /*
113 * Privileged users can go above max_files
114 */
115 if (get_nr_files() >= files_stat.max_files && !capable(CAP_SYS_ADMIN)) {
116 /*
117 * percpu_counters are inaccurate. Do an expensive check before
118 * we go and fail.
119 */
120 if (percpu_counter_sum_positive(&nr_files) >= files_stat.max_files)
121 goto over;
122 }
124 f = kmem_cache_zalloc(filp_cachep, GFP_KERNEL);
125 if (f == NULL)
126 goto fail;
128 percpu_counter_inc(&nr_files);
129 f->f_cred = get_cred(cred);
130 if (security_file_alloc(f))
131 goto fail_sec;
133 INIT_LIST_HEAD(&f->f_u.fu_list);
134 atomic_long_set(&f->f_count, 1);
135 rwlock_init(&f->f_owner.lock);
136 spin_lock_init(&f->f_lock);
137 eventpoll_init_file(f);
138 /* f->f_version: 0 */
139 return f;
141 over:
142 /* Ran out of filps - report that */
143 if (get_nr_files() > old_max) {
144 pr_info("VFS: file-max limit %lu reached\n", get_max_files());
145 old_max = get_nr_files();
146 }
147 goto fail;
149 fail_sec:
150 file_free(f);
151 fail:
152 return NULL;
153 }
155 /**
156 * alloc_file - allocate and initialize a 'struct file'
157 * @mnt: the vfsmount on which the file will reside
158 * @dentry: the dentry representing the new file
159 * @mode: the mode with which the new file will be opened
160 * @fop: the 'struct file_operations' for the new file
161 *
162 * Use this instead of get_empty_filp() to get a new
163 * 'struct file'. Do so because of the same initialization
164 * pitfalls reasons listed for init_file(). This is a
165 * preferred interface to using init_file().
166 *
167 * If all the callers of init_file() are eliminated, its
168 * code should be moved into this function.
169 */
170 struct file *alloc_file(struct path *path, fmode_t mode,
171 const struct file_operations *fop)
172 {
173 struct file *file;
175 file = get_empty_filp();
176 if (!file)
177 return NULL;
179 file->f_path = *path;
180 file->f_mapping = path->dentry->d_inode->i_mapping;
181 file->f_mode = mode;
182 file->f_op = fop;
184 /*
185 * These mounts don't really matter in practice
186 * for r/o bind mounts. They aren't userspace-
187 * visible. We do this for consistency, and so
188 * that we can do debugging checks at __fput()
189 */
190 if ((mode & FMODE_WRITE) && !special_file(path->dentry->d_inode->i_mode)) {
191 file_take_write(file);
192 WARN_ON(mnt_clone_write(path->mnt));
193 }
194 if ((mode & (FMODE_READ | FMODE_WRITE)) == FMODE_READ)
195 i_readcount_inc(path->dentry->d_inode);
196 return file;
197 }
198 EXPORT_SYMBOL(alloc_file);
200 /**
201 * drop_file_write_access - give up ability to write to a file
202 * @file: the file to which we will stop writing
203 *
204 * This is a central place which will give up the ability
205 * to write to @file, along with access to write through
206 * its vfsmount.
207 */
208 static void drop_file_write_access(struct file *file)
209 {
210 struct vfsmount *mnt = file->f_path.mnt;
211 struct dentry *dentry = file->f_path.dentry;
212 struct inode *inode = dentry->d_inode;
214 put_write_access(inode);
216 if (special_file(inode->i_mode))
217 return;
218 if (file_check_writeable(file) != 0)
219 return;
220 __mnt_drop_write(mnt);
221 file_release_write(file);
222 }
224 /* the real guts of fput() - releasing the last reference to file
225 */
226 static void __fput(struct file *file)
227 {
228 struct dentry *dentry = file->f_path.dentry;
229 struct vfsmount *mnt = file->f_path.mnt;
230 struct inode *inode = dentry->d_inode;
232 might_sleep();
234 fsnotify_close(file);
235 /*
236 * The function eventpoll_release() should be the first called
237 * in the file cleanup chain.
238 */
239 eventpoll_release(file);
240 locks_remove_flock(file);
242 if (unlikely(file->f_flags & FASYNC)) {
243 if (file->f_op && file->f_op->fasync)
244 file->f_op->fasync(-1, file, 0);
245 }
246 ima_file_free(file);
247 if (file->f_op && file->f_op->release)
248 file->f_op->release(inode, file);
249 security_file_free(file);
250 if (unlikely(S_ISCHR(inode->i_mode) && inode->i_cdev != NULL &&
251 !(file->f_mode & FMODE_PATH))) {
252 cdev_put(inode->i_cdev);
253 }
254 fops_put(file->f_op);
255 put_pid(file->f_owner.pid);
256 if ((file->f_mode & (FMODE_READ | FMODE_WRITE)) == FMODE_READ)
257 i_readcount_dec(inode);
258 if (file->f_mode & FMODE_WRITE)
259 drop_file_write_access(file);
260 file->f_path.dentry = NULL;
261 file->f_path.mnt = NULL;
262 file_free(file);
263 dput(dentry);
264 mntput(mnt);
265 }
267 static DEFINE_SPINLOCK(delayed_fput_lock);
268 static LIST_HEAD(delayed_fput_list);
269 static void delayed_fput(struct work_struct *unused)
270 {
271 LIST_HEAD(head);
272 spin_lock_irq(&delayed_fput_lock);
273 list_splice_init(&delayed_fput_list, &head);
274 spin_unlock_irq(&delayed_fput_lock);
275 while (!list_empty(&head)) {
276 struct file *f = list_first_entry(&head, struct file, f_u.fu_list);
277 list_del_init(&f->f_u.fu_list);
278 __fput(f);
279 }
280 }
282 static void ____fput(struct callback_head *work)
283 {
284 __fput(container_of(work, struct file, f_u.fu_rcuhead));
285 }
287 /*
288 * If kernel thread really needs to have the final fput() it has done
289 * to complete, call this. The only user right now is the boot - we
290 * *do* need to make sure our writes to binaries on initramfs has
291 * not left us with opened struct file waiting for __fput() - execve()
292 * won't work without that. Please, don't add more callers without
293 * very good reasons; in particular, never call that with locks
294 * held and never call that from a thread that might need to do
295 * some work on any kind of umount.
296 */
297 void flush_delayed_fput(void)
298 {
299 delayed_fput(NULL);
300 }
302 static DECLARE_WORK(delayed_fput_work, delayed_fput);
304 void fput(struct file *file)
305 {
306 if (atomic_long_dec_and_test(&file->f_count)) {
307 struct task_struct *task = current;
308 file_sb_list_del(file);
309 if (unlikely(in_interrupt() || task->flags & PF_KTHREAD)) {
310 unsigned long flags;
311 spin_lock_irqsave(&delayed_fput_lock, flags);
312 list_add(&file->f_u.fu_list, &delayed_fput_list);
313 schedule_work(&delayed_fput_work);
314 spin_unlock_irqrestore(&delayed_fput_lock, flags);
315 return;
316 }
317 init_task_work(&file->f_u.fu_rcuhead, ____fput);
318 task_work_add(task, &file->f_u.fu_rcuhead, true);
319 }
320 }
322 /*
323 * synchronous analog of fput(); for kernel threads that might be needed
324 * in some umount() (and thus can't use flush_delayed_fput() without
325 * risking deadlocks), need to wait for completion of __fput() and know
326 * for this specific struct file it won't involve anything that would
327 * need them. Use only if you really need it - at the very least,
328 * don't blindly convert fput() by kernel thread to that.
329 */
330 void __fput_sync(struct file *file)
331 {
332 if (atomic_long_dec_and_test(&file->f_count)) {
333 struct task_struct *task = current;
334 file_sb_list_del(file);
335 BUG_ON(!(task->flags & PF_KTHREAD));
336 __fput(file);
337 }
338 }
340 EXPORT_SYMBOL(fput);
342 void put_filp(struct file *file)
343 {
344 if (atomic_long_dec_and_test(&file->f_count)) {
345 security_file_free(file);
346 file_sb_list_del(file);
347 file_free(file);
348 }
349 }
351 static inline int file_list_cpu(struct file *file)
352 {
353 #ifdef CONFIG_SMP
354 return file->f_sb_list_cpu;
355 #else
356 return smp_processor_id();
357 #endif
358 }
360 /* helper for file_sb_list_add to reduce ifdefs */
361 static inline void __file_sb_list_add(struct file *file, struct super_block *sb)
362 {
363 struct list_head *list;
364 #ifdef CONFIG_SMP
365 int cpu;
366 cpu = smp_processor_id();
367 file->f_sb_list_cpu = cpu;
368 list = per_cpu_ptr(sb->s_files, cpu);
369 #else
370 list = &sb->s_files;
371 #endif
372 list_add(&file->f_u.fu_list, list);
373 }
375 /**
376 * file_sb_list_add - add a file to the sb's file list
377 * @file: file to add
378 * @sb: sb to add it to
379 *
380 * Use this function to associate a file with the superblock of the inode it
381 * refers to.
382 */
383 void file_sb_list_add(struct file *file, struct super_block *sb)
384 {
385 lg_local_lock(&files_lglock);
386 __file_sb_list_add(file, sb);
387 lg_local_unlock(&files_lglock);
388 }
390 /**
391 * file_sb_list_del - remove a file from the sb's file list
392 * @file: file to remove
393 * @sb: sb to remove it from
394 *
395 * Use this function to remove a file from its superblock.
396 */
397 void file_sb_list_del(struct file *file)
398 {
399 if (!list_empty(&file->f_u.fu_list)) {
400 lg_local_lock_cpu(&files_lglock, file_list_cpu(file));
401 list_del_init(&file->f_u.fu_list);
402 lg_local_unlock_cpu(&files_lglock, file_list_cpu(file));
403 }
404 }
406 #ifdef CONFIG_SMP
408 /*
409 * These macros iterate all files on all CPUs for a given superblock.
410 * files_lglock must be held globally.
411 */
412 #define do_file_list_for_each_entry(__sb, __file) \
413 { \
414 int i; \
415 for_each_possible_cpu(i) { \
416 struct list_head *list; \
417 list = per_cpu_ptr((__sb)->s_files, i); \
418 list_for_each_entry((__file), list, f_u.fu_list)
420 #define while_file_list_for_each_entry \
421 } \
422 }
424 #else
426 #define do_file_list_for_each_entry(__sb, __file) \
427 { \
428 struct list_head *list; \
429 list = &(sb)->s_files; \
430 list_for_each_entry((__file), list, f_u.fu_list)
432 #define while_file_list_for_each_entry \
433 }
435 #endif
437 /**
438 * mark_files_ro - mark all files read-only
439 * @sb: superblock in question
440 *
441 * All files are marked read-only. We don't care about pending
442 * delete files so this should be used in 'force' mode only.
443 */
444 void mark_files_ro(struct super_block *sb)
445 {
446 struct file *f;
448 lg_global_lock(&files_lglock);
449 do_file_list_for_each_entry(sb, f) {
450 if (!S_ISREG(f->f_path.dentry->d_inode->i_mode))
451 continue;
452 if (!file_count(f))
453 continue;
454 if (!(f->f_mode & FMODE_WRITE))
455 continue;
456 spin_lock(&f->f_lock);
457 f->f_mode &= ~FMODE_WRITE;
458 spin_unlock(&f->f_lock);
459 if (file_check_writeable(f) != 0)
460 continue;
461 __mnt_drop_write(f->f_path.mnt);
462 file_release_write(f);
463 } while_file_list_for_each_entry;
464 lg_global_unlock(&files_lglock);
465 }
467 void __init files_init(unsigned long mempages)
468 {
469 unsigned long n;
471 filp_cachep = kmem_cache_create("filp", sizeof(struct file), 0,
472 SLAB_HWCACHE_ALIGN | SLAB_PANIC, NULL);
474 /*
475 * One file with associated inode and dcache is very roughly 1K.
476 * Per default don't use more than 10% of our memory for files.
477 */
479 n = (mempages * (PAGE_SIZE / 1024)) / 10;
480 files_stat.max_files = max_t(unsigned long, n, NR_FILE);
481 files_defer_init();
482 lg_lock_init(&files_lglock, "files_lglock");
483 percpu_counter_init(&nr_files, 0);
484 }