]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/blob - fs/seq_file.c
ARM: OMAP5/DRA7: hwmod: add ADDR_TYPE_RT to bb2d address flags
[android-sdk/kernel-video.git] / fs / seq_file.c
1 /*
2  * linux/fs/seq_file.c
3  *
4  * helper functions for making synthetic files from sequences of records.
5  * initial implementation -- AV, Oct 2001.
6  */
8 #include <linux/fs.h>
9 #include <linux/export.h>
10 #include <linux/seq_file.h>
11 #include <linux/slab.h>
12 #include <linux/cred.h>
14 #include <asm/uaccess.h>
15 #include <asm/page.h>
18 /*
19  * seq_files have a buffer which can may overflow. When this happens a larger
20  * buffer is reallocated and all the data will be printed again.
21  * The overflow state is true when m->count == m->size.
22  */
23 static bool seq_overflow(struct seq_file *m)
24 {
25         return m->count == m->size;
26 }
28 static void seq_set_overflow(struct seq_file *m)
29 {
30         m->count = m->size;
31 }
33 /**
34  *      seq_open -      initialize sequential file
35  *      @file: file we initialize
36  *      @op: method table describing the sequence
37  *
38  *      seq_open() sets @file, associating it with a sequence described
39  *      by @op.  @op->start() sets the iterator up and returns the first
40  *      element of sequence. @op->stop() shuts it down.  @op->next()
41  *      returns the next element of sequence.  @op->show() prints element
42  *      into the buffer.  In case of error ->start() and ->next() return
43  *      ERR_PTR(error).  In the end of sequence they return %NULL. ->show()
44  *      returns 0 in case of success and negative number in case of error.
45  *      Returning SEQ_SKIP means "discard this element and move on".
46  */
47 int seq_open(struct file *file, const struct seq_operations *op)
48 {
49         struct seq_file *p = file->private_data;
51         if (!p) {
52                 p = kmalloc(sizeof(*p), GFP_KERNEL);
53                 if (!p)
54                         return -ENOMEM;
55                 file->private_data = p;
56         }
57         memset(p, 0, sizeof(*p));
58         mutex_init(&p->lock);
59         p->op = op;
60 #ifdef CONFIG_USER_NS
61         p->user_ns = file->f_cred->user_ns;
62 #endif
64         /*
65          * Wrappers around seq_open(e.g. swaps_open) need to be
66          * aware of this. If they set f_version themselves, they
67          * should call seq_open first and then set f_version.
68          */
69         file->f_version = 0;
71         /*
72          * seq_files support lseek() and pread().  They do not implement
73          * write() at all, but we clear FMODE_PWRITE here for historical
74          * reasons.
75          *
76          * If a client of seq_files a) implements file.write() and b) wishes to
77          * support pwrite() then that client will need to implement its own
78          * file.open() which calls seq_open() and then sets FMODE_PWRITE.
79          */
80         file->f_mode &= ~FMODE_PWRITE;
81         return 0;
82 }
83 EXPORT_SYMBOL(seq_open);
85 static int traverse(struct seq_file *m, loff_t offset)
86 {
87         loff_t pos = 0, index;
88         int error = 0;
89         void *p;
91         m->version = 0;
92         index = 0;
93         m->count = m->from = 0;
94         if (!offset) {
95                 m->index = index;
96                 return 0;
97         }
98         if (!m->buf) {
99                 m->buf = kmalloc(m->size = PAGE_SIZE, GFP_KERNEL);
100                 if (!m->buf)
101                         return -ENOMEM;
102         }
103         p = m->op->start(m, &index);
104         while (p) {
105                 error = PTR_ERR(p);
106                 if (IS_ERR(p))
107                         break;
108                 error = m->op->show(m, p);
109                 if (error < 0)
110                         break;
111                 if (unlikely(error)) {
112                         error = 0;
113                         m->count = 0;
114                 }
115                 if (seq_overflow(m))
116                         goto Eoverflow;
117                 if (pos + m->count > offset) {
118                         m->from = offset - pos;
119                         m->count -= m->from;
120                         m->index = index;
121                         break;
122                 }
123                 pos += m->count;
124                 m->count = 0;
125                 if (pos == offset) {
126                         index++;
127                         m->index = index;
128                         break;
129                 }
130                 p = m->op->next(m, p, &index);
131         }
132         m->op->stop(m, p);
133         m->index = index;
134         return error;
136 Eoverflow:
137         m->op->stop(m, p);
138         kfree(m->buf);
139         m->buf = kmalloc(m->size <<= 1, GFP_KERNEL);
140         return !m->buf ? -ENOMEM : -EAGAIN;
143 /**
144  *      seq_read -      ->read() method for sequential files.
145  *      @file: the file to read from
146  *      @buf: the buffer to read to
147  *      @size: the maximum number of bytes to read
148  *      @ppos: the current position in the file
149  *
150  *      Ready-made ->f_op->read()
151  */
152 ssize_t seq_read(struct file *file, char __user *buf, size_t size, loff_t *ppos)
154         struct seq_file *m = file->private_data;
155         size_t copied = 0;
156         loff_t pos;
157         size_t n;
158         void *p;
159         int err = 0;
161         mutex_lock(&m->lock);
163         /*
164          * seq_file->op->..m_start/m_stop/m_next may do special actions
165          * or optimisations based on the file->f_version, so we want to
166          * pass the file->f_version to those methods.
167          *
168          * seq_file->version is just copy of f_version, and seq_file
169          * methods can treat it simply as file version.
170          * It is copied in first and copied out after all operations.
171          * It is convenient to have it as  part of structure to avoid the
172          * need of passing another argument to all the seq_file methods.
173          */
174         m->version = file->f_version;
176         /* Don't assume *ppos is where we left it */
177         if (unlikely(*ppos != m->read_pos)) {
178                 while ((err = traverse(m, *ppos)) == -EAGAIN)
179                         ;
180                 if (err) {
181                         /* With prejudice... */
182                         m->read_pos = 0;
183                         m->version = 0;
184                         m->index = 0;
185                         m->count = 0;
186                         goto Done;
187                 } else {
188                         m->read_pos = *ppos;
189                 }
190         }
192         /* grab buffer if we didn't have one */
193         if (!m->buf) {
194                 m->buf = kmalloc(m->size = PAGE_SIZE, GFP_KERNEL);
195                 if (!m->buf)
196                         goto Enomem;
197         }
198         /* if not empty - flush it first */
199         if (m->count) {
200                 n = min(m->count, size);
201                 err = copy_to_user(buf, m->buf + m->from, n);
202                 if (err)
203                         goto Efault;
204                 m->count -= n;
205                 m->from += n;
206                 size -= n;
207                 buf += n;
208                 copied += n;
209                 if (!m->count)
210                         m->index++;
211                 if (!size)
212                         goto Done;
213         }
214         /* we need at least one record in buffer */
215         pos = m->index;
216         p = m->op->start(m, &pos);
217         while (1) {
218                 err = PTR_ERR(p);
219                 if (!p || IS_ERR(p))
220                         break;
221                 err = m->op->show(m, p);
222                 if (err < 0)
223                         break;
224                 if (unlikely(err))
225                         m->count = 0;
226                 if (unlikely(!m->count)) {
227                         p = m->op->next(m, p, &pos);
228                         m->index = pos;
229                         continue;
230                 }
231                 if (m->count < m->size)
232                         goto Fill;
233                 m->op->stop(m, p);
234                 kfree(m->buf);
235                 m->buf = kmalloc(m->size <<= 1, GFP_KERNEL);
236                 if (!m->buf)
237                         goto Enomem;
238                 m->count = 0;
239                 m->version = 0;
240                 pos = m->index;
241                 p = m->op->start(m, &pos);
242         }
243         m->op->stop(m, p);
244         m->count = 0;
245         goto Done;
246 Fill:
247         /* they want more? let's try to get some more */
248         while (m->count < size) {
249                 size_t offs = m->count;
250                 loff_t next = pos;
251                 p = m->op->next(m, p, &next);
252                 if (!p || IS_ERR(p)) {
253                         err = PTR_ERR(p);
254                         break;
255                 }
256                 err = m->op->show(m, p);
257                 if (seq_overflow(m) || err) {
258                         m->count = offs;
259                         if (likely(err <= 0))
260                                 break;
261                 }
262                 pos = next;
263         }
264         m->op->stop(m, p);
265         n = min(m->count, size);
266         err = copy_to_user(buf, m->buf, n);
267         if (err)
268                 goto Efault;
269         copied += n;
270         m->count -= n;
271         if (m->count)
272                 m->from = n;
273         else
274                 pos++;
275         m->index = pos;
276 Done:
277         if (!copied)
278                 copied = err;
279         else {
280                 *ppos += copied;
281                 m->read_pos += copied;
282         }
283         file->f_version = m->version;
284         mutex_unlock(&m->lock);
285         return copied;
286 Enomem:
287         err = -ENOMEM;
288         goto Done;
289 Efault:
290         err = -EFAULT;
291         goto Done;
293 EXPORT_SYMBOL(seq_read);
295 /**
296  *      seq_lseek -     ->llseek() method for sequential files.
297  *      @file: the file in question
298  *      @offset: new position
299  *      @whence: 0 for absolute, 1 for relative position
300  *
301  *      Ready-made ->f_op->llseek()
302  */
303 loff_t seq_lseek(struct file *file, loff_t offset, int whence)
305         struct seq_file *m = file->private_data;
306         loff_t retval = -EINVAL;
308         mutex_lock(&m->lock);
309         m->version = file->f_version;
310         switch (whence) {
311                 case 1:
312                         offset += file->f_pos;
313                 case 0:
314                         if (offset < 0)
315                                 break;
316                         retval = offset;
317                         if (offset != m->read_pos) {
318                                 while ((retval=traverse(m, offset)) == -EAGAIN)
319                                         ;
320                                 if (retval) {
321                                         /* with extreme prejudice... */
322                                         file->f_pos = 0;
323                                         m->read_pos = 0;
324                                         m->version = 0;
325                                         m->index = 0;
326                                         m->count = 0;
327                                 } else {
328                                         m->read_pos = offset;
329                                         retval = file->f_pos = offset;
330                                 }
331                         }
332         }
333         file->f_version = m->version;
334         mutex_unlock(&m->lock);
335         return retval;
337 EXPORT_SYMBOL(seq_lseek);
339 /**
340  *      seq_release -   free the structures associated with sequential file.
341  *      @file: file in question
342  *      @inode: file->f_path.dentry->d_inode
343  *
344  *      Frees the structures associated with sequential file; can be used
345  *      as ->f_op->release() if you don't have private data to destroy.
346  */
347 int seq_release(struct inode *inode, struct file *file)
349         struct seq_file *m = file->private_data;
350         kfree(m->buf);
351         kfree(m);
352         return 0;
354 EXPORT_SYMBOL(seq_release);
356 /**
357  *      seq_escape -    print string into buffer, escaping some characters
358  *      @m:     target buffer
359  *      @s:     string
360  *      @esc:   set of characters that need escaping
361  *
362  *      Puts string into buffer, replacing each occurrence of character from
363  *      @esc with usual octal escape.  Returns 0 in case of success, -1 - in
364  *      case of overflow.
365  */
366 int seq_escape(struct seq_file *m, const char *s, const char *esc)
368         char *end = m->buf + m->size;
369         char *p;
370         char c;
372         for (p = m->buf + m->count; (c = *s) != '\0' && p < end; s++) {
373                 if (!strchr(esc, c)) {
374                         *p++ = c;
375                         continue;
376                 }
377                 if (p + 3 < end) {
378                         *p++ = '\\';
379                         *p++ = '0' + ((c & 0300) >> 6);
380                         *p++ = '0' + ((c & 070) >> 3);
381                         *p++ = '0' + (c & 07);
382                         continue;
383                 }
384                 seq_set_overflow(m);
385                 return -1;
386         }
387         m->count = p - m->buf;
388         return 0;
390 EXPORT_SYMBOL(seq_escape);
392 int seq_vprintf(struct seq_file *m, const char *f, va_list args)
394         int len;
396         if (m->count < m->size) {
397                 len = vsnprintf(m->buf + m->count, m->size - m->count, f, args);
398                 if (m->count + len < m->size) {
399                         m->count += len;
400                         return 0;
401                 }
402         }
403         seq_set_overflow(m);
404         return -1;
406 EXPORT_SYMBOL(seq_vprintf);
408 int seq_printf(struct seq_file *m, const char *f, ...)
410         int ret;
411         va_list args;
413         va_start(args, f);
414         ret = seq_vprintf(m, f, args);
415         va_end(args);
417         return ret;
419 EXPORT_SYMBOL(seq_printf);
421 /**
422  *      mangle_path -   mangle and copy path to buffer beginning
423  *      @s: buffer start
424  *      @p: beginning of path in above buffer
425  *      @esc: set of characters that need escaping
426  *
427  *      Copy the path from @p to @s, replacing each occurrence of character from
428  *      @esc with usual octal escape.
429  *      Returns pointer past last written character in @s, or NULL in case of
430  *      failure.
431  */
432 char *mangle_path(char *s, const char *p, const char *esc)
434         while (s <= p) {
435                 char c = *p++;
436                 if (!c) {
437                         return s;
438                 } else if (!strchr(esc, c)) {
439                         *s++ = c;
440                 } else if (s + 4 > p) {
441                         break;
442                 } else {
443                         *s++ = '\\';
444                         *s++ = '0' + ((c & 0300) >> 6);
445                         *s++ = '0' + ((c & 070) >> 3);
446                         *s++ = '0' + (c & 07);
447                 }
448         }
449         return NULL;
451 EXPORT_SYMBOL(mangle_path);
453 /**
454  * seq_path - seq_file interface to print a pathname
455  * @m: the seq_file handle
456  * @path: the struct path to print
457  * @esc: set of characters to escape in the output
458  *
459  * return the absolute path of 'path', as represented by the
460  * dentry / mnt pair in the path parameter.
461  */
462 int seq_path(struct seq_file *m, const struct path *path, const char *esc)
464         char *buf;
465         size_t size = seq_get_buf(m, &buf);
466         int res = -1;
468         if (size) {
469                 char *p = d_path(path, buf, size);
470                 if (!IS_ERR(p)) {
471                         char *end = mangle_path(buf, p, esc);
472                         if (end)
473                                 res = end - buf;
474                 }
475         }
476         seq_commit(m, res);
478         return res;
480 EXPORT_SYMBOL(seq_path);
482 /*
483  * Same as seq_path, but relative to supplied root.
484  */
485 int seq_path_root(struct seq_file *m, const struct path *path,
486                   const struct path *root, const char *esc)
488         char *buf;
489         size_t size = seq_get_buf(m, &buf);
490         int res = -ENAMETOOLONG;
492         if (size) {
493                 char *p;
495                 p = __d_path(path, root, buf, size);
496                 if (!p)
497                         return SEQ_SKIP;
498                 res = PTR_ERR(p);
499                 if (!IS_ERR(p)) {
500                         char *end = mangle_path(buf, p, esc);
501                         if (end)
502                                 res = end - buf;
503                         else
504                                 res = -ENAMETOOLONG;
505                 }
506         }
507         seq_commit(m, res);
509         return res < 0 && res != -ENAMETOOLONG ? res : 0;
512 /*
513  * returns the path of the 'dentry' from the root of its filesystem.
514  */
515 int seq_dentry(struct seq_file *m, struct dentry *dentry, const char *esc)
517         char *buf;
518         size_t size = seq_get_buf(m, &buf);
519         int res = -1;
521         if (size) {
522                 char *p = dentry_path(dentry, buf, size);
523                 if (!IS_ERR(p)) {
524                         char *end = mangle_path(buf, p, esc);
525                         if (end)
526                                 res = end - buf;
527                 }
528         }
529         seq_commit(m, res);
531         return res;
534 int seq_bitmap(struct seq_file *m, const unsigned long *bits,
535                                    unsigned int nr_bits)
537         if (m->count < m->size) {
538                 int len = bitmap_scnprintf(m->buf + m->count,
539                                 m->size - m->count, bits, nr_bits);
540                 if (m->count + len < m->size) {
541                         m->count += len;
542                         return 0;
543                 }
544         }
545         seq_set_overflow(m);
546         return -1;
548 EXPORT_SYMBOL(seq_bitmap);
550 int seq_bitmap_list(struct seq_file *m, const unsigned long *bits,
551                 unsigned int nr_bits)
553         if (m->count < m->size) {
554                 int len = bitmap_scnlistprintf(m->buf + m->count,
555                                 m->size - m->count, bits, nr_bits);
556                 if (m->count + len < m->size) {
557                         m->count += len;
558                         return 0;
559                 }
560         }
561         seq_set_overflow(m);
562         return -1;
564 EXPORT_SYMBOL(seq_bitmap_list);
566 static void *single_start(struct seq_file *p, loff_t *pos)
568         return NULL + (*pos == 0);
571 static void *single_next(struct seq_file *p, void *v, loff_t *pos)
573         ++*pos;
574         return NULL;
577 static void single_stop(struct seq_file *p, void *v)
581 int single_open(struct file *file, int (*show)(struct seq_file *, void *),
582                 void *data)
584         struct seq_operations *op = kmalloc(sizeof(*op), GFP_KERNEL);
585         int res = -ENOMEM;
587         if (op) {
588                 op->start = single_start;
589                 op->next = single_next;
590                 op->stop = single_stop;
591                 op->show = show;
592                 res = seq_open(file, op);
593                 if (!res)
594                         ((struct seq_file *)file->private_data)->private = data;
595                 else
596                         kfree(op);
597         }
598         return res;
600 EXPORT_SYMBOL(single_open);
602 int single_release(struct inode *inode, struct file *file)
604         const struct seq_operations *op = ((struct seq_file *)file->private_data)->op;
605         int res = seq_release(inode, file);
606         kfree(op);
607         return res;
609 EXPORT_SYMBOL(single_release);
611 int seq_release_private(struct inode *inode, struct file *file)
613         struct seq_file *seq = file->private_data;
615         kfree(seq->private);
616         seq->private = NULL;
617         return seq_release(inode, file);
619 EXPORT_SYMBOL(seq_release_private);
621 void *__seq_open_private(struct file *f, const struct seq_operations *ops,
622                 int psize)
624         int rc;
625         void *private;
626         struct seq_file *seq;
628         private = kzalloc(psize, GFP_KERNEL);
629         if (private == NULL)
630                 goto out;
632         rc = seq_open(f, ops);
633         if (rc < 0)
634                 goto out_free;
636         seq = f->private_data;
637         seq->private = private;
638         return private;
640 out_free:
641         kfree(private);
642 out:
643         return NULL;
645 EXPORT_SYMBOL(__seq_open_private);
647 int seq_open_private(struct file *filp, const struct seq_operations *ops,
648                 int psize)
650         return __seq_open_private(filp, ops, psize) ? 0 : -ENOMEM;
652 EXPORT_SYMBOL(seq_open_private);
654 int seq_putc(struct seq_file *m, char c)
656         if (m->count < m->size) {
657                 m->buf[m->count++] = c;
658                 return 0;
659         }
660         return -1;
662 EXPORT_SYMBOL(seq_putc);
664 int seq_puts(struct seq_file *m, const char *s)
666         int len = strlen(s);
667         if (m->count + len < m->size) {
668                 memcpy(m->buf + m->count, s, len);
669                 m->count += len;
670                 return 0;
671         }
672         seq_set_overflow(m);
673         return -1;
675 EXPORT_SYMBOL(seq_puts);
677 /*
678  * A helper routine for putting decimal numbers without rich format of printf().
679  * only 'unsigned long long' is supported.
680  * This routine will put one byte delimiter + number into seq_file.
681  * This routine is very quick when you show lots of numbers.
682  * In usual cases, it will be better to use seq_printf(). It's easier to read.
683  */
684 int seq_put_decimal_ull(struct seq_file *m, char delimiter,
685                         unsigned long long num)
687         int len;
689         if (m->count + 2 >= m->size) /* we'll write 2 bytes at least */
690                 goto overflow;
692         if (delimiter)
693                 m->buf[m->count++] = delimiter;
695         if (num < 10) {
696                 m->buf[m->count++] = num + '0';
697                 return 0;
698         }
700         len = num_to_str(m->buf + m->count, m->size - m->count, num);
701         if (!len)
702                 goto overflow;
703         m->count += len;
704         return 0;
705 overflow:
706         seq_set_overflow(m);
707         return -1;
709 EXPORT_SYMBOL(seq_put_decimal_ull);
711 int seq_put_decimal_ll(struct seq_file *m, char delimiter,
712                         long long num)
714         if (num < 0) {
715                 if (m->count + 3 >= m->size) {
716                         seq_set_overflow(m);
717                         return -1;
718                 }
719                 if (delimiter)
720                         m->buf[m->count++] = delimiter;
721                 num = -num;
722                 delimiter = '-';
723         }
724         return seq_put_decimal_ull(m, delimiter, num);
727 EXPORT_SYMBOL(seq_put_decimal_ll);
729 /**
730  * seq_write - write arbitrary data to buffer
731  * @seq: seq_file identifying the buffer to which data should be written
732  * @data: data address
733  * @len: number of bytes
734  *
735  * Return 0 on success, non-zero otherwise.
736  */
737 int seq_write(struct seq_file *seq, const void *data, size_t len)
739         if (seq->count + len < seq->size) {
740                 memcpy(seq->buf + seq->count, data, len);
741                 seq->count += len;
742                 return 0;
743         }
744         seq_set_overflow(seq);
745         return -1;
747 EXPORT_SYMBOL(seq_write);
749 struct list_head *seq_list_start(struct list_head *head, loff_t pos)
751         struct list_head *lh;
753         list_for_each(lh, head)
754                 if (pos-- == 0)
755                         return lh;
757         return NULL;
759 EXPORT_SYMBOL(seq_list_start);
761 struct list_head *seq_list_start_head(struct list_head *head, loff_t pos)
763         if (!pos)
764                 return head;
766         return seq_list_start(head, pos - 1);
768 EXPORT_SYMBOL(seq_list_start_head);
770 struct list_head *seq_list_next(void *v, struct list_head *head, loff_t *ppos)
772         struct list_head *lh;
774         lh = ((struct list_head *)v)->next;
775         ++*ppos;
776         return lh == head ? NULL : lh;
778 EXPORT_SYMBOL(seq_list_next);
780 /**
781  * seq_hlist_start - start an iteration of a hlist
782  * @head: the head of the hlist
783  * @pos:  the start position of the sequence
784  *
785  * Called at seq_file->op->start().
786  */
787 struct hlist_node *seq_hlist_start(struct hlist_head *head, loff_t pos)
789         struct hlist_node *node;
791         hlist_for_each(node, head)
792                 if (pos-- == 0)
793                         return node;
794         return NULL;
796 EXPORT_SYMBOL(seq_hlist_start);
798 /**
799  * seq_hlist_start_head - start an iteration of a hlist
800  * @head: the head of the hlist
801  * @pos:  the start position of the sequence
802  *
803  * Called at seq_file->op->start(). Call this function if you want to
804  * print a header at the top of the output.
805  */
806 struct hlist_node *seq_hlist_start_head(struct hlist_head *head, loff_t pos)
808         if (!pos)
809                 return SEQ_START_TOKEN;
811         return seq_hlist_start(head, pos - 1);
813 EXPORT_SYMBOL(seq_hlist_start_head);
815 /**
816  * seq_hlist_next - move to the next position of the hlist
817  * @v:    the current iterator
818  * @head: the head of the hlist
819  * @ppos: the current position
820  *
821  * Called at seq_file->op->next().
822  */
823 struct hlist_node *seq_hlist_next(void *v, struct hlist_head *head,
824                                   loff_t *ppos)
826         struct hlist_node *node = v;
828         ++*ppos;
829         if (v == SEQ_START_TOKEN)
830                 return head->first;
831         else
832                 return node->next;
834 EXPORT_SYMBOL(seq_hlist_next);
836 /**
837  * seq_hlist_start_rcu - start an iteration of a hlist protected by RCU
838  * @head: the head of the hlist
839  * @pos:  the start position of the sequence
840  *
841  * Called at seq_file->op->start().
842  *
843  * This list-traversal primitive may safely run concurrently with
844  * the _rcu list-mutation primitives such as hlist_add_head_rcu()
845  * as long as the traversal is guarded by rcu_read_lock().
846  */
847 struct hlist_node *seq_hlist_start_rcu(struct hlist_head *head,
848                                        loff_t pos)
850         struct hlist_node *node;
852         __hlist_for_each_rcu(node, head)
853                 if (pos-- == 0)
854                         return node;
855         return NULL;
857 EXPORT_SYMBOL(seq_hlist_start_rcu);
859 /**
860  * seq_hlist_start_head_rcu - start an iteration of a hlist protected by RCU
861  * @head: the head of the hlist
862  * @pos:  the start position of the sequence
863  *
864  * Called at seq_file->op->start(). Call this function if you want to
865  * print a header at the top of the output.
866  *
867  * This list-traversal primitive may safely run concurrently with
868  * the _rcu list-mutation primitives such as hlist_add_head_rcu()
869  * as long as the traversal is guarded by rcu_read_lock().
870  */
871 struct hlist_node *seq_hlist_start_head_rcu(struct hlist_head *head,
872                                             loff_t pos)
874         if (!pos)
875                 return SEQ_START_TOKEN;
877         return seq_hlist_start_rcu(head, pos - 1);
879 EXPORT_SYMBOL(seq_hlist_start_head_rcu);
881 /**
882  * seq_hlist_next_rcu - move to the next position of the hlist protected by RCU
883  * @v:    the current iterator
884  * @head: the head of the hlist
885  * @ppos: the current position
886  *
887  * Called at seq_file->op->next().
888  *
889  * This list-traversal primitive may safely run concurrently with
890  * the _rcu list-mutation primitives such as hlist_add_head_rcu()
891  * as long as the traversal is guarded by rcu_read_lock().
892  */
893 struct hlist_node *seq_hlist_next_rcu(void *v,
894                                       struct hlist_head *head,
895                                       loff_t *ppos)
897         struct hlist_node *node = v;
899         ++*ppos;
900         if (v == SEQ_START_TOKEN)
901                 return rcu_dereference(head->first);
902         else
903                 return rcu_dereference(node->next);
905 EXPORT_SYMBOL(seq_hlist_next_rcu);