]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/blob - include/linux/atomic.h
Merge branch 'p-ti-linux-3.8.y' into p-ti-android-3.8.y
[android-sdk/kernel-video.git] / include / linux / atomic.h
1 /* Atomic operations usable in machine independent code */
2 #ifndef _LINUX_ATOMIC_H
3 #define _LINUX_ATOMIC_H
4 #include <asm/atomic.h>
6 /**
7  * atomic_add_unless - add unless the number is already a given value
8  * @v: pointer of type atomic_t
9  * @a: the amount to add to v...
10  * @u: ...unless v is equal to u.
11  *
12  * Atomically adds @a to @v, so long as @v was not already @u.
13  * Returns non-zero if @v was not @u, and zero otherwise.
14  */
15 static inline int atomic_add_unless(atomic_t *v, int a, int u)
16 {
17         return __atomic_add_unless(v, a, u) != u;
18 }
20 /**
21  * atomic_inc_not_zero - increment unless the number is zero
22  * @v: pointer of type atomic_t
23  *
24  * Atomically increments @v by 1, so long as @v is non-zero.
25  * Returns non-zero if @v was non-zero, and zero otherwise.
26  */
27 #ifndef atomic_inc_not_zero
28 #define atomic_inc_not_zero(v)          atomic_add_unless((v), 1, 0)
29 #endif
31 /**
32  * atomic_inc_not_zero_hint - increment if not null
33  * @v: pointer of type atomic_t
34  * @hint: probable value of the atomic before the increment
35  *
36  * This version of atomic_inc_not_zero() gives a hint of probable
37  * value of the atomic. This helps processor to not read the memory
38  * before doing the atomic read/modify/write cycle, lowering
39  * number of bus transactions on some arches.
40  *
41  * Returns: 0 if increment was not done, 1 otherwise.
42  */
43 #ifndef atomic_inc_not_zero_hint
44 static inline int atomic_inc_not_zero_hint(atomic_t *v, int hint)
45 {
46         int val, c = hint;
48         /* sanity test, should be removed by compiler if hint is a constant */
49         if (!hint)
50                 return atomic_inc_not_zero(v);
52         do {
53                 val = atomic_cmpxchg(v, c, c + 1);
54                 if (val == c)
55                         return 1;
56                 c = val;
57         } while (c);
59         return 0;
60 }
61 #endif
63 #ifndef atomic_inc_unless_negative
64 static inline int atomic_inc_unless_negative(atomic_t *p)
65 {
66         int v, v1;
67         for (v = 0; v >= 0; v = v1) {
68                 v1 = atomic_cmpxchg(p, v, v + 1);
69                 if (likely(v1 == v))
70                         return 1;
71         }
72         return 0;
73 }
74 #endif
76 #ifndef atomic_dec_unless_positive
77 static inline int atomic_dec_unless_positive(atomic_t *p)
78 {
79         int v, v1;
80         for (v = 0; v <= 0; v = v1) {
81                 v1 = atomic_cmpxchg(p, v, v - 1);
82                 if (likely(v1 == v))
83                         return 1;
84         }
85         return 0;
86 }
87 #endif
89 /*
90  * atomic_dec_if_positive - decrement by 1 if old value positive
91  * @v: pointer of type atomic_t
92  *
93  * The function returns the old value of *v minus 1, even if
94  * the atomic variable, v, was not decremented.
95  */
96 #ifndef atomic_dec_if_positive
97 static inline int atomic_dec_if_positive(atomic_t *v)
98 {
99         int c, old, dec;
100         c = atomic_read(v);
101         for (;;) {
102                 dec = c - 1;
103                 if (unlikely(dec < 0))
104                         break;
105                 old = atomic_cmpxchg((v), c, dec);
106                 if (likely(old == c))
107                         break;
108                 c = old;
109         }
110         return dec;
112 #endif
114 #ifndef CONFIG_ARCH_HAS_ATOMIC_OR
115 static inline void atomic_or(int i, atomic_t *v)
117         int old;
118         int new;
120         do {
121                 old = atomic_read(v);
122                 new = old | i;
123         } while (atomic_cmpxchg(v, old, new) != old);
125 #endif /* #ifndef CONFIG_ARCH_HAS_ATOMIC_OR */
127 #include <asm-generic/atomic-long.h>
128 #ifdef CONFIG_GENERIC_ATOMIC64
129 #include <asm-generic/atomic64.h>
130 #endif
131 #endif /* _LINUX_ATOMIC_H */