]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/blob - include/linux/cgroup.h
Merge branch 'p-ti-linux-3.8.y' into p-ti-android-3.8.y
[android-sdk/kernel-video.git] / include / linux / cgroup.h
1 #ifndef _LINUX_CGROUP_H
2 #define _LINUX_CGROUP_H
3 /*
4  *  cgroup interface
5  *
6  *  Copyright (C) 2003 BULL SA
7  *  Copyright (C) 2004-2006 Silicon Graphics, Inc.
8  *
9  */
11 #include <linux/sched.h>
12 #include <linux/cpumask.h>
13 #include <linux/nodemask.h>
14 #include <linux/rcupdate.h>
15 #include <linux/rculist.h>
16 #include <linux/cgroupstats.h>
17 #include <linux/prio_heap.h>
18 #include <linux/rwsem.h>
19 #include <linux/idr.h>
20 #include <linux/workqueue.h>
21 #include <linux/xattr.h>
23 #ifdef CONFIG_CGROUPS
25 struct cgroupfs_root;
26 struct cgroup_subsys;
27 struct inode;
28 struct cgroup;
29 struct css_id;
31 extern int cgroup_init_early(void);
32 extern int cgroup_init(void);
33 extern void cgroup_lock(void);
34 extern int cgroup_lock_is_held(void);
35 extern bool cgroup_lock_live_group(struct cgroup *cgrp);
36 extern void cgroup_unlock(void);
37 extern void cgroup_fork(struct task_struct *p);
38 extern void cgroup_post_fork(struct task_struct *p);
39 extern void cgroup_exit(struct task_struct *p, int run_callbacks);
40 extern int cgroupstats_build(struct cgroupstats *stats,
41                                 struct dentry *dentry);
42 extern int cgroup_load_subsys(struct cgroup_subsys *ss);
43 extern void cgroup_unload_subsys(struct cgroup_subsys *ss);
45 extern const struct file_operations proc_cgroup_operations;
47 /* Define the enumeration of all builtin cgroup subsystems */
48 #define SUBSYS(_x) _x ## _subsys_id,
49 #define IS_SUBSYS_ENABLED(option) IS_ENABLED(option)
50 enum cgroup_subsys_id {
51 #include <linux/cgroup_subsys.h>
52         CGROUP_SUBSYS_COUNT,
53 };
54 #undef IS_SUBSYS_ENABLED
55 #undef SUBSYS
57 /* Per-subsystem/per-cgroup state maintained by the system. */
58 struct cgroup_subsys_state {
59         /*
60          * The cgroup that this subsystem is attached to. Useful
61          * for subsystems that want to know about the cgroup
62          * hierarchy structure
63          */
64         struct cgroup *cgroup;
66         /*
67          * State maintained by the cgroup system to allow subsystems
68          * to be "busy". Should be accessed via css_get(),
69          * css_tryget() and css_put().
70          */
72         atomic_t refcnt;
74         unsigned long flags;
75         /* ID for this css, if possible */
76         struct css_id __rcu *id;
78         /* Used to put @cgroup->dentry on the last css_put() */
79         struct work_struct dput_work;
80 };
82 /* bits in struct cgroup_subsys_state flags field */
83 enum {
84         CSS_ROOT        = (1 << 0), /* this CSS is the root of the subsystem */
85         CSS_ONLINE      = (1 << 1), /* between ->css_online() and ->css_offline() */
86 };
88 /* Caller must verify that the css is not for root cgroup */
89 static inline void __css_get(struct cgroup_subsys_state *css, int count)
90 {
91         atomic_add(count, &css->refcnt);
92 }
94 /*
95  * Call css_get() to hold a reference on the css; it can be used
96  * for a reference obtained via:
97  * - an existing ref-counted reference to the css
98  * - task->cgroups for a locked task
99  */
101 static inline void css_get(struct cgroup_subsys_state *css)
103         /* We don't need to reference count the root state */
104         if (!(css->flags & CSS_ROOT))
105                 __css_get(css, 1);
108 /*
109  * Call css_tryget() to take a reference on a css if your existing
110  * (known-valid) reference isn't already ref-counted. Returns false if
111  * the css has been destroyed.
112  */
114 extern bool __css_tryget(struct cgroup_subsys_state *css);
115 static inline bool css_tryget(struct cgroup_subsys_state *css)
117         if (css->flags & CSS_ROOT)
118                 return true;
119         return __css_tryget(css);
122 /*
123  * css_put() should be called to release a reference taken by
124  * css_get() or css_tryget()
125  */
127 extern void __css_put(struct cgroup_subsys_state *css);
128 static inline void css_put(struct cgroup_subsys_state *css)
130         if (!(css->flags & CSS_ROOT))
131                 __css_put(css);
134 /* bits in struct cgroup flags field */
135 enum {
136         /* Control Group is dead */
137         CGRP_REMOVED,
138         /*
139          * Control Group has previously had a child cgroup or a task,
140          * but no longer (only if CGRP_NOTIFY_ON_RELEASE is set)
141          */
142         CGRP_RELEASABLE,
143         /* Control Group requires release notifications to userspace */
144         CGRP_NOTIFY_ON_RELEASE,
145         /*
146          * Clone the parent's configuration when creating a new child
147          * cpuset cgroup.  For historical reasons, this option can be
148          * specified at mount time and thus is implemented here.
149          */
150         CGRP_CPUSET_CLONE_CHILDREN,
151 };
153 struct cgroup {
154         unsigned long flags;            /* "unsigned long" so bitops work */
156         /*
157          * count users of this cgroup. >0 means busy, but doesn't
158          * necessarily indicate the number of tasks in the cgroup
159          */
160         atomic_t count;
162         int id;                         /* ida allocated in-hierarchy ID */
164         /*
165          * We link our 'sibling' struct into our parent's 'children'.
166          * Our children link their 'sibling' into our 'children'.
167          */
168         struct list_head sibling;       /* my parent's children */
169         struct list_head children;      /* my children */
170         struct list_head files;         /* my files */
172         struct cgroup *parent;          /* my parent */
173         struct dentry *dentry;          /* cgroup fs entry, RCU protected */
175         /* Private pointers for each registered subsystem */
176         struct cgroup_subsys_state *subsys[CGROUP_SUBSYS_COUNT];
178         struct cgroupfs_root *root;
179         struct cgroup *top_cgroup;
181         /*
182          * List of cg_cgroup_links pointing at css_sets with
183          * tasks in this cgroup. Protected by css_set_lock
184          */
185         struct list_head css_sets;
187         struct list_head allcg_node;    /* cgroupfs_root->allcg_list */
188         struct list_head cft_q_node;    /* used during cftype add/rm */
190         /*
191          * Linked list running through all cgroups that can
192          * potentially be reaped by the release agent. Protected by
193          * release_list_lock
194          */
195         struct list_head release_list;
197         /*
198          * list of pidlists, up to two for each namespace (one for procs, one
199          * for tasks); created on demand.
200          */
201         struct list_head pidlists;
202         struct mutex pidlist_mutex;
204         /* For RCU-protected deletion */
205         struct rcu_head rcu_head;
207         /* List of events which userspace want to receive */
208         struct list_head event_list;
209         spinlock_t event_list_lock;
211         /* directory xattrs */
212         struct simple_xattrs xattrs;
213 };
215 /*
216  * A css_set is a structure holding pointers to a set of
217  * cgroup_subsys_state objects. This saves space in the task struct
218  * object and speeds up fork()/exit(), since a single inc/dec and a
219  * list_add()/del() can bump the reference count on the entire cgroup
220  * set for a task.
221  */
223 struct css_set {
225         /* Reference count */
226         atomic_t refcount;
228         /*
229          * List running through all cgroup groups in the same hash
230          * slot. Protected by css_set_lock
231          */
232         struct hlist_node hlist;
234         /*
235          * List running through all tasks using this cgroup
236          * group. Protected by css_set_lock
237          */
238         struct list_head tasks;
240         /*
241          * List of cg_cgroup_link objects on link chains from
242          * cgroups referenced from this css_set. Protected by
243          * css_set_lock
244          */
245         struct list_head cg_links;
247         /*
248          * Set of subsystem states, one for each subsystem. This array
249          * is immutable after creation apart from the init_css_set
250          * during subsystem registration (at boot time) and modular subsystem
251          * loading/unloading.
252          */
253         struct cgroup_subsys_state *subsys[CGROUP_SUBSYS_COUNT];
255         /* For RCU-protected deletion */
256         struct rcu_head rcu_head;
257 };
259 /*
260  * cgroup_map_cb is an abstract callback API for reporting map-valued
261  * control files
262  */
264 struct cgroup_map_cb {
265         int (*fill)(struct cgroup_map_cb *cb, const char *key, u64 value);
266         void *state;
267 };
269 /*
270  * struct cftype: handler definitions for cgroup control files
271  *
272  * When reading/writing to a file:
273  *      - the cgroup to use is file->f_dentry->d_parent->d_fsdata
274  *      - the 'cftype' of the file is file->f_dentry->d_fsdata
275  */
277 /* cftype->flags */
278 #define CFTYPE_ONLY_ON_ROOT     (1U << 0)       /* only create on root cg */
279 #define CFTYPE_NOT_ON_ROOT      (1U << 1)       /* don't create on root cg */
281 #define MAX_CFTYPE_NAME         64
283 struct cftype {
284         /*
285          * By convention, the name should begin with the name of the
286          * subsystem, followed by a period.  Zero length string indicates
287          * end of cftype array.
288          */
289         char name[MAX_CFTYPE_NAME];
290         int private;
291         /*
292          * If not 0, file mode is set to this value, otherwise it will
293          * be figured out automatically
294          */
295         umode_t mode;
297         /*
298          * If non-zero, defines the maximum length of string that can
299          * be passed to write_string; defaults to 64
300          */
301         size_t max_write_len;
303         /* CFTYPE_* flags */
304         unsigned int flags;
306         int (*open)(struct inode *inode, struct file *file);
307         ssize_t (*read)(struct cgroup *cgrp, struct cftype *cft,
308                         struct file *file,
309                         char __user *buf, size_t nbytes, loff_t *ppos);
310         /*
311          * read_u64() is a shortcut for the common case of returning a
312          * single integer. Use it in place of read()
313          */
314         u64 (*read_u64)(struct cgroup *cgrp, struct cftype *cft);
315         /*
316          * read_s64() is a signed version of read_u64()
317          */
318         s64 (*read_s64)(struct cgroup *cgrp, struct cftype *cft);
319         /*
320          * read_map() is used for defining a map of key/value
321          * pairs. It should call cb->fill(cb, key, value) for each
322          * entry. The key/value pairs (and their ordering) should not
323          * change between reboots.
324          */
325         int (*read_map)(struct cgroup *cont, struct cftype *cft,
326                         struct cgroup_map_cb *cb);
327         /*
328          * read_seq_string() is used for outputting a simple sequence
329          * using seqfile.
330          */
331         int (*read_seq_string)(struct cgroup *cont, struct cftype *cft,
332                                struct seq_file *m);
334         ssize_t (*write)(struct cgroup *cgrp, struct cftype *cft,
335                          struct file *file,
336                          const char __user *buf, size_t nbytes, loff_t *ppos);
338         /*
339          * write_u64() is a shortcut for the common case of accepting
340          * a single integer (as parsed by simple_strtoull) from
341          * userspace. Use in place of write(); return 0 or error.
342          */
343         int (*write_u64)(struct cgroup *cgrp, struct cftype *cft, u64 val);
344         /*
345          * write_s64() is a signed version of write_u64()
346          */
347         int (*write_s64)(struct cgroup *cgrp, struct cftype *cft, s64 val);
349         /*
350          * write_string() is passed a nul-terminated kernelspace
351          * buffer of maximum length determined by max_write_len.
352          * Returns 0 or -ve error code.
353          */
354         int (*write_string)(struct cgroup *cgrp, struct cftype *cft,
355                             const char *buffer);
356         /*
357          * trigger() callback can be used to get some kick from the
358          * userspace, when the actual string written is not important
359          * at all. The private field can be used to determine the
360          * kick type for multiplexing.
361          */
362         int (*trigger)(struct cgroup *cgrp, unsigned int event);
364         int (*release)(struct inode *inode, struct file *file);
366         /*
367          * register_event() callback will be used to add new userspace
368          * waiter for changes related to the cftype. Implement it if
369          * you want to provide this functionality. Use eventfd_signal()
370          * on eventfd to send notification to userspace.
371          */
372         int (*register_event)(struct cgroup *cgrp, struct cftype *cft,
373                         struct eventfd_ctx *eventfd, const char *args);
374         /*
375          * unregister_event() callback will be called when userspace
376          * closes the eventfd or on cgroup removing.
377          * This callback must be implemented, if you want provide
378          * notification functionality.
379          */
380         void (*unregister_event)(struct cgroup *cgrp, struct cftype *cft,
381                         struct eventfd_ctx *eventfd);
382 };
384 /*
385  * cftype_sets describe cftypes belonging to a subsystem and are chained at
386  * cgroup_subsys->cftsets.  Each cftset points to an array of cftypes
387  * terminated by zero length name.
388  */
389 struct cftype_set {
390         struct list_head                node;   /* chained at subsys->cftsets */
391         struct cftype                   *cfts;
392 };
394 struct cgroup_scanner {
395         struct cgroup *cg;
396         int (*test_task)(struct task_struct *p, struct cgroup_scanner *scan);
397         void (*process_task)(struct task_struct *p,
398                         struct cgroup_scanner *scan);
399         struct ptr_heap *heap;
400         void *data;
401 };
403 int cgroup_add_cftypes(struct cgroup_subsys *ss, struct cftype *cfts);
404 int cgroup_rm_cftypes(struct cgroup_subsys *ss, struct cftype *cfts);
406 int cgroup_is_removed(const struct cgroup *cgrp);
408 int cgroup_path(const struct cgroup *cgrp, char *buf, int buflen);
410 int cgroup_task_count(const struct cgroup *cgrp);
412 /* Return true if cgrp is a descendant of the task's cgroup */
413 int cgroup_is_descendant(const struct cgroup *cgrp, struct task_struct *task);
415 /*
416  * Control Group taskset, used to pass around set of tasks to cgroup_subsys
417  * methods.
418  */
419 struct cgroup_taskset;
420 struct task_struct *cgroup_taskset_first(struct cgroup_taskset *tset);
421 struct task_struct *cgroup_taskset_next(struct cgroup_taskset *tset);
422 struct cgroup *cgroup_taskset_cur_cgroup(struct cgroup_taskset *tset);
423 int cgroup_taskset_size(struct cgroup_taskset *tset);
425 /**
426  * cgroup_taskset_for_each - iterate cgroup_taskset
427  * @task: the loop cursor
428  * @skip_cgrp: skip if task's cgroup matches this, %NULL to iterate through all
429  * @tset: taskset to iterate
430  */
431 #define cgroup_taskset_for_each(task, skip_cgrp, tset)                  \
432         for ((task) = cgroup_taskset_first((tset)); (task);             \
433              (task) = cgroup_taskset_next((tset)))                      \
434                 if (!(skip_cgrp) ||                                     \
435                     cgroup_taskset_cur_cgroup((tset)) != (skip_cgrp))
437 /*
438  * Control Group subsystem type.
439  * See Documentation/cgroups/cgroups.txt for details
440  */
442 struct cgroup_subsys {
443         struct cgroup_subsys_state *(*css_alloc)(struct cgroup *cgrp);
444         int (*css_online)(struct cgroup *cgrp);
445         void (*css_offline)(struct cgroup *cgrp);
446         void (*css_free)(struct cgroup *cgrp);
448         int (*allow_attach)(struct cgroup *cgrp, struct cgroup_taskset *tset);
449         int (*can_attach)(struct cgroup *cgrp, struct cgroup_taskset *tset);
450         void (*cancel_attach)(struct cgroup *cgrp, struct cgroup_taskset *tset);
451         void (*attach)(struct cgroup *cgrp, struct cgroup_taskset *tset);
452         void (*fork)(struct task_struct *task);
453         void (*exit)(struct cgroup *cgrp, struct cgroup *old_cgrp,
454                      struct task_struct *task);
455         void (*bind)(struct cgroup *root);
457         int subsys_id;
458         int active;
459         int disabled;
460         int early_init;
461         /*
462          * True if this subsys uses ID. ID is not available before cgroup_init()
463          * (not available in early_init time.)
464          */
465         bool use_id;
467         /*
468          * If %false, this subsystem is properly hierarchical -
469          * configuration, resource accounting and restriction on a parent
470          * cgroup cover those of its children.  If %true, hierarchy support
471          * is broken in some ways - some subsystems ignore hierarchy
472          * completely while others are only implemented half-way.
473          *
474          * It's now disallowed to create nested cgroups if the subsystem is
475          * broken and cgroup core will emit a warning message on such
476          * cases.  Eventually, all subsystems will be made properly
477          * hierarchical and this will go away.
478          */
479         bool broken_hierarchy;
480         bool warned_broken_hierarchy;
482 #define MAX_CGROUP_TYPE_NAMELEN 32
483         const char *name;
485         /*
486          * Link to parent, and list entry in parent's children.
487          * Protected by cgroup_lock()
488          */
489         struct cgroupfs_root *root;
490         struct list_head sibling;
491         /* used when use_id == true */
492         struct idr idr;
493         spinlock_t id_lock;
495         /* list of cftype_sets */
496         struct list_head cftsets;
498         /* base cftypes, automatically [de]registered with subsys itself */
499         struct cftype *base_cftypes;
500         struct cftype_set base_cftset;
502         /* should be defined only by modular subsystems */
503         struct module *module;
504 };
506 #define SUBSYS(_x) extern struct cgroup_subsys _x ## _subsys;
507 #define IS_SUBSYS_ENABLED(option) IS_BUILTIN(option)
508 #include <linux/cgroup_subsys.h>
509 #undef IS_SUBSYS_ENABLED
510 #undef SUBSYS
512 static inline struct cgroup_subsys_state *cgroup_subsys_state(
513         struct cgroup *cgrp, int subsys_id)
515         return cgrp->subsys[subsys_id];
518 /*
519  * function to get the cgroup_subsys_state which allows for extra
520  * rcu_dereference_check() conditions, such as locks used during the
521  * cgroup_subsys::attach() methods.
522  */
523 #define task_subsys_state_check(task, subsys_id, __c)                   \
524         rcu_dereference_check(task->cgroups->subsys[subsys_id],         \
525                               lockdep_is_held(&task->alloc_lock) ||     \
526                               cgroup_lock_is_held() || (__c))
528 static inline struct cgroup_subsys_state *
529 task_subsys_state(struct task_struct *task, int subsys_id)
531         return task_subsys_state_check(task, subsys_id, false);
534 static inline struct cgroup* task_cgroup(struct task_struct *task,
535                                                int subsys_id)
537         return task_subsys_state(task, subsys_id)->cgroup;
540 /**
541  * cgroup_for_each_child - iterate through children of a cgroup
542  * @pos: the cgroup * to use as the loop cursor
543  * @cgroup: cgroup whose children to walk
544  *
545  * Walk @cgroup's children.  Must be called under rcu_read_lock().  A child
546  * cgroup which hasn't finished ->css_online() or already has finished
547  * ->css_offline() may show up during traversal and it's each subsystem's
548  * responsibility to verify that each @pos is alive.
549  *
550  * If a subsystem synchronizes against the parent in its ->css_online() and
551  * before starting iterating, a cgroup which finished ->css_online() is
552  * guaranteed to be visible in the future iterations.
553  */
554 #define cgroup_for_each_child(pos, cgroup)                              \
555         list_for_each_entry_rcu(pos, &(cgroup)->children, sibling)
557 struct cgroup *cgroup_next_descendant_pre(struct cgroup *pos,
558                                           struct cgroup *cgroup);
560 /**
561  * cgroup_for_each_descendant_pre - pre-order walk of a cgroup's descendants
562  * @pos: the cgroup * to use as the loop cursor
563  * @cgroup: cgroup whose descendants to walk
564  *
565  * Walk @cgroup's descendants.  Must be called under rcu_read_lock().  A
566  * descendant cgroup which hasn't finished ->css_online() or already has
567  * finished ->css_offline() may show up during traversal and it's each
568  * subsystem's responsibility to verify that each @pos is alive.
569  *
570  * If a subsystem synchronizes against the parent in its ->css_online() and
571  * before starting iterating, and synchronizes against @pos on each
572  * iteration, any descendant cgroup which finished ->css_offline() is
573  * guaranteed to be visible in the future iterations.
574  *
575  * In other words, the following guarantees that a descendant can't escape
576  * state updates of its ancestors.
577  *
578  * my_online(@cgrp)
579  * {
580  *      Lock @cgrp->parent and @cgrp;
581  *      Inherit state from @cgrp->parent;
582  *      Unlock both.
583  * }
584  *
585  * my_update_state(@cgrp)
586  * {
587  *      Lock @cgrp;
588  *      Update @cgrp's state;
589  *      Unlock @cgrp;
590  *
591  *      cgroup_for_each_descendant_pre(@pos, @cgrp) {
592  *              Lock @pos;
593  *              Verify @pos is alive and inherit state from @pos->parent;
594  *              Unlock @pos;
595  *      }
596  * }
597  *
598  * As long as the inheriting step, including checking the parent state, is
599  * enclosed inside @pos locking, double-locking the parent isn't necessary
600  * while inheriting.  The state update to the parent is guaranteed to be
601  * visible by walking order and, as long as inheriting operations to the
602  * same @pos are atomic to each other, multiple updates racing each other
603  * still result in the correct state.  It's guaranateed that at least one
604  * inheritance happens for any cgroup after the latest update to its
605  * parent.
606  *
607  * If checking parent's state requires locking the parent, each inheriting
608  * iteration should lock and unlock both @pos->parent and @pos.
609  *
610  * Alternatively, a subsystem may choose to use a single global lock to
611  * synchronize ->css_online() and ->css_offline() against tree-walking
612  * operations.
613  */
614 #define cgroup_for_each_descendant_pre(pos, cgroup)                     \
615         for (pos = cgroup_next_descendant_pre(NULL, (cgroup)); (pos);   \
616              pos = cgroup_next_descendant_pre((pos), (cgroup)))
618 struct cgroup *cgroup_next_descendant_post(struct cgroup *pos,
619                                            struct cgroup *cgroup);
621 /**
622  * cgroup_for_each_descendant_post - post-order walk of a cgroup's descendants
623  * @pos: the cgroup * to use as the loop cursor
624  * @cgroup: cgroup whose descendants to walk
625  *
626  * Similar to cgroup_for_each_descendant_pre() but performs post-order
627  * traversal instead.  Note that the walk visibility guarantee described in
628  * pre-order walk doesn't apply the same to post-order walks.
629  */
630 #define cgroup_for_each_descendant_post(pos, cgroup)                    \
631         for (pos = cgroup_next_descendant_post(NULL, (cgroup)); (pos);  \
632              pos = cgroup_next_descendant_post((pos), (cgroup)))
634 /* A cgroup_iter should be treated as an opaque object */
635 struct cgroup_iter {
636         struct list_head *cg_link;
637         struct list_head *task;
638 };
640 /*
641  * To iterate across the tasks in a cgroup:
642  *
643  * 1) call cgroup_iter_start to initialize an iterator
644  *
645  * 2) call cgroup_iter_next() to retrieve member tasks until it
646  *    returns NULL or until you want to end the iteration
647  *
648  * 3) call cgroup_iter_end() to destroy the iterator.
649  *
650  * Or, call cgroup_scan_tasks() to iterate through every task in a
651  * cgroup - cgroup_scan_tasks() holds the css_set_lock when calling
652  * the test_task() callback, but not while calling the process_task()
653  * callback.
654  */
655 void cgroup_iter_start(struct cgroup *cgrp, struct cgroup_iter *it);
656 struct task_struct *cgroup_iter_next(struct cgroup *cgrp,
657                                         struct cgroup_iter *it);
658 void cgroup_iter_end(struct cgroup *cgrp, struct cgroup_iter *it);
659 int cgroup_scan_tasks(struct cgroup_scanner *scan);
660 int cgroup_attach_task(struct cgroup *, struct task_struct *);
661 int cgroup_attach_task_all(struct task_struct *from, struct task_struct *);
663 /*
664  * CSS ID is ID for cgroup_subsys_state structs under subsys. This only works
665  * if cgroup_subsys.use_id == true. It can be used for looking up and scanning.
666  * CSS ID is assigned at cgroup allocation (create) automatically
667  * and removed when subsys calls free_css_id() function. This is because
668  * the lifetime of cgroup_subsys_state is subsys's matter.
669  *
670  * Looking up and scanning function should be called under rcu_read_lock().
671  * Taking cgroup_mutex is not necessary for following calls.
672  * But the css returned by this routine can be "not populated yet" or "being
673  * destroyed". The caller should check css and cgroup's status.
674  */
676 /*
677  * Typically Called at ->destroy(), or somewhere the subsys frees
678  * cgroup_subsys_state.
679  */
680 void free_css_id(struct cgroup_subsys *ss, struct cgroup_subsys_state *css);
682 /* Find a cgroup_subsys_state which has given ID */
684 struct cgroup_subsys_state *css_lookup(struct cgroup_subsys *ss, int id);
686 /*
687  * Get a cgroup whose id is greater than or equal to id under tree of root.
688  * Returning a cgroup_subsys_state or NULL.
689  */
690 struct cgroup_subsys_state *css_get_next(struct cgroup_subsys *ss, int id,
691                 struct cgroup_subsys_state *root, int *foundid);
693 /* Returns true if root is ancestor of cg */
694 bool css_is_ancestor(struct cgroup_subsys_state *cg,
695                      const struct cgroup_subsys_state *root);
697 /* Get id and depth of css */
698 unsigned short css_id(struct cgroup_subsys_state *css);
699 unsigned short css_depth(struct cgroup_subsys_state *css);
700 struct cgroup_subsys_state *cgroup_css_from_dir(struct file *f, int id);
702 #else /* !CONFIG_CGROUPS */
704 static inline int cgroup_init_early(void) { return 0; }
705 static inline int cgroup_init(void) { return 0; }
706 static inline void cgroup_fork(struct task_struct *p) {}
707 static inline void cgroup_fork_callbacks(struct task_struct *p) {}
708 static inline void cgroup_post_fork(struct task_struct *p) {}
709 static inline void cgroup_exit(struct task_struct *p, int callbacks) {}
711 static inline void cgroup_lock(void) {}
712 static inline void cgroup_unlock(void) {}
713 static inline int cgroupstats_build(struct cgroupstats *stats,
714                                         struct dentry *dentry)
716         return -EINVAL;
719 /* No cgroups - nothing to do */
720 static inline int cgroup_attach_task_all(struct task_struct *from,
721                                          struct task_struct *t)
723         return 0;
726 #endif /* !CONFIG_CGROUPS */
728 #endif /* _LINUX_CGROUP_H */