1 /*
2 * linux/include/linux/clk-provider.h
3 *
4 * Copyright (c) 2010-2011 Jeremy Kerr <jeremy.kerr@canonical.com>
5 * Copyright (C) 2011-2012 Linaro Ltd <mturquette@linaro.org>
6 *
7 * This program is free software; you can redistribute it and/or modify
8 * it under the terms of the GNU General Public License version 2 as
9 * published by the Free Software Foundation.
10 */
11 #ifndef __LINUX_CLK_PROVIDER_H
12 #define __LINUX_CLK_PROVIDER_H
14 #include <linux/clk.h>
16 #ifdef CONFIG_COMMON_CLK
18 /*
19 * flags used across common struct clk. these flags should only affect the
20 * top-level framework. custom flags for dealing with hardware specifics
21 * belong in struct clk_foo
22 */
23 #define CLK_SET_RATE_GATE BIT(0) /* must be gated across rate change */
24 #define CLK_SET_PARENT_GATE BIT(1) /* must be gated across re-parent */
25 #define CLK_SET_RATE_PARENT BIT(2) /* propagate rate change up one level */
26 #define CLK_IGNORE_UNUSED BIT(3) /* do not gate even if unused */
27 #define CLK_IS_ROOT BIT(4) /* root clk, has no parent */
28 #define CLK_IS_BASIC BIT(5) /* Basic clk, can't do a to_clk_foo() */
29 #define CLK_GET_RATE_NOCACHE BIT(6) /* do not use the cached clk rate */
31 struct clk_hw;
33 /**
34 * struct clk_ops - Callback operations for hardware clocks; these are to
35 * be provided by the clock implementation, and will be called by drivers
36 * through the clk_* api.
37 *
38 * @prepare: Prepare the clock for enabling. This must not return until
39 * the clock is fully prepared, and it's safe to call clk_enable.
40 * This callback is intended to allow clock implementations to
41 * do any initialisation that may sleep. Called with
42 * prepare_lock held.
43 *
44 * @unprepare: Release the clock from its prepared state. This will typically
45 * undo any work done in the @prepare callback. Called with
46 * prepare_lock held.
47 *
48 * @enable: Enable the clock atomically. This must not return until the
49 * clock is generating a valid clock signal, usable by consumer
50 * devices. Called with enable_lock held. This function must not
51 * sleep.
52 *
53 * @disable: Disable the clock atomically. Called with enable_lock held.
54 * This function must not sleep.
55 *
56 * @is_enabled: Queries the hardware to determine if the clock is enabled.
57 * This function must not sleep. Optional, if this op is not
58 * set then the enable count will be used.
59 *
60 * @disable_unused: Disable the clock atomically. Only called from
61 * clk_disable_unused for gate clocks with special needs.
62 * Called with enable_lock held. This function must not
63 * sleep.
64 *
65 * @recalc_rate Recalculate the rate of this clock, by querying hardware. The
66 * parent rate is an input parameter. It is up to the caller to
67 * ensure that the prepare_mutex is held across this call.
68 * Returns the calculated rate. Optional, but recommended - if
69 * this op is not set then clock rate will be initialized to 0.
70 *
71 * @round_rate: Given a target rate as input, returns the closest rate actually
72 * supported by the clock.
73 *
74 * @get_parent: Queries the hardware to determine the parent of a clock. The
75 * return value is a u8 which specifies the index corresponding to
76 * the parent clock. This index can be applied to either the
77 * .parent_names or .parents arrays. In short, this function
78 * translates the parent value read from hardware into an array
79 * index. Currently only called when the clock is initialized by
80 * __clk_init. This callback is mandatory for clocks with
81 * multiple parents. It is optional (and unnecessary) for clocks
82 * with 0 or 1 parents.
83 *
84 * @set_parent: Change the input source of this clock; for clocks with multiple
85 * possible parents specify a new parent by passing in the index
86 * as a u8 corresponding to the parent in either the .parent_names
87 * or .parents arrays. This function in affect translates an
88 * array index into the value programmed into the hardware.
89 * Returns 0 on success, -EERROR otherwise.
90 *
91 * @set_rate: Change the rate of this clock. The requested rate is specified
92 * by the second argument, which should typically be the return
93 * of .round_rate call. The third argument gives the parent rate
94 * which is likely helpful for most .set_rate implementation.
95 * Returns 0 on success, -EERROR otherwise.
96 *
97 * The clk_enable/clk_disable and clk_prepare/clk_unprepare pairs allow
98 * implementations to split any work between atomic (enable) and sleepable
99 * (prepare) contexts. If enabling a clock requires code that might sleep,
100 * this must be done in clk_prepare. Clock enable code that will never be
101 * called in a sleepable context may be implemented in clk_enable.
102 *
103 * Typically, drivers will call clk_prepare when a clock may be needed later
104 * (eg. when a device is opened), and clk_enable when the clock is actually
105 * required (eg. from an interrupt). Note that clk_prepare MUST have been
106 * called before clk_enable.
107 */
108 struct clk_ops {
109 int (*prepare)(struct clk_hw *hw);
110 void (*unprepare)(struct clk_hw *hw);
111 int (*enable)(struct clk_hw *hw);
112 void (*disable)(struct clk_hw *hw);
113 int (*is_enabled)(struct clk_hw *hw);
114 void (*disable_unused)(struct clk_hw *hw);
115 unsigned long (*recalc_rate)(struct clk_hw *hw,
116 unsigned long parent_rate);
117 long (*round_rate)(struct clk_hw *hw, unsigned long,
118 unsigned long *);
119 int (*set_parent)(struct clk_hw *hw, u8 index);
120 u8 (*get_parent)(struct clk_hw *hw);
121 int (*set_rate)(struct clk_hw *hw, unsigned long,
122 unsigned long);
123 void (*init)(struct clk_hw *hw);
124 };
126 /**
127 * struct clk_init_data - holds init data that's common to all clocks and is
128 * shared between the clock provider and the common clock framework.
129 *
130 * @name: clock name
131 * @ops: operations this clock supports
132 * @parent_names: array of string names for all possible parents
133 * @num_parents: number of possible parents
134 * @flags: framework-level hints and quirks
135 */
136 struct clk_init_data {
137 const char *name;
138 const struct clk_ops *ops;
139 const char **parent_names;
140 u8 num_parents;
141 unsigned long flags;
142 };
144 /**
145 * struct clk_hw - handle for traversing from a struct clk to its corresponding
146 * hardware-specific structure. struct clk_hw should be declared within struct
147 * clk_foo and then referenced by the struct clk instance that uses struct
148 * clk_foo's clk_ops
149 *
150 * @clk: pointer to the struct clk instance that points back to this struct
151 * clk_hw instance
152 *
153 * @init: pointer to struct clk_init_data that contains the init data shared
154 * with the common clock framework.
155 */
156 struct clk_hw {
157 struct clk *clk;
158 const struct clk_init_data *init;
159 };
161 /*
162 * DOC: Basic clock implementations common to many platforms
163 *
164 * Each basic clock hardware type is comprised of a structure describing the
165 * clock hardware, implementations of the relevant callbacks in struct clk_ops,
166 * unique flags for that hardware type, a registration function and an
167 * alternative macro for static initialization
168 */
170 /**
171 * struct clk_fixed_rate - fixed-rate clock
172 * @hw: handle between common and hardware-specific interfaces
173 * @fixed_rate: constant frequency of clock
174 */
175 struct clk_fixed_rate {
176 struct clk_hw hw;
177 unsigned long fixed_rate;
178 u8 flags;
179 };
181 extern const struct clk_ops clk_fixed_rate_ops;
182 struct clk *clk_register_fixed_rate(struct device *dev, const char *name,
183 const char *parent_name, unsigned long flags,
184 unsigned long fixed_rate);
186 void of_fixed_clk_setup(struct device_node *np);
188 /**
189 * struct clk_gate - gating clock
190 *
191 * @hw: handle between common and hardware-specific interfaces
192 * @reg: register controlling gate
193 * @bit_idx: single bit controlling gate
194 * @flags: hardware-specific flags
195 * @lock: register lock
196 *
197 * Clock which can gate its output. Implements .enable & .disable
198 *
199 * Flags:
200 * CLK_GATE_SET_TO_DISABLE - by default this clock sets the bit at bit_idx to
201 * enable the clock. Setting this flag does the opposite: setting the bit
202 * disable the clock and clearing it enables the clock
203 */
204 struct clk_gate {
205 struct clk_hw hw;
206 void __iomem *reg;
207 u8 bit_idx;
208 u8 flags;
209 spinlock_t *lock;
210 };
212 #define CLK_GATE_SET_TO_DISABLE BIT(0)
214 extern const struct clk_ops clk_gate_ops;
215 struct clk *clk_register_gate(struct device *dev, const char *name,
216 const char *parent_name, unsigned long flags,
217 void __iomem *reg, u8 bit_idx,
218 u8 clk_gate_flags, spinlock_t *lock);
220 struct clk_div_table {
221 unsigned int val;
222 unsigned int div;
223 };
225 /**
226 * struct clk_divider - adjustable divider clock
227 *
228 * @hw: handle between common and hardware-specific interfaces
229 * @reg: register containing the divider
230 * @shift: shift to the divider bit field
231 * @width: width of the divider bit field
232 * @table: array of value/divider pairs, last entry should have div = 0
233 * @lock: register lock
234 *
235 * Clock with an adjustable divider affecting its output frequency. Implements
236 * .recalc_rate, .set_rate and .round_rate
237 *
238 * Flags:
239 * CLK_DIVIDER_ONE_BASED - by default the divisor is the value read from the
240 * register plus one. If CLK_DIVIDER_ONE_BASED is set then the divider is
241 * the raw value read from the register, with the value of zero considered
242 * invalid
243 * CLK_DIVIDER_POWER_OF_TWO - clock divisor is 2 raised to the value read from
244 * the hardware register
245 */
246 struct clk_divider {
247 struct clk_hw hw;
248 void __iomem *reg;
249 u8 shift;
250 u8 width;
251 u8 flags;
252 const struct clk_div_table *table;
253 spinlock_t *lock;
254 };
256 #define CLK_DIVIDER_ONE_BASED BIT(0)
257 #define CLK_DIVIDER_POWER_OF_TWO BIT(1)
259 extern const struct clk_ops clk_divider_ops;
260 struct clk *clk_register_divider(struct device *dev, const char *name,
261 const char *parent_name, unsigned long flags,
262 void __iomem *reg, u8 shift, u8 width,
263 u8 clk_divider_flags, spinlock_t *lock);
264 struct clk *clk_register_divider_table(struct device *dev, const char *name,
265 const char *parent_name, unsigned long flags,
266 void __iomem *reg, u8 shift, u8 width,
267 u8 clk_divider_flags, const struct clk_div_table *table,
268 spinlock_t *lock);
270 /**
271 * struct clk_mux - multiplexer clock
272 *
273 * @hw: handle between common and hardware-specific interfaces
274 * @reg: register controlling multiplexer
275 * @shift: shift to multiplexer bit field
276 * @width: width of mutliplexer bit field
277 * @num_clks: number of parent clocks
278 * @lock: register lock
279 *
280 * Clock with multiple selectable parents. Implements .get_parent, .set_parent
281 * and .recalc_rate
282 *
283 * Flags:
284 * CLK_MUX_INDEX_ONE - register index starts at 1, not 0
285 * CLK_MUX_INDEX_BIT - register index is a single bit (power of two)
286 */
287 struct clk_mux {
288 struct clk_hw hw;
289 void __iomem *reg;
290 u8 shift;
291 u8 width;
292 u8 flags;
293 spinlock_t *lock;
294 };
296 #define CLK_MUX_INDEX_ONE BIT(0)
297 #define CLK_MUX_INDEX_BIT BIT(1)
299 extern const struct clk_ops clk_mux_ops;
300 struct clk *clk_register_mux(struct device *dev, const char *name,
301 const char **parent_names, u8 num_parents, unsigned long flags,
302 void __iomem *reg, u8 shift, u8 width,
303 u8 clk_mux_flags, spinlock_t *lock);
305 /**
306 * struct clk_fixed_factor - fixed multiplier and divider clock
307 *
308 * @hw: handle between common and hardware-specific interfaces
309 * @mult: multiplier
310 * @div: divider
311 *
312 * Clock with a fixed multiplier and divider. The output frequency is the
313 * parent clock rate divided by div and multiplied by mult.
314 * Implements .recalc_rate, .set_rate and .round_rate
315 */
317 struct clk_fixed_factor {
318 struct clk_hw hw;
319 unsigned int mult;
320 unsigned int div;
321 };
323 extern struct clk_ops clk_fixed_factor_ops;
324 struct clk *clk_register_fixed_factor(struct device *dev, const char *name,
325 const char *parent_name, unsigned long flags,
326 unsigned int mult, unsigned int div);
328 /**
329 * clk_register - allocate a new clock, register it and return an opaque cookie
330 * @dev: device that is registering this clock
331 * @hw: link to hardware-specific clock data
332 *
333 * clk_register is the primary interface for populating the clock tree with new
334 * clock nodes. It returns a pointer to the newly allocated struct clk which
335 * cannot be dereferenced by driver code but may be used in conjuction with the
336 * rest of the clock API. In the event of an error clk_register will return an
337 * error code; drivers must test for an error code after calling clk_register.
338 */
339 struct clk *clk_register(struct device *dev, struct clk_hw *hw);
340 struct clk *devm_clk_register(struct device *dev, struct clk_hw *hw);
342 void clk_unregister(struct clk *clk);
343 void devm_clk_unregister(struct device *dev, struct clk *clk);
345 /* helper functions */
346 const char *__clk_get_name(struct clk *clk);
347 struct clk_hw *__clk_get_hw(struct clk *clk);
348 u8 __clk_get_num_parents(struct clk *clk);
349 struct clk *__clk_get_parent(struct clk *clk);
350 unsigned int __clk_get_enable_count(struct clk *clk);
351 unsigned int __clk_get_prepare_count(struct clk *clk);
352 unsigned long __clk_get_rate(struct clk *clk);
353 unsigned long __clk_get_flags(struct clk *clk);
354 bool __clk_is_enabled(struct clk *clk);
355 struct clk *__clk_lookup(const char *name);
357 /*
358 * FIXME clock api without lock protection
359 */
360 int __clk_prepare(struct clk *clk);
361 void __clk_unprepare(struct clk *clk);
362 void __clk_reparent(struct clk *clk, struct clk *new_parent);
363 unsigned long __clk_round_rate(struct clk *clk, unsigned long rate);
365 struct of_device_id;
367 typedef void (*of_clk_init_cb_t)(struct device_node *);
369 int of_clk_add_provider(struct device_node *np,
370 struct clk *(*clk_src_get)(struct of_phandle_args *args,
371 void *data),
372 void *data);
373 void of_clk_del_provider(struct device_node *np);
374 struct clk *of_clk_src_simple_get(struct of_phandle_args *clkspec,
375 void *data);
376 struct clk_onecell_data {
377 struct clk **clks;
378 unsigned int clk_num;
379 };
380 struct clk *of_clk_src_onecell_get(struct of_phandle_args *clkspec, void *data);
381 const char *of_clk_get_parent_name(struct device_node *np, int index);
382 void of_clk_init(const struct of_device_id *matches);
384 #endif /* CONFIG_COMMON_CLK */
385 #endif /* CLK_PROVIDER_H */