]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/blob - include/linux/cpufreq.h
Merge branch 'p-ti-linux-3.8.y' into p-ti-android-3.8.y
[android-sdk/kernel-video.git] / include / linux / cpufreq.h
1 /*
2  *  linux/include/linux/cpufreq.h
3  *
4  *  Copyright (C) 2001 Russell King
5  *            (C) 2002 - 2003 Dominik Brodowski <linux@brodo.de>
6  *
7  * This program is free software; you can redistribute it and/or modify
8  * it under the terms of the GNU General Public License version 2 as
9  * published by the Free Software Foundation.
10  */
11 #ifndef _LINUX_CPUFREQ_H
12 #define _LINUX_CPUFREQ_H
14 #include <asm/cputime.h>
15 #include <linux/mutex.h>
16 #include <linux/notifier.h>
17 #include <linux/threads.h>
18 #include <linux/kobject.h>
19 #include <linux/sysfs.h>
20 #include <linux/completion.h>
21 #include <linux/workqueue.h>
22 #include <linux/cpumask.h>
23 #include <asm/div64.h>
25 #define CPUFREQ_NAME_LEN 16
26 /* Print length for names. Extra 1 space for accomodating '\n' in prints */
27 #define CPUFREQ_NAME_PLEN (CPUFREQ_NAME_LEN + 1)
30 /*********************************************************************
31  *                     CPUFREQ NOTIFIER INTERFACE                    *
32  *********************************************************************/
34 #define CPUFREQ_TRANSITION_NOTIFIER     (0)
35 #define CPUFREQ_POLICY_NOTIFIER         (1)
37 #ifdef CONFIG_CPU_FREQ
38 int cpufreq_register_notifier(struct notifier_block *nb, unsigned int list);
39 int cpufreq_unregister_notifier(struct notifier_block *nb, unsigned int list);
40 extern void disable_cpufreq(void);
41 #else           /* CONFIG_CPU_FREQ */
42 static inline int cpufreq_register_notifier(struct notifier_block *nb,
43                                                 unsigned int list)
44 {
45         return 0;
46 }
47 static inline int cpufreq_unregister_notifier(struct notifier_block *nb,
48                                                 unsigned int list)
49 {
50         return 0;
51 }
52 static inline void disable_cpufreq(void) { }
53 #endif          /* CONFIG_CPU_FREQ */
55 /* if (cpufreq_driver->target) exists, the ->governor decides what frequency
56  * within the limits is used. If (cpufreq_driver->setpolicy> exists, these
57  * two generic policies are available:
58  */
60 #define CPUFREQ_POLICY_POWERSAVE        (1)
61 #define CPUFREQ_POLICY_PERFORMANCE      (2)
63 /* Frequency values here are CPU kHz so that hardware which doesn't run
64  * with some frequencies can complain without having to guess what per
65  * cent / per mille means.
66  * Maximum transition latency is in nanoseconds - if it's unknown,
67  * CPUFREQ_ETERNAL shall be used.
68  */
70 struct cpufreq_governor;
72 /* /sys/devices/system/cpu/cpufreq: entry point for global variables */
73 extern struct kobject *cpufreq_global_kobject;
75 #define CPUFREQ_ETERNAL                 (-1)
76 struct cpufreq_cpuinfo {
77         unsigned int            max_freq;
78         unsigned int            min_freq;
80         /* in 10^(-9) s = nanoseconds */
81         unsigned int            transition_latency;
82 };
84 struct cpufreq_real_policy {
85         unsigned int            min;    /* in kHz */
86         unsigned int            max;    /* in kHz */
87         unsigned int            policy; /* see above */
88         struct cpufreq_governor *governor; /* see below */
89 };
91 struct cpufreq_policy {
92         cpumask_var_t           cpus;   /* CPUs requiring sw coordination */
93         cpumask_var_t           related_cpus; /* CPUs with any coordination */
94         unsigned int            shared_type; /* ANY or ALL affected CPUs
95                                                 should set cpufreq */
96         unsigned int            cpu;    /* cpu nr of registered CPU */
97         struct cpufreq_cpuinfo  cpuinfo;/* see above */
99         unsigned int            min;    /* in kHz */
100         unsigned int            max;    /* in kHz */
101         unsigned int            cur;    /* in kHz, only needed if cpufreq
102                                          * governors are used */
103         unsigned int            policy; /* see above */
104         struct cpufreq_governor *governor; /* see below */
106         struct work_struct      update; /* if update_policy() needs to be
107                                          * called, but you're in IRQ context */
109         struct cpufreq_real_policy      user_policy;
111         struct kobject          kobj;
112         struct completion       kobj_unregister;
113 };
115 #define CPUFREQ_ADJUST          (0)
116 #define CPUFREQ_INCOMPATIBLE    (1)
117 #define CPUFREQ_NOTIFY          (2)
118 #define CPUFREQ_START           (3)
120 #define CPUFREQ_SHARED_TYPE_NONE (0) /* None */
121 #define CPUFREQ_SHARED_TYPE_HW   (1) /* HW does needed coordination */
122 #define CPUFREQ_SHARED_TYPE_ALL  (2) /* All dependent CPUs should set freq */
123 #define CPUFREQ_SHARED_TYPE_ANY  (3) /* Freq can be set from any dependent CPU*/
125 /******************** cpufreq transition notifiers *******************/
127 #define CPUFREQ_PRECHANGE       (0)
128 #define CPUFREQ_POSTCHANGE      (1)
129 #define CPUFREQ_RESUMECHANGE    (8)
130 #define CPUFREQ_SUSPENDCHANGE   (9)
132 struct cpufreq_freqs {
133         unsigned int cpu;       /* cpu nr */
134         unsigned int old;
135         unsigned int new;
136         u8 flags;               /* flags of cpufreq_driver, see below. */
137 };
140 /**
141  * cpufreq_scale - "old * mult / div" calculation for large values (32-bit-arch safe)
142  * @old:   old value
143  * @div:   divisor
144  * @mult:  multiplier
145  *
146  *
147  *    new = old * mult / div
148  */
149 static inline unsigned long cpufreq_scale(unsigned long old, u_int div, u_int mult)
151 #if BITS_PER_LONG == 32
153         u64 result = ((u64) old) * ((u64) mult);
154         do_div(result, div);
155         return (unsigned long) result;
157 #elif BITS_PER_LONG == 64
159         unsigned long result = old * ((u64) mult);
160         result /= div;
161         return result;
163 #endif
164 };
166 /*********************************************************************
167  *                          CPUFREQ GOVERNORS                        *
168  *********************************************************************/
170 #define CPUFREQ_GOV_START  1
171 #define CPUFREQ_GOV_STOP   2
172 #define CPUFREQ_GOV_LIMITS 3
174 struct cpufreq_governor {
175         char    name[CPUFREQ_NAME_LEN];
176         int     (*governor)     (struct cpufreq_policy *policy,
177                                  unsigned int event);
178         ssize_t (*show_setspeed)        (struct cpufreq_policy *policy,
179                                          char *buf);
180         int     (*store_setspeed)       (struct cpufreq_policy *policy,
181                                          unsigned int freq);
182         unsigned int max_transition_latency; /* HW must be able to switch to
183                         next freq faster than this value in nano secs or we
184                         will fallback to performance governor */
185         struct list_head        governor_list;
186         struct module           *owner;
187 };
189 /*
190  * Pass a target to the cpufreq driver.
191  */
192 extern int cpufreq_driver_target(struct cpufreq_policy *policy,
193                                  unsigned int target_freq,
194                                  unsigned int relation);
195 extern int __cpufreq_driver_target(struct cpufreq_policy *policy,
196                                    unsigned int target_freq,
197                                    unsigned int relation);
200 extern int __cpufreq_driver_getavg(struct cpufreq_policy *policy,
201                                    unsigned int cpu);
203 int cpufreq_register_governor(struct cpufreq_governor *governor);
204 void cpufreq_unregister_governor(struct cpufreq_governor *governor);
207 /*********************************************************************
208  *                      CPUFREQ DRIVER INTERFACE                     *
209  *********************************************************************/
211 #define CPUFREQ_RELATION_L 0  /* lowest frequency at or above target */
212 #define CPUFREQ_RELATION_H 1  /* highest frequency below or at target */
214 struct freq_attr;
216 struct cpufreq_driver {
217         struct module           *owner;
218         char                    name[CPUFREQ_NAME_LEN];
219         u8                      flags;
221         /* needed by all drivers */
222         int     (*init)         (struct cpufreq_policy *policy);
223         int     (*verify)       (struct cpufreq_policy *policy);
225         /* define one out of two */
226         int     (*setpolicy)    (struct cpufreq_policy *policy);
227         int     (*target)       (struct cpufreq_policy *policy,
228                                  unsigned int target_freq,
229                                  unsigned int relation);
231         /* should be defined, if possible */
232         unsigned int    (*get)  (unsigned int cpu);
234         /* optional */
235         unsigned int (*getavg)  (struct cpufreq_policy *policy,
236                                  unsigned int cpu);
237         int     (*bios_limit)   (int cpu, unsigned int *limit);
239         int     (*exit)         (struct cpufreq_policy *policy);
240         int     (*suspend)      (struct cpufreq_policy *policy);
241         int     (*resume)       (struct cpufreq_policy *policy);
242         struct freq_attr        **attr;
243 };
245 /* flags */
247 #define CPUFREQ_STICKY          0x01    /* the driver isn't removed even if
248                                          * all ->init() calls failed */
249 #define CPUFREQ_CONST_LOOPS     0x02    /* loops_per_jiffy or other kernel
250                                          * "constants" aren't affected by
251                                          * frequency transitions */
252 #define CPUFREQ_PM_NO_WARN      0x04    /* don't warn on suspend/resume speed
253                                          * mismatches */
255 int cpufreq_register_driver(struct cpufreq_driver *driver_data);
256 int cpufreq_unregister_driver(struct cpufreq_driver *driver_data);
259 void cpufreq_notify_transition(struct cpufreq_freqs *freqs, unsigned int state);
262 static inline void cpufreq_verify_within_limits(struct cpufreq_policy *policy, unsigned int min, unsigned int max)
264         if (policy->min < min)
265                 policy->min = min;
266         if (policy->max < min)
267                 policy->max = min;
268         if (policy->min > max)
269                 policy->min = max;
270         if (policy->max > max)
271                 policy->max = max;
272         if (policy->min > policy->max)
273                 policy->min = policy->max;
274         return;
277 struct freq_attr {
278         struct attribute attr;
279         ssize_t (*show)(struct cpufreq_policy *, char *);
280         ssize_t (*store)(struct cpufreq_policy *, const char *, size_t count);
281 };
283 #define cpufreq_freq_attr_ro(_name)             \
284 static struct freq_attr _name =                 \
285 __ATTR(_name, 0444, show_##_name, NULL)
287 #define cpufreq_freq_attr_ro_perm(_name, _perm) \
288 static struct freq_attr _name =                 \
289 __ATTR(_name, _perm, show_##_name, NULL)
291 #define cpufreq_freq_attr_rw(_name)             \
292 static struct freq_attr _name =                 \
293 __ATTR(_name, 0644, show_##_name, store_##_name)
295 struct global_attr {
296         struct attribute attr;
297         ssize_t (*show)(struct kobject *kobj,
298                         struct attribute *attr, char *buf);
299         ssize_t (*store)(struct kobject *a, struct attribute *b,
300                          const char *c, size_t count);
301 };
303 #define define_one_global_ro(_name)             \
304 static struct global_attr _name =               \
305 __ATTR(_name, 0444, show_##_name, NULL)
307 #define define_one_global_rw(_name)             \
308 static struct global_attr _name =               \
309 __ATTR(_name, 0644, show_##_name, store_##_name)
312 /*********************************************************************
313  *                        CPUFREQ 2.6. INTERFACE                     *
314  *********************************************************************/
315 int cpufreq_get_policy(struct cpufreq_policy *policy, unsigned int cpu);
316 int cpufreq_update_policy(unsigned int cpu);
318 #ifdef CONFIG_CPU_FREQ
319 /* query the current CPU frequency (in kHz). If zero, cpufreq couldn't detect it */
320 unsigned int cpufreq_get(unsigned int cpu);
321 #else
322 static inline unsigned int cpufreq_get(unsigned int cpu)
324         return 0;
326 #endif
328 /* query the last known CPU freq (in kHz). If zero, cpufreq couldn't detect it */
329 #ifdef CONFIG_CPU_FREQ
330 unsigned int cpufreq_quick_get(unsigned int cpu);
331 unsigned int cpufreq_quick_get_max(unsigned int cpu);
332 #else
333 static inline unsigned int cpufreq_quick_get(unsigned int cpu)
335         return 0;
337 static inline unsigned int cpufreq_quick_get_max(unsigned int cpu)
339         return 0;
341 #endif
344 /*********************************************************************
345  *                       CPUFREQ DEFAULT GOVERNOR                    *
346  *********************************************************************/
349 /*
350   Performance governor is fallback governor if any other gov failed to
351   auto load due latency restrictions
352 */
353 #ifdef CONFIG_CPU_FREQ_GOV_PERFORMANCE
354 extern struct cpufreq_governor cpufreq_gov_performance;
355 #endif
356 #ifdef CONFIG_CPU_FREQ_DEFAULT_GOV_PERFORMANCE
357 #define CPUFREQ_DEFAULT_GOVERNOR        (&cpufreq_gov_performance)
358 #elif defined(CONFIG_CPU_FREQ_DEFAULT_GOV_POWERSAVE)
359 extern struct cpufreq_governor cpufreq_gov_powersave;
360 #define CPUFREQ_DEFAULT_GOVERNOR        (&cpufreq_gov_powersave)
361 #elif defined(CONFIG_CPU_FREQ_DEFAULT_GOV_USERSPACE)
362 extern struct cpufreq_governor cpufreq_gov_userspace;
363 #define CPUFREQ_DEFAULT_GOVERNOR        (&cpufreq_gov_userspace)
364 #elif defined(CONFIG_CPU_FREQ_DEFAULT_GOV_ONDEMAND)
365 extern struct cpufreq_governor cpufreq_gov_ondemand;
366 #define CPUFREQ_DEFAULT_GOVERNOR        (&cpufreq_gov_ondemand)
367 #elif defined(CONFIG_CPU_FREQ_DEFAULT_GOV_CONSERVATIVE)
368 extern struct cpufreq_governor cpufreq_gov_conservative;
369 #define CPUFREQ_DEFAULT_GOVERNOR        (&cpufreq_gov_conservative)
370 #elif defined(CONFIG_CPU_FREQ_DEFAULT_GOV_INTERACTIVE)
371 extern struct cpufreq_governor cpufreq_gov_interactive;
372 #define CPUFREQ_DEFAULT_GOVERNOR        (&cpufreq_gov_interactive)
373 #endif
376 /*********************************************************************
377  *                     FREQUENCY TABLE HELPERS                       *
378  *********************************************************************/
380 #define CPUFREQ_ENTRY_INVALID ~0
381 #define CPUFREQ_TABLE_END     ~1
383 struct cpufreq_frequency_table {
384         unsigned int    index;     /* any */
385         unsigned int    frequency; /* kHz - doesn't need to be in ascending
386                                     * order */
387 };
389 int cpufreq_frequency_table_cpuinfo(struct cpufreq_policy *policy,
390                                     struct cpufreq_frequency_table *table);
392 int cpufreq_frequency_table_verify(struct cpufreq_policy *policy,
393                                    struct cpufreq_frequency_table *table);
395 int cpufreq_frequency_table_target(struct cpufreq_policy *policy,
396                                    struct cpufreq_frequency_table *table,
397                                    unsigned int target_freq,
398                                    unsigned int relation,
399                                    unsigned int *index);
401 /* the following 3 funtions are for cpufreq core use only */
402 struct cpufreq_frequency_table *cpufreq_frequency_get_table(unsigned int cpu);
403 struct cpufreq_policy *cpufreq_cpu_get(unsigned int cpu);
404 void   cpufreq_cpu_put(struct cpufreq_policy *data);
406 /* the following are really really optional */
407 extern struct freq_attr cpufreq_freq_attr_scaling_available_freqs;
409 void cpufreq_frequency_table_get_attr(struct cpufreq_frequency_table *table,
410                                       unsigned int cpu);
412 void cpufreq_frequency_table_put_attr(unsigned int cpu);
413 const char *cpufreq_get_current_driver(void);
414 #endif /* _LINUX_CPUFREQ_H */