1 /*
2 * linux/include/linux/cpufreq.h
3 *
4 * Copyright (C) 2001 Russell King
5 * (C) 2002 - 2003 Dominik Brodowski <linux@brodo.de>
6 *
7 * This program is free software; you can redistribute it and/or modify
8 * it under the terms of the GNU General Public License version 2 as
9 * published by the Free Software Foundation.
10 */
11 #ifndef _LINUX_CPUFREQ_H
12 #define _LINUX_CPUFREQ_H
14 #include <asm/cputime.h>
15 #include <linux/mutex.h>
16 #include <linux/notifier.h>
17 #include <linux/threads.h>
18 #include <linux/kobject.h>
19 #include <linux/sysfs.h>
20 #include <linux/completion.h>
21 #include <linux/workqueue.h>
22 #include <linux/cpumask.h>
23 #include <asm/div64.h>
25 #define CPUFREQ_NAME_LEN 16
26 /* Print length for names. Extra 1 space for accomodating '\n' in prints */
27 #define CPUFREQ_NAME_PLEN (CPUFREQ_NAME_LEN + 1)
30 /*********************************************************************
31 * CPUFREQ NOTIFIER INTERFACE *
32 *********************************************************************/
34 #define CPUFREQ_TRANSITION_NOTIFIER (0)
35 #define CPUFREQ_POLICY_NOTIFIER (1)
37 #ifdef CONFIG_CPU_FREQ
38 int cpufreq_register_notifier(struct notifier_block *nb, unsigned int list);
39 int cpufreq_unregister_notifier(struct notifier_block *nb, unsigned int list);
40 extern void disable_cpufreq(void);
41 #else /* CONFIG_CPU_FREQ */
42 static inline int cpufreq_register_notifier(struct notifier_block *nb,
43 unsigned int list)
44 {
45 return 0;
46 }
47 static inline int cpufreq_unregister_notifier(struct notifier_block *nb,
48 unsigned int list)
49 {
50 return 0;
51 }
52 static inline void disable_cpufreq(void) { }
53 #endif /* CONFIG_CPU_FREQ */
55 /* if (cpufreq_driver->target) exists, the ->governor decides what frequency
56 * within the limits is used. If (cpufreq_driver->setpolicy> exists, these
57 * two generic policies are available:
58 */
60 #define CPUFREQ_POLICY_POWERSAVE (1)
61 #define CPUFREQ_POLICY_PERFORMANCE (2)
63 /* Frequency values here are CPU kHz so that hardware which doesn't run
64 * with some frequencies can complain without having to guess what per
65 * cent / per mille means.
66 * Maximum transition latency is in nanoseconds - if it's unknown,
67 * CPUFREQ_ETERNAL shall be used.
68 */
70 struct cpufreq_governor;
72 /* /sys/devices/system/cpu/cpufreq: entry point for global variables */
73 extern struct kobject *cpufreq_global_kobject;
75 #define CPUFREQ_ETERNAL (-1)
76 struct cpufreq_cpuinfo {
77 unsigned int max_freq;
78 unsigned int min_freq;
80 /* in 10^(-9) s = nanoseconds */
81 unsigned int transition_latency;
82 };
84 struct cpufreq_real_policy {
85 unsigned int min; /* in kHz */
86 unsigned int max; /* in kHz */
87 unsigned int policy; /* see above */
88 struct cpufreq_governor *governor; /* see below */
89 };
91 struct cpufreq_policy {
92 cpumask_var_t cpus; /* CPUs requiring sw coordination */
93 cpumask_var_t related_cpus; /* CPUs with any coordination */
94 unsigned int shared_type; /* ANY or ALL affected CPUs
95 should set cpufreq */
96 unsigned int cpu; /* cpu nr of registered CPU */
97 struct cpufreq_cpuinfo cpuinfo;/* see above */
99 unsigned int min; /* in kHz */
100 unsigned int max; /* in kHz */
101 unsigned int cur; /* in kHz, only needed if cpufreq
102 * governors are used */
103 unsigned int policy; /* see above */
104 struct cpufreq_governor *governor; /* see below */
106 struct work_struct update; /* if update_policy() needs to be
107 * called, but you're in IRQ context */
109 struct cpufreq_real_policy user_policy;
111 struct kobject kobj;
112 struct completion kobj_unregister;
113 };
115 #define CPUFREQ_ADJUST (0)
116 #define CPUFREQ_INCOMPATIBLE (1)
117 #define CPUFREQ_NOTIFY (2)
118 #define CPUFREQ_START (3)
120 #define CPUFREQ_SHARED_TYPE_NONE (0) /* None */
121 #define CPUFREQ_SHARED_TYPE_HW (1) /* HW does needed coordination */
122 #define CPUFREQ_SHARED_TYPE_ALL (2) /* All dependent CPUs should set freq */
123 #define CPUFREQ_SHARED_TYPE_ANY (3) /* Freq can be set from any dependent CPU*/
125 /******************** cpufreq transition notifiers *******************/
127 #define CPUFREQ_PRECHANGE (0)
128 #define CPUFREQ_POSTCHANGE (1)
129 #define CPUFREQ_RESUMECHANGE (8)
130 #define CPUFREQ_SUSPENDCHANGE (9)
132 struct cpufreq_freqs {
133 unsigned int cpu; /* cpu nr */
134 unsigned int old;
135 unsigned int new;
136 u8 flags; /* flags of cpufreq_driver, see below. */
137 };
140 /**
141 * cpufreq_scale - "old * mult / div" calculation for large values (32-bit-arch safe)
142 * @old: old value
143 * @div: divisor
144 * @mult: multiplier
145 *
146 *
147 * new = old * mult / div
148 */
149 static inline unsigned long cpufreq_scale(unsigned long old, u_int div, u_int mult)
150 {
151 #if BITS_PER_LONG == 32
153 u64 result = ((u64) old) * ((u64) mult);
154 do_div(result, div);
155 return (unsigned long) result;
157 #elif BITS_PER_LONG == 64
159 unsigned long result = old * ((u64) mult);
160 result /= div;
161 return result;
163 #endif
164 };
166 /*********************************************************************
167 * CPUFREQ GOVERNORS *
168 *********************************************************************/
170 #define CPUFREQ_GOV_START 1
171 #define CPUFREQ_GOV_STOP 2
172 #define CPUFREQ_GOV_LIMITS 3
174 struct cpufreq_governor {
175 char name[CPUFREQ_NAME_LEN];
176 int (*governor) (struct cpufreq_policy *policy,
177 unsigned int event);
178 ssize_t (*show_setspeed) (struct cpufreq_policy *policy,
179 char *buf);
180 int (*store_setspeed) (struct cpufreq_policy *policy,
181 unsigned int freq);
182 unsigned int max_transition_latency; /* HW must be able to switch to
183 next freq faster than this value in nano secs or we
184 will fallback to performance governor */
185 struct list_head governor_list;
186 struct module *owner;
187 };
189 /*
190 * Pass a target to the cpufreq driver.
191 */
192 extern int cpufreq_driver_target(struct cpufreq_policy *policy,
193 unsigned int target_freq,
194 unsigned int relation);
195 extern int __cpufreq_driver_target(struct cpufreq_policy *policy,
196 unsigned int target_freq,
197 unsigned int relation);
200 extern int __cpufreq_driver_getavg(struct cpufreq_policy *policy,
201 unsigned int cpu);
203 int cpufreq_register_governor(struct cpufreq_governor *governor);
204 void cpufreq_unregister_governor(struct cpufreq_governor *governor);
207 /*********************************************************************
208 * CPUFREQ DRIVER INTERFACE *
209 *********************************************************************/
211 #define CPUFREQ_RELATION_L 0 /* lowest frequency at or above target */
212 #define CPUFREQ_RELATION_H 1 /* highest frequency below or at target */
214 struct freq_attr;
216 struct cpufreq_driver {
217 struct module *owner;
218 char name[CPUFREQ_NAME_LEN];
219 u8 flags;
221 /* needed by all drivers */
222 int (*init) (struct cpufreq_policy *policy);
223 int (*verify) (struct cpufreq_policy *policy);
225 /* define one out of two */
226 int (*setpolicy) (struct cpufreq_policy *policy);
227 int (*target) (struct cpufreq_policy *policy,
228 unsigned int target_freq,
229 unsigned int relation);
231 /* should be defined, if possible */
232 unsigned int (*get) (unsigned int cpu);
234 /* optional */
235 unsigned int (*getavg) (struct cpufreq_policy *policy,
236 unsigned int cpu);
237 int (*bios_limit) (int cpu, unsigned int *limit);
239 int (*exit) (struct cpufreq_policy *policy);
240 int (*suspend) (struct cpufreq_policy *policy);
241 int (*resume) (struct cpufreq_policy *policy);
242 struct freq_attr **attr;
243 };
245 /* flags */
247 #define CPUFREQ_STICKY 0x01 /* the driver isn't removed even if
248 * all ->init() calls failed */
249 #define CPUFREQ_CONST_LOOPS 0x02 /* loops_per_jiffy or other kernel
250 * "constants" aren't affected by
251 * frequency transitions */
252 #define CPUFREQ_PM_NO_WARN 0x04 /* don't warn on suspend/resume speed
253 * mismatches */
255 int cpufreq_register_driver(struct cpufreq_driver *driver_data);
256 int cpufreq_unregister_driver(struct cpufreq_driver *driver_data);
259 void cpufreq_notify_transition(struct cpufreq_freqs *freqs, unsigned int state);
262 static inline void cpufreq_verify_within_limits(struct cpufreq_policy *policy, unsigned int min, unsigned int max)
263 {
264 if (policy->min < min)
265 policy->min = min;
266 if (policy->max < min)
267 policy->max = min;
268 if (policy->min > max)
269 policy->min = max;
270 if (policy->max > max)
271 policy->max = max;
272 if (policy->min > policy->max)
273 policy->min = policy->max;
274 return;
275 }
277 struct freq_attr {
278 struct attribute attr;
279 ssize_t (*show)(struct cpufreq_policy *, char *);
280 ssize_t (*store)(struct cpufreq_policy *, const char *, size_t count);
281 };
283 #define cpufreq_freq_attr_ro(_name) \
284 static struct freq_attr _name = \
285 __ATTR(_name, 0444, show_##_name, NULL)
287 #define cpufreq_freq_attr_ro_perm(_name, _perm) \
288 static struct freq_attr _name = \
289 __ATTR(_name, _perm, show_##_name, NULL)
291 #define cpufreq_freq_attr_rw(_name) \
292 static struct freq_attr _name = \
293 __ATTR(_name, 0644, show_##_name, store_##_name)
295 struct global_attr {
296 struct attribute attr;
297 ssize_t (*show)(struct kobject *kobj,
298 struct attribute *attr, char *buf);
299 ssize_t (*store)(struct kobject *a, struct attribute *b,
300 const char *c, size_t count);
301 };
303 #define define_one_global_ro(_name) \
304 static struct global_attr _name = \
305 __ATTR(_name, 0444, show_##_name, NULL)
307 #define define_one_global_rw(_name) \
308 static struct global_attr _name = \
309 __ATTR(_name, 0644, show_##_name, store_##_name)
312 /*********************************************************************
313 * CPUFREQ 2.6. INTERFACE *
314 *********************************************************************/
315 int cpufreq_get_policy(struct cpufreq_policy *policy, unsigned int cpu);
316 int cpufreq_update_policy(unsigned int cpu);
318 #ifdef CONFIG_CPU_FREQ
319 /* query the current CPU frequency (in kHz). If zero, cpufreq couldn't detect it */
320 unsigned int cpufreq_get(unsigned int cpu);
321 #else
322 static inline unsigned int cpufreq_get(unsigned int cpu)
323 {
324 return 0;
325 }
326 #endif
328 /* query the last known CPU freq (in kHz). If zero, cpufreq couldn't detect it */
329 #ifdef CONFIG_CPU_FREQ
330 unsigned int cpufreq_quick_get(unsigned int cpu);
331 unsigned int cpufreq_quick_get_max(unsigned int cpu);
332 #else
333 static inline unsigned int cpufreq_quick_get(unsigned int cpu)
334 {
335 return 0;
336 }
337 static inline unsigned int cpufreq_quick_get_max(unsigned int cpu)
338 {
339 return 0;
340 }
341 #endif
344 /*********************************************************************
345 * CPUFREQ DEFAULT GOVERNOR *
346 *********************************************************************/
349 /*
350 Performance governor is fallback governor if any other gov failed to
351 auto load due latency restrictions
352 */
353 #ifdef CONFIG_CPU_FREQ_GOV_PERFORMANCE
354 extern struct cpufreq_governor cpufreq_gov_performance;
355 #endif
356 #ifdef CONFIG_CPU_FREQ_DEFAULT_GOV_PERFORMANCE
357 #define CPUFREQ_DEFAULT_GOVERNOR (&cpufreq_gov_performance)
358 #elif defined(CONFIG_CPU_FREQ_DEFAULT_GOV_POWERSAVE)
359 extern struct cpufreq_governor cpufreq_gov_powersave;
360 #define CPUFREQ_DEFAULT_GOVERNOR (&cpufreq_gov_powersave)
361 #elif defined(CONFIG_CPU_FREQ_DEFAULT_GOV_USERSPACE)
362 extern struct cpufreq_governor cpufreq_gov_userspace;
363 #define CPUFREQ_DEFAULT_GOVERNOR (&cpufreq_gov_userspace)
364 #elif defined(CONFIG_CPU_FREQ_DEFAULT_GOV_ONDEMAND)
365 extern struct cpufreq_governor cpufreq_gov_ondemand;
366 #define CPUFREQ_DEFAULT_GOVERNOR (&cpufreq_gov_ondemand)
367 #elif defined(CONFIG_CPU_FREQ_DEFAULT_GOV_CONSERVATIVE)
368 extern struct cpufreq_governor cpufreq_gov_conservative;
369 #define CPUFREQ_DEFAULT_GOVERNOR (&cpufreq_gov_conservative)
370 #elif defined(CONFIG_CPU_FREQ_DEFAULT_GOV_INTERACTIVE)
371 extern struct cpufreq_governor cpufreq_gov_interactive;
372 #define CPUFREQ_DEFAULT_GOVERNOR (&cpufreq_gov_interactive)
373 #endif
376 /*********************************************************************
377 * FREQUENCY TABLE HELPERS *
378 *********************************************************************/
380 #define CPUFREQ_ENTRY_INVALID ~0
381 #define CPUFREQ_TABLE_END ~1
383 struct cpufreq_frequency_table {
384 unsigned int index; /* any */
385 unsigned int frequency; /* kHz - doesn't need to be in ascending
386 * order */
387 };
389 int cpufreq_frequency_table_cpuinfo(struct cpufreq_policy *policy,
390 struct cpufreq_frequency_table *table);
392 int cpufreq_frequency_table_verify(struct cpufreq_policy *policy,
393 struct cpufreq_frequency_table *table);
395 int cpufreq_frequency_table_target(struct cpufreq_policy *policy,
396 struct cpufreq_frequency_table *table,
397 unsigned int target_freq,
398 unsigned int relation,
399 unsigned int *index);
401 /* the following 3 funtions are for cpufreq core use only */
402 struct cpufreq_frequency_table *cpufreq_frequency_get_table(unsigned int cpu);
403 struct cpufreq_policy *cpufreq_cpu_get(unsigned int cpu);
404 void cpufreq_cpu_put(struct cpufreq_policy *data);
406 /* the following are really really optional */
407 extern struct freq_attr cpufreq_freq_attr_scaling_available_freqs;
409 void cpufreq_frequency_table_get_attr(struct cpufreq_frequency_table *table,
410 unsigned int cpu);
412 void cpufreq_frequency_table_put_attr(unsigned int cpu);
413 #endif /* _LINUX_CPUFREQ_H */