]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/blob - include/linux/devfreq.h
Merge branch 'p-ti-linux-3.8.y' into p-ti-android-3.8.y
[android-sdk/kernel-video.git] / include / linux / devfreq.h
1 /*
2  * devfreq: Generic Dynamic Voltage and Frequency Scaling (DVFS) Framework
3  *          for Non-CPU Devices.
4  *
5  * Copyright (C) 2011 Samsung Electronics
6  *      MyungJoo Ham <myungjoo.ham@samsung.com>
7  *
8  * This program is free software; you can redistribute it and/or modify
9  * it under the terms of the GNU General Public License version 2 as
10  * published by the Free Software Foundation.
11  */
13 #ifndef __LINUX_DEVFREQ_H__
14 #define __LINUX_DEVFREQ_H__
16 #include <linux/device.h>
17 #include <linux/notifier.h>
18 #include <linux/opp.h>
20 #define DEVFREQ_NAME_LEN 16
22 struct devfreq;
24 /**
25  * struct devfreq_dev_status - Data given from devfreq user device to
26  *                           governors. Represents the performance
27  *                           statistics.
28  * @total_time:         The total time represented by this instance of
29  *                      devfreq_dev_status
30  * @busy_time:          The time that the device was working among the
31  *                      total_time.
32  * @current_frequency:  The operating frequency.
33  * @private_data:       An entry not specified by the devfreq framework.
34  *                      A device and a specific governor may have their
35  *                      own protocol with private_data. However, because
36  *                      this is governor-specific, a governor using this
37  *                      will be only compatible with devices aware of it.
38  */
39 struct devfreq_dev_status {
40         /* both since the last measure */
41         unsigned long total_time;
42         unsigned long busy_time;
43         unsigned long current_frequency;
44         void *private_data;
45 };
47 /*
48  * The resulting frequency should be at most this. (this bound is the
49  * least upper bound; thus, the resulting freq should be lower or same)
50  * If the flag is not set, the resulting frequency should be at most the
51  * bound (greatest lower bound)
52  */
53 #define DEVFREQ_FLAG_LEAST_UPPER_BOUND          0x1
55 /**
56  * struct devfreq_dev_profile - Devfreq's user device profile
57  * @initial_freq:       The operating frequency when devfreq_add_device() is
58  *                      called.
59  * @polling_ms:         The polling interval in ms. 0 disables polling.
60  * @target:             The device should set its operating frequency at
61  *                      freq or lowest-upper-than-freq value. If freq is
62  *                      higher than any operable frequency, set maximum.
63  *                      Before returning, target function should set
64  *                      freq at the current frequency.
65  *                      The "flags" parameter's possible values are
66  *                      explained above with "DEVFREQ_FLAG_*" macros.
67  * @get_dev_status:     The device should provide the current performance
68  *                      status to devfreq, which is used by governors.
69  * @get_cur_freq:       The device should provide the current frequency
70  *                      at which it is operating.
71  * @exit:               An optional callback that is called when devfreq
72  *                      is removing the devfreq object due to error or
73  *                      from devfreq_remove_device() call. If the user
74  *                      has registered devfreq->nb at a notifier-head,
75  *                      this is the time to unregister it.
76  * @freq_table: Optional list of frequencies to support statistics.
77  * @max_state:  The size of freq_table.
78  */
79 struct devfreq_dev_profile {
80         unsigned long initial_freq;
81         unsigned int polling_ms;
83         int (*target)(struct device *dev, unsigned long *freq, u32 flags);
84         int (*get_dev_status)(struct device *dev,
85                               struct devfreq_dev_status *stat);
86         int (*get_cur_freq)(struct device *dev, unsigned long *freq);
87         void (*exit)(struct device *dev);
89         unsigned int *freq_table;
90         unsigned int max_state;
91 };
93 /**
94  * struct devfreq_governor - Devfreq policy governor
95  * @node:               list node - contains registered devfreq governors
96  * @name:               Governor's name
97  * @get_target_freq:    Returns desired operating frequency for the device.
98  *                      Basically, get_target_freq will run
99  *                      devfreq_dev_profile.get_dev_status() to get the
100  *                      status of the device (load = busy_time / total_time).
101  *                      If no_central_polling is set, this callback is called
102  *                      only with update_devfreq() notified by OPP.
103  * @event_handler:      Callback for devfreq core framework to notify events
104  *                      to governors. Events include per device governor
105  *                      init and exit, opp changes out of devfreq, suspend
106  *                      and resume of per device devfreq during device idle.
107  *
108  * Note that the callbacks are called with devfreq->lock locked by devfreq.
109  */
110 struct devfreq_governor {
111         struct list_head node;
113         const char name[DEVFREQ_NAME_LEN];
114         int (*get_target_freq)(struct devfreq *this, unsigned long *freq);
115         int (*event_handler)(struct devfreq *devfreq,
116                                 unsigned int event, void *data);
117 };
119 /**
120  * struct devfreq - Device devfreq structure
121  * @node:       list node - contains the devices with devfreq that have been
122  *              registered.
123  * @lock:       a mutex to protect accessing devfreq.
124  * @dev:        device registered by devfreq class. dev.parent is the device
125  *              using devfreq.
126  * @profile:    device-specific devfreq profile
127  * @governor:   method how to choose frequency based on the usage.
128  * @governor_name:      devfreq governor name for use with this devfreq
129  * @nb:         notifier block used to notify devfreq object that it should
130  *              reevaluate operable frequencies. Devfreq users may use
131  *              devfreq.nb to the corresponding register notifier call chain.
132  * @work:       delayed work for load monitoring.
133  * @previous_freq:      previously configured frequency value.
134  * @data:       Private data of the governor. The devfreq framework does not
135  *              touch this.
136  * @min_freq:   Limit minimum frequency requested by user (0: none)
137  * @max_freq:   Limit maximum frequency requested by user (0: none)
138  * @stop_polling:        devfreq polling status of a device.
139  * @total_trans:        Number of devfreq transitions
140  * @trans_table:        Statistics of devfreq transitions
141  * @time_in_state:      Statistics of devfreq states
142  * @last_stat_updated:  The last time stat updated
143  *
144  * This structure stores the devfreq information for a give device.
145  *
146  * Note that when a governor accesses entries in struct devfreq in its
147  * functions except for the context of callbacks defined in struct
148  * devfreq_governor, the governor should protect its access with the
149  * struct mutex lock in struct devfreq. A governor may use this mutex
150  * to protect its own private data in void *data as well.
151  */
152 struct devfreq {
153         struct list_head node;
155         struct mutex lock;
156         struct device dev;
157         struct devfreq_dev_profile *profile;
158         const struct devfreq_governor *governor;
159         char governor_name[DEVFREQ_NAME_LEN];
160         struct notifier_block nb;
161         struct delayed_work work;
163         unsigned long previous_freq;
165         void *data; /* private data for governors */
167         unsigned long min_freq;
168         unsigned long max_freq;
169         bool stop_polling;
171         /* information for device freqeuncy transition */
172         unsigned int total_trans;
173         unsigned int *trans_table;
174         unsigned long *time_in_state;
175         unsigned long last_stat_updated;
176 };
178 #if defined(CONFIG_PM_DEVFREQ)
179 extern struct devfreq *devfreq_add_device(struct device *dev,
180                                   struct devfreq_dev_profile *profile,
181                                   const char *governor_name,
182                                   void *data);
183 extern int devfreq_remove_device(struct devfreq *devfreq);
184 extern int devfreq_suspend_device(struct devfreq *devfreq);
185 extern int devfreq_resume_device(struct devfreq *devfreq);
187 /* Helper functions for devfreq user device driver with OPP. */
188 extern struct opp *devfreq_recommended_opp(struct device *dev,
189                                            unsigned long *freq, u32 flags);
190 extern int devfreq_register_opp_notifier(struct device *dev,
191                                          struct devfreq *devfreq);
192 extern int devfreq_unregister_opp_notifier(struct device *dev,
193                                            struct devfreq *devfreq);
195 #if IS_ENABLED(CONFIG_DEVFREQ_GOV_SIMPLE_ONDEMAND)
196 /**
197  * struct devfreq_simple_ondemand_data - void *data fed to struct devfreq
198  *      and devfreq_add_device
199  * @upthreshold:        If the load is over this value, the frequency jumps.
200  *                      Specify 0 to use the default. Valid value = 0 to 100.
201  * @downdifferential:   If the load is under upthreshold - downdifferential,
202  *                      the governor may consider slowing the frequency down.
203  *                      Specify 0 to use the default. Valid value = 0 to 100.
204  *                      downdifferential < upthreshold must hold.
205  *
206  * If the fed devfreq_simple_ondemand_data pointer is NULL to the governor,
207  * the governor uses the default values.
208  */
209 struct devfreq_simple_ondemand_data {
210         unsigned int upthreshold;
211         unsigned int downdifferential;
212 };
213 #endif
215 #else /* !CONFIG_PM_DEVFREQ */
216 static struct devfreq *devfreq_add_device(struct device *dev,
217                                           struct devfreq_dev_profile *profile,
218                                           const char *governor_name,
219                                           void *data)
221         return NULL;
224 static int devfreq_remove_device(struct devfreq *devfreq)
226         return 0;
229 static int devfreq_suspend_device(struct devfreq *devfreq)
231         return 0;
234 static int devfreq_resume_device(struct devfreq *devfreq)
236         return 0;
239 static struct opp *devfreq_recommended_opp(struct device *dev,
240                                            unsigned long *freq, u32 flags)
242         return -EINVAL;
245 static int devfreq_register_opp_notifier(struct device *dev,
246                                          struct devfreq *devfreq)
248         return -EINVAL;
251 static int devfreq_unregister_opp_notifier(struct device *dev,
252                                            struct devfreq *devfreq)
254         return -EINVAL;
257 #endif /* CONFIG_PM_DEVFREQ */
259 #endif /* __LINUX_DEVFREQ_H__ */