1 /*
2 * device.h - generic, centralized driver model
3 *
4 * Copyright (c) 2001-2003 Patrick Mochel <mochel@osdl.org>
5 * Copyright (c) 2004-2009 Greg Kroah-Hartman <gregkh@suse.de>
6 * Copyright (c) 2008-2009 Novell Inc.
7 *
8 * This file is released under the GPLv2
9 *
10 * See Documentation/driver-model/ for more information.
11 */
13 #ifndef _DEVICE_H_
14 #define _DEVICE_H_
16 #include <linux/ioport.h>
17 #include <linux/kobject.h>
18 #include <linux/klist.h>
19 #include <linux/list.h>
20 #include <linux/lockdep.h>
21 #include <linux/compiler.h>
22 #include <linux/types.h>
23 #include <linux/mutex.h>
24 #include <linux/pm.h>
25 #include <linux/atomic.h>
26 #include <linux/ratelimit.h>
27 #include <asm/device.h>
29 struct device;
30 struct device_private;
31 struct device_driver;
32 struct driver_private;
33 struct module;
34 struct class;
35 struct subsys_private;
36 struct bus_type;
37 struct device_node;
38 struct iommu_ops;
39 struct iommu_group;
41 struct bus_attribute {
42 struct attribute attr;
43 ssize_t (*show)(struct bus_type *bus, char *buf);
44 ssize_t (*store)(struct bus_type *bus, const char *buf, size_t count);
45 };
47 #define BUS_ATTR(_name, _mode, _show, _store) \
48 struct bus_attribute bus_attr_##_name = __ATTR(_name, _mode, _show, _store)
50 extern int __must_check bus_create_file(struct bus_type *,
51 struct bus_attribute *);
52 extern void bus_remove_file(struct bus_type *, struct bus_attribute *);
54 /**
55 * struct bus_type - The bus type of the device
56 *
57 * @name: The name of the bus.
58 * @dev_name: Used for subsystems to enumerate devices like ("foo%u", dev->id).
59 * @dev_root: Default device to use as the parent.
60 * @bus_attrs: Default attributes of the bus.
61 * @dev_attrs: Default attributes of the devices on the bus.
62 * @drv_attrs: Default attributes of the device drivers on the bus.
63 * @match: Called, perhaps multiple times, whenever a new device or driver
64 * is added for this bus. It should return a nonzero value if the
65 * given device can be handled by the given driver.
66 * @uevent: Called when a device is added, removed, or a few other things
67 * that generate uevents to add the environment variables.
68 * @probe: Called when a new device or driver add to this bus, and callback
69 * the specific driver's probe to initial the matched device.
70 * @remove: Called when a device removed from this bus.
71 * @shutdown: Called at shut-down time to quiesce the device.
72 * @suspend: Called when a device on this bus wants to go to sleep mode.
73 * @resume: Called to bring a device on this bus out of sleep mode.
74 * @pm: Power management operations of this bus, callback the specific
75 * device driver's pm-ops.
76 * @iommu_ops: IOMMU specific operations for this bus, used to attach IOMMU
77 * driver implementations to a bus and allow the driver to do
78 * bus-specific setup
79 * @p: The private data of the driver core, only the driver core can
80 * touch this.
81 *
82 * A bus is a channel between the processor and one or more devices. For the
83 * purposes of the device model, all devices are connected via a bus, even if
84 * it is an internal, virtual, "platform" bus. Buses can plug into each other.
85 * A USB controller is usually a PCI device, for example. The device model
86 * represents the actual connections between buses and the devices they control.
87 * A bus is represented by the bus_type structure. It contains the name, the
88 * default attributes, the bus' methods, PM operations, and the driver core's
89 * private data.
90 */
91 struct bus_type {
92 const char *name;
93 const char *dev_name;
94 struct device *dev_root;
95 struct bus_attribute *bus_attrs;
96 struct device_attribute *dev_attrs;
97 struct driver_attribute *drv_attrs;
99 int (*match)(struct device *dev, struct device_driver *drv);
100 int (*uevent)(struct device *dev, struct kobj_uevent_env *env);
101 int (*probe)(struct device *dev);
102 int (*remove)(struct device *dev);
103 void (*shutdown)(struct device *dev);
105 int (*suspend)(struct device *dev, pm_message_t state);
106 int (*resume)(struct device *dev);
108 const struct dev_pm_ops *pm;
110 struct iommu_ops *iommu_ops;
112 struct subsys_private *p;
113 };
115 /* This is a #define to keep the compiler from merging different
116 * instances of the __key variable */
117 #define bus_register(subsys) \
118 ({ \
119 static struct lock_class_key __key; \
120 __bus_register(subsys, &__key); \
121 })
122 extern int __must_check __bus_register(struct bus_type *bus,
123 struct lock_class_key *key);
124 extern void bus_unregister(struct bus_type *bus);
126 extern int __must_check bus_rescan_devices(struct bus_type *bus);
128 /* iterator helpers for buses */
129 struct subsys_dev_iter {
130 struct klist_iter ki;
131 const struct device_type *type;
132 };
133 void subsys_dev_iter_init(struct subsys_dev_iter *iter,
134 struct bus_type *subsys,
135 struct device *start,
136 const struct device_type *type);
137 struct device *subsys_dev_iter_next(struct subsys_dev_iter *iter);
138 void subsys_dev_iter_exit(struct subsys_dev_iter *iter);
140 int bus_for_each_dev(struct bus_type *bus, struct device *start, void *data,
141 int (*fn)(struct device *dev, void *data));
142 struct device *bus_find_device(struct bus_type *bus, struct device *start,
143 void *data,
144 int (*match)(struct device *dev, void *data));
145 struct device *bus_find_device_by_name(struct bus_type *bus,
146 struct device *start,
147 const char *name);
148 struct device *subsys_find_device_by_id(struct bus_type *bus, unsigned int id,
149 struct device *hint);
150 int bus_for_each_drv(struct bus_type *bus, struct device_driver *start,
151 void *data, int (*fn)(struct device_driver *, void *));
152 void bus_sort_breadthfirst(struct bus_type *bus,
153 int (*compare)(const struct device *a,
154 const struct device *b));
155 /*
156 * Bus notifiers: Get notified of addition/removal of devices
157 * and binding/unbinding of drivers to devices.
158 * In the long run, it should be a replacement for the platform
159 * notify hooks.
160 */
161 struct notifier_block;
163 extern int bus_register_notifier(struct bus_type *bus,
164 struct notifier_block *nb);
165 extern int bus_unregister_notifier(struct bus_type *bus,
166 struct notifier_block *nb);
168 /* All 4 notifers below get called with the target struct device *
169 * as an argument. Note that those functions are likely to be called
170 * with the device lock held in the core, so be careful.
171 */
172 #define BUS_NOTIFY_ADD_DEVICE 0x00000001 /* device added */
173 #define BUS_NOTIFY_DEL_DEVICE 0x00000002 /* device removed */
174 #define BUS_NOTIFY_BIND_DRIVER 0x00000003 /* driver about to be
175 bound */
176 #define BUS_NOTIFY_BOUND_DRIVER 0x00000004 /* driver bound to device */
177 #define BUS_NOTIFY_UNBIND_DRIVER 0x00000005 /* driver about to be
178 unbound */
179 #define BUS_NOTIFY_UNBOUND_DRIVER 0x00000006 /* driver is unbound
180 from the device */
182 extern struct kset *bus_get_kset(struct bus_type *bus);
183 extern struct klist *bus_get_device_klist(struct bus_type *bus);
185 /**
186 * struct device_driver - The basic device driver structure
187 * @name: Name of the device driver.
188 * @bus: The bus which the device of this driver belongs to.
189 * @owner: The module owner.
190 * @mod_name: Used for built-in modules.
191 * @suppress_bind_attrs: Disables bind/unbind via sysfs.
192 * @of_match_table: The open firmware table.
193 * @acpi_match_table: The ACPI match table.
194 * @probe: Called to query the existence of a specific device,
195 * whether this driver can work with it, and bind the driver
196 * to a specific device.
197 * @remove: Called when the device is removed from the system to
198 * unbind a device from this driver.
199 * @shutdown: Called at shut-down time to quiesce the device.
200 * @suspend: Called to put the device to sleep mode. Usually to a
201 * low power state.
202 * @resume: Called to bring a device from sleep mode.
203 * @groups: Default attributes that get created by the driver core
204 * automatically.
205 * @pm: Power management operations of the device which matched
206 * this driver.
207 * @p: Driver core's private data, no one other than the driver
208 * core can touch this.
209 *
210 * The device driver-model tracks all of the drivers known to the system.
211 * The main reason for this tracking is to enable the driver core to match
212 * up drivers with new devices. Once drivers are known objects within the
213 * system, however, a number of other things become possible. Device drivers
214 * can export information and configuration variables that are independent
215 * of any specific device.
216 */
217 struct device_driver {
218 const char *name;
219 struct bus_type *bus;
221 struct module *owner;
222 const char *mod_name; /* used for built-in modules */
224 bool suppress_bind_attrs; /* disables bind/unbind via sysfs */
226 const struct of_device_id *of_match_table;
227 const struct acpi_device_id *acpi_match_table;
229 int (*probe) (struct device *dev);
230 int (*remove) (struct device *dev);
231 void (*shutdown) (struct device *dev);
232 int (*suspend) (struct device *dev, pm_message_t state);
233 int (*resume) (struct device *dev);
234 const struct attribute_group **groups;
236 const struct dev_pm_ops *pm;
238 struct driver_private *p;
239 };
242 extern int __must_check driver_register(struct device_driver *drv);
243 extern void driver_unregister(struct device_driver *drv);
245 extern struct device_driver *driver_find(const char *name,
246 struct bus_type *bus);
247 extern int driver_probe_done(void);
248 extern void wait_for_device_probe(void);
251 /* sysfs interface for exporting driver attributes */
253 struct driver_attribute {
254 struct attribute attr;
255 ssize_t (*show)(struct device_driver *driver, char *buf);
256 ssize_t (*store)(struct device_driver *driver, const char *buf,
257 size_t count);
258 };
260 #define DRIVER_ATTR(_name, _mode, _show, _store) \
261 struct driver_attribute driver_attr_##_name = \
262 __ATTR(_name, _mode, _show, _store)
264 extern int __must_check driver_create_file(struct device_driver *driver,
265 const struct driver_attribute *attr);
266 extern void driver_remove_file(struct device_driver *driver,
267 const struct driver_attribute *attr);
269 extern int __must_check driver_for_each_device(struct device_driver *drv,
270 struct device *start,
271 void *data,
272 int (*fn)(struct device *dev,
273 void *));
274 struct device *driver_find_device(struct device_driver *drv,
275 struct device *start, void *data,
276 int (*match)(struct device *dev, void *data));
278 /**
279 * struct subsys_interface - interfaces to device functions
280 * @name: name of the device function
281 * @subsys: subsytem of the devices to attach to
282 * @node: the list of functions registered at the subsystem
283 * @add_dev: device hookup to device function handler
284 * @remove_dev: device hookup to device function handler
285 *
286 * Simple interfaces attached to a subsystem. Multiple interfaces can
287 * attach to a subsystem and its devices. Unlike drivers, they do not
288 * exclusively claim or control devices. Interfaces usually represent
289 * a specific functionality of a subsystem/class of devices.
290 */
291 struct subsys_interface {
292 const char *name;
293 struct bus_type *subsys;
294 struct list_head node;
295 int (*add_dev)(struct device *dev, struct subsys_interface *sif);
296 int (*remove_dev)(struct device *dev, struct subsys_interface *sif);
297 };
299 int subsys_interface_register(struct subsys_interface *sif);
300 void subsys_interface_unregister(struct subsys_interface *sif);
302 int subsys_system_register(struct bus_type *subsys,
303 const struct attribute_group **groups);
305 /**
306 * struct class - device classes
307 * @name: Name of the class.
308 * @owner: The module owner.
309 * @class_attrs: Default attributes of this class.
310 * @dev_attrs: Default attributes of the devices belong to the class.
311 * @dev_bin_attrs: Default binary attributes of the devices belong to the class.
312 * @dev_kobj: The kobject that represents this class and links it into the hierarchy.
313 * @dev_uevent: Called when a device is added, removed from this class, or a
314 * few other things that generate uevents to add the environment
315 * variables.
316 * @devnode: Callback to provide the devtmpfs.
317 * @class_release: Called to release this class.
318 * @dev_release: Called to release the device.
319 * @suspend: Used to put the device to sleep mode, usually to a low power
320 * state.
321 * @resume: Used to bring the device from the sleep mode.
322 * @ns_type: Callbacks so sysfs can detemine namespaces.
323 * @namespace: Namespace of the device belongs to this class.
324 * @pm: The default device power management operations of this class.
325 * @p: The private data of the driver core, no one other than the
326 * driver core can touch this.
327 *
328 * A class is a higher-level view of a device that abstracts out low-level
329 * implementation details. Drivers may see a SCSI disk or an ATA disk, but,
330 * at the class level, they are all simply disks. Classes allow user space
331 * to work with devices based on what they do, rather than how they are
332 * connected or how they work.
333 */
334 struct class {
335 const char *name;
336 struct module *owner;
338 struct class_attribute *class_attrs;
339 struct device_attribute *dev_attrs;
340 struct bin_attribute *dev_bin_attrs;
341 struct kobject *dev_kobj;
343 int (*dev_uevent)(struct device *dev, struct kobj_uevent_env *env);
344 char *(*devnode)(struct device *dev, umode_t *mode);
346 void (*class_release)(struct class *class);
347 void (*dev_release)(struct device *dev);
349 int (*suspend)(struct device *dev, pm_message_t state);
350 int (*resume)(struct device *dev);
352 const struct kobj_ns_type_operations *ns_type;
353 const void *(*namespace)(struct device *dev);
355 const struct dev_pm_ops *pm;
357 struct subsys_private *p;
358 };
360 struct class_dev_iter {
361 struct klist_iter ki;
362 const struct device_type *type;
363 };
365 extern struct kobject *sysfs_dev_block_kobj;
366 extern struct kobject *sysfs_dev_char_kobj;
367 extern int __must_check __class_register(struct class *class,
368 struct lock_class_key *key);
369 extern void class_unregister(struct class *class);
371 /* This is a #define to keep the compiler from merging different
372 * instances of the __key variable */
373 #define class_register(class) \
374 ({ \
375 static struct lock_class_key __key; \
376 __class_register(class, &__key); \
377 })
379 struct class_compat;
380 struct class_compat *class_compat_register(const char *name);
381 void class_compat_unregister(struct class_compat *cls);
382 int class_compat_create_link(struct class_compat *cls, struct device *dev,
383 struct device *device_link);
384 void class_compat_remove_link(struct class_compat *cls, struct device *dev,
385 struct device *device_link);
387 extern void class_dev_iter_init(struct class_dev_iter *iter,
388 struct class *class,
389 struct device *start,
390 const struct device_type *type);
391 extern struct device *class_dev_iter_next(struct class_dev_iter *iter);
392 extern void class_dev_iter_exit(struct class_dev_iter *iter);
394 extern int class_for_each_device(struct class *class, struct device *start,
395 void *data,
396 int (*fn)(struct device *dev, void *data));
397 extern struct device *class_find_device(struct class *class,
398 struct device *start, void *data,
399 int (*match)(struct device *, void *));
401 struct class_attribute {
402 struct attribute attr;
403 ssize_t (*show)(struct class *class, struct class_attribute *attr,
404 char *buf);
405 ssize_t (*store)(struct class *class, struct class_attribute *attr,
406 const char *buf, size_t count);
407 const void *(*namespace)(struct class *class,
408 const struct class_attribute *attr);
409 };
411 #define CLASS_ATTR(_name, _mode, _show, _store) \
412 struct class_attribute class_attr_##_name = __ATTR(_name, _mode, _show, _store)
414 extern int __must_check class_create_file(struct class *class,
415 const struct class_attribute *attr);
416 extern void class_remove_file(struct class *class,
417 const struct class_attribute *attr);
419 /* Simple class attribute that is just a static string */
421 struct class_attribute_string {
422 struct class_attribute attr;
423 char *str;
424 };
426 /* Currently read-only only */
427 #define _CLASS_ATTR_STRING(_name, _mode, _str) \
428 { __ATTR(_name, _mode, show_class_attr_string, NULL), _str }
429 #define CLASS_ATTR_STRING(_name, _mode, _str) \
430 struct class_attribute_string class_attr_##_name = \
431 _CLASS_ATTR_STRING(_name, _mode, _str)
433 extern ssize_t show_class_attr_string(struct class *class, struct class_attribute *attr,
434 char *buf);
436 struct class_interface {
437 struct list_head node;
438 struct class *class;
440 int (*add_dev) (struct device *, struct class_interface *);
441 void (*remove_dev) (struct device *, struct class_interface *);
442 };
444 extern int __must_check class_interface_register(struct class_interface *);
445 extern void class_interface_unregister(struct class_interface *);
447 extern struct class * __must_check __class_create(struct module *owner,
448 const char *name,
449 struct lock_class_key *key);
450 extern void class_destroy(struct class *cls);
452 /* This is a #define to keep the compiler from merging different
453 * instances of the __key variable */
454 #define class_create(owner, name) \
455 ({ \
456 static struct lock_class_key __key; \
457 __class_create(owner, name, &__key); \
458 })
460 /*
461 * The type of device, "struct device" is embedded in. A class
462 * or bus can contain devices of different types
463 * like "partitions" and "disks", "mouse" and "event".
464 * This identifies the device type and carries type-specific
465 * information, equivalent to the kobj_type of a kobject.
466 * If "name" is specified, the uevent will contain it in
467 * the DEVTYPE variable.
468 */
469 struct device_type {
470 const char *name;
471 const struct attribute_group **groups;
472 int (*uevent)(struct device *dev, struct kobj_uevent_env *env);
473 char *(*devnode)(struct device *dev, umode_t *mode);
474 void (*release)(struct device *dev);
476 const struct dev_pm_ops *pm;
477 };
479 /* interface for exporting device attributes */
480 struct device_attribute {
481 struct attribute attr;
482 ssize_t (*show)(struct device *dev, struct device_attribute *attr,
483 char *buf);
484 ssize_t (*store)(struct device *dev, struct device_attribute *attr,
485 const char *buf, size_t count);
486 };
488 struct dev_ext_attribute {
489 struct device_attribute attr;
490 void *var;
491 };
493 ssize_t device_show_ulong(struct device *dev, struct device_attribute *attr,
494 char *buf);
495 ssize_t device_store_ulong(struct device *dev, struct device_attribute *attr,
496 const char *buf, size_t count);
497 ssize_t device_show_int(struct device *dev, struct device_attribute *attr,
498 char *buf);
499 ssize_t device_store_int(struct device *dev, struct device_attribute *attr,
500 const char *buf, size_t count);
501 ssize_t device_show_bool(struct device *dev, struct device_attribute *attr,
502 char *buf);
503 ssize_t device_store_bool(struct device *dev, struct device_attribute *attr,
504 const char *buf, size_t count);
506 #define DEVICE_ATTR(_name, _mode, _show, _store) \
507 struct device_attribute dev_attr_##_name = __ATTR(_name, _mode, _show, _store)
508 #define DEVICE_ULONG_ATTR(_name, _mode, _var) \
509 struct dev_ext_attribute dev_attr_##_name = \
510 { __ATTR(_name, _mode, device_show_ulong, device_store_ulong), &(_var) }
511 #define DEVICE_INT_ATTR(_name, _mode, _var) \
512 struct dev_ext_attribute dev_attr_##_name = \
513 { __ATTR(_name, _mode, device_show_int, device_store_int), &(_var) }
514 #define DEVICE_BOOL_ATTR(_name, _mode, _var) \
515 struct dev_ext_attribute dev_attr_##_name = \
516 { __ATTR(_name, _mode, device_show_bool, device_store_bool), &(_var) }
517 #define DEVICE_ATTR_IGNORE_LOCKDEP(_name, _mode, _show, _store) \
518 struct device_attribute dev_attr_##_name = \
519 __ATTR_IGNORE_LOCKDEP(_name, _mode, _show, _store)
521 extern int device_create_file(struct device *device,
522 const struct device_attribute *entry);
523 extern void device_remove_file(struct device *dev,
524 const struct device_attribute *attr);
525 extern int __must_check device_create_bin_file(struct device *dev,
526 const struct bin_attribute *attr);
527 extern void device_remove_bin_file(struct device *dev,
528 const struct bin_attribute *attr);
529 extern int device_schedule_callback_owner(struct device *dev,
530 void (*func)(struct device *dev), struct module *owner);
532 /* This is a macro to avoid include problems with THIS_MODULE */
533 #define device_schedule_callback(dev, func) \
534 device_schedule_callback_owner(dev, func, THIS_MODULE)
536 /* device resource management */
537 typedef void (*dr_release_t)(struct device *dev, void *res);
538 typedef int (*dr_match_t)(struct device *dev, void *res, void *match_data);
540 #ifdef CONFIG_DEBUG_DEVRES
541 extern void *__devres_alloc(dr_release_t release, size_t size, gfp_t gfp,
542 const char *name);
543 #define devres_alloc(release, size, gfp) \
544 __devres_alloc(release, size, gfp, #release)
545 #else
546 extern void *devres_alloc(dr_release_t release, size_t size, gfp_t gfp);
547 #endif
548 extern void devres_for_each_res(struct device *dev, dr_release_t release,
549 dr_match_t match, void *match_data,
550 void (*fn)(struct device *, void *, void *),
551 void *data);
552 extern void devres_free(void *res);
553 extern void devres_add(struct device *dev, void *res);
554 extern void *devres_find(struct device *dev, dr_release_t release,
555 dr_match_t match, void *match_data);
556 extern void *devres_get(struct device *dev, void *new_res,
557 dr_match_t match, void *match_data);
558 extern void *devres_remove(struct device *dev, dr_release_t release,
559 dr_match_t match, void *match_data);
560 extern int devres_destroy(struct device *dev, dr_release_t release,
561 dr_match_t match, void *match_data);
562 extern int devres_release(struct device *dev, dr_release_t release,
563 dr_match_t match, void *match_data);
565 /* devres group */
566 extern void * __must_check devres_open_group(struct device *dev, void *id,
567 gfp_t gfp);
568 extern void devres_close_group(struct device *dev, void *id);
569 extern void devres_remove_group(struct device *dev, void *id);
570 extern int devres_release_group(struct device *dev, void *id);
572 /* managed kzalloc/kfree for device drivers, no kmalloc, always use kzalloc */
573 extern void *devm_kzalloc(struct device *dev, size_t size, gfp_t gfp);
574 extern void devm_kfree(struct device *dev, void *p);
576 void __iomem *devm_request_and_ioremap(struct device *dev,
577 struct resource *res);
579 struct device_dma_parameters {
580 /*
581 * a low level driver may set these to teach IOMMU code about
582 * sg limitations.
583 */
584 unsigned int max_segment_size;
585 unsigned long segment_boundary_mask;
586 };
588 struct acpi_dev_node {
589 #ifdef CONFIG_ACPI
590 void *handle;
591 #endif
592 };
594 /**
595 * struct device - The basic device structure
596 * @parent: The device's "parent" device, the device to which it is attached.
597 * In most cases, a parent device is some sort of bus or host
598 * controller. If parent is NULL, the device, is a top-level device,
599 * which is not usually what you want.
600 * @p: Holds the private data of the driver core portions of the device.
601 * See the comment of the struct device_private for detail.
602 * @kobj: A top-level, abstract class from which other classes are derived.
603 * @init_name: Initial name of the device.
604 * @type: The type of device.
605 * This identifies the device type and carries type-specific
606 * information.
607 * @mutex: Mutex to synchronize calls to its driver.
608 * @bus: Type of bus device is on.
609 * @driver: Which driver has allocated this
610 * @platform_data: Platform data specific to the device.
611 * Example: For devices on custom boards, as typical of embedded
612 * and SOC based hardware, Linux often uses platform_data to point
613 * to board-specific structures describing devices and how they
614 * are wired. That can include what ports are available, chip
615 * variants, which GPIO pins act in what additional roles, and so
616 * on. This shrinks the "Board Support Packages" (BSPs) and
617 * minimizes board-specific #ifdefs in drivers.
618 * @power: For device power management.
619 * See Documentation/power/devices.txt for details.
620 * @pm_domain: Provide callbacks that are executed during system suspend,
621 * hibernation, system resume and during runtime PM transitions
622 * along with subsystem-level and driver-level callbacks.
623 * @numa_node: NUMA node this device is close to.
624 * @dma_mask: Dma mask (if dma'ble device).
625 * @coherent_dma_mask: Like dma_mask, but for alloc_coherent mapping as not all
626 * hardware supports 64-bit addresses for consistent allocations
627 * such descriptors.
628 * @dma_parms: A low level driver may set these to teach IOMMU code about
629 * segment limitations.
630 * @dma_pools: Dma pools (if dma'ble device).
631 * @dma_mem: Internal for coherent mem override.
632 * @archdata: For arch-specific additions.
633 * @of_node: Associated device tree node.
634 * @acpi_node: Associated ACPI device node.
635 * @devt: For creating the sysfs "dev".
636 * @id: device instance
637 * @devres_lock: Spinlock to protect the resource of the device.
638 * @devres_head: The resources list of the device.
639 * @knode_class: The node used to add the device to the class list.
640 * @class: The class of the device.
641 * @groups: Optional attribute groups.
642 * @release: Callback to free the device after all references have
643 * gone away. This should be set by the allocator of the
644 * device (i.e. the bus driver that discovered the device).
645 *
646 * At the lowest level, every device in a Linux system is represented by an
647 * instance of struct device. The device structure contains the information
648 * that the device model core needs to model the system. Most subsystems,
649 * however, track additional information about the devices they host. As a
650 * result, it is rare for devices to be represented by bare device structures;
651 * instead, that structure, like kobject structures, is usually embedded within
652 * a higher-level representation of the device.
653 */
654 struct device {
655 struct device *parent;
657 struct device_private *p;
659 struct kobject kobj;
660 const char *init_name; /* initial name of the device */
661 const struct device_type *type;
663 struct mutex mutex; /* mutex to synchronize calls to
664 * its driver.
665 */
667 struct bus_type *bus; /* type of bus device is on */
668 struct device_driver *driver; /* which driver has allocated this
669 device */
670 void *platform_data; /* Platform specific data, device
671 core doesn't touch it */
672 struct dev_pm_info power;
673 struct dev_pm_domain *pm_domain;
675 #ifdef CONFIG_NUMA
676 int numa_node; /* NUMA node this device is close to */
677 #endif
678 u64 *dma_mask; /* dma mask (if dma'able device) */
679 u64 coherent_dma_mask;/* Like dma_mask, but for
680 alloc_coherent mappings as
681 not all hardware supports
682 64 bit addresses for consistent
683 allocations such descriptors. */
685 struct device_dma_parameters *dma_parms;
687 struct list_head dma_pools; /* dma pools (if dma'ble) */
689 struct dma_coherent_mem *dma_mem; /* internal for coherent mem
690 override */
691 #ifdef CONFIG_CMA
692 struct cma *cma_area; /* contiguous memory area for dma
693 allocations */
694 #endif
695 /* arch specific additions */
696 struct dev_archdata archdata;
698 struct device_node *of_node; /* associated device tree node */
699 struct acpi_dev_node acpi_node; /* associated ACPI device node */
701 dev_t devt; /* dev_t, creates the sysfs "dev" */
702 u32 id; /* device instance */
704 spinlock_t devres_lock;
705 struct list_head devres_head;
707 struct klist_node knode_class;
708 struct class *class;
709 const struct attribute_group **groups; /* optional groups */
711 void (*release)(struct device *dev);
712 struct iommu_group *iommu_group;
713 };
715 static inline struct device *kobj_to_dev(struct kobject *kobj)
716 {
717 return container_of(kobj, struct device, kobj);
718 }
720 #ifdef CONFIG_ACPI
721 #define ACPI_HANDLE(dev) ((dev)->acpi_node.handle)
722 #define ACPI_HANDLE_SET(dev, _handle_) (dev)->acpi_node.handle = (_handle_)
723 #else
724 #define ACPI_HANDLE(dev) (NULL)
725 #define ACPI_HANDLE_SET(dev, _handle_) do { } while (0)
726 #endif
728 /* Get the wakeup routines, which depend on struct device */
729 #include <linux/pm_wakeup.h>
731 static inline const char *dev_name(const struct device *dev)
732 {
733 /* Use the init name until the kobject becomes available */
734 if (dev->init_name)
735 return dev->init_name;
737 return kobject_name(&dev->kobj);
738 }
740 extern __printf(2, 3)
741 int dev_set_name(struct device *dev, const char *name, ...);
743 #ifdef CONFIG_NUMA
744 static inline int dev_to_node(struct device *dev)
745 {
746 return dev->numa_node;
747 }
748 static inline void set_dev_node(struct device *dev, int node)
749 {
750 dev->numa_node = node;
751 }
752 #else
753 static inline int dev_to_node(struct device *dev)
754 {
755 return -1;
756 }
757 static inline void set_dev_node(struct device *dev, int node)
758 {
759 }
760 #endif
762 static inline struct pm_subsys_data *dev_to_psd(struct device *dev)
763 {
764 return dev ? dev->power.subsys_data : NULL;
765 }
767 static inline unsigned int dev_get_uevent_suppress(const struct device *dev)
768 {
769 return dev->kobj.uevent_suppress;
770 }
772 static inline void dev_set_uevent_suppress(struct device *dev, int val)
773 {
774 dev->kobj.uevent_suppress = val;
775 }
777 static inline int device_is_registered(struct device *dev)
778 {
779 return dev->kobj.state_in_sysfs;
780 }
782 static inline void device_enable_async_suspend(struct device *dev)
783 {
784 if (!dev->power.is_prepared)
785 dev->power.async_suspend = true;
786 }
788 static inline void device_disable_async_suspend(struct device *dev)
789 {
790 if (!dev->power.is_prepared)
791 dev->power.async_suspend = false;
792 }
794 static inline bool device_async_suspend_enabled(struct device *dev)
795 {
796 return !!dev->power.async_suspend;
797 }
799 static inline void pm_suspend_ignore_children(struct device *dev, bool enable)
800 {
801 dev->power.ignore_children = enable;
802 }
804 static inline void dev_pm_syscore_device(struct device *dev, bool val)
805 {
806 #ifdef CONFIG_PM_SLEEP
807 dev->power.syscore = val;
808 #endif
809 }
811 static inline void device_lock(struct device *dev)
812 {
813 mutex_lock(&dev->mutex);
814 }
816 static inline int device_trylock(struct device *dev)
817 {
818 return mutex_trylock(&dev->mutex);
819 }
821 static inline void device_unlock(struct device *dev)
822 {
823 mutex_unlock(&dev->mutex);
824 }
826 void driver_init(void);
828 /*
829 * High level routines for use by the bus drivers
830 */
831 extern int __must_check device_register(struct device *dev);
832 extern void device_unregister(struct device *dev);
833 extern void device_initialize(struct device *dev);
834 extern int __must_check device_add(struct device *dev);
835 extern void device_del(struct device *dev);
836 extern int device_for_each_child(struct device *dev, void *data,
837 int (*fn)(struct device *dev, void *data));
838 extern struct device *device_find_child(struct device *dev, void *data,
839 int (*match)(struct device *dev, void *data));
840 extern int device_rename(struct device *dev, const char *new_name);
841 extern int device_move(struct device *dev, struct device *new_parent,
842 enum dpm_order dpm_order);
843 extern const char *device_get_devnode(struct device *dev,
844 umode_t *mode, const char **tmp);
845 extern void *dev_get_drvdata(const struct device *dev);
846 extern int dev_set_drvdata(struct device *dev, void *data);
848 /*
849 * Root device objects for grouping under /sys/devices
850 */
851 extern struct device *__root_device_register(const char *name,
852 struct module *owner);
854 /*
855 * This is a macro to avoid include problems with THIS_MODULE,
856 * just as per what is done for device_schedule_callback() above.
857 */
858 #define root_device_register(name) \
859 __root_device_register(name, THIS_MODULE)
861 extern void root_device_unregister(struct device *root);
863 static inline void *dev_get_platdata(const struct device *dev)
864 {
865 return dev->platform_data;
866 }
868 /*
869 * Manual binding of a device to driver. See drivers/base/bus.c
870 * for information on use.
871 */
872 extern int __must_check device_bind_driver(struct device *dev);
873 extern void device_release_driver(struct device *dev);
874 extern int __must_check device_attach(struct device *dev);
875 extern int __must_check driver_attach(struct device_driver *drv);
876 extern int __must_check device_reprobe(struct device *dev);
878 /*
879 * Easy functions for dynamically creating devices on the fly
880 */
881 extern struct device *device_create_vargs(struct class *cls,
882 struct device *parent,
883 dev_t devt,
884 void *drvdata,
885 const char *fmt,
886 va_list vargs);
887 extern __printf(5, 6)
888 struct device *device_create(struct class *cls, struct device *parent,
889 dev_t devt, void *drvdata,
890 const char *fmt, ...);
891 extern void device_destroy(struct class *cls, dev_t devt);
893 /*
894 * Platform "fixup" functions - allow the platform to have their say
895 * about devices and actions that the general device layer doesn't
896 * know about.
897 */
898 /* Notify platform of device discovery */
899 extern int (*platform_notify)(struct device *dev);
901 extern int (*platform_notify_remove)(struct device *dev);
904 /*
905 * get_device - atomically increment the reference count for the device.
906 *
907 */
908 extern struct device *get_device(struct device *dev);
909 extern void put_device(struct device *dev);
911 #ifdef CONFIG_DEVTMPFS
912 extern int devtmpfs_create_node(struct device *dev);
913 extern int devtmpfs_delete_node(struct device *dev);
914 extern int devtmpfs_mount(const char *mntdir);
915 #else
916 static inline int devtmpfs_create_node(struct device *dev) { return 0; }
917 static inline int devtmpfs_delete_node(struct device *dev) { return 0; }
918 static inline int devtmpfs_mount(const char *mountpoint) { return 0; }
919 #endif
921 /* drivers/base/power/shutdown.c */
922 extern void device_shutdown(void);
924 /* debugging and troubleshooting/diagnostic helpers. */
925 extern const char *dev_driver_string(const struct device *dev);
928 #ifdef CONFIG_PRINTK
930 extern __printf(3, 0)
931 int dev_vprintk_emit(int level, const struct device *dev,
932 const char *fmt, va_list args);
933 extern __printf(3, 4)
934 int dev_printk_emit(int level, const struct device *dev, const char *fmt, ...);
936 extern __printf(3, 4)
937 int dev_printk(const char *level, const struct device *dev,
938 const char *fmt, ...);
939 extern __printf(2, 3)
940 int dev_emerg(const struct device *dev, const char *fmt, ...);
941 extern __printf(2, 3)
942 int dev_alert(const struct device *dev, const char *fmt, ...);
943 extern __printf(2, 3)
944 int dev_crit(const struct device *dev, const char *fmt, ...);
945 extern __printf(2, 3)
946 int dev_err(const struct device *dev, const char *fmt, ...);
947 extern __printf(2, 3)
948 int dev_warn(const struct device *dev, const char *fmt, ...);
949 extern __printf(2, 3)
950 int dev_notice(const struct device *dev, const char *fmt, ...);
951 extern __printf(2, 3)
952 int _dev_info(const struct device *dev, const char *fmt, ...);
954 #else
956 static inline __printf(3, 0)
957 int dev_vprintk_emit(int level, const struct device *dev,
958 const char *fmt, va_list args)
959 { return 0; }
960 static inline __printf(3, 4)
961 int dev_printk_emit(int level, const struct device *dev, const char *fmt, ...)
962 { return 0; }
964 static inline int __dev_printk(const char *level, const struct device *dev,
965 struct va_format *vaf)
966 { return 0; }
967 static inline __printf(3, 4)
968 int dev_printk(const char *level, const struct device *dev,
969 const char *fmt, ...)
970 { return 0; }
972 static inline __printf(2, 3)
973 int dev_emerg(const struct device *dev, const char *fmt, ...)
974 { return 0; }
975 static inline __printf(2, 3)
976 int dev_crit(const struct device *dev, const char *fmt, ...)
977 { return 0; }
978 static inline __printf(2, 3)
979 int dev_alert(const struct device *dev, const char *fmt, ...)
980 { return 0; }
981 static inline __printf(2, 3)
982 int dev_err(const struct device *dev, const char *fmt, ...)
983 { return 0; }
984 static inline __printf(2, 3)
985 int dev_warn(const struct device *dev, const char *fmt, ...)
986 { return 0; }
987 static inline __printf(2, 3)
988 int dev_notice(const struct device *dev, const char *fmt, ...)
989 { return 0; }
990 static inline __printf(2, 3)
991 int _dev_info(const struct device *dev, const char *fmt, ...)
992 { return 0; }
994 #endif
996 /*
997 * Stupid hackaround for existing uses of non-printk uses dev_info
998 *
999 * Note that the definition of dev_info below is actually _dev_info
1000 * and a macro is used to avoid redefining dev_info
1001 */
1003 #define dev_info(dev, fmt, arg...) _dev_info(dev, fmt, ##arg)
1005 #if defined(CONFIG_DYNAMIC_DEBUG)
1006 #define dev_dbg(dev, format, ...) \
1007 do { \
1008 dynamic_dev_dbg(dev, format, ##__VA_ARGS__); \
1009 } while (0)
1010 #elif defined(DEBUG)
1011 #define dev_dbg(dev, format, arg...) \
1012 dev_printk(KERN_DEBUG, dev, format, ##arg)
1013 #else
1014 #define dev_dbg(dev, format, arg...) \
1015 ({ \
1016 if (0) \
1017 dev_printk(KERN_DEBUG, dev, format, ##arg); \
1018 0; \
1019 })
1020 #endif
1022 #define dev_level_ratelimited(dev_level, dev, fmt, ...) \
1023 do { \
1024 static DEFINE_RATELIMIT_STATE(_rs, \
1025 DEFAULT_RATELIMIT_INTERVAL, \
1026 DEFAULT_RATELIMIT_BURST); \
1027 if (__ratelimit(&_rs)) \
1028 dev_level(dev, fmt, ##__VA_ARGS__); \
1029 } while (0)
1031 #define dev_emerg_ratelimited(dev, fmt, ...) \
1032 dev_level_ratelimited(dev_emerg, dev, fmt, ##__VA_ARGS__)
1033 #define dev_alert_ratelimited(dev, fmt, ...) \
1034 dev_level_ratelimited(dev_alert, dev, fmt, ##__VA_ARGS__)
1035 #define dev_crit_ratelimited(dev, fmt, ...) \
1036 dev_level_ratelimited(dev_crit, dev, fmt, ##__VA_ARGS__)
1037 #define dev_err_ratelimited(dev, fmt, ...) \
1038 dev_level_ratelimited(dev_err, dev, fmt, ##__VA_ARGS__)
1039 #define dev_warn_ratelimited(dev, fmt, ...) \
1040 dev_level_ratelimited(dev_warn, dev, fmt, ##__VA_ARGS__)
1041 #define dev_notice_ratelimited(dev, fmt, ...) \
1042 dev_level_ratelimited(dev_notice, dev, fmt, ##__VA_ARGS__)
1043 #define dev_info_ratelimited(dev, fmt, ...) \
1044 dev_level_ratelimited(dev_info, dev, fmt, ##__VA_ARGS__)
1045 #if defined(CONFIG_DYNAMIC_DEBUG) || defined(DEBUG)
1046 #define dev_dbg_ratelimited(dev, fmt, ...) \
1047 do { \
1048 static DEFINE_RATELIMIT_STATE(_rs, \
1049 DEFAULT_RATELIMIT_INTERVAL, \
1050 DEFAULT_RATELIMIT_BURST); \
1051 DEFINE_DYNAMIC_DEBUG_METADATA(descriptor, fmt); \
1052 if (unlikely(descriptor.flags & _DPRINTK_FLAGS_PRINT) && \
1053 __ratelimit(&_rs)) \
1054 __dynamic_pr_debug(&descriptor, pr_fmt(fmt), \
1055 ##__VA_ARGS__); \
1056 } while (0)
1057 #else
1058 #define dev_dbg_ratelimited(dev, fmt, ...) \
1059 no_printk(KERN_DEBUG pr_fmt(fmt), ##__VA_ARGS__)
1060 #endif
1062 #ifdef VERBOSE_DEBUG
1063 #define dev_vdbg dev_dbg
1064 #else
1065 #define dev_vdbg(dev, format, arg...) \
1066 ({ \
1067 if (0) \
1068 dev_printk(KERN_DEBUG, dev, format, ##arg); \
1069 0; \
1070 })
1071 #endif
1073 /*
1074 * dev_WARN*() acts like dev_printk(), but with the key difference
1075 * of using a WARN/WARN_ON to get the message out, including the
1076 * file/line information and a backtrace.
1077 */
1078 #define dev_WARN(dev, format, arg...) \
1079 WARN(1, "Device: %s\n" format, dev_driver_string(dev), ## arg);
1081 #define dev_WARN_ONCE(dev, condition, format, arg...) \
1082 WARN_ONCE(condition, "Device %s\n" format, \
1083 dev_driver_string(dev), ## arg)
1085 /* Create alias, so I can be autoloaded. */
1086 #define MODULE_ALIAS_CHARDEV(major,minor) \
1087 MODULE_ALIAS("char-major-" __stringify(major) "-" __stringify(minor))
1088 #define MODULE_ALIAS_CHARDEV_MAJOR(major) \
1089 MODULE_ALIAS("char-major-" __stringify(major) "-*")
1091 #ifdef CONFIG_SYSFS_DEPRECATED
1092 extern long sysfs_deprecated;
1093 #else
1094 #define sysfs_deprecated 0
1095 #endif
1097 /**
1098 * module_driver() - Helper macro for drivers that don't do anything
1099 * special in module init/exit. This eliminates a lot of boilerplate.
1100 * Each module may only use this macro once, and calling it replaces
1101 * module_init() and module_exit().
1102 *
1103 * @__driver: driver name
1104 * @__register: register function for this driver type
1105 * @__unregister: unregister function for this driver type
1106 * @...: Additional arguments to be passed to __register and __unregister.
1107 *
1108 * Use this macro to construct bus specific macros for registering
1109 * drivers, and do not use it on its own.
1110 */
1111 #define module_driver(__driver, __register, __unregister, ...) \
1112 static int __init __driver##_init(void) \
1113 { \
1114 return __register(&(__driver) , ##__VA_ARGS__); \
1115 } \
1116 module_init(__driver##_init); \
1117 static void __exit __driver##_exit(void) \
1118 { \
1119 __unregister(&(__driver) , ##__VA_ARGS__); \
1120 } \
1121 module_exit(__driver##_exit);
1123 #endif /* _DEVICE_H_ */