]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/blob - include/linux/ethtool.h
Merge branch 'p-ti-linux-3.8.y' into p-ti-android-3.8.y
[android-sdk/kernel-video.git] / include / linux / ethtool.h
1 /*
2  * ethtool.h: Defines for Linux ethtool.
3  *
4  * Copyright (C) 1998 David S. Miller (davem@redhat.com)
5  * Copyright 2001 Jeff Garzik <jgarzik@pobox.com>
6  * Portions Copyright 2001 Sun Microsystems (thockin@sun.com)
7  * Portions Copyright 2002 Intel (eli.kupermann@intel.com,
8  *                                christopher.leech@intel.com,
9  *                                scott.feldman@intel.com)
10  * Portions Copyright (C) Sun Microsystems 2008
11  */
12 #ifndef _LINUX_ETHTOOL_H
13 #define _LINUX_ETHTOOL_H
15 #include <linux/compat.h>
16 #include <uapi/linux/ethtool.h>
18 #ifdef CONFIG_COMPAT
20 struct compat_ethtool_rx_flow_spec {
21         u32             flow_type;
22         union ethtool_flow_union h_u;
23         struct ethtool_flow_ext h_ext;
24         union ethtool_flow_union m_u;
25         struct ethtool_flow_ext m_ext;
26         compat_u64      ring_cookie;
27         u32             location;
28 };
30 struct compat_ethtool_rxnfc {
31         u32                             cmd;
32         u32                             flow_type;
33         compat_u64                      data;
34         struct compat_ethtool_rx_flow_spec fs;
35         u32                             rule_cnt;
36         u32                             rule_locs[0];
37 };
39 #endif /* CONFIG_COMPAT */
41 #include <linux/rculist.h>
43 extern int __ethtool_get_settings(struct net_device *dev,
44                                   struct ethtool_cmd *cmd);
46 /**
47  * enum ethtool_phys_id_state - indicator state for physical identification
48  * @ETHTOOL_ID_INACTIVE: Physical ID indicator should be deactivated
49  * @ETHTOOL_ID_ACTIVE: Physical ID indicator should be activated
50  * @ETHTOOL_ID_ON: LED should be turned on (used iff %ETHTOOL_ID_ACTIVE
51  *      is not supported)
52  * @ETHTOOL_ID_OFF: LED should be turned off (used iff %ETHTOOL_ID_ACTIVE
53  *      is not supported)
54  */
55 enum ethtool_phys_id_state {
56         ETHTOOL_ID_INACTIVE,
57         ETHTOOL_ID_ACTIVE,
58         ETHTOOL_ID_ON,
59         ETHTOOL_ID_OFF
60 };
62 struct net_device;
64 /* Some generic methods drivers may use in their ethtool_ops */
65 u32 ethtool_op_get_link(struct net_device *dev);
66 int ethtool_op_get_ts_info(struct net_device *dev, struct ethtool_ts_info *eti);
68 /**
69  * ethtool_rxfh_indir_default - get default value for RX flow hash indirection
70  * @index: Index in RX flow hash indirection table
71  * @n_rx_rings: Number of RX rings to use
72  *
73  * This function provides the default policy for RX flow hash indirection.
74  */
75 static inline u32 ethtool_rxfh_indir_default(u32 index, u32 n_rx_rings)
76 {
77         return index % n_rx_rings;
78 }
80 /**
81  * struct ethtool_ops - optional netdev operations
82  * @get_settings: Get various device settings including Ethernet link
83  *      settings. The @cmd parameter is expected to have been cleared
84  *      before get_settings is called. Returns a negative error code or
85  *      zero.
86  * @set_settings: Set various device settings including Ethernet link
87  *      settings.  Returns a negative error code or zero.
88  * @get_drvinfo: Report driver/device information.  Should only set the
89  *      @driver, @version, @fw_version and @bus_info fields.  If not
90  *      implemented, the @driver and @bus_info fields will be filled in
91  *      according to the netdev's parent device.
92  * @get_regs_len: Get buffer length required for @get_regs
93  * @get_regs: Get device registers
94  * @get_wol: Report whether Wake-on-Lan is enabled
95  * @set_wol: Turn Wake-on-Lan on or off.  Returns a negative error code
96  *      or zero.
97  * @get_msglevel: Report driver message level.  This should be the value
98  *      of the @msg_enable field used by netif logging functions.
99  * @set_msglevel: Set driver message level
100  * @nway_reset: Restart autonegotiation.  Returns a negative error code
101  *      or zero.
102  * @get_link: Report whether physical link is up.  Will only be called if
103  *      the netdev is up.  Should usually be set to ethtool_op_get_link(),
104  *      which uses netif_carrier_ok().
105  * @get_eeprom: Read data from the device EEPROM.
106  *      Should fill in the magic field.  Don't need to check len for zero
107  *      or wraparound.  Fill in the data argument with the eeprom values
108  *      from offset to offset + len.  Update len to the amount read.
109  *      Returns an error or zero.
110  * @set_eeprom: Write data to the device EEPROM.
111  *      Should validate the magic field.  Don't need to check len for zero
112  *      or wraparound.  Update len to the amount written.  Returns an error
113  *      or zero.
114  * @get_coalesce: Get interrupt coalescing parameters.  Returns a negative
115  *      error code or zero.
116  * @set_coalesce: Set interrupt coalescing parameters.  Returns a negative
117  *      error code or zero.
118  * @get_ringparam: Report ring sizes
119  * @set_ringparam: Set ring sizes.  Returns a negative error code or zero.
120  * @get_pauseparam: Report pause parameters
121  * @set_pauseparam: Set pause parameters.  Returns a negative error code
122  *      or zero.
123  * @self_test: Run specified self-tests
124  * @get_strings: Return a set of strings that describe the requested objects
125  * @set_phys_id: Identify the physical devices, e.g. by flashing an LED
126  *      attached to it.  The implementation may update the indicator
127  *      asynchronously or synchronously, but in either case it must return
128  *      quickly.  It is initially called with the argument %ETHTOOL_ID_ACTIVE,
129  *      and must either activate asynchronous updates and return zero, return
130  *      a negative error or return a positive frequency for synchronous
131  *      indication (e.g. 1 for one on/off cycle per second).  If it returns
132  *      a frequency then it will be called again at intervals with the
133  *      argument %ETHTOOL_ID_ON or %ETHTOOL_ID_OFF and should set the state of
134  *      the indicator accordingly.  Finally, it is called with the argument
135  *      %ETHTOOL_ID_INACTIVE and must deactivate the indicator.  Returns a
136  *      negative error code or zero.
137  * @get_ethtool_stats: Return extended statistics about the device.
138  *      This is only useful if the device maintains statistics not
139  *      included in &struct rtnl_link_stats64.
140  * @begin: Function to be called before any other operation.  Returns a
141  *      negative error code or zero.
142  * @complete: Function to be called after any other operation except
143  *      @begin.  Will be called even if the other operation failed.
144  * @get_priv_flags: Report driver-specific feature flags.
145  * @set_priv_flags: Set driver-specific feature flags.  Returns a negative
146  *      error code or zero.
147  * @get_sset_count: Get number of strings that @get_strings will write.
148  * @get_rxnfc: Get RX flow classification rules.  Returns a negative
149  *      error code or zero.
150  * @set_rxnfc: Set RX flow classification rules.  Returns a negative
151  *      error code or zero.
152  * @flash_device: Write a firmware image to device's flash memory.
153  *      Returns a negative error code or zero.
154  * @reset: Reset (part of) the device, as specified by a bitmask of
155  *      flags from &enum ethtool_reset_flags.  Returns a negative
156  *      error code or zero.
157  * @get_rxfh_indir_size: Get the size of the RX flow hash indirection table.
158  *      Returns zero if not supported for this specific device.
159  * @get_rxfh_indir: Get the contents of the RX flow hash indirection table.
160  *      Will not be called if @get_rxfh_indir_size returns zero.
161  *      Returns a negative error code or zero.
162  * @set_rxfh_indir: Set the contents of the RX flow hash indirection table.
163  *      Will not be called if @get_rxfh_indir_size returns zero.
164  *      Returns a negative error code or zero.
165  * @get_channels: Get number of channels.
166  * @set_channels: Set number of channels.  Returns a negative error code or
167  *      zero.
168  * @get_dump_flag: Get dump flag indicating current dump length, version,
169  *                 and flag of the device.
170  * @get_dump_data: Get dump data.
171  * @set_dump: Set dump specific flags to the device.
172  * @get_ts_info: Get the time stamping and PTP hardware clock capabilities.
173  *      Drivers supporting transmit time stamps in software should set this to
174  *      ethtool_op_get_ts_info().
175  * @get_module_info: Get the size and type of the eeprom contained within
176  *      a plug-in module.
177  * @get_module_eeprom: Get the eeprom information from the plug-in module
178  * @get_eee: Get Energy-Efficient (EEE) supported and status.
179  * @set_eee: Set EEE status (enable/disable) as well as LPI timers.
180  *
181  * All operations are optional (i.e. the function pointer may be set
182  * to %NULL) and callers must take this into account.  Callers must
183  * hold the RTNL lock.
184  *
185  * See the structures used by these operations for further documentation.
186  *
187  * See &struct net_device and &struct net_device_ops for documentation
188  * of the generic netdev features interface.
189  */
190 struct ethtool_ops {
191         int     (*get_settings)(struct net_device *, struct ethtool_cmd *);
192         int     (*set_settings)(struct net_device *, struct ethtool_cmd *);
193         void    (*get_drvinfo)(struct net_device *, struct ethtool_drvinfo *);
194         int     (*get_regs_len)(struct net_device *);
195         void    (*get_regs)(struct net_device *, struct ethtool_regs *, void *);
196         void    (*get_wol)(struct net_device *, struct ethtool_wolinfo *);
197         int     (*set_wol)(struct net_device *, struct ethtool_wolinfo *);
198         u32     (*get_msglevel)(struct net_device *);
199         void    (*set_msglevel)(struct net_device *, u32);
200         int     (*nway_reset)(struct net_device *);
201         u32     (*get_link)(struct net_device *);
202         int     (*get_eeprom_len)(struct net_device *);
203         int     (*get_eeprom)(struct net_device *,
204                               struct ethtool_eeprom *, u8 *);
205         int     (*set_eeprom)(struct net_device *,
206                               struct ethtool_eeprom *, u8 *);
207         int     (*get_coalesce)(struct net_device *, struct ethtool_coalesce *);
208         int     (*set_coalesce)(struct net_device *, struct ethtool_coalesce *);
209         void    (*get_ringparam)(struct net_device *,
210                                  struct ethtool_ringparam *);
211         int     (*set_ringparam)(struct net_device *,
212                                  struct ethtool_ringparam *);
213         void    (*get_pauseparam)(struct net_device *,
214                                   struct ethtool_pauseparam*);
215         int     (*set_pauseparam)(struct net_device *,
216                                   struct ethtool_pauseparam*);
217         void    (*self_test)(struct net_device *, struct ethtool_test *, u64 *);
218         void    (*get_strings)(struct net_device *, u32 stringset, u8 *);
219         int     (*set_phys_id)(struct net_device *, enum ethtool_phys_id_state);
220         void    (*get_ethtool_stats)(struct net_device *,
221                                      struct ethtool_stats *, u64 *);
222         int     (*begin)(struct net_device *);
223         void    (*complete)(struct net_device *);
224         u32     (*get_priv_flags)(struct net_device *);
225         int     (*set_priv_flags)(struct net_device *, u32);
226         int     (*get_sset_count)(struct net_device *, int);
227         int     (*get_rxnfc)(struct net_device *,
228                              struct ethtool_rxnfc *, u32 *rule_locs);
229         int     (*set_rxnfc)(struct net_device *, struct ethtool_rxnfc *);
230         int     (*flash_device)(struct net_device *, struct ethtool_flash *);
231         int     (*reset)(struct net_device *, u32 *);
232         u32     (*get_rxfh_indir_size)(struct net_device *);
233         int     (*get_rxfh_indir)(struct net_device *, u32 *);
234         int     (*set_rxfh_indir)(struct net_device *, const u32 *);
235         void    (*get_channels)(struct net_device *, struct ethtool_channels *);
236         int     (*set_channels)(struct net_device *, struct ethtool_channels *);
237         int     (*get_dump_flag)(struct net_device *, struct ethtool_dump *);
238         int     (*get_dump_data)(struct net_device *,
239                                  struct ethtool_dump *, void *);
240         int     (*set_dump)(struct net_device *, struct ethtool_dump *);
241         int     (*get_ts_info)(struct net_device *, struct ethtool_ts_info *);
242         int     (*get_module_info)(struct net_device *,
243                                    struct ethtool_modinfo *);
244         int     (*get_module_eeprom)(struct net_device *,
245                                      struct ethtool_eeprom *, u8 *);
246         int     (*get_eee)(struct net_device *, struct ethtool_eee *);
247         int     (*set_eee)(struct net_device *, struct ethtool_eee *);
250 };
251 #endif /* _LINUX_ETHTOOL_H */