1 /* ------------------------------------------------------------------------- */
2 /* */
3 /* i2c.h - definitions for the i2c-bus interface */
4 /* */
5 /* ------------------------------------------------------------------------- */
6 /* Copyright (C) 1995-2000 Simon G. Vogl
8 This program is free software; you can redistribute it and/or modify
9 it under the terms of the GNU General Public License as published by
10 the Free Software Foundation; either version 2 of the License, or
11 (at your option) any later version.
13 This program is distributed in the hope that it will be useful,
14 but WITHOUT ANY WARRANTY; without even the implied warranty of
15 MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
16 GNU General Public License for more details.
18 You should have received a copy of the GNU General Public License
19 along with this program; if not, write to the Free Software
20 Foundation, Inc., 51 Franklin Street, Fifth Floor, Boston,
21 MA 02110-1301 USA. */
22 /* ------------------------------------------------------------------------- */
24 /* With some changes from Kyösti Mälkki <kmalkki@cc.hut.fi> and
25 Frodo Looijaard <frodol@dds.nl> */
26 #ifndef _LINUX_I2C_H
27 #define _LINUX_I2C_H
29 #include <linux/mod_devicetable.h>
30 #include <linux/device.h> /* for struct device */
31 #include <linux/sched.h> /* for completion */
32 #include <linux/mutex.h>
33 #include <linux/of.h> /* for struct device_node */
34 #include <linux/swab.h> /* for swab16 */
35 #include <uapi/linux/i2c.h>
37 extern struct bus_type i2c_bus_type;
38 extern struct device_type i2c_adapter_type;
40 /* --- General options ------------------------------------------------ */
42 struct i2c_msg;
43 struct i2c_algorithm;
44 struct i2c_adapter;
45 struct i2c_client;
46 struct i2c_driver;
47 union i2c_smbus_data;
48 struct i2c_board_info;
50 struct module;
52 #if defined(CONFIG_I2C) || defined(CONFIG_I2C_MODULE)
53 /*
54 * The master routines are the ones normally used to transmit data to devices
55 * on a bus (or read from them). Apart from two basic transfer functions to
56 * transmit one message at a time, a more complex version can be used to
57 * transmit an arbitrary number of messages without interruption.
58 * @count must be be less than 64k since msg.len is u16.
59 */
60 extern int i2c_master_send(const struct i2c_client *client, const char *buf,
61 int count);
62 extern int i2c_master_recv(const struct i2c_client *client, char *buf,
63 int count);
65 /* Transfer num messages.
66 */
67 extern int i2c_transfer(struct i2c_adapter *adap, struct i2c_msg *msgs,
68 int num);
69 /* Unlocked flavor */
70 extern int __i2c_transfer(struct i2c_adapter *adap, struct i2c_msg *msgs,
71 int num);
73 /* This is the very generalized SMBus access routine. You probably do not
74 want to use this, though; one of the functions below may be much easier,
75 and probably just as fast.
76 Note that we use i2c_adapter here, because you do not need a specific
77 smbus adapter to call this function. */
78 extern s32 i2c_smbus_xfer(struct i2c_adapter *adapter, u16 addr,
79 unsigned short flags, char read_write, u8 command,
80 int size, union i2c_smbus_data *data);
82 /* Now follow the 'nice' access routines. These also document the calling
83 conventions of i2c_smbus_xfer. */
85 extern s32 i2c_smbus_read_byte(const struct i2c_client *client);
86 extern s32 i2c_smbus_write_byte(const struct i2c_client *client, u8 value);
87 extern s32 i2c_smbus_read_byte_data(const struct i2c_client *client,
88 u8 command);
89 extern s32 i2c_smbus_write_byte_data(const struct i2c_client *client,
90 u8 command, u8 value);
91 extern s32 i2c_smbus_read_word_data(const struct i2c_client *client,
92 u8 command);
93 extern s32 i2c_smbus_write_word_data(const struct i2c_client *client,
94 u8 command, u16 value);
96 static inline s32
97 i2c_smbus_read_word_swapped(const struct i2c_client *client, u8 command)
98 {
99 s32 value = i2c_smbus_read_word_data(client, command);
101 return (value < 0) ? value : swab16(value);
102 }
104 static inline s32
105 i2c_smbus_write_word_swapped(const struct i2c_client *client,
106 u8 command, u16 value)
107 {
108 return i2c_smbus_write_word_data(client, command, swab16(value));
109 }
111 /* Returns the number of read bytes */
112 extern s32 i2c_smbus_read_block_data(const struct i2c_client *client,
113 u8 command, u8 *values);
114 extern s32 i2c_smbus_write_block_data(const struct i2c_client *client,
115 u8 command, u8 length, const u8 *values);
116 /* Returns the number of read bytes */
117 extern s32 i2c_smbus_read_i2c_block_data(const struct i2c_client *client,
118 u8 command, u8 length, u8 *values);
119 extern s32 i2c_smbus_write_i2c_block_data(const struct i2c_client *client,
120 u8 command, u8 length,
121 const u8 *values);
122 #endif /* I2C */
124 /**
125 * struct i2c_driver - represent an I2C device driver
126 * @class: What kind of i2c device we instantiate (for detect)
127 * @attach_adapter: Callback for bus addition (deprecated)
128 * @detach_adapter: Callback for bus removal (deprecated)
129 * @probe: Callback for device binding
130 * @remove: Callback for device unbinding
131 * @shutdown: Callback for device shutdown
132 * @suspend: Callback for device suspend
133 * @resume: Callback for device resume
134 * @alert: Alert callback, for example for the SMBus alert protocol
135 * @command: Callback for bus-wide signaling (optional)
136 * @driver: Device driver model driver
137 * @id_table: List of I2C devices supported by this driver
138 * @detect: Callback for device detection
139 * @address_list: The I2C addresses to probe (for detect)
140 * @clients: List of detected clients we created (for i2c-core use only)
141 *
142 * The driver.owner field should be set to the module owner of this driver.
143 * The driver.name field should be set to the name of this driver.
144 *
145 * For automatic device detection, both @detect and @address_list must
146 * be defined. @class should also be set, otherwise only devices forced
147 * with module parameters will be created. The detect function must
148 * fill at least the name field of the i2c_board_info structure it is
149 * handed upon successful detection, and possibly also the flags field.
150 *
151 * If @detect is missing, the driver will still work fine for enumerated
152 * devices. Detected devices simply won't be supported. This is expected
153 * for the many I2C/SMBus devices which can't be detected reliably, and
154 * the ones which can always be enumerated in practice.
155 *
156 * The i2c_client structure which is handed to the @detect callback is
157 * not a real i2c_client. It is initialized just enough so that you can
158 * call i2c_smbus_read_byte_data and friends on it. Don't do anything
159 * else with it. In particular, calling dev_dbg and friends on it is
160 * not allowed.
161 */
162 struct i2c_driver {
163 unsigned int class;
165 /* Notifies the driver that a new bus has appeared or is about to be
166 * removed. You should avoid using this, it will be removed in a
167 * near future.
168 */
169 int (*attach_adapter)(struct i2c_adapter *) __deprecated;
170 int (*detach_adapter)(struct i2c_adapter *) __deprecated;
172 /* Standard driver model interfaces */
173 int (*probe)(struct i2c_client *, const struct i2c_device_id *);
174 int (*remove)(struct i2c_client *);
176 /* driver model interfaces that don't relate to enumeration */
177 void (*shutdown)(struct i2c_client *);
178 int (*suspend)(struct i2c_client *, pm_message_t mesg);
179 int (*resume)(struct i2c_client *);
181 /* Alert callback, for example for the SMBus alert protocol.
182 * The format and meaning of the data value depends on the protocol.
183 * For the SMBus alert protocol, there is a single bit of data passed
184 * as the alert response's low bit ("event flag").
185 */
186 void (*alert)(struct i2c_client *, unsigned int data);
188 /* a ioctl like command that can be used to perform specific functions
189 * with the device.
190 */
191 int (*command)(struct i2c_client *client, unsigned int cmd, void *arg);
193 struct device_driver driver;
194 const struct i2c_device_id *id_table;
196 /* Device detection callback for automatic device creation */
197 int (*detect)(struct i2c_client *, struct i2c_board_info *);
198 const unsigned short *address_list;
199 struct list_head clients;
200 };
201 #define to_i2c_driver(d) container_of(d, struct i2c_driver, driver)
203 /**
204 * struct i2c_client - represent an I2C slave device
205 * @flags: I2C_CLIENT_TEN indicates the device uses a ten bit chip address;
206 * I2C_CLIENT_PEC indicates it uses SMBus Packet Error Checking
207 * @addr: Address used on the I2C bus connected to the parent adapter.
208 * @name: Indicates the type of the device, usually a chip name that's
209 * generic enough to hide second-sourcing and compatible revisions.
210 * @adapter: manages the bus segment hosting this I2C device
211 * @driver: device's driver, hence pointer to access routines
212 * @dev: Driver model device node for the slave.
213 * @irq: indicates the IRQ generated by this device (if any)
214 * @detected: member of an i2c_driver.clients list or i2c-core's
215 * userspace_devices list
216 *
217 * An i2c_client identifies a single device (i.e. chip) connected to an
218 * i2c bus. The behaviour exposed to Linux is defined by the driver
219 * managing the device.
220 */
221 struct i2c_client {
222 unsigned short flags; /* div., see below */
223 unsigned short addr; /* chip address - NOTE: 7bit */
224 /* addresses are stored in the */
225 /* _LOWER_ 7 bits */
226 char name[I2C_NAME_SIZE];
227 struct i2c_adapter *adapter; /* the adapter we sit on */
228 struct i2c_driver *driver; /* and our access routines */
229 struct device dev; /* the device structure */
230 int irq; /* irq issued by device */
231 struct list_head detected;
232 };
233 #define to_i2c_client(d) container_of(d, struct i2c_client, dev)
235 extern struct i2c_client *i2c_verify_client(struct device *dev);
236 extern struct i2c_adapter *i2c_verify_adapter(struct device *dev);
238 static inline struct i2c_client *kobj_to_i2c_client(struct kobject *kobj)
239 {
240 struct device * const dev = container_of(kobj, struct device, kobj);
241 return to_i2c_client(dev);
242 }
244 static inline void *i2c_get_clientdata(const struct i2c_client *dev)
245 {
246 return dev_get_drvdata(&dev->dev);
247 }
249 static inline void i2c_set_clientdata(struct i2c_client *dev, void *data)
250 {
251 dev_set_drvdata(&dev->dev, data);
252 }
254 /**
255 * struct i2c_board_info - template for device creation
256 * @type: chip type, to initialize i2c_client.name
257 * @flags: to initialize i2c_client.flags
258 * @addr: stored in i2c_client.addr
259 * @platform_data: stored in i2c_client.dev.platform_data
260 * @archdata: copied into i2c_client.dev.archdata
261 * @of_node: pointer to OpenFirmware device node
262 * @acpi_node: ACPI device node
263 * @irq: stored in i2c_client.irq
264 *
265 * I2C doesn't actually support hardware probing, although controllers and
266 * devices may be able to use I2C_SMBUS_QUICK to tell whether or not there's
267 * a device at a given address. Drivers commonly need more information than
268 * that, such as chip type, configuration, associated IRQ, and so on.
269 *
270 * i2c_board_info is used to build tables of information listing I2C devices
271 * that are present. This information is used to grow the driver model tree.
272 * For mainboards this is done statically using i2c_register_board_info();
273 * bus numbers identify adapters that aren't yet available. For add-on boards,
274 * i2c_new_device() does this dynamically with the adapter already known.
275 */
276 struct i2c_board_info {
277 char type[I2C_NAME_SIZE];
278 unsigned short flags;
279 unsigned short addr;
280 void *platform_data;
281 struct dev_archdata *archdata;
282 struct device_node *of_node;
283 struct acpi_dev_node acpi_node;
284 int irq;
285 };
287 /**
288 * I2C_BOARD_INFO - macro used to list an i2c device and its address
289 * @dev_type: identifies the device type
290 * @dev_addr: the device's address on the bus.
291 *
292 * This macro initializes essential fields of a struct i2c_board_info,
293 * declaring what has been provided on a particular board. Optional
294 * fields (such as associated irq, or device-specific platform_data)
295 * are provided using conventional syntax.
296 */
297 #define I2C_BOARD_INFO(dev_type, dev_addr) \
298 .type = dev_type, .addr = (dev_addr)
301 #if defined(CONFIG_I2C) || defined(CONFIG_I2C_MODULE)
302 /* Add-on boards should register/unregister their devices; e.g. a board
303 * with integrated I2C, a config eeprom, sensors, and a codec that's
304 * used in conjunction with the primary hardware.
305 */
306 extern struct i2c_client *
307 i2c_new_device(struct i2c_adapter *adap, struct i2c_board_info const *info);
309 /* If you don't know the exact address of an I2C device, use this variant
310 * instead, which can probe for device presence in a list of possible
311 * addresses. The "probe" callback function is optional. If it is provided,
312 * it must return 1 on successful probe, 0 otherwise. If it is not provided,
313 * a default probing method is used.
314 */
315 extern struct i2c_client *
316 i2c_new_probed_device(struct i2c_adapter *adap,
317 struct i2c_board_info *info,
318 unsigned short const *addr_list,
319 int (*probe)(struct i2c_adapter *, unsigned short addr));
321 /* Common custom probe functions */
322 extern int i2c_probe_func_quick_read(struct i2c_adapter *, unsigned short addr);
324 /* For devices that use several addresses, use i2c_new_dummy() to make
325 * client handles for the extra addresses.
326 */
327 extern struct i2c_client *
328 i2c_new_dummy(struct i2c_adapter *adap, u16 address);
330 extern void i2c_unregister_device(struct i2c_client *);
331 #endif /* I2C */
333 /* Mainboard arch_initcall() code should register all its I2C devices.
334 * This is done at arch_initcall time, before declaring any i2c adapters.
335 * Modules for add-on boards must use other calls.
336 */
337 #ifdef CONFIG_I2C_BOARDINFO
338 extern int
339 i2c_register_board_info(int busnum, struct i2c_board_info const *info,
340 unsigned n);
341 #else
342 static inline int
343 i2c_register_board_info(int busnum, struct i2c_board_info const *info,
344 unsigned n)
345 {
346 return 0;
347 }
348 #endif /* I2C_BOARDINFO */
350 /*
351 * The following structs are for those who like to implement new bus drivers:
352 * i2c_algorithm is the interface to a class of hardware solutions which can
353 * be addressed using the same bus algorithms - i.e. bit-banging or the PCF8584
354 * to name two of the most common.
355 */
356 struct i2c_algorithm {
357 /* If an adapter algorithm can't do I2C-level access, set master_xfer
358 to NULL. If an adapter algorithm can do SMBus access, set
359 smbus_xfer. If set to NULL, the SMBus protocol is simulated
360 using common I2C messages */
361 /* master_xfer should return the number of messages successfully
362 processed, or a negative value on error */
363 int (*master_xfer)(struct i2c_adapter *adap, struct i2c_msg *msgs,
364 int num);
365 int (*smbus_xfer) (struct i2c_adapter *adap, u16 addr,
366 unsigned short flags, char read_write,
367 u8 command, int size, union i2c_smbus_data *data);
369 /* To determine what the adapter supports */
370 u32 (*functionality) (struct i2c_adapter *);
371 };
373 /*
374 * i2c_adapter is the structure used to identify a physical i2c bus along
375 * with the access algorithms necessary to access it.
376 */
377 struct i2c_adapter {
378 struct module *owner;
379 unsigned int class; /* classes to allow probing for */
380 const struct i2c_algorithm *algo; /* the algorithm to access the bus */
381 void *algo_data;
383 /* data fields that are valid for all devices */
384 struct rt_mutex bus_lock;
386 int timeout; /* in jiffies */
387 int retries;
388 struct device dev; /* the adapter device */
390 int nr;
391 char name[48];
392 struct completion dev_released;
394 struct mutex userspace_clients_lock;
395 struct list_head userspace_clients;
396 };
397 #define to_i2c_adapter(d) container_of(d, struct i2c_adapter, dev)
399 static inline void *i2c_get_adapdata(const struct i2c_adapter *dev)
400 {
401 return dev_get_drvdata(&dev->dev);
402 }
404 static inline void i2c_set_adapdata(struct i2c_adapter *dev, void *data)
405 {
406 dev_set_drvdata(&dev->dev, data);
407 }
409 static inline struct i2c_adapter *
410 i2c_parent_is_i2c_adapter(const struct i2c_adapter *adapter)
411 {
412 struct device *parent = adapter->dev.parent;
414 if (parent != NULL && parent->type == &i2c_adapter_type)
415 return to_i2c_adapter(parent);
416 else
417 return NULL;
418 }
420 int i2c_for_each_dev(void *data, int (*fn)(struct device *, void *));
422 /* Adapter locking functions, exported for shared pin cases */
423 void i2c_lock_adapter(struct i2c_adapter *);
424 void i2c_unlock_adapter(struct i2c_adapter *);
426 /*flags for the client struct: */
427 #define I2C_CLIENT_PEC 0x04 /* Use Packet Error Checking */
428 #define I2C_CLIENT_TEN 0x10 /* we have a ten bit chip address */
429 /* Must equal I2C_M_TEN below */
430 #define I2C_CLIENT_WAKE 0x80 /* for board_info; true iff can wake */
431 #define I2C_CLIENT_SCCB 0x9000 /* Use Omnivision SCCB protocol */
432 /* Must match I2C_M_STOP|IGNORE_NAK */
434 /* i2c adapter classes (bitmask) */
435 #define I2C_CLASS_HWMON (1<<0) /* lm_sensors, ... */
436 #define I2C_CLASS_DDC (1<<3) /* DDC bus on graphics adapters */
437 #define I2C_CLASS_SPD (1<<7) /* Memory modules */
439 /* Internal numbers to terminate lists */
440 #define I2C_CLIENT_END 0xfffeU
442 /* Construct an I2C_CLIENT_END-terminated array of i2c addresses */
443 #define I2C_ADDRS(addr, addrs...) \
444 ((const unsigned short []){ addr, ## addrs, I2C_CLIENT_END })
447 /* ----- functions exported by i2c.o */
449 /* administration...
450 */
451 #if defined(CONFIG_I2C) || defined(CONFIG_I2C_MODULE)
452 extern int i2c_add_adapter(struct i2c_adapter *);
453 extern int i2c_del_adapter(struct i2c_adapter *);
454 extern int i2c_add_numbered_adapter(struct i2c_adapter *);
456 extern int i2c_register_driver(struct module *, struct i2c_driver *);
457 extern void i2c_del_driver(struct i2c_driver *);
459 /* use a define to avoid include chaining to get THIS_MODULE */
460 #define i2c_add_driver(driver) \
461 i2c_register_driver(THIS_MODULE, driver)
463 extern struct i2c_client *i2c_use_client(struct i2c_client *client);
464 extern void i2c_release_client(struct i2c_client *client);
466 /* call the i2c_client->command() of all attached clients with
467 * the given arguments */
468 extern void i2c_clients_command(struct i2c_adapter *adap,
469 unsigned int cmd, void *arg);
471 extern struct i2c_adapter *i2c_get_adapter(int nr);
472 extern void i2c_put_adapter(struct i2c_adapter *adap);
475 /* Return the functionality mask */
476 static inline u32 i2c_get_functionality(struct i2c_adapter *adap)
477 {
478 return adap->algo->functionality(adap);
479 }
481 /* Return 1 if adapter supports everything we need, 0 if not. */
482 static inline int i2c_check_functionality(struct i2c_adapter *adap, u32 func)
483 {
484 return (func & i2c_get_functionality(adap)) == func;
485 }
487 /* Return the adapter number for a specific adapter */
488 static inline int i2c_adapter_id(struct i2c_adapter *adap)
489 {
490 return adap->nr;
491 }
493 /**
494 * module_i2c_driver() - Helper macro for registering a I2C driver
495 * @__i2c_driver: i2c_driver struct
496 *
497 * Helper macro for I2C drivers which do not do anything special in module
498 * init/exit. This eliminates a lot of boilerplate. Each module may only
499 * use this macro once, and calling it replaces module_init() and module_exit()
500 */
501 #define module_i2c_driver(__i2c_driver) \
502 module_driver(__i2c_driver, i2c_add_driver, \
503 i2c_del_driver)
505 #endif /* I2C */
507 #if IS_ENABLED(CONFIG_ACPI_I2C)
508 extern void acpi_i2c_register_devices(struct i2c_adapter *adap);
509 #else
510 static inline void acpi_i2c_register_devices(struct i2c_adapter *adap) {}
511 #endif
513 #endif /* _LINUX_I2C_H */