gpu: ion: add support for more cache operations
[android-sdk/kernel-video.git] / include / linux / ion.h
1 /*
2  * include/linux/ion.h
3  *
4  * Copyright (C) 2011 Google, Inc.
5  *
6  * This software is licensed under the terms of the GNU General Public
7  * License version 2, as published by the Free Software Foundation, and
8  * may be copied, distributed, and modified under those terms.
9  *
10  * This program is distributed in the hope that it will be useful,
11  * but WITHOUT ANY WARRANTY; without even the implied warranty of
12  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
13  * GNU General Public License for more details.
14  *
15  */
17 #ifndef _LINUX_ION_H
18 #define _LINUX_ION_H
20 #include <linux/types.h>
22 struct ion_handle;
23 /**
24  * enum ion_heap_types - list of all possible types of heaps
25  * @ION_HEAP_TYPE_SYSTEM:        memory allocated via vmalloc
26  * @ION_HEAP_TYPE_SYSTEM_CONTIG: memory allocated via kmalloc
27  * @ION_HEAP_TYPE_CARVEOUT:      memory allocated from a prereserved
28  *                               carveout heap, allocations are physically
29  *                               contiguous
30  * @ION_NUM_HEAPS:               helper for iterating over heaps, a bit mask
31  *                               is used to identify the heaps, so only 32
32  *                               total heap types are supported
33  */
34 enum ion_heap_type {
35         ION_HEAP_TYPE_SYSTEM,
36         ION_HEAP_TYPE_SYSTEM_CONTIG,
37         ION_HEAP_TYPE_CARVEOUT,
38         ION_HEAP_TYPE_CHUNK,
39         ION_HEAP_TYPE_CUSTOM, /* must be last so device specific heaps always
40                                  are at the end of this enum */
41         ION_NUM_HEAPS = 16,
42 };
44 /**
45  * enum ion_data_direction - sync operation arguments
46  * @ION_BIDIRECTIONAL:   memory written to & read from device
47  * @ION_TO_DEVICE: memory going to be transferred to device
48  * @ION_FROM_DEVICE:     memory populated by device
49  * @ION_NONE:            None of the above
50  */
51 enum ion_data_direction {
52         ION_BIDIRECTIONAL = 0,
53         ION_TO_DEVICE = 1,
54         ION_FROM_DEVICE = 2,
55         ION_NONE = 3,
56 };
59 #define ION_HEAP_SYSTEM_MASK            (1 << ION_HEAP_TYPE_SYSTEM)
60 #define ION_HEAP_SYSTEM_CONTIG_MASK     (1 << ION_HEAP_TYPE_SYSTEM_CONTIG)
61 #define ION_HEAP_CARVEOUT_MASK          (1 << ION_HEAP_TYPE_CARVEOUT)
63 #define ION_NUM_HEAP_IDS                sizeof(unsigned int) * 8
65 /**
66  * heap flags - the lower 16 bits are used by core ion, the upper 16
67  * bits are reserved for use by the heaps themselves.
68  */
69 #define ION_FLAG_CACHED 1               /* mappings of this buffer should be
70                                            cached, ion will do cache
71                                            maintenance when the buffer is
72                                            mapped for dma */
73 #define ION_FLAG_CACHED_NEEDS_SYNC 2    /* mappings of this buffer will created
74                                            at mmap time, if this is set
75                                            caches must be managed manually */
77 #ifdef __KERNEL__
78 struct ion_device;
79 struct ion_heap;
80 struct ion_mapper;
81 struct ion_client;
82 struct ion_buffer;
84 /* This should be removed some day when phys_addr_t's are fully
85    plumbed in the kernel, and all instances of ion_phys_addr_t should
86    be converted to phys_addr_t.  For the time being many kernel interfaces
87    do not accept phys_addr_t's that would have to */
88 #define ion_phys_addr_t unsigned long
90 /**
91  * struct ion_platform_heap - defines a heap in the given platform
92  * @type:       type of the heap from ion_heap_type enum
93  * @id:         unique identifier for heap.  When allocating higher numbers
94  *              will be allocated from first.  At allocation these are passed
95  *              as a bit mask and therefore can not exceed ION_NUM_HEAP_IDS.
96  * @name:       used for debug purposes
97  * @base:       base address of heap in physical memory if applicable
98  * @size:       size of the heap in bytes if applicable
99  * @align:      required alignment in physical memory if applicable
100  * @priv:       private info passed from the board file
101  *
102  * Provided by the board file.
103  */
104 struct ion_platform_heap {
105         enum ion_heap_type type;
106         unsigned int id;
107         const char *name;
108         ion_phys_addr_t base;
109         size_t size;
110         ion_phys_addr_t align;
111         void *priv;
112 };
114 /**
115  * struct ion_platform_data - array of platform heaps passed from board file
116  * @nr:         number of structures in the array
117  * @heaps:      array of platform_heap structions
118  *
119  * Provided by the board file in the form of platform data to a platform device.
120  */
121 struct ion_platform_data {
122         int nr;
123         struct ion_platform_heap heaps[];
124 };
126 /**
127  * ion_reserve() - reserve memory for ion heaps if applicable
128  * @data:       platform data specifying starting physical address and
129  *              size
130  *
131  * Calls memblock reserve to set aside memory for heaps that are
132  * located at specific memory addresses or of specfic sizes not
133  * managed by the kernel
134  */
135 void ion_reserve(struct ion_platform_data *data);
137 /**
138  * ion_client_create() -  allocate a client and returns it
139  * @dev:                the global ion device
140  * @heap_type_mask:     mask of heaps this client can allocate from
141  * @name:               used for debugging
142  */
143 struct ion_client *ion_client_create(struct ion_device *dev,
144                                      const char *name);
146 /**
147  * ion_client_destroy() -  free's a client and all it's handles
148  * @client:     the client
149  *
150  * Free the provided client and all it's resources including
151  * any handles it is holding.
152  */
153 void ion_client_destroy(struct ion_client *client);
155 /**
156  * ion_alloc - allocate ion memory
157  * @client:             the client
158  * @len:                size of the allocation
159  * @align:              requested allocation alignment, lots of hardware blocks
160  *                      have alignment requirements of some kind
161  * @heap_id_mask:       mask of heaps to allocate from, if multiple bits are set
162  *                      heaps will be tried in order from highest to lowest
163  *                      id
164  * @flags:              heap flags, the low 16 bits are consumed by ion, the
165  *                      high 16 bits are passed on to the respective heap and
166  *                      can be heap custom
167  *
168  * Allocate memory in one of the heaps provided in heap mask and return
169  * an opaque handle to it.
170  */
171 struct ion_handle *ion_alloc(struct ion_client *client, size_t len,
172                              size_t align, unsigned int heap_id_mask,
173                              unsigned int flags);
175 /**
176  * ion_free - free a handle
177  * @client:     the client
178  * @handle:     the handle to free
179  *
180  * Free the provided handle.
181  */
182 void ion_free(struct ion_client *client, struct ion_handle *handle);
184 /**
185  * ion_phys - returns the physical address and len of a handle
186  * @client:     the client
187  * @handle:     the handle
188  * @addr:       a pointer to put the address in
189  * @len:        a pointer to put the length in
190  *
191  * This function queries the heap for a particular handle to get the
192  * handle's physical address.  It't output is only correct if
193  * a heap returns physically contiguous memory -- in other cases
194  * this api should not be implemented -- ion_sg_table should be used
195  * instead.  Returns -EINVAL if the handle is invalid.  This has
196  * no implications on the reference counting of the handle --
197  * the returned value may not be valid if the caller is not
198  * holding a reference.
199  */
200 int ion_phys(struct ion_client *client, struct ion_handle *handle,
201              ion_phys_addr_t *addr, size_t *len);
203 /**
204  * ion_map_dma - return an sg_table describing a handle
205  * @client:     the client
206  * @handle:     the handle
207  *
208  * This function returns the sg_table describing
209  * a particular ion handle.
210  */
211 struct sg_table *ion_sg_table(struct ion_client *client,
212                               struct ion_handle *handle);
214 /**
215  * ion_map_kernel - create mapping for the given handle
216  * @client:     the client
217  * @handle:     handle to map
218  *
219  * Map the given handle into the kernel and return a kernel address that
220  * can be used to access this address.
221  */
222 void *ion_map_kernel(struct ion_client *client, struct ion_handle *handle);
224 /**
225  * ion_unmap_kernel() - destroy a kernel mapping for a handle
226  * @client:     the client
227  * @handle:     handle to unmap
228  */
229 void ion_unmap_kernel(struct ion_client *client, struct ion_handle *handle);
231 /**
232  * ion_share_dma_buf() - given an ion client, create a dma-buf fd
233  * @client:     the client
234  * @handle:     the handle
235  */
236 int ion_share_dma_buf(struct ion_client *client, struct ion_handle *handle);
238 /**
239  * ion_import_dma_buf() - given an dma-buf fd from the ion exporter get handle
240  * @client:     the client
241  * @fd:         the dma-buf fd
242  *
243  * Given an dma-buf fd that was allocated through ion via ion_share_dma_buf,
244  * import that fd and return a handle representing it.  If a dma-buf from
245  * another exporter is passed in this function will return ERR_PTR(-EINVAL)
246  */
247 struct ion_handle *ion_import_dma_buf(struct ion_client *client, int fd);
249 #endif /* __KERNEL__ */
251 /**
252  * DOC: Ion Userspace API
253  *
254  * create a client by opening /dev/ion
255  * most operations handled via following ioctls
256  *
257  */
259 /**
260  * struct ion_allocation_data - metadata passed from userspace for allocations
261  * @len:                size of the allocation
262  * @align:              required alignment of the allocation
263  * @heap_id_mask:       mask of heap ids to allocate from
264  * @flags:              flags passed to heap
265  * @handle:             pointer that will be populated with a cookie to use to 
266  *                      refer to this allocation
267  *
268  * Provided by userspace as an argument to the ioctl
269  */
270 struct ion_allocation_data {
271         size_t len;
272         size_t align;
273         unsigned int heap_id_mask;
274         unsigned int flags;
275         struct ion_handle *handle;
276 };
278 /**
279  * struct ion_fd_data - metadata passed to/from userspace for a handle/fd pair
280  * @handle:     a handle
281  * @fd:         a file descriptor representing that handle
282  *
283  * For ION_IOC_SHARE or ION_IOC_MAP userspace populates the handle field with
284  * the handle returned from ion alloc, and the kernel returns the file
285  * descriptor to share or map in the fd field.  For ION_IOC_IMPORT, userspace
286  * provides the file descriptor and the kernel returns the handle.
287  */
288 struct ion_fd_data {
289         struct ion_handle *handle;
290         int fd;
291         enum ion_data_direction dir;
292 };
294 /**
295  * struct ion_handle_data - a handle passed to/from the kernel
296  * @handle:     a handle
297  */
298 struct ion_handle_data {
299         struct ion_handle *handle;
300 };
302 /**
303  * struct ion_custom_data - metadata passed to/from userspace for a custom ioctl
304  * @cmd:        the custom ioctl function to call
305  * @arg:        additional data to pass to the custom ioctl, typically a user
306  *              pointer to a predefined structure
307  *
308  * This works just like the regular cmd and arg fields of an ioctl.
309  */
310 struct ion_custom_data {
311         unsigned int cmd;
312         unsigned long arg;
313 };
315 #define ION_IOC_MAGIC           'I'
317 /**
318  * DOC: ION_IOC_ALLOC - allocate memory
319  *
320  * Takes an ion_allocation_data struct and returns it with the handle field
321  * populated with the opaque handle for the allocation.
322  */
323 #define ION_IOC_ALLOC           _IOWR(ION_IOC_MAGIC, 0, \
324                                       struct ion_allocation_data)
326 /**
327  * DOC: ION_IOC_FREE - free memory
328  *
329  * Takes an ion_handle_data struct and frees the handle.
330  */
331 #define ION_IOC_FREE            _IOWR(ION_IOC_MAGIC, 1, struct ion_handle_data)
333 /**
334  * DOC: ION_IOC_MAP - get a file descriptor to mmap
335  *
336  * Takes an ion_fd_data struct with the handle field populated with a valid
337  * opaque handle.  Returns the struct with the fd field set to a file
338  * descriptor open in the current address space.  This file descriptor
339  * can then be used as an argument to mmap.
340  */
341 #define ION_IOC_MAP             _IOWR(ION_IOC_MAGIC, 2, struct ion_fd_data)
343 /**
344  * DOC: ION_IOC_SHARE - creates a file descriptor to use to share an allocation
345  *
346  * Takes an ion_fd_data struct with the handle field populated with a valid
347  * opaque handle.  Returns the struct with the fd field set to a file
348  * descriptor open in the current address space.  This file descriptor
349  * can then be passed to another process.  The corresponding opaque handle can
350  * be retrieved via ION_IOC_IMPORT.
351  */
352 #define ION_IOC_SHARE           _IOWR(ION_IOC_MAGIC, 4, struct ion_fd_data)
354 /**
355  * DOC: ION_IOC_IMPORT - imports a shared file descriptor
356  *
357  * Takes an ion_fd_data struct with the fd field populated with a valid file
358  * descriptor obtained from ION_IOC_SHARE and returns the struct with the handle
359  * filed set to the corresponding opaque handle.
360  */
361 #define ION_IOC_IMPORT          _IOWR(ION_IOC_MAGIC, 5, struct ion_fd_data)
363 /**
364  * DOC: ION_IOC_SYNC - syncs a shared file descriptors to memory
365  *
366  * Deprecated in favor of using the dma_buf api's correctly (syncing
367  * will happend automatically when the buffer is mapped to a device).
368  * If necessary should be used after touching a cached buffer from the cpu,
369  * this will make the buffer in memory coherent.
370  */
371 #define ION_IOC_SYNC            _IOWR(ION_IOC_MAGIC, 7, struct ion_fd_data)
373 /**
374  * DOC: ION_IOC_CUSTOM - call architecture specific ion ioctl
375  *
376  * Takes the argument of the architecture specific ioctl to call and
377  * passes appropriate userdata for that ioctl
378  */
379 #define ION_IOC_CUSTOM          _IOWR(ION_IOC_MAGIC, 6, struct ion_custom_data)
381 #endif /* _LINUX_ION_H */