]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/blob - include/linux/ion.h
gpu: ion: Add ION Memory Manager
[android-sdk/kernel-video.git] / include / linux / ion.h
1 /*
2  * include/linux/ion.h
3  *
4  * Copyright (C) 2011 Google, Inc.
5  *
6  * This software is licensed under the terms of the GNU General Public
7  * License version 2, as published by the Free Software Foundation, and
8  * may be copied, distributed, and modified under those terms.
9  *
10  * This program is distributed in the hope that it will be useful,
11  * but WITHOUT ANY WARRANTY; without even the implied warranty of
12  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
13  * GNU General Public License for more details.
14  *
15  */
17 #ifndef _LINUX_ION_H
18 #define _LINUX_ION_H
20 #include <linux/types.h>
22 struct ion_handle;
23 /**
24  * enum ion_heap_types - list of all possible types of heaps
25  * @ION_HEAP_TYPE_SYSTEM:        memory allocated via vmalloc
26  * @ION_HEAP_TYPE_SYSTEM_CONTIG: memory allocated via kmalloc
27  * @ION_HEAP_TYPE_CARVEOUT:      memory allocated from a prereserved
28  *                               carveout heap, allocations are physically
29  *                               contiguous
30  * @ION_HEAP_END:                helper for iterating over heaps
31  */
32 enum ion_heap_type {
33         ION_HEAP_TYPE_SYSTEM,
34         ION_HEAP_TYPE_SYSTEM_CONTIG,
35         ION_HEAP_TYPE_CARVEOUT,
36         ION_HEAP_TYPE_CUSTOM, /* must be last so device specific heaps always
37                                  are at the end of this enum */
38         ION_NUM_HEAPS,
39 };
41 #define ION_HEAP_SYSTEM_MASK            (1 << ION_HEAP_TYPE_SYSTEM)
42 #define ION_HEAP_SYSTEM_CONTIG_MASK     (1 << ION_HEAP_TYPE_SYSTEM_CONTIG)
43 #define ION_HEAP_CARVEOUT_MASK          (1 << ION_HEAP_TYPE_CARVEOUT)
45 #ifdef __KERNEL__
46 struct ion_device;
47 struct ion_heap;
48 struct ion_mapper;
49 struct ion_client;
50 struct ion_buffer;
52 /* This should be removed some day when phys_addr_t's are fully
53    plumbed in the kernel, and all instances of ion_phys_addr_t should
54    be converted to phys_addr_t.  For the time being many kernel interfaces
55    do not accept phys_addr_t's that would have to */
56 #define ion_phys_addr_t unsigned long
58 /**
59  * struct ion_platform_heap - defines a heap in the given platform
60  * @type:       type of the heap from ion_heap_type enum
61  * @id:         unique identifier for heap.  When allocating (lower numbers 
62  *              will be allocated from first)
63  * @name:       used for debug purposes
64  * @base:       base address of heap in physical memory if applicable
65  * @size:       size of the heap in bytes if applicable
66  *
67  * Provided by the board file.
68  */
69 struct ion_platform_heap {
70         enum ion_heap_type type;
71         unsigned int id;
72         const char *name;
73         ion_phys_addr_t base;
74         size_t size;
75 };
77 /**
78  * struct ion_platform_data - array of platform heaps passed from board file
79  * @nr:         number of structures in the array
80  * @heaps:      array of platform_heap structions
81  *
82  * Provided by the board file in the form of platform data to a platform device.
83  */
84 struct ion_platform_data {
85         int nr;
86         struct ion_platform_heap heaps[];
87 };
89 /**
90  * ion_client_create() -  allocate a client and returns it
91  * @dev:        the global ion device
92  * @heap_mask:  mask of heaps this client can allocate from
93  * @name:       used for debugging
94  */
95 struct ion_client *ion_client_create(struct ion_device *dev,
96                                      unsigned int heap_mask, const char *name);
98 /**
99  * ion_client_destroy() -  free's a client and all it's handles
100  * @client:     the client
101  *
102  * Free the provided client and all it's resources including
103  * any handles it is holding.
104  */
105 void ion_client_destroy(struct ion_client *client);
107 /**
108  * ion_alloc - allocate ion memory
109  * @client:     the client
110  * @len:        size of the allocation
111  * @align:      requested allocation alignment, lots of hardware blocks have
112  *              alignment requirements of some kind
113  * @flags:      mask of heaps to allocate from, if multiple bits are set
114  *              heaps will be tried in order from lowest to highest order bit
115  *
116  * Allocate memory in one of the heaps provided in heap mask and return
117  * an opaque handle to it.
118  */
119 struct ion_handle *ion_alloc(struct ion_client *client, size_t len,
120                              size_t align, unsigned int flags);
122 /**
123  * ion_free - free a handle
124  * @client:     the client
125  * @handle:     the handle to free
126  *
127  * Free the provided handle.
128  */
129 void ion_free(struct ion_client *client, struct ion_handle *handle);
131 /**
132  * ion_phys - returns the physical address and len of a handle
133  * @client:     the client
134  * @handle:     the handle
135  * @addr:       a pointer to put the address in
136  * @len:        a pointer to put the length in
137  *
138  * This function queries the heap for a particular handle to get the
139  * handle's physical address.  It't output is only correct if
140  * a heap returns physically contiguous memory -- in other cases
141  * this api should not be implemented -- ion_map_dma should be used
142  * instead.  Returns -EINVAL if the handle is invalid.  This has
143  * no implications on the reference counting of the handle --
144  * the returned value may not be valid if the caller is not
145  * holding a reference.
146  */
147 int ion_phys(struct ion_client *client, struct ion_handle *handle,
148              ion_phys_addr_t *addr, size_t *len);
150 /**
151  * ion_map_kernel - create mapping for the given handle
152  * @client:     the client
153  * @handle:     handle to map
154  *
155  * Map the given handle into the kernel and return a kernel address that
156  * can be used to access this address.
157  */
158 void *ion_map_kernel(struct ion_client *client, struct ion_handle *handle);
160 /**
161  * ion_unmap_kernel() - destroy a kernel mapping for a handle
162  * @client:     the client
163  * @handle:     handle to unmap
164  */
165 void ion_unmap_kernel(struct ion_client *client, struct ion_handle *handle);
167 /**
168  * ion_map_dma - create a dma mapping for a given handle
169  * @client:     the client
170  * @handle:     handle to map
171  *
172  * Return an sglist describing the given handle
173  */
174 struct scatterlist *ion_map_dma(struct ion_client *client,
175                                 struct ion_handle *handle);
177 /**
178  * ion_unmap_dma() - destroy a dma mapping for a handle
179  * @client:     the client
180  * @handle:     handle to unmap
181  */
182 void ion_unmap_dma(struct ion_client *client, struct ion_handle *handle);
184 /**
185  * ion_share() - given a handle, obtain a buffer to pass to other clients
186  * @client:     the client
187  * @handle:     the handle to share
188  *
189  * Given a handle, return a buffer, which exists in a global name
190  * space, and can be passed to other clients.  Should be passed into ion_import
191  * to obtain a new handle for this buffer.
192  *
193  * NOTE: This function does do not an extra reference.  The burden is on the
194  * caller to make sure the buffer doesn't go away while it's being passed to
195  * another client.  That is, ion_free should not be called on this handle until
196  * the buffer has been imported into the other client.
197  */
198 struct ion_buffer *ion_share(struct ion_client *client,
199                              struct ion_handle *handle);
201 /**
202  * ion_import() - given an buffer in another client, import it
203  * @client:     this blocks client
204  * @buffer:     the buffer to import (as obtained from ion_share)
205  *
206  * Given a buffer, add it to the client and return the handle to use to refer
207  * to it further.  This is called to share a handle from one kernel client to
208  * another.
209  */
210 struct ion_handle *ion_import(struct ion_client *client,
211                               struct ion_buffer *buffer);
213 /**
214  * ion_import_fd() - given an fd obtained via ION_IOC_SHARE ioctl, import it
215  * @client:     this blocks client
216  * @fd:         the fd
217  *
218  * A helper function for drivers that will be recieving ion buffers shared
219  * with them from userspace.  These buffers are represented by a file
220  * descriptor obtained as the return from the ION_IOC_SHARE ioctl.
221  * This function coverts that fd into the underlying buffer, and returns
222  * the handle to use to refer to it further.
223  */
224 struct ion_handle *ion_import_fd(struct ion_client *client, int fd);
225 #endif /* __KERNEL__ */
227 /**
228  * DOC: Ion Userspace API
229  *
230  * create a client by opening /dev/ion
231  * most operations handled via following ioctls
232  *
233  */
235 /**
236  * struct ion_allocation_data - metadata passed from userspace for allocations
237  * @len:        size of the allocation
238  * @align:      required alignment of the allocation
239  * @flags:      flags passed to heap
240  * @handle:     pointer that will be populated with a cookie to use to refer
241  *              to this allocation
242  *
243  * Provided by userspace as an argument to the ioctl
244  */
245 struct ion_allocation_data {
246         size_t len;
247         size_t align;
248         unsigned int flags;
249         struct ion_handle *handle;
250 };
252 /**
253  * struct ion_fd_data - metadata passed to/from userspace for a handle/fd pair
254  * @handle:     a handle
255  * @fd:         a file descriptor representing that handle
256  *
257  * For ION_IOC_SHARE or ION_IOC_MAP userspace populates the handle field with
258  * the handle returned from ion alloc, and the kernel returns the file
259  * descriptor to share or map in the fd field.  For ION_IOC_IMPORT, userspace
260  * provides the file descriptor and the kernel returns the handle.
261  */
262 struct ion_fd_data {
263         struct ion_handle *handle;
264         int fd;
265 };
267 /**
268  * struct ion_handle_data - a handle passed to/from the kernel
269  * @handle:     a handle
270  */
271 struct ion_handle_data {
272         struct ion_handle *handle;
273 };
275 /**
276  * struct ion_custom_data - metadata passed to/from userspace for a custom ioctl
277  * @cmd:        the custom ioctl function to call
278  * @arg:        additional data to pass to the custom ioctl, typically a user
279  *              pointer to a predefined structure
280  *
281  * This works just like the regular cmd and arg fields of an ioctl.
282  */
283 struct ion_custom_data {
284         unsigned int cmd;
285         unsigned long arg;
286 };
288 #define ION_IOC_MAGIC           'I'
290 /**
291  * DOC: ION_IOC_ALLOC - allocate memory
292  *
293  * Takes an ion_allocation_data struct and returns it with the handle field
294  * populated with the opaque handle for the allocation.
295  */
296 #define ION_IOC_ALLOC           _IOWR(ION_IOC_MAGIC, 0, \
297                                       struct ion_allocation_data)
299 /**
300  * DOC: ION_IOC_FREE - free memory
301  *
302  * Takes an ion_handle_data struct and frees the handle.
303  */
304 #define ION_IOC_FREE            _IOWR(ION_IOC_MAGIC, 1, struct ion_handle_data)
306 /**
307  * DOC: ION_IOC_MAP - get a file descriptor to mmap
308  *
309  * Takes an ion_fd_data struct with the handle field populated with a valid
310  * opaque handle.  Returns the struct with the fd field set to a file
311  * descriptor open in the current address space.  This file descriptor
312  * can then be used as an argument to mmap.
313  */
314 #define ION_IOC_MAP             _IOWR(ION_IOC_MAGIC, 2, struct ion_fd_data)
316 /**
317  * DOC: ION_IOC_SHARE - creates a file descriptor to use to share an allocation
318  *
319  * Takes an ion_fd_data struct with the handle field populated with a valid
320  * opaque handle.  Returns the struct with the fd field set to a file
321  * descriptor open in the current address space.  This file descriptor
322  * can then be passed to another process.  The corresponding opaque handle can
323  * be retrieved via ION_IOC_IMPORT.
324  */
325 #define ION_IOC_SHARE           _IOWR(ION_IOC_MAGIC, 4, struct ion_fd_data)
327 /**
328  * DOC: ION_IOC_IMPORT - imports a shared file descriptor
329  *
330  * Takes an ion_fd_data struct with the fd field populated with a valid file
331  * descriptor obtained from ION_IOC_SHARE and returns the struct with the handle
332  * filed set to the corresponding opaque handle.
333  */
334 #define ION_IOC_IMPORT          _IOWR(ION_IOC_MAGIC, 5, int)
336 /**
337  * DOC: ION_IOC_CUSTOM - call architecture specific ion ioctl
338  *
339  * Takes the argument of the architecture specific ioctl to call and
340  * passes appropriate userdata for that ioctl
341  */
342 #define ION_IOC_CUSTOM          _IOWR(ION_IOC_MAGIC, 6, struct ion_custom_data)
344 #endif /* _LINUX_ION_H */