1 #ifndef _LINUX_MM_TYPES_H
2 #define _LINUX_MM_TYPES_H
4 #include <linux/auxvec.h>
5 #include <linux/types.h>
6 #include <linux/threads.h>
7 #include <linux/list.h>
8 #include <linux/spinlock.h>
9 #include <linux/rbtree.h>
10 #include <linux/rwsem.h>
11 #include <linux/completion.h>
12 #include <linux/cpumask.h>
13 #include <linux/page-debug-flags.h>
14 #include <linux/uprobes.h>
15 #include <linux/page-flags-layout.h>
16 #include <asm/page.h>
17 #include <asm/mmu.h>
19 #ifndef AT_VECTOR_SIZE_ARCH
20 #define AT_VECTOR_SIZE_ARCH 0
21 #endif
22 #define AT_VECTOR_SIZE (2*(AT_VECTOR_SIZE_ARCH + AT_VECTOR_SIZE_BASE + 1))
24 struct address_space;
26 #define USE_SPLIT_PTE_PTLOCKS (NR_CPUS >= CONFIG_SPLIT_PTLOCK_CPUS)
27 #define USE_SPLIT_PMD_PTLOCKS (USE_SPLIT_PTE_PTLOCKS && \
28 IS_ENABLED(CONFIG_ARCH_ENABLE_SPLIT_PMD_PTLOCK))
29 #define ALLOC_SPLIT_PTLOCKS (SPINLOCK_SIZE > BITS_PER_LONG/8)
31 /*
32 * Each physical page in the system has a struct page associated with
33 * it to keep track of whatever it is we are using the page for at the
34 * moment. Note that we have no way to track which tasks are using
35 * a page, though if it is a pagecache page, rmap structures can tell us
36 * who is mapping it.
37 *
38 * The objects in struct page are organized in double word blocks in
39 * order to allows us to use atomic double word operations on portions
40 * of struct page. That is currently only used by slub but the arrangement
41 * allows the use of atomic double word operations on the flags/mapping
42 * and lru list pointers also.
43 */
44 struct page {
45 /* First double word block */
46 unsigned long flags; /* Atomic flags, some possibly
47 * updated asynchronously */
48 union {
49 struct address_space *mapping; /* If low bit clear, points to
50 * inode address_space, or NULL.
51 * If page mapped as anonymous
52 * memory, low bit is set, and
53 * it points to anon_vma object:
54 * see PAGE_MAPPING_ANON below.
55 */
56 void *s_mem; /* slab first object */
57 };
59 /* Second double word */
60 struct {
61 union {
62 pgoff_t index; /* Our offset within mapping. */
63 void *freelist; /* sl[aou]b first free object */
64 bool pfmemalloc; /* If set by the page allocator,
65 * ALLOC_NO_WATERMARKS was set
66 * and the low watermark was not
67 * met implying that the system
68 * is under some pressure. The
69 * caller should try ensure
70 * this page is only used to
71 * free other pages.
72 */
73 };
75 union {
76 #if defined(CONFIG_HAVE_CMPXCHG_DOUBLE) && \
77 defined(CONFIG_HAVE_ALIGNED_STRUCT_PAGE)
78 /* Used for cmpxchg_double in slub */
79 unsigned long counters;
80 #else
81 /*
82 * Keep _count separate from slub cmpxchg_double data.
83 * As the rest of the double word is protected by
84 * slab_lock but _count is not.
85 */
86 unsigned counters;
87 #endif
89 struct {
91 union {
92 /*
93 * Count of ptes mapped in
94 * mms, to show when page is
95 * mapped & limit reverse map
96 * searches.
97 *
98 * Used also for tail pages
99 * refcounting instead of
100 * _count. Tail pages cannot
101 * be mapped and keeping the
102 * tail page _count zero at
103 * all times guarantees
104 * get_page_unless_zero() will
105 * never succeed on tail
106 * pages.
107 */
108 atomic_t _mapcount;
110 struct { /* SLUB */
111 unsigned inuse:16;
112 unsigned objects:15;
113 unsigned frozen:1;
114 };
115 int units; /* SLOB */
116 };
117 atomic_t _count; /* Usage count, see below. */
118 };
119 unsigned int active; /* SLAB */
120 };
121 };
123 /* Third double word block */
124 union {
125 struct list_head lru; /* Pageout list, eg. active_list
126 * protected by zone->lru_lock !
127 */
128 struct { /* slub per cpu partial pages */
129 struct page *next; /* Next partial slab */
130 #ifdef CONFIG_64BIT
131 int pages; /* Nr of partial slabs left */
132 int pobjects; /* Approximate # of objects */
133 #else
134 short int pages;
135 short int pobjects;
136 #endif
137 };
139 struct list_head list; /* slobs list of pages */
140 struct slab *slab_page; /* slab fields */
141 struct rcu_head rcu_head; /* Used by SLAB
142 * when destroying via RCU
143 */
144 #if defined(CONFIG_TRANSPARENT_HUGEPAGE) && USE_SPLIT_PMD_PTLOCKS
145 pgtable_t pmd_huge_pte; /* protected by page->ptl */
146 #endif
147 };
149 /* Remainder is not double word aligned */
150 union {
151 unsigned long private; /* Mapping-private opaque data:
152 * usually used for buffer_heads
153 * if PagePrivate set; used for
154 * swp_entry_t if PageSwapCache;
155 * indicates order in the buddy
156 * system if PG_buddy is set.
157 */
158 #if USE_SPLIT_PTE_PTLOCKS
159 #if ALLOC_SPLIT_PTLOCKS
160 spinlock_t *ptl;
161 #else
162 spinlock_t ptl;
163 #endif
164 #endif
165 struct kmem_cache *slab_cache; /* SL[AU]B: Pointer to slab */
166 struct page *first_page; /* Compound tail pages */
167 };
169 /*
170 * On machines where all RAM is mapped into kernel address space,
171 * we can simply calculate the virtual address. On machines with
172 * highmem some memory is mapped into kernel virtual memory
173 * dynamically, so we need a place to store that address.
174 * Note that this field could be 16 bits on x86 ... ;)
175 *
176 * Architectures with slow multiplication can define
177 * WANT_PAGE_VIRTUAL in asm/page.h
178 */
179 #if defined(WANT_PAGE_VIRTUAL)
180 void *virtual; /* Kernel virtual address (NULL if
181 not kmapped, ie. highmem) */
182 #endif /* WANT_PAGE_VIRTUAL */
183 #ifdef CONFIG_WANT_PAGE_DEBUG_FLAGS
184 unsigned long debug_flags; /* Use atomic bitops on this */
185 #endif
187 #ifdef CONFIG_KMEMCHECK
188 /*
189 * kmemcheck wants to track the status of each byte in a page; this
190 * is a pointer to such a status block. NULL if not tracked.
191 */
192 void *shadow;
193 #endif
195 #ifdef LAST_CPUPID_NOT_IN_PAGE_FLAGS
196 int _last_cpupid;
197 #endif
198 }
199 /*
200 * The struct page can be forced to be double word aligned so that atomic ops
201 * on double words work. The SLUB allocator can make use of such a feature.
202 */
203 #ifdef CONFIG_HAVE_ALIGNED_STRUCT_PAGE
204 __aligned(2 * sizeof(unsigned long))
205 #endif
206 ;
208 struct page_frag {
209 struct page *page;
210 #if (BITS_PER_LONG > 32) || (PAGE_SIZE >= 65536)
211 __u32 offset;
212 __u32 size;
213 #else
214 __u16 offset;
215 __u16 size;
216 #endif
217 };
219 typedef unsigned long __nocast vm_flags_t;
221 /*
222 * A region containing a mapping of a non-memory backed file under NOMMU
223 * conditions. These are held in a global tree and are pinned by the VMAs that
224 * map parts of them.
225 */
226 struct vm_region {
227 struct rb_node vm_rb; /* link in global region tree */
228 vm_flags_t vm_flags; /* VMA vm_flags */
229 unsigned long vm_start; /* start address of region */
230 unsigned long vm_end; /* region initialised to here */
231 unsigned long vm_top; /* region allocated to here */
232 unsigned long vm_pgoff; /* the offset in vm_file corresponding to vm_start */
233 struct file *vm_file; /* the backing file or NULL */
235 int vm_usage; /* region usage count (access under nommu_region_sem) */
236 bool vm_icache_flushed : 1; /* true if the icache has been flushed for
237 * this region */
238 };
240 /*
241 * This struct defines a memory VMM memory area. There is one of these
242 * per VM-area/task. A VM area is any part of the process virtual memory
243 * space that has a special rule for the page-fault handlers (ie a shared
244 * library, the executable area etc).
245 */
246 struct vm_area_struct {
247 /* The first cache line has the info for VMA tree walking. */
249 unsigned long vm_start; /* Our start address within vm_mm. */
250 unsigned long vm_end; /* The first byte after our end address
251 within vm_mm. */
253 /* linked list of VM areas per task, sorted by address */
254 struct vm_area_struct *vm_next, *vm_prev;
256 struct rb_node vm_rb;
258 /*
259 * Largest free memory gap in bytes to the left of this VMA.
260 * Either between this VMA and vma->vm_prev, or between one of the
261 * VMAs below us in the VMA rbtree and its ->vm_prev. This helps
262 * get_unmapped_area find a free area of the right size.
263 */
264 unsigned long rb_subtree_gap;
266 /* Second cache line starts here. */
268 struct mm_struct *vm_mm; /* The address space we belong to. */
269 pgprot_t vm_page_prot; /* Access permissions of this VMA. */
270 unsigned long vm_flags; /* Flags, see mm.h. */
272 /*
273 * For areas with an address space and backing store,
274 * linkage into the address_space->i_mmap interval tree, or
275 * linkage of vma in the address_space->i_mmap_nonlinear list.
276 *
277 * For private anonymous mappings, a pointer to a null terminated string
278 * in the user process containing the name given to the vma, or NULL
279 * if unnamed.
280 */
281 union {
282 struct {
283 struct rb_node rb;
284 unsigned long rb_subtree_last;
285 } linear;
286 struct list_head nonlinear;
287 const char __user *anon_name;
288 } shared;
290 /*
291 * A file's MAP_PRIVATE vma can be in both i_mmap tree and anon_vma
292 * list, after a COW of one of the file pages. A MAP_SHARED vma
293 * can only be in the i_mmap tree. An anonymous MAP_PRIVATE, stack
294 * or brk vma (with NULL file) can only be in an anon_vma list.
295 */
296 struct list_head anon_vma_chain; /* Serialized by mmap_sem &
297 * page_table_lock */
298 struct anon_vma *anon_vma; /* Serialized by page_table_lock */
300 /* Function pointers to deal with this struct. */
301 const struct vm_operations_struct *vm_ops;
303 /* Information about our backing store: */
304 unsigned long vm_pgoff; /* Offset (within vm_file) in PAGE_SIZE
305 units, *not* PAGE_CACHE_SIZE */
306 struct file * vm_file; /* File we map to (can be NULL). */
307 void * vm_private_data; /* was vm_pte (shared mem) */
309 #ifndef CONFIG_MMU
310 struct vm_region *vm_region; /* NOMMU mapping region */
311 #endif
312 #ifdef CONFIG_NUMA
313 struct mempolicy *vm_policy; /* NUMA policy for the VMA */
314 #endif
315 };
317 struct core_thread {
318 struct task_struct *task;
319 struct core_thread *next;
320 };
322 struct core_state {
323 atomic_t nr_threads;
324 struct core_thread dumper;
325 struct completion startup;
326 };
328 enum {
329 MM_FILEPAGES,
330 MM_ANONPAGES,
331 MM_SWAPENTS,
332 NR_MM_COUNTERS
333 };
335 #if USE_SPLIT_PTE_PTLOCKS && defined(CONFIG_MMU)
336 #define SPLIT_RSS_COUNTING
337 /* per-thread cached information, */
338 struct task_rss_stat {
339 int events; /* for synchronization threshold */
340 int count[NR_MM_COUNTERS];
341 };
342 #endif /* USE_SPLIT_PTE_PTLOCKS */
344 struct mm_rss_stat {
345 atomic_long_t count[NR_MM_COUNTERS];
346 };
348 struct kioctx_table;
349 struct mm_struct {
350 struct vm_area_struct *mmap; /* list of VMAs */
351 struct rb_root mm_rb;
352 u32 vmacache_seqnum; /* per-thread vmacache */
353 #ifdef CONFIG_MMU
354 unsigned long (*get_unmapped_area) (struct file *filp,
355 unsigned long addr, unsigned long len,
356 unsigned long pgoff, unsigned long flags);
357 #endif
358 unsigned long mmap_base; /* base of mmap area */
359 unsigned long mmap_legacy_base; /* base of mmap area in bottom-up allocations */
360 unsigned long task_size; /* size of task vm space */
361 unsigned long highest_vm_end; /* highest vma end address */
362 pgd_t * pgd;
363 atomic_t mm_users; /* How many users with user space? */
364 atomic_t mm_count; /* How many references to "struct mm_struct" (users count as 1) */
365 atomic_long_t nr_ptes; /* Page table pages */
366 int map_count; /* number of VMAs */
368 spinlock_t page_table_lock; /* Protects page tables and some counters */
369 struct rw_semaphore mmap_sem;
371 struct list_head mmlist; /* List of maybe swapped mm's. These are globally strung
372 * together off init_mm.mmlist, and are protected
373 * by mmlist_lock
374 */
377 unsigned long hiwater_rss; /* High-watermark of RSS usage */
378 unsigned long hiwater_vm; /* High-water virtual memory usage */
380 unsigned long total_vm; /* Total pages mapped */
381 unsigned long locked_vm; /* Pages that have PG_mlocked set */
382 unsigned long pinned_vm; /* Refcount permanently increased */
383 unsigned long shared_vm; /* Shared pages (files) */
384 unsigned long exec_vm; /* VM_EXEC & ~VM_WRITE */
385 unsigned long stack_vm; /* VM_GROWSUP/DOWN */
386 unsigned long def_flags;
387 unsigned long start_code, end_code, start_data, end_data;
388 unsigned long start_brk, brk, start_stack;
389 unsigned long arg_start, arg_end, env_start, env_end;
391 unsigned long saved_auxv[AT_VECTOR_SIZE]; /* for /proc/PID/auxv */
393 /*
394 * Special counters, in some configurations protected by the
395 * page_table_lock, in other configurations by being atomic.
396 */
397 struct mm_rss_stat rss_stat;
399 struct linux_binfmt *binfmt;
401 cpumask_var_t cpu_vm_mask_var;
403 /* Architecture-specific MM context */
404 mm_context_t context;
406 unsigned long flags; /* Must use atomic bitops to access the bits */
408 struct core_state *core_state; /* coredumping support */
409 #ifdef CONFIG_AIO
410 spinlock_t ioctx_lock;
411 struct kioctx_table __rcu *ioctx_table;
412 #endif
413 #ifdef CONFIG_MM_OWNER
414 /*
415 * "owner" points to a task that is regarded as the canonical
416 * user/owner of this mm. All of the following must be true in
417 * order for it to be changed:
418 *
419 * current == mm->owner
420 * current->mm != mm
421 * new_owner->mm == mm
422 * new_owner->alloc_lock is held
423 */
424 struct task_struct __rcu *owner;
425 #endif
427 /* store ref to file /proc/<pid>/exe symlink points to */
428 struct file *exe_file;
429 #ifdef CONFIG_MMU_NOTIFIER
430 struct mmu_notifier_mm *mmu_notifier_mm;
431 #endif
432 #if defined(CONFIG_TRANSPARENT_HUGEPAGE) && !USE_SPLIT_PMD_PTLOCKS
433 pgtable_t pmd_huge_pte; /* protected by page_table_lock */
434 #endif
435 #ifdef CONFIG_CPUMASK_OFFSTACK
436 struct cpumask cpumask_allocation;
437 #endif
438 #ifdef CONFIG_NUMA_BALANCING
439 /*
440 * numa_next_scan is the next time that the PTEs will be marked
441 * pte_numa. NUMA hinting faults will gather statistics and migrate
442 * pages to new nodes if necessary.
443 */
444 unsigned long numa_next_scan;
446 /* Restart point for scanning and setting pte_numa */
447 unsigned long numa_scan_offset;
449 /* numa_scan_seq prevents two threads setting pte_numa */
450 int numa_scan_seq;
451 #endif
452 #if defined(CONFIG_NUMA_BALANCING) || defined(CONFIG_COMPACTION)
453 /*
454 * An operation with batched TLB flushing is going on. Anything that
455 * can move process memory needs to flush the TLB when moving a
456 * PROT_NONE or PROT_NUMA mapped page.
457 */
458 bool tlb_flush_pending;
459 #endif
460 struct uprobes_state uprobes_state;
461 };
463 static inline void mm_init_cpumask(struct mm_struct *mm)
464 {
465 #ifdef CONFIG_CPUMASK_OFFSTACK
466 mm->cpu_vm_mask_var = &mm->cpumask_allocation;
467 #endif
468 }
470 /* Future-safe accessor for struct mm_struct's cpu_vm_mask. */
471 static inline cpumask_t *mm_cpumask(struct mm_struct *mm)
472 {
473 return mm->cpu_vm_mask_var;
474 }
476 #if defined(CONFIG_NUMA_BALANCING) || defined(CONFIG_COMPACTION)
477 /*
478 * Memory barriers to keep this state in sync are graciously provided by
479 * the page table locks, outside of which no page table modifications happen.
480 * The barriers below prevent the compiler from re-ordering the instructions
481 * around the memory barriers that are already present in the code.
482 */
483 static inline bool mm_tlb_flush_pending(struct mm_struct *mm)
484 {
485 barrier();
486 return mm->tlb_flush_pending;
487 }
488 static inline void set_tlb_flush_pending(struct mm_struct *mm)
489 {
490 mm->tlb_flush_pending = true;
492 /*
493 * Guarantee that the tlb_flush_pending store does not leak into the
494 * critical section updating the page tables
495 */
496 smp_mb__before_spinlock();
497 }
498 /* Clearing is done after a TLB flush, which also provides a barrier. */
499 static inline void clear_tlb_flush_pending(struct mm_struct *mm)
500 {
501 barrier();
502 mm->tlb_flush_pending = false;
503 }
504 #else
505 static inline bool mm_tlb_flush_pending(struct mm_struct *mm)
506 {
507 return false;
508 }
509 static inline void set_tlb_flush_pending(struct mm_struct *mm)
510 {
511 }
512 static inline void clear_tlb_flush_pending(struct mm_struct *mm)
513 {
514 }
515 #endif
517 /* Return the name for an anonymous mapping or NULL for a file-backed mapping */
518 static inline const char __user *vma_get_anon_name(struct vm_area_struct *vma)
519 {
520 if (vma->vm_file)
521 return NULL;
523 return vma->shared.anon_name;
524 }
526 #endif /* _LINUX_MM_TYPES_H */