1 #ifndef _LINUX_MM_TYPES_H
2 #define _LINUX_MM_TYPES_H
4 #include <linux/auxvec.h>
5 #include <linux/types.h>
6 #include <linux/threads.h>
7 #include <linux/list.h>
8 #include <linux/spinlock.h>
9 #include <linux/rbtree.h>
10 #include <linux/rwsem.h>
11 #include <linux/completion.h>
12 #include <linux/cpumask.h>
13 #include <linux/page-debug-flags.h>
14 #include <linux/uprobes.h>
15 #include <asm/page.h>
16 #include <asm/mmu.h>
18 #ifndef AT_VECTOR_SIZE_ARCH
19 #define AT_VECTOR_SIZE_ARCH 0
20 #endif
21 #define AT_VECTOR_SIZE (2*(AT_VECTOR_SIZE_ARCH + AT_VECTOR_SIZE_BASE + 1))
23 struct address_space;
25 #define USE_SPLIT_PTLOCKS (NR_CPUS >= CONFIG_SPLIT_PTLOCK_CPUS)
27 /*
28 * Each physical page in the system has a struct page associated with
29 * it to keep track of whatever it is we are using the page for at the
30 * moment. Note that we have no way to track which tasks are using
31 * a page, though if it is a pagecache page, rmap structures can tell us
32 * who is mapping it.
33 *
34 * The objects in struct page are organized in double word blocks in
35 * order to allows us to use atomic double word operations on portions
36 * of struct page. That is currently only used by slub but the arrangement
37 * allows the use of atomic double word operations on the flags/mapping
38 * and lru list pointers also.
39 */
40 struct page {
41 /* First double word block */
42 unsigned long flags; /* Atomic flags, some possibly
43 * updated asynchronously */
44 struct address_space *mapping; /* If low bit clear, points to
45 * inode address_space, or NULL.
46 * If page mapped as anonymous
47 * memory, low bit is set, and
48 * it points to anon_vma object:
49 * see PAGE_MAPPING_ANON below.
50 */
51 /* Second double word */
52 struct {
53 union {
54 pgoff_t index; /* Our offset within mapping. */
55 void *freelist; /* slub/slob first free object */
56 bool pfmemalloc; /* If set by the page allocator,
57 * ALLOC_NO_WATERMARKS was set
58 * and the low watermark was not
59 * met implying that the system
60 * is under some pressure. The
61 * caller should try ensure
62 * this page is only used to
63 * free other pages.
64 */
65 };
67 union {
68 #if defined(CONFIG_HAVE_CMPXCHG_DOUBLE) && \
69 defined(CONFIG_HAVE_ALIGNED_STRUCT_PAGE)
70 /* Used for cmpxchg_double in slub */
71 unsigned long counters;
72 #else
73 /*
74 * Keep _count separate from slub cmpxchg_double data.
75 * As the rest of the double word is protected by
76 * slab_lock but _count is not.
77 */
78 unsigned counters;
79 #endif
81 struct {
83 union {
84 /*
85 * Count of ptes mapped in
86 * mms, to show when page is
87 * mapped & limit reverse map
88 * searches.
89 *
90 * Used also for tail pages
91 * refcounting instead of
92 * _count. Tail pages cannot
93 * be mapped and keeping the
94 * tail page _count zero at
95 * all times guarantees
96 * get_page_unless_zero() will
97 * never succeed on tail
98 * pages.
99 */
100 atomic_t _mapcount;
102 struct { /* SLUB */
103 unsigned inuse:16;
104 unsigned objects:15;
105 unsigned frozen:1;
106 };
107 int units; /* SLOB */
108 };
109 atomic_t _count; /* Usage count, see below. */
110 };
111 };
112 };
114 /* Third double word block */
115 union {
116 struct list_head lru; /* Pageout list, eg. active_list
117 * protected by zone->lru_lock !
118 */
119 struct { /* slub per cpu partial pages */
120 struct page *next; /* Next partial slab */
121 #ifdef CONFIG_64BIT
122 int pages; /* Nr of partial slabs left */
123 int pobjects; /* Approximate # of objects */
124 #else
125 short int pages;
126 short int pobjects;
127 #endif
128 };
130 struct list_head list; /* slobs list of pages */
131 struct slab *slab_page; /* slab fields */
132 };
134 /* Remainder is not double word aligned */
135 union {
136 unsigned long private; /* Mapping-private opaque data:
137 * usually used for buffer_heads
138 * if PagePrivate set; used for
139 * swp_entry_t if PageSwapCache;
140 * indicates order in the buddy
141 * system if PG_buddy is set.
142 */
143 #if USE_SPLIT_PTLOCKS
144 spinlock_t ptl;
145 #endif
146 struct kmem_cache *slab_cache; /* SL[AU]B: Pointer to slab */
147 struct page *first_page; /* Compound tail pages */
148 };
150 /*
151 * On machines where all RAM is mapped into kernel address space,
152 * we can simply calculate the virtual address. On machines with
153 * highmem some memory is mapped into kernel virtual memory
154 * dynamically, so we need a place to store that address.
155 * Note that this field could be 16 bits on x86 ... ;)
156 *
157 * Architectures with slow multiplication can define
158 * WANT_PAGE_VIRTUAL in asm/page.h
159 */
160 #if defined(WANT_PAGE_VIRTUAL)
161 void *virtual; /* Kernel virtual address (NULL if
162 not kmapped, ie. highmem) */
163 #endif /* WANT_PAGE_VIRTUAL */
164 #ifdef CONFIG_WANT_PAGE_DEBUG_FLAGS
165 unsigned long debug_flags; /* Use atomic bitops on this */
166 #endif
168 #ifdef CONFIG_KMEMCHECK
169 /*
170 * kmemcheck wants to track the status of each byte in a page; this
171 * is a pointer to such a status block. NULL if not tracked.
172 */
173 void *shadow;
174 #endif
176 #ifdef CONFIG_NUMA_BALANCING
177 int _last_nid;
178 #endif
179 }
180 /*
181 * The struct page can be forced to be double word aligned so that atomic ops
182 * on double words work. The SLUB allocator can make use of such a feature.
183 */
184 #ifdef CONFIG_HAVE_ALIGNED_STRUCT_PAGE
185 __aligned(2 * sizeof(unsigned long))
186 #endif
187 ;
189 struct page_frag {
190 struct page *page;
191 #if (BITS_PER_LONG > 32) || (PAGE_SIZE >= 65536)
192 __u32 offset;
193 __u32 size;
194 #else
195 __u16 offset;
196 __u16 size;
197 #endif
198 };
200 typedef unsigned long __nocast vm_flags_t;
202 /*
203 * A region containing a mapping of a non-memory backed file under NOMMU
204 * conditions. These are held in a global tree and are pinned by the VMAs that
205 * map parts of them.
206 */
207 struct vm_region {
208 struct rb_node vm_rb; /* link in global region tree */
209 vm_flags_t vm_flags; /* VMA vm_flags */
210 unsigned long vm_start; /* start address of region */
211 unsigned long vm_end; /* region initialised to here */
212 unsigned long vm_top; /* region allocated to here */
213 unsigned long vm_pgoff; /* the offset in vm_file corresponding to vm_start */
214 struct file *vm_file; /* the backing file or NULL */
216 int vm_usage; /* region usage count (access under nommu_region_sem) */
217 bool vm_icache_flushed : 1; /* true if the icache has been flushed for
218 * this region */
219 };
221 /*
222 * This struct defines a memory VMM memory area. There is one of these
223 * per VM-area/task. A VM area is any part of the process virtual memory
224 * space that has a special rule for the page-fault handlers (ie a shared
225 * library, the executable area etc).
226 */
227 struct vm_area_struct {
228 /* The first cache line has the info for VMA tree walking. */
230 unsigned long vm_start; /* Our start address within vm_mm. */
231 unsigned long vm_end; /* The first byte after our end address
232 within vm_mm. */
234 /* linked list of VM areas per task, sorted by address */
235 struct vm_area_struct *vm_next, *vm_prev;
237 struct rb_node vm_rb;
239 /*
240 * Largest free memory gap in bytes to the left of this VMA.
241 * Either between this VMA and vma->vm_prev, or between one of the
242 * VMAs below us in the VMA rbtree and its ->vm_prev. This helps
243 * get_unmapped_area find a free area of the right size.
244 */
245 unsigned long rb_subtree_gap;
247 /* Second cache line starts here. */
249 struct mm_struct *vm_mm; /* The address space we belong to. */
250 pgprot_t vm_page_prot; /* Access permissions of this VMA. */
251 unsigned long vm_flags; /* Flags, see mm.h. */
253 /*
254 * For areas with an address space and backing store,
255 * linkage into the address_space->i_mmap interval tree, or
256 * linkage of vma in the address_space->i_mmap_nonlinear list.
257 */
258 union {
259 struct {
260 struct rb_node rb;
261 unsigned long rb_subtree_last;
262 } linear;
263 struct list_head nonlinear;
264 } shared;
266 /*
267 * A file's MAP_PRIVATE vma can be in both i_mmap tree and anon_vma
268 * list, after a COW of one of the file pages. A MAP_SHARED vma
269 * can only be in the i_mmap tree. An anonymous MAP_PRIVATE, stack
270 * or brk vma (with NULL file) can only be in an anon_vma list.
271 */
272 struct list_head anon_vma_chain; /* Serialized by mmap_sem &
273 * page_table_lock */
274 struct anon_vma *anon_vma; /* Serialized by page_table_lock */
276 /* Function pointers to deal with this struct. */
277 const struct vm_operations_struct *vm_ops;
279 /* Information about our backing store: */
280 unsigned long vm_pgoff; /* Offset (within vm_file) in PAGE_SIZE
281 units, *not* PAGE_CACHE_SIZE */
282 struct file * vm_file; /* File we map to (can be NULL). */
283 void * vm_private_data; /* was vm_pte (shared mem) */
285 #ifndef CONFIG_MMU
286 struct vm_region *vm_region; /* NOMMU mapping region */
287 #endif
288 #ifdef CONFIG_NUMA
289 struct mempolicy *vm_policy; /* NUMA policy for the VMA */
290 #endif
291 };
293 struct core_thread {
294 struct task_struct *task;
295 struct core_thread *next;
296 };
298 struct core_state {
299 atomic_t nr_threads;
300 struct core_thread dumper;
301 struct completion startup;
302 };
304 enum {
305 MM_FILEPAGES,
306 MM_ANONPAGES,
307 MM_SWAPENTS,
308 NR_MM_COUNTERS
309 };
311 #if USE_SPLIT_PTLOCKS && defined(CONFIG_MMU)
312 #define SPLIT_RSS_COUNTING
313 /* per-thread cached information, */
314 struct task_rss_stat {
315 int events; /* for synchronization threshold */
316 int count[NR_MM_COUNTERS];
317 };
318 #endif /* USE_SPLIT_PTLOCKS */
320 struct mm_rss_stat {
321 atomic_long_t count[NR_MM_COUNTERS];
322 };
324 struct mm_struct {
325 struct vm_area_struct * mmap; /* list of VMAs */
326 struct rb_root mm_rb;
327 struct vm_area_struct * mmap_cache; /* last find_vma result */
328 #ifdef CONFIG_MMU
329 unsigned long (*get_unmapped_area) (struct file *filp,
330 unsigned long addr, unsigned long len,
331 unsigned long pgoff, unsigned long flags);
332 void (*unmap_area) (struct mm_struct *mm, unsigned long addr);
333 #endif
334 unsigned long mmap_base; /* base of mmap area */
335 unsigned long task_size; /* size of task vm space */
336 unsigned long cached_hole_size; /* if non-zero, the largest hole below free_area_cache */
337 unsigned long free_area_cache; /* first hole of size cached_hole_size or larger */
338 unsigned long highest_vm_end; /* highest vma end address */
339 pgd_t * pgd;
340 atomic_t mm_users; /* How many users with user space? */
341 atomic_t mm_count; /* How many references to "struct mm_struct" (users count as 1) */
342 int map_count; /* number of VMAs */
344 spinlock_t page_table_lock; /* Protects page tables and some counters */
345 struct rw_semaphore mmap_sem;
347 struct list_head mmlist; /* List of maybe swapped mm's. These are globally strung
348 * together off init_mm.mmlist, and are protected
349 * by mmlist_lock
350 */
353 unsigned long hiwater_rss; /* High-watermark of RSS usage */
354 unsigned long hiwater_vm; /* High-water virtual memory usage */
356 unsigned long total_vm; /* Total pages mapped */
357 unsigned long locked_vm; /* Pages that have PG_mlocked set */
358 unsigned long pinned_vm; /* Refcount permanently increased */
359 unsigned long shared_vm; /* Shared pages (files) */
360 unsigned long exec_vm; /* VM_EXEC & ~VM_WRITE */
361 unsigned long stack_vm; /* VM_GROWSUP/DOWN */
362 unsigned long def_flags;
363 unsigned long nr_ptes; /* Page table pages */
364 unsigned long start_code, end_code, start_data, end_data;
365 unsigned long start_brk, brk, start_stack;
366 unsigned long arg_start, arg_end, env_start, env_end;
368 unsigned long saved_auxv[AT_VECTOR_SIZE]; /* for /proc/PID/auxv */
370 /*
371 * Special counters, in some configurations protected by the
372 * page_table_lock, in other configurations by being atomic.
373 */
374 struct mm_rss_stat rss_stat;
376 struct linux_binfmt *binfmt;
378 cpumask_var_t cpu_vm_mask_var;
380 /* Architecture-specific MM context */
381 mm_context_t context;
383 unsigned long flags; /* Must use atomic bitops to access the bits */
385 struct core_state *core_state; /* coredumping support */
386 #ifdef CONFIG_AIO
387 spinlock_t ioctx_lock;
388 struct hlist_head ioctx_list;
389 #endif
390 #ifdef CONFIG_MM_OWNER
391 /*
392 * "owner" points to a task that is regarded as the canonical
393 * user/owner of this mm. All of the following must be true in
394 * order for it to be changed:
395 *
396 * current == mm->owner
397 * current->mm != mm
398 * new_owner->mm == mm
399 * new_owner->alloc_lock is held
400 */
401 struct task_struct __rcu *owner;
402 #endif
404 /* store ref to file /proc/<pid>/exe symlink points to */
405 struct file *exe_file;
406 #ifdef CONFIG_MMU_NOTIFIER
407 struct mmu_notifier_mm *mmu_notifier_mm;
408 #endif
409 #ifdef CONFIG_TRANSPARENT_HUGEPAGE
410 pgtable_t pmd_huge_pte; /* protected by page_table_lock */
411 #endif
412 #ifdef CONFIG_CPUMASK_OFFSTACK
413 struct cpumask cpumask_allocation;
414 #endif
415 #ifdef CONFIG_NUMA_BALANCING
416 /*
417 * numa_next_scan is the next time when the PTEs will me marked
418 * pte_numa to gather statistics and migrate pages to new nodes
419 * if necessary
420 */
421 unsigned long numa_next_scan;
423 /* numa_next_reset is when the PTE scanner period will be reset */
424 unsigned long numa_next_reset;
426 /* Restart point for scanning and setting pte_numa */
427 unsigned long numa_scan_offset;
429 /* numa_scan_seq prevents two threads setting pte_numa */
430 int numa_scan_seq;
432 /*
433 * The first node a task was scheduled on. If a task runs on
434 * a different node than Make PTE Scan Go Now.
435 */
436 int first_nid;
437 #endif
438 struct uprobes_state uprobes_state;
439 };
441 /* first nid will either be a valid NID or one of these values */
442 #define NUMA_PTE_SCAN_INIT -1
443 #define NUMA_PTE_SCAN_ACTIVE -2
445 static inline void mm_init_cpumask(struct mm_struct *mm)
446 {
447 #ifdef CONFIG_CPUMASK_OFFSTACK
448 mm->cpu_vm_mask_var = &mm->cpumask_allocation;
449 #endif
450 }
452 /* Future-safe accessor for struct mm_struct's cpu_vm_mask. */
453 static inline cpumask_t *mm_cpumask(struct mm_struct *mm)
454 {
455 return mm->cpu_vm_mask_var;
456 }
458 #endif /* _LINUX_MM_TYPES_H */