1 /**
2 * @file oprofile.h
3 *
4 * API for machine-specific interrupts to interface
5 * to oprofile.
6 *
7 * @remark Copyright 2002 OProfile authors
8 * @remark Read the file COPYING
9 *
10 * @author John Levon <levon@movementarian.org>
11 */
13 #ifndef OPROFILE_H
14 #define OPROFILE_H
16 #include <linux/types.h>
17 #include <linux/spinlock.h>
18 #include <linux/init.h>
19 #include <linux/errno.h>
20 #include <linux/printk.h>
21 #include <linux/atomic.h>
23 /* Each escaped entry is prefixed by ESCAPE_CODE
24 * then one of the following codes, then the
25 * relevant data.
26 * These #defines live in this file so that arch-specific
27 * buffer sync'ing code can access them.
28 */
29 #define ESCAPE_CODE ~0UL
30 #define CTX_SWITCH_CODE 1
31 #define CPU_SWITCH_CODE 2
32 #define COOKIE_SWITCH_CODE 3
33 #define KERNEL_ENTER_SWITCH_CODE 4
34 #define KERNEL_EXIT_SWITCH_CODE 5
35 #define MODULE_LOADED_CODE 6
36 #define CTX_TGID_CODE 7
37 #define TRACE_BEGIN_CODE 8
38 #define TRACE_END_CODE 9
39 #define XEN_ENTER_SWITCH_CODE 10
40 #define SPU_PROFILING_CODE 11
41 #define SPU_CTX_SWITCH_CODE 12
42 #define IBS_FETCH_CODE 13
43 #define IBS_OP_CODE 14
45 struct super_block;
46 struct dentry;
47 struct file_operations;
48 struct pt_regs;
50 /* Operations structure to be filled in */
51 struct oprofile_operations {
52 /* create any necessary configuration files in the oprofile fs.
53 * Optional. */
54 int (*create_files)(struct super_block * sb, struct dentry * root);
55 /* Do any necessary interrupt setup. Optional. */
56 int (*setup)(void);
57 /* Do any necessary interrupt shutdown. Optional. */
58 void (*shutdown)(void);
59 /* Start delivering interrupts. */
60 int (*start)(void);
61 /* Stop delivering interrupts. */
62 void (*stop)(void);
63 /* Arch-specific buffer sync functions.
64 * Return value = 0: Success
65 * Return value = -1: Failure
66 * Return value = 1: Run generic sync function
67 */
68 int (*sync_start)(void);
69 int (*sync_stop)(void);
71 /* Initiate a stack backtrace. Optional. */
72 void (*backtrace)(struct pt_regs * const regs, unsigned int depth);
74 /* Multiplex between different events. Optional. */
75 int (*switch_events)(void);
76 /* CPU identification string. */
77 char * cpu_type;
78 };
80 /**
81 * One-time initialisation. *ops must be set to a filled-in
82 * operations structure. This is called even in timer interrupt
83 * mode so an arch can set a backtrace callback.
84 *
85 * If an error occurs, the fields should be left untouched.
86 */
87 int oprofile_arch_init(struct oprofile_operations * ops);
89 /**
90 * One-time exit/cleanup for the arch.
91 */
92 void oprofile_arch_exit(void);
94 /**
95 * Add a sample. This may be called from any context.
96 */
97 void oprofile_add_sample(struct pt_regs * const regs, unsigned long event);
99 /**
100 * Add an extended sample. Use this when the PC is not from the regs, and
101 * we cannot determine if we're in kernel mode from the regs.
102 *
103 * This function does perform a backtrace.
104 *
105 */
106 void oprofile_add_ext_sample(unsigned long pc, struct pt_regs * const regs,
107 unsigned long event, int is_kernel);
109 /**
110 * Add an hardware sample.
111 */
112 void oprofile_add_ext_hw_sample(unsigned long pc, struct pt_regs * const regs,
113 unsigned long event, int is_kernel,
114 struct task_struct *task);
116 /* Use this instead when the PC value is not from the regs. Doesn't
117 * backtrace. */
118 void oprofile_add_pc(unsigned long pc, int is_kernel, unsigned long event);
120 /* add a backtrace entry, to be called from the ->backtrace callback */
121 void oprofile_add_trace(unsigned long eip);
124 /**
125 * Create a file of the given name as a child of the given root, with
126 * the specified file operations.
127 */
128 int oprofilefs_create_file(struct super_block * sb, struct dentry * root,
129 char const * name, const struct file_operations * fops);
131 int oprofilefs_create_file_perm(struct super_block * sb, struct dentry * root,
132 char const * name, const struct file_operations * fops, int perm);
134 /** Create a file for read/write access to an unsigned long. */
135 int oprofilefs_create_ulong(struct super_block * sb, struct dentry * root,
136 char const * name, ulong * val);
138 /** Create a file for read-only access to an unsigned long. */
139 int oprofilefs_create_ro_ulong(struct super_block * sb, struct dentry * root,
140 char const * name, ulong * val);
142 /** Create a file for read-only access to an atomic_t. */
143 int oprofilefs_create_ro_atomic(struct super_block * sb, struct dentry * root,
144 char const * name, atomic_t * val);
146 /** create a directory */
147 struct dentry * oprofilefs_mkdir(struct super_block * sb, struct dentry * root,
148 char const * name);
150 /**
151 * Write the given asciz string to the given user buffer @buf, updating *offset
152 * appropriately. Returns bytes written or -EFAULT.
153 */
154 ssize_t oprofilefs_str_to_user(char const * str, char __user * buf, size_t count, loff_t * offset);
156 /**
157 * Convert an unsigned long value into ASCII and copy it to the user buffer @buf,
158 * updating *offset appropriately. Returns bytes written or -EFAULT.
159 */
160 ssize_t oprofilefs_ulong_to_user(unsigned long val, char __user * buf, size_t count, loff_t * offset);
162 /**
163 * Read an ASCII string for a number from a userspace buffer and fill *val on success.
164 * Returns 0 on success, < 0 on error.
165 */
166 int oprofilefs_ulong_from_user(unsigned long * val, char const __user * buf, size_t count);
168 /** lock for read/write safety */
169 extern raw_spinlock_t oprofilefs_lock;
171 /**
172 * Add the contents of a circular buffer to the event buffer.
173 */
174 void oprofile_put_buff(unsigned long *buf, unsigned int start,
175 unsigned int stop, unsigned int max);
177 unsigned long oprofile_get_cpu_buffer_size(void);
178 void oprofile_cpu_buffer_inc_smpl_lost(void);
180 /* cpu buffer functions */
182 struct op_sample;
184 struct op_entry {
185 struct ring_buffer_event *event;
186 struct op_sample *sample;
187 unsigned long size;
188 unsigned long *data;
189 };
191 void oprofile_write_reserve(struct op_entry *entry,
192 struct pt_regs * const regs,
193 unsigned long pc, int code, int size);
194 int oprofile_add_data(struct op_entry *entry, unsigned long val);
195 int oprofile_add_data64(struct op_entry *entry, u64 val);
196 int oprofile_write_commit(struct op_entry *entry);
198 #ifdef CONFIG_HW_PERF_EVENTS
199 int __init oprofile_perf_init(struct oprofile_operations *ops);
200 void oprofile_perf_exit(void);
201 char *op_name_from_perf_id(void);
202 #else
203 static inline int __init oprofile_perf_init(struct oprofile_operations *ops)
204 {
205 pr_info("oprofile: hardware counters not available\n");
206 return -ENODEV;
207 }
208 static inline void oprofile_perf_exit(void) { }
209 #endif /* CONFIG_HW_PERF_EVENTS */
211 #endif /* OPROFILE_H */