platform_data: Added platform data for GC320
[android-sdk/kernel-video.git] / include / linux / platform_data / omap_gcx.h
1 /*
2  *  arch/arm/plat-omap/include/plat/omap_gcx.h
3  *
4  * This program is free software; you can redistribute it and/or modify
5  * it under the terms of the GNU General Public License as published by
6  * the Free Software Foundation; either version 2 of the License, or
7  * (at your option) any later version.
8  *
9  * This program is distributed in the hope that it will be useful,
10  * but WITHOUT ANY WARRANTY; without even the implied warranty of
11  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
12  * GNU General Public License for more details.
13  *
14  * You should have received a copy of the GNU General Public License
15  * along with this program; if not, write to the Free Software
16  * Foundation, Inc., 59 Temple Place, Suite 330, Boston, MA 02111-1307 USA
17  */
19 #ifndef OMAP_GCX_H
20 #define OMAP_GCX_H
22 struct omap_gcx_platform_data {
23         bool is_hw_present;
24         void *regbase;
25         /*bool (*was_context_lost)(struct device *dev);*/
26         int (*get_context_loss_count)(struct device *dev);
27         /* device scale */
28         int (*scale_dev)(struct device *dev, unsigned long freq);
29         /* bandwith */
30         int (*set_bw)(struct device *dev, unsigned long v);
31 };
33 #endif