1 /*
2 * PTP 1588 clock support
3 *
4 * Copyright (C) 2010 OMICRON electronics GmbH
5 *
6 * This program is free software; you can redistribute it and/or modify
7 * it under the terms of the GNU General Public License as published by
8 * the Free Software Foundation; either version 2 of the License, or
9 * (at your option) any later version.
10 *
11 * This program is distributed in the hope that it will be useful,
12 * but WITHOUT ANY WARRANTY; without even the implied warranty of
13 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
14 * GNU General Public License for more details.
15 *
16 * You should have received a copy of the GNU General Public License
17 * along with this program; if not, write to the Free Software
18 * Foundation, Inc., 675 Mass Ave, Cambridge, MA 02139, USA.
19 */
21 #ifndef _PTP_CLOCK_KERNEL_H_
22 #define _PTP_CLOCK_KERNEL_H_
24 #include <linux/device.h>
25 #include <linux/pps_kernel.h>
26 #include <linux/ptp_clock.h>
29 struct ptp_clock_request {
30 enum {
31 PTP_CLK_REQ_EXTTS,
32 PTP_CLK_REQ_PEROUT,
33 PTP_CLK_REQ_PPS,
34 } type;
35 union {
36 struct ptp_extts_request extts;
37 struct ptp_perout_request perout;
38 };
39 };
41 /**
42 * struct ptp_clock_info - decribes a PTP hardware clock
43 *
44 * @owner: The clock driver should set to THIS_MODULE.
45 * @name: A short "friendly name" to identify the clock and to
46 * help distinguish PHY based devices from MAC based ones.
47 * The string is not meant to be a unique id.
48 * @max_adj: The maximum possible frequency adjustment, in parts per billon.
49 * @n_alarm: The number of programmable alarms.
50 * @n_ext_ts: The number of external time stamp channels.
51 * @n_per_out: The number of programmable periodic signals.
52 * @pps: Indicates whether the clock supports a PPS callback.
53 *
54 * clock operations
55 *
56 * @adjfreq: Adjusts the frequency of the hardware clock.
57 * parameter delta: Desired frequency offset from nominal frequency
58 * in parts per billion
59 *
60 * @adjtime: Shifts the time of the hardware clock.
61 * parameter delta: Desired change in nanoseconds.
62 *
63 * @gettime: Reads the current time from the hardware clock.
64 * parameter ts: Holds the result.
65 *
66 * @settime: Set the current time on the hardware clock.
67 * parameter ts: Time value to set.
68 *
69 * @enable: Request driver to enable or disable an ancillary feature.
70 * parameter request: Desired resource to enable or disable.
71 * parameter on: Caller passes one to enable or zero to disable.
72 *
73 * Drivers should embed their ptp_clock_info within a private
74 * structure, obtaining a reference to it using container_of().
75 *
76 * The callbacks must all return zero on success, non-zero otherwise.
77 */
79 struct ptp_clock_info {
80 struct module *owner;
81 char name[16];
82 s32 max_adj;
83 int n_alarm;
84 int n_ext_ts;
85 int n_per_out;
86 int pps;
87 int (*adjfreq)(struct ptp_clock_info *ptp, s32 delta);
88 int (*adjtime)(struct ptp_clock_info *ptp, s64 delta);
89 int (*gettime)(struct ptp_clock_info *ptp, struct timespec *ts);
90 int (*settime)(struct ptp_clock_info *ptp, const struct timespec *ts);
91 int (*enable)(struct ptp_clock_info *ptp,
92 struct ptp_clock_request *request, int on);
93 };
95 struct ptp_clock;
97 /**
98 * ptp_clock_register() - register a PTP hardware clock driver
99 *
100 * @info: Structure describing the new clock.
101 * @parent: Pointer to the parent device of the new clock.
102 */
104 extern struct ptp_clock *ptp_clock_register(struct ptp_clock_info *info,
105 struct device *parent);
107 /**
108 * ptp_clock_unregister() - unregister a PTP hardware clock driver
109 *
110 * @ptp: The clock to remove from service.
111 */
113 extern int ptp_clock_unregister(struct ptp_clock *ptp);
116 enum ptp_clock_events {
117 PTP_CLOCK_ALARM,
118 PTP_CLOCK_EXTTS,
119 PTP_CLOCK_PPS,
120 PTP_CLOCK_PPSUSR,
121 };
123 /**
124 * struct ptp_clock_event - decribes a PTP hardware clock event
125 *
126 * @type: One of the ptp_clock_events enumeration values.
127 * @index: Identifies the source of the event.
128 * @timestamp: When the event occurred (%PTP_CLOCK_EXTTS only).
129 * @pps_times: When the event occurred (%PTP_CLOCK_PPSUSR only).
130 */
132 struct ptp_clock_event {
133 int type;
134 int index;
135 union {
136 u64 timestamp;
137 struct pps_event_time pps_times;
138 };
139 };
141 /**
142 * ptp_clock_event() - notify the PTP layer about an event
143 *
144 * @ptp: The clock obtained from ptp_clock_register().
145 * @event: Message structure describing the event.
146 */
148 extern void ptp_clock_event(struct ptp_clock *ptp,
149 struct ptp_clock_event *event);
151 /**
152 * ptp_clock_index() - obtain the device index of a PTP clock
153 *
154 * @ptp: The clock obtained from ptp_clock_register().
155 */
157 extern int ptp_clock_index(struct ptp_clock *ptp);
159 #endif