1 /*
2 * linux/drivers/char/serial_core.h
3 *
4 * Copyright (C) 2000 Deep Blue Solutions Ltd.
5 *
6 * This program is free software; you can redistribute it and/or modify
7 * it under the terms of the GNU General Public License as published by
8 * the Free Software Foundation; either version 2 of the License, or
9 * (at your option) any later version.
10 *
11 * This program is distributed in the hope that it will be useful,
12 * but WITHOUT ANY WARRANTY; without even the implied warranty of
13 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
14 * GNU General Public License for more details.
15 *
16 * You should have received a copy of the GNU General Public License
17 * along with this program; if not, write to the Free Software
18 * Foundation, Inc., 59 Temple Place, Suite 330, Boston, MA 02111-1307 USA
19 */
20 #ifndef LINUX_SERIAL_CORE_H
21 #define LINUX_SERIAL_CORE_H
24 #include <linux/compiler.h>
25 #include <linux/interrupt.h>
26 #include <linux/circ_buf.h>
27 #include <linux/spinlock.h>
28 #include <linux/sched.h>
29 #include <linux/tty.h>
30 #include <linux/mutex.h>
31 #include <linux/sysrq.h>
32 #include <linux/pps_kernel.h>
33 #include <uapi/linux/serial_core.h>
35 struct uart_port;
36 struct serial_struct;
37 struct device;
39 /*
40 * This structure describes all the operations that can be
41 * done on the physical hardware.
42 */
43 struct uart_ops {
44 unsigned int (*tx_empty)(struct uart_port *);
45 void (*set_mctrl)(struct uart_port *, unsigned int mctrl);
46 unsigned int (*get_mctrl)(struct uart_port *);
47 void (*stop_tx)(struct uart_port *);
48 void (*start_tx)(struct uart_port *);
49 void (*throttle)(struct uart_port *);
50 void (*unthrottle)(struct uart_port *);
51 void (*send_xchar)(struct uart_port *, char ch);
52 void (*stop_rx)(struct uart_port *);
53 void (*enable_ms)(struct uart_port *);
54 void (*break_ctl)(struct uart_port *, int ctl);
55 int (*startup)(struct uart_port *);
56 void (*shutdown)(struct uart_port *);
57 void (*flush_buffer)(struct uart_port *);
58 void (*set_termios)(struct uart_port *, struct ktermios *new,
59 struct ktermios *old);
60 void (*set_ldisc)(struct uart_port *, int new);
61 void (*pm)(struct uart_port *, unsigned int state,
62 unsigned int oldstate);
63 int (*set_wake)(struct uart_port *, unsigned int state);
65 /*
66 * Return a string describing the type of the port
67 */
68 const char *(*type)(struct uart_port *);
70 /*
71 * Release IO and memory resources used by the port.
72 * This includes iounmap if necessary.
73 */
74 void (*release_port)(struct uart_port *);
76 /*
77 * Request IO and memory resources used by the port.
78 * This includes iomapping the port if necessary.
79 */
80 int (*request_port)(struct uart_port *);
81 void (*config_port)(struct uart_port *, int);
82 int (*verify_port)(struct uart_port *, struct serial_struct *);
83 int (*ioctl)(struct uart_port *, unsigned int, unsigned long);
84 #ifdef CONFIG_CONSOLE_POLL
85 int (*poll_init)(struct uart_port *);
86 void (*poll_put_char)(struct uart_port *, unsigned char);
87 int (*poll_get_char)(struct uart_port *);
88 #endif
89 };
91 #define NO_POLL_CHAR 0x00ff0000
92 #define UART_CONFIG_TYPE (1 << 0)
93 #define UART_CONFIG_IRQ (1 << 1)
95 struct uart_icount {
96 __u32 cts;
97 __u32 dsr;
98 __u32 rng;
99 __u32 dcd;
100 __u32 rx;
101 __u32 tx;
102 __u32 frame;
103 __u32 overrun;
104 __u32 parity;
105 __u32 brk;
106 __u32 buf_overrun;
107 };
109 typedef unsigned int __bitwise__ upf_t;
111 struct uart_port {
112 spinlock_t lock; /* port lock */
113 unsigned long iobase; /* in/out[bwl] */
114 unsigned char __iomem *membase; /* read/write[bwl] */
115 unsigned int (*serial_in)(struct uart_port *, int);
116 void (*serial_out)(struct uart_port *, int, int);
117 void (*set_termios)(struct uart_port *,
118 struct ktermios *new,
119 struct ktermios *old);
120 int (*handle_irq)(struct uart_port *);
121 void (*pm)(struct uart_port *, unsigned int state,
122 unsigned int old);
123 void (*handle_break)(struct uart_port *);
124 unsigned int irq; /* irq number */
125 unsigned long irqflags; /* irq flags */
126 unsigned int uartclk; /* base uart clock */
127 unsigned int fifosize; /* tx fifo size */
128 unsigned char x_char; /* xon/xoff char */
129 unsigned char regshift; /* reg offset shift */
130 unsigned char iotype; /* io access style */
131 unsigned char unused1;
133 #define UPIO_PORT (0)
134 #define UPIO_HUB6 (1)
135 #define UPIO_MEM (2)
136 #define UPIO_MEM32 (3)
137 #define UPIO_AU (4) /* Au1x00 type IO */
138 #define UPIO_TSI (5) /* Tsi108/109 type IO */
139 #define UPIO_RM9000 (6) /* RM9000 type IO */
141 unsigned int read_status_mask; /* driver specific */
142 unsigned int ignore_status_mask; /* driver specific */
143 struct uart_state *state; /* pointer to parent state */
144 struct uart_icount icount; /* statistics */
146 struct console *cons; /* struct console, if any */
147 #if defined(CONFIG_SERIAL_CORE_CONSOLE) || defined(SUPPORT_SYSRQ)
148 unsigned long sysrq; /* sysrq timeout */
149 #endif
151 upf_t flags;
153 #define UPF_FOURPORT ((__force upf_t) (1 << 1))
154 #define UPF_SAK ((__force upf_t) (1 << 2))
155 #define UPF_SPD_MASK ((__force upf_t) (0x1030))
156 #define UPF_SPD_HI ((__force upf_t) (0x0010))
157 #define UPF_SPD_VHI ((__force upf_t) (0x0020))
158 #define UPF_SPD_CUST ((__force upf_t) (0x0030))
159 #define UPF_SPD_SHI ((__force upf_t) (0x1000))
160 #define UPF_SPD_WARP ((__force upf_t) (0x1010))
161 #define UPF_SKIP_TEST ((__force upf_t) (1 << 6))
162 #define UPF_AUTO_IRQ ((__force upf_t) (1 << 7))
163 #define UPF_HARDPPS_CD ((__force upf_t) (1 << 11))
164 #define UPF_LOW_LATENCY ((__force upf_t) (1 << 13))
165 #define UPF_BUGGY_UART ((__force upf_t) (1 << 14))
166 #define UPF_NO_TXEN_TEST ((__force upf_t) (1 << 15))
167 #define UPF_MAGIC_MULTIPLIER ((__force upf_t) (1 << 16))
168 /* Port has hardware-assisted h/w flow control (iow, auto-RTS *not* auto-CTS) */
169 #define UPF_HARD_FLOW ((__force upf_t) (1 << 21))
170 /* Port has hardware-assisted s/w flow control */
171 #define UPF_SOFT_FLOW ((__force upf_t) (1 << 22))
172 #define UPF_CONS_FLOW ((__force upf_t) (1 << 23))
173 #define UPF_SHARE_IRQ ((__force upf_t) (1 << 24))
174 #define UPF_EXAR_EFR ((__force upf_t) (1 << 25))
175 #define UPF_BUG_THRE ((__force upf_t) (1 << 26))
176 /* The exact UART type is known and should not be probed. */
177 #define UPF_FIXED_TYPE ((__force upf_t) (1 << 27))
178 #define UPF_BOOT_AUTOCONF ((__force upf_t) (1 << 28))
179 #define UPF_FIXED_PORT ((__force upf_t) (1 << 29))
180 #define UPF_DEAD ((__force upf_t) (1 << 30))
181 #define UPF_IOREMAP ((__force upf_t) (1 << 31))
183 #define UPF_CHANGE_MASK ((__force upf_t) (0x17fff))
184 #define UPF_USR_MASK ((__force upf_t) (UPF_SPD_MASK|UPF_LOW_LATENCY))
186 unsigned int mctrl; /* current modem ctrl settings */
187 unsigned int timeout; /* character-based timeout */
188 unsigned int type; /* port type */
189 const struct uart_ops *ops;
190 unsigned int custom_divisor;
191 unsigned int line; /* port index */
192 resource_size_t mapbase; /* for ioremap */
193 struct device *dev; /* parent device */
194 unsigned char hub6; /* this should be in the 8250 driver */
195 unsigned char suspended;
196 unsigned char irq_wake;
197 unsigned char unused[2];
198 void *private_data; /* generic platform data pointer */
199 };
201 static inline int serial_port_in(struct uart_port *up, int offset)
202 {
203 return up->serial_in(up, offset);
204 }
206 static inline void serial_port_out(struct uart_port *up, int offset, int value)
207 {
208 up->serial_out(up, offset, value);
209 }
211 /*
212 * This is the state information which is persistent across opens.
213 */
214 struct uart_state {
215 struct tty_port port;
217 int pm_state;
218 struct circ_buf xmit;
220 struct uart_port *uart_port;
221 };
223 #define UART_XMIT_SIZE PAGE_SIZE
226 /* number of characters left in xmit buffer before we ask for more */
227 #define WAKEUP_CHARS 256
229 struct module;
230 struct tty_driver;
232 struct uart_driver {
233 struct module *owner;
234 const char *driver_name;
235 const char *dev_name;
236 int major;
237 int minor;
238 int nr;
239 struct console *cons;
241 /*
242 * these are private; the low level driver should not
243 * touch these; they should be initialised to NULL
244 */
245 struct uart_state *state;
246 struct tty_driver *tty_driver;
247 };
249 void uart_write_wakeup(struct uart_port *port);
251 /*
252 * Baud rate helpers.
253 */
254 void uart_update_timeout(struct uart_port *port, unsigned int cflag,
255 unsigned int baud);
256 unsigned int uart_get_baud_rate(struct uart_port *port, struct ktermios *termios,
257 struct ktermios *old, unsigned int min,
258 unsigned int max);
259 unsigned int uart_get_divisor(struct uart_port *port, unsigned int baud);
261 /* Base timer interval for polling */
262 static inline int uart_poll_timeout(struct uart_port *port)
263 {
264 int timeout = port->timeout;
266 return timeout > 6 ? (timeout / 2 - 2) : 1;
267 }
269 /*
270 * Console helpers.
271 */
272 struct uart_port *uart_get_console(struct uart_port *ports, int nr,
273 struct console *c);
274 void uart_parse_options(char *options, int *baud, int *parity, int *bits,
275 int *flow);
276 int uart_set_options(struct uart_port *port, struct console *co, int baud,
277 int parity, int bits, int flow);
278 struct tty_driver *uart_console_device(struct console *co, int *index);
279 void uart_console_write(struct uart_port *port, const char *s,
280 unsigned int count,
281 void (*putchar)(struct uart_port *, int));
283 /*
284 * Port/driver registration/removal
285 */
286 int uart_register_driver(struct uart_driver *uart);
287 void uart_unregister_driver(struct uart_driver *uart);
288 int uart_add_one_port(struct uart_driver *reg, struct uart_port *port);
289 int uart_remove_one_port(struct uart_driver *reg, struct uart_port *port);
290 int uart_match_port(struct uart_port *port1, struct uart_port *port2);
292 /*
293 * Power Management
294 */
295 int uart_suspend_port(struct uart_driver *reg, struct uart_port *port);
296 int uart_resume_port(struct uart_driver *reg, struct uart_port *port);
298 #define uart_circ_empty(circ) ((circ)->head == (circ)->tail)
299 #define uart_circ_clear(circ) ((circ)->head = (circ)->tail = 0)
301 #define uart_circ_chars_pending(circ) \
302 (CIRC_CNT((circ)->head, (circ)->tail, UART_XMIT_SIZE))
304 #define uart_circ_chars_free(circ) \
305 (CIRC_SPACE((circ)->head, (circ)->tail, UART_XMIT_SIZE))
307 static inline int uart_tx_stopped(struct uart_port *port)
308 {
309 struct tty_struct *tty = port->state->port.tty;
310 if(tty->stopped || tty->hw_stopped)
311 return 1;
312 return 0;
313 }
315 /*
316 * The following are helper functions for the low level drivers.
317 */
319 extern void uart_handle_dcd_change(struct uart_port *uport,
320 unsigned int status);
321 extern void uart_handle_cts_change(struct uart_port *uport,
322 unsigned int status);
324 extern void uart_insert_char(struct uart_port *port, unsigned int status,
325 unsigned int overrun, unsigned int ch, unsigned int flag);
327 #ifdef SUPPORT_SYSRQ
328 static inline int
329 uart_handle_sysrq_char(struct uart_port *port, unsigned int ch)
330 {
331 if (port->sysrq) {
332 if (ch && time_before(jiffies, port->sysrq)) {
333 handle_sysrq(ch);
334 port->sysrq = 0;
335 return 1;
336 }
337 port->sysrq = 0;
338 }
339 return 0;
340 }
341 #else
342 #define uart_handle_sysrq_char(port,ch) ({ (void)port; 0; })
343 #endif
345 /*
346 * We do the SysRQ and SAK checking like this...
347 */
348 static inline int uart_handle_break(struct uart_port *port)
349 {
350 struct uart_state *state = port->state;
352 if (port->handle_break)
353 port->handle_break(port);
355 #ifdef SUPPORT_SYSRQ
356 if (port->cons && port->cons->index == port->line) {
357 if (!port->sysrq) {
358 port->sysrq = jiffies + HZ*5;
359 return 1;
360 }
361 port->sysrq = 0;
362 }
363 #endif
364 if (port->flags & UPF_SAK)
365 do_SAK(state->port.tty);
366 return 0;
367 }
369 /*
370 * UART_ENABLE_MS - determine if port should enable modem status irqs
371 */
372 #define UART_ENABLE_MS(port,cflag) ((port)->flags & UPF_HARDPPS_CD || \
373 (cflag) & CRTSCTS || \
374 !((cflag) & CLOCAL))
376 #endif /* LINUX_SERIAL_CORE_H */