]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/blob - include/linux/serial_core.h
Merge remote-tracking branch 'asoc/fix/wm2200' into tmp
[android-sdk/kernel-video.git] / include / linux / serial_core.h
1 /*
2  *  linux/drivers/char/serial_core.h
3  *
4  *  Copyright (C) 2000 Deep Blue Solutions Ltd.
5  *
6  * This program is free software; you can redistribute it and/or modify
7  * it under the terms of the GNU General Public License as published by
8  * the Free Software Foundation; either version 2 of the License, or
9  * (at your option) any later version.
10  *
11  * This program is distributed in the hope that it will be useful,
12  * but WITHOUT ANY WARRANTY; without even the implied warranty of
13  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
14  * GNU General Public License for more details.
15  *
16  * You should have received a copy of the GNU General Public License
17  * along with this program; if not, write to the Free Software
18  * Foundation, Inc., 59 Temple Place, Suite 330, Boston, MA  02111-1307  USA
19  */
20 #ifndef LINUX_SERIAL_CORE_H
21 #define LINUX_SERIAL_CORE_H
24 #include <linux/compiler.h>
25 #include <linux/interrupt.h>
26 #include <linux/circ_buf.h>
27 #include <linux/spinlock.h>
28 #include <linux/sched.h>
29 #include <linux/tty.h>
30 #include <linux/mutex.h>
31 #include <linux/sysrq.h>
32 #include <linux/pps_kernel.h>
33 #include <uapi/linux/serial_core.h>
35 struct uart_port;
36 struct serial_struct;
37 struct device;
39 /*
40  * This structure describes all the operations that can be
41  * done on the physical hardware.
42  */
43 struct uart_ops {
44         unsigned int    (*tx_empty)(struct uart_port *);
45         void            (*set_mctrl)(struct uart_port *, unsigned int mctrl);
46         unsigned int    (*get_mctrl)(struct uart_port *);
47         void            (*stop_tx)(struct uart_port *);
48         void            (*start_tx)(struct uart_port *);
49         void            (*throttle)(struct uart_port *);
50         void            (*unthrottle)(struct uart_port *);
51         void            (*send_xchar)(struct uart_port *, char ch);
52         void            (*stop_rx)(struct uart_port *);
53         void            (*enable_ms)(struct uart_port *);
54         void            (*break_ctl)(struct uart_port *, int ctl);
55         int             (*startup)(struct uart_port *);
56         void            (*shutdown)(struct uart_port *);
57         void            (*flush_buffer)(struct uart_port *);
58         void            (*set_termios)(struct uart_port *, struct ktermios *new,
59                                        struct ktermios *old);
60         void            (*set_ldisc)(struct uart_port *, int new);
61         void            (*pm)(struct uart_port *, unsigned int state,
62                               unsigned int oldstate);
63         int             (*set_wake)(struct uart_port *, unsigned int state);
65         /*
66          * Return a string describing the type of the port
67          */
68         const char *(*type)(struct uart_port *);
70         /*
71          * Release IO and memory resources used by the port.
72          * This includes iounmap if necessary.
73          */
74         void            (*release_port)(struct uart_port *);
76         /*
77          * Request IO and memory resources used by the port.
78          * This includes iomapping the port if necessary.
79          */
80         int             (*request_port)(struct uart_port *);
81         void            (*config_port)(struct uart_port *, int);
82         int             (*verify_port)(struct uart_port *, struct serial_struct *);
83         int             (*ioctl)(struct uart_port *, unsigned int, unsigned long);
84 #ifdef CONFIG_CONSOLE_POLL
85         int             (*poll_init)(struct uart_port *);
86         void    (*poll_put_char)(struct uart_port *, unsigned char);
87         int             (*poll_get_char)(struct uart_port *);
88 #endif
89 };
91 #define NO_POLL_CHAR            0x00ff0000
92 #define UART_CONFIG_TYPE        (1 << 0)
93 #define UART_CONFIG_IRQ         (1 << 1)
95 struct uart_icount {
96         __u32   cts;
97         __u32   dsr;
98         __u32   rng;
99         __u32   dcd;
100         __u32   rx;
101         __u32   tx;
102         __u32   frame;
103         __u32   overrun;
104         __u32   parity;
105         __u32   brk;
106         __u32   buf_overrun;
107 };
109 typedef unsigned int __bitwise__ upf_t;
111 struct uart_port {
112         spinlock_t              lock;                   /* port lock */
113         unsigned long           iobase;                 /* in/out[bwl] */
114         unsigned char __iomem   *membase;               /* read/write[bwl] */
115         unsigned int            (*serial_in)(struct uart_port *, int);
116         void                    (*serial_out)(struct uart_port *, int, int);
117         void                    (*set_termios)(struct uart_port *,
118                                                struct ktermios *new,
119                                                struct ktermios *old);
120         int                     (*handle_irq)(struct uart_port *);
121         void                    (*pm)(struct uart_port *, unsigned int state,
122                                       unsigned int old);
123         void                    (*handle_break)(struct uart_port *);
124         unsigned int            irq;                    /* irq number */
125         unsigned long           irqflags;               /* irq flags  */
126         unsigned int            uartclk;                /* base uart clock */
127         unsigned int            fifosize;               /* tx fifo size */
128         unsigned char           x_char;                 /* xon/xoff char */
129         unsigned char           regshift;               /* reg offset shift */
130         unsigned char           iotype;                 /* io access style */
131         unsigned char           unused1;
133 #define UPIO_PORT               (0)
134 #define UPIO_HUB6               (1)
135 #define UPIO_MEM                (2)
136 #define UPIO_MEM32              (3)
137 #define UPIO_AU                 (4)                     /* Au1x00 type IO */
138 #define UPIO_TSI                (5)                     /* Tsi108/109 type IO */
139 #define UPIO_RM9000             (6)                     /* RM9000 type IO */
141         unsigned int            read_status_mask;       /* driver specific */
142         unsigned int            ignore_status_mask;     /* driver specific */
143         struct uart_state       *state;                 /* pointer to parent state */
144         struct uart_icount      icount;                 /* statistics */
146         struct console          *cons;                  /* struct console, if any */
147 #if defined(CONFIG_SERIAL_CORE_CONSOLE) || defined(SUPPORT_SYSRQ)
148         unsigned long           sysrq;                  /* sysrq timeout */
149 #endif
151         upf_t                   flags;
153 #define UPF_FOURPORT            ((__force upf_t) (1 << 1))
154 #define UPF_SAK                 ((__force upf_t) (1 << 2))
155 #define UPF_SPD_MASK            ((__force upf_t) (0x1030))
156 #define UPF_SPD_HI              ((__force upf_t) (0x0010))
157 #define UPF_SPD_VHI             ((__force upf_t) (0x0020))
158 #define UPF_SPD_CUST            ((__force upf_t) (0x0030))
159 #define UPF_SPD_SHI             ((__force upf_t) (0x1000))
160 #define UPF_SPD_WARP            ((__force upf_t) (0x1010))
161 #define UPF_SKIP_TEST           ((__force upf_t) (1 << 6))
162 #define UPF_AUTO_IRQ            ((__force upf_t) (1 << 7))
163 #define UPF_HARDPPS_CD          ((__force upf_t) (1 << 11))
164 #define UPF_LOW_LATENCY         ((__force upf_t) (1 << 13))
165 #define UPF_BUGGY_UART          ((__force upf_t) (1 << 14))
166 #define UPF_NO_TXEN_TEST        ((__force upf_t) (1 << 15))
167 #define UPF_MAGIC_MULTIPLIER    ((__force upf_t) (1 << 16))
168 /* Port has hardware-assisted h/w flow control (iow, auto-RTS *not* auto-CTS) */
169 #define UPF_HARD_FLOW           ((__force upf_t) (1 << 21))
170 /* Port has hardware-assisted s/w flow control */
171 #define UPF_SOFT_FLOW           ((__force upf_t) (1 << 22))
172 #define UPF_CONS_FLOW           ((__force upf_t) (1 << 23))
173 #define UPF_SHARE_IRQ           ((__force upf_t) (1 << 24))
174 #define UPF_EXAR_EFR            ((__force upf_t) (1 << 25))
175 #define UPF_BUG_THRE            ((__force upf_t) (1 << 26))
176 /* The exact UART type is known and should not be probed.  */
177 #define UPF_FIXED_TYPE          ((__force upf_t) (1 << 27))
178 #define UPF_BOOT_AUTOCONF       ((__force upf_t) (1 << 28))
179 #define UPF_FIXED_PORT          ((__force upf_t) (1 << 29))
180 #define UPF_DEAD                ((__force upf_t) (1 << 30))
181 #define UPF_IOREMAP             ((__force upf_t) (1 << 31))
183 #define UPF_CHANGE_MASK         ((__force upf_t) (0x17fff))
184 #define UPF_USR_MASK            ((__force upf_t) (UPF_SPD_MASK|UPF_LOW_LATENCY))
186         unsigned int            mctrl;                  /* current modem ctrl settings */
187         unsigned int            timeout;                /* character-based timeout */
188         unsigned int            type;                   /* port type */
189         const struct uart_ops   *ops;
190         unsigned int            custom_divisor;
191         unsigned int            line;                   /* port index */
192         resource_size_t         mapbase;                /* for ioremap */
193         struct device           *dev;                   /* parent device */
194         unsigned char           hub6;                   /* this should be in the 8250 driver */
195         unsigned char           suspended;
196         unsigned char           irq_wake;
197         unsigned char           unused[2];
198         void                    *private_data;          /* generic platform data pointer */
199 };
201 static inline int serial_port_in(struct uart_port *up, int offset)
203         return up->serial_in(up, offset);
206 static inline void serial_port_out(struct uart_port *up, int offset, int value)
208         up->serial_out(up, offset, value);
211 /*
212  * This is the state information which is persistent across opens.
213  */
214 struct uart_state {
215         struct tty_port         port;
217         int                     pm_state;
218         struct circ_buf         xmit;
220         struct uart_port        *uart_port;
221 };
223 #define UART_XMIT_SIZE  PAGE_SIZE
226 /* number of characters left in xmit buffer before we ask for more */
227 #define WAKEUP_CHARS            256
229 struct module;
230 struct tty_driver;
232 struct uart_driver {
233         struct module           *owner;
234         const char              *driver_name;
235         const char              *dev_name;
236         int                      major;
237         int                      minor;
238         int                      nr;
239         struct console          *cons;
241         /*
242          * these are private; the low level driver should not
243          * touch these; they should be initialised to NULL
244          */
245         struct uart_state       *state;
246         struct tty_driver       *tty_driver;
247 };
249 void uart_write_wakeup(struct uart_port *port);
251 /*
252  * Baud rate helpers.
253  */
254 void uart_update_timeout(struct uart_port *port, unsigned int cflag,
255                          unsigned int baud);
256 unsigned int uart_get_baud_rate(struct uart_port *port, struct ktermios *termios,
257                                 struct ktermios *old, unsigned int min,
258                                 unsigned int max);
259 unsigned int uart_get_divisor(struct uart_port *port, unsigned int baud);
261 /* Base timer interval for polling */
262 static inline int uart_poll_timeout(struct uart_port *port)
264         int timeout = port->timeout;
266         return timeout > 6 ? (timeout / 2 - 2) : 1;
269 /*
270  * Console helpers.
271  */
272 struct uart_port *uart_get_console(struct uart_port *ports, int nr,
273                                    struct console *c);
274 void uart_parse_options(char *options, int *baud, int *parity, int *bits,
275                         int *flow);
276 int uart_set_options(struct uart_port *port, struct console *co, int baud,
277                      int parity, int bits, int flow);
278 struct tty_driver *uart_console_device(struct console *co, int *index);
279 void uart_console_write(struct uart_port *port, const char *s,
280                         unsigned int count,
281                         void (*putchar)(struct uart_port *, int));
283 /*
284  * Port/driver registration/removal
285  */
286 int uart_register_driver(struct uart_driver *uart);
287 void uart_unregister_driver(struct uart_driver *uart);
288 int uart_add_one_port(struct uart_driver *reg, struct uart_port *port);
289 int uart_remove_one_port(struct uart_driver *reg, struct uart_port *port);
290 int uart_match_port(struct uart_port *port1, struct uart_port *port2);
292 /*
293  * Power Management
294  */
295 int uart_suspend_port(struct uart_driver *reg, struct uart_port *port);
296 int uart_resume_port(struct uart_driver *reg, struct uart_port *port);
298 #define uart_circ_empty(circ)           ((circ)->head == (circ)->tail)
299 #define uart_circ_clear(circ)           ((circ)->head = (circ)->tail = 0)
301 #define uart_circ_chars_pending(circ)   \
302         (CIRC_CNT((circ)->head, (circ)->tail, UART_XMIT_SIZE))
304 #define uart_circ_chars_free(circ)      \
305         (CIRC_SPACE((circ)->head, (circ)->tail, UART_XMIT_SIZE))
307 static inline int uart_tx_stopped(struct uart_port *port)
309         struct tty_struct *tty = port->state->port.tty;
310         if(tty->stopped || tty->hw_stopped)
311                 return 1;
312         return 0;
315 /*
316  * The following are helper functions for the low level drivers.
317  */
319 extern void uart_handle_dcd_change(struct uart_port *uport,
320                 unsigned int status);
321 extern void uart_handle_cts_change(struct uart_port *uport,
322                 unsigned int status);
324 extern void uart_insert_char(struct uart_port *port, unsigned int status,
325                  unsigned int overrun, unsigned int ch, unsigned int flag);
327 #ifdef SUPPORT_SYSRQ
328 static inline int
329 uart_handle_sysrq_char(struct uart_port *port, unsigned int ch)
331         if (port->sysrq) {
332                 if (ch && time_before(jiffies, port->sysrq)) {
333                         handle_sysrq(ch);
334                         port->sysrq = 0;
335                         return 1;
336                 }
337                 port->sysrq = 0;
338         }
339         return 0;
341 #else
342 #define uart_handle_sysrq_char(port,ch) ({ (void)port; 0; })
343 #endif
345 /*
346  * We do the SysRQ and SAK checking like this...
347  */
348 static inline int uart_handle_break(struct uart_port *port)
350         struct uart_state *state = port->state;
352         if (port->handle_break)
353                 port->handle_break(port);
355 #ifdef SUPPORT_SYSRQ
356         if (port->cons && port->cons->index == port->line) {
357                 if (!port->sysrq) {
358                         port->sysrq = jiffies + HZ*5;
359                         return 1;
360                 }
361                 port->sysrq = 0;
362         }
363 #endif
364         if (port->flags & UPF_SAK)
365                 do_SAK(state->port.tty);
366         return 0;
369 /*
370  *      UART_ENABLE_MS - determine if port should enable modem status irqs
371  */
372 #define UART_ENABLE_MS(port,cflag)      ((port)->flags & UPF_HARDPPS_CD || \
373                                          (cflag) & CRTSCTS || \
374                                          !((cflag) & CLOCAL))
376 #endif /* LINUX_SERIAL_CORE_H */