1 #ifndef _LINUX_SLUB_DEF_H
2 #define _LINUX_SLUB_DEF_H
4 /*
5 * SLUB : A Slab allocator without object queues.
6 *
7 * (C) 2007 SGI, Christoph Lameter
8 */
9 #include <linux/types.h>
10 #include <linux/gfp.h>
11 #include <linux/bug.h>
12 #include <linux/workqueue.h>
13 #include <linux/kobject.h>
15 #include <linux/kmemleak.h>
17 enum stat_item {
18 ALLOC_FASTPATH, /* Allocation from cpu slab */
19 ALLOC_SLOWPATH, /* Allocation by getting a new cpu slab */
20 FREE_FASTPATH, /* Free to cpu slub */
21 FREE_SLOWPATH, /* Freeing not to cpu slab */
22 FREE_FROZEN, /* Freeing to frozen slab */
23 FREE_ADD_PARTIAL, /* Freeing moves slab to partial list */
24 FREE_REMOVE_PARTIAL, /* Freeing removes last object */
25 ALLOC_FROM_PARTIAL, /* Cpu slab acquired from node partial list */
26 ALLOC_SLAB, /* Cpu slab acquired from page allocator */
27 ALLOC_REFILL, /* Refill cpu slab from slab freelist */
28 ALLOC_NODE_MISMATCH, /* Switching cpu slab */
29 FREE_SLAB, /* Slab freed to the page allocator */
30 CPUSLAB_FLUSH, /* Abandoning of the cpu slab */
31 DEACTIVATE_FULL, /* Cpu slab was full when deactivated */
32 DEACTIVATE_EMPTY, /* Cpu slab was empty when deactivated */
33 DEACTIVATE_TO_HEAD, /* Cpu slab was moved to the head of partials */
34 DEACTIVATE_TO_TAIL, /* Cpu slab was moved to the tail of partials */
35 DEACTIVATE_REMOTE_FREES,/* Slab contained remotely freed objects */
36 DEACTIVATE_BYPASS, /* Implicit deactivation */
37 ORDER_FALLBACK, /* Number of times fallback was necessary */
38 CMPXCHG_DOUBLE_CPU_FAIL,/* Failure of this_cpu_cmpxchg_double */
39 CMPXCHG_DOUBLE_FAIL, /* Number of times that cmpxchg double did not match */
40 CPU_PARTIAL_ALLOC, /* Used cpu partial on alloc */
41 CPU_PARTIAL_FREE, /* Refill cpu partial on free */
42 CPU_PARTIAL_NODE, /* Refill cpu partial from node partial */
43 CPU_PARTIAL_DRAIN, /* Drain cpu partial to node partial */
44 NR_SLUB_STAT_ITEMS };
46 struct kmem_cache_cpu {
47 void **freelist; /* Pointer to next available object */
48 unsigned long tid; /* Globally unique transaction id */
49 struct page *page; /* The slab from which we are allocating */
50 struct page *partial; /* Partially allocated frozen slabs */
51 #ifdef CONFIG_SLUB_STATS
52 unsigned stat[NR_SLUB_STAT_ITEMS];
53 #endif
54 };
56 struct kmem_cache_node {
57 spinlock_t list_lock; /* Protect partial list and nr_partial */
58 unsigned long nr_partial;
59 struct list_head partial;
60 #ifdef CONFIG_SLUB_DEBUG
61 atomic_long_t nr_slabs;
62 atomic_long_t total_objects;
63 struct list_head full;
64 #endif
65 };
67 /*
68 * Word size structure that can be atomically updated or read and that
69 * contains both the order and the number of objects that a slab of the
70 * given order would contain.
71 */
72 struct kmem_cache_order_objects {
73 unsigned long x;
74 };
76 /*
77 * Slab cache management.
78 */
79 struct kmem_cache {
80 struct kmem_cache_cpu __percpu *cpu_slab;
81 /* Used for retriving partial slabs etc */
82 unsigned long flags;
83 unsigned long min_partial;
84 int size; /* The size of an object including meta data */
85 int object_size; /* The size of an object without meta data */
86 int offset; /* Free pointer offset. */
87 int cpu_partial; /* Number of per cpu partial objects to keep around */
88 struct kmem_cache_order_objects oo;
90 /* Allocation and freeing of slabs */
91 struct kmem_cache_order_objects max;
92 struct kmem_cache_order_objects min;
93 gfp_t allocflags; /* gfp flags to use on each alloc */
94 int refcount; /* Refcount for slab cache destroy */
95 void (*ctor)(void *);
96 int inuse; /* Offset to metadata */
97 int align; /* Alignment */
98 int reserved; /* Reserved bytes at the end of slabs */
99 const char *name; /* Name (only for display!) */
100 struct list_head list; /* List of slab caches */
101 #ifdef CONFIG_SYSFS
102 struct kobject kobj; /* For sysfs */
103 #endif
104 #ifdef CONFIG_MEMCG_KMEM
105 struct memcg_cache_params *memcg_params;
106 int max_attr_size; /* for propagation, maximum size of a stored attr */
107 #endif
109 #ifdef CONFIG_NUMA
110 /*
111 * Defragmentation by allocating from a remote node.
112 */
113 int remote_node_defrag_ratio;
114 #endif
115 struct kmem_cache_node *node[MAX_NUMNODES];
116 };
118 /*
119 * Kmalloc subsystem.
120 */
121 #if defined(ARCH_DMA_MINALIGN) && ARCH_DMA_MINALIGN > 8
122 #define KMALLOC_MIN_SIZE ARCH_DMA_MINALIGN
123 #else
124 #define KMALLOC_MIN_SIZE 8
125 #endif
127 #define KMALLOC_SHIFT_LOW ilog2(KMALLOC_MIN_SIZE)
129 /*
130 * Maximum kmalloc object size handled by SLUB. Larger object allocations
131 * are passed through to the page allocator. The page allocator "fastpath"
132 * is relatively slow so we need this value sufficiently high so that
133 * performance critical objects are allocated through the SLUB fastpath.
134 *
135 * This should be dropped to PAGE_SIZE / 2 once the page allocator
136 * "fastpath" becomes competitive with the slab allocator fastpaths.
137 */
138 #define SLUB_MAX_SIZE (2 * PAGE_SIZE)
140 #define SLUB_PAGE_SHIFT (PAGE_SHIFT + 2)
142 #ifdef CONFIG_ZONE_DMA
143 #define SLUB_DMA __GFP_DMA
144 #else
145 /* Disable DMA functionality */
146 #define SLUB_DMA (__force gfp_t)0
147 #endif
149 /*
150 * We keep the general caches in an array of slab caches that are used for
151 * 2^x bytes of allocations.
152 */
153 extern struct kmem_cache *kmalloc_caches[SLUB_PAGE_SHIFT];
155 /*
156 * Sorry that the following has to be that ugly but some versions of GCC
157 * have trouble with constant propagation and loops.
158 */
159 static __always_inline int kmalloc_index(size_t size)
160 {
161 if (!size)
162 return 0;
164 if (size <= KMALLOC_MIN_SIZE)
165 return KMALLOC_SHIFT_LOW;
167 if (KMALLOC_MIN_SIZE <= 32 && size > 64 && size <= 96)
168 return 1;
169 if (KMALLOC_MIN_SIZE <= 64 && size > 128 && size <= 192)
170 return 2;
171 if (size <= 8) return 3;
172 if (size <= 16) return 4;
173 if (size <= 32) return 5;
174 if (size <= 64) return 6;
175 if (size <= 128) return 7;
176 if (size <= 256) return 8;
177 if (size <= 512) return 9;
178 if (size <= 1024) return 10;
179 if (size <= 2 * 1024) return 11;
180 if (size <= 4 * 1024) return 12;
181 /*
182 * The following is only needed to support architectures with a larger page
183 * size than 4k. We need to support 2 * PAGE_SIZE here. So for a 64k page
184 * size we would have to go up to 128k.
185 */
186 if (size <= 8 * 1024) return 13;
187 if (size <= 16 * 1024) return 14;
188 if (size <= 32 * 1024) return 15;
189 if (size <= 64 * 1024) return 16;
190 if (size <= 128 * 1024) return 17;
191 if (size <= 256 * 1024) return 18;
192 if (size <= 512 * 1024) return 19;
193 if (size <= 1024 * 1024) return 20;
194 if (size <= 2 * 1024 * 1024) return 21;
195 BUG();
196 return -1; /* Will never be reached */
198 /*
199 * What we really wanted to do and cannot do because of compiler issues is:
200 * int i;
201 * for (i = KMALLOC_SHIFT_LOW; i <= KMALLOC_SHIFT_HIGH; i++)
202 * if (size <= (1 << i))
203 * return i;
204 */
205 }
207 /*
208 * Find the slab cache for a given combination of allocation flags and size.
209 *
210 * This ought to end up with a global pointer to the right cache
211 * in kmalloc_caches.
212 */
213 static __always_inline struct kmem_cache *kmalloc_slab(size_t size)
214 {
215 int index = kmalloc_index(size);
217 if (index == 0)
218 return NULL;
220 return kmalloc_caches[index];
221 }
223 void *kmem_cache_alloc(struct kmem_cache *, gfp_t);
224 void *__kmalloc(size_t size, gfp_t flags);
226 static __always_inline void *
227 kmalloc_order(size_t size, gfp_t flags, unsigned int order)
228 {
229 void *ret;
231 flags |= (__GFP_COMP | __GFP_KMEMCG);
232 ret = (void *) __get_free_pages(flags, order);
233 kmemleak_alloc(ret, size, 1, flags);
234 return ret;
235 }
237 /**
238 * Calling this on allocated memory will check that the memory
239 * is expected to be in use, and print warnings if not.
240 */
241 #ifdef CONFIG_SLUB_DEBUG
242 extern bool verify_mem_not_deleted(const void *x);
243 #else
244 static inline bool verify_mem_not_deleted(const void *x)
245 {
246 return true;
247 }
248 #endif
250 #ifdef CONFIG_TRACING
251 extern void *
252 kmem_cache_alloc_trace(struct kmem_cache *s, gfp_t gfpflags, size_t size);
253 extern void *kmalloc_order_trace(size_t size, gfp_t flags, unsigned int order);
254 #else
255 static __always_inline void *
256 kmem_cache_alloc_trace(struct kmem_cache *s, gfp_t gfpflags, size_t size)
257 {
258 return kmem_cache_alloc(s, gfpflags);
259 }
261 static __always_inline void *
262 kmalloc_order_trace(size_t size, gfp_t flags, unsigned int order)
263 {
264 return kmalloc_order(size, flags, order);
265 }
266 #endif
268 static __always_inline void *kmalloc_large(size_t size, gfp_t flags)
269 {
270 unsigned int order = get_order(size);
271 return kmalloc_order_trace(size, flags, order);
272 }
274 static __always_inline void *kmalloc(size_t size, gfp_t flags)
275 {
276 if (__builtin_constant_p(size)) {
277 if (size > SLUB_MAX_SIZE)
278 return kmalloc_large(size, flags);
280 if (!(flags & SLUB_DMA)) {
281 struct kmem_cache *s = kmalloc_slab(size);
283 if (!s)
284 return ZERO_SIZE_PTR;
286 return kmem_cache_alloc_trace(s, flags, size);
287 }
288 }
289 return __kmalloc(size, flags);
290 }
292 #ifdef CONFIG_NUMA
293 void *__kmalloc_node(size_t size, gfp_t flags, int node);
294 void *kmem_cache_alloc_node(struct kmem_cache *, gfp_t flags, int node);
296 #ifdef CONFIG_TRACING
297 extern void *kmem_cache_alloc_node_trace(struct kmem_cache *s,
298 gfp_t gfpflags,
299 int node, size_t size);
300 #else
301 static __always_inline void *
302 kmem_cache_alloc_node_trace(struct kmem_cache *s,
303 gfp_t gfpflags,
304 int node, size_t size)
305 {
306 return kmem_cache_alloc_node(s, gfpflags, node);
307 }
308 #endif
310 static __always_inline void *kmalloc_node(size_t size, gfp_t flags, int node)
311 {
312 if (__builtin_constant_p(size) &&
313 size <= SLUB_MAX_SIZE && !(flags & SLUB_DMA)) {
314 struct kmem_cache *s = kmalloc_slab(size);
316 if (!s)
317 return ZERO_SIZE_PTR;
319 return kmem_cache_alloc_node_trace(s, flags, node, size);
320 }
321 return __kmalloc_node(size, flags, node);
322 }
323 #endif
325 #endif /* _LINUX_SLUB_DEF_H */