1 #ifndef _LINUX_SUSPEND_H
2 #define _LINUX_SUSPEND_H
4 #include <linux/swap.h>
5 #include <linux/notifier.h>
6 #include <linux/init.h>
7 #include <linux/pm.h>
8 #include <linux/mm.h>
9 #include <linux/freezer.h>
10 #include <asm/errno.h>
12 #ifdef CONFIG_VT
13 extern void pm_set_vt_switch(int);
14 #else
15 static inline void pm_set_vt_switch(int do_switch)
16 {
17 }
18 #endif
20 #ifdef CONFIG_VT_CONSOLE_SLEEP
21 extern int pm_prepare_console(void);
22 extern void pm_restore_console(void);
23 #else
24 static inline int pm_prepare_console(void)
25 {
26 return 0;
27 }
29 static inline void pm_restore_console(void)
30 {
31 }
32 #endif
34 typedef int __bitwise suspend_state_t;
36 #define PM_SUSPEND_ON ((__force suspend_state_t) 0)
37 #define PM_SUSPEND_FREEZE ((__force suspend_state_t) 1)
38 #define PM_SUSPEND_STANDBY ((__force suspend_state_t) 2)
39 #define PM_SUSPEND_MEM ((__force suspend_state_t) 3)
40 #define PM_SUSPEND_MIN PM_SUSPEND_FREEZE
41 #define PM_SUSPEND_MAX ((__force suspend_state_t) 4)
43 enum suspend_stat_step {
44 SUSPEND_FREEZE = 1,
45 SUSPEND_PREPARE,
46 SUSPEND_SUSPEND,
47 SUSPEND_SUSPEND_LATE,
48 SUSPEND_SUSPEND_NOIRQ,
49 SUSPEND_RESUME_NOIRQ,
50 SUSPEND_RESUME_EARLY,
51 SUSPEND_RESUME
52 };
54 struct suspend_stats {
55 int success;
56 int fail;
57 int failed_freeze;
58 int failed_prepare;
59 int failed_suspend;
60 int failed_suspend_late;
61 int failed_suspend_noirq;
62 int failed_resume;
63 int failed_resume_early;
64 int failed_resume_noirq;
65 #define REC_FAILED_NUM 2
66 int last_failed_dev;
67 char failed_devs[REC_FAILED_NUM][40];
68 int last_failed_errno;
69 int errno[REC_FAILED_NUM];
70 int last_failed_step;
71 enum suspend_stat_step failed_steps[REC_FAILED_NUM];
72 };
74 extern struct suspend_stats suspend_stats;
76 static inline void dpm_save_failed_dev(const char *name)
77 {
78 strlcpy(suspend_stats.failed_devs[suspend_stats.last_failed_dev],
79 name,
80 sizeof(suspend_stats.failed_devs[0]));
81 suspend_stats.last_failed_dev++;
82 suspend_stats.last_failed_dev %= REC_FAILED_NUM;
83 }
85 static inline void dpm_save_failed_errno(int err)
86 {
87 suspend_stats.errno[suspend_stats.last_failed_errno] = err;
88 suspend_stats.last_failed_errno++;
89 suspend_stats.last_failed_errno %= REC_FAILED_NUM;
90 }
92 static inline void dpm_save_failed_step(enum suspend_stat_step step)
93 {
94 suspend_stats.failed_steps[suspend_stats.last_failed_step] = step;
95 suspend_stats.last_failed_step++;
96 suspend_stats.last_failed_step %= REC_FAILED_NUM;
97 }
99 /**
100 * struct platform_suspend_ops - Callbacks for managing platform dependent
101 * system sleep states.
102 *
103 * @valid: Callback to determine if given system sleep state is supported by
104 * the platform.
105 * Valid (ie. supported) states are advertised in /sys/power/state. Note
106 * that it still may be impossible to enter given system sleep state if the
107 * conditions aren't right.
108 * There is the %suspend_valid_only_mem function available that can be
109 * assigned to this if the platform only supports mem sleep.
110 *
111 * @begin: Initialise a transition to given system sleep state.
112 * @begin() is executed right prior to suspending devices. The information
113 * conveyed to the platform code by @begin() should be disregarded by it as
114 * soon as @end() is executed. If @begin() fails (ie. returns nonzero),
115 * @prepare(), @enter() and @finish() will not be called by the PM core.
116 * This callback is optional. However, if it is implemented, the argument
117 * passed to @enter() is redundant and should be ignored.
118 *
119 * @prepare: Prepare the platform for entering the system sleep state indicated
120 * by @begin().
121 * @prepare() is called right after devices have been suspended (ie. the
122 * appropriate .suspend() method has been executed for each device) and
123 * before device drivers' late suspend callbacks are executed. It returns
124 * 0 on success or a negative error code otherwise, in which case the
125 * system cannot enter the desired sleep state (@prepare_late(), @enter(),
126 * and @wake() will not be called in that case).
127 *
128 * @prepare_late: Finish preparing the platform for entering the system sleep
129 * state indicated by @begin().
130 * @prepare_late is called before disabling nonboot CPUs and after
131 * device drivers' late suspend callbacks have been executed. It returns
132 * 0 on success or a negative error code otherwise, in which case the
133 * system cannot enter the desired sleep state (@enter() will not be
134 * executed).
135 *
136 * @enter: Enter the system sleep state indicated by @begin() or represented by
137 * the argument if @begin() is not implemented.
138 * This callback is mandatory. It returns 0 on success or a negative
139 * error code otherwise, in which case the system cannot enter the desired
140 * sleep state.
141 *
142 * @wake: Called when the system has just left a sleep state, right after
143 * the nonboot CPUs have been enabled and before device drivers' early
144 * resume callbacks are executed.
145 * This callback is optional, but should be implemented by the platforms
146 * that implement @prepare_late(). If implemented, it is always called
147 * after @prepare_late and @enter(), even if one of them fails.
148 *
149 * @finish: Finish wake-up of the platform.
150 * @finish is called right prior to calling device drivers' regular suspend
151 * callbacks.
152 * This callback is optional, but should be implemented by the platforms
153 * that implement @prepare(). If implemented, it is always called after
154 * @enter() and @wake(), even if any of them fails. It is executed after
155 * a failing @prepare.
156 *
157 * @suspend_again: Returns whether the system should suspend again (true) or
158 * not (false). If the platform wants to poll sensors or execute some
159 * code during suspended without invoking userspace and most of devices,
160 * suspend_again callback is the place assuming that periodic-wakeup or
161 * alarm-wakeup is already setup. This allows to execute some codes while
162 * being kept suspended in the view of userland and devices.
163 *
164 * @end: Called by the PM core right after resuming devices, to indicate to
165 * the platform that the system has returned to the working state or
166 * the transition to the sleep state has been aborted.
167 * This callback is optional, but should be implemented by the platforms
168 * that implement @begin(). Accordingly, platforms implementing @begin()
169 * should also provide a @end() which cleans up transitions aborted before
170 * @enter().
171 *
172 * @recover: Recover the platform from a suspend failure.
173 * Called by the PM core if the suspending of devices fails.
174 * This callback is optional and should only be implemented by platforms
175 * which require special recovery actions in that situation.
176 */
177 struct platform_suspend_ops {
178 int (*valid)(suspend_state_t state);
179 int (*begin)(suspend_state_t state);
180 int (*prepare)(void);
181 int (*prepare_late)(void);
182 int (*enter)(suspend_state_t state);
183 void (*wake)(void);
184 void (*finish)(void);
185 bool (*suspend_again)(void);
186 void (*end)(void);
187 void (*recover)(void);
188 };
190 #ifdef CONFIG_SUSPEND
191 /**
192 * suspend_set_ops - set platform dependent suspend operations
193 * @ops: The new suspend operations to set.
194 */
195 extern void suspend_set_ops(const struct platform_suspend_ops *ops);
196 extern int suspend_valid_only_mem(suspend_state_t state);
197 extern void freeze_wake(void);
199 /**
200 * arch_suspend_disable_irqs - disable IRQs for suspend
201 *
202 * Disables IRQs (in the default case). This is a weak symbol in the common
203 * code and thus allows architectures to override it if more needs to be
204 * done. Not called for suspend to disk.
205 */
206 extern void arch_suspend_disable_irqs(void);
208 /**
209 * arch_suspend_enable_irqs - enable IRQs after suspend
210 *
211 * Enables IRQs (in the default case). This is a weak symbol in the common
212 * code and thus allows architectures to override it if more needs to be
213 * done. Not called for suspend to disk.
214 */
215 extern void arch_suspend_enable_irqs(void);
217 extern int pm_suspend(suspend_state_t state);
218 #else /* !CONFIG_SUSPEND */
219 #define suspend_valid_only_mem NULL
221 static inline void suspend_set_ops(const struct platform_suspend_ops *ops) {}
222 static inline int pm_suspend(suspend_state_t state) { return -ENOSYS; }
223 static inline void freeze_wake(void) {}
224 #endif /* !CONFIG_SUSPEND */
226 /* struct pbe is used for creating lists of pages that should be restored
227 * atomically during the resume from disk, because the page frames they have
228 * occupied before the suspend are in use.
229 */
230 struct pbe {
231 void *address; /* address of the copy */
232 void *orig_address; /* original address of a page */
233 struct pbe *next;
234 };
236 /* mm/page_alloc.c */
237 extern void mark_free_pages(struct zone *zone);
239 /**
240 * struct platform_hibernation_ops - hibernation platform support
241 *
242 * The methods in this structure allow a platform to carry out special
243 * operations required by it during a hibernation transition.
244 *
245 * All the methods below, except for @recover(), must be implemented.
246 *
247 * @begin: Tell the platform driver that we're starting hibernation.
248 * Called right after shrinking memory and before freezing devices.
249 *
250 * @end: Called by the PM core right after resuming devices, to indicate to
251 * the platform that the system has returned to the working state.
252 *
253 * @pre_snapshot: Prepare the platform for creating the hibernation image.
254 * Called right after devices have been frozen and before the nonboot
255 * CPUs are disabled (runs with IRQs on).
256 *
257 * @finish: Restore the previous state of the platform after the hibernation
258 * image has been created *or* put the platform into the normal operation
259 * mode after the hibernation (the same method is executed in both cases).
260 * Called right after the nonboot CPUs have been enabled and before
261 * thawing devices (runs with IRQs on).
262 *
263 * @prepare: Prepare the platform for entering the low power state.
264 * Called right after the hibernation image has been saved and before
265 * devices are prepared for entering the low power state.
266 *
267 * @enter: Put the system into the low power state after the hibernation image
268 * has been saved to disk.
269 * Called after the nonboot CPUs have been disabled and all of the low
270 * level devices have been shut down (runs with IRQs off).
271 *
272 * @leave: Perform the first stage of the cleanup after the system sleep state
273 * indicated by @set_target() has been left.
274 * Called right after the control has been passed from the boot kernel to
275 * the image kernel, before the nonboot CPUs are enabled and before devices
276 * are resumed. Executed with interrupts disabled.
277 *
278 * @pre_restore: Prepare system for the restoration from a hibernation image.
279 * Called right after devices have been frozen and before the nonboot
280 * CPUs are disabled (runs with IRQs on).
281 *
282 * @restore_cleanup: Clean up after a failing image restoration.
283 * Called right after the nonboot CPUs have been enabled and before
284 * thawing devices (runs with IRQs on).
285 *
286 * @recover: Recover the platform from a failure to suspend devices.
287 * Called by the PM core if the suspending of devices during hibernation
288 * fails. This callback is optional and should only be implemented by
289 * platforms which require special recovery actions in that situation.
290 */
291 struct platform_hibernation_ops {
292 int (*begin)(void);
293 void (*end)(void);
294 int (*pre_snapshot)(void);
295 void (*finish)(void);
296 int (*prepare)(void);
297 int (*enter)(void);
298 void (*leave)(void);
299 int (*pre_restore)(void);
300 void (*restore_cleanup)(void);
301 void (*recover)(void);
302 };
304 #ifdef CONFIG_HIBERNATION
305 /* kernel/power/snapshot.c */
306 extern void __register_nosave_region(unsigned long b, unsigned long e, int km);
307 static inline void __init register_nosave_region(unsigned long b, unsigned long e)
308 {
309 __register_nosave_region(b, e, 0);
310 }
311 static inline void __init register_nosave_region_late(unsigned long b, unsigned long e)
312 {
313 __register_nosave_region(b, e, 1);
314 }
315 extern int swsusp_page_is_forbidden(struct page *);
316 extern void swsusp_set_page_free(struct page *);
317 extern void swsusp_unset_page_free(struct page *);
318 extern unsigned long get_safe_page(gfp_t gfp_mask);
320 extern void hibernation_set_ops(const struct platform_hibernation_ops *ops);
321 extern int hibernate(void);
322 extern bool system_entering_hibernation(void);
323 #else /* CONFIG_HIBERNATION */
324 static inline void register_nosave_region(unsigned long b, unsigned long e) {}
325 static inline void register_nosave_region_late(unsigned long b, unsigned long e) {}
326 static inline int swsusp_page_is_forbidden(struct page *p) { return 0; }
327 static inline void swsusp_set_page_free(struct page *p) {}
328 static inline void swsusp_unset_page_free(struct page *p) {}
330 static inline void hibernation_set_ops(const struct platform_hibernation_ops *ops) {}
331 static inline int hibernate(void) { return -ENOSYS; }
332 static inline bool system_entering_hibernation(void) { return false; }
333 #endif /* CONFIG_HIBERNATION */
335 /* Hibernation and suspend events */
336 #define PM_HIBERNATION_PREPARE 0x0001 /* Going to hibernate */
337 #define PM_POST_HIBERNATION 0x0002 /* Hibernation finished */
338 #define PM_SUSPEND_PREPARE 0x0003 /* Going to suspend the system */
339 #define PM_POST_SUSPEND 0x0004 /* Suspend finished */
340 #define PM_RESTORE_PREPARE 0x0005 /* Going to restore a saved image */
341 #define PM_POST_RESTORE 0x0006 /* Restore failed */
343 extern struct mutex pm_mutex;
345 #ifdef CONFIG_PM_SLEEP
346 void save_processor_state(void);
347 void restore_processor_state(void);
349 /* kernel/power/main.c */
350 extern int register_pm_notifier(struct notifier_block *nb);
351 extern int unregister_pm_notifier(struct notifier_block *nb);
353 #define pm_notifier(fn, pri) { \
354 static struct notifier_block fn##_nb = \
355 { .notifier_call = fn, .priority = pri }; \
356 register_pm_notifier(&fn##_nb); \
357 }
359 /* drivers/base/power/wakeup.c */
360 extern bool events_check_enabled;
362 extern bool pm_wakeup_pending(void);
363 extern bool pm_get_wakeup_count(unsigned int *count, bool block);
364 extern bool pm_save_wakeup_count(unsigned int count);
365 extern void pm_wakep_autosleep_enabled(bool set);
366 extern void pm_print_active_wakeup_sources(void);
367 extern void pm_get_active_wakeup_sources(char *pending_sources, size_t max);
369 static inline void lock_system_sleep(void)
370 {
371 current->flags |= PF_FREEZER_SKIP;
372 mutex_lock(&pm_mutex);
373 }
375 static inline void unlock_system_sleep(void)
376 {
377 /*
378 * Don't use freezer_count() because we don't want the call to
379 * try_to_freeze() here.
380 *
381 * Reason:
382 * Fundamentally, we just don't need it, because freezing condition
383 * doesn't come into effect until we release the pm_mutex lock,
384 * since the freezer always works with pm_mutex held.
385 *
386 * More importantly, in the case of hibernation,
387 * unlock_system_sleep() gets called in snapshot_read() and
388 * snapshot_write() when the freezing condition is still in effect.
389 * Which means, if we use try_to_freeze() here, it would make them
390 * enter the refrigerator, thus causing hibernation to lockup.
391 */
392 current->flags &= ~PF_FREEZER_SKIP;
393 mutex_unlock(&pm_mutex);
394 }
396 #else /* !CONFIG_PM_SLEEP */
398 static inline int register_pm_notifier(struct notifier_block *nb)
399 {
400 return 0;
401 }
403 static inline int unregister_pm_notifier(struct notifier_block *nb)
404 {
405 return 0;
406 }
408 #define pm_notifier(fn, pri) do { (void)(fn); } while (0)
410 static inline bool pm_wakeup_pending(void) { return false; }
412 static inline void lock_system_sleep(void) {}
413 static inline void unlock_system_sleep(void) {}
415 #endif /* !CONFIG_PM_SLEEP */
417 #ifdef CONFIG_PM_SLEEP_DEBUG
418 extern bool pm_print_times_enabled;
419 #else
420 #define pm_print_times_enabled (false)
421 #endif
423 #ifdef CONFIG_PM_AUTOSLEEP
425 /* kernel/power/autosleep.c */
426 void queue_up_suspend_work(void);
428 #else /* !CONFIG_PM_AUTOSLEEP */
430 static inline void queue_up_suspend_work(void) {}
432 #endif /* !CONFIG_PM_AUTOSLEEP */
434 #ifdef CONFIG_ARCH_SAVE_PAGE_KEYS
435 /*
436 * The ARCH_SAVE_PAGE_KEYS functions can be used by an architecture
437 * to save/restore additional information to/from the array of page
438 * frame numbers in the hibernation image. For s390 this is used to
439 * save and restore the storage key for each page that is included
440 * in the hibernation image.
441 */
442 unsigned long page_key_additional_pages(unsigned long pages);
443 int page_key_alloc(unsigned long pages);
444 void page_key_free(void);
445 void page_key_read(unsigned long *pfn);
446 void page_key_memorize(unsigned long *pfn);
447 void page_key_write(void *address);
449 #else /* !CONFIG_ARCH_SAVE_PAGE_KEYS */
451 static inline unsigned long page_key_additional_pages(unsigned long pages)
452 {
453 return 0;
454 }
456 static inline int page_key_alloc(unsigned long pages)
457 {
458 return 0;
459 }
461 static inline void page_key_free(void) {}
462 static inline void page_key_read(unsigned long *pfn) {}
463 static inline void page_key_memorize(unsigned long *pfn) {}
464 static inline void page_key_write(void *address) {}
466 #endif /* !CONFIG_ARCH_SAVE_PAGE_KEYS */
468 #endif /* _LINUX_SUSPEND_H */