1 /*
2 * thermal.h ($Revision: 0 $)
3 *
4 * Copyright (C) 2008 Intel Corp
5 * Copyright (C) 2008 Zhang Rui <rui.zhang@intel.com>
6 * Copyright (C) 2008 Sujith Thomas <sujith.thomas@intel.com>
7 *
8 * ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
9 * This program is free software; you can redistribute it and/or modify
10 * it under the terms of the GNU General Public License as published by
11 * the Free Software Foundation; version 2 of the License.
12 *
13 * This program is distributed in the hope that it will be useful, but
14 * WITHOUT ANY WARRANTY; without even the implied warranty of
15 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
16 * General Public License for more details.
17 *
18 * You should have received a copy of the GNU General Public License along
19 * with this program; if not, write to the Free Software Foundation, Inc.,
20 * 59 Temple Place, Suite 330, Boston, MA 02111-1307 USA.
21 *
22 * ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
23 */
25 #ifndef __THERMAL_H__
26 #define __THERMAL_H__
28 #include <linux/idr.h>
29 #include <linux/device.h>
30 #include <linux/workqueue.h>
32 #define THERMAL_TRIPS_NONE -1
33 #define THERMAL_MAX_TRIPS 12
34 #define THERMAL_NAME_LENGTH 20
36 /* No upper/lower limit requirement */
37 #define THERMAL_NO_LIMIT -1UL
39 /* Unit conversion macros */
40 #define KELVIN_TO_CELSIUS(t) (long)(((long)t-2732 >= 0) ? \
41 ((long)t-2732+5)/10 : ((long)t-2732-5)/10)
42 #define CELSIUS_TO_KELVIN(t) ((t)*10+2732)
44 /* Adding event notification support elements */
45 #define THERMAL_GENL_FAMILY_NAME "thermal_event"
46 #define THERMAL_GENL_VERSION 0x01
47 #define THERMAL_GENL_MCAST_GROUP_NAME "thermal_mc_group"
49 /* Default Thermal Governor */
50 #if defined(CONFIG_THERMAL_DEFAULT_GOV_STEP_WISE)
51 #define DEFAULT_THERMAL_GOVERNOR "step_wise"
52 #elif defined(CONFIG_THERMAL_DEFAULT_GOV_FAIR_SHARE)
53 #define DEFAULT_THERMAL_GOVERNOR "fair_share"
54 #elif defined(CONFIG_THERMAL_DEFAULT_GOV_USER_SPACE)
55 #define DEFAULT_THERMAL_GOVERNOR "user_space"
56 #endif
58 struct thermal_zone_device;
59 struct thermal_cooling_device;
61 enum thermal_device_mode {
62 THERMAL_DEVICE_DISABLED = 0,
63 THERMAL_DEVICE_ENABLED,
64 };
66 enum thermal_trip_type {
67 THERMAL_TRIP_ACTIVE = 0,
68 THERMAL_TRIP_PASSIVE,
69 THERMAL_TRIP_HOT,
70 THERMAL_TRIP_CRITICAL,
71 };
73 enum thermal_trend {
74 THERMAL_TREND_STABLE, /* temperature is stable */
75 THERMAL_TREND_RAISING, /* temperature is raising */
76 THERMAL_TREND_DROPPING, /* temperature is dropping */
77 THERMAL_TREND_RAISE_FULL, /* apply highest cooling action */
78 THERMAL_TREND_DROP_FULL, /* apply lowest cooling action */
79 };
81 /* Events supported by Thermal Netlink */
82 enum events {
83 THERMAL_AUX0,
84 THERMAL_AUX1,
85 THERMAL_CRITICAL,
86 THERMAL_DEV_FAULT,
87 };
89 /* attributes of thermal_genl_family */
90 enum {
91 THERMAL_GENL_ATTR_UNSPEC,
92 THERMAL_GENL_ATTR_EVENT,
93 __THERMAL_GENL_ATTR_MAX,
94 };
95 #define THERMAL_GENL_ATTR_MAX (__THERMAL_GENL_ATTR_MAX - 1)
97 /* commands supported by the thermal_genl_family */
98 enum {
99 THERMAL_GENL_CMD_UNSPEC,
100 THERMAL_GENL_CMD_EVENT,
101 __THERMAL_GENL_CMD_MAX,
102 };
103 #define THERMAL_GENL_CMD_MAX (__THERMAL_GENL_CMD_MAX - 1)
105 struct thermal_zone_device_ops {
106 int (*bind) (struct thermal_zone_device *,
107 struct thermal_cooling_device *);
108 int (*unbind) (struct thermal_zone_device *,
109 struct thermal_cooling_device *);
110 int (*get_temp) (struct thermal_zone_device *, unsigned long *);
111 int (*get_mode) (struct thermal_zone_device *,
112 enum thermal_device_mode *);
113 int (*set_mode) (struct thermal_zone_device *,
114 enum thermal_device_mode);
115 int (*get_trip_type) (struct thermal_zone_device *, int,
116 enum thermal_trip_type *);
117 int (*get_trip_temp) (struct thermal_zone_device *, int,
118 unsigned long *);
119 int (*set_trip_temp) (struct thermal_zone_device *, int,
120 unsigned long);
121 int (*get_trip_hyst) (struct thermal_zone_device *, int,
122 unsigned long *);
123 int (*set_trip_hyst) (struct thermal_zone_device *, int,
124 unsigned long);
125 int (*get_crit_temp) (struct thermal_zone_device *, unsigned long *);
126 int (*set_emul_temp) (struct thermal_zone_device *, unsigned long);
127 int (*get_trend) (struct thermal_zone_device *, int,
128 enum thermal_trend *);
129 int (*notify) (struct thermal_zone_device *, int,
130 enum thermal_trip_type);
131 };
133 struct thermal_cooling_device_ops {
134 int (*get_max_state) (struct thermal_cooling_device *, unsigned long *);
135 int (*get_cur_state) (struct thermal_cooling_device *, unsigned long *);
136 int (*set_cur_state) (struct thermal_cooling_device *, unsigned long);
137 };
139 struct thermal_cooling_device {
140 int id;
141 char type[THERMAL_NAME_LENGTH];
142 struct device device;
143 void *devdata;
144 const struct thermal_cooling_device_ops *ops;
145 bool updated; /* true if the cooling device does not need update */
146 struct mutex lock; /* protect thermal_instances list */
147 struct list_head thermal_instances;
148 struct list_head node;
149 };
151 struct thermal_attr {
152 struct device_attribute attr;
153 char name[THERMAL_NAME_LENGTH];
154 };
156 struct thermal_zone_device {
157 int id;
158 char type[THERMAL_NAME_LENGTH];
159 struct device device;
160 struct thermal_attr *trip_temp_attrs;
161 struct thermal_attr *trip_type_attrs;
162 struct thermal_attr *trip_hyst_attrs;
163 void *devdata;
164 int trips;
165 int passive_delay;
166 int polling_delay;
167 int temperature;
168 int last_temperature;
169 int emul_temperature;
170 int passive;
171 unsigned int forced_passive;
172 const struct thermal_zone_device_ops *ops;
173 const struct thermal_zone_params *tzp;
174 struct thermal_governor *governor;
175 struct list_head thermal_instances;
176 struct idr idr;
177 struct mutex lock; /* protect thermal_instances list */
178 struct list_head node;
179 struct delayed_work poll_queue;
180 };
182 /* Structure that holds thermal governor information */
183 struct thermal_governor {
184 char name[THERMAL_NAME_LENGTH];
185 int (*throttle)(struct thermal_zone_device *tz, int trip);
186 struct list_head governor_list;
187 struct module *owner;
188 };
190 /* Structure that holds binding parameters for a zone */
191 struct thermal_bind_params {
192 struct thermal_cooling_device *cdev;
194 /*
195 * This is a measure of 'how effectively these devices can
196 * cool 'this' thermal zone. The shall be determined by platform
197 * characterization. This is on a 'percentage' scale.
198 * See Documentation/thermal/sysfs-api.txt for more information.
199 */
200 int weight;
202 /*
203 * This is a bit mask that gives the binding relation between this
204 * thermal zone and cdev, for a particular trip point.
205 * See Documentation/thermal/sysfs-api.txt for more information.
206 */
207 int trip_mask;
208 int (*match) (struct thermal_zone_device *tz,
209 struct thermal_cooling_device *cdev);
210 };
212 /* Structure to define Thermal Zone parameters */
213 struct thermal_zone_params {
214 char governor_name[THERMAL_NAME_LENGTH];
215 int num_tbps; /* Number of tbp entries */
216 struct thermal_bind_params *tbp;
217 };
219 struct thermal_genl_event {
220 u32 orig;
221 enum events event;
222 };
224 /* Function declarations */
225 struct thermal_zone_device *thermal_zone_device_register(const char *, int, int,
226 void *, const struct thermal_zone_device_ops *,
227 const struct thermal_zone_params *, int, int);
228 void thermal_zone_device_unregister(struct thermal_zone_device *);
230 int thermal_zone_bind_cooling_device(struct thermal_zone_device *, int,
231 struct thermal_cooling_device *,
232 unsigned long, unsigned long);
233 int thermal_zone_unbind_cooling_device(struct thermal_zone_device *, int,
234 struct thermal_cooling_device *);
235 void thermal_zone_device_update(struct thermal_zone_device *);
237 struct thermal_cooling_device *thermal_cooling_device_register(char *, void *,
238 const struct thermal_cooling_device_ops *);
239 void thermal_cooling_device_unregister(struct thermal_cooling_device *);
240 struct thermal_zone_device *thermal_zone_get_zone_by_name(const char *name);
242 int get_tz_trend(struct thermal_zone_device *, int);
243 struct thermal_instance *get_thermal_instance(struct thermal_zone_device *,
244 struct thermal_cooling_device *, int);
245 void thermal_cdev_update(struct thermal_cooling_device *);
246 void notify_thermal_framework(struct thermal_zone_device *, int);
248 int thermal_register_governor(struct thermal_governor *);
249 void thermal_unregister_governor(struct thermal_governor *);
251 #ifdef CONFIG_NET
252 extern int thermal_generate_netlink_event(struct thermal_zone_device *tz,
253 enum events event);
254 #else
255 static int thermal_generate_netlink_event(struct thermal_zone_device *tz,
256 enum events event)
257 {
258 return 0;
259 }
260 #endif
262 #endif /* __THERMAL_H__ */