]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/blob - include/linux/timb_gpio.h
Merge branch 'p-ti-linux-3.8.y' into p-ti-android-3.8.y
[android-sdk/kernel-video.git] / include / linux / timb_gpio.h
1 /*
2  * timb_gpio.h timberdale FPGA GPIO driver, platform data definition
3  * Copyright (c) 2009 Intel Corporation
4  *
5  * This program is free software; you can redistribute it and/or modify
6  * it under the terms of the GNU General Public License version 2 as
7  * published by the Free Software Foundation.
8  *
9  * This program is distributed in the hope that it will be useful,
10  * but WITHOUT ANY WARRANTY; without even the implied warranty of
11  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
12  * GNU General Public License for more details.
13  *
14  * You should have received a copy of the GNU General Public License
15  * along with this program; if not, write to the Free Software
16  * Foundation, Inc., 675 Mass Ave, Cambridge, MA 02139, USA.
17  */
19 #ifndef _LINUX_TIMB_GPIO_H
20 #define _LINUX_TIMB_GPIO_H
22 /**
23  * struct timbgpio_platform_data - Platform data of the Timberdale GPIO driver
24  * @gpio_base           The number of the first GPIO pin, set to -1 for
25  *                      dynamic number allocation.
26  * @nr_pins             Number of pins that is supported by the hardware (1-32)
27  * @irq_base            If IRQ is supported by the hardware, this is the base
28  *                      number of IRQ:s. One IRQ per pin will be used. Set to
29  *                      -1 if IRQ:s is not supported.
30  */
31 struct timbgpio_platform_data {
32         int gpio_base;
33         int nr_pins;
34         int irq_base;
35 };
37 #endif