]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/blob - include/linux/timex.h
Merge branch 'p-ti-linux-3.8.y' into p-ti-android-3.8.y
[android-sdk/kernel-video.git] / include / linux / timex.h
1 /*****************************************************************************
2  *                                                                           *
3  * Copyright (c) David L. Mills 1993                                         *
4  *                                                                           *
5  * Permission to use, copy, modify, and distribute this software and its     *
6  * documentation for any purpose and without fee is hereby granted, provided *
7  * that the above copyright notice appears in all copies and that both the   *
8  * copyright notice and this permission notice appear in supporting          *
9  * documentation, and that the name University of Delaware not be used in    *
10  * advertising or publicity pertaining to distribution of the software       *
11  * without specific, written prior permission.  The University of Delaware   *
12  * makes no representations about the suitability this software for any      *
13  * purpose.  It is provided "as is" without express or implied warranty.     *
14  *                                                                           *
15  *****************************************************************************/
17 /*
18  * Modification history timex.h
19  *
20  * 29 Dec 97    Russell King
21  *      Moved CLOCK_TICK_RATE, CLOCK_TICK_FACTOR and FINETUNE to asm/timex.h
22  *      for ARM machines
23  *
24  *  9 Jan 97    Adrian Sun
25  *      Shifted LATCH define to allow access to alpha machines.
26  *
27  * 26 Sep 94    David L. Mills
28  *      Added defines for hybrid phase/frequency-lock loop.
29  *
30  * 19 Mar 94    David L. Mills
31  *      Moved defines from kernel routines to header file and added new
32  *      defines for PPS phase-lock loop.
33  *
34  * 20 Feb 94    David L. Mills
35  *      Revised status codes and structures for external clock and PPS
36  *      signal discipline.
37  *
38  * 28 Nov 93    David L. Mills
39  *      Adjusted parameters to improve stability and increase poll
40  *      interval.
41  *
42  * 17 Sep 93    David L. Mills
43  *      Created file $NTP/include/sys/timex.h
44  * 07 Oct 93    Torsten Duwe
45  *      Derived linux/timex.h
46  * 1995-08-13    Torsten Duwe
47  *      kernel PLL updated to 1994-12-13 specs (rfc-1589)
48  * 1997-08-30    Ulrich Windl
49  *      Added new constant NTP_PHASE_LIMIT
50  * 2004-08-12    Christoph Lameter
51  *      Reworked time interpolation logic
52  */
53 #ifndef _LINUX_TIMEX_H
54 #define _LINUX_TIMEX_H
56 #include <uapi/linux/timex.h>
58 #define ADJ_ADJTIME             0x8000  /* switch between adjtime/adjtimex modes */
59 #define ADJ_OFFSET_SINGLESHOT   0x0001  /* old-fashioned adjtime */
60 #define ADJ_OFFSET_READONLY     0x2000  /* read-only adjtime */
61 #include <linux/compiler.h>
62 #include <linux/types.h>
63 #include <linux/param.h>
65 #include <asm/timex.h>
67 /*
68  * SHIFT_PLL is used as a dampening factor to define how much we
69  * adjust the frequency correction for a given offset in PLL mode.
70  * It also used in dampening the offset correction, to define how
71  * much of the current value in time_offset we correct for each
72  * second. Changing this value changes the stiffness of the ntp
73  * adjustment code. A lower value makes it more flexible, reducing
74  * NTP convergence time. A higher value makes it stiffer, increasing
75  * convergence time, but making the clock more stable.
76  *
77  * In David Mills' nanokernel reference implementation SHIFT_PLL is 4.
78  * However this seems to increase convergence time much too long.
79  *
80  * https://lists.ntp.org/pipermail/hackers/2008-January/003487.html
81  *
82  * In the above mailing list discussion, it seems the value of 4
83  * was appropriate for other Unix systems with HZ=100, and that
84  * SHIFT_PLL should be decreased as HZ increases. However, Linux's
85  * clock steering implementation is HZ independent.
86  *
87  * Through experimentation, a SHIFT_PLL value of 2 was found to allow
88  * for fast convergence (very similar to the NTPv3 code used prior to
89  * v2.6.19), with good clock stability.
90  *
91  *
92  * SHIFT_FLL is used as a dampening factor to define how much we
93  * adjust the frequency correction for a given offset in FLL mode.
94  * In David Mills' nanokernel reference implementation SHIFT_FLL is 2.
95  *
96  * MAXTC establishes the maximum time constant of the PLL.
97  */
98 #define SHIFT_PLL       2       /* PLL frequency factor (shift) */
99 #define SHIFT_FLL       2       /* FLL frequency factor (shift) */
100 #define MAXTC           10      /* maximum time constant (shift) */
102 /*
103  * SHIFT_USEC defines the scaling (shift) of the time_freq and
104  * time_tolerance variables, which represent the current frequency
105  * offset and maximum frequency tolerance.
106  */
107 #define SHIFT_USEC 16           /* frequency offset scale (shift) */
108 #define PPM_SCALE ((s64)NSEC_PER_USEC << (NTP_SCALE_SHIFT - SHIFT_USEC))
109 #define PPM_SCALE_INV_SHIFT 19
110 #define PPM_SCALE_INV ((1LL << (PPM_SCALE_INV_SHIFT + NTP_SCALE_SHIFT)) / \
111                        PPM_SCALE + 1)
113 #define MAXPHASE 500000000L     /* max phase error (ns) */
114 #define MAXFREQ 500000          /* max frequency error (ns/s) */
115 #define MAXFREQ_SCALED ((s64)MAXFREQ << NTP_SCALE_SHIFT)
116 #define MINSEC 256              /* min interval between updates (s) */
117 #define MAXSEC 2048             /* max interval between updates (s) */
118 #define NTP_PHASE_LIMIT ((MAXPHASE / NSEC_PER_USEC) << 5) /* beyond max. dispersion */
120 /*
121  * kernel variables
122  * Note: maximum error = NTP synch distance = dispersion + delay / 2;
123  * estimated error = NTP dispersion.
124  */
125 extern unsigned long tick_usec;         /* USER_HZ period (usec) */
126 extern unsigned long tick_nsec;         /* SHIFTED_HZ period (nsec) */
128 extern void ntp_init(void);
129 extern void ntp_clear(void);
131 /* Required to safely shift negative values */
132 #define shift_right(x, s) ({    \
133         __typeof__(x) __x = (x);        \
134         __typeof__(s) __s = (s);        \
135         __x < 0 ? -(-__x >> __s) : __x >> __s;  \
136 })
138 #define NTP_SCALE_SHIFT         32
140 #define NTP_INTERVAL_FREQ  (HZ)
141 #define NTP_INTERVAL_LENGTH (NSEC_PER_SEC/NTP_INTERVAL_FREQ)
143 /* Returns how long ticks are at present, in ns / 2^NTP_SCALE_SHIFT. */
144 extern u64 ntp_tick_length(void);
146 extern int second_overflow(unsigned long secs);
147 extern int do_adjtimex(struct timex *);
148 extern void hardpps(const struct timespec *, const struct timespec *);
150 int read_current_timer(unsigned long *timer_val);
152 /* The clock frequency of the i8253/i8254 PIT */
153 #define PIT_TICK_RATE 1193182ul
155 #endif /* LINUX_TIMEX_H */