1 #ifndef _LINUX_TTY_LDISC_H
2 #define _LINUX_TTY_LDISC_H
4 /*
5 * This structure defines the interface between the tty line discipline
6 * implementation and the tty routines. The following routines can be
7 * defined; unless noted otherwise, they are optional, and can be
8 * filled in with a null pointer.
9 *
10 * int (*open)(struct tty_struct *);
11 *
12 * This function is called when the line discipline is associated
13 * with the tty. The line discipline can use this as an
14 * opportunity to initialize any state needed by the ldisc routines.
15 *
16 * void (*close)(struct tty_struct *);
17 *
18 * This function is called when the line discipline is being
19 * shutdown, either because the tty is being closed or because
20 * the tty is being changed to use a new line discipline
21 *
22 * void (*flush_buffer)(struct tty_struct *tty);
23 *
24 * This function instructs the line discipline to clear its
25 * buffers of any input characters it may have queued to be
26 * delivered to the user mode process.
27 *
28 * ssize_t (*chars_in_buffer)(struct tty_struct *tty);
29 *
30 * This function returns the number of input characters the line
31 * discipline may have queued up to be delivered to the user mode
32 * process.
33 *
34 * ssize_t (*read)(struct tty_struct * tty, struct file * file,
35 * unsigned char * buf, size_t nr);
36 *
37 * This function is called when the user requests to read from
38 * the tty. The line discipline will return whatever characters
39 * it has buffered up for the user. If this function is not
40 * defined, the user will receive an EIO error.
41 *
42 * ssize_t (*write)(struct tty_struct * tty, struct file * file,
43 * const unsigned char * buf, size_t nr);
44 *
45 * This function is called when the user requests to write to the
46 * tty. The line discipline will deliver the characters to the
47 * low-level tty device for transmission, optionally performing
48 * some processing on the characters first. If this function is
49 * not defined, the user will receive an EIO error.
50 *
51 * int (*ioctl)(struct tty_struct * tty, struct file * file,
52 * unsigned int cmd, unsigned long arg);
53 *
54 * This function is called when the user requests an ioctl which
55 * is not handled by the tty layer or the low-level tty driver.
56 * It is intended for ioctls which affect line discpline
57 * operation. Note that the search order for ioctls is (1) tty
58 * layer, (2) tty low-level driver, (3) line discpline. So a
59 * low-level driver can "grab" an ioctl request before the line
60 * discpline has a chance to see it.
61 *
62 * long (*compat_ioctl)(struct tty_struct * tty, struct file * file,
63 * unsigned int cmd, unsigned long arg);
64 *
65 * Process ioctl calls from 32-bit process on 64-bit system
66 *
67 * void (*set_termios)(struct tty_struct *tty, struct ktermios * old);
68 *
69 * This function notifies the line discpline that a change has
70 * been made to the termios structure.
71 *
72 * int (*poll)(struct tty_struct * tty, struct file * file,
73 * poll_table *wait);
74 *
75 * This function is called when a user attempts to select/poll on a
76 * tty device. It is solely the responsibility of the line
77 * discipline to handle poll requests.
78 *
79 * void (*receive_buf)(struct tty_struct *, const unsigned char *cp,
80 * char *fp, int count);
81 *
82 * This function is called by the low-level tty driver to send
83 * characters received by the hardware to the line discpline for
84 * processing. <cp> is a pointer to the buffer of input
85 * character received by the device. <fp> is a pointer to a
86 * pointer of flag bytes which indicate whether a character was
87 * received with a parity error, etc.
88 *
89 * void (*write_wakeup)(struct tty_struct *);
90 *
91 * This function is called by the low-level tty driver to signal
92 * that line discpline should try to send more characters to the
93 * low-level driver for transmission. If the line discpline does
94 * not have any more data to send, it can just return.
95 *
96 * int (*hangup)(struct tty_struct *)
97 *
98 * Called on a hangup. Tells the discipline that it should
99 * cease I/O to the tty driver. Can sleep. The driver should
100 * seek to perform this action quickly but should wait until
101 * any pending driver I/O is completed.
102 *
103 * void (*dcd_change)(struct tty_struct *tty, unsigned int status,
104 * struct pps_event_time *ts)
105 *
106 * Tells the discipline that the DCD pin has changed its status and
107 * the relative timestamp. Pointer ts cannot be NULL.
108 */
110 #include <linux/fs.h>
111 #include <linux/wait.h>
112 #include <linux/pps_kernel.h>
113 #include <linux/wait.h>
115 struct tty_ldisc_ops {
116 int magic;
117 char *name;
118 int num;
119 int flags;
121 /*
122 * The following routines are called from above.
123 */
124 int (*open)(struct tty_struct *);
125 void (*close)(struct tty_struct *);
126 void (*flush_buffer)(struct tty_struct *tty);
127 ssize_t (*chars_in_buffer)(struct tty_struct *tty);
128 ssize_t (*read)(struct tty_struct * tty, struct file * file,
129 unsigned char __user * buf, size_t nr);
130 ssize_t (*write)(struct tty_struct * tty, struct file * file,
131 const unsigned char * buf, size_t nr);
132 int (*ioctl)(struct tty_struct * tty, struct file * file,
133 unsigned int cmd, unsigned long arg);
134 long (*compat_ioctl)(struct tty_struct * tty, struct file * file,
135 unsigned int cmd, unsigned long arg);
136 void (*set_termios)(struct tty_struct *tty, struct ktermios * old);
137 unsigned int (*poll)(struct tty_struct *, struct file *,
138 struct poll_table_struct *);
139 int (*hangup)(struct tty_struct *tty);
141 /*
142 * The following routines are called from below.
143 */
144 void (*receive_buf)(struct tty_struct *, const unsigned char *cp,
145 char *fp, int count);
146 void (*write_wakeup)(struct tty_struct *);
147 void (*dcd_change)(struct tty_struct *, unsigned int,
148 struct pps_event_time *);
150 struct module *owner;
152 int refcount;
153 };
155 struct tty_ldisc {
156 struct tty_ldisc_ops *ops;
157 atomic_t users;
158 wait_queue_head_t wq_idle;
159 };
161 #define TTY_LDISC_MAGIC 0x5403
163 #define LDISC_FLAG_DEFINED 0x00000001
165 #define MODULE_ALIAS_LDISC(ldisc) \
166 MODULE_ALIAS("tty-ldisc-" __stringify(ldisc))
168 #endif /* _LINUX_TTY_LDISC_H */