1 /*
2 * Many of the syscalls used in this file expect some of the arguments
3 * to be __user pointers not __kernel pointers. To limit the sparse
4 * noise, turn off sparse checking for this file.
5 */
6 #ifdef __CHECKER__
7 #undef __CHECKER__
8 #warning "Sparse checking disabled for this file"
9 #endif
11 #include <linux/unistd.h>
12 #include <linux/kernel.h>
13 #include <linux/fs.h>
14 #include <linux/minix_fs.h>
15 #include <linux/romfs_fs.h>
16 #include <linux/initrd.h>
17 #include <linux/sched.h>
18 #include <linux/freezer.h>
19 #include <linux/kmod.h>
21 #include "do_mounts.h"
23 unsigned long initrd_start, initrd_end;
24 int initrd_below_start_ok;
25 unsigned int real_root_dev; /* do_proc_dointvec cannot handle kdev_t */
26 static int __initdata mount_initrd = 1;
28 static int __init no_initrd(char *str)
29 {
30 mount_initrd = 0;
31 return 1;
32 }
34 __setup("noinitrd", no_initrd);
36 static int init_linuxrc(struct subprocess_info *info, struct cred *new)
37 {
38 sys_unshare(CLONE_FS | CLONE_FILES);
39 /* stdin/stdout/stderr for /linuxrc */
40 sys_open("/dev/console", O_RDWR, 0);
41 sys_dup(0);
42 sys_dup(0);
43 /* move initrd over / and chdir/chroot in initrd root */
44 sys_chdir("/root");
45 sys_mount(".", "/", NULL, MS_MOVE, NULL);
46 sys_chroot(".");
47 sys_setsid();
48 return 0;
49 }
51 static void __init handle_initrd(void)
52 {
53 static char *argv[] = { "linuxrc", NULL, };
54 extern char *envp_init[];
55 int error;
57 real_root_dev = new_encode_dev(ROOT_DEV);
58 create_dev("/dev/root.old", Root_RAM0);
59 /* mount initrd on rootfs' /root */
60 mount_block_root("/dev/root.old", root_mountflags & ~MS_RDONLY);
61 sys_mkdir("/old", 0700);
62 sys_chdir("/old");
64 /*
65 * In case that a resume from disk is carried out by linuxrc or one of
66 * its children, we need to tell the freezer not to wait for us.
67 */
68 current->flags |= PF_FREEZER_SKIP;
70 call_usermodehelper_fns("/linuxrc", argv, envp_init, UMH_WAIT_PROC,
71 init_linuxrc, NULL, NULL);
73 current->flags &= ~PF_FREEZER_SKIP;
75 /* move initrd to rootfs' /old */
76 sys_mount("..", ".", NULL, MS_MOVE, NULL);
77 /* switch root and cwd back to / of rootfs */
78 sys_chroot("..");
80 if (new_decode_dev(real_root_dev) == Root_RAM0) {
81 sys_chdir("/old");
82 return;
83 }
85 sys_chdir("/");
86 ROOT_DEV = new_decode_dev(real_root_dev);
87 mount_root();
89 printk(KERN_NOTICE "Trying to move old root to /initrd ... ");
90 error = sys_mount("/old", "/root/initrd", NULL, MS_MOVE, NULL);
91 if (!error)
92 printk("okay\n");
93 else {
94 int fd = sys_open("/dev/root.old", O_RDWR, 0);
95 if (error == -ENOENT)
96 printk("/initrd does not exist. Ignored.\n");
97 else
98 printk("failed\n");
99 printk(KERN_NOTICE "Unmounting old root\n");
100 sys_umount("/old", MNT_DETACH);
101 printk(KERN_NOTICE "Trying to free ramdisk memory ... ");
102 if (fd < 0) {
103 error = fd;
104 } else {
105 error = sys_ioctl(fd, BLKFLSBUF, 0);
106 sys_close(fd);
107 }
108 printk(!error ? "okay\n" : "failed\n");
109 }
110 }
112 int __init initrd_load(void)
113 {
114 if (mount_initrd) {
115 create_dev("/dev/ram", Root_RAM0);
116 /*
117 * Load the initrd data into /dev/ram0. Execute it as initrd
118 * unless /dev/ram0 is supposed to be our actual root device,
119 * in that case the ram disk is just set up here, and gets
120 * mounted in the normal path.
121 */
122 if (rd_load_image("/initrd.image") && ROOT_DEV != Root_RAM0) {
123 sys_unlink("/initrd.image");
124 handle_initrd();
125 return 1;
126 }
127 }
128 sys_unlink("/initrd.image");
129 return 0;
130 }