1 /*
2 * linux/kernel/acct.c
3 *
4 * BSD Process Accounting for Linux
5 *
6 * Author: Marco van Wieringen <mvw@planets.elm.net>
7 *
8 * Some code based on ideas and code from:
9 * Thomas K. Dyas <tdyas@eden.rutgers.edu>
10 *
11 * This file implements BSD-style process accounting. Whenever any
12 * process exits, an accounting record of type "struct acct" is
13 * written to the file specified with the acct() system call. It is
14 * up to user-level programs to do useful things with the accounting
15 * log. The kernel just provides the raw accounting information.
16 *
17 * (C) Copyright 1995 - 1997 Marco van Wieringen - ELM Consultancy B.V.
18 *
19 * Plugged two leaks. 1) It didn't return acct_file into the free_filps if
20 * the file happened to be read-only. 2) If the accounting was suspended
21 * due to the lack of space it happily allowed to reopen it and completely
22 * lost the old acct_file. 3/10/98, Al Viro.
23 *
24 * Now we silently close acct_file on attempt to reopen. Cleaned sys_acct().
25 * XTerms and EMACS are manifestations of pure evil. 21/10/98, AV.
26 *
27 * Fixed a nasty interaction with with sys_umount(). If the accointing
28 * was suspeneded we failed to stop it on umount(). Messy.
29 * Another one: remount to readonly didn't stop accounting.
30 * Question: what should we do if we have CAP_SYS_ADMIN but not
31 * CAP_SYS_PACCT? Current code does the following: umount returns -EBUSY
32 * unless we are messing with the root. In that case we are getting a
33 * real mess with do_remount_sb(). 9/11/98, AV.
34 *
35 * Fixed a bunch of races (and pair of leaks). Probably not the best way,
36 * but this one obviously doesn't introduce deadlocks. Later. BTW, found
37 * one race (and leak) in BSD implementation.
38 * OK, that's better. ANOTHER race and leak in BSD variant. There always
39 * is one more bug... 10/11/98, AV.
40 *
41 * Oh, fsck... Oopsable SMP race in do_process_acct() - we must hold
42 * ->mmap_sem to walk the vma list of current->mm. Nasty, since it leaks
43 * a struct file opened for write. Fixed. 2/6/2000, AV.
44 */
46 #include <linux/mm.h>
47 #include <linux/slab.h>
48 #include <linux/acct.h>
49 #include <linux/capability.h>
50 #include <linux/file.h>
51 #include <linux/tty.h>
52 #include <linux/security.h>
53 #include <linux/vfs.h>
54 #include <linux/jiffies.h>
55 #include <linux/times.h>
56 #include <linux/syscalls.h>
57 #include <linux/mount.h>
58 #include <asm/uaccess.h>
59 #include <asm/div64.h>
60 #include <linux/blkdev.h> /* sector_div */
61 #include <linux/pid_namespace.h>
63 /*
64 * These constants control the amount of freespace that suspend and
65 * resume the process accounting system, and the time delay between
66 * each check.
67 * Turned into sysctl-controllable parameters. AV, 12/11/98
68 */
70 int acct_parm[3] = {4, 2, 30};
71 #define RESUME (acct_parm[0]) /* >foo% free space - resume */
72 #define SUSPEND (acct_parm[1]) /* <foo% free space - suspend */
73 #define ACCT_TIMEOUT (acct_parm[2]) /* foo second timeout between checks */
75 /*
76 * External references and all of the globals.
77 */
78 static void do_acct_process(struct bsd_acct_struct *acct,
79 struct pid_namespace *ns, struct file *);
81 /*
82 * This structure is used so that all the data protected by lock
83 * can be placed in the same cache line as the lock. This primes
84 * the cache line to have the data after getting the lock.
85 */
86 struct bsd_acct_struct {
87 int active;
88 unsigned long needcheck;
89 struct file *file;
90 struct pid_namespace *ns;
91 struct list_head list;
92 };
94 static DEFINE_SPINLOCK(acct_lock);
95 static LIST_HEAD(acct_list);
97 /*
98 * Check the amount of free space and suspend/resume accordingly.
99 */
100 static int check_free_space(struct bsd_acct_struct *acct, struct file *file)
101 {
102 struct kstatfs sbuf;
103 int res;
104 int act;
105 u64 resume;
106 u64 suspend;
108 spin_lock(&acct_lock);
109 res = acct->active;
110 if (!file || time_is_before_jiffies(acct->needcheck))
111 goto out;
112 spin_unlock(&acct_lock);
114 /* May block */
115 if (vfs_statfs(&file->f_path, &sbuf))
116 return res;
117 suspend = sbuf.f_blocks * SUSPEND;
118 resume = sbuf.f_blocks * RESUME;
120 do_div(suspend, 100);
121 do_div(resume, 100);
123 if (sbuf.f_bavail <= suspend)
124 act = -1;
125 else if (sbuf.f_bavail >= resume)
126 act = 1;
127 else
128 act = 0;
130 /*
131 * If some joker switched acct->file under us we'ld better be
132 * silent and _not_ touch anything.
133 */
134 spin_lock(&acct_lock);
135 if (file != acct->file) {
136 if (act)
137 res = act>0;
138 goto out;
139 }
141 if (acct->active) {
142 if (act < 0) {
143 acct->active = 0;
144 printk(KERN_INFO "Process accounting paused\n");
145 }
146 } else {
147 if (act > 0) {
148 acct->active = 1;
149 printk(KERN_INFO "Process accounting resumed\n");
150 }
151 }
153 acct->needcheck = jiffies + ACCT_TIMEOUT*HZ;
154 res = acct->active;
155 out:
156 spin_unlock(&acct_lock);
157 return res;
158 }
160 /*
161 * Close the old accounting file (if currently open) and then replace
162 * it with file (if non-NULL).
163 *
164 * NOTE: acct_lock MUST be held on entry and exit.
165 */
166 static void acct_file_reopen(struct bsd_acct_struct *acct, struct file *file,
167 struct pid_namespace *ns)
168 {
169 struct file *old_acct = NULL;
170 struct pid_namespace *old_ns = NULL;
172 if (acct->file) {
173 old_acct = acct->file;
174 old_ns = acct->ns;
175 acct->active = 0;
176 acct->file = NULL;
177 acct->ns = NULL;
178 list_del(&acct->list);
179 }
180 if (file) {
181 acct->file = file;
182 acct->ns = ns;
183 acct->needcheck = jiffies + ACCT_TIMEOUT*HZ;
184 acct->active = 1;
185 list_add(&acct->list, &acct_list);
186 }
187 if (old_acct) {
188 mnt_unpin(old_acct->f_path.mnt);
189 spin_unlock(&acct_lock);
190 do_acct_process(acct, old_ns, old_acct);
191 filp_close(old_acct, NULL);
192 spin_lock(&acct_lock);
193 }
194 }
196 static int acct_on(struct filename *pathname)
197 {
198 struct file *file;
199 struct vfsmount *mnt;
200 struct pid_namespace *ns;
201 struct bsd_acct_struct *acct = NULL;
203 /* Difference from BSD - they don't do O_APPEND */
204 file = file_open_name(pathname, O_WRONLY|O_APPEND|O_LARGEFILE, 0);
205 if (IS_ERR(file))
206 return PTR_ERR(file);
208 if (!S_ISREG(file->f_path.dentry->d_inode->i_mode)) {
209 filp_close(file, NULL);
210 return -EACCES;
211 }
213 if (!file->f_op->write) {
214 filp_close(file, NULL);
215 return -EIO;
216 }
218 ns = task_active_pid_ns(current);
219 if (ns->bacct == NULL) {
220 acct = kzalloc(sizeof(struct bsd_acct_struct), GFP_KERNEL);
221 if (acct == NULL) {
222 filp_close(file, NULL);
223 return -ENOMEM;
224 }
225 }
227 spin_lock(&acct_lock);
228 if (ns->bacct == NULL) {
229 ns->bacct = acct;
230 acct = NULL;
231 }
233 mnt = file->f_path.mnt;
234 mnt_pin(mnt);
235 acct_file_reopen(ns->bacct, file, ns);
236 spin_unlock(&acct_lock);
238 mntput(mnt); /* it's pinned, now give up active reference */
239 kfree(acct);
241 return 0;
242 }
244 /**
245 * sys_acct - enable/disable process accounting
246 * @name: file name for accounting records or NULL to shutdown accounting
247 *
248 * Returns 0 for success or negative errno values for failure.
249 *
250 * sys_acct() is the only system call needed to implement process
251 * accounting. It takes the name of the file where accounting records
252 * should be written. If the filename is NULL, accounting will be
253 * shutdown.
254 */
255 SYSCALL_DEFINE1(acct, const char __user *, name)
256 {
257 int error = 0;
259 if (!capable(CAP_SYS_PACCT))
260 return -EPERM;
262 if (name) {
263 struct filename *tmp = getname(name);
264 if (IS_ERR(tmp))
265 return (PTR_ERR(tmp));
266 error = acct_on(tmp);
267 putname(tmp);
268 } else {
269 struct bsd_acct_struct *acct;
271 acct = task_active_pid_ns(current)->bacct;
272 if (acct == NULL)
273 return 0;
275 spin_lock(&acct_lock);
276 acct_file_reopen(acct, NULL, NULL);
277 spin_unlock(&acct_lock);
278 }
280 return error;
281 }
283 /**
284 * acct_auto_close - turn off a filesystem's accounting if it is on
285 * @m: vfsmount being shut down
286 *
287 * If the accounting is turned on for a file in the subtree pointed to
288 * to by m, turn accounting off. Done when m is about to die.
289 */
290 void acct_auto_close_mnt(struct vfsmount *m)
291 {
292 struct bsd_acct_struct *acct;
294 spin_lock(&acct_lock);
295 restart:
296 list_for_each_entry(acct, &acct_list, list)
297 if (acct->file && acct->file->f_path.mnt == m) {
298 acct_file_reopen(acct, NULL, NULL);
299 goto restart;
300 }
301 spin_unlock(&acct_lock);
302 }
304 /**
305 * acct_auto_close - turn off a filesystem's accounting if it is on
306 * @sb: super block for the filesystem
307 *
308 * If the accounting is turned on for a file in the filesystem pointed
309 * to by sb, turn accounting off.
310 */
311 void acct_auto_close(struct super_block *sb)
312 {
313 struct bsd_acct_struct *acct;
315 spin_lock(&acct_lock);
316 restart:
317 list_for_each_entry(acct, &acct_list, list)
318 if (acct->file && acct->file->f_path.dentry->d_sb == sb) {
319 acct_file_reopen(acct, NULL, NULL);
320 goto restart;
321 }
322 spin_unlock(&acct_lock);
323 }
325 void acct_exit_ns(struct pid_namespace *ns)
326 {
327 struct bsd_acct_struct *acct = ns->bacct;
329 if (acct == NULL)
330 return;
332 spin_lock(&acct_lock);
333 if (acct->file != NULL)
334 acct_file_reopen(acct, NULL, NULL);
335 spin_unlock(&acct_lock);
337 kfree(acct);
338 }
340 /*
341 * encode an unsigned long into a comp_t
342 *
343 * This routine has been adopted from the encode_comp_t() function in
344 * the kern_acct.c file of the FreeBSD operating system. The encoding
345 * is a 13-bit fraction with a 3-bit (base 8) exponent.
346 */
348 #define MANTSIZE 13 /* 13 bit mantissa. */
349 #define EXPSIZE 3 /* Base 8 (3 bit) exponent. */
350 #define MAXFRACT ((1 << MANTSIZE) - 1) /* Maximum fractional value. */
352 static comp_t encode_comp_t(unsigned long value)
353 {
354 int exp, rnd;
356 exp = rnd = 0;
357 while (value > MAXFRACT) {
358 rnd = value & (1 << (EXPSIZE - 1)); /* Round up? */
359 value >>= EXPSIZE; /* Base 8 exponent == 3 bit shift. */
360 exp++;
361 }
363 /*
364 * If we need to round up, do it (and handle overflow correctly).
365 */
366 if (rnd && (++value > MAXFRACT)) {
367 value >>= EXPSIZE;
368 exp++;
369 }
371 /*
372 * Clean it up and polish it off.
373 */
374 exp <<= MANTSIZE; /* Shift the exponent into place */
375 exp += value; /* and add on the mantissa. */
376 return exp;
377 }
379 #if ACCT_VERSION==1 || ACCT_VERSION==2
380 /*
381 * encode an u64 into a comp2_t (24 bits)
382 *
383 * Format: 5 bit base 2 exponent, 20 bits mantissa.
384 * The leading bit of the mantissa is not stored, but implied for
385 * non-zero exponents.
386 * Largest encodable value is 50 bits.
387 */
389 #define MANTSIZE2 20 /* 20 bit mantissa. */
390 #define EXPSIZE2 5 /* 5 bit base 2 exponent. */
391 #define MAXFRACT2 ((1ul << MANTSIZE2) - 1) /* Maximum fractional value. */
392 #define MAXEXP2 ((1 <<EXPSIZE2) - 1) /* Maximum exponent. */
394 static comp2_t encode_comp2_t(u64 value)
395 {
396 int exp, rnd;
398 exp = (value > (MAXFRACT2>>1));
399 rnd = 0;
400 while (value > MAXFRACT2) {
401 rnd = value & 1;
402 value >>= 1;
403 exp++;
404 }
406 /*
407 * If we need to round up, do it (and handle overflow correctly).
408 */
409 if (rnd && (++value > MAXFRACT2)) {
410 value >>= 1;
411 exp++;
412 }
414 if (exp > MAXEXP2) {
415 /* Overflow. Return largest representable number instead. */
416 return (1ul << (MANTSIZE2+EXPSIZE2-1)) - 1;
417 } else {
418 return (value & (MAXFRACT2>>1)) | (exp << (MANTSIZE2-1));
419 }
420 }
421 #endif
423 #if ACCT_VERSION==3
424 /*
425 * encode an u64 into a 32 bit IEEE float
426 */
427 static u32 encode_float(u64 value)
428 {
429 unsigned exp = 190;
430 unsigned u;
432 if (value==0) return 0;
433 while ((s64)value > 0){
434 value <<= 1;
435 exp--;
436 }
437 u = (u32)(value >> 40) & 0x7fffffu;
438 return u | (exp << 23);
439 }
440 #endif
442 /*
443 * Write an accounting entry for an exiting process
444 *
445 * The acct_process() call is the workhorse of the process
446 * accounting system. The struct acct is built here and then written
447 * into the accounting file. This function should only be called from
448 * do_exit() or when switching to a different output file.
449 */
451 /*
452 * do_acct_process does all actual work. Caller holds the reference to file.
453 */
454 static void do_acct_process(struct bsd_acct_struct *acct,
455 struct pid_namespace *ns, struct file *file)
456 {
457 struct pacct_struct *pacct = ¤t->signal->pacct;
458 acct_t ac;
459 mm_segment_t fs;
460 unsigned long flim;
461 u64 elapsed;
462 u64 run_time;
463 struct timespec uptime;
464 struct tty_struct *tty;
465 const struct cred *orig_cred;
467 /* Perform file operations on behalf of whoever enabled accounting */
468 orig_cred = override_creds(file->f_cred);
470 /*
471 * First check to see if there is enough free_space to continue
472 * the process accounting system.
473 */
474 if (!check_free_space(acct, file))
475 goto out;
477 /*
478 * Fill the accounting struct with the needed info as recorded
479 * by the different kernel functions.
480 */
481 memset(&ac, 0, sizeof(acct_t));
483 ac.ac_version = ACCT_VERSION | ACCT_BYTEORDER;
484 strlcpy(ac.ac_comm, current->comm, sizeof(ac.ac_comm));
486 /* calculate run_time in nsec*/
487 do_posix_clock_monotonic_gettime(&uptime);
488 run_time = (u64)uptime.tv_sec*NSEC_PER_SEC + uptime.tv_nsec;
489 run_time -= (u64)current->group_leader->start_time.tv_sec * NSEC_PER_SEC
490 + current->group_leader->start_time.tv_nsec;
491 /* convert nsec -> AHZ */
492 elapsed = nsec_to_AHZ(run_time);
493 #if ACCT_VERSION==3
494 ac.ac_etime = encode_float(elapsed);
495 #else
496 ac.ac_etime = encode_comp_t(elapsed < (unsigned long) -1l ?
497 (unsigned long) elapsed : (unsigned long) -1l);
498 #endif
499 #if ACCT_VERSION==1 || ACCT_VERSION==2
500 {
501 /* new enlarged etime field */
502 comp2_t etime = encode_comp2_t(elapsed);
503 ac.ac_etime_hi = etime >> 16;
504 ac.ac_etime_lo = (u16) etime;
505 }
506 #endif
507 do_div(elapsed, AHZ);
508 ac.ac_btime = get_seconds() - elapsed;
509 /* we really need to bite the bullet and change layout */
510 ac.ac_uid = from_kuid_munged(file->f_cred->user_ns, orig_cred->uid);
511 ac.ac_gid = from_kgid_munged(file->f_cred->user_ns, orig_cred->gid);
512 #if ACCT_VERSION==2
513 ac.ac_ahz = AHZ;
514 #endif
515 #if ACCT_VERSION==1 || ACCT_VERSION==2
516 /* backward-compatible 16 bit fields */
517 ac.ac_uid16 = ac.ac_uid;
518 ac.ac_gid16 = ac.ac_gid;
519 #endif
520 #if ACCT_VERSION==3
521 ac.ac_pid = task_tgid_nr_ns(current, ns);
522 rcu_read_lock();
523 ac.ac_ppid = task_tgid_nr_ns(rcu_dereference(current->real_parent), ns);
524 rcu_read_unlock();
525 #endif
527 spin_lock_irq(¤t->sighand->siglock);
528 tty = current->signal->tty; /* Safe as we hold the siglock */
529 ac.ac_tty = tty ? old_encode_dev(tty_devnum(tty)) : 0;
530 ac.ac_utime = encode_comp_t(jiffies_to_AHZ(cputime_to_jiffies(pacct->ac_utime)));
531 ac.ac_stime = encode_comp_t(jiffies_to_AHZ(cputime_to_jiffies(pacct->ac_stime)));
532 ac.ac_flag = pacct->ac_flag;
533 ac.ac_mem = encode_comp_t(pacct->ac_mem);
534 ac.ac_minflt = encode_comp_t(pacct->ac_minflt);
535 ac.ac_majflt = encode_comp_t(pacct->ac_majflt);
536 ac.ac_exitcode = pacct->ac_exitcode;
537 spin_unlock_irq(¤t->sighand->siglock);
538 ac.ac_io = encode_comp_t(0 /* current->io_usage */); /* %% */
539 ac.ac_rw = encode_comp_t(ac.ac_io / 1024);
540 ac.ac_swaps = encode_comp_t(0);
542 /*
543 * Kernel segment override to datasegment and write it
544 * to the accounting file.
545 */
546 fs = get_fs();
547 set_fs(KERNEL_DS);
548 /*
549 * Accounting records are not subject to resource limits.
550 */
551 flim = current->signal->rlim[RLIMIT_FSIZE].rlim_cur;
552 current->signal->rlim[RLIMIT_FSIZE].rlim_cur = RLIM_INFINITY;
553 file->f_op->write(file, (char *)&ac,
554 sizeof(acct_t), &file->f_pos);
555 current->signal->rlim[RLIMIT_FSIZE].rlim_cur = flim;
556 set_fs(fs);
557 out:
558 revert_creds(orig_cred);
559 }
561 /**
562 * acct_collect - collect accounting information into pacct_struct
563 * @exitcode: task exit code
564 * @group_dead: not 0, if this thread is the last one in the process.
565 */
566 void acct_collect(long exitcode, int group_dead)
567 {
568 struct pacct_struct *pacct = ¤t->signal->pacct;
569 unsigned long vsize = 0;
571 if (group_dead && current->mm) {
572 struct vm_area_struct *vma;
573 down_read(¤t->mm->mmap_sem);
574 vma = current->mm->mmap;
575 while (vma) {
576 vsize += vma->vm_end - vma->vm_start;
577 vma = vma->vm_next;
578 }
579 up_read(¤t->mm->mmap_sem);
580 }
582 spin_lock_irq(¤t->sighand->siglock);
583 if (group_dead)
584 pacct->ac_mem = vsize / 1024;
585 if (thread_group_leader(current)) {
586 pacct->ac_exitcode = exitcode;
587 if (current->flags & PF_FORKNOEXEC)
588 pacct->ac_flag |= AFORK;
589 }
590 if (current->flags & PF_SUPERPRIV)
591 pacct->ac_flag |= ASU;
592 if (current->flags & PF_DUMPCORE)
593 pacct->ac_flag |= ACORE;
594 if (current->flags & PF_SIGNALED)
595 pacct->ac_flag |= AXSIG;
596 pacct->ac_utime += current->utime;
597 pacct->ac_stime += current->stime;
598 pacct->ac_minflt += current->min_flt;
599 pacct->ac_majflt += current->maj_flt;
600 spin_unlock_irq(¤t->sighand->siglock);
601 }
603 static void acct_process_in_ns(struct pid_namespace *ns)
604 {
605 struct file *file = NULL;
606 struct bsd_acct_struct *acct;
608 acct = ns->bacct;
609 /*
610 * accelerate the common fastpath:
611 */
612 if (!acct || !acct->file)
613 return;
615 spin_lock(&acct_lock);
616 file = acct->file;
617 if (unlikely(!file)) {
618 spin_unlock(&acct_lock);
619 return;
620 }
621 get_file(file);
622 spin_unlock(&acct_lock);
624 do_acct_process(acct, ns, file);
625 fput(file);
626 }
628 /**
629 * acct_process - now just a wrapper around acct_process_in_ns,
630 * which in turn is a wrapper around do_acct_process.
631 *
632 * handles process accounting for an exiting task
633 */
634 void acct_process(void)
635 {
636 struct pid_namespace *ns;
638 /*
639 * This loop is safe lockless, since current is still
640 * alive and holds its namespace, which in turn holds
641 * its parent.
642 */
643 for (ns = task_active_pid_ns(current); ns != NULL; ns = ns->parent)
644 acct_process_in_ns(ns);
645 }