1 /*
2 * async.c: Asynchronous function calls for boot performance
3 *
4 * (C) Copyright 2009 Intel Corporation
5 * Author: Arjan van de Ven <arjan@linux.intel.com>
6 *
7 * This program is free software; you can redistribute it and/or
8 * modify it under the terms of the GNU General Public License
9 * as published by the Free Software Foundation; version 2
10 * of the License.
11 */
14 /*
16 Goals and Theory of Operation
18 The primary goal of this feature is to reduce the kernel boot time,
19 by doing various independent hardware delays and discovery operations
20 decoupled and not strictly serialized.
22 More specifically, the asynchronous function call concept allows
23 certain operations (primarily during system boot) to happen
24 asynchronously, out of order, while these operations still
25 have their externally visible parts happen sequentially and in-order.
26 (not unlike how out-of-order CPUs retire their instructions in order)
28 Key to the asynchronous function call implementation is the concept of
29 a "sequence cookie" (which, although it has an abstracted type, can be
30 thought of as a monotonically incrementing number).
32 The async core will assign each scheduled event such a sequence cookie and
33 pass this to the called functions.
35 The asynchronously called function should before doing a globally visible
36 operation, such as registering device numbers, call the
37 async_synchronize_cookie() function and pass in its own cookie. The
38 async_synchronize_cookie() function will make sure that all asynchronous
39 operations that were scheduled prior to the operation corresponding with the
40 cookie have completed.
42 Subsystem/driver initialization code that scheduled asynchronous probe
43 functions, but which shares global resources with other drivers/subsystems
44 that do not use the asynchronous call feature, need to do a full
45 synchronization with the async_synchronize_full() function, before returning
46 from their init function. This is to maintain strict ordering between the
47 asynchronous and synchronous parts of the kernel.
49 */
51 #include <linux/async.h>
52 #include <linux/atomic.h>
53 #include <linux/ktime.h>
54 #include <linux/export.h>
55 #include <linux/wait.h>
56 #include <linux/sched.h>
57 #include <linux/slab.h>
58 #include <linux/workqueue.h>
60 static async_cookie_t next_cookie = 1;
62 #define MAX_WORK 32768
64 static LIST_HEAD(async_pending);
65 static ASYNC_DOMAIN(async_running);
66 static LIST_HEAD(async_domains);
67 static DEFINE_SPINLOCK(async_lock);
68 static DEFINE_MUTEX(async_register_mutex);
70 struct async_entry {
71 struct list_head list;
72 struct work_struct work;
73 async_cookie_t cookie;
74 async_func_ptr *func;
75 void *data;
76 struct async_domain *running;
77 };
79 static DECLARE_WAIT_QUEUE_HEAD(async_done);
81 static atomic_t entry_count;
84 /*
85 * MUST be called with the lock held!
86 */
87 static async_cookie_t __lowest_in_progress(struct async_domain *running)
88 {
89 async_cookie_t first_running = next_cookie; /* infinity value */
90 async_cookie_t first_pending = next_cookie; /* ditto */
91 struct async_entry *entry;
93 /*
94 * Both running and pending lists are sorted but not disjoint.
95 * Take the first cookies from both and return the min.
96 */
97 if (!list_empty(&running->domain)) {
98 entry = list_first_entry(&running->domain, typeof(*entry), list);
99 first_running = entry->cookie;
100 }
102 list_for_each_entry(entry, &async_pending, list) {
103 if (entry->running == running) {
104 first_pending = entry->cookie;
105 break;
106 }
107 }
109 return min(first_running, first_pending);
110 }
112 static async_cookie_t lowest_in_progress(struct async_domain *running)
113 {
114 unsigned long flags;
115 async_cookie_t ret;
117 spin_lock_irqsave(&async_lock, flags);
118 ret = __lowest_in_progress(running);
119 spin_unlock_irqrestore(&async_lock, flags);
120 return ret;
121 }
123 /*
124 * pick the first pending entry and run it
125 */
126 static void async_run_entry_fn(struct work_struct *work)
127 {
128 struct async_entry *entry =
129 container_of(work, struct async_entry, work);
130 struct async_entry *pos;
131 unsigned long flags;
132 ktime_t uninitialized_var(calltime), delta, rettime;
133 struct async_domain *running = entry->running;
135 /* 1) move self to the running queue, make sure it stays sorted */
136 spin_lock_irqsave(&async_lock, flags);
137 list_for_each_entry_reverse(pos, &running->domain, list)
138 if (entry->cookie < pos->cookie)
139 break;
140 list_move_tail(&entry->list, &pos->list);
141 spin_unlock_irqrestore(&async_lock, flags);
143 /* 2) run (and print duration) */
144 if (initcall_debug && system_state == SYSTEM_BOOTING) {
145 printk(KERN_DEBUG "calling %lli_%pF @ %i\n",
146 (long long)entry->cookie,
147 entry->func, task_pid_nr(current));
148 calltime = ktime_get();
149 }
150 entry->func(entry->data, entry->cookie);
151 if (initcall_debug && system_state == SYSTEM_BOOTING) {
152 rettime = ktime_get();
153 delta = ktime_sub(rettime, calltime);
154 printk(KERN_DEBUG "initcall %lli_%pF returned 0 after %lld usecs\n",
155 (long long)entry->cookie,
156 entry->func,
157 (long long)ktime_to_ns(delta) >> 10);
158 }
160 /* 3) remove self from the running queue */
161 spin_lock_irqsave(&async_lock, flags);
162 list_del(&entry->list);
163 if (running->registered && --running->count == 0)
164 list_del_init(&running->node);
166 /* 4) free the entry */
167 kfree(entry);
168 atomic_dec(&entry_count);
170 spin_unlock_irqrestore(&async_lock, flags);
172 /* 5) wake up any waiters */
173 wake_up(&async_done);
174 }
176 static async_cookie_t __async_schedule(async_func_ptr *ptr, void *data, struct async_domain *running)
177 {
178 struct async_entry *entry;
179 unsigned long flags;
180 async_cookie_t newcookie;
182 /* allow irq-off callers */
183 entry = kzalloc(sizeof(struct async_entry), GFP_ATOMIC);
185 /*
186 * If we're out of memory or if there's too much work
187 * pending already, we execute synchronously.
188 */
189 if (!entry || atomic_read(&entry_count) > MAX_WORK) {
190 kfree(entry);
191 spin_lock_irqsave(&async_lock, flags);
192 newcookie = next_cookie++;
193 spin_unlock_irqrestore(&async_lock, flags);
195 /* low on memory.. run synchronously */
196 ptr(data, newcookie);
197 return newcookie;
198 }
199 INIT_WORK(&entry->work, async_run_entry_fn);
200 entry->func = ptr;
201 entry->data = data;
202 entry->running = running;
204 spin_lock_irqsave(&async_lock, flags);
205 newcookie = entry->cookie = next_cookie++;
206 list_add_tail(&entry->list, &async_pending);
207 if (running->registered && running->count++ == 0)
208 list_add_tail(&running->node, &async_domains);
209 atomic_inc(&entry_count);
210 spin_unlock_irqrestore(&async_lock, flags);
212 /* mark that this task has queued an async job, used by module init */
213 current->flags |= PF_USED_ASYNC;
215 /* schedule for execution */
216 queue_work(system_unbound_wq, &entry->work);
218 return newcookie;
219 }
221 /**
222 * async_schedule - schedule a function for asynchronous execution
223 * @ptr: function to execute asynchronously
224 * @data: data pointer to pass to the function
225 *
226 * Returns an async_cookie_t that may be used for checkpointing later.
227 * Note: This function may be called from atomic or non-atomic contexts.
228 */
229 async_cookie_t async_schedule(async_func_ptr *ptr, void *data)
230 {
231 return __async_schedule(ptr, data, &async_running);
232 }
233 EXPORT_SYMBOL_GPL(async_schedule);
235 /**
236 * async_schedule_domain - schedule a function for asynchronous execution within a certain domain
237 * @ptr: function to execute asynchronously
238 * @data: data pointer to pass to the function
239 * @running: running list for the domain
240 *
241 * Returns an async_cookie_t that may be used for checkpointing later.
242 * @running may be used in the async_synchronize_*_domain() functions
243 * to wait within a certain synchronization domain rather than globally.
244 * A synchronization domain is specified via the running queue @running to use.
245 * Note: This function may be called from atomic or non-atomic contexts.
246 */
247 async_cookie_t async_schedule_domain(async_func_ptr *ptr, void *data,
248 struct async_domain *running)
249 {
250 return __async_schedule(ptr, data, running);
251 }
252 EXPORT_SYMBOL_GPL(async_schedule_domain);
254 /**
255 * async_synchronize_full - synchronize all asynchronous function calls
256 *
257 * This function waits until all asynchronous function calls have been done.
258 */
259 void async_synchronize_full(void)
260 {
261 mutex_lock(&async_register_mutex);
262 do {
263 struct async_domain *domain = NULL;
265 spin_lock_irq(&async_lock);
266 if (!list_empty(&async_domains))
267 domain = list_first_entry(&async_domains, typeof(*domain), node);
268 spin_unlock_irq(&async_lock);
270 async_synchronize_cookie_domain(next_cookie, domain);
271 } while (!list_empty(&async_domains));
272 mutex_unlock(&async_register_mutex);
273 }
274 EXPORT_SYMBOL_GPL(async_synchronize_full);
276 /**
277 * async_unregister_domain - ensure no more anonymous waiters on this domain
278 * @domain: idle domain to flush out of any async_synchronize_full instances
279 *
280 * async_synchronize_{cookie|full}_domain() are not flushed since callers
281 * of these routines should know the lifetime of @domain
282 *
283 * Prefer ASYNC_DOMAIN_EXCLUSIVE() declarations over flushing
284 */
285 void async_unregister_domain(struct async_domain *domain)
286 {
287 mutex_lock(&async_register_mutex);
288 spin_lock_irq(&async_lock);
289 WARN_ON(!domain->registered || !list_empty(&domain->node) ||
290 !list_empty(&domain->domain));
291 domain->registered = 0;
292 spin_unlock_irq(&async_lock);
293 mutex_unlock(&async_register_mutex);
294 }
295 EXPORT_SYMBOL_GPL(async_unregister_domain);
297 /**
298 * async_synchronize_full_domain - synchronize all asynchronous function within a certain domain
299 * @domain: running list to synchronize on
300 *
301 * This function waits until all asynchronous function calls for the
302 * synchronization domain specified by the running list @domain have been done.
303 */
304 void async_synchronize_full_domain(struct async_domain *domain)
305 {
306 async_synchronize_cookie_domain(next_cookie, domain);
307 }
308 EXPORT_SYMBOL_GPL(async_synchronize_full_domain);
310 /**
311 * async_synchronize_cookie_domain - synchronize asynchronous function calls within a certain domain with cookie checkpointing
312 * @cookie: async_cookie_t to use as checkpoint
313 * @running: running list to synchronize on
314 *
315 * This function waits until all asynchronous function calls for the
316 * synchronization domain specified by running list @running submitted
317 * prior to @cookie have been done.
318 */
319 void async_synchronize_cookie_domain(async_cookie_t cookie, struct async_domain *running)
320 {
321 ktime_t uninitialized_var(starttime), delta, endtime;
323 if (!running)
324 return;
326 if (initcall_debug && system_state == SYSTEM_BOOTING) {
327 printk(KERN_DEBUG "async_waiting @ %i\n", task_pid_nr(current));
328 starttime = ktime_get();
329 }
331 wait_event(async_done, lowest_in_progress(running) >= cookie);
333 if (initcall_debug && system_state == SYSTEM_BOOTING) {
334 endtime = ktime_get();
335 delta = ktime_sub(endtime, starttime);
337 printk(KERN_DEBUG "async_continuing @ %i after %lli usec\n",
338 task_pid_nr(current),
339 (long long)ktime_to_ns(delta) >> 10);
340 }
341 }
342 EXPORT_SYMBOL_GPL(async_synchronize_cookie_domain);
344 /**
345 * async_synchronize_cookie - synchronize asynchronous function calls with cookie checkpointing
346 * @cookie: async_cookie_t to use as checkpoint
347 *
348 * This function waits until all asynchronous function calls prior to @cookie
349 * have been done.
350 */
351 void async_synchronize_cookie(async_cookie_t cookie)
352 {
353 async_synchronize_cookie_domain(cookie, &async_running);
354 }
355 EXPORT_SYMBOL_GPL(async_synchronize_cookie);