]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/blob - kernel/exit.c
ARM: dts: dra72: enable dss node
[android-sdk/kernel-video.git] / kernel / exit.c
1 /*
2  *  linux/kernel/exit.c
3  *
4  *  Copyright (C) 1991, 1992  Linus Torvalds
5  */
7 #include <linux/mm.h>
8 #include <linux/slab.h>
9 #include <linux/interrupt.h>
10 #include <linux/module.h>
11 #include <linux/capability.h>
12 #include <linux/completion.h>
13 #include <linux/personality.h>
14 #include <linux/tty.h>
15 #include <linux/iocontext.h>
16 #include <linux/key.h>
17 #include <linux/security.h>
18 #include <linux/cpu.h>
19 #include <linux/acct.h>
20 #include <linux/tsacct_kern.h>
21 #include <linux/file.h>
22 #include <linux/fdtable.h>
23 #include <linux/freezer.h>
24 #include <linux/binfmts.h>
25 #include <linux/nsproxy.h>
26 #include <linux/pid_namespace.h>
27 #include <linux/ptrace.h>
28 #include <linux/profile.h>
29 #include <linux/mount.h>
30 #include <linux/proc_fs.h>
31 #include <linux/kthread.h>
32 #include <linux/mempolicy.h>
33 #include <linux/taskstats_kern.h>
34 #include <linux/delayacct.h>
35 #include <linux/cgroup.h>
36 #include <linux/syscalls.h>
37 #include <linux/signal.h>
38 #include <linux/posix-timers.h>
39 #include <linux/cn_proc.h>
40 #include <linux/mutex.h>
41 #include <linux/futex.h>
42 #include <linux/pipe_fs_i.h>
43 #include <linux/audit.h> /* for audit_free() */
44 #include <linux/resource.h>
45 #include <linux/blkdev.h>
46 #include <linux/task_io_accounting_ops.h>
47 #include <linux/tracehook.h>
48 #include <linux/fs_struct.h>
49 #include <linux/init_task.h>
50 #include <linux/perf_event.h>
51 #include <trace/events/sched.h>
52 #include <linux/hw_breakpoint.h>
53 #include <linux/oom.h>
54 #include <linux/writeback.h>
55 #include <linux/shm.h>
57 #include <asm/uaccess.h>
58 #include <asm/unistd.h>
59 #include <asm/pgtable.h>
60 #include <asm/mmu_context.h>
62 static void exit_mm(struct task_struct * tsk);
64 static void __unhash_process(struct task_struct *p, bool group_dead)
65 {
66         nr_threads--;
67         detach_pid(p, PIDTYPE_PID);
68         if (group_dead) {
69                 detach_pid(p, PIDTYPE_PGID);
70                 detach_pid(p, PIDTYPE_SID);
72                 list_del_rcu(&p->tasks);
73                 list_del_init(&p->sibling);
74                 __this_cpu_dec(process_counts);
75         }
76         list_del_rcu(&p->thread_group);
77         list_del_rcu(&p->thread_node);
78 }
80 /*
81  * This function expects the tasklist_lock write-locked.
82  */
83 static void __exit_signal(struct task_struct *tsk)
84 {
85         struct signal_struct *sig = tsk->signal;
86         bool group_dead = thread_group_leader(tsk);
87         struct sighand_struct *sighand;
88         struct tty_struct *uninitialized_var(tty);
89         cputime_t utime, stime;
91         sighand = rcu_dereference_check(tsk->sighand,
92                                         lockdep_tasklist_lock_is_held());
93         spin_lock(&sighand->siglock);
95         posix_cpu_timers_exit(tsk);
96         if (group_dead) {
97                 posix_cpu_timers_exit_group(tsk);
98                 tty = sig->tty;
99                 sig->tty = NULL;
100         } else {
101                 /*
102                  * This can only happen if the caller is de_thread().
103                  * FIXME: this is the temporary hack, we should teach
104                  * posix-cpu-timers to handle this case correctly.
105                  */
106                 if (unlikely(has_group_leader_pid(tsk)))
107                         posix_cpu_timers_exit_group(tsk);
109                 /*
110                  * If there is any task waiting for the group exit
111                  * then notify it:
112                  */
113                 if (sig->notify_count > 0 && !--sig->notify_count)
114                         wake_up_process(sig->group_exit_task);
116                 if (tsk == sig->curr_target)
117                         sig->curr_target = next_thread(tsk);
118                 /*
119                  * Accumulate here the counters for all threads but the
120                  * group leader as they die, so they can be added into
121                  * the process-wide totals when those are taken.
122                  * The group leader stays around as a zombie as long
123                  * as there are other threads.  When it gets reaped,
124                  * the exit.c code will add its counts into these totals.
125                  * We won't ever get here for the group leader, since it
126                  * will have been the last reference on the signal_struct.
127                  */
128                 task_cputime(tsk, &utime, &stime);
129                 sig->utime += utime;
130                 sig->stime += stime;
131                 sig->gtime += task_gtime(tsk);
132                 sig->min_flt += tsk->min_flt;
133                 sig->maj_flt += tsk->maj_flt;
134                 sig->nvcsw += tsk->nvcsw;
135                 sig->nivcsw += tsk->nivcsw;
136                 sig->inblock += task_io_get_inblock(tsk);
137                 sig->oublock += task_io_get_oublock(tsk);
138                 task_io_accounting_add(&sig->ioac, &tsk->ioac);
139                 sig->sum_sched_runtime += tsk->se.sum_exec_runtime;
140         }
142         sig->nr_threads--;
143         __unhash_process(tsk, group_dead);
145         /*
146          * Do this under ->siglock, we can race with another thread
147          * doing sigqueue_free() if we have SIGQUEUE_PREALLOC signals.
148          */
149         flush_sigqueue(&tsk->pending);
150         tsk->sighand = NULL;
151         spin_unlock(&sighand->siglock);
153         __cleanup_sighand(sighand);
154         clear_tsk_thread_flag(tsk,TIF_SIGPENDING);
155         if (group_dead) {
156                 flush_sigqueue(&sig->shared_pending);
157                 tty_kref_put(tty);
158         }
161 static void delayed_put_task_struct(struct rcu_head *rhp)
163         struct task_struct *tsk = container_of(rhp, struct task_struct, rcu);
165         perf_event_delayed_put(tsk);
166         trace_sched_process_free(tsk);
167         put_task_struct(tsk);
171 void release_task(struct task_struct * p)
173         struct task_struct *leader;
174         int zap_leader;
175 repeat:
176         /* don't need to get the RCU readlock here - the process is dead and
177          * can't be modifying its own credentials. But shut RCU-lockdep up */
178         rcu_read_lock();
179         atomic_dec(&__task_cred(p)->user->processes);
180         rcu_read_unlock();
182         proc_flush_task(p);
184         write_lock_irq(&tasklist_lock);
185         ptrace_release_task(p);
186         __exit_signal(p);
188         /*
189          * If we are the last non-leader member of the thread
190          * group, and the leader is zombie, then notify the
191          * group leader's parent process. (if it wants notification.)
192          */
193         zap_leader = 0;
194         leader = p->group_leader;
195         if (leader != p && thread_group_empty(leader) && leader->exit_state == EXIT_ZOMBIE) {
196                 /*
197                  * If we were the last child thread and the leader has
198                  * exited already, and the leader's parent ignores SIGCHLD,
199                  * then we are the one who should release the leader.
200                  */
201                 zap_leader = do_notify_parent(leader, leader->exit_signal);
202                 if (zap_leader)
203                         leader->exit_state = EXIT_DEAD;
204         }
206         write_unlock_irq(&tasklist_lock);
207         release_thread(p);
208         call_rcu(&p->rcu, delayed_put_task_struct);
210         p = leader;
211         if (unlikely(zap_leader))
212                 goto repeat;
215 /*
216  * This checks not only the pgrp, but falls back on the pid if no
217  * satisfactory pgrp is found. I dunno - gdb doesn't work correctly
218  * without this...
219  *
220  * The caller must hold rcu lock or the tasklist lock.
221  */
222 struct pid *session_of_pgrp(struct pid *pgrp)
224         struct task_struct *p;
225         struct pid *sid = NULL;
227         p = pid_task(pgrp, PIDTYPE_PGID);
228         if (p == NULL)
229                 p = pid_task(pgrp, PIDTYPE_PID);
230         if (p != NULL)
231                 sid = task_session(p);
233         return sid;
236 /*
237  * Determine if a process group is "orphaned", according to the POSIX
238  * definition in 2.2.2.52.  Orphaned process groups are not to be affected
239  * by terminal-generated stop signals.  Newly orphaned process groups are
240  * to receive a SIGHUP and a SIGCONT.
241  *
242  * "I ask you, have you ever known what it is to be an orphan?"
243  */
244 static int will_become_orphaned_pgrp(struct pid *pgrp, struct task_struct *ignored_task)
246         struct task_struct *p;
248         do_each_pid_task(pgrp, PIDTYPE_PGID, p) {
249                 if ((p == ignored_task) ||
250                     (p->exit_state && thread_group_empty(p)) ||
251                     is_global_init(p->real_parent))
252                         continue;
254                 if (task_pgrp(p->real_parent) != pgrp &&
255                     task_session(p->real_parent) == task_session(p))
256                         return 0;
257         } while_each_pid_task(pgrp, PIDTYPE_PGID, p);
259         return 1;
262 int is_current_pgrp_orphaned(void)
264         int retval;
266         read_lock(&tasklist_lock);
267         retval = will_become_orphaned_pgrp(task_pgrp(current), NULL);
268         read_unlock(&tasklist_lock);
270         return retval;
273 static bool has_stopped_jobs(struct pid *pgrp)
275         struct task_struct *p;
277         do_each_pid_task(pgrp, PIDTYPE_PGID, p) {
278                 if (p->signal->flags & SIGNAL_STOP_STOPPED)
279                         return true;
280         } while_each_pid_task(pgrp, PIDTYPE_PGID, p);
282         return false;
285 /*
286  * Check to see if any process groups have become orphaned as
287  * a result of our exiting, and if they have any stopped jobs,
288  * send them a SIGHUP and then a SIGCONT. (POSIX 3.2.2.2)
289  */
290 static void
291 kill_orphaned_pgrp(struct task_struct *tsk, struct task_struct *parent)
293         struct pid *pgrp = task_pgrp(tsk);
294         struct task_struct *ignored_task = tsk;
296         if (!parent)
297                  /* exit: our father is in a different pgrp than
298                   * we are and we were the only connection outside.
299                   */
300                 parent = tsk->real_parent;
301         else
302                 /* reparent: our child is in a different pgrp than
303                  * we are, and it was the only connection outside.
304                  */
305                 ignored_task = NULL;
307         if (task_pgrp(parent) != pgrp &&
308             task_session(parent) == task_session(tsk) &&
309             will_become_orphaned_pgrp(pgrp, ignored_task) &&
310             has_stopped_jobs(pgrp)) {
311                 __kill_pgrp_info(SIGHUP, SEND_SIG_PRIV, pgrp);
312                 __kill_pgrp_info(SIGCONT, SEND_SIG_PRIV, pgrp);
313         }
316 /*
317  * Let kernel threads use this to say that they allow a certain signal.
318  * Must not be used if kthread was cloned with CLONE_SIGHAND.
319  */
320 int allow_signal(int sig)
322         if (!valid_signal(sig) || sig < 1)
323                 return -EINVAL;
325         spin_lock_irq(&current->sighand->siglock);
326         /* This is only needed for daemonize()'ed kthreads */
327         sigdelset(&current->blocked, sig);
328         /*
329          * Kernel threads handle their own signals. Let the signal code
330          * know it'll be handled, so that they don't get converted to
331          * SIGKILL or just silently dropped.
332          */
333         current->sighand->action[(sig)-1].sa.sa_handler = (void __user *)2;
334         recalc_sigpending();
335         spin_unlock_irq(&current->sighand->siglock);
336         return 0;
339 EXPORT_SYMBOL(allow_signal);
341 int disallow_signal(int sig)
343         if (!valid_signal(sig) || sig < 1)
344                 return -EINVAL;
346         spin_lock_irq(&current->sighand->siglock);
347         current->sighand->action[(sig)-1].sa.sa_handler = SIG_IGN;
348         recalc_sigpending();
349         spin_unlock_irq(&current->sighand->siglock);
350         return 0;
353 EXPORT_SYMBOL(disallow_signal);
355 #ifdef CONFIG_MM_OWNER
356 /*
357  * A task is exiting.   If it owned this mm, find a new owner for the mm.
358  */
359 void mm_update_next_owner(struct mm_struct *mm)
361         struct task_struct *c, *g, *p = current;
363 retry:
364         /*
365          * If the exiting or execing task is not the owner, it's
366          * someone else's problem.
367          */
368         if (mm->owner != p)
369                 return;
370         /*
371          * The current owner is exiting/execing and there are no other
372          * candidates.  Do not leave the mm pointing to a possibly
373          * freed task structure.
374          */
375         if (atomic_read(&mm->mm_users) <= 1) {
376                 mm->owner = NULL;
377                 return;
378         }
380         read_lock(&tasklist_lock);
381         /*
382          * Search in the children
383          */
384         list_for_each_entry(c, &p->children, sibling) {
385                 if (c->mm == mm)
386                         goto assign_new_owner;
387         }
389         /*
390          * Search in the siblings
391          */
392         list_for_each_entry(c, &p->real_parent->children, sibling) {
393                 if (c->mm == mm)
394                         goto assign_new_owner;
395         }
397         /*
398          * Search through everything else. We should not get
399          * here often
400          */
401         do_each_thread(g, c) {
402                 if (c->mm == mm)
403                         goto assign_new_owner;
404         } while_each_thread(g, c);
406         read_unlock(&tasklist_lock);
407         /*
408          * We found no owner yet mm_users > 1: this implies that we are
409          * most likely racing with swapoff (try_to_unuse()) or /proc or
410          * ptrace or page migration (get_task_mm()).  Mark owner as NULL.
411          */
412         mm->owner = NULL;
413         return;
415 assign_new_owner:
416         BUG_ON(c == p);
417         get_task_struct(c);
418         /*
419          * The task_lock protects c->mm from changing.
420          * We always want mm->owner->mm == mm
421          */
422         task_lock(c);
423         /*
424          * Delay read_unlock() till we have the task_lock()
425          * to ensure that c does not slip away underneath us
426          */
427         read_unlock(&tasklist_lock);
428         if (c->mm != mm) {
429                 task_unlock(c);
430                 put_task_struct(c);
431                 goto retry;
432         }
433         mm->owner = c;
434         task_unlock(c);
435         put_task_struct(c);
437 #endif /* CONFIG_MM_OWNER */
439 /*
440  * Turn us into a lazy TLB process if we
441  * aren't already..
442  */
443 static void exit_mm(struct task_struct * tsk)
445         struct mm_struct *mm = tsk->mm;
446         struct core_state *core_state;
448         mm_release(tsk, mm);
449         if (!mm)
450                 return;
451         sync_mm_rss(mm);
452         /*
453          * Serialize with any possible pending coredump.
454          * We must hold mmap_sem around checking core_state
455          * and clearing tsk->mm.  The core-inducing thread
456          * will increment ->nr_threads for each thread in the
457          * group with ->mm != NULL.
458          */
459         down_read(&mm->mmap_sem);
460         core_state = mm->core_state;
461         if (core_state) {
462                 struct core_thread self;
463                 up_read(&mm->mmap_sem);
465                 self.task = tsk;
466                 self.next = xchg(&core_state->dumper.next, &self);
467                 /*
468                  * Implies mb(), the result of xchg() must be visible
469                  * to core_state->dumper.
470                  */
471                 if (atomic_dec_and_test(&core_state->nr_threads))
472                         complete(&core_state->startup);
474                 for (;;) {
475                         set_task_state(tsk, TASK_UNINTERRUPTIBLE);
476                         if (!self.task) /* see coredump_finish() */
477                                 break;
478                         freezable_schedule();
479                 }
480                 __set_task_state(tsk, TASK_RUNNING);
481                 down_read(&mm->mmap_sem);
482         }
483         atomic_inc(&mm->mm_count);
484         BUG_ON(mm != tsk->active_mm);
485         /* more a memory barrier than a real lock */
486         task_lock(tsk);
487         tsk->mm = NULL;
488         up_read(&mm->mmap_sem);
489         enter_lazy_tlb(mm, current);
490         task_unlock(tsk);
491         mm_update_next_owner(mm);
492         mmput(mm);
495 /*
496  * When we die, we re-parent all our children, and try to:
497  * 1. give them to another thread in our thread group, if such a member exists
498  * 2. give it to the first ancestor process which prctl'd itself as a
499  *    child_subreaper for its children (like a service manager)
500  * 3. give it to the init process (PID 1) in our pid namespace
501  */
502 static struct task_struct *find_new_reaper(struct task_struct *father)
503         __releases(&tasklist_lock)
504         __acquires(&tasklist_lock)
506         struct pid_namespace *pid_ns = task_active_pid_ns(father);
507         struct task_struct *thread;
509         thread = father;
510         while_each_thread(father, thread) {
511                 if (thread->flags & PF_EXITING)
512                         continue;
513                 if (unlikely(pid_ns->child_reaper == father))
514                         pid_ns->child_reaper = thread;
515                 return thread;
516         }
518         if (unlikely(pid_ns->child_reaper == father)) {
519                 write_unlock_irq(&tasklist_lock);
520                 if (unlikely(pid_ns == &init_pid_ns)) {
521                         panic("Attempted to kill init! exitcode=0x%08x\n",
522                                 father->signal->group_exit_code ?:
523                                         father->exit_code);
524                 }
526                 zap_pid_ns_processes(pid_ns);
527                 write_lock_irq(&tasklist_lock);
528         } else if (father->signal->has_child_subreaper) {
529                 struct task_struct *reaper;
531                 /*
532                  * Find the first ancestor marked as child_subreaper.
533                  * Note that the code below checks same_thread_group(reaper,
534                  * pid_ns->child_reaper).  This is what we need to DTRT in a
535                  * PID namespace. However we still need the check above, see
536                  * http://marc.info/?l=linux-kernel&m=131385460420380
537                  */
538                 for (reaper = father->real_parent;
539                      reaper != &init_task;
540                      reaper = reaper->real_parent) {
541                         if (same_thread_group(reaper, pid_ns->child_reaper))
542                                 break;
543                         if (!reaper->signal->is_child_subreaper)
544                                 continue;
545                         thread = reaper;
546                         do {
547                                 if (!(thread->flags & PF_EXITING))
548                                         return reaper;
549                         } while_each_thread(reaper, thread);
550                 }
551         }
553         return pid_ns->child_reaper;
556 /*
557 * Any that need to be release_task'd are put on the @dead list.
558  */
559 static void reparent_leader(struct task_struct *father, struct task_struct *p,
560                                 struct list_head *dead)
562         list_move_tail(&p->sibling, &p->real_parent->children);
563         /*
564          * If this is a threaded reparent there is no need to
565          * notify anyone anything has happened.
566          */
567         if (same_thread_group(p->real_parent, father))
568                 return;
570         /*
571          * We don't want people slaying init.
572          *
573          * Note: we do this even if it is EXIT_DEAD, wait_task_zombie()
574          * can change ->exit_state to EXIT_ZOMBIE. If this is the final
575          * state, do_notify_parent() was already called and ->exit_signal
576          * doesn't matter.
577          */
578         p->exit_signal = SIGCHLD;
580         if (p->exit_state == EXIT_DEAD)
581                 return;
583         /* If it has exited notify the new parent about this child's death. */
584         if (!p->ptrace &&
585             p->exit_state == EXIT_ZOMBIE && thread_group_empty(p)) {
586                 if (do_notify_parent(p, p->exit_signal)) {
587                         p->exit_state = EXIT_DEAD;
588                         list_move_tail(&p->sibling, dead);
589                 }
590         }
592         kill_orphaned_pgrp(p, father);
595 static void forget_original_parent(struct task_struct *father)
597         struct task_struct *p, *n, *reaper;
598         LIST_HEAD(dead_children);
600         write_lock_irq(&tasklist_lock);
601         /*
602          * Note that exit_ptrace() and find_new_reaper() might
603          * drop tasklist_lock and reacquire it.
604          */
605         exit_ptrace(father);
606         reaper = find_new_reaper(father);
608         list_for_each_entry_safe(p, n, &father->children, sibling) {
609                 struct task_struct *t = p;
610                 do {
611                         t->real_parent = reaper;
612                         if (t->parent == father) {
613                                 BUG_ON(t->ptrace);
614                                 t->parent = t->real_parent;
615                         }
616                         if (t->pdeath_signal)
617                                 group_send_sig_info(t->pdeath_signal,
618                                                     SEND_SIG_NOINFO, t);
619                 } while_each_thread(p, t);
620                 reparent_leader(father, p, &dead_children);
621         }
622         write_unlock_irq(&tasklist_lock);
624         BUG_ON(!list_empty(&father->children));
626         list_for_each_entry_safe(p, n, &dead_children, sibling) {
627                 list_del_init(&p->sibling);
628                 release_task(p);
629         }
632 /*
633  * Send signals to all our closest relatives so that they know
634  * to properly mourn us..
635  */
636 static void exit_notify(struct task_struct *tsk, int group_dead)
638         bool autoreap;
640         /*
641          * This does two things:
642          *
643          * A.  Make init inherit all the child processes
644          * B.  Check to see if any process groups have become orphaned
645          *      as a result of our exiting, and if they have any stopped
646          *      jobs, send them a SIGHUP and then a SIGCONT.  (POSIX 3.2.2.2)
647          */
648         forget_original_parent(tsk);
650         write_lock_irq(&tasklist_lock);
651         if (group_dead)
652                 kill_orphaned_pgrp(tsk->group_leader, NULL);
654         if (unlikely(tsk->ptrace)) {
655                 int sig = thread_group_leader(tsk) &&
656                                 thread_group_empty(tsk) &&
657                                 !ptrace_reparented(tsk) ?
658                         tsk->exit_signal : SIGCHLD;
659                 autoreap = do_notify_parent(tsk, sig);
660         } else if (thread_group_leader(tsk)) {
661                 autoreap = thread_group_empty(tsk) &&
662                         do_notify_parent(tsk, tsk->exit_signal);
663         } else {
664                 autoreap = true;
665         }
667         tsk->exit_state = autoreap ? EXIT_DEAD : EXIT_ZOMBIE;
669         /* mt-exec, de_thread() is waiting for group leader */
670         if (unlikely(tsk->signal->notify_count < 0))
671                 wake_up_process(tsk->signal->group_exit_task);
672         write_unlock_irq(&tasklist_lock);
674         /* If the process is dead, release it - nobody will wait for it */
675         if (autoreap)
676                 release_task(tsk);
679 #ifdef CONFIG_DEBUG_STACK_USAGE
680 static void check_stack_usage(void)
682         static DEFINE_SPINLOCK(low_water_lock);
683         static int lowest_to_date = THREAD_SIZE;
684         unsigned long free;
686         free = stack_not_used(current);
688         if (free >= lowest_to_date)
689                 return;
691         spin_lock(&low_water_lock);
692         if (free < lowest_to_date) {
693                 printk(KERN_WARNING "%s (%d) used greatest stack depth: "
694                                 "%lu bytes left\n",
695                                 current->comm, task_pid_nr(current), free);
696                 lowest_to_date = free;
697         }
698         spin_unlock(&low_water_lock);
700 #else
701 static inline void check_stack_usage(void) {}
702 #endif
704 void do_exit(long code)
706         struct task_struct *tsk = current;
707         int group_dead;
709         profile_task_exit(tsk);
711         WARN_ON(blk_needs_flush_plug(tsk));
713         if (unlikely(in_interrupt()))
714                 panic("Aiee, killing interrupt handler!");
715         if (unlikely(!tsk->pid))
716                 panic("Attempted to kill the idle task!");
718         /*
719          * If do_exit is called because this processes oopsed, it's possible
720          * that get_fs() was left as KERNEL_DS, so reset it to USER_DS before
721          * continuing. Amongst other possible reasons, this is to prevent
722          * mm_release()->clear_child_tid() from writing to a user-controlled
723          * kernel address.
724          */
725         set_fs(USER_DS);
727         ptrace_event(PTRACE_EVENT_EXIT, code);
729         validate_creds_for_do_exit(tsk);
731         /*
732          * We're taking recursive faults here in do_exit. Safest is to just
733          * leave this task alone and wait for reboot.
734          */
735         if (unlikely(tsk->flags & PF_EXITING)) {
736                 printk(KERN_ALERT
737                         "Fixing recursive fault but reboot is needed!\n");
738                 /*
739                  * We can do this unlocked here. The futex code uses
740                  * this flag just to verify whether the pi state
741                  * cleanup has been done or not. In the worst case it
742                  * loops once more. We pretend that the cleanup was
743                  * done as there is no way to return. Either the
744                  * OWNER_DIED bit is set by now or we push the blocked
745                  * task into the wait for ever nirwana as well.
746                  */
747                 tsk->flags |= PF_EXITPIDONE;
748                 set_current_state(TASK_UNINTERRUPTIBLE);
749                 schedule();
750         }
752         exit_signals(tsk);  /* sets PF_EXITING */
753         /*
754          * tsk->flags are checked in the futex code to protect against
755          * an exiting task cleaning up the robust pi futexes.
756          */
757         smp_mb();
758         raw_spin_unlock_wait(&tsk->pi_lock);
760         if (unlikely(in_atomic()))
761                 printk(KERN_INFO "note: %s[%d] exited with preempt_count %d\n",
762                                 current->comm, task_pid_nr(current),
763                                 preempt_count());
765         acct_update_integrals(tsk);
766         /* sync mm's RSS info before statistics gathering */
767         if (tsk->mm)
768                 sync_mm_rss(tsk->mm);
769         group_dead = atomic_dec_and_test(&tsk->signal->live);
770         if (group_dead) {
771                 hrtimer_cancel(&tsk->signal->real_timer);
772                 exit_itimers(tsk->signal);
773                 if (tsk->mm)
774                         setmax_mm_hiwater_rss(&tsk->signal->maxrss, tsk->mm);
775         }
776         acct_collect(code, group_dead);
777         if (group_dead)
778                 tty_audit_exit();
779         audit_free(tsk);
781         tsk->exit_code = code;
782         taskstats_exit(tsk, group_dead);
784         exit_mm(tsk);
786         if (group_dead)
787                 acct_process();
788         trace_sched_process_exit(tsk);
790         exit_sem(tsk);
791         exit_shm(tsk);
792         exit_files(tsk);
793         exit_fs(tsk);
794         if (group_dead)
795                 disassociate_ctty(1);
796         exit_task_namespaces(tsk);
797         exit_task_work(tsk);
798         check_stack_usage();
799         exit_thread();
801         /*
802          * Flush inherited counters to the parent - before the parent
803          * gets woken up by child-exit notifications.
804          *
805          * because of cgroup mode, must be called before cgroup_exit()
806          */
807         perf_event_exit_task(tsk);
809         cgroup_exit(tsk, 1);
811         module_put(task_thread_info(tsk)->exec_domain->module);
813         proc_exit_connector(tsk);
814         /*
815          * FIXME: do that only when needed, using sched_exit tracepoint
816          */
817         flush_ptrace_hw_breakpoint(tsk);
819         exit_notify(tsk, group_dead);
820 #ifdef CONFIG_NUMA
821         task_lock(tsk);
822         mpol_put(tsk->mempolicy);
823         tsk->mempolicy = NULL;
824         task_unlock(tsk);
825 #endif
826 #ifdef CONFIG_FUTEX
827         if (unlikely(current->pi_state_cache))
828                 kfree(current->pi_state_cache);
829 #endif
830         /*
831          * Make sure we are holding no locks:
832          */
833         debug_check_no_locks_held();
834         /*
835          * We can do this unlocked here. The futex code uses this flag
836          * just to verify whether the pi state cleanup has been done
837          * or not. In the worst case it loops once more.
838          */
839         tsk->flags |= PF_EXITPIDONE;
841         if (tsk->io_context)
842                 exit_io_context(tsk);
844         if (tsk->splice_pipe)
845                 free_pipe_info(tsk->splice_pipe);
847         if (tsk->task_frag.page)
848                 put_page(tsk->task_frag.page);
850         validate_creds_for_do_exit(tsk);
852         preempt_disable();
853         if (tsk->nr_dirtied)
854                 __this_cpu_add(dirty_throttle_leaks, tsk->nr_dirtied);
855         exit_rcu();
857         /*
858          * The setting of TASK_RUNNING by try_to_wake_up() may be delayed
859          * when the following two conditions become true.
860          *   - There is race condition of mmap_sem (It is acquired by
861          *     exit_mm()), and
862          *   - SMI occurs before setting TASK_RUNINNG.
863          *     (or hypervisor of virtual machine switches to other guest)
864          *  As a result, we may become TASK_RUNNING after becoming TASK_DEAD
865          *
866          * To avoid it, we have to wait for releasing tsk->pi_lock which
867          * is held by try_to_wake_up()
868          */
869         smp_mb();
870         raw_spin_unlock_wait(&tsk->pi_lock);
872         /* causes final put_task_struct in finish_task_switch(). */
873         tsk->state = TASK_DEAD;
874         tsk->flags |= PF_NOFREEZE;      /* tell freezer to ignore us */
875         schedule();
876         BUG();
877         /* Avoid "noreturn function does return".  */
878         for (;;)
879                 cpu_relax();    /* For when BUG is null */
882 EXPORT_SYMBOL_GPL(do_exit);
884 void complete_and_exit(struct completion *comp, long code)
886         if (comp)
887                 complete(comp);
889         do_exit(code);
892 EXPORT_SYMBOL(complete_and_exit);
894 SYSCALL_DEFINE1(exit, int, error_code)
896         do_exit((error_code&0xff)<<8);
899 /*
900  * Take down every thread in the group.  This is called by fatal signals
901  * as well as by sys_exit_group (below).
902  */
903 void
904 do_group_exit(int exit_code)
906         struct signal_struct *sig = current->signal;
908         BUG_ON(exit_code & 0x80); /* core dumps don't get here */
910         if (signal_group_exit(sig))
911                 exit_code = sig->group_exit_code;
912         else if (!thread_group_empty(current)) {
913                 struct sighand_struct *const sighand = current->sighand;
914                 spin_lock_irq(&sighand->siglock);
915                 if (signal_group_exit(sig))
916                         /* Another thread got here before we took the lock.  */
917                         exit_code = sig->group_exit_code;
918                 else {
919                         sig->group_exit_code = exit_code;
920                         sig->flags = SIGNAL_GROUP_EXIT;
921                         zap_other_threads(current);
922                 }
923                 spin_unlock_irq(&sighand->siglock);
924         }
926         do_exit(exit_code);
927         /* NOTREACHED */
930 /*
931  * this kills every thread in the thread group. Note that any externally
932  * wait4()-ing process will get the correct exit code - even if this
933  * thread is not the thread group leader.
934  */
935 SYSCALL_DEFINE1(exit_group, int, error_code)
937         do_group_exit((error_code & 0xff) << 8);
938         /* NOTREACHED */
939         return 0;
942 struct wait_opts {
943         enum pid_type           wo_type;
944         int                     wo_flags;
945         struct pid              *wo_pid;
947         struct siginfo __user   *wo_info;
948         int __user              *wo_stat;
949         struct rusage __user    *wo_rusage;
951         wait_queue_t            child_wait;
952         int                     notask_error;
953 };
955 static inline
956 struct pid *task_pid_type(struct task_struct *task, enum pid_type type)
958         if (type != PIDTYPE_PID)
959                 task = task->group_leader;
960         return task->pids[type].pid;
963 static int eligible_pid(struct wait_opts *wo, struct task_struct *p)
965         return  wo->wo_type == PIDTYPE_MAX ||
966                 task_pid_type(p, wo->wo_type) == wo->wo_pid;
969 static int eligible_child(struct wait_opts *wo, struct task_struct *p)
971         if (!eligible_pid(wo, p))
972                 return 0;
973         /* Wait for all children (clone and not) if __WALL is set;
974          * otherwise, wait for clone children *only* if __WCLONE is
975          * set; otherwise, wait for non-clone children *only*.  (Note:
976          * A "clone" child here is one that reports to its parent
977          * using a signal other than SIGCHLD.) */
978         if (((p->exit_signal != SIGCHLD) ^ !!(wo->wo_flags & __WCLONE))
979             && !(wo->wo_flags & __WALL))
980                 return 0;
982         return 1;
985 static int wait_noreap_copyout(struct wait_opts *wo, struct task_struct *p,
986                                 pid_t pid, uid_t uid, int why, int status)
988         struct siginfo __user *infop;
989         int retval = wo->wo_rusage
990                 ? getrusage(p, RUSAGE_BOTH, wo->wo_rusage) : 0;
992         put_task_struct(p);
993         infop = wo->wo_info;
994         if (infop) {
995                 if (!retval)
996                         retval = put_user(SIGCHLD, &infop->si_signo);
997                 if (!retval)
998                         retval = put_user(0, &infop->si_errno);
999                 if (!retval)
1000                         retval = put_user((short)why, &infop->si_code);
1001                 if (!retval)
1002                         retval = put_user(pid, &infop->si_pid);
1003                 if (!retval)
1004                         retval = put_user(uid, &infop->si_uid);
1005                 if (!retval)
1006                         retval = put_user(status, &infop->si_status);
1007         }
1008         if (!retval)
1009                 retval = pid;
1010         return retval;
1013 /*
1014  * Handle sys_wait4 work for one task in state EXIT_ZOMBIE.  We hold
1015  * read_lock(&tasklist_lock) on entry.  If we return zero, we still hold
1016  * the lock and this task is uninteresting.  If we return nonzero, we have
1017  * released the lock and the system call should return.
1018  */
1019 static int wait_task_zombie(struct wait_opts *wo, struct task_struct *p)
1021         unsigned long state;
1022         int retval, status, traced;
1023         pid_t pid = task_pid_vnr(p);
1024         uid_t uid = from_kuid_munged(current_user_ns(), task_uid(p));
1025         struct siginfo __user *infop;
1027         if (!likely(wo->wo_flags & WEXITED))
1028                 return 0;
1030         if (unlikely(wo->wo_flags & WNOWAIT)) {
1031                 int exit_code = p->exit_code;
1032                 int why;
1034                 get_task_struct(p);
1035                 read_unlock(&tasklist_lock);
1036                 if ((exit_code & 0x7f) == 0) {
1037                         why = CLD_EXITED;
1038                         status = exit_code >> 8;
1039                 } else {
1040                         why = (exit_code & 0x80) ? CLD_DUMPED : CLD_KILLED;
1041                         status = exit_code & 0x7f;
1042                 }
1043                 return wait_noreap_copyout(wo, p, pid, uid, why, status);
1044         }
1046         /*
1047          * Try to move the task's state to DEAD
1048          * only one thread is allowed to do this:
1049          */
1050         state = xchg(&p->exit_state, EXIT_DEAD);
1051         if (state != EXIT_ZOMBIE) {
1052                 BUG_ON(state != EXIT_DEAD);
1053                 return 0;
1054         }
1056         traced = ptrace_reparented(p);
1057         /*
1058          * It can be ptraced but not reparented, check
1059          * thread_group_leader() to filter out sub-threads.
1060          */
1061         if (likely(!traced) && thread_group_leader(p)) {
1062                 struct signal_struct *psig;
1063                 struct signal_struct *sig;
1064                 unsigned long maxrss;
1065                 cputime_t tgutime, tgstime;
1067                 /*
1068                  * The resource counters for the group leader are in its
1069                  * own task_struct.  Those for dead threads in the group
1070                  * are in its signal_struct, as are those for the child
1071                  * processes it has previously reaped.  All these
1072                  * accumulate in the parent's signal_struct c* fields.
1073                  *
1074                  * We don't bother to take a lock here to protect these
1075                  * p->signal fields, because they are only touched by
1076                  * __exit_signal, which runs with tasklist_lock
1077                  * write-locked anyway, and so is excluded here.  We do
1078                  * need to protect the access to parent->signal fields,
1079                  * as other threads in the parent group can be right
1080                  * here reaping other children at the same time.
1081                  *
1082                  * We use thread_group_cputime_adjusted() to get times for the thread
1083                  * group, which consolidates times for all threads in the
1084                  * group including the group leader.
1085                  */
1086                 thread_group_cputime_adjusted(p, &tgutime, &tgstime);
1087                 spin_lock_irq(&p->real_parent->sighand->siglock);
1088                 psig = p->real_parent->signal;
1089                 sig = p->signal;
1090                 psig->cutime += tgutime + sig->cutime;
1091                 psig->cstime += tgstime + sig->cstime;
1092                 psig->cgtime += task_gtime(p) + sig->gtime + sig->cgtime;
1093                 psig->cmin_flt +=
1094                         p->min_flt + sig->min_flt + sig->cmin_flt;
1095                 psig->cmaj_flt +=
1096                         p->maj_flt + sig->maj_flt + sig->cmaj_flt;
1097                 psig->cnvcsw +=
1098                         p->nvcsw + sig->nvcsw + sig->cnvcsw;
1099                 psig->cnivcsw +=
1100                         p->nivcsw + sig->nivcsw + sig->cnivcsw;
1101                 psig->cinblock +=
1102                         task_io_get_inblock(p) +
1103                         sig->inblock + sig->cinblock;
1104                 psig->coublock +=
1105                         task_io_get_oublock(p) +
1106                         sig->oublock + sig->coublock;
1107                 maxrss = max(sig->maxrss, sig->cmaxrss);
1108                 if (psig->cmaxrss < maxrss)
1109                         psig->cmaxrss = maxrss;
1110                 task_io_accounting_add(&psig->ioac, &p->ioac);
1111                 task_io_accounting_add(&psig->ioac, &sig->ioac);
1112                 spin_unlock_irq(&p->real_parent->sighand->siglock);
1113         }
1115         /*
1116          * Now we are sure this task is interesting, and no other
1117          * thread can reap it because we set its state to EXIT_DEAD.
1118          */
1119         read_unlock(&tasklist_lock);
1121         retval = wo->wo_rusage
1122                 ? getrusage(p, RUSAGE_BOTH, wo->wo_rusage) : 0;
1123         status = (p->signal->flags & SIGNAL_GROUP_EXIT)
1124                 ? p->signal->group_exit_code : p->exit_code;
1125         if (!retval && wo->wo_stat)
1126                 retval = put_user(status, wo->wo_stat);
1128         infop = wo->wo_info;
1129         if (!retval && infop)
1130                 retval = put_user(SIGCHLD, &infop->si_signo);
1131         if (!retval && infop)
1132                 retval = put_user(0, &infop->si_errno);
1133         if (!retval && infop) {
1134                 int why;
1136                 if ((status & 0x7f) == 0) {
1137                         why = CLD_EXITED;
1138                         status >>= 8;
1139                 } else {
1140                         why = (status & 0x80) ? CLD_DUMPED : CLD_KILLED;
1141                         status &= 0x7f;
1142                 }
1143                 retval = put_user((short)why, &infop->si_code);
1144                 if (!retval)
1145                         retval = put_user(status, &infop->si_status);
1146         }
1147         if (!retval && infop)
1148                 retval = put_user(pid, &infop->si_pid);
1149         if (!retval && infop)
1150                 retval = put_user(uid, &infop->si_uid);
1151         if (!retval)
1152                 retval = pid;
1154         if (traced) {
1155                 write_lock_irq(&tasklist_lock);
1156                 /* We dropped tasklist, ptracer could die and untrace */
1157                 ptrace_unlink(p);
1158                 /*
1159                  * If this is not a sub-thread, notify the parent.
1160                  * If parent wants a zombie, don't release it now.
1161                  */
1162                 if (thread_group_leader(p) &&
1163                     !do_notify_parent(p, p->exit_signal)) {
1164                         p->exit_state = EXIT_ZOMBIE;
1165                         p = NULL;
1166                 }
1167                 write_unlock_irq(&tasklist_lock);
1168         }
1169         if (p != NULL)
1170                 release_task(p);
1172         return retval;
1175 static int *task_stopped_code(struct task_struct *p, bool ptrace)
1177         if (ptrace) {
1178                 if (task_is_stopped_or_traced(p) &&
1179                     !(p->jobctl & JOBCTL_LISTENING))
1180                         return &p->exit_code;
1181         } else {
1182                 if (p->signal->flags & SIGNAL_STOP_STOPPED)
1183                         return &p->signal->group_exit_code;
1184         }
1185         return NULL;
1188 /**
1189  * wait_task_stopped - Wait for %TASK_STOPPED or %TASK_TRACED
1190  * @wo: wait options
1191  * @ptrace: is the wait for ptrace
1192  * @p: task to wait for
1193  *
1194  * Handle sys_wait4() work for %p in state %TASK_STOPPED or %TASK_TRACED.
1195  *
1196  * CONTEXT:
1197  * read_lock(&tasklist_lock), which is released if return value is
1198  * non-zero.  Also, grabs and releases @p->sighand->siglock.
1199  *
1200  * RETURNS:
1201  * 0 if wait condition didn't exist and search for other wait conditions
1202  * should continue.  Non-zero return, -errno on failure and @p's pid on
1203  * success, implies that tasklist_lock is released and wait condition
1204  * search should terminate.
1205  */
1206 static int wait_task_stopped(struct wait_opts *wo,
1207                                 int ptrace, struct task_struct *p)
1209         struct siginfo __user *infop;
1210         int retval, exit_code, *p_code, why;
1211         uid_t uid = 0; /* unneeded, required by compiler */
1212         pid_t pid;
1214         /*
1215          * Traditionally we see ptrace'd stopped tasks regardless of options.
1216          */
1217         if (!ptrace && !(wo->wo_flags & WUNTRACED))
1218                 return 0;
1220         if (!task_stopped_code(p, ptrace))
1221                 return 0;
1223         exit_code = 0;
1224         spin_lock_irq(&p->sighand->siglock);
1226         p_code = task_stopped_code(p, ptrace);
1227         if (unlikely(!p_code))
1228                 goto unlock_sig;
1230         exit_code = *p_code;
1231         if (!exit_code)
1232                 goto unlock_sig;
1234         if (!unlikely(wo->wo_flags & WNOWAIT))
1235                 *p_code = 0;
1237         uid = from_kuid_munged(current_user_ns(), task_uid(p));
1238 unlock_sig:
1239         spin_unlock_irq(&p->sighand->siglock);
1240         if (!exit_code)
1241                 return 0;
1243         /*
1244          * Now we are pretty sure this task is interesting.
1245          * Make sure it doesn't get reaped out from under us while we
1246          * give up the lock and then examine it below.  We don't want to
1247          * keep holding onto the tasklist_lock while we call getrusage and
1248          * possibly take page faults for user memory.
1249          */
1250         get_task_struct(p);
1251         pid = task_pid_vnr(p);
1252         why = ptrace ? CLD_TRAPPED : CLD_STOPPED;
1253         read_unlock(&tasklist_lock);
1255         if (unlikely(wo->wo_flags & WNOWAIT))
1256                 return wait_noreap_copyout(wo, p, pid, uid, why, exit_code);
1258         retval = wo->wo_rusage
1259                 ? getrusage(p, RUSAGE_BOTH, wo->wo_rusage) : 0;
1260         if (!retval && wo->wo_stat)
1261                 retval = put_user((exit_code << 8) | 0x7f, wo->wo_stat);
1263         infop = wo->wo_info;
1264         if (!retval && infop)
1265                 retval = put_user(SIGCHLD, &infop->si_signo);
1266         if (!retval && infop)
1267                 retval = put_user(0, &infop->si_errno);
1268         if (!retval && infop)
1269                 retval = put_user((short)why, &infop->si_code);
1270         if (!retval && infop)
1271                 retval = put_user(exit_code, &infop->si_status);
1272         if (!retval && infop)
1273                 retval = put_user(pid, &infop->si_pid);
1274         if (!retval && infop)
1275                 retval = put_user(uid, &infop->si_uid);
1276         if (!retval)
1277                 retval = pid;
1278         put_task_struct(p);
1280         BUG_ON(!retval);
1281         return retval;
1284 /*
1285  * Handle do_wait work for one task in a live, non-stopped state.
1286  * read_lock(&tasklist_lock) on entry.  If we return zero, we still hold
1287  * the lock and this task is uninteresting.  If we return nonzero, we have
1288  * released the lock and the system call should return.
1289  */
1290 static int wait_task_continued(struct wait_opts *wo, struct task_struct *p)
1292         int retval;
1293         pid_t pid;
1294         uid_t uid;
1296         if (!unlikely(wo->wo_flags & WCONTINUED))
1297                 return 0;
1299         if (!(p->signal->flags & SIGNAL_STOP_CONTINUED))
1300                 return 0;
1302         spin_lock_irq(&p->sighand->siglock);
1303         /* Re-check with the lock held.  */
1304         if (!(p->signal->flags & SIGNAL_STOP_CONTINUED)) {
1305                 spin_unlock_irq(&p->sighand->siglock);
1306                 return 0;
1307         }
1308         if (!unlikely(wo->wo_flags & WNOWAIT))
1309                 p->signal->flags &= ~SIGNAL_STOP_CONTINUED;
1310         uid = from_kuid_munged(current_user_ns(), task_uid(p));
1311         spin_unlock_irq(&p->sighand->siglock);
1313         pid = task_pid_vnr(p);
1314         get_task_struct(p);
1315         read_unlock(&tasklist_lock);
1317         if (!wo->wo_info) {
1318                 retval = wo->wo_rusage
1319                         ? getrusage(p, RUSAGE_BOTH, wo->wo_rusage) : 0;
1320                 put_task_struct(p);
1321                 if (!retval && wo->wo_stat)
1322                         retval = put_user(0xffff, wo->wo_stat);
1323                 if (!retval)
1324                         retval = pid;
1325         } else {
1326                 retval = wait_noreap_copyout(wo, p, pid, uid,
1327                                              CLD_CONTINUED, SIGCONT);
1328                 BUG_ON(retval == 0);
1329         }
1331         return retval;
1334 /*
1335  * Consider @p for a wait by @parent.
1336  *
1337  * -ECHILD should be in ->notask_error before the first call.
1338  * Returns nonzero for a final return, when we have unlocked tasklist_lock.
1339  * Returns zero if the search for a child should continue;
1340  * then ->notask_error is 0 if @p is an eligible child,
1341  * or another error from security_task_wait(), or still -ECHILD.
1342  */
1343 static int wait_consider_task(struct wait_opts *wo, int ptrace,
1344                                 struct task_struct *p)
1346         int ret = eligible_child(wo, p);
1347         if (!ret)
1348                 return ret;
1350         ret = security_task_wait(p);
1351         if (unlikely(ret < 0)) {
1352                 /*
1353                  * If we have not yet seen any eligible child,
1354                  * then let this error code replace -ECHILD.
1355                  * A permission error will give the user a clue
1356                  * to look for security policy problems, rather
1357                  * than for mysterious wait bugs.
1358                  */
1359                 if (wo->notask_error)
1360                         wo->notask_error = ret;
1361                 return 0;
1362         }
1364         /* dead body doesn't have much to contribute */
1365         if (unlikely(p->exit_state == EXIT_DEAD)) {
1366                 /*
1367                  * But do not ignore this task until the tracer does
1368                  * wait_task_zombie()->do_notify_parent().
1369                  */
1370                 if (likely(!ptrace) && unlikely(ptrace_reparented(p)))
1371                         wo->notask_error = 0;
1372                 return 0;
1373         }
1375         /* slay zombie? */
1376         if (p->exit_state == EXIT_ZOMBIE) {
1377                 /*
1378                  * A zombie ptracee is only visible to its ptracer.
1379                  * Notification and reaping will be cascaded to the real
1380                  * parent when the ptracer detaches.
1381                  */
1382                 if (likely(!ptrace) && unlikely(p->ptrace)) {
1383                         /* it will become visible, clear notask_error */
1384                         wo->notask_error = 0;
1385                         return 0;
1386                 }
1388                 /* we don't reap group leaders with subthreads */
1389                 if (!delay_group_leader(p))
1390                         return wait_task_zombie(wo, p);
1392                 /*
1393                  * Allow access to stopped/continued state via zombie by
1394                  * falling through.  Clearing of notask_error is complex.
1395                  *
1396                  * When !@ptrace:
1397                  *
1398                  * If WEXITED is set, notask_error should naturally be
1399                  * cleared.  If not, subset of WSTOPPED|WCONTINUED is set,
1400                  * so, if there are live subthreads, there are events to
1401                  * wait for.  If all subthreads are dead, it's still safe
1402                  * to clear - this function will be called again in finite
1403                  * amount time once all the subthreads are released and
1404                  * will then return without clearing.
1405                  *
1406                  * When @ptrace:
1407                  *
1408                  * Stopped state is per-task and thus can't change once the
1409                  * target task dies.  Only continued and exited can happen.
1410                  * Clear notask_error if WCONTINUED | WEXITED.
1411                  */
1412                 if (likely(!ptrace) || (wo->wo_flags & (WCONTINUED | WEXITED)))
1413                         wo->notask_error = 0;
1414         } else {
1415                 /*
1416                  * If @p is ptraced by a task in its real parent's group,
1417                  * hide group stop/continued state when looking at @p as
1418                  * the real parent; otherwise, a single stop can be
1419                  * reported twice as group and ptrace stops.
1420                  *
1421                  * If a ptracer wants to distinguish the two events for its
1422                  * own children, it should create a separate process which
1423                  * takes the role of real parent.
1424                  */
1425                 if (likely(!ptrace) && p->ptrace && !ptrace_reparented(p))
1426                         return 0;
1428                 /*
1429                  * @p is alive and it's gonna stop, continue or exit, so
1430                  * there always is something to wait for.
1431                  */
1432                 wo->notask_error = 0;
1433         }
1435         /*
1436          * Wait for stopped.  Depending on @ptrace, different stopped state
1437          * is used and the two don't interact with each other.
1438          */
1439         ret = wait_task_stopped(wo, ptrace, p);
1440         if (ret)
1441                 return ret;
1443         /*
1444          * Wait for continued.  There's only one continued state and the
1445          * ptracer can consume it which can confuse the real parent.  Don't
1446          * use WCONTINUED from ptracer.  You don't need or want it.
1447          */
1448         return wait_task_continued(wo, p);
1451 /*
1452  * Do the work of do_wait() for one thread in the group, @tsk.
1453  *
1454  * -ECHILD should be in ->notask_error before the first call.
1455  * Returns nonzero for a final return, when we have unlocked tasklist_lock.
1456  * Returns zero if the search for a child should continue; then
1457  * ->notask_error is 0 if there were any eligible children,
1458  * or another error from security_task_wait(), or still -ECHILD.
1459  */
1460 static int do_wait_thread(struct wait_opts *wo, struct task_struct *tsk)
1462         struct task_struct *p;
1464         list_for_each_entry(p, &tsk->children, sibling) {
1465                 int ret = wait_consider_task(wo, 0, p);
1466                 if (ret)
1467                         return ret;
1468         }
1470         return 0;
1473 static int ptrace_do_wait(struct wait_opts *wo, struct task_struct *tsk)
1475         struct task_struct *p;
1477         list_for_each_entry(p, &tsk->ptraced, ptrace_entry) {
1478                 int ret = wait_consider_task(wo, 1, p);
1479                 if (ret)
1480                         return ret;
1481         }
1483         return 0;
1486 static int child_wait_callback(wait_queue_t *wait, unsigned mode,
1487                                 int sync, void *key)
1489         struct wait_opts *wo = container_of(wait, struct wait_opts,
1490                                                 child_wait);
1491         struct task_struct *p = key;
1493         if (!eligible_pid(wo, p))
1494                 return 0;
1496         if ((wo->wo_flags & __WNOTHREAD) && wait->private != p->parent)
1497                 return 0;
1499         return default_wake_function(wait, mode, sync, key);
1502 void __wake_up_parent(struct task_struct *p, struct task_struct *parent)
1504         __wake_up_sync_key(&parent->signal->wait_chldexit,
1505                                 TASK_INTERRUPTIBLE, 1, p);
1508 static long do_wait(struct wait_opts *wo)
1510         struct task_struct *tsk;
1511         int retval;
1513         trace_sched_process_wait(wo->wo_pid);
1515         init_waitqueue_func_entry(&wo->child_wait, child_wait_callback);
1516         wo->child_wait.private = current;
1517         add_wait_queue(&current->signal->wait_chldexit, &wo->child_wait);
1518 repeat:
1519         /*
1520          * If there is nothing that can match our critiera just get out.
1521          * We will clear ->notask_error to zero if we see any child that
1522          * might later match our criteria, even if we are not able to reap
1523          * it yet.
1524          */
1525         wo->notask_error = -ECHILD;
1526         if ((wo->wo_type < PIDTYPE_MAX) &&
1527            (!wo->wo_pid || hlist_empty(&wo->wo_pid->tasks[wo->wo_type])))
1528                 goto notask;
1530         set_current_state(TASK_INTERRUPTIBLE);
1531         read_lock(&tasklist_lock);
1532         tsk = current;
1533         do {
1534                 retval = do_wait_thread(wo, tsk);
1535                 if (retval)
1536                         goto end;
1538                 retval = ptrace_do_wait(wo, tsk);
1539                 if (retval)
1540                         goto end;
1542                 if (wo->wo_flags & __WNOTHREAD)
1543                         break;
1544         } while_each_thread(current, tsk);
1545         read_unlock(&tasklist_lock);
1547 notask:
1548         retval = wo->notask_error;
1549         if (!retval && !(wo->wo_flags & WNOHANG)) {
1550                 retval = -ERESTARTSYS;
1551                 if (!signal_pending(current)) {
1552                         schedule();
1553                         goto repeat;
1554                 }
1555         }
1556 end:
1557         __set_current_state(TASK_RUNNING);
1558         remove_wait_queue(&current->signal->wait_chldexit, &wo->child_wait);
1559         return retval;
1562 SYSCALL_DEFINE5(waitid, int, which, pid_t, upid, struct siginfo __user *,
1563                 infop, int, options, struct rusage __user *, ru)
1565         struct wait_opts wo;
1566         struct pid *pid = NULL;
1567         enum pid_type type;
1568         long ret;
1570         if (options & ~(WNOHANG|WNOWAIT|WEXITED|WSTOPPED|WCONTINUED))
1571                 return -EINVAL;
1572         if (!(options & (WEXITED|WSTOPPED|WCONTINUED)))
1573                 return -EINVAL;
1575         switch (which) {
1576         case P_ALL:
1577                 type = PIDTYPE_MAX;
1578                 break;
1579         case P_PID:
1580                 type = PIDTYPE_PID;
1581                 if (upid <= 0)
1582                         return -EINVAL;
1583                 break;
1584         case P_PGID:
1585                 type = PIDTYPE_PGID;
1586                 if (upid <= 0)
1587                         return -EINVAL;
1588                 break;
1589         default:
1590                 return -EINVAL;
1591         }
1593         if (type < PIDTYPE_MAX)
1594                 pid = find_get_pid(upid);
1596         wo.wo_type      = type;
1597         wo.wo_pid       = pid;
1598         wo.wo_flags     = options;
1599         wo.wo_info      = infop;
1600         wo.wo_stat      = NULL;
1601         wo.wo_rusage    = ru;
1602         ret = do_wait(&wo);
1604         if (ret > 0) {
1605                 ret = 0;
1606         } else if (infop) {
1607                 /*
1608                  * For a WNOHANG return, clear out all the fields
1609                  * we would set so the user can easily tell the
1610                  * difference.
1611                  */
1612                 if (!ret)
1613                         ret = put_user(0, &infop->si_signo);
1614                 if (!ret)
1615                         ret = put_user(0, &infop->si_errno);
1616                 if (!ret)
1617                         ret = put_user(0, &infop->si_code);
1618                 if (!ret)
1619                         ret = put_user(0, &infop->si_pid);
1620                 if (!ret)
1621                         ret = put_user(0, &infop->si_uid);
1622                 if (!ret)
1623                         ret = put_user(0, &infop->si_status);
1624         }
1626         put_pid(pid);
1627         return ret;
1630 SYSCALL_DEFINE4(wait4, pid_t, upid, int __user *, stat_addr,
1631                 int, options, struct rusage __user *, ru)
1633         struct wait_opts wo;
1634         struct pid *pid = NULL;
1635         enum pid_type type;
1636         long ret;
1638         if (options & ~(WNOHANG|WUNTRACED|WCONTINUED|
1639                         __WNOTHREAD|__WCLONE|__WALL))
1640                 return -EINVAL;
1642         if (upid == -1)
1643                 type = PIDTYPE_MAX;
1644         else if (upid < 0) {
1645                 type = PIDTYPE_PGID;
1646                 pid = find_get_pid(-upid);
1647         } else if (upid == 0) {
1648                 type = PIDTYPE_PGID;
1649                 pid = get_task_pid(current, PIDTYPE_PGID);
1650         } else /* upid > 0 */ {
1651                 type = PIDTYPE_PID;
1652                 pid = find_get_pid(upid);
1653         }
1655         wo.wo_type      = type;
1656         wo.wo_pid       = pid;
1657         wo.wo_flags     = options | WEXITED;
1658         wo.wo_info      = NULL;
1659         wo.wo_stat      = stat_addr;
1660         wo.wo_rusage    = ru;
1661         ret = do_wait(&wo);
1662         put_pid(pid);
1664         return ret;
1667 #ifdef __ARCH_WANT_SYS_WAITPID
1669 /*
1670  * sys_waitpid() remains for compatibility. waitpid() should be
1671  * implemented by calling sys_wait4() from libc.a.
1672  */
1673 SYSCALL_DEFINE3(waitpid, pid_t, pid, int __user *, stat_addr, int, options)
1675         return sys_wait4(pid, stat_addr, options, NULL);
1678 #endif