1 /*
2 * linux/kernel/ptrace.c
3 *
4 * (C) Copyright 1999 Linus Torvalds
5 *
6 * Common interfaces for "ptrace()" which we do not want
7 * to continually duplicate across every architecture.
8 */
10 #include <linux/capability.h>
11 #include <linux/export.h>
12 #include <linux/sched.h>
13 #include <linux/errno.h>
14 #include <linux/mm.h>
15 #include <linux/highmem.h>
16 #include <linux/pagemap.h>
17 #include <linux/ptrace.h>
18 #include <linux/security.h>
19 #include <linux/signal.h>
20 #include <linux/audit.h>
21 #include <linux/pid_namespace.h>
22 #include <linux/syscalls.h>
23 #include <linux/uaccess.h>
24 #include <linux/regset.h>
25 #include <linux/hw_breakpoint.h>
26 #include <linux/cn_proc.h>
29 static int ptrace_trapping_sleep_fn(void *flags)
30 {
31 schedule();
32 return 0;
33 }
35 /*
36 * ptrace a task: make the debugger its new parent and
37 * move it to the ptrace list.
38 *
39 * Must be called with the tasklist lock write-held.
40 */
41 void __ptrace_link(struct task_struct *child, struct task_struct *new_parent)
42 {
43 BUG_ON(!list_empty(&child->ptrace_entry));
44 list_add(&child->ptrace_entry, &new_parent->ptraced);
45 child->parent = new_parent;
46 }
48 /**
49 * __ptrace_unlink - unlink ptracee and restore its execution state
50 * @child: ptracee to be unlinked
51 *
52 * Remove @child from the ptrace list, move it back to the original parent,
53 * and restore the execution state so that it conforms to the group stop
54 * state.
55 *
56 * Unlinking can happen via two paths - explicit PTRACE_DETACH or ptracer
57 * exiting. For PTRACE_DETACH, unless the ptracee has been killed between
58 * ptrace_check_attach() and here, it's guaranteed to be in TASK_TRACED.
59 * If the ptracer is exiting, the ptracee can be in any state.
60 *
61 * After detach, the ptracee should be in a state which conforms to the
62 * group stop. If the group is stopped or in the process of stopping, the
63 * ptracee should be put into TASK_STOPPED; otherwise, it should be woken
64 * up from TASK_TRACED.
65 *
66 * If the ptracee is in TASK_TRACED and needs to be moved to TASK_STOPPED,
67 * it goes through TRACED -> RUNNING -> STOPPED transition which is similar
68 * to but in the opposite direction of what happens while attaching to a
69 * stopped task. However, in this direction, the intermediate RUNNING
70 * state is not hidden even from the current ptracer and if it immediately
71 * re-attaches and performs a WNOHANG wait(2), it may fail.
72 *
73 * CONTEXT:
74 * write_lock_irq(tasklist_lock)
75 */
76 void __ptrace_unlink(struct task_struct *child)
77 {
78 BUG_ON(!child->ptrace);
80 child->ptrace = 0;
81 child->parent = child->real_parent;
82 list_del_init(&child->ptrace_entry);
84 spin_lock(&child->sighand->siglock);
86 /*
87 * Clear all pending traps and TRAPPING. TRAPPING should be
88 * cleared regardless of JOBCTL_STOP_PENDING. Do it explicitly.
89 */
90 task_clear_jobctl_pending(child, JOBCTL_TRAP_MASK);
91 task_clear_jobctl_trapping(child);
93 /*
94 * Reinstate JOBCTL_STOP_PENDING if group stop is in effect and
95 * @child isn't dead.
96 */
97 if (!(child->flags & PF_EXITING) &&
98 (child->signal->flags & SIGNAL_STOP_STOPPED ||
99 child->signal->group_stop_count)) {
100 child->jobctl |= JOBCTL_STOP_PENDING;
102 /*
103 * This is only possible if this thread was cloned by the
104 * traced task running in the stopped group, set the signal
105 * for the future reports.
106 * FIXME: we should change ptrace_init_task() to handle this
107 * case.
108 */
109 if (!(child->jobctl & JOBCTL_STOP_SIGMASK))
110 child->jobctl |= SIGSTOP;
111 }
113 /*
114 * If transition to TASK_STOPPED is pending or in TASK_TRACED, kick
115 * @child in the butt. Note that @resume should be used iff @child
116 * is in TASK_TRACED; otherwise, we might unduly disrupt
117 * TASK_KILLABLE sleeps.
118 */
119 if (child->jobctl & JOBCTL_STOP_PENDING || task_is_traced(child))
120 ptrace_signal_wake_up(child, true);
122 spin_unlock(&child->sighand->siglock);
123 }
125 /* Ensure that nothing can wake it up, even SIGKILL */
126 static bool ptrace_freeze_traced(struct task_struct *task)
127 {
128 bool ret = false;
130 /* Lockless, nobody but us can set this flag */
131 if (task->jobctl & JOBCTL_LISTENING)
132 return ret;
134 spin_lock_irq(&task->sighand->siglock);
135 if (task_is_traced(task) && !__fatal_signal_pending(task)) {
136 task->state = __TASK_TRACED;
137 ret = true;
138 }
139 spin_unlock_irq(&task->sighand->siglock);
141 return ret;
142 }
144 static void ptrace_unfreeze_traced(struct task_struct *task)
145 {
146 if (task->state != __TASK_TRACED)
147 return;
149 WARN_ON(!task->ptrace || task->parent != current);
151 spin_lock_irq(&task->sighand->siglock);
152 if (__fatal_signal_pending(task))
153 wake_up_state(task, __TASK_TRACED);
154 else
155 task->state = TASK_TRACED;
156 spin_unlock_irq(&task->sighand->siglock);
157 }
159 /**
160 * ptrace_check_attach - check whether ptracee is ready for ptrace operation
161 * @child: ptracee to check for
162 * @ignore_state: don't check whether @child is currently %TASK_TRACED
163 *
164 * Check whether @child is being ptraced by %current and ready for further
165 * ptrace operations. If @ignore_state is %false, @child also should be in
166 * %TASK_TRACED state and on return the child is guaranteed to be traced
167 * and not executing. If @ignore_state is %true, @child can be in any
168 * state.
169 *
170 * CONTEXT:
171 * Grabs and releases tasklist_lock and @child->sighand->siglock.
172 *
173 * RETURNS:
174 * 0 on success, -ESRCH if %child is not ready.
175 */
176 static int ptrace_check_attach(struct task_struct *child, bool ignore_state)
177 {
178 int ret = -ESRCH;
180 /*
181 * We take the read lock around doing both checks to close a
182 * possible race where someone else was tracing our child and
183 * detached between these two checks. After this locked check,
184 * we are sure that this is our traced child and that can only
185 * be changed by us so it's not changing right after this.
186 */
187 read_lock(&tasklist_lock);
188 if (child->ptrace && child->parent == current) {
189 WARN_ON(child->state == __TASK_TRACED);
190 /*
191 * child->sighand can't be NULL, release_task()
192 * does ptrace_unlink() before __exit_signal().
193 */
194 if (ignore_state || ptrace_freeze_traced(child))
195 ret = 0;
196 }
197 read_unlock(&tasklist_lock);
199 if (!ret && !ignore_state) {
200 if (!wait_task_inactive(child, __TASK_TRACED)) {
201 /*
202 * This can only happen if may_ptrace_stop() fails and
203 * ptrace_stop() changes ->state back to TASK_RUNNING,
204 * so we should not worry about leaking __TASK_TRACED.
205 */
206 WARN_ON(child->state == __TASK_TRACED);
207 ret = -ESRCH;
208 }
209 }
211 return ret;
212 }
214 static int ptrace_has_cap(struct user_namespace *ns, unsigned int mode)
215 {
216 if (mode & PTRACE_MODE_NOAUDIT)
217 return has_ns_capability_noaudit(current, ns, CAP_SYS_PTRACE);
218 else
219 return has_ns_capability(current, ns, CAP_SYS_PTRACE);
220 }
222 /* Returns 0 on success, -errno on denial. */
223 static int __ptrace_may_access(struct task_struct *task, unsigned int mode)
224 {
225 const struct cred *cred = current_cred(), *tcred;
227 /* May we inspect the given task?
228 * This check is used both for attaching with ptrace
229 * and for allowing access to sensitive information in /proc.
230 *
231 * ptrace_attach denies several cases that /proc allows
232 * because setting up the necessary parent/child relationship
233 * or halting the specified task is impossible.
234 */
235 int dumpable = 0;
236 /* Don't let security modules deny introspection */
237 if (task == current)
238 return 0;
239 rcu_read_lock();
240 tcred = __task_cred(task);
241 if (uid_eq(cred->uid, tcred->euid) &&
242 uid_eq(cred->uid, tcred->suid) &&
243 uid_eq(cred->uid, tcred->uid) &&
244 gid_eq(cred->gid, tcred->egid) &&
245 gid_eq(cred->gid, tcred->sgid) &&
246 gid_eq(cred->gid, tcred->gid))
247 goto ok;
248 if (ptrace_has_cap(tcred->user_ns, mode))
249 goto ok;
250 rcu_read_unlock();
251 return -EPERM;
252 ok:
253 rcu_read_unlock();
254 smp_rmb();
255 if (task->mm)
256 dumpable = get_dumpable(task->mm);
257 rcu_read_lock();
258 if (!dumpable && !ptrace_has_cap(__task_cred(task)->user_ns, mode)) {
259 rcu_read_unlock();
260 return -EPERM;
261 }
262 rcu_read_unlock();
264 return security_ptrace_access_check(task, mode);
265 }
267 bool ptrace_may_access(struct task_struct *task, unsigned int mode)
268 {
269 int err;
270 task_lock(task);
271 err = __ptrace_may_access(task, mode);
272 task_unlock(task);
273 return !err;
274 }
276 static int ptrace_attach(struct task_struct *task, long request,
277 unsigned long addr,
278 unsigned long flags)
279 {
280 bool seize = (request == PTRACE_SEIZE);
281 int retval;
283 retval = -EIO;
284 if (seize) {
285 if (addr != 0)
286 goto out;
287 if (flags & ~(unsigned long)PTRACE_O_MASK)
288 goto out;
289 flags = PT_PTRACED | PT_SEIZED | (flags << PT_OPT_FLAG_SHIFT);
290 } else {
291 flags = PT_PTRACED;
292 }
294 audit_ptrace(task);
296 retval = -EPERM;
297 if (unlikely(task->flags & PF_KTHREAD))
298 goto out;
299 if (same_thread_group(task, current))
300 goto out;
302 /*
303 * Protect exec's credential calculations against our interference;
304 * SUID, SGID and LSM creds get determined differently
305 * under ptrace.
306 */
307 retval = -ERESTARTNOINTR;
308 if (mutex_lock_interruptible(&task->signal->cred_guard_mutex))
309 goto out;
311 task_lock(task);
312 retval = __ptrace_may_access(task, PTRACE_MODE_ATTACH);
313 task_unlock(task);
314 if (retval)
315 goto unlock_creds;
317 write_lock_irq(&tasklist_lock);
318 retval = -EPERM;
319 if (unlikely(task->exit_state))
320 goto unlock_tasklist;
321 if (task->ptrace)
322 goto unlock_tasklist;
324 if (seize)
325 flags |= PT_SEIZED;
326 rcu_read_lock();
327 if (ns_capable(__task_cred(task)->user_ns, CAP_SYS_PTRACE))
328 flags |= PT_PTRACE_CAP;
329 rcu_read_unlock();
330 task->ptrace = flags;
332 __ptrace_link(task, current);
334 /* SEIZE doesn't trap tracee on attach */
335 if (!seize)
336 send_sig_info(SIGSTOP, SEND_SIG_FORCED, task);
338 spin_lock(&task->sighand->siglock);
340 /*
341 * If the task is already STOPPED, set JOBCTL_TRAP_STOP and
342 * TRAPPING, and kick it so that it transits to TRACED. TRAPPING
343 * will be cleared if the child completes the transition or any
344 * event which clears the group stop states happens. We'll wait
345 * for the transition to complete before returning from this
346 * function.
347 *
348 * This hides STOPPED -> RUNNING -> TRACED transition from the
349 * attaching thread but a different thread in the same group can
350 * still observe the transient RUNNING state. IOW, if another
351 * thread's WNOHANG wait(2) on the stopped tracee races against
352 * ATTACH, the wait(2) may fail due to the transient RUNNING.
353 *
354 * The following task_is_stopped() test is safe as both transitions
355 * in and out of STOPPED are protected by siglock.
356 */
357 if (task_is_stopped(task) &&
358 task_set_jobctl_pending(task, JOBCTL_TRAP_STOP | JOBCTL_TRAPPING))
359 signal_wake_up_state(task, __TASK_STOPPED);
361 spin_unlock(&task->sighand->siglock);
363 retval = 0;
364 unlock_tasklist:
365 write_unlock_irq(&tasklist_lock);
366 unlock_creds:
367 mutex_unlock(&task->signal->cred_guard_mutex);
368 out:
369 if (!retval) {
370 wait_on_bit(&task->jobctl, JOBCTL_TRAPPING_BIT,
371 ptrace_trapping_sleep_fn, TASK_UNINTERRUPTIBLE);
372 proc_ptrace_connector(task, PTRACE_ATTACH);
373 }
375 return retval;
376 }
378 /**
379 * ptrace_traceme -- helper for PTRACE_TRACEME
380 *
381 * Performs checks and sets PT_PTRACED.
382 * Should be used by all ptrace implementations for PTRACE_TRACEME.
383 */
384 static int ptrace_traceme(void)
385 {
386 int ret = -EPERM;
388 write_lock_irq(&tasklist_lock);
389 /* Are we already being traced? */
390 if (!current->ptrace) {
391 ret = security_ptrace_traceme(current->parent);
392 /*
393 * Check PF_EXITING to ensure ->real_parent has not passed
394 * exit_ptrace(). Otherwise we don't report the error but
395 * pretend ->real_parent untraces us right after return.
396 */
397 if (!ret && !(current->real_parent->flags & PF_EXITING)) {
398 current->ptrace = PT_PTRACED;
399 __ptrace_link(current, current->real_parent);
400 }
401 }
402 write_unlock_irq(&tasklist_lock);
404 return ret;
405 }
407 /*
408 * Called with irqs disabled, returns true if childs should reap themselves.
409 */
410 static int ignoring_children(struct sighand_struct *sigh)
411 {
412 int ret;
413 spin_lock(&sigh->siglock);
414 ret = (sigh->action[SIGCHLD-1].sa.sa_handler == SIG_IGN) ||
415 (sigh->action[SIGCHLD-1].sa.sa_flags & SA_NOCLDWAIT);
416 spin_unlock(&sigh->siglock);
417 return ret;
418 }
420 /*
421 * Called with tasklist_lock held for writing.
422 * Unlink a traced task, and clean it up if it was a traced zombie.
423 * Return true if it needs to be reaped with release_task().
424 * (We can't call release_task() here because we already hold tasklist_lock.)
425 *
426 * If it's a zombie, our attachedness prevented normal parent notification
427 * or self-reaping. Do notification now if it would have happened earlier.
428 * If it should reap itself, return true.
429 *
430 * If it's our own child, there is no notification to do. But if our normal
431 * children self-reap, then this child was prevented by ptrace and we must
432 * reap it now, in that case we must also wake up sub-threads sleeping in
433 * do_wait().
434 */
435 static bool __ptrace_detach(struct task_struct *tracer, struct task_struct *p)
436 {
437 bool dead;
439 __ptrace_unlink(p);
441 if (p->exit_state != EXIT_ZOMBIE)
442 return false;
444 dead = !thread_group_leader(p);
446 if (!dead && thread_group_empty(p)) {
447 if (!same_thread_group(p->real_parent, tracer))
448 dead = do_notify_parent(p, p->exit_signal);
449 else if (ignoring_children(tracer->sighand)) {
450 __wake_up_parent(p, tracer);
451 dead = true;
452 }
453 }
454 /* Mark it as in the process of being reaped. */
455 if (dead)
456 p->exit_state = EXIT_DEAD;
457 return dead;
458 }
460 static int ptrace_detach(struct task_struct *child, unsigned int data)
461 {
462 bool dead = false;
464 if (!valid_signal(data))
465 return -EIO;
467 /* Architecture-specific hardware disable .. */
468 ptrace_disable(child);
469 clear_tsk_thread_flag(child, TIF_SYSCALL_TRACE);
471 write_lock_irq(&tasklist_lock);
472 /*
473 * This child can be already killed. Make sure de_thread() or
474 * our sub-thread doing do_wait() didn't do release_task() yet.
475 */
476 if (child->ptrace) {
477 child->exit_code = data;
478 dead = __ptrace_detach(current, child);
479 }
480 write_unlock_irq(&tasklist_lock);
482 proc_ptrace_connector(child, PTRACE_DETACH);
483 if (unlikely(dead))
484 release_task(child);
486 return 0;
487 }
489 /*
490 * Detach all tasks we were using ptrace on. Called with tasklist held
491 * for writing, and returns with it held too. But note it can release
492 * and reacquire the lock.
493 */
494 void exit_ptrace(struct task_struct *tracer)
495 __releases(&tasklist_lock)
496 __acquires(&tasklist_lock)
497 {
498 struct task_struct *p, *n;
499 LIST_HEAD(ptrace_dead);
501 if (likely(list_empty(&tracer->ptraced)))
502 return;
504 list_for_each_entry_safe(p, n, &tracer->ptraced, ptrace_entry) {
505 if (unlikely(p->ptrace & PT_EXITKILL))
506 send_sig_info(SIGKILL, SEND_SIG_FORCED, p);
508 if (__ptrace_detach(tracer, p))
509 list_add(&p->ptrace_entry, &ptrace_dead);
510 }
512 write_unlock_irq(&tasklist_lock);
513 BUG_ON(!list_empty(&tracer->ptraced));
515 list_for_each_entry_safe(p, n, &ptrace_dead, ptrace_entry) {
516 list_del_init(&p->ptrace_entry);
517 release_task(p);
518 }
520 write_lock_irq(&tasklist_lock);
521 }
523 int ptrace_readdata(struct task_struct *tsk, unsigned long src, char __user *dst, int len)
524 {
525 int copied = 0;
527 while (len > 0) {
528 char buf[128];
529 int this_len, retval;
531 this_len = (len > sizeof(buf)) ? sizeof(buf) : len;
532 retval = access_process_vm(tsk, src, buf, this_len, 0);
533 if (!retval) {
534 if (copied)
535 break;
536 return -EIO;
537 }
538 if (copy_to_user(dst, buf, retval))
539 return -EFAULT;
540 copied += retval;
541 src += retval;
542 dst += retval;
543 len -= retval;
544 }
545 return copied;
546 }
548 int ptrace_writedata(struct task_struct *tsk, char __user *src, unsigned long dst, int len)
549 {
550 int copied = 0;
552 while (len > 0) {
553 char buf[128];
554 int this_len, retval;
556 this_len = (len > sizeof(buf)) ? sizeof(buf) : len;
557 if (copy_from_user(buf, src, this_len))
558 return -EFAULT;
559 retval = access_process_vm(tsk, dst, buf, this_len, 1);
560 if (!retval) {
561 if (copied)
562 break;
563 return -EIO;
564 }
565 copied += retval;
566 src += retval;
567 dst += retval;
568 len -= retval;
569 }
570 return copied;
571 }
573 static int ptrace_setoptions(struct task_struct *child, unsigned long data)
574 {
575 unsigned flags;
577 if (data & ~(unsigned long)PTRACE_O_MASK)
578 return -EINVAL;
580 /* Avoid intermediate state when all opts are cleared */
581 flags = child->ptrace;
582 flags &= ~(PTRACE_O_MASK << PT_OPT_FLAG_SHIFT);
583 flags |= (data << PT_OPT_FLAG_SHIFT);
584 child->ptrace = flags;
586 return 0;
587 }
589 static int ptrace_getsiginfo(struct task_struct *child, siginfo_t *info)
590 {
591 unsigned long flags;
592 int error = -ESRCH;
594 if (lock_task_sighand(child, &flags)) {
595 error = -EINVAL;
596 if (likely(child->last_siginfo != NULL)) {
597 *info = *child->last_siginfo;
598 error = 0;
599 }
600 unlock_task_sighand(child, &flags);
601 }
602 return error;
603 }
605 static int ptrace_setsiginfo(struct task_struct *child, const siginfo_t *info)
606 {
607 unsigned long flags;
608 int error = -ESRCH;
610 if (lock_task_sighand(child, &flags)) {
611 error = -EINVAL;
612 if (likely(child->last_siginfo != NULL)) {
613 *child->last_siginfo = *info;
614 error = 0;
615 }
616 unlock_task_sighand(child, &flags);
617 }
618 return error;
619 }
622 #ifdef PTRACE_SINGLESTEP
623 #define is_singlestep(request) ((request) == PTRACE_SINGLESTEP)
624 #else
625 #define is_singlestep(request) 0
626 #endif
628 #ifdef PTRACE_SINGLEBLOCK
629 #define is_singleblock(request) ((request) == PTRACE_SINGLEBLOCK)
630 #else
631 #define is_singleblock(request) 0
632 #endif
634 #ifdef PTRACE_SYSEMU
635 #define is_sysemu_singlestep(request) ((request) == PTRACE_SYSEMU_SINGLESTEP)
636 #else
637 #define is_sysemu_singlestep(request) 0
638 #endif
640 static int ptrace_resume(struct task_struct *child, long request,
641 unsigned long data)
642 {
643 if (!valid_signal(data))
644 return -EIO;
646 if (request == PTRACE_SYSCALL)
647 set_tsk_thread_flag(child, TIF_SYSCALL_TRACE);
648 else
649 clear_tsk_thread_flag(child, TIF_SYSCALL_TRACE);
651 #ifdef TIF_SYSCALL_EMU
652 if (request == PTRACE_SYSEMU || request == PTRACE_SYSEMU_SINGLESTEP)
653 set_tsk_thread_flag(child, TIF_SYSCALL_EMU);
654 else
655 clear_tsk_thread_flag(child, TIF_SYSCALL_EMU);
656 #endif
658 if (is_singleblock(request)) {
659 if (unlikely(!arch_has_block_step()))
660 return -EIO;
661 user_enable_block_step(child);
662 } else if (is_singlestep(request) || is_sysemu_singlestep(request)) {
663 if (unlikely(!arch_has_single_step()))
664 return -EIO;
665 user_enable_single_step(child);
666 } else {
667 user_disable_single_step(child);
668 }
670 child->exit_code = data;
671 wake_up_state(child, __TASK_TRACED);
673 return 0;
674 }
676 #ifdef CONFIG_HAVE_ARCH_TRACEHOOK
678 static const struct user_regset *
679 find_regset(const struct user_regset_view *view, unsigned int type)
680 {
681 const struct user_regset *regset;
682 int n;
684 for (n = 0; n < view->n; ++n) {
685 regset = view->regsets + n;
686 if (regset->core_note_type == type)
687 return regset;
688 }
690 return NULL;
691 }
693 static int ptrace_regset(struct task_struct *task, int req, unsigned int type,
694 struct iovec *kiov)
695 {
696 const struct user_regset_view *view = task_user_regset_view(task);
697 const struct user_regset *regset = find_regset(view, type);
698 int regset_no;
700 if (!regset || (kiov->iov_len % regset->size) != 0)
701 return -EINVAL;
703 regset_no = regset - view->regsets;
704 kiov->iov_len = min(kiov->iov_len,
705 (__kernel_size_t) (regset->n * regset->size));
707 if (req == PTRACE_GETREGSET)
708 return copy_regset_to_user(task, view, regset_no, 0,
709 kiov->iov_len, kiov->iov_base);
710 else
711 return copy_regset_from_user(task, view, regset_no, 0,
712 kiov->iov_len, kiov->iov_base);
713 }
715 #endif
717 int ptrace_request(struct task_struct *child, long request,
718 unsigned long addr, unsigned long data)
719 {
720 bool seized = child->ptrace & PT_SEIZED;
721 int ret = -EIO;
722 siginfo_t siginfo, *si;
723 void __user *datavp = (void __user *) data;
724 unsigned long __user *datalp = datavp;
725 unsigned long flags;
727 switch (request) {
728 case PTRACE_PEEKTEXT:
729 case PTRACE_PEEKDATA:
730 return generic_ptrace_peekdata(child, addr, data);
731 case PTRACE_POKETEXT:
732 case PTRACE_POKEDATA:
733 return generic_ptrace_pokedata(child, addr, data);
735 #ifdef PTRACE_OLDSETOPTIONS
736 case PTRACE_OLDSETOPTIONS:
737 #endif
738 case PTRACE_SETOPTIONS:
739 ret = ptrace_setoptions(child, data);
740 break;
741 case PTRACE_GETEVENTMSG:
742 ret = put_user(child->ptrace_message, datalp);
743 break;
745 case PTRACE_GETSIGINFO:
746 ret = ptrace_getsiginfo(child, &siginfo);
747 if (!ret)
748 ret = copy_siginfo_to_user(datavp, &siginfo);
749 break;
751 case PTRACE_SETSIGINFO:
752 if (copy_from_user(&siginfo, datavp, sizeof siginfo))
753 ret = -EFAULT;
754 else
755 ret = ptrace_setsiginfo(child, &siginfo);
756 break;
758 case PTRACE_INTERRUPT:
759 /*
760 * Stop tracee without any side-effect on signal or job
761 * control. At least one trap is guaranteed to happen
762 * after this request. If @child is already trapped, the
763 * current trap is not disturbed and another trap will
764 * happen after the current trap is ended with PTRACE_CONT.
765 *
766 * The actual trap might not be PTRACE_EVENT_STOP trap but
767 * the pending condition is cleared regardless.
768 */
769 if (unlikely(!seized || !lock_task_sighand(child, &flags)))
770 break;
772 /*
773 * INTERRUPT doesn't disturb existing trap sans one
774 * exception. If ptracer issued LISTEN for the current
775 * STOP, this INTERRUPT should clear LISTEN and re-trap
776 * tracee into STOP.
777 */
778 if (likely(task_set_jobctl_pending(child, JOBCTL_TRAP_STOP)))
779 ptrace_signal_wake_up(child, child->jobctl & JOBCTL_LISTENING);
781 unlock_task_sighand(child, &flags);
782 ret = 0;
783 break;
785 case PTRACE_LISTEN:
786 /*
787 * Listen for events. Tracee must be in STOP. It's not
788 * resumed per-se but is not considered to be in TRACED by
789 * wait(2) or ptrace(2). If an async event (e.g. group
790 * stop state change) happens, tracee will enter STOP trap
791 * again. Alternatively, ptracer can issue INTERRUPT to
792 * finish listening and re-trap tracee into STOP.
793 */
794 if (unlikely(!seized || !lock_task_sighand(child, &flags)))
795 break;
797 si = child->last_siginfo;
798 if (likely(si && (si->si_code >> 8) == PTRACE_EVENT_STOP)) {
799 child->jobctl |= JOBCTL_LISTENING;
800 /*
801 * If NOTIFY is set, it means event happened between
802 * start of this trap and now. Trigger re-trap.
803 */
804 if (child->jobctl & JOBCTL_TRAP_NOTIFY)
805 ptrace_signal_wake_up(child, true);
806 ret = 0;
807 }
808 unlock_task_sighand(child, &flags);
809 break;
811 case PTRACE_DETACH: /* detach a process that was attached. */
812 ret = ptrace_detach(child, data);
813 break;
815 #ifdef CONFIG_BINFMT_ELF_FDPIC
816 case PTRACE_GETFDPIC: {
817 struct mm_struct *mm = get_task_mm(child);
818 unsigned long tmp = 0;
820 ret = -ESRCH;
821 if (!mm)
822 break;
824 switch (addr) {
825 case PTRACE_GETFDPIC_EXEC:
826 tmp = mm->context.exec_fdpic_loadmap;
827 break;
828 case PTRACE_GETFDPIC_INTERP:
829 tmp = mm->context.interp_fdpic_loadmap;
830 break;
831 default:
832 break;
833 }
834 mmput(mm);
836 ret = put_user(tmp, datalp);
837 break;
838 }
839 #endif
841 #ifdef PTRACE_SINGLESTEP
842 case PTRACE_SINGLESTEP:
843 #endif
844 #ifdef PTRACE_SINGLEBLOCK
845 case PTRACE_SINGLEBLOCK:
846 #endif
847 #ifdef PTRACE_SYSEMU
848 case PTRACE_SYSEMU:
849 case PTRACE_SYSEMU_SINGLESTEP:
850 #endif
851 case PTRACE_SYSCALL:
852 case PTRACE_CONT:
853 return ptrace_resume(child, request, data);
855 case PTRACE_KILL:
856 if (child->exit_state) /* already dead */
857 return 0;
858 return ptrace_resume(child, request, SIGKILL);
860 #ifdef CONFIG_HAVE_ARCH_TRACEHOOK
861 case PTRACE_GETREGSET:
862 case PTRACE_SETREGSET:
863 {
864 struct iovec kiov;
865 struct iovec __user *uiov = datavp;
867 if (!access_ok(VERIFY_WRITE, uiov, sizeof(*uiov)))
868 return -EFAULT;
870 if (__get_user(kiov.iov_base, &uiov->iov_base) ||
871 __get_user(kiov.iov_len, &uiov->iov_len))
872 return -EFAULT;
874 ret = ptrace_regset(child, request, addr, &kiov);
875 if (!ret)
876 ret = __put_user(kiov.iov_len, &uiov->iov_len);
877 break;
878 }
879 #endif
880 default:
881 break;
882 }
884 return ret;
885 }
887 static struct task_struct *ptrace_get_task_struct(pid_t pid)
888 {
889 struct task_struct *child;
891 rcu_read_lock();
892 child = find_task_by_vpid(pid);
893 if (child)
894 get_task_struct(child);
895 rcu_read_unlock();
897 if (!child)
898 return ERR_PTR(-ESRCH);
899 return child;
900 }
902 #ifndef arch_ptrace_attach
903 #define arch_ptrace_attach(child) do { } while (0)
904 #endif
906 SYSCALL_DEFINE4(ptrace, long, request, long, pid, unsigned long, addr,
907 unsigned long, data)
908 {
909 struct task_struct *child;
910 long ret;
912 if (request == PTRACE_TRACEME) {
913 ret = ptrace_traceme();
914 if (!ret)
915 arch_ptrace_attach(current);
916 goto out;
917 }
919 child = ptrace_get_task_struct(pid);
920 if (IS_ERR(child)) {
921 ret = PTR_ERR(child);
922 goto out;
923 }
925 if (request == PTRACE_ATTACH || request == PTRACE_SEIZE) {
926 ret = ptrace_attach(child, request, addr, data);
927 /*
928 * Some architectures need to do book-keeping after
929 * a ptrace attach.
930 */
931 if (!ret)
932 arch_ptrace_attach(child);
933 goto out_put_task_struct;
934 }
936 ret = ptrace_check_attach(child, request == PTRACE_KILL ||
937 request == PTRACE_INTERRUPT);
938 if (ret < 0)
939 goto out_put_task_struct;
941 ret = arch_ptrace(child, request, addr, data);
942 if (ret || request != PTRACE_DETACH)
943 ptrace_unfreeze_traced(child);
945 out_put_task_struct:
946 put_task_struct(child);
947 out:
948 return ret;
949 }
951 int generic_ptrace_peekdata(struct task_struct *tsk, unsigned long addr,
952 unsigned long data)
953 {
954 unsigned long tmp;
955 int copied;
957 copied = access_process_vm(tsk, addr, &tmp, sizeof(tmp), 0);
958 if (copied != sizeof(tmp))
959 return -EIO;
960 return put_user(tmp, (unsigned long __user *)data);
961 }
963 int generic_ptrace_pokedata(struct task_struct *tsk, unsigned long addr,
964 unsigned long data)
965 {
966 int copied;
968 copied = access_process_vm(tsk, addr, &data, sizeof(data), 1);
969 return (copied == sizeof(data)) ? 0 : -EIO;
970 }
972 #if defined CONFIG_COMPAT
973 #include <linux/compat.h>
975 int compat_ptrace_request(struct task_struct *child, compat_long_t request,
976 compat_ulong_t addr, compat_ulong_t data)
977 {
978 compat_ulong_t __user *datap = compat_ptr(data);
979 compat_ulong_t word;
980 siginfo_t siginfo;
981 int ret;
983 switch (request) {
984 case PTRACE_PEEKTEXT:
985 case PTRACE_PEEKDATA:
986 ret = access_process_vm(child, addr, &word, sizeof(word), 0);
987 if (ret != sizeof(word))
988 ret = -EIO;
989 else
990 ret = put_user(word, datap);
991 break;
993 case PTRACE_POKETEXT:
994 case PTRACE_POKEDATA:
995 ret = access_process_vm(child, addr, &data, sizeof(data), 1);
996 ret = (ret != sizeof(data) ? -EIO : 0);
997 break;
999 case PTRACE_GETEVENTMSG:
1000 ret = put_user((compat_ulong_t) child->ptrace_message, datap);
1001 break;
1003 case PTRACE_GETSIGINFO:
1004 ret = ptrace_getsiginfo(child, &siginfo);
1005 if (!ret)
1006 ret = copy_siginfo_to_user32(
1007 (struct compat_siginfo __user *) datap,
1008 &siginfo);
1009 break;
1011 case PTRACE_SETSIGINFO:
1012 memset(&siginfo, 0, sizeof siginfo);
1013 if (copy_siginfo_from_user32(
1014 &siginfo, (struct compat_siginfo __user *) datap))
1015 ret = -EFAULT;
1016 else
1017 ret = ptrace_setsiginfo(child, &siginfo);
1018 break;
1019 #ifdef CONFIG_HAVE_ARCH_TRACEHOOK
1020 case PTRACE_GETREGSET:
1021 case PTRACE_SETREGSET:
1022 {
1023 struct iovec kiov;
1024 struct compat_iovec __user *uiov =
1025 (struct compat_iovec __user *) datap;
1026 compat_uptr_t ptr;
1027 compat_size_t len;
1029 if (!access_ok(VERIFY_WRITE, uiov, sizeof(*uiov)))
1030 return -EFAULT;
1032 if (__get_user(ptr, &uiov->iov_base) ||
1033 __get_user(len, &uiov->iov_len))
1034 return -EFAULT;
1036 kiov.iov_base = compat_ptr(ptr);
1037 kiov.iov_len = len;
1039 ret = ptrace_regset(child, request, addr, &kiov);
1040 if (!ret)
1041 ret = __put_user(kiov.iov_len, &uiov->iov_len);
1042 break;
1043 }
1044 #endif
1046 default:
1047 ret = ptrace_request(child, request, addr, data);
1048 }
1050 return ret;
1051 }
1053 asmlinkage long compat_sys_ptrace(compat_long_t request, compat_long_t pid,
1054 compat_long_t addr, compat_long_t data)
1055 {
1056 struct task_struct *child;
1057 long ret;
1059 if (request == PTRACE_TRACEME) {
1060 ret = ptrace_traceme();
1061 goto out;
1062 }
1064 child = ptrace_get_task_struct(pid);
1065 if (IS_ERR(child)) {
1066 ret = PTR_ERR(child);
1067 goto out;
1068 }
1070 if (request == PTRACE_ATTACH || request == PTRACE_SEIZE) {
1071 ret = ptrace_attach(child, request, addr, data);
1072 /*
1073 * Some architectures need to do book-keeping after
1074 * a ptrace attach.
1075 */
1076 if (!ret)
1077 arch_ptrace_attach(child);
1078 goto out_put_task_struct;
1079 }
1081 ret = ptrace_check_attach(child, request == PTRACE_KILL ||
1082 request == PTRACE_INTERRUPT);
1083 if (!ret) {
1084 ret = compat_arch_ptrace(child, request, addr, data);
1085 if (ret || request != PTRACE_DETACH)
1086 ptrace_unfreeze_traced(child);
1087 }
1089 out_put_task_struct:
1090 put_task_struct(child);
1091 out:
1092 return ret;
1093 }
1094 #endif /* CONFIG_COMPAT */
1096 #ifdef CONFIG_HAVE_HW_BREAKPOINT
1097 int ptrace_get_breakpoints(struct task_struct *tsk)
1098 {
1099 if (atomic_inc_not_zero(&tsk->ptrace_bp_refcnt))
1100 return 0;
1102 return -1;
1103 }
1105 void ptrace_put_breakpoints(struct task_struct *tsk)
1106 {
1107 if (atomic_dec_and_test(&tsk->ptrace_bp_refcnt))
1108 flush_ptrace_hw_breakpoint(tsk);
1109 }
1110 #endif /* CONFIG_HAVE_HW_BREAKPOINT */