]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/blob - kernel/srcu.c
Merge branch 'p-ti-android-3.8.y-video'
[android-sdk/kernel-video.git] / kernel / srcu.c
1 /*
2  * Sleepable Read-Copy Update mechanism for mutual exclusion.
3  *
4  * This program is free software; you can redistribute it and/or modify
5  * it under the terms of the GNU General Public License as published by
6  * the Free Software Foundation; either version 2 of the License, or
7  * (at your option) any later version.
8  *
9  * This program is distributed in the hope that it will be useful,
10  * but WITHOUT ANY WARRANTY; without even the implied warranty of
11  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
12  * GNU General Public License for more details.
13  *
14  * You should have received a copy of the GNU General Public License
15  * along with this program; if not, write to the Free Software
16  * Foundation, Inc., 59 Temple Place - Suite 330, Boston, MA 02111-1307, USA.
17  *
18  * Copyright (C) IBM Corporation, 2006
19  * Copyright (C) Fujitsu, 2012
20  *
21  * Author: Paul McKenney <paulmck@us.ibm.com>
22  *         Lai Jiangshan <laijs@cn.fujitsu.com>
23  *
24  * For detailed explanation of Read-Copy Update mechanism see -
25  *              Documentation/RCU/ *.txt
26  *
27  */
29 #include <linux/export.h>
30 #include <linux/mutex.h>
31 #include <linux/percpu.h>
32 #include <linux/preempt.h>
33 #include <linux/rcupdate.h>
34 #include <linux/sched.h>
35 #include <linux/smp.h>
36 #include <linux/delay.h>
37 #include <linux/srcu.h>
39 #include <trace/events/rcu.h>
41 #include "rcu.h"
43 /*
44  * Initialize an rcu_batch structure to empty.
45  */
46 static inline void rcu_batch_init(struct rcu_batch *b)
47 {
48         b->head = NULL;
49         b->tail = &b->head;
50 }
52 /*
53  * Enqueue a callback onto the tail of the specified rcu_batch structure.
54  */
55 static inline void rcu_batch_queue(struct rcu_batch *b, struct rcu_head *head)
56 {
57         *b->tail = head;
58         b->tail = &head->next;
59 }
61 /*
62  * Is the specified rcu_batch structure empty?
63  */
64 static inline bool rcu_batch_empty(struct rcu_batch *b)
65 {
66         return b->tail == &b->head;
67 }
69 /*
70  * Remove the callback at the head of the specified rcu_batch structure
71  * and return a pointer to it, or return NULL if the structure is empty.
72  */
73 static inline struct rcu_head *rcu_batch_dequeue(struct rcu_batch *b)
74 {
75         struct rcu_head *head;
77         if (rcu_batch_empty(b))
78                 return NULL;
80         head = b->head;
81         b->head = head->next;
82         if (b->tail == &head->next)
83                 rcu_batch_init(b);
85         return head;
86 }
88 /*
89  * Move all callbacks from the rcu_batch structure specified by "from" to
90  * the structure specified by "to".
91  */
92 static inline void rcu_batch_move(struct rcu_batch *to, struct rcu_batch *from)
93 {
94         if (!rcu_batch_empty(from)) {
95                 *to->tail = from->head;
96                 to->tail = from->tail;
97                 rcu_batch_init(from);
98         }
99 }
101 static int init_srcu_struct_fields(struct srcu_struct *sp)
103         sp->completed = 0;
104         spin_lock_init(&sp->queue_lock);
105         sp->running = false;
106         rcu_batch_init(&sp->batch_queue);
107         rcu_batch_init(&sp->batch_check0);
108         rcu_batch_init(&sp->batch_check1);
109         rcu_batch_init(&sp->batch_done);
110         INIT_DELAYED_WORK(&sp->work, process_srcu);
111         sp->per_cpu_ref = alloc_percpu(struct srcu_struct_array);
112         return sp->per_cpu_ref ? 0 : -ENOMEM;
115 #ifdef CONFIG_DEBUG_LOCK_ALLOC
117 int __init_srcu_struct(struct srcu_struct *sp, const char *name,
118                        struct lock_class_key *key)
120         /* Don't re-initialize a lock while it is held. */
121         debug_check_no_locks_freed((void *)sp, sizeof(*sp));
122         lockdep_init_map(&sp->dep_map, name, key, 0);
123         return init_srcu_struct_fields(sp);
125 EXPORT_SYMBOL_GPL(__init_srcu_struct);
127 #else /* #ifdef CONFIG_DEBUG_LOCK_ALLOC */
129 /**
130  * init_srcu_struct - initialize a sleep-RCU structure
131  * @sp: structure to initialize.
132  *
133  * Must invoke this on a given srcu_struct before passing that srcu_struct
134  * to any other function.  Each srcu_struct represents a separate domain
135  * of SRCU protection.
136  */
137 int init_srcu_struct(struct srcu_struct *sp)
139         return init_srcu_struct_fields(sp);
141 EXPORT_SYMBOL_GPL(init_srcu_struct);
143 #endif /* #else #ifdef CONFIG_DEBUG_LOCK_ALLOC */
145 /*
146  * Returns approximate total of the readers' ->seq[] values for the
147  * rank of per-CPU counters specified by idx.
148  */
149 static unsigned long srcu_readers_seq_idx(struct srcu_struct *sp, int idx)
151         int cpu;
152         unsigned long sum = 0;
153         unsigned long t;
155         for_each_possible_cpu(cpu) {
156                 t = ACCESS_ONCE(per_cpu_ptr(sp->per_cpu_ref, cpu)->seq[idx]);
157                 sum += t;
158         }
159         return sum;
162 /*
163  * Returns approximate number of readers active on the specified rank
164  * of the per-CPU ->c[] counters.
165  */
166 static unsigned long srcu_readers_active_idx(struct srcu_struct *sp, int idx)
168         int cpu;
169         unsigned long sum = 0;
170         unsigned long t;
172         for_each_possible_cpu(cpu) {
173                 t = ACCESS_ONCE(per_cpu_ptr(sp->per_cpu_ref, cpu)->c[idx]);
174                 sum += t;
175         }
176         return sum;
179 /*
180  * Return true if the number of pre-existing readers is determined to
181  * be stably zero.  An example unstable zero can occur if the call
182  * to srcu_readers_active_idx() misses an __srcu_read_lock() increment,
183  * but due to task migration, sees the corresponding __srcu_read_unlock()
184  * decrement.  This can happen because srcu_readers_active_idx() takes
185  * time to sum the array, and might in fact be interrupted or preempted
186  * partway through the summation.
187  */
188 static bool srcu_readers_active_idx_check(struct srcu_struct *sp, int idx)
190         unsigned long seq;
192         seq = srcu_readers_seq_idx(sp, idx);
194         /*
195          * The following smp_mb() A pairs with the smp_mb() B located in
196          * __srcu_read_lock().  This pairing ensures that if an
197          * __srcu_read_lock() increments its counter after the summation
198          * in srcu_readers_active_idx(), then the corresponding SRCU read-side
199          * critical section will see any changes made prior to the start
200          * of the current SRCU grace period.
201          *
202          * Also, if the above call to srcu_readers_seq_idx() saw the
203          * increment of ->seq[], then the call to srcu_readers_active_idx()
204          * must see the increment of ->c[].
205          */
206         smp_mb(); /* A */
208         /*
209          * Note that srcu_readers_active_idx() can incorrectly return
210          * zero even though there is a pre-existing reader throughout.
211          * To see this, suppose that task A is in a very long SRCU
212          * read-side critical section that started on CPU 0, and that
213          * no other reader exists, so that the sum of the counters
214          * is equal to one.  Then suppose that task B starts executing
215          * srcu_readers_active_idx(), summing up to CPU 1, and then that
216          * task C starts reading on CPU 0, so that its increment is not
217          * summed, but finishes reading on CPU 2, so that its decrement
218          * -is- summed.  Then when task B completes its sum, it will
219          * incorrectly get zero, despite the fact that task A has been
220          * in its SRCU read-side critical section the whole time.
221          *
222          * We therefore do a validation step should srcu_readers_active_idx()
223          * return zero.
224          */
225         if (srcu_readers_active_idx(sp, idx) != 0)
226                 return false;
228         /*
229          * The remainder of this function is the validation step.
230          * The following smp_mb() D pairs with the smp_mb() C in
231          * __srcu_read_unlock().  If the __srcu_read_unlock() was seen
232          * by srcu_readers_active_idx() above, then any destructive
233          * operation performed after the grace period will happen after
234          * the corresponding SRCU read-side critical section.
235          *
236          * Note that there can be at most NR_CPUS worth of readers using
237          * the old index, which is not enough to overflow even a 32-bit
238          * integer.  (Yes, this does mean that systems having more than
239          * a billion or so CPUs need to be 64-bit systems.)  Therefore,
240          * the sum of the ->seq[] counters cannot possibly overflow.
241          * Therefore, the only way that the return values of the two
242          * calls to srcu_readers_seq_idx() can be equal is if there were
243          * no increments of the corresponding rank of ->seq[] counts
244          * in the interim.  But the missed-increment scenario laid out
245          * above includes an increment of the ->seq[] counter by
246          * the corresponding __srcu_read_lock().  Therefore, if this
247          * scenario occurs, the return values from the two calls to
248          * srcu_readers_seq_idx() will differ, and thus the validation
249          * step below suffices.
250          */
251         smp_mb(); /* D */
253         return srcu_readers_seq_idx(sp, idx) == seq;
256 /**
257  * srcu_readers_active - returns approximate number of readers.
258  * @sp: which srcu_struct to count active readers (holding srcu_read_lock).
259  *
260  * Note that this is not an atomic primitive, and can therefore suffer
261  * severe errors when invoked on an active srcu_struct.  That said, it
262  * can be useful as an error check at cleanup time.
263  */
264 static int srcu_readers_active(struct srcu_struct *sp)
266         int cpu;
267         unsigned long sum = 0;
269         for_each_possible_cpu(cpu) {
270                 sum += ACCESS_ONCE(per_cpu_ptr(sp->per_cpu_ref, cpu)->c[0]);
271                 sum += ACCESS_ONCE(per_cpu_ptr(sp->per_cpu_ref, cpu)->c[1]);
272         }
273         return sum;
276 /**
277  * cleanup_srcu_struct - deconstruct a sleep-RCU structure
278  * @sp: structure to clean up.
279  *
280  * Must invoke this after you are finished using a given srcu_struct that
281  * was initialized via init_srcu_struct(), else you leak memory.
282  */
283 void cleanup_srcu_struct(struct srcu_struct *sp)
285         int sum;
287         sum = srcu_readers_active(sp);
288         WARN_ON(sum);  /* Leakage unless caller handles error. */
289         if (sum != 0)
290                 return;
291         free_percpu(sp->per_cpu_ref);
292         sp->per_cpu_ref = NULL;
294 EXPORT_SYMBOL_GPL(cleanup_srcu_struct);
296 /*
297  * Counts the new reader in the appropriate per-CPU element of the
298  * srcu_struct.  Must be called from process context.
299  * Returns an index that must be passed to the matching srcu_read_unlock().
300  */
301 int __srcu_read_lock(struct srcu_struct *sp)
303         int idx;
305         preempt_disable();
306         idx = rcu_dereference_index_check(sp->completed,
307                                           rcu_read_lock_sched_held()) & 0x1;
308         ACCESS_ONCE(this_cpu_ptr(sp->per_cpu_ref)->c[idx]) += 1;
309         smp_mb(); /* B */  /* Avoid leaking the critical section. */
310         ACCESS_ONCE(this_cpu_ptr(sp->per_cpu_ref)->seq[idx]) += 1;
311         preempt_enable();
312         return idx;
314 EXPORT_SYMBOL_GPL(__srcu_read_lock);
316 /*
317  * Removes the count for the old reader from the appropriate per-CPU
318  * element of the srcu_struct.  Note that this may well be a different
319  * CPU than that which was incremented by the corresponding srcu_read_lock().
320  * Must be called from process context.
321  */
322 void __srcu_read_unlock(struct srcu_struct *sp, int idx)
324         preempt_disable();
325         smp_mb(); /* C */  /* Avoid leaking the critical section. */
326         ACCESS_ONCE(this_cpu_ptr(sp->per_cpu_ref)->c[idx]) -= 1;
327         preempt_enable();
329 EXPORT_SYMBOL_GPL(__srcu_read_unlock);
331 /*
332  * We use an adaptive strategy for synchronize_srcu() and especially for
333  * synchronize_srcu_expedited().  We spin for a fixed time period
334  * (defined below) to allow SRCU readers to exit their read-side critical
335  * sections.  If there are still some readers after 10 microseconds,
336  * we repeatedly block for 1-millisecond time periods.  This approach
337  * has done well in testing, so there is no need for a config parameter.
338  */
339 #define SRCU_RETRY_CHECK_DELAY          5
340 #define SYNCHRONIZE_SRCU_TRYCOUNT       2
341 #define SYNCHRONIZE_SRCU_EXP_TRYCOUNT   12
343 /*
344  * @@@ Wait until all pre-existing readers complete.  Such readers
345  * will have used the index specified by "idx".
346  * the caller should ensures the ->completed is not changed while checking
347  * and idx = (->completed & 1) ^ 1
348  */
349 static bool try_check_zero(struct srcu_struct *sp, int idx, int trycount)
351         for (;;) {
352                 if (srcu_readers_active_idx_check(sp, idx))
353                         return true;
354                 if (--trycount <= 0)
355                         return false;
356                 udelay(SRCU_RETRY_CHECK_DELAY);
357         }
360 /*
361  * Increment the ->completed counter so that future SRCU readers will
362  * use the other rank of the ->c[] and ->seq[] arrays.  This allows
363  * us to wait for pre-existing readers in a starvation-free manner.
364  */
365 static void srcu_flip(struct srcu_struct *sp)
367         sp->completed++;
370 /*
371  * Enqueue an SRCU callback on the specified srcu_struct structure,
372  * initiating grace-period processing if it is not already running.
373  */
374 void call_srcu(struct srcu_struct *sp, struct rcu_head *head,
375                 void (*func)(struct rcu_head *head))
377         unsigned long flags;
379         head->next = NULL;
380         head->func = func;
381         spin_lock_irqsave(&sp->queue_lock, flags);
382         rcu_batch_queue(&sp->batch_queue, head);
383         if (!sp->running) {
384                 sp->running = true;
385                 schedule_delayed_work(&sp->work, 0);
386         }
387         spin_unlock_irqrestore(&sp->queue_lock, flags);
389 EXPORT_SYMBOL_GPL(call_srcu);
391 struct rcu_synchronize {
392         struct rcu_head head;
393         struct completion completion;
394 };
396 /*
397  * Awaken the corresponding synchronize_srcu() instance now that a
398  * grace period has elapsed.
399  */
400 static void wakeme_after_rcu(struct rcu_head *head)
402         struct rcu_synchronize *rcu;
404         rcu = container_of(head, struct rcu_synchronize, head);
405         complete(&rcu->completion);
408 static void srcu_advance_batches(struct srcu_struct *sp, int trycount);
409 static void srcu_reschedule(struct srcu_struct *sp);
411 /*
412  * Helper function for synchronize_srcu() and synchronize_srcu_expedited().
413  */
414 static void __synchronize_srcu(struct srcu_struct *sp, int trycount)
416         struct rcu_synchronize rcu;
417         struct rcu_head *head = &rcu.head;
418         bool done = false;
420         rcu_lockdep_assert(!lock_is_held(&sp->dep_map) &&
421                            !lock_is_held(&rcu_bh_lock_map) &&
422                            !lock_is_held(&rcu_lock_map) &&
423                            !lock_is_held(&rcu_sched_lock_map),
424                            "Illegal synchronize_srcu() in same-type SRCU (or RCU) read-side critical section");
426         init_completion(&rcu.completion);
428         head->next = NULL;
429         head->func = wakeme_after_rcu;
430         spin_lock_irq(&sp->queue_lock);
431         if (!sp->running) {
432                 /* steal the processing owner */
433                 sp->running = true;
434                 rcu_batch_queue(&sp->batch_check0, head);
435                 spin_unlock_irq(&sp->queue_lock);
437                 srcu_advance_batches(sp, trycount);
438                 if (!rcu_batch_empty(&sp->batch_done)) {
439                         BUG_ON(sp->batch_done.head != head);
440                         rcu_batch_dequeue(&sp->batch_done);
441                         done = true;
442                 }
443                 /* give the processing owner to work_struct */
444                 srcu_reschedule(sp);
445         } else {
446                 rcu_batch_queue(&sp->batch_queue, head);
447                 spin_unlock_irq(&sp->queue_lock);
448         }
450         if (!done)
451                 wait_for_completion(&rcu.completion);
454 /**
455  * synchronize_srcu - wait for prior SRCU read-side critical-section completion
456  * @sp: srcu_struct with which to synchronize.
457  *
458  * Flip the completed counter, and wait for the old count to drain to zero.
459  * As with classic RCU, the updater must use some separate means of
460  * synchronizing concurrent updates.  Can block; must be called from
461  * process context.
462  *
463  * Note that it is illegal to call synchronize_srcu() from the corresponding
464  * SRCU read-side critical section; doing so will result in deadlock.
465  * However, it is perfectly legal to call synchronize_srcu() on one
466  * srcu_struct from some other srcu_struct's read-side critical section.
467  */
468 void synchronize_srcu(struct srcu_struct *sp)
470         __synchronize_srcu(sp, rcu_expedited
471                            ? SYNCHRONIZE_SRCU_EXP_TRYCOUNT
472                            : SYNCHRONIZE_SRCU_TRYCOUNT);
474 EXPORT_SYMBOL_GPL(synchronize_srcu);
476 /**
477  * synchronize_srcu_expedited - Brute-force SRCU grace period
478  * @sp: srcu_struct with which to synchronize.
479  *
480  * Wait for an SRCU grace period to elapse, but be more aggressive about
481  * spinning rather than blocking when waiting.
482  *
483  * Note that it is illegal to call this function while holding any lock
484  * that is acquired by a CPU-hotplug notifier.  It is also illegal to call
485  * synchronize_srcu_expedited() from the corresponding SRCU read-side
486  * critical section; doing so will result in deadlock.  However, it is
487  * perfectly legal to call synchronize_srcu_expedited() on one srcu_struct
488  * from some other srcu_struct's read-side critical section, as long as
489  * the resulting graph of srcu_structs is acyclic.
490  */
491 void synchronize_srcu_expedited(struct srcu_struct *sp)
493         __synchronize_srcu(sp, SYNCHRONIZE_SRCU_EXP_TRYCOUNT);
495 EXPORT_SYMBOL_GPL(synchronize_srcu_expedited);
497 /**
498  * srcu_barrier - Wait until all in-flight call_srcu() callbacks complete.
499  */
500 void srcu_barrier(struct srcu_struct *sp)
502         synchronize_srcu(sp);
504 EXPORT_SYMBOL_GPL(srcu_barrier);
506 /**
507  * srcu_batches_completed - return batches completed.
508  * @sp: srcu_struct on which to report batch completion.
509  *
510  * Report the number of batches, correlated with, but not necessarily
511  * precisely the same as, the number of grace periods that have elapsed.
512  */
513 long srcu_batches_completed(struct srcu_struct *sp)
515         return sp->completed;
517 EXPORT_SYMBOL_GPL(srcu_batches_completed);
519 #define SRCU_CALLBACK_BATCH     10
520 #define SRCU_INTERVAL           1
522 /*
523  * Move any new SRCU callbacks to the first stage of the SRCU grace
524  * period pipeline.
525  */
526 static void srcu_collect_new(struct srcu_struct *sp)
528         if (!rcu_batch_empty(&sp->batch_queue)) {
529                 spin_lock_irq(&sp->queue_lock);
530                 rcu_batch_move(&sp->batch_check0, &sp->batch_queue);
531                 spin_unlock_irq(&sp->queue_lock);
532         }
535 /*
536  * Core SRCU state machine.  Advance callbacks from ->batch_check0 to
537  * ->batch_check1 and then to ->batch_done as readers drain.
538  */
539 static void srcu_advance_batches(struct srcu_struct *sp, int trycount)
541         int idx = 1 ^ (sp->completed & 1);
543         /*
544          * Because readers might be delayed for an extended period after
545          * fetching ->completed for their index, at any point in time there
546          * might well be readers using both idx=0 and idx=1.  We therefore
547          * need to wait for readers to clear from both index values before
548          * invoking a callback.
549          */
551         if (rcu_batch_empty(&sp->batch_check0) &&
552             rcu_batch_empty(&sp->batch_check1))
553                 return; /* no callbacks need to be advanced */
555         if (!try_check_zero(sp, idx, trycount))
556                 return; /* failed to advance, will try after SRCU_INTERVAL */
558         /*
559          * The callbacks in ->batch_check1 have already done with their
560          * first zero check and flip back when they were enqueued on
561          * ->batch_check0 in a previous invocation of srcu_advance_batches().
562          * (Presumably try_check_zero() returned false during that
563          * invocation, leaving the callbacks stranded on ->batch_check1.)
564          * They are therefore ready to invoke, so move them to ->batch_done.
565          */
566         rcu_batch_move(&sp->batch_done, &sp->batch_check1);
568         if (rcu_batch_empty(&sp->batch_check0))
569                 return; /* no callbacks need to be advanced */
570         srcu_flip(sp);
572         /*
573          * The callbacks in ->batch_check0 just finished their
574          * first check zero and flip, so move them to ->batch_check1
575          * for future checking on the other idx.
576          */
577         rcu_batch_move(&sp->batch_check1, &sp->batch_check0);
579         /*
580          * SRCU read-side critical sections are normally short, so check
581          * at least twice in quick succession after a flip.
582          */
583         trycount = trycount < 2 ? 2 : trycount;
584         if (!try_check_zero(sp, idx^1, trycount))
585                 return; /* failed to advance, will try after SRCU_INTERVAL */
587         /*
588          * The callbacks in ->batch_check1 have now waited for all
589          * pre-existing readers using both idx values.  They are therefore
590          * ready to invoke, so move them to ->batch_done.
591          */
592         rcu_batch_move(&sp->batch_done, &sp->batch_check1);
595 /*
596  * Invoke a limited number of SRCU callbacks that have passed through
597  * their grace period.  If there are more to do, SRCU will reschedule
598  * the workqueue.
599  */
600 static void srcu_invoke_callbacks(struct srcu_struct *sp)
602         int i;
603         struct rcu_head *head;
605         for (i = 0; i < SRCU_CALLBACK_BATCH; i++) {
606                 head = rcu_batch_dequeue(&sp->batch_done);
607                 if (!head)
608                         break;
609                 local_bh_disable();
610                 head->func(head);
611                 local_bh_enable();
612         }
615 /*
616  * Finished one round of SRCU grace period.  Start another if there are
617  * more SRCU callbacks queued, otherwise put SRCU into not-running state.
618  */
619 static void srcu_reschedule(struct srcu_struct *sp)
621         bool pending = true;
623         if (rcu_batch_empty(&sp->batch_done) &&
624             rcu_batch_empty(&sp->batch_check1) &&
625             rcu_batch_empty(&sp->batch_check0) &&
626             rcu_batch_empty(&sp->batch_queue)) {
627                 spin_lock_irq(&sp->queue_lock);
628                 if (rcu_batch_empty(&sp->batch_done) &&
629                     rcu_batch_empty(&sp->batch_check1) &&
630                     rcu_batch_empty(&sp->batch_check0) &&
631                     rcu_batch_empty(&sp->batch_queue)) {
632                         sp->running = false;
633                         pending = false;
634                 }
635                 spin_unlock_irq(&sp->queue_lock);
636         }
638         if (pending)
639                 schedule_delayed_work(&sp->work, SRCU_INTERVAL);
642 /*
643  * This is the work-queue function that handles SRCU grace periods.
644  */
645 void process_srcu(struct work_struct *work)
647         struct srcu_struct *sp;
649         sp = container_of(work, struct srcu_struct, work.work);
651         srcu_collect_new(sp);
652         srcu_advance_batches(sp, 1);
653         srcu_invoke_callbacks(sp);
654         srcu_reschedule(sp);
656 EXPORT_SYMBOL_GPL(process_srcu);