1 #include <linux/spinlock.h>
2 #include <linux/task_work.h>
3 #include <linux/tracehook.h>
5 static struct callback_head work_exited; /* all we need is ->next == NULL */
7 int
8 task_work_add(struct task_struct *task, struct callback_head *work, bool notify)
9 {
10 struct callback_head *head;
12 do {
13 head = ACCESS_ONCE(task->task_works);
14 if (unlikely(head == &work_exited))
15 return -ESRCH;
16 work->next = head;
17 } while (cmpxchg(&task->task_works, head, work) != head);
19 if (notify)
20 set_notify_resume(task);
21 return 0;
22 }
24 struct callback_head *
25 task_work_cancel(struct task_struct *task, task_work_func_t func)
26 {
27 struct callback_head **pprev = &task->task_works;
28 struct callback_head *work = NULL;
29 unsigned long flags;
30 /*
31 * If cmpxchg() fails we continue without updating pprev.
32 * Either we raced with task_work_add() which added the
33 * new entry before this work, we will find it again. Or
34 * we raced with task_work_run(), *pprev == NULL/exited.
35 */
36 raw_spin_lock_irqsave(&task->pi_lock, flags);
37 while ((work = ACCESS_ONCE(*pprev))) {
38 read_barrier_depends();
39 if (work->func != func)
40 pprev = &work->next;
41 else if (cmpxchg(pprev, work, work->next) == work)
42 break;
43 }
44 raw_spin_unlock_irqrestore(&task->pi_lock, flags);
46 return work;
47 }
49 void task_work_run(void)
50 {
51 struct task_struct *task = current;
52 struct callback_head *work, *head, *next;
54 for (;;) {
55 /*
56 * work->func() can do task_work_add(), do not set
57 * work_exited unless the list is empty.
58 */
59 do {
60 work = ACCESS_ONCE(task->task_works);
61 head = !work && (task->flags & PF_EXITING) ?
62 &work_exited : NULL;
63 } while (cmpxchg(&task->task_works, work, head) != work);
65 if (!work)
66 break;
67 /*
68 * Synchronize with task_work_cancel(). It can't remove
69 * the first entry == work, cmpxchg(task_works) should
70 * fail, but it can play with *work and other entries.
71 */
72 raw_spin_unlock_wait(&task->pi_lock);
73 smp_mb();
75 /* Reverse the list to run the works in fifo order */
76 head = NULL;
77 do {
78 next = work->next;
79 work->next = head;
80 head = work;
81 work = next;
82 } while (work);
84 work = head;
85 do {
86 next = work->next;
87 work->func(work);
88 work = next;
89 cond_resched();
90 } while (work);
91 }
92 }