1 #
2 # Library configuration
3 #
5 config BINARY_PRINTF
6 def_bool n
8 menu "Library routines"
10 config RAID6_PQ
11 tristate
13 config BITREVERSE
14 tristate
16 config RATIONAL
17 boolean
19 config GENERIC_STRNCPY_FROM_USER
20 bool
22 config GENERIC_STRNLEN_USER
23 bool
25 config GENERIC_FIND_FIRST_BIT
26 bool
28 config NO_GENERIC_PCI_IOPORT_MAP
29 bool
31 config GENERIC_PCI_IOMAP
32 bool
34 config GENERIC_IOMAP
35 bool
36 select GENERIC_PCI_IOMAP
38 config GENERIC_IO
39 boolean
40 default n
42 config STMP_DEVICE
43 bool
45 config PERCPU_RWSEM
46 boolean
48 config CRC_CCITT
49 tristate "CRC-CCITT functions"
50 help
51 This option is provided for the case where no in-kernel-tree
52 modules require CRC-CCITT functions, but a module built outside
53 the kernel tree does. Such modules that use library CRC-CCITT
54 functions require M here.
56 config CRC16
57 tristate "CRC16 functions"
58 help
59 This option is provided for the case where no in-kernel-tree
60 modules require CRC16 functions, but a module built outside
61 the kernel tree does. Such modules that use library CRC16
62 functions require M here.
64 config CRC_T10DIF
65 tristate "CRC calculation for the T10 Data Integrity Field"
66 help
67 This option is only needed if a module that's not in the
68 kernel tree needs to calculate CRC checks for use with the
69 SCSI data integrity subsystem.
71 config CRC_ITU_T
72 tristate "CRC ITU-T V.41 functions"
73 help
74 This option is provided for the case where no in-kernel-tree
75 modules require CRC ITU-T V.41 functions, but a module built outside
76 the kernel tree does. Such modules that use library CRC ITU-T V.41
77 functions require M here.
79 config CRC32
80 tristate "CRC32/CRC32c functions"
81 default y
82 select BITREVERSE
83 help
84 This option is provided for the case where no in-kernel-tree
85 modules require CRC32/CRC32c functions, but a module built outside
86 the kernel tree does. Such modules that use library CRC32/CRC32c
87 functions require M here.
89 config CRC32_SELFTEST
90 bool "CRC32 perform self test on init"
91 default n
92 depends on CRC32
93 help
94 This option enables the CRC32 library functions to perform a
95 self test on initialization. The self test computes crc32_le
96 and crc32_be over byte strings with random alignment and length
97 and computes the total elapsed time and number of bytes processed.
99 choice
100 prompt "CRC32 implementation"
101 depends on CRC32
102 default CRC32_SLICEBY8
103 help
104 This option allows a kernel builder to override the default choice
105 of CRC32 algorithm. Choose the default ("slice by 8") unless you
106 know that you need one of the others.
108 config CRC32_SLICEBY8
109 bool "Slice by 8 bytes"
110 help
111 Calculate checksum 8 bytes at a time with a clever slicing algorithm.
112 This is the fastest algorithm, but comes with a 8KiB lookup table.
113 Most modern processors have enough cache to hold this table without
114 thrashing the cache.
116 This is the default implementation choice. Choose this one unless
117 you have a good reason not to.
119 config CRC32_SLICEBY4
120 bool "Slice by 4 bytes"
121 help
122 Calculate checksum 4 bytes at a time with a clever slicing algorithm.
123 This is a bit slower than slice by 8, but has a smaller 4KiB lookup
124 table.
126 Only choose this option if you know what you are doing.
128 config CRC32_SARWATE
129 bool "Sarwate's Algorithm (one byte at a time)"
130 help
131 Calculate checksum a byte at a time using Sarwate's algorithm. This
132 is not particularly fast, but has a small 256 byte lookup table.
134 Only choose this option if you know what you are doing.
136 config CRC32_BIT
137 bool "Classic Algorithm (one bit at a time)"
138 help
139 Calculate checksum one bit at a time. This is VERY slow, but has
140 no lookup table. This is provided as a debugging option.
142 Only choose this option if you are debugging crc32.
144 endchoice
146 config CRC7
147 tristate "CRC7 functions"
148 help
149 This option is provided for the case where no in-kernel-tree
150 modules require CRC7 functions, but a module built outside
151 the kernel tree does. Such modules that use library CRC7
152 functions require M here.
154 config LIBCRC32C
155 tristate "CRC32c (Castagnoli, et al) Cyclic Redundancy-Check"
156 select CRYPTO
157 select CRYPTO_CRC32C
158 help
159 This option is provided for the case where no in-kernel-tree
160 modules require CRC32c functions, but a module built outside the
161 kernel tree does. Such modules that use library CRC32c functions
162 require M here. See Castagnoli93.
163 Module will be libcrc32c.
165 config CRC8
166 tristate "CRC8 function"
167 help
168 This option provides CRC8 function. Drivers may select this
169 when they need to do cyclic redundancy check according CRC8
170 algorithm. Module will be called crc8.
172 config AUDIT_GENERIC
173 bool
174 depends on AUDIT && !AUDIT_ARCH
175 default y
177 #
178 # compression support is select'ed if needed
179 #
180 config ZLIB_INFLATE
181 tristate
183 config ZLIB_DEFLATE
184 tristate
186 config LZO_COMPRESS
187 tristate
189 config LZO_DECOMPRESS
190 tristate
192 source "lib/xz/Kconfig"
194 #
195 # These all provide a common interface (hence the apparent duplication with
196 # ZLIB_INFLATE; DECOMPRESS_GZIP is just a wrapper.)
197 #
198 config DECOMPRESS_GZIP
199 select ZLIB_INFLATE
200 tristate
202 config DECOMPRESS_BZIP2
203 tristate
205 config DECOMPRESS_LZMA
206 tristate
208 config DECOMPRESS_XZ
209 select XZ_DEC
210 tristate
212 config DECOMPRESS_LZO
213 select LZO_DECOMPRESS
214 tristate
216 #
217 # Generic allocator support is selected if needed
218 #
219 config GENERIC_ALLOCATOR
220 boolean
222 #
223 # reed solomon support is select'ed if needed
224 #
225 config REED_SOLOMON
226 tristate
228 config REED_SOLOMON_ENC8
229 boolean
231 config REED_SOLOMON_DEC8
232 boolean
234 config REED_SOLOMON_ENC16
235 boolean
237 config REED_SOLOMON_DEC16
238 boolean
240 #
241 # BCH support is selected if needed
242 #
243 config BCH
244 tristate
246 config BCH_CONST_PARAMS
247 boolean
248 help
249 Drivers may select this option to force specific constant
250 values for parameters 'm' (Galois field order) and 't'
251 (error correction capability). Those specific values must
252 be set by declaring default values for symbols BCH_CONST_M
253 and BCH_CONST_T.
254 Doing so will enable extra compiler optimizations,
255 improving encoding and decoding performance up to 2x for
256 usual (m,t) values (typically such that m*t < 200).
257 When this option is selected, the BCH library supports
258 only a single (m,t) configuration. This is mainly useful
259 for NAND flash board drivers requiring known, fixed BCH
260 parameters.
262 config BCH_CONST_M
263 int
264 range 5 15
265 help
266 Constant value for Galois field order 'm'. If 'k' is the
267 number of data bits to protect, 'm' should be chosen such
268 that (k + m*t) <= 2**m - 1.
269 Drivers should declare a default value for this symbol if
270 they select option BCH_CONST_PARAMS.
272 config BCH_CONST_T
273 int
274 help
275 Constant value for error correction capability in bits 't'.
276 Drivers should declare a default value for this symbol if
277 they select option BCH_CONST_PARAMS.
279 #
280 # Textsearch support is select'ed if needed
281 #
282 config TEXTSEARCH
283 boolean
285 config TEXTSEARCH_KMP
286 tristate
288 config TEXTSEARCH_BM
289 tristate
291 config TEXTSEARCH_FSM
292 tristate
294 config BTREE
295 boolean
297 config HAS_IOMEM
298 boolean
299 depends on !NO_IOMEM
300 select GENERIC_IO
301 default y
303 config HAS_IOPORT
304 boolean
305 depends on HAS_IOMEM && !NO_IOPORT
306 default y
308 config HAS_DMA
309 boolean
310 depends on !NO_DMA
311 default y
313 config CHECK_SIGNATURE
314 bool
316 config CPUMASK_OFFSTACK
317 bool "Force CPU masks off stack" if DEBUG_PER_CPU_MAPS
318 help
319 Use dynamic allocation for cpumask_var_t, instead of putting
320 them on the stack. This is a bit more expensive, but avoids
321 stack overflow.
323 config DISABLE_OBSOLETE_CPUMASK_FUNCTIONS
324 bool "Disable obsolete cpumask functions" if DEBUG_PER_CPU_MAPS
325 depends on EXPERIMENTAL && BROKEN
327 config CPU_RMAP
328 bool
329 depends on SMP
331 config DQL
332 bool
334 #
335 # Netlink attribute parsing support is select'ed if needed
336 #
337 config NLATTR
338 bool
340 #
341 # Generic 64-bit atomic support is selected if needed
342 #
343 config GENERIC_ATOMIC64
344 bool
346 config ARCH_HAS_ATOMIC64_DEC_IF_POSITIVE
347 def_bool y if GENERIC_ATOMIC64
349 config LRU_CACHE
350 tristate
352 config AVERAGE
353 bool "Averaging functions"
354 help
355 This option is provided for the case where no in-kernel-tree
356 modules require averaging functions, but a module built outside
357 the kernel tree does. Such modules that use library averaging
358 functions require Y here.
360 If unsure, say N.
362 config CLZ_TAB
363 bool
365 config CORDIC
366 tristate "CORDIC algorithm"
367 help
368 This option provides an implementation of the CORDIC algorithm;
369 calculations are in fixed point. Module will be called cordic.
371 config DDR
372 bool "JEDEC DDR data"
373 help
374 Data from JEDEC specs for DDR SDRAM memories,
375 particularly the AC timing parameters and addressing
376 information. This data is useful for drivers handling
377 DDR SDRAM controllers.
379 config MPILIB
380 tristate
381 select CLZ_TAB
382 help
383 Multiprecision maths library from GnuPG.
384 It is used to implement RSA digital signature verification,
385 which is used by IMA/EVM digital signature extension.
387 config SIGNATURE
388 tristate
389 depends on KEYS && CRYPTO
390 select CRYPTO_SHA1
391 select MPILIB
392 help
393 Digital signature verification. Currently only RSA is supported.
394 Implementation is done using GnuPG MPI library
396 #
397 # libfdt files, only selected if needed.
398 #
399 config LIBFDT
400 bool
402 config OID_REGISTRY
403 tristate
404 help
405 Enable fast lookup object identifier registry.
407 endmenu