]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/blob - lib/bug.c
Merge branch 'p-ti-android-3.8.y-video'
[android-sdk/kernel-video.git] / lib / bug.c
1 /*
2   Generic support for BUG()
4   This respects the following config options:
6   CONFIG_BUG - emit BUG traps.  Nothing happens without this.
7   CONFIG_GENERIC_BUG - enable this code.
8   CONFIG_GENERIC_BUG_RELATIVE_POINTERS - use 32-bit pointers relative to
9         the containing struct bug_entry for bug_addr and file.
10   CONFIG_DEBUG_BUGVERBOSE - emit full file+line information for each BUG
12   CONFIG_BUG and CONFIG_DEBUG_BUGVERBOSE are potentially user-settable
13   (though they're generally always on).
15   CONFIG_GENERIC_BUG is set by each architecture using this code.
17   To use this, your architecture must:
19   1. Set up the config options:
20      - Enable CONFIG_GENERIC_BUG if CONFIG_BUG
22   2. Implement BUG (and optionally BUG_ON, WARN, WARN_ON)
23      - Define HAVE_ARCH_BUG
24      - Implement BUG() to generate a faulting instruction
25      - NOTE: struct bug_entry does not have "file" or "line" entries
26        when CONFIG_DEBUG_BUGVERBOSE is not enabled, so you must generate
27        the values accordingly.
29   3. Implement the trap
30      - In the illegal instruction trap handler (typically), verify
31        that the fault was in kernel mode, and call report_bug()
32      - report_bug() will return whether it was a false alarm, a warning,
33        or an actual bug.
34      - You must implement the is_valid_bugaddr(bugaddr) callback which
35        returns true if the eip is a real kernel address, and it points
36        to the expected BUG trap instruction.
38     Jeremy Fitzhardinge <jeremy@goop.org> 2006
39  */
40 #include <linux/list.h>
41 #include <linux/module.h>
42 #include <linux/kernel.h>
43 #include <linux/bug.h>
44 #include <linux/sched.h>
46 extern const struct bug_entry __start___bug_table[], __stop___bug_table[];
48 static inline unsigned long bug_addr(const struct bug_entry *bug)
49 {
50 #ifndef CONFIG_GENERIC_BUG_RELATIVE_POINTERS
51         return bug->bug_addr;
52 #else
53         return (unsigned long)bug + bug->bug_addr_disp;
54 #endif
55 }
57 #ifdef CONFIG_MODULES
58 /* Updates are protected by module mutex */
59 static LIST_HEAD(module_bug_list);
61 static const struct bug_entry *module_find_bug(unsigned long bugaddr)
62 {
63         struct module *mod;
65         list_for_each_entry(mod, &module_bug_list, bug_list) {
66                 const struct bug_entry *bug = mod->bug_table;
67                 unsigned i;
69                 for (i = 0; i < mod->num_bugs; ++i, ++bug)
70                         if (bugaddr == bug_addr(bug))
71                                 return bug;
72         }
73         return NULL;
74 }
76 void module_bug_finalize(const Elf_Ehdr *hdr, const Elf_Shdr *sechdrs,
77                          struct module *mod)
78 {
79         char *secstrings;
80         unsigned int i;
82         mod->bug_table = NULL;
83         mod->num_bugs = 0;
85         /* Find the __bug_table section, if present */
86         secstrings = (char *)hdr + sechdrs[hdr->e_shstrndx].sh_offset;
87         for (i = 1; i < hdr->e_shnum; i++) {
88                 if (strcmp(secstrings+sechdrs[i].sh_name, "__bug_table"))
89                         continue;
90                 mod->bug_table = (void *) sechdrs[i].sh_addr;
91                 mod->num_bugs = sechdrs[i].sh_size / sizeof(struct bug_entry);
92                 break;
93         }
95         /*
96          * Strictly speaking this should have a spinlock to protect against
97          * traversals, but since we only traverse on BUG()s, a spinlock
98          * could potentially lead to deadlock and thus be counter-productive.
99          */
100         list_add(&mod->bug_list, &module_bug_list);
103 void module_bug_cleanup(struct module *mod)
105         list_del(&mod->bug_list);
108 #else
110 static inline const struct bug_entry *module_find_bug(unsigned long bugaddr)
112         return NULL;
114 #endif
116 const struct bug_entry *find_bug(unsigned long bugaddr)
118         const struct bug_entry *bug;
120         for (bug = __start___bug_table; bug < __stop___bug_table; ++bug)
121                 if (bugaddr == bug_addr(bug))
122                         return bug;
124         return module_find_bug(bugaddr);
127 enum bug_trap_type report_bug(unsigned long bugaddr, struct pt_regs *regs)
129         const struct bug_entry *bug;
130         const char *file;
131         unsigned line, warning;
133         if (!is_valid_bugaddr(bugaddr))
134                 return BUG_TRAP_TYPE_NONE;
136         bug = find_bug(bugaddr);
138         file = NULL;
139         line = 0;
140         warning = 0;
142         if (bug) {
143 #ifdef CONFIG_DEBUG_BUGVERBOSE
144 #ifndef CONFIG_GENERIC_BUG_RELATIVE_POINTERS
145                 file = bug->file;
146 #else
147                 file = (const char *)bug + bug->file_disp;
148 #endif
149                 line = bug->line;
150 #endif
151                 warning = (bug->flags & BUGFLAG_WARNING) != 0;
152         }
154         if (warning) {
155                 /* this is a WARN_ON rather than BUG/BUG_ON */
156                 printk(KERN_WARNING "------------[ cut here ]------------\n");
158                 if (file)
159                         printk(KERN_WARNING "WARNING: at %s:%u\n",
160                                file, line);
161                 else
162                         printk(KERN_WARNING "WARNING: at %p "
163                                "[verbose debug info unavailable]\n",
164                                (void *)bugaddr);
166                 print_modules();
167                 show_regs(regs);
168                 print_oops_end_marker();
169                 add_taint(BUG_GET_TAINT(bug));
170                 return BUG_TRAP_TYPE_WARN;
171         }
173         printk(KERN_DEFAULT "------------[ cut here ]------------\n");
175         if (file)
176                 printk(KERN_CRIT "kernel BUG at %s:%u!\n",
177                        file, line);
178         else
179                 printk(KERN_CRIT "Kernel BUG at %p "
180                        "[verbose debug info unavailable]\n",
181                        (void *)bugaddr);
183         return BUG_TRAP_TYPE_BUG;