]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/blob - mm/dmapool.c
ARM: OMAP5/DRA7: hwmod: add ADDR_TYPE_RT to bb2d address flags
[android-sdk/kernel-video.git] / mm / dmapool.c
1 /*
2  * DMA Pool allocator
3  *
4  * Copyright 2001 David Brownell
5  * Copyright 2007 Intel Corporation
6  *   Author: Matthew Wilcox <willy@linux.intel.com>
7  *
8  * This software may be redistributed and/or modified under the terms of
9  * the GNU General Public License ("GPL") version 2 as published by the
10  * Free Software Foundation.
11  *
12  * This allocator returns small blocks of a given size which are DMA-able by
13  * the given device.  It uses the dma_alloc_coherent page allocator to get
14  * new pages, then splits them up into blocks of the required size.
15  * Many older drivers still have their own code to do this.
16  *
17  * The current design of this allocator is fairly simple.  The pool is
18  * represented by the 'struct dma_pool' which keeps a doubly-linked list of
19  * allocated pages.  Each page in the page_list is split into blocks of at
20  * least 'size' bytes.  Free blocks are tracked in an unsorted singly-linked
21  * list of free blocks within the page.  Used blocks aren't tracked, but we
22  * keep a count of how many are currently allocated from each page.
23  */
25 #include <linux/device.h>
26 #include <linux/dma-mapping.h>
27 #include <linux/dmapool.h>
28 #include <linux/kernel.h>
29 #include <linux/list.h>
30 #include <linux/export.h>
31 #include <linux/mutex.h>
32 #include <linux/poison.h>
33 #include <linux/sched.h>
34 #include <linux/slab.h>
35 #include <linux/stat.h>
36 #include <linux/spinlock.h>
37 #include <linux/string.h>
38 #include <linux/types.h>
39 #include <linux/wait.h>
41 #if defined(CONFIG_DEBUG_SLAB) || defined(CONFIG_SLUB_DEBUG_ON)
42 #define DMAPOOL_DEBUG 1
43 #endif
45 struct dma_pool {               /* the pool */
46         struct list_head page_list;
47         spinlock_t lock;
48         size_t size;
49         struct device *dev;
50         size_t allocation;
51         size_t boundary;
52         char name[32];
53         struct list_head pools;
54 };
56 struct dma_page {               /* cacheable header for 'allocation' bytes */
57         struct list_head page_list;
58         void *vaddr;
59         dma_addr_t dma;
60         unsigned int in_use;
61         unsigned int offset;
62 };
64 static DEFINE_MUTEX(pools_lock);
66 static ssize_t
67 show_pools(struct device *dev, struct device_attribute *attr, char *buf)
68 {
69         unsigned temp;
70         unsigned size;
71         char *next;
72         struct dma_page *page;
73         struct dma_pool *pool;
75         next = buf;
76         size = PAGE_SIZE;
78         temp = scnprintf(next, size, "poolinfo - 0.1\n");
79         size -= temp;
80         next += temp;
82         mutex_lock(&pools_lock);
83         list_for_each_entry(pool, &dev->dma_pools, pools) {
84                 unsigned pages = 0;
85                 unsigned blocks = 0;
87                 spin_lock_irq(&pool->lock);
88                 list_for_each_entry(page, &pool->page_list, page_list) {
89                         pages++;
90                         blocks += page->in_use;
91                 }
92                 spin_unlock_irq(&pool->lock);
94                 /* per-pool info, no real statistics yet */
95                 temp = scnprintf(next, size, "%-16s %4u %4Zu %4Zu %2u\n",
96                                  pool->name, blocks,
97                                  pages * (pool->allocation / pool->size),
98                                  pool->size, pages);
99                 size -= temp;
100                 next += temp;
101         }
102         mutex_unlock(&pools_lock);
104         return PAGE_SIZE - size;
107 static DEVICE_ATTR(pools, S_IRUGO, show_pools, NULL);
109 /**
110  * dma_pool_create - Creates a pool of consistent memory blocks, for dma.
111  * @name: name of pool, for diagnostics
112  * @dev: device that will be doing the DMA
113  * @size: size of the blocks in this pool.
114  * @align: alignment requirement for blocks; must be a power of two
115  * @boundary: returned blocks won't cross this power of two boundary
116  * Context: !in_interrupt()
117  *
118  * Returns a dma allocation pool with the requested characteristics, or
119  * null if one can't be created.  Given one of these pools, dma_pool_alloc()
120  * may be used to allocate memory.  Such memory will all have "consistent"
121  * DMA mappings, accessible by the device and its driver without using
122  * cache flushing primitives.  The actual size of blocks allocated may be
123  * larger than requested because of alignment.
124  *
125  * If @boundary is nonzero, objects returned from dma_pool_alloc() won't
126  * cross that size boundary.  This is useful for devices which have
127  * addressing restrictions on individual DMA transfers, such as not crossing
128  * boundaries of 4KBytes.
129  */
130 struct dma_pool *dma_pool_create(const char *name, struct device *dev,
131                                  size_t size, size_t align, size_t boundary)
133         struct dma_pool *retval;
134         size_t allocation;
136         if (align == 0) {
137                 align = 1;
138         } else if (align & (align - 1)) {
139                 return NULL;
140         }
142         if (size == 0) {
143                 return NULL;
144         } else if (size < 4) {
145                 size = 4;
146         }
148         if ((size % align) != 0)
149                 size = ALIGN(size, align);
151         allocation = max_t(size_t, size, PAGE_SIZE);
153         if (!boundary) {
154                 boundary = allocation;
155         } else if ((boundary < size) || (boundary & (boundary - 1))) {
156                 return NULL;
157         }
159         retval = kmalloc_node(sizeof(*retval), GFP_KERNEL, dev_to_node(dev));
160         if (!retval)
161                 return retval;
163         strlcpy(retval->name, name, sizeof(retval->name));
165         retval->dev = dev;
167         INIT_LIST_HEAD(&retval->page_list);
168         spin_lock_init(&retval->lock);
169         retval->size = size;
170         retval->boundary = boundary;
171         retval->allocation = allocation;
173         if (dev) {
174                 int ret;
176                 mutex_lock(&pools_lock);
177                 if (list_empty(&dev->dma_pools))
178                         ret = device_create_file(dev, &dev_attr_pools);
179                 else
180                         ret = 0;
181                 /* note:  not currently insisting "name" be unique */
182                 if (!ret)
183                         list_add(&retval->pools, &dev->dma_pools);
184                 else {
185                         kfree(retval);
186                         retval = NULL;
187                 }
188                 mutex_unlock(&pools_lock);
189         } else
190                 INIT_LIST_HEAD(&retval->pools);
192         return retval;
194 EXPORT_SYMBOL(dma_pool_create);
196 static void pool_initialise_page(struct dma_pool *pool, struct dma_page *page)
198         unsigned int offset = 0;
199         unsigned int next_boundary = pool->boundary;
201         do {
202                 unsigned int next = offset + pool->size;
203                 if (unlikely((next + pool->size) >= next_boundary)) {
204                         next = next_boundary;
205                         next_boundary += pool->boundary;
206                 }
207                 *(int *)(page->vaddr + offset) = next;
208                 offset = next;
209         } while (offset < pool->allocation);
212 static struct dma_page *pool_alloc_page(struct dma_pool *pool, gfp_t mem_flags)
214         struct dma_page *page;
216         page = kmalloc(sizeof(*page), mem_flags);
217         if (!page)
218                 return NULL;
219         page->vaddr = dma_alloc_coherent(pool->dev, pool->allocation,
220                                          &page->dma, mem_flags);
221         if (page->vaddr) {
222 #ifdef  DMAPOOL_DEBUG
223                 memset(page->vaddr, POOL_POISON_FREED, pool->allocation);
224 #endif
225                 pool_initialise_page(pool, page);
226                 page->in_use = 0;
227                 page->offset = 0;
228         } else {
229                 kfree(page);
230                 page = NULL;
231         }
232         return page;
235 static inline int is_page_busy(struct dma_page *page)
237         return page->in_use != 0;
240 static void pool_free_page(struct dma_pool *pool, struct dma_page *page)
242         dma_addr_t dma = page->dma;
244 #ifdef  DMAPOOL_DEBUG
245         memset(page->vaddr, POOL_POISON_FREED, pool->allocation);
246 #endif
247         dma_free_coherent(pool->dev, pool->allocation, page->vaddr, dma);
248         list_del(&page->page_list);
249         kfree(page);
252 /**
253  * dma_pool_destroy - destroys a pool of dma memory blocks.
254  * @pool: dma pool that will be destroyed
255  * Context: !in_interrupt()
256  *
257  * Caller guarantees that no more memory from the pool is in use,
258  * and that nothing will try to use the pool after this call.
259  */
260 void dma_pool_destroy(struct dma_pool *pool)
262         mutex_lock(&pools_lock);
263         list_del(&pool->pools);
264         if (pool->dev && list_empty(&pool->dev->dma_pools))
265                 device_remove_file(pool->dev, &dev_attr_pools);
266         mutex_unlock(&pools_lock);
268         while (!list_empty(&pool->page_list)) {
269                 struct dma_page *page;
270                 page = list_entry(pool->page_list.next,
271                                   struct dma_page, page_list);
272                 if (is_page_busy(page)) {
273                         if (pool->dev)
274                                 dev_err(pool->dev,
275                                         "dma_pool_destroy %s, %p busy\n",
276                                         pool->name, page->vaddr);
277                         else
278                                 printk(KERN_ERR
279                                        "dma_pool_destroy %s, %p busy\n",
280                                        pool->name, page->vaddr);
281                         /* leak the still-in-use consistent memory */
282                         list_del(&page->page_list);
283                         kfree(page);
284                 } else
285                         pool_free_page(pool, page);
286         }
288         kfree(pool);
290 EXPORT_SYMBOL(dma_pool_destroy);
292 /**
293  * dma_pool_alloc - get a block of consistent memory
294  * @pool: dma pool that will produce the block
295  * @mem_flags: GFP_* bitmask
296  * @handle: pointer to dma address of block
297  *
298  * This returns the kernel virtual address of a currently unused block,
299  * and reports its dma address through the handle.
300  * If such a memory block can't be allocated, %NULL is returned.
301  */
302 void *dma_pool_alloc(struct dma_pool *pool, gfp_t mem_flags,
303                      dma_addr_t *handle)
305         unsigned long flags;
306         struct dma_page *page;
307         size_t offset;
308         void *retval;
310         might_sleep_if(mem_flags & __GFP_WAIT);
312         spin_lock_irqsave(&pool->lock, flags);
313         list_for_each_entry(page, &pool->page_list, page_list) {
314                 if (page->offset < pool->allocation)
315                         goto ready;
316         }
318         /* pool_alloc_page() might sleep, so temporarily drop &pool->lock */
319         spin_unlock_irqrestore(&pool->lock, flags);
321         page = pool_alloc_page(pool, mem_flags);
322         if (!page)
323                 return NULL;
325         spin_lock_irqsave(&pool->lock, flags);
327         list_add(&page->page_list, &pool->page_list);
328  ready:
329         page->in_use++;
330         offset = page->offset;
331         page->offset = *(int *)(page->vaddr + offset);
332         retval = offset + page->vaddr;
333         *handle = offset + page->dma;
334 #ifdef  DMAPOOL_DEBUG
335         {
336                 int i;
337                 u8 *data = retval;
338                 /* page->offset is stored in first 4 bytes */
339                 for (i = sizeof(page->offset); i < pool->size; i++) {
340                         if (data[i] == POOL_POISON_FREED)
341                                 continue;
342                         if (pool->dev)
343                                 dev_err(pool->dev,
344                                         "dma_pool_alloc %s, %p (corruped)\n",
345                                         pool->name, retval);
346                         else
347                                 pr_err("dma_pool_alloc %s, %p (corruped)\n",
348                                         pool->name, retval);
350                         /*
351                          * Dump the first 4 bytes even if they are not
352                          * POOL_POISON_FREED
353                          */
354                         print_hex_dump(KERN_ERR, "", DUMP_PREFIX_OFFSET, 16, 1,
355                                         data, pool->size, 1);
356                         break;
357                 }
358         }
359         memset(retval, POOL_POISON_ALLOCATED, pool->size);
360 #endif
361         spin_unlock_irqrestore(&pool->lock, flags);
362         return retval;
364 EXPORT_SYMBOL(dma_pool_alloc);
366 static struct dma_page *pool_find_page(struct dma_pool *pool, dma_addr_t dma)
368         struct dma_page *page;
370         list_for_each_entry(page, &pool->page_list, page_list) {
371                 if (dma < page->dma)
372                         continue;
373                 if (dma < (page->dma + pool->allocation))
374                         return page;
375         }
376         return NULL;
379 /**
380  * dma_pool_free - put block back into dma pool
381  * @pool: the dma pool holding the block
382  * @vaddr: virtual address of block
383  * @dma: dma address of block
384  *
385  * Caller promises neither device nor driver will again touch this block
386  * unless it is first re-allocated.
387  */
388 void dma_pool_free(struct dma_pool *pool, void *vaddr, dma_addr_t dma)
390         struct dma_page *page;
391         unsigned long flags;
392         unsigned int offset;
394         spin_lock_irqsave(&pool->lock, flags);
395         page = pool_find_page(pool, dma);
396         if (!page) {
397                 spin_unlock_irqrestore(&pool->lock, flags);
398                 if (pool->dev)
399                         dev_err(pool->dev,
400                                 "dma_pool_free %s, %p/%lx (bad dma)\n",
401                                 pool->name, vaddr, (unsigned long)dma);
402                 else
403                         printk(KERN_ERR "dma_pool_free %s, %p/%lx (bad dma)\n",
404                                pool->name, vaddr, (unsigned long)dma);
405                 return;
406         }
408         offset = vaddr - page->vaddr;
409 #ifdef  DMAPOOL_DEBUG
410         if ((dma - page->dma) != offset) {
411                 spin_unlock_irqrestore(&pool->lock, flags);
412                 if (pool->dev)
413                         dev_err(pool->dev,
414                                 "dma_pool_free %s, %p (bad vaddr)/%Lx\n",
415                                 pool->name, vaddr, (unsigned long long)dma);
416                 else
417                         printk(KERN_ERR
418                                "dma_pool_free %s, %p (bad vaddr)/%Lx\n",
419                                pool->name, vaddr, (unsigned long long)dma);
420                 return;
421         }
422         {
423                 unsigned int chain = page->offset;
424                 while (chain < pool->allocation) {
425                         if (chain != offset) {
426                                 chain = *(int *)(page->vaddr + chain);
427                                 continue;
428                         }
429                         spin_unlock_irqrestore(&pool->lock, flags);
430                         if (pool->dev)
431                                 dev_err(pool->dev, "dma_pool_free %s, dma %Lx "
432                                         "already free\n", pool->name,
433                                         (unsigned long long)dma);
434                         else
435                                 printk(KERN_ERR "dma_pool_free %s, dma %Lx "
436                                         "already free\n", pool->name,
437                                         (unsigned long long)dma);
438                         return;
439                 }
440         }
441         memset(vaddr, POOL_POISON_FREED, pool->size);
442 #endif
444         page->in_use--;
445         *(int *)vaddr = page->offset;
446         page->offset = offset;
447         /*
448          * Resist a temptation to do
449          *    if (!is_page_busy(page)) pool_free_page(pool, page);
450          * Better have a few empty pages hang around.
451          */
452         spin_unlock_irqrestore(&pool->lock, flags);
454 EXPORT_SYMBOL(dma_pool_free);
456 /*
457  * Managed DMA pool
458  */
459 static void dmam_pool_release(struct device *dev, void *res)
461         struct dma_pool *pool = *(struct dma_pool **)res;
463         dma_pool_destroy(pool);
466 static int dmam_pool_match(struct device *dev, void *res, void *match_data)
468         return *(struct dma_pool **)res == match_data;
471 /**
472  * dmam_pool_create - Managed dma_pool_create()
473  * @name: name of pool, for diagnostics
474  * @dev: device that will be doing the DMA
475  * @size: size of the blocks in this pool.
476  * @align: alignment requirement for blocks; must be a power of two
477  * @allocation: returned blocks won't cross this boundary (or zero)
478  *
479  * Managed dma_pool_create().  DMA pool created with this function is
480  * automatically destroyed on driver detach.
481  */
482 struct dma_pool *dmam_pool_create(const char *name, struct device *dev,
483                                   size_t size, size_t align, size_t allocation)
485         struct dma_pool **ptr, *pool;
487         ptr = devres_alloc(dmam_pool_release, sizeof(*ptr), GFP_KERNEL);
488         if (!ptr)
489                 return NULL;
491         pool = *ptr = dma_pool_create(name, dev, size, align, allocation);
492         if (pool)
493                 devres_add(dev, ptr);
494         else
495                 devres_free(ptr);
497         return pool;
499 EXPORT_SYMBOL(dmam_pool_create);
501 /**
502  * dmam_pool_destroy - Managed dma_pool_destroy()
503  * @pool: dma pool that will be destroyed
504  *
505  * Managed dma_pool_destroy().
506  */
507 void dmam_pool_destroy(struct dma_pool *pool)
509         struct device *dev = pool->dev;
511         WARN_ON(devres_destroy(dev, dmam_pool_release, dmam_pool_match, pool));
512         dma_pool_destroy(pool);
514 EXPORT_SYMBOL(dmam_pool_destroy);