]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/blob - mm/mempool.c
ARM: OMAP5/DRA7: hwmod: add ADDR_TYPE_RT to bb2d address flags
[android-sdk/kernel-video.git] / mm / mempool.c
1 /*
2  *  linux/mm/mempool.c
3  *
4  *  memory buffer pool support. Such pools are mostly used
5  *  for guaranteed, deadlock-free memory allocations during
6  *  extreme VM load.
7  *
8  *  started by Ingo Molnar, Copyright (C) 2001
9  */
11 #include <linux/mm.h>
12 #include <linux/slab.h>
13 #include <linux/export.h>
14 #include <linux/mempool.h>
15 #include <linux/blkdev.h>
16 #include <linux/writeback.h>
18 static void add_element(mempool_t *pool, void *element)
19 {
20         BUG_ON(pool->curr_nr >= pool->min_nr);
21         pool->elements[pool->curr_nr++] = element;
22 }
24 static void *remove_element(mempool_t *pool)
25 {
26         BUG_ON(pool->curr_nr <= 0);
27         return pool->elements[--pool->curr_nr];
28 }
30 /**
31  * mempool_destroy - deallocate a memory pool
32  * @pool:      pointer to the memory pool which was allocated via
33  *             mempool_create().
34  *
35  * Free all reserved elements in @pool and @pool itself.  This function
36  * only sleeps if the free_fn() function sleeps.
37  */
38 void mempool_destroy(mempool_t *pool)
39 {
40         while (pool->curr_nr) {
41                 void *element = remove_element(pool);
42                 pool->free(element, pool->pool_data);
43         }
44         kfree(pool->elements);
45         kfree(pool);
46 }
47 EXPORT_SYMBOL(mempool_destroy);
49 /**
50  * mempool_create - create a memory pool
51  * @min_nr:    the minimum number of elements guaranteed to be
52  *             allocated for this pool.
53  * @alloc_fn:  user-defined element-allocation function.
54  * @free_fn:   user-defined element-freeing function.
55  * @pool_data: optional private data available to the user-defined functions.
56  *
57  * this function creates and allocates a guaranteed size, preallocated
58  * memory pool. The pool can be used from the mempool_alloc() and mempool_free()
59  * functions. This function might sleep. Both the alloc_fn() and the free_fn()
60  * functions might sleep - as long as the mempool_alloc() function is not called
61  * from IRQ contexts.
62  */
63 mempool_t *mempool_create(int min_nr, mempool_alloc_t *alloc_fn,
64                                 mempool_free_t *free_fn, void *pool_data)
65 {
66         return mempool_create_node(min_nr,alloc_fn,free_fn, pool_data,
67                                    GFP_KERNEL, NUMA_NO_NODE);
68 }
69 EXPORT_SYMBOL(mempool_create);
71 mempool_t *mempool_create_node(int min_nr, mempool_alloc_t *alloc_fn,
72                                mempool_free_t *free_fn, void *pool_data,
73                                gfp_t gfp_mask, int node_id)
74 {
75         mempool_t *pool;
76         pool = kmalloc_node(sizeof(*pool), gfp_mask | __GFP_ZERO, node_id);
77         if (!pool)
78                 return NULL;
79         pool->elements = kmalloc_node(min_nr * sizeof(void *),
80                                       gfp_mask, node_id);
81         if (!pool->elements) {
82                 kfree(pool);
83                 return NULL;
84         }
85         spin_lock_init(&pool->lock);
86         pool->min_nr = min_nr;
87         pool->pool_data = pool_data;
88         init_waitqueue_head(&pool->wait);
89         pool->alloc = alloc_fn;
90         pool->free = free_fn;
92         /*
93          * First pre-allocate the guaranteed number of buffers.
94          */
95         while (pool->curr_nr < pool->min_nr) {
96                 void *element;
98                 element = pool->alloc(gfp_mask, pool->pool_data);
99                 if (unlikely(!element)) {
100                         mempool_destroy(pool);
101                         return NULL;
102                 }
103                 add_element(pool, element);
104         }
105         return pool;
107 EXPORT_SYMBOL(mempool_create_node);
109 /**
110  * mempool_resize - resize an existing memory pool
111  * @pool:       pointer to the memory pool which was allocated via
112  *              mempool_create().
113  * @new_min_nr: the new minimum number of elements guaranteed to be
114  *              allocated for this pool.
115  * @gfp_mask:   the usual allocation bitmask.
116  *
117  * This function shrinks/grows the pool. In the case of growing,
118  * it cannot be guaranteed that the pool will be grown to the new
119  * size immediately, but new mempool_free() calls will refill it.
120  *
121  * Note, the caller must guarantee that no mempool_destroy is called
122  * while this function is running. mempool_alloc() & mempool_free()
123  * might be called (eg. from IRQ contexts) while this function executes.
124  */
125 int mempool_resize(mempool_t *pool, int new_min_nr, gfp_t gfp_mask)
127         void *element;
128         void **new_elements;
129         unsigned long flags;
131         BUG_ON(new_min_nr <= 0);
133         spin_lock_irqsave(&pool->lock, flags);
134         if (new_min_nr <= pool->min_nr) {
135                 while (new_min_nr < pool->curr_nr) {
136                         element = remove_element(pool);
137                         spin_unlock_irqrestore(&pool->lock, flags);
138                         pool->free(element, pool->pool_data);
139                         spin_lock_irqsave(&pool->lock, flags);
140                 }
141                 pool->min_nr = new_min_nr;
142                 goto out_unlock;
143         }
144         spin_unlock_irqrestore(&pool->lock, flags);
146         /* Grow the pool */
147         new_elements = kmalloc(new_min_nr * sizeof(*new_elements), gfp_mask);
148         if (!new_elements)
149                 return -ENOMEM;
151         spin_lock_irqsave(&pool->lock, flags);
152         if (unlikely(new_min_nr <= pool->min_nr)) {
153                 /* Raced, other resize will do our work */
154                 spin_unlock_irqrestore(&pool->lock, flags);
155                 kfree(new_elements);
156                 goto out;
157         }
158         memcpy(new_elements, pool->elements,
159                         pool->curr_nr * sizeof(*new_elements));
160         kfree(pool->elements);
161         pool->elements = new_elements;
162         pool->min_nr = new_min_nr;
164         while (pool->curr_nr < pool->min_nr) {
165                 spin_unlock_irqrestore(&pool->lock, flags);
166                 element = pool->alloc(gfp_mask, pool->pool_data);
167                 if (!element)
168                         goto out;
169                 spin_lock_irqsave(&pool->lock, flags);
170                 if (pool->curr_nr < pool->min_nr) {
171                         add_element(pool, element);
172                 } else {
173                         spin_unlock_irqrestore(&pool->lock, flags);
174                         pool->free(element, pool->pool_data);   /* Raced */
175                         goto out;
176                 }
177         }
178 out_unlock:
179         spin_unlock_irqrestore(&pool->lock, flags);
180 out:
181         return 0;
183 EXPORT_SYMBOL(mempool_resize);
185 /**
186  * mempool_alloc - allocate an element from a specific memory pool
187  * @pool:      pointer to the memory pool which was allocated via
188  *             mempool_create().
189  * @gfp_mask:  the usual allocation bitmask.
190  *
191  * this function only sleeps if the alloc_fn() function sleeps or
192  * returns NULL. Note that due to preallocation, this function
193  * *never* fails when called from process contexts. (it might
194  * fail if called from an IRQ context.)
195  */
196 void * mempool_alloc(mempool_t *pool, gfp_t gfp_mask)
198         void *element;
199         unsigned long flags;
200         wait_queue_t wait;
201         gfp_t gfp_temp;
203         might_sleep_if(gfp_mask & __GFP_WAIT);
205         gfp_mask |= __GFP_NOMEMALLOC;   /* don't allocate emergency reserves */
206         gfp_mask |= __GFP_NORETRY;      /* don't loop in __alloc_pages */
207         gfp_mask |= __GFP_NOWARN;       /* failures are OK */
209         gfp_temp = gfp_mask & ~(__GFP_WAIT|__GFP_IO);
211 repeat_alloc:
213         element = pool->alloc(gfp_temp, pool->pool_data);
214         if (likely(element != NULL))
215                 return element;
217         spin_lock_irqsave(&pool->lock, flags);
218         if (likely(pool->curr_nr)) {
219                 element = remove_element(pool);
220                 spin_unlock_irqrestore(&pool->lock, flags);
221                 /* paired with rmb in mempool_free(), read comment there */
222                 smp_wmb();
223                 return element;
224         }
226         /*
227          * We use gfp mask w/o __GFP_WAIT or IO for the first round.  If
228          * alloc failed with that and @pool was empty, retry immediately.
229          */
230         if (gfp_temp != gfp_mask) {
231                 spin_unlock_irqrestore(&pool->lock, flags);
232                 gfp_temp = gfp_mask;
233                 goto repeat_alloc;
234         }
236         /* We must not sleep if !__GFP_WAIT */
237         if (!(gfp_mask & __GFP_WAIT)) {
238                 spin_unlock_irqrestore(&pool->lock, flags);
239                 return NULL;
240         }
242         /* Let's wait for someone else to return an element to @pool */
243         init_wait(&wait);
244         prepare_to_wait(&pool->wait, &wait, TASK_UNINTERRUPTIBLE);
246         spin_unlock_irqrestore(&pool->lock, flags);
248         /*
249          * FIXME: this should be io_schedule().  The timeout is there as a
250          * workaround for some DM problems in 2.6.18.
251          */
252         io_schedule_timeout(5*HZ);
254         finish_wait(&pool->wait, &wait);
255         goto repeat_alloc;
257 EXPORT_SYMBOL(mempool_alloc);
259 /**
260  * mempool_free - return an element to the pool.
261  * @element:   pool element pointer.
262  * @pool:      pointer to the memory pool which was allocated via
263  *             mempool_create().
264  *
265  * this function only sleeps if the free_fn() function sleeps.
266  */
267 void mempool_free(void *element, mempool_t *pool)
269         unsigned long flags;
271         if (unlikely(element == NULL))
272                 return;
274         /*
275          * Paired with the wmb in mempool_alloc().  The preceding read is
276          * for @element and the following @pool->curr_nr.  This ensures
277          * that the visible value of @pool->curr_nr is from after the
278          * allocation of @element.  This is necessary for fringe cases
279          * where @element was passed to this task without going through
280          * barriers.
281          *
282          * For example, assume @p is %NULL at the beginning and one task
283          * performs "p = mempool_alloc(...);" while another task is doing
284          * "while (!p) cpu_relax(); mempool_free(p, ...);".  This function
285          * may end up using curr_nr value which is from before allocation
286          * of @p without the following rmb.
287          */
288         smp_rmb();
290         /*
291          * For correctness, we need a test which is guaranteed to trigger
292          * if curr_nr + #allocated == min_nr.  Testing curr_nr < min_nr
293          * without locking achieves that and refilling as soon as possible
294          * is desirable.
295          *
296          * Because curr_nr visible here is always a value after the
297          * allocation of @element, any task which decremented curr_nr below
298          * min_nr is guaranteed to see curr_nr < min_nr unless curr_nr gets
299          * incremented to min_nr afterwards.  If curr_nr gets incremented
300          * to min_nr after the allocation of @element, the elements
301          * allocated after that are subject to the same guarantee.
302          *
303          * Waiters happen iff curr_nr is 0 and the above guarantee also
304          * ensures that there will be frees which return elements to the
305          * pool waking up the waiters.
306          */
307         if (pool->curr_nr < pool->min_nr) {
308                 spin_lock_irqsave(&pool->lock, flags);
309                 if (pool->curr_nr < pool->min_nr) {
310                         add_element(pool, element);
311                         spin_unlock_irqrestore(&pool->lock, flags);
312                         wake_up(&pool->wait);
313                         return;
314                 }
315                 spin_unlock_irqrestore(&pool->lock, flags);
316         }
317         pool->free(element, pool->pool_data);
319 EXPORT_SYMBOL(mempool_free);
321 /*
322  * A commonly used alloc and free fn.
323  */
324 void *mempool_alloc_slab(gfp_t gfp_mask, void *pool_data)
326         struct kmem_cache *mem = pool_data;
327         return kmem_cache_alloc(mem, gfp_mask);
329 EXPORT_SYMBOL(mempool_alloc_slab);
331 void mempool_free_slab(void *element, void *pool_data)
333         struct kmem_cache *mem = pool_data;
334         kmem_cache_free(mem, element);
336 EXPORT_SYMBOL(mempool_free_slab);
338 /*
339  * A commonly used alloc and free fn that kmalloc/kfrees the amount of memory
340  * specified by pool_data
341  */
342 void *mempool_kmalloc(gfp_t gfp_mask, void *pool_data)
344         size_t size = (size_t)pool_data;
345         return kmalloc(size, gfp_mask);
347 EXPORT_SYMBOL(mempool_kmalloc);
349 void mempool_kfree(void *element, void *pool_data)
351         kfree(element);
353 EXPORT_SYMBOL(mempool_kfree);
355 /*
356  * A simple mempool-backed page allocator that allocates pages
357  * of the order specified by pool_data.
358  */
359 void *mempool_alloc_pages(gfp_t gfp_mask, void *pool_data)
361         int order = (int)(long)pool_data;
362         return alloc_pages(gfp_mask, order);
364 EXPORT_SYMBOL(mempool_alloc_pages);
366 void mempool_free_pages(void *element, void *pool_data)
368         int order = (int)(long)pool_data;
369         __free_pages(element, order);
371 EXPORT_SYMBOL(mempool_free_pages);