1 menu "Core Netfilter Configuration"
2 depends on NET && INET && NETFILTER
4 config NETFILTER_NETLINK
5 tristate
7 config NETFILTER_NETLINK_ACCT
8 tristate "Netfilter NFACCT over NFNETLINK interface"
9 depends on NETFILTER_ADVANCED
10 select NETFILTER_NETLINK
11 help
12 If this option is enabled, the kernel will include support
13 for extended accounting via NFNETLINK.
15 config NETFILTER_NETLINK_QUEUE
16 tristate "Netfilter NFQUEUE over NFNETLINK interface"
17 depends on NETFILTER_ADVANCED
18 select NETFILTER_NETLINK
19 help
20 If this option is enabled, the kernel will include support
21 for queueing packets via NFNETLINK.
23 config NETFILTER_NETLINK_LOG
24 tristate "Netfilter LOG over NFNETLINK interface"
25 default m if NETFILTER_ADVANCED=n
26 select NETFILTER_NETLINK
27 help
28 If this option is enabled, the kernel will include support
29 for logging packets via NFNETLINK.
31 This obsoletes the existing ipt_ULOG and ebg_ulog mechanisms,
32 and is also scheduled to replace the old syslog-based ipt_LOG
33 and ip6t_LOG modules.
35 config NF_CONNTRACK
36 tristate "Netfilter connection tracking support"
37 default m if NETFILTER_ADVANCED=n
38 help
39 Connection tracking keeps a record of what packets have passed
40 through your machine, in order to figure out how they are related
41 into connections.
43 This is required to do Masquerading or other kinds of Network
44 Address Translation. It can also be used to enhance packet
45 filtering (see `Connection state match support' below).
47 To compile it as a module, choose M here. If unsure, say N.
49 if NF_CONNTRACK
51 config NF_CONNTRACK_MARK
52 bool 'Connection mark tracking support'
53 depends on NETFILTER_ADVANCED
54 help
55 This option enables support for connection marks, used by the
56 `CONNMARK' target and `connmark' match. Similar to the mark value
57 of packets, but this mark value is kept in the conntrack session
58 instead of the individual packets.
60 config NF_CONNTRACK_SECMARK
61 bool 'Connection tracking security mark support'
62 depends on NETWORK_SECMARK
63 default m if NETFILTER_ADVANCED=n
64 help
65 This option enables security markings to be applied to
66 connections. Typically they are copied to connections from
67 packets using the CONNSECMARK target and copied back from
68 connections to packets with the same target, with the packets
69 being originally labeled via SECMARK.
71 If unsure, say 'N'.
73 config NF_CONNTRACK_ZONES
74 bool 'Connection tracking zones'
75 depends on NETFILTER_ADVANCED
76 depends on NETFILTER_XT_TARGET_CT
77 help
78 This option enables support for connection tracking zones.
79 Normally, each connection needs to have a unique system wide
80 identity. Connection tracking zones allow to have multiple
81 connections using the same identity, as long as they are
82 contained in different zones.
84 If unsure, say `N'.
86 config NF_CONNTRACK_PROCFS
87 bool "Supply CT list in procfs (OBSOLETE)"
88 default y
89 depends on PROC_FS
90 ---help---
91 This option enables for the list of known conntrack entries
92 to be shown in procfs under net/netfilter/nf_conntrack. This
93 is considered obsolete in favor of using the conntrack(8)
94 tool which uses Netlink.
96 config NF_CONNTRACK_EVENTS
97 bool "Connection tracking events"
98 depends on NETFILTER_ADVANCED
99 help
100 If this option is enabled, the connection tracking code will
101 provide a notifier chain that can be used by other kernel code
102 to get notified about changes in the connection tracking state.
104 If unsure, say `N'.
106 config NF_CONNTRACK_TIMEOUT
107 bool 'Connection tracking timeout'
108 depends on NETFILTER_ADVANCED
109 help
110 This option enables support for connection tracking timeout
111 extension. This allows you to attach timeout policies to flow
112 via the CT target.
114 If unsure, say `N'.
116 config NF_CONNTRACK_TIMESTAMP
117 bool 'Connection tracking timestamping'
118 depends on NETFILTER_ADVANCED
119 help
120 This option enables support for connection tracking timestamping.
121 This allows you to store the flow start-time and to obtain
122 the flow-stop time (once it has been destroyed) via Connection
123 tracking events.
125 If unsure, say `N'.
127 config NF_CONNTRACK_LABELS
128 bool
129 help
130 This option enables support for assigning user-defined flag bits
131 to connection tracking entries. It selected by the connlabel match.
133 config NF_CT_PROTO_DCCP
134 tristate 'DCCP protocol connection tracking support'
135 depends on NETFILTER_ADVANCED
136 default IP_DCCP
137 help
138 With this option enabled, the layer 3 independent connection
139 tracking code will be able to do state tracking on DCCP connections.
141 If unsure, say 'N'.
143 config NF_CT_PROTO_GRE
144 tristate
146 config NF_CT_PROTO_SCTP
147 tristate 'SCTP protocol connection tracking support'
148 depends on NETFILTER_ADVANCED
149 default IP_SCTP
150 help
151 With this option enabled, the layer 3 independent connection
152 tracking code will be able to do state tracking on SCTP connections.
154 If you want to compile it as a module, say M here and read
155 <file:Documentation/kbuild/modules.txt>. If unsure, say `N'.
157 config NF_CT_PROTO_UDPLITE
158 tristate 'UDP-Lite protocol connection tracking support'
159 depends on NETFILTER_ADVANCED
160 help
161 With this option enabled, the layer 3 independent connection
162 tracking code will be able to do state tracking on UDP-Lite
163 connections.
165 To compile it as a module, choose M here. If unsure, say N.
167 config NF_CONNTRACK_AMANDA
168 tristate "Amanda backup protocol support"
169 depends on NETFILTER_ADVANCED
170 select TEXTSEARCH
171 select TEXTSEARCH_KMP
172 help
173 If you are running the Amanda backup package <http://www.amanda.org/>
174 on this machine or machines that will be MASQUERADED through this
175 machine, then you may want to enable this feature. This allows the
176 connection tracking and natting code to allow the sub-channels that
177 Amanda requires for communication of the backup data, messages and
178 index.
180 To compile it as a module, choose M here. If unsure, say N.
182 config NF_CONNTRACK_FTP
183 tristate "FTP protocol support"
184 default m if NETFILTER_ADVANCED=n
185 help
186 Tracking FTP connections is problematic: special helpers are
187 required for tracking them, and doing masquerading and other forms
188 of Network Address Translation on them.
190 This is FTP support on Layer 3 independent connection tracking.
191 Layer 3 independent connection tracking is experimental scheme
192 which generalize ip_conntrack to support other layer 3 protocols.
194 To compile it as a module, choose M here. If unsure, say N.
196 config NF_CONNTRACK_H323
197 tristate "H.323 protocol support"
198 depends on (IPV6 || IPV6=n)
199 depends on NETFILTER_ADVANCED
200 help
201 H.323 is a VoIP signalling protocol from ITU-T. As one of the most
202 important VoIP protocols, it is widely used by voice hardware and
203 software including voice gateways, IP phones, Netmeeting, OpenPhone,
204 Gnomemeeting, etc.
206 With this module you can support H.323 on a connection tracking/NAT
207 firewall.
209 This module supports RAS, Fast Start, H.245 Tunnelling, Call
210 Forwarding, RTP/RTCP and T.120 based audio, video, fax, chat,
211 whiteboard, file transfer, etc. For more information, please
212 visit http://nath323.sourceforge.net/.
214 To compile it as a module, choose M here. If unsure, say N.
216 config NF_CONNTRACK_IRC
217 tristate "IRC protocol support"
218 default m if NETFILTER_ADVANCED=n
219 help
220 There is a commonly-used extension to IRC called
221 Direct Client-to-Client Protocol (DCC). This enables users to send
222 files to each other, and also chat to each other without the need
223 of a server. DCC Sending is used anywhere you send files over IRC,
224 and DCC Chat is most commonly used by Eggdrop bots. If you are
225 using NAT, this extension will enable you to send files and initiate
226 chats. Note that you do NOT need this extension to get files or
227 have others initiate chats, or everything else in IRC.
229 To compile it as a module, choose M here. If unsure, say N.
231 config NF_CONNTRACK_BROADCAST
232 tristate
234 config NF_CONNTRACK_NETBIOS_NS
235 tristate "NetBIOS name service protocol support"
236 select NF_CONNTRACK_BROADCAST
237 help
238 NetBIOS name service requests are sent as broadcast messages from an
239 unprivileged port and responded to with unicast messages to the
240 same port. This make them hard to firewall properly because connection
241 tracking doesn't deal with broadcasts. This helper tracks locally
242 originating NetBIOS name service requests and the corresponding
243 responses. It relies on correct IP address configuration, specifically
244 netmask and broadcast address. When properly configured, the output
245 of "ip address show" should look similar to this:
247 $ ip -4 address show eth0
248 4: eth0: <BROADCAST,MULTICAST,UP> mtu 1500 qdisc pfifo_fast qlen 1000
249 inet 172.16.2.252/24 brd 172.16.2.255 scope global eth0
251 To compile it as a module, choose M here. If unsure, say N.
253 config NF_CONNTRACK_SNMP
254 tristate "SNMP service protocol support"
255 depends on NETFILTER_ADVANCED
256 select NF_CONNTRACK_BROADCAST
257 help
258 SNMP service requests are sent as broadcast messages from an
259 unprivileged port and responded to with unicast messages to the
260 same port. This make them hard to firewall properly because connection
261 tracking doesn't deal with broadcasts. This helper tracks locally
262 originating SNMP service requests and the corresponding
263 responses. It relies on correct IP address configuration, specifically
264 netmask and broadcast address.
266 To compile it as a module, choose M here. If unsure, say N.
268 config NF_CONNTRACK_PPTP
269 tristate "PPtP protocol support"
270 depends on NETFILTER_ADVANCED
271 select NF_CT_PROTO_GRE
272 help
273 This module adds support for PPTP (Point to Point Tunnelling
274 Protocol, RFC2637) connection tracking and NAT.
276 If you are running PPTP sessions over a stateful firewall or NAT
277 box, you may want to enable this feature.
279 Please note that not all PPTP modes of operation are supported yet.
280 Specifically these limitations exist:
281 - Blindly assumes that control connections are always established
282 in PNS->PAC direction. This is a violation of RFC2637.
283 - Only supports a single call within each session
285 To compile it as a module, choose M here. If unsure, say N.
287 config NF_CONNTRACK_SANE
288 tristate "SANE protocol support"
289 depends on NETFILTER_ADVANCED
290 help
291 SANE is a protocol for remote access to scanners as implemented
292 by the 'saned' daemon. Like FTP, it uses separate control and
293 data connections.
295 With this module you can support SANE on a connection tracking
296 firewall.
298 To compile it as a module, choose M here. If unsure, say N.
300 config NF_CONNTRACK_SIP
301 tristate "SIP protocol support"
302 default m if NETFILTER_ADVANCED=n
303 help
304 SIP is an application-layer control protocol that can establish,
305 modify, and terminate multimedia sessions (conferences) such as
306 Internet telephony calls. With the ip_conntrack_sip and
307 the nf_nat_sip modules you can support the protocol on a connection
308 tracking/NATing firewall.
310 To compile it as a module, choose M here. If unsure, say N.
312 config NF_CONNTRACK_TFTP
313 tristate "TFTP protocol support"
314 depends on NETFILTER_ADVANCED
315 help
316 TFTP connection tracking helper, this is required depending
317 on how restrictive your ruleset is.
318 If you are using a tftp client behind -j SNAT or -j MASQUERADING
319 you will need this.
321 To compile it as a module, choose M here. If unsure, say N.
323 config NF_CT_NETLINK
324 tristate 'Connection tracking netlink interface'
325 select NETFILTER_NETLINK
326 default m if NETFILTER_ADVANCED=n
327 help
328 This option enables support for a netlink-based userspace interface
330 config NF_CT_NETLINK_TIMEOUT
331 tristate 'Connection tracking timeout tuning via Netlink'
332 select NETFILTER_NETLINK
333 depends on NETFILTER_ADVANCED
334 help
335 This option enables support for connection tracking timeout
336 fine-grain tuning. This allows you to attach specific timeout
337 policies to flows, instead of using the global timeout policy.
339 If unsure, say `N'.
341 config NF_CT_NETLINK_HELPER
342 tristate 'Connection tracking helpers in user-space via Netlink'
343 select NETFILTER_NETLINK
344 depends on NF_CT_NETLINK
345 depends on NETFILTER_NETLINK_QUEUE
346 depends on NETFILTER_NETLINK_QUEUE_CT
347 depends on NETFILTER_ADVANCED
348 help
349 This option enables the user-space connection tracking helpers
350 infrastructure.
352 If unsure, say `N'.
354 config NETFILTER_NETLINK_QUEUE_CT
355 bool "NFQUEUE integration with Connection Tracking"
356 default n
357 depends on NETFILTER_NETLINK_QUEUE
358 help
359 If this option is enabled, NFQUEUE can include Connection Tracking
360 information together with the packet is the enqueued via NFNETLINK.
362 config NF_NAT
363 tristate
365 config NF_NAT_NEEDED
366 bool
367 depends on NF_NAT
368 default y
370 config NF_NAT_PROTO_DCCP
371 tristate
372 depends on NF_NAT && NF_CT_PROTO_DCCP
373 default NF_NAT && NF_CT_PROTO_DCCP
375 config NF_NAT_PROTO_UDPLITE
376 tristate
377 depends on NF_NAT && NF_CT_PROTO_UDPLITE
378 default NF_NAT && NF_CT_PROTO_UDPLITE
380 config NF_NAT_PROTO_SCTP
381 tristate
382 default NF_NAT && NF_CT_PROTO_SCTP
383 depends on NF_NAT && NF_CT_PROTO_SCTP
384 select LIBCRC32C
386 config NF_NAT_AMANDA
387 tristate
388 depends on NF_CONNTRACK && NF_NAT
389 default NF_NAT && NF_CONNTRACK_AMANDA
391 config NF_NAT_FTP
392 tristate
393 depends on NF_CONNTRACK && NF_NAT
394 default NF_NAT && NF_CONNTRACK_FTP
396 config NF_NAT_IRC
397 tristate
398 depends on NF_CONNTRACK && NF_NAT
399 default NF_NAT && NF_CONNTRACK_IRC
401 config NF_NAT_SIP
402 tristate
403 depends on NF_CONNTRACK && NF_NAT
404 default NF_NAT && NF_CONNTRACK_SIP
406 config NF_NAT_TFTP
407 tristate
408 depends on NF_CONNTRACK && NF_NAT
409 default NF_NAT && NF_CONNTRACK_TFTP
411 config NETFILTER_SYNPROXY
412 tristate
414 endif # NF_CONNTRACK
416 config NF_TABLES
417 select NETFILTER_NETLINK
418 tristate "Netfilter nf_tables support"
419 help
420 nftables is the new packet classification framework that intends to
421 replace the existing {ip,ip6,arp,eb}_tables infrastructure. It
422 provides a pseudo-state machine with an extensible instruction-set
423 (also known as expressions) that the userspace 'nft' utility
424 (http://www.netfilter.org/projects/nftables) uses to build the
425 rule-set. It also comes with the generic set infrastructure that
426 allows you to construct mappings between matchings and actions
427 for performance lookups.
429 To compile it as a module, choose M here.
431 config NF_TABLES_INET
432 depends on NF_TABLES && IPV6
433 select NF_TABLES_IPV4
434 select NF_TABLES_IPV6
435 tristate "Netfilter nf_tables mixed IPv4/IPv6 tables support"
436 help
437 This option enables support for a mixed IPv4/IPv6 "inet" table.
439 config NFT_EXTHDR
440 depends on NF_TABLES
441 tristate "Netfilter nf_tables IPv6 exthdr module"
442 help
443 This option adds the "exthdr" expression that you can use to match
444 IPv6 extension headers.
446 config NFT_META
447 depends on NF_TABLES
448 tristate "Netfilter nf_tables meta module"
449 help
450 This option adds the "meta" expression that you can use to match and
451 to set packet metainformation such as the packet mark.
453 config NFT_CT
454 depends on NF_TABLES
455 depends on NF_CONNTRACK
456 tristate "Netfilter nf_tables conntrack module"
457 help
458 This option adds the "meta" expression that you can use to match
459 connection tracking information such as the flow state.
461 config NFT_RBTREE
462 depends on NF_TABLES
463 tristate "Netfilter nf_tables rbtree set module"
464 help
465 This option adds the "rbtree" set type (Red Black tree) that is used
466 to build interval-based sets.
468 config NFT_HASH
469 depends on NF_TABLES
470 tristate "Netfilter nf_tables hash set module"
471 help
472 This option adds the "hash" set type that is used to build one-way
473 mappings between matchings and actions.
475 config NFT_COUNTER
476 depends on NF_TABLES
477 tristate "Netfilter nf_tables counter module"
478 help
479 This option adds the "counter" expression that you can use to
480 include packet and byte counters in a rule.
482 config NFT_LOG
483 depends on NF_TABLES
484 tristate "Netfilter nf_tables log module"
485 help
486 This option adds the "log" expression that you can use to log
487 packets matching some criteria.
489 config NFT_LIMIT
490 depends on NF_TABLES
491 tristate "Netfilter nf_tables limit module"
492 help
493 This option adds the "limit" expression that you can use to
494 ratelimit rule matchings.
496 config NFT_NAT
497 depends on NF_TABLES
498 depends on NF_CONNTRACK
499 depends on NF_NAT
500 tristate "Netfilter nf_tables nat module"
501 help
502 This option adds the "nat" expression that you can use to perform
503 typical Network Address Translation (NAT) packet transformations.
505 config NFT_QUEUE
506 depends on NF_TABLES
507 depends on NETFILTER_XTABLES
508 depends on NETFILTER_NETLINK_QUEUE
509 tristate "Netfilter nf_tables queue module"
510 help
511 This is required if you intend to use the userspace queueing
512 infrastructure (also known as NFQUEUE) from nftables.
514 config NFT_REJECT
515 depends on NF_TABLES
516 default m if NETFILTER_ADVANCED=n
517 tristate "Netfilter nf_tables reject support"
518 help
519 This option adds the "reject" expression that you can use to
520 explicitly deny and notify via TCP reset/ICMP informational errors
521 unallowed traffic.
523 config NFT_REJECT_INET
524 depends on NF_TABLES_INET
525 default NFT_REJECT
526 tristate
528 config NFT_COMPAT
529 depends on NF_TABLES
530 depends on NETFILTER_XTABLES
531 tristate "Netfilter x_tables over nf_tables module"
532 help
533 This is required if you intend to use any of existing
534 x_tables match/target extensions over the nf_tables
535 framework.
537 config NETFILTER_XTABLES
538 tristate "Netfilter Xtables support (required for ip_tables)"
539 default m if NETFILTER_ADVANCED=n
540 help
541 This is required if you intend to use any of ip_tables,
542 ip6_tables or arp_tables.
544 if NETFILTER_XTABLES
546 comment "Xtables combined modules"
548 config NETFILTER_XT_MARK
549 tristate 'nfmark target and match support'
550 default m if NETFILTER_ADVANCED=n
551 ---help---
552 This option adds the "MARK" target and "mark" match.
554 Netfilter mark matching allows you to match packets based on the
555 "nfmark" value in the packet.
556 The target allows you to create rules in the "mangle" table which alter
557 the netfilter mark (nfmark) field associated with the packet.
559 Prior to routing, the nfmark can influence the routing method (see
560 "Use netfilter MARK value as routing key") and can also be used by
561 other subsystems to change their behavior.
563 config NETFILTER_XT_CONNMARK
564 tristate 'ctmark target and match support'
565 depends on NF_CONNTRACK
566 depends on NETFILTER_ADVANCED
567 select NF_CONNTRACK_MARK
568 ---help---
569 This option adds the "CONNMARK" target and "connmark" match.
571 Netfilter allows you to store a mark value per connection (a.k.a.
572 ctmark), similarly to the packet mark (nfmark). Using this
573 target and match, you can set and match on this mark.
575 config NETFILTER_XT_SET
576 tristate 'set target and match support'
577 depends on IP_SET
578 depends on NETFILTER_ADVANCED
579 help
580 This option adds the "SET" target and "set" match.
582 Using this target and match, you can add/delete and match
583 elements in the sets created by ipset(8).
585 To compile it as a module, choose M here. If unsure, say N.
587 # alphabetically ordered list of targets
589 comment "Xtables targets"
591 config NETFILTER_XT_TARGET_AUDIT
592 tristate "AUDIT target support"
593 depends on AUDIT
594 depends on NETFILTER_ADVANCED
595 ---help---
596 This option adds a 'AUDIT' target, which can be used to create
597 audit records for packets dropped/accepted.
599 To compileit as a module, choose M here. If unsure, say N.
601 config NETFILTER_XT_TARGET_CHECKSUM
602 tristate "CHECKSUM target support"
603 depends on IP_NF_MANGLE || IP6_NF_MANGLE
604 depends on NETFILTER_ADVANCED
605 ---help---
606 This option adds a `CHECKSUM' target, which can be used in the iptables mangle
607 table.
609 You can use this target to compute and fill in the checksum in
610 a packet that lacks a checksum. This is particularly useful,
611 if you need to work around old applications such as dhcp clients,
612 that do not work well with checksum offloads, but don't want to disable
613 checksum offload in your device.
615 To compile it as a module, choose M here. If unsure, say N.
617 config NETFILTER_XT_TARGET_CLASSIFY
618 tristate '"CLASSIFY" target support'
619 depends on NETFILTER_ADVANCED
620 help
621 This option adds a `CLASSIFY' target, which enables the user to set
622 the priority of a packet. Some qdiscs can use this value for
623 classification, among these are:
625 atm, cbq, dsmark, pfifo_fast, htb, prio
627 To compile it as a module, choose M here. If unsure, say N.
629 config NETFILTER_XT_TARGET_CONNMARK
630 tristate '"CONNMARK" target support'
631 depends on NF_CONNTRACK
632 depends on NETFILTER_ADVANCED
633 select NETFILTER_XT_CONNMARK
634 ---help---
635 This is a backwards-compat option for the user's convenience
636 (e.g. when running oldconfig). It selects
637 CONFIG_NETFILTER_XT_CONNMARK (combined connmark/CONNMARK module).
639 config NETFILTER_XT_TARGET_CONNSECMARK
640 tristate '"CONNSECMARK" target support'
641 depends on NF_CONNTRACK && NF_CONNTRACK_SECMARK
642 default m if NETFILTER_ADVANCED=n
643 help
644 The CONNSECMARK target copies security markings from packets
645 to connections, and restores security markings from connections
646 to packets (if the packets are not already marked). This would
647 normally be used in conjunction with the SECMARK target.
649 To compile it as a module, choose M here. If unsure, say N.
651 config NETFILTER_XT_TARGET_CT
652 tristate '"CT" target support'
653 depends on NF_CONNTRACK
654 depends on IP_NF_RAW || IP6_NF_RAW
655 depends on NETFILTER_ADVANCED
656 help
657 This options adds a `CT' target, which allows to specify initial
658 connection tracking parameters like events to be delivered and
659 the helper to be used.
661 To compile it as a module, choose M here. If unsure, say N.
663 config NETFILTER_XT_TARGET_DSCP
664 tristate '"DSCP" and "TOS" target support'
665 depends on IP_NF_MANGLE || IP6_NF_MANGLE
666 depends on NETFILTER_ADVANCED
667 help
668 This option adds a `DSCP' target, which allows you to manipulate
669 the IPv4/IPv6 header DSCP field (differentiated services codepoint).
671 The DSCP field can have any value between 0x0 and 0x3f inclusive.
673 It also adds the "TOS" target, which allows you to create rules in
674 the "mangle" table which alter the Type Of Service field of an IPv4
675 or the Priority field of an IPv6 packet, prior to routing.
677 To compile it as a module, choose M here. If unsure, say N.
679 config NETFILTER_XT_TARGET_HL
680 tristate '"HL" hoplimit target support'
681 depends on IP_NF_MANGLE || IP6_NF_MANGLE
682 depends on NETFILTER_ADVANCED
683 ---help---
684 This option adds the "HL" (for IPv6) and "TTL" (for IPv4)
685 targets, which enable the user to change the
686 hoplimit/time-to-live value of the IP header.
688 While it is safe to decrement the hoplimit/TTL value, the
689 modules also allow to increment and set the hoplimit value of
690 the header to arbitrary values. This is EXTREMELY DANGEROUS
691 since you can easily create immortal packets that loop
692 forever on the network.
694 config NETFILTER_XT_TARGET_HMARK
695 tristate '"HMARK" target support'
696 depends on (IP6_NF_IPTABLES || IP6_NF_IPTABLES=n)
697 depends on NETFILTER_ADVANCED
698 ---help---
699 This option adds the "HMARK" target.
701 The target allows you to create rules in the "raw" and "mangle" tables
702 which set the skbuff mark by means of hash calculation within a given
703 range. The nfmark can influence the routing method (see "Use netfilter
704 MARK value as routing key") and can also be used by other subsystems to
705 change their behaviour.
707 To compile it as a module, choose M here. If unsure, say N.
709 config NETFILTER_XT_TARGET_IDLETIMER
710 tristate "IDLETIMER target support"
711 depends on NETFILTER_ADVANCED
712 help
714 This option adds the `IDLETIMER' target. Each matching packet
715 resets the timer associated with label specified when the rule is
716 added. When the timer expires, it triggers a sysfs notification.
717 The remaining time for expiration can be read via sysfs.
719 To compile it as a module, choose M here. If unsure, say N.
721 config NETFILTER_XT_TARGET_LED
722 tristate '"LED" target support'
723 depends on LEDS_CLASS && LEDS_TRIGGERS
724 depends on NETFILTER_ADVANCED
725 help
726 This option adds a `LED' target, which allows you to blink LEDs in
727 response to particular packets passing through your machine.
729 This can be used to turn a spare LED into a network activity LED,
730 which only flashes in response to FTP transfers, for example. Or
731 you could have an LED which lights up for a minute or two every time
732 somebody connects to your machine via SSH.
734 You will need support for the "led" class to make this work.
736 To create an LED trigger for incoming SSH traffic:
737 iptables -A INPUT -p tcp --dport 22 -j LED --led-trigger-id ssh --led-delay 1000
739 Then attach the new trigger to an LED on your system:
740 echo netfilter-ssh > /sys/class/leds/<ledname>/trigger
742 For more information on the LEDs available on your system, see
743 Documentation/leds/leds-class.txt
745 config NETFILTER_XT_TARGET_LOG
746 tristate "LOG target support"
747 default m if NETFILTER_ADVANCED=n
748 help
749 This option adds a `LOG' target, which allows you to create rules in
750 any iptables table which records the packet header to the syslog.
752 To compile it as a module, choose M here. If unsure, say N.
754 config NETFILTER_XT_TARGET_MARK
755 tristate '"MARK" target support'
756 depends on NETFILTER_ADVANCED
757 select NETFILTER_XT_MARK
758 ---help---
759 This is a backwards-compat option for the user's convenience
760 (e.g. when running oldconfig). It selects
761 CONFIG_NETFILTER_XT_MARK (combined mark/MARK module).
763 config NETFILTER_XT_TARGET_NETMAP
764 tristate '"NETMAP" target support'
765 depends on NF_NAT
766 ---help---
767 NETMAP is an implementation of static 1:1 NAT mapping of network
768 addresses. It maps the network address part, while keeping the host
769 address part intact.
771 To compile it as a module, choose M here. If unsure, say N.
773 config NETFILTER_XT_TARGET_NFLOG
774 tristate '"NFLOG" target support'
775 default m if NETFILTER_ADVANCED=n
776 select NETFILTER_NETLINK_LOG
777 help
778 This option enables the NFLOG target, which allows to LOG
779 messages through nfnetlink_log.
781 To compile it as a module, choose M here. If unsure, say N.
783 config NETFILTER_XT_TARGET_NFQUEUE
784 tristate '"NFQUEUE" target Support'
785 depends on NETFILTER_ADVANCED
786 select NETFILTER_NETLINK_QUEUE
787 help
788 This target replaced the old obsolete QUEUE target.
790 As opposed to QUEUE, it supports 65535 different queues,
791 not just one.
793 To compile it as a module, choose M here. If unsure, say N.
795 config NETFILTER_XT_TARGET_NOTRACK
796 tristate '"NOTRACK" target support (DEPRECATED)'
797 depends on NF_CONNTRACK
798 depends on IP_NF_RAW || IP6_NF_RAW
799 depends on NETFILTER_ADVANCED
800 select NETFILTER_XT_TARGET_CT
802 config NETFILTER_XT_TARGET_RATEEST
803 tristate '"RATEEST" target support'
804 depends on NETFILTER_ADVANCED
805 help
806 This option adds a `RATEEST' target, which allows to measure
807 rates similar to TC estimators. The `rateest' match can be
808 used to match on the measured rates.
810 To compile it as a module, choose M here. If unsure, say N.
812 config NETFILTER_XT_TARGET_REDIRECT
813 tristate "REDIRECT target support"
814 depends on NF_NAT
815 ---help---
816 REDIRECT is a special case of NAT: all incoming connections are
817 mapped onto the incoming interface's address, causing the packets to
818 come to the local machine instead of passing through. This is
819 useful for transparent proxies.
821 To compile it as a module, choose M here. If unsure, say N.
823 config NETFILTER_XT_TARGET_TEE
824 tristate '"TEE" - packet cloning to alternate destination'
825 depends on NETFILTER_ADVANCED
826 depends on (IPV6 || IPV6=n)
827 depends on !NF_CONNTRACK || NF_CONNTRACK
828 ---help---
829 This option adds a "TEE" target with which a packet can be cloned and
830 this clone be rerouted to another nexthop.
832 config NETFILTER_XT_TARGET_TPROXY
833 tristate '"TPROXY" target transparent proxying support'
834 depends on NETFILTER_XTABLES
835 depends on NETFILTER_ADVANCED
836 depends on IP_NF_MANGLE
837 select NF_DEFRAG_IPV4
838 select NF_DEFRAG_IPV6 if IP6_NF_IPTABLES
839 help
840 This option adds a `TPROXY' target, which is somewhat similar to
841 REDIRECT. It can only be used in the mangle table and is useful
842 to redirect traffic to a transparent proxy. It does _not_ depend
843 on Netfilter connection tracking and NAT, unlike REDIRECT.
844 For it to work you will have to configure certain iptables rules
845 and use policy routing. For more information on how to set it up
846 see Documentation/networking/tproxy.txt.
848 To compile it as a module, choose M here. If unsure, say N.
850 config NETFILTER_XT_TARGET_TRACE
851 tristate '"TRACE" target support'
852 depends on IP_NF_RAW || IP6_NF_RAW
853 depends on NETFILTER_ADVANCED
854 help
855 The TRACE target allows you to mark packets so that the kernel
856 will log every rule which match the packets as those traverse
857 the tables, chains, rules.
859 If you want to compile it as a module, say M here and read
860 <file:Documentation/kbuild/modules.txt>. If unsure, say `N'.
862 config NETFILTER_XT_TARGET_SECMARK
863 tristate '"SECMARK" target support'
864 depends on NETWORK_SECMARK
865 default m if NETFILTER_ADVANCED=n
866 help
867 The SECMARK target allows security marking of network
868 packets, for use with security subsystems.
870 To compile it as a module, choose M here. If unsure, say N.
872 config NETFILTER_XT_TARGET_TCPMSS
873 tristate '"TCPMSS" target support'
874 depends on (IPV6 || IPV6=n)
875 default m if NETFILTER_ADVANCED=n
876 ---help---
877 This option adds a `TCPMSS' target, which allows you to alter the
878 MSS value of TCP SYN packets, to control the maximum size for that
879 connection (usually limiting it to your outgoing interface's MTU
880 minus 40).
882 This is used to overcome criminally braindead ISPs or servers which
883 block ICMP Fragmentation Needed packets. The symptoms of this
884 problem are that everything works fine from your Linux
885 firewall/router, but machines behind it can never exchange large
886 packets:
887 1) Web browsers connect, then hang with no data received.
888 2) Small mail works fine, but large emails hang.
889 3) ssh works fine, but scp hangs after initial handshaking.
891 Workaround: activate this option and add a rule to your firewall
892 configuration like:
894 iptables -A FORWARD -p tcp --tcp-flags SYN,RST SYN \
895 -j TCPMSS --clamp-mss-to-pmtu
897 To compile it as a module, choose M here. If unsure, say N.
899 config NETFILTER_XT_TARGET_TCPOPTSTRIP
900 tristate '"TCPOPTSTRIP" target support'
901 depends on IP_NF_MANGLE || IP6_NF_MANGLE
902 depends on NETFILTER_ADVANCED
903 help
904 This option adds a "TCPOPTSTRIP" target, which allows you to strip
905 TCP options from TCP packets.
907 # alphabetically ordered list of matches
909 comment "Xtables matches"
911 config NETFILTER_XT_MATCH_ADDRTYPE
912 tristate '"addrtype" address type match support'
913 depends on NETFILTER_ADVANCED
914 ---help---
915 This option allows you to match what routing thinks of an address,
916 eg. UNICAST, LOCAL, BROADCAST, ...
918 If you want to compile it as a module, say M here and read
919 <file:Documentation/kbuild/modules.txt>. If unsure, say `N'.
921 config NETFILTER_XT_MATCH_BPF
922 tristate '"bpf" match support'
923 depends on NETFILTER_ADVANCED
924 help
925 BPF matching applies a linux socket filter to each packet and
926 accepts those for which the filter returns non-zero.
928 To compile it as a module, choose M here. If unsure, say N.
930 config NETFILTER_XT_MATCH_CGROUP
931 tristate '"control group" match support'
932 depends on NETFILTER_ADVANCED
933 depends on CGROUPS
934 select CGROUP_NET_CLASSID
935 ---help---
936 Socket/process control group matching allows you to match locally
937 generated packets based on which net_cls control group processes
938 belong to.
940 config NETFILTER_XT_MATCH_CLUSTER
941 tristate '"cluster" match support'
942 depends on NF_CONNTRACK
943 depends on NETFILTER_ADVANCED
944 ---help---
945 This option allows you to build work-load-sharing clusters of
946 network servers/stateful firewalls without having a dedicated
947 load-balancing router/server/switch. Basically, this match returns
948 true when the packet must be handled by this cluster node. Thus,
949 all nodes see all packets and this match decides which node handles
950 what packets. The work-load sharing algorithm is based on source
951 address hashing.
953 If you say Y or M here, try `iptables -m cluster --help` for
954 more information.
956 config NETFILTER_XT_MATCH_COMMENT
957 tristate '"comment" match support'
958 depends on NETFILTER_ADVANCED
959 help
960 This option adds a `comment' dummy-match, which allows you to put
961 comments in your iptables ruleset.
963 If you want to compile it as a module, say M here and read
964 <file:Documentation/kbuild/modules.txt>. If unsure, say `N'.
966 config NETFILTER_XT_MATCH_CONNBYTES
967 tristate '"connbytes" per-connection counter match support'
968 depends on NF_CONNTRACK
969 depends on NETFILTER_ADVANCED
970 help
971 This option adds a `connbytes' match, which allows you to match the
972 number of bytes and/or packets for each direction within a connection.
974 If you want to compile it as a module, say M here and read
975 <file:Documentation/kbuild/modules.txt>. If unsure, say `N'.
977 config NETFILTER_XT_MATCH_CONNLABEL
978 tristate '"connlabel" match support'
979 select NF_CONNTRACK_LABELS
980 depends on NF_CONNTRACK
981 depends on NETFILTER_ADVANCED
982 ---help---
983 This match allows you to test and assign userspace-defined labels names
984 to a connection. The kernel only stores bit values - mapping
985 names to bits is done by userspace.
987 Unlike connmark, more than 32 flag bits may be assigned to a
988 connection simultaneously.
990 config NETFILTER_XT_MATCH_CONNLIMIT
991 tristate '"connlimit" match support'
992 depends on NF_CONNTRACK
993 depends on NETFILTER_ADVANCED
994 ---help---
995 This match allows you to match against the number of parallel
996 connections to a server per client IP address (or address block).
998 config NETFILTER_XT_MATCH_CONNMARK
999 tristate '"connmark" connection mark match support'
1000 depends on NF_CONNTRACK
1001 depends on NETFILTER_ADVANCED
1002 select NETFILTER_XT_CONNMARK
1003 ---help---
1004 This is a backwards-compat option for the user's convenience
1005 (e.g. when running oldconfig). It selects
1006 CONFIG_NETFILTER_XT_CONNMARK (combined connmark/CONNMARK module).
1008 config NETFILTER_XT_MATCH_CONNTRACK
1009 tristate '"conntrack" connection tracking match support'
1010 depends on NF_CONNTRACK
1011 default m if NETFILTER_ADVANCED=n
1012 help
1013 This is a general conntrack match module, a superset of the state match.
1015 It allows matching on additional conntrack information, which is
1016 useful in complex configurations, such as NAT gateways with multiple
1017 internet links or tunnels.
1019 To compile it as a module, choose M here. If unsure, say N.
1021 config NETFILTER_XT_MATCH_CPU
1022 tristate '"cpu" match support'
1023 depends on NETFILTER_ADVANCED
1024 help
1025 CPU matching allows you to match packets based on the CPU
1026 currently handling the packet.
1028 To compile it as a module, choose M here. If unsure, say N.
1030 config NETFILTER_XT_MATCH_DCCP
1031 tristate '"dccp" protocol match support'
1032 depends on NETFILTER_ADVANCED
1033 default IP_DCCP
1034 help
1035 With this option enabled, you will be able to use the iptables
1036 `dccp' match in order to match on DCCP source/destination ports
1037 and DCCP flags.
1039 If you want to compile it as a module, say M here and read
1040 <file:Documentation/kbuild/modules.txt>. If unsure, say `N'.
1042 config NETFILTER_XT_MATCH_DEVGROUP
1043 tristate '"devgroup" match support'
1044 depends on NETFILTER_ADVANCED
1045 help
1046 This options adds a `devgroup' match, which allows to match on the
1047 device group a network device is assigned to.
1049 To compile it as a module, choose M here. If unsure, say N.
1051 config NETFILTER_XT_MATCH_DSCP
1052 tristate '"dscp" and "tos" match support'
1053 depends on NETFILTER_ADVANCED
1054 help
1055 This option adds a `DSCP' match, which allows you to match against
1056 the IPv4/IPv6 header DSCP field (differentiated services codepoint).
1058 The DSCP field can have any value between 0x0 and 0x3f inclusive.
1060 It will also add a "tos" match, which allows you to match packets
1061 based on the Type Of Service fields of the IPv4 packet (which share
1062 the same bits as DSCP).
1064 To compile it as a module, choose M here. If unsure, say N.
1066 config NETFILTER_XT_MATCH_ECN
1067 tristate '"ecn" match support'
1068 depends on NETFILTER_ADVANCED
1069 ---help---
1070 This option adds an "ECN" match, which allows you to match against
1071 the IPv4 and TCP header ECN fields.
1073 To compile it as a module, choose M here. If unsure, say N.
1075 config NETFILTER_XT_MATCH_ESP
1076 tristate '"esp" match support'
1077 depends on NETFILTER_ADVANCED
1078 help
1079 This match extension allows you to match a range of SPIs
1080 inside ESP header of IPSec packets.
1082 To compile it as a module, choose M here. If unsure, say N.
1084 config NETFILTER_XT_MATCH_HASHLIMIT
1085 tristate '"hashlimit" match support'
1086 depends on (IP6_NF_IPTABLES || IP6_NF_IPTABLES=n)
1087 depends on NETFILTER_ADVANCED
1088 help
1089 This option adds a `hashlimit' match.
1091 As opposed to `limit', this match dynamically creates a hash table
1092 of limit buckets, based on your selection of source/destination
1093 addresses and/or ports.
1095 It enables you to express policies like `10kpps for any given
1096 destination address' or `500pps from any given source address'
1097 with a single rule.
1099 config NETFILTER_XT_MATCH_HELPER
1100 tristate '"helper" match support'
1101 depends on NF_CONNTRACK
1102 depends on NETFILTER_ADVANCED
1103 help
1104 Helper matching allows you to match packets in dynamic connections
1105 tracked by a conntrack-helper, ie. ip_conntrack_ftp
1107 To compile it as a module, choose M here. If unsure, say Y.
1109 config NETFILTER_XT_MATCH_HL
1110 tristate '"hl" hoplimit/TTL match support'
1111 depends on NETFILTER_ADVANCED
1112 ---help---
1113 HL matching allows you to match packets based on the hoplimit
1114 in the IPv6 header, or the time-to-live field in the IPv4
1115 header of the packet.
1117 config NETFILTER_XT_MATCH_IPCOMP
1118 tristate '"ipcomp" match support'
1119 depends on NETFILTER_ADVANCED
1120 help
1121 This match extension allows you to match a range of CPIs(16 bits)
1122 inside IPComp header of IPSec packets.
1124 To compile it as a module, choose M here. If unsure, say N.
1126 config NETFILTER_XT_MATCH_IPRANGE
1127 tristate '"iprange" address range match support'
1128 depends on NETFILTER_ADVANCED
1129 ---help---
1130 This option adds a "iprange" match, which allows you to match based on
1131 an IP address range. (Normal iptables only matches on single addresses
1132 with an optional mask.)
1134 If unsure, say M.
1136 config NETFILTER_XT_MATCH_IPVS
1137 tristate '"ipvs" match support'
1138 depends on IP_VS
1139 depends on NETFILTER_ADVANCED
1140 depends on NF_CONNTRACK
1141 help
1142 This option allows you to match against IPVS properties of a packet.
1144 If unsure, say N.
1146 config NETFILTER_XT_MATCH_L2TP
1147 tristate '"l2tp" match support'
1148 depends on NETFILTER_ADVANCED
1149 default L2TP
1150 ---help---
1151 This option adds an "L2TP" match, which allows you to match against
1152 L2TP protocol header fields.
1154 To compile it as a module, choose M here. If unsure, say N.
1156 config NETFILTER_XT_MATCH_LENGTH
1157 tristate '"length" match support'
1158 depends on NETFILTER_ADVANCED
1159 help
1160 This option allows you to match the length of a packet against a
1161 specific value or range of values.
1163 To compile it as a module, choose M here. If unsure, say N.
1165 config NETFILTER_XT_MATCH_LIMIT
1166 tristate '"limit" match support'
1167 depends on NETFILTER_ADVANCED
1168 help
1169 limit matching allows you to control the rate at which a rule can be
1170 matched: mainly useful in combination with the LOG target ("LOG
1171 target support", below) and to avoid some Denial of Service attacks.
1173 To compile it as a module, choose M here. If unsure, say N.
1175 config NETFILTER_XT_MATCH_MAC
1176 tristate '"mac" address match support'
1177 depends on NETFILTER_ADVANCED
1178 help
1179 MAC matching allows you to match packets based on the source
1180 Ethernet address of the packet.
1182 To compile it as a module, choose M here. If unsure, say N.
1184 config NETFILTER_XT_MATCH_MARK
1185 tristate '"mark" match support'
1186 depends on NETFILTER_ADVANCED
1187 select NETFILTER_XT_MARK
1188 ---help---
1189 This is a backwards-compat option for the user's convenience
1190 (e.g. when running oldconfig). It selects
1191 CONFIG_NETFILTER_XT_MARK (combined mark/MARK module).
1193 config NETFILTER_XT_MATCH_MULTIPORT
1194 tristate '"multiport" Multiple port match support'
1195 depends on NETFILTER_ADVANCED
1196 help
1197 Multiport matching allows you to match TCP or UDP packets based on
1198 a series of source or destination ports: normally a rule can only
1199 match a single range of ports.
1201 To compile it as a module, choose M here. If unsure, say N.
1203 config NETFILTER_XT_MATCH_NFACCT
1204 tristate '"nfacct" match support'
1205 depends on NETFILTER_ADVANCED
1206 select NETFILTER_NETLINK_ACCT
1207 help
1208 This option allows you to use the extended accounting through
1209 nfnetlink_acct.
1211 To compile it as a module, choose M here. If unsure, say N.
1213 config NETFILTER_XT_MATCH_OSF
1214 tristate '"osf" Passive OS fingerprint match'
1215 depends on NETFILTER_ADVANCED && NETFILTER_NETLINK
1216 help
1217 This option selects the Passive OS Fingerprinting match module
1218 that allows to passively match the remote operating system by
1219 analyzing incoming TCP SYN packets.
1221 Rules and loading software can be downloaded from
1222 http://www.ioremap.net/projects/osf
1224 To compile it as a module, choose M here. If unsure, say N.
1226 config NETFILTER_XT_MATCH_OWNER
1227 tristate '"owner" match support'
1228 depends on NETFILTER_ADVANCED
1229 ---help---
1230 Socket owner matching allows you to match locally-generated packets
1231 based on who created the socket: the user or group. It is also
1232 possible to check whether a socket actually exists.
1234 Conflicts with '"quota, tag, uid" match'
1236 config NETFILTER_XT_MATCH_POLICY
1237 tristate 'IPsec "policy" match support'
1238 depends on XFRM
1239 default m if NETFILTER_ADVANCED=n
1240 help
1241 Policy matching allows you to match packets based on the
1242 IPsec policy that was used during decapsulation/will
1243 be used during encapsulation.
1245 To compile it as a module, choose M here. If unsure, say N.
1247 config NETFILTER_XT_MATCH_PHYSDEV
1248 tristate '"physdev" match support'
1249 depends on BRIDGE && BRIDGE_NETFILTER
1250 depends on NETFILTER_ADVANCED
1251 help
1252 Physdev packet matching matches against the physical bridge ports
1253 the IP packet arrived on or will leave by.
1255 To compile it as a module, choose M here. If unsure, say N.
1257 config NETFILTER_XT_MATCH_PKTTYPE
1258 tristate '"pkttype" packet type match support'
1259 depends on NETFILTER_ADVANCED
1260 help
1261 Packet type matching allows you to match a packet by
1262 its "class", eg. BROADCAST, MULTICAST, ...
1264 Typical usage:
1265 iptables -A INPUT -m pkttype --pkt-type broadcast -j LOG
1267 To compile it as a module, choose M here. If unsure, say N.
1269 config NETFILTER_XT_MATCH_QTAGUID
1270 bool '"quota, tag, owner" match and stats support'
1271 depends on NETFILTER_XT_MATCH_SOCKET
1272 depends on NETFILTER_XT_MATCH_OWNER=n
1273 help
1274 This option replaces the `owner' match. In addition to matching
1275 on uid, it keeps stats based on a tag assigned to a socket.
1276 The full tag is comprised of a UID and an accounting tag.
1277 The tags are assignable to sockets from user space (e.g. a download
1278 manager can assign the socket to another UID for accounting).
1279 Stats and control are done via /proc/net/xt_qtaguid/.
1280 It replaces owner as it takes the same arguments, but should
1281 really be recognized by the iptables tool.
1283 If unsure, say `N'.
1285 config NETFILTER_XT_MATCH_QUOTA
1286 tristate '"quota" match support'
1287 depends on NETFILTER_ADVANCED
1288 help
1289 This option adds a `quota' match, which allows to match on a
1290 byte counter.
1292 If you want to compile it as a module, say M here and read
1293 <file:Documentation/kbuild/modules.txt>. If unsure, say `N'.
1295 config NETFILTER_XT_MATCH_QUOTA2
1296 tristate '"quota2" match support'
1297 depends on NETFILTER_ADVANCED
1298 help
1299 This option adds a `quota2' match, which allows to match on a
1300 byte counter correctly and not per CPU.
1301 It allows naming the quotas.
1302 This is based on http://xtables-addons.git.sourceforge.net
1304 If you want to compile it as a module, say M here and read
1305 <file:Documentation/kbuild/modules.txt>. If unsure, say `N'.
1307 config NETFILTER_XT_MATCH_QUOTA2_LOG
1308 bool '"quota2" Netfilter LOG support'
1309 depends on NETFILTER_XT_MATCH_QUOTA2
1310 depends on IP_NF_TARGET_ULOG=n # not yes, not module, just no
1311 default n
1312 help
1313 This option allows `quota2' to log ONCE when a quota limit
1314 is passed. It logs via NETLINK using the NETLINK_NFLOG family.
1315 It logs similarly to how ipt_ULOG would without data.
1317 If unsure, say `N'.
1319 config NETFILTER_XT_MATCH_RATEEST
1320 tristate '"rateest" match support'
1321 depends on NETFILTER_ADVANCED
1322 select NETFILTER_XT_TARGET_RATEEST
1323 help
1324 This option adds a `rateest' match, which allows to match on the
1325 rate estimated by the RATEEST target.
1327 To compile it as a module, choose M here. If unsure, say N.
1329 config NETFILTER_XT_MATCH_REALM
1330 tristate '"realm" match support'
1331 depends on NETFILTER_ADVANCED
1332 select IP_ROUTE_CLASSID
1333 help
1334 This option adds a `realm' match, which allows you to use the realm
1335 key from the routing subsystem inside iptables.
1337 This match pretty much resembles the CONFIG_NET_CLS_ROUTE4 option
1338 in tc world.
1340 If you want to compile it as a module, say M here and read
1341 <file:Documentation/kbuild/modules.txt>. If unsure, say `N'.
1343 config NETFILTER_XT_MATCH_RECENT
1344 tristate '"recent" match support'
1345 depends on NETFILTER_ADVANCED
1346 ---help---
1347 This match is used for creating one or many lists of recently
1348 used addresses and then matching against that/those list(s).
1350 Short options are available by using 'iptables -m recent -h'
1351 Official Website: <http://snowman.net/projects/ipt_recent/>
1353 config NETFILTER_XT_MATCH_SCTP
1354 tristate '"sctp" protocol match support'
1355 depends on NETFILTER_ADVANCED
1356 default IP_SCTP
1357 help
1358 With this option enabled, you will be able to use the
1359 `sctp' match in order to match on SCTP source/destination ports
1360 and SCTP chunk types.
1362 If you want to compile it as a module, say M here and read
1363 <file:Documentation/kbuild/modules.txt>. If unsure, say `N'.
1365 config NETFILTER_XT_MATCH_SOCKET
1366 tristate '"socket" match support'
1367 depends on NETFILTER_XTABLES
1368 depends on NETFILTER_ADVANCED
1369 depends on !NF_CONNTRACK || NF_CONNTRACK
1370 depends on (IPV6 || IPV6=n)
1371 select NF_DEFRAG_IPV4
1372 select NF_DEFRAG_IPV6 if IP6_NF_IPTABLES
1373 help
1374 This option adds a `socket' match, which can be used to match
1375 packets for which a TCP or UDP socket lookup finds a valid socket.
1376 It can be used in combination with the MARK target and policy
1377 routing to implement full featured non-locally bound sockets.
1379 To compile it as a module, choose M here. If unsure, say N.
1381 config NETFILTER_XT_MATCH_STATE
1382 tristate '"state" match support'
1383 depends on NF_CONNTRACK
1384 default m if NETFILTER_ADVANCED=n
1385 help
1386 Connection state matching allows you to match packets based on their
1387 relationship to a tracked connection (ie. previous packets). This
1388 is a powerful tool for packet classification.
1390 To compile it as a module, choose M here. If unsure, say N.
1392 config NETFILTER_XT_MATCH_STATISTIC
1393 tristate '"statistic" match support'
1394 depends on NETFILTER_ADVANCED
1395 help
1396 This option adds a `statistic' match, which allows you to match
1397 on packets periodically or randomly with a given percentage.
1399 To compile it as a module, choose M here. If unsure, say N.
1401 config NETFILTER_XT_MATCH_STRING
1402 tristate '"string" match support'
1403 depends on NETFILTER_ADVANCED
1404 select TEXTSEARCH
1405 select TEXTSEARCH_KMP
1406 select TEXTSEARCH_BM
1407 select TEXTSEARCH_FSM
1408 help
1409 This option adds a `string' match, which allows you to look for
1410 pattern matchings in packets.
1412 To compile it as a module, choose M here. If unsure, say N.
1414 config NETFILTER_XT_MATCH_TCPMSS
1415 tristate '"tcpmss" match support'
1416 depends on NETFILTER_ADVANCED
1417 help
1418 This option adds a `tcpmss' match, which allows you to examine the
1419 MSS value of TCP SYN packets, which control the maximum packet size
1420 for that connection.
1422 To compile it as a module, choose M here. If unsure, say N.
1424 config NETFILTER_XT_MATCH_TIME
1425 tristate '"time" match support'
1426 depends on NETFILTER_ADVANCED
1427 ---help---
1428 This option adds a "time" match, which allows you to match based on
1429 the packet arrival time (at the machine which netfilter is running)
1430 on) or departure time/date (for locally generated packets).
1432 If you say Y here, try `iptables -m time --help` for
1433 more information.
1435 If you want to compile it as a module, say M here.
1436 If unsure, say N.
1438 config NETFILTER_XT_MATCH_U32
1439 tristate '"u32" match support'
1440 depends on NETFILTER_ADVANCED
1441 ---help---
1442 u32 allows you to extract quantities of up to 4 bytes from a packet,
1443 AND them with specified masks, shift them by specified amounts and
1444 test whether the results are in any of a set of specified ranges.
1445 The specification of what to extract is general enough to skip over
1446 headers with lengths stored in the packet, as in IP or TCP header
1447 lengths.
1449 Details and examples are in the kernel module source.
1451 endif # NETFILTER_XTABLES
1453 endmenu
1455 source "net/netfilter/ipset/Kconfig"
1457 source "net/netfilter/ipvs/Kconfig"