]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/blob - usr/Kconfig
Merge branch 'for-jens' of git://git.drbd.org/linux-drbd into for-linus
[android-sdk/kernel-video.git] / usr / Kconfig
1 #
2 # Configuration for initramfs
3 #
5 config INITRAMFS_SOURCE
6         string "Initramfs source file(s)"
7         default ""
8         help
9           This can be either a single cpio archive with a .cpio suffix or a
10           space-separated list of directories and files for building the
11           initramfs image.  A cpio archive should contain a filesystem archive
12           to be used as an initramfs image.  Directories should contain a
13           filesystem layout to be included in the initramfs image.  Files
14           should contain entries according to the format described by the
15           "usr/gen_init_cpio" program in the kernel tree.
17           When multiple directories and files are specified then the
18           initramfs image will be the aggregate of all of them.
20           See <file:Documentation/early-userspace/README> for more details.
22           If you are not sure, leave it blank.
24 config INITRAMFS_ROOT_UID
25         int "User ID to map to 0 (user root)"
26         depends on INITRAMFS_SOURCE!=""
27         default "0"
28         help
29           This setting is only meaningful if the INITRAMFS_SOURCE is
30           contains a directory.  Setting this user ID (UID) to something
31           other than "0" will cause all files owned by that UID to be
32           owned by user root in the initial ramdisk image.
34           If you are not sure, leave it set to "0".
36 config INITRAMFS_ROOT_GID
37         int "Group ID to map to 0 (group root)"
38         depends on INITRAMFS_SOURCE!=""
39         default "0"
40         help
41           This setting is only meaningful if the INITRAMFS_SOURCE is
42           contains a directory.  Setting this group ID (GID) to something
43           other than "0" will cause all files owned by that GID to be
44           owned by group root in the initial ramdisk image.
46           If you are not sure, leave it set to "0".
48 config RD_GZIP
49         bool "Support initial ramdisks compressed using gzip" if EXPERT
50         default y
51         depends on BLK_DEV_INITRD
52         select DECOMPRESS_GZIP
53         help
54           Support loading of a gzip encoded initial ramdisk or cpio buffer.
55           If unsure, say Y.
57 config RD_BZIP2
58         bool "Support initial ramdisks compressed using bzip2" if EXPERT
59         default !EXPERT
60         depends on BLK_DEV_INITRD
61         select DECOMPRESS_BZIP2
62         help
63           Support loading of a bzip2 encoded initial ramdisk or cpio buffer
64           If unsure, say N.
66 config RD_LZMA
67         bool "Support initial ramdisks compressed using LZMA" if EXPERT
68         default !EXPERT
69         depends on BLK_DEV_INITRD
70         select DECOMPRESS_LZMA
71         help
72           Support loading of a LZMA encoded initial ramdisk or cpio buffer
73           If unsure, say N.
75 config RD_XZ
76         bool "Support initial ramdisks compressed using XZ" if EXPERT
77         default !EXPERT
78         depends on BLK_DEV_INITRD
79         select DECOMPRESS_XZ
80         help
81           Support loading of a XZ encoded initial ramdisk or cpio buffer.
82           If unsure, say N.
84 config RD_LZO
85         bool "Support initial ramdisks compressed using LZO" if EXPERT
86         default !EXPERT
87         depends on BLK_DEV_INITRD
88         select DECOMPRESS_LZO
89         help
90           Support loading of a LZO encoded initial ramdisk or cpio buffer
91           If unsure, say N.
93 choice
94         prompt "Built-in initramfs compression mode" if INITRAMFS_SOURCE!=""
95         help
96           This option decides by which algorithm the builtin initramfs
97           will be compressed.  Several compression algorithms are
98           available, which differ in efficiency, compression and
99           decompression speed.  Compression speed is only relevant
100           when building a kernel.  Decompression speed is relevant at
101           each boot.
103           If you have any problems with bzip2 or LZMA compressed
104           initramfs, mail me (Alain Knaff) <alain@knaff.lu>.
106           High compression options are mostly useful for users who are
107           low on RAM, since it reduces the memory consumption during
108           boot.
110           If in doubt, select 'gzip'
112 config INITRAMFS_COMPRESSION_NONE
113         bool "None"
114         help
115           Do not compress the built-in initramfs at all. This may
116           sound wasteful in space, but, you should be aware that the
117           built-in initramfs will be compressed at a later stage
118           anyways along with the rest of the kernel, on those
119           architectures that support this.
120           However, not compressing the initramfs may lead to slightly
121           higher memory consumption during a short time at boot, while
122           both the cpio image and the unpacked filesystem image will
123           be present in memory simultaneously
125 config INITRAMFS_COMPRESSION_GZIP
126         bool "Gzip"
127         depends on RD_GZIP
128         help
129           The old and tried gzip compression. It provides a good balance
130           between compression ratio and decompression speed.
132 config INITRAMFS_COMPRESSION_BZIP2
133         bool "Bzip2"
134         depends on RD_BZIP2
135         help
136           Its compression ratio and speed is intermediate.
137           Decompression speed is slowest among the choices.  The initramfs
138           size is about 10% smaller with bzip2, in comparison to gzip.
139           Bzip2 uses a large amount of memory. For modern kernels you
140           will need at least 8MB RAM or more for booting.
142 config INITRAMFS_COMPRESSION_LZMA
143         bool "LZMA"
144         depends on RD_LZMA
145         help
146           This algorithm's compression ratio is best.
147           Decompression speed is between the other choices.
148           Compression is slowest. The initramfs size is about 33%
149           smaller with LZMA in comparison to gzip.
151 config INITRAMFS_COMPRESSION_XZ
152         bool "XZ"
153         depends on RD_XZ
154         help
155           XZ uses the LZMA2 algorithm. The initramfs size is about 30%
156           smaller with XZ in comparison to gzip. Decompression speed
157           is better than that of bzip2 but worse than gzip and LZO.
158           Compression is slow.
160 config INITRAMFS_COMPRESSION_LZO
161         bool "LZO"
162         depends on RD_LZO
163         help
164           Its compression ratio is the poorest among the choices. The kernel
165           size is about 10% bigger than gzip; however its speed
166           (both compression and decompression) is the fastest.
168 endchoice