config ARM
bool
default y
select ARCH_BINFMT_ELF_RANDOMIZE_PIE
select ARCH_HAS_ATOMIC64_DEC_IF_POSITIVE
select ARCH_HAVE_CUSTOM_GPIO_H
select ARCH_WANT_IPC_PARSE_VERSION
select BUILDTIME_EXTABLE_SORT if MMU
select CPU_PM if (SUSPEND || CPU_IDLE)
select DCACHE_WORD_ACCESS if (CPU_V6 || CPU_V6K || CPU_V7) && !CPU_BIG_ENDIAN && MMU
select GENERIC_ATOMIC64 if (CPU_V6 || !CPU_32v6K || !AEABI)
select GENERIC_CLOCKEVENTS_BROADCAST if SMP
select GENERIC_IRQ_PROBE
select GENERIC_IRQ_SHOW
select GENERIC_PCI_IOMAP
select GENERIC_SMP_IDLE_THREAD
select GENERIC_STRNCPY_FROM_USER
select GENERIC_STRNLEN_USER
select HARDIRQS_SW_RESEND
select HAVE_AOUT
select HAVE_ARCH_JUMP_LABEL if !XIP_KERNEL
select HAVE_ARCH_KGDB
select HAVE_ARCH_SECCOMP_FILTER
select HAVE_ARCH_TRACEHOOK
select HAVE_BPF_JIT
select HAVE_C_RECORDMCOUNT
select HAVE_DEBUG_KMEMLEAK
select HAVE_DMA_API_DEBUG
select HAVE_DMA_ATTRS
select HAVE_DMA_CONTIGUOUS if MMU
select HAVE_DYNAMIC_FTRACE if (!XIP_KERNEL)
select HAVE_FTRACE_MCOUNT_RECORD if (!XIP_KERNEL)
select HAVE_FUNCTION_GRAPH_TRACER if (!THUMB2_KERNEL)
select HAVE_FUNCTION_TRACER if (!XIP_KERNEL)
select HAVE_GENERIC_DMA_COHERENT
select HAVE_GENERIC_HARDIRQS
select HAVE_HW_BREAKPOINT if (PERF_EVENTS && (CPU_V6 || CPU_V6K || CPU_V7))
select HAVE_IDE if PCI || ISA || PCMCIA
select HAVE_IRQ_WORK
select HAVE_KERNEL_GZIP
select HAVE_KERNEL_LZMA
select HAVE_KERNEL_LZO
select HAVE_KERNEL_XZ
select HAVE_KPROBES if !XIP_KERNEL
select HAVE_KRETPROBES if (HAVE_KPROBES)
select HAVE_MEMBLOCK
select HAVE_OPROFILE if (HAVE_PERF_EVENTS)
select HAVE_PERF_EVENTS
select HAVE_REGS_AND_STACK_ACCESS_API
select HAVE_SYSCALL_TRACEPOINTS
select HAVE_UID16
select KTIME_SCALAR
select PERF_USE_VMALLOC
select RTC_LIB
select SYS_SUPPORTS_APM_EMULATION
select HAVE_MOD_ARCH_SPECIFIC if ARM_UNWIND
select MODULES_USE_ELF_REL
select CLONE_BACKWARDS
help
The ARM series is a line of low-power-consumption RISC chip designs
licensed by ARM Ltd and targeted at embedded applications and
handhelds such as the Compaq IPAQ. ARM-based PCs are no longer
manufactured, but legacy ARM-based PC hardware remains popular in
Europe. There is an ARM Linux project with a web page at
.
config ARM_HAS_SG_CHAIN
bool
config NEED_SG_DMA_LENGTH
bool
config ARM_DMA_USE_IOMMU
bool
select ARM_HAS_SG_CHAIN
select NEED_SG_DMA_LENGTH
config HAVE_PWM
bool
config MIGHT_HAVE_PCI
bool
config SYS_SUPPORTS_APM_EMULATION
bool
config GENERIC_GPIO
bool
config HAVE_TCM
bool
select GENERIC_ALLOCATOR
config HAVE_PROC_CPU
bool
config NO_IOPORT
bool
config EISA
bool
---help---
The Extended Industry Standard Architecture (EISA) bus was
developed as an open alternative to the IBM MicroChannel bus.
The EISA bus provided some of the features of the IBM MicroChannel
bus while maintaining backward compatibility with cards made for
the older ISA bus. The EISA bus saw limited use between 1988 and
1995 when it was made obsolete by the PCI bus.
Say Y here if you are building a kernel for an EISA-based machine.
Otherwise, say N.
config SBUS
bool
config STACKTRACE_SUPPORT
bool
default y
config HAVE_LATENCYTOP_SUPPORT
bool
depends on !SMP
default y
config LOCKDEP_SUPPORT
bool
default y
config TRACE_IRQFLAGS_SUPPORT
bool
default y
config RWSEM_GENERIC_SPINLOCK
bool
default y
config RWSEM_XCHGADD_ALGORITHM
bool
config ARCH_HAS_ILOG2_U32
bool
config ARCH_HAS_ILOG2_U64
bool
config ARCH_HAS_CPUFREQ
bool
help
Internal node to signify that the ARCH has CPUFREQ support
and that the relevant menu configurations are displayed for
it.
config GENERIC_HWEIGHT
bool
default y
config GENERIC_CALIBRATE_DELAY
bool
default y
config ARCH_MAY_HAVE_PC_FDC
bool
config ZONE_DMA
bool
config NEED_DMA_MAP_STATE
def_bool y
config ARCH_HAS_DMA_SET_COHERENT_MASK
bool
config GENERIC_ISA_DMA
bool
config FIQ
bool
config NEED_RET_TO_USER
bool
config ARCH_MTD_XIP
bool
config VECTORS_BASE
hex
default 0xffff0000 if MMU || CPU_HIGH_VECTOR
default DRAM_BASE if REMAP_VECTORS_TO_RAM
default 0x00000000
help
The base address of exception vectors.
config ARM_PATCH_PHYS_VIRT
bool "Patch physical to virtual translations at runtime" if EMBEDDED
default y
depends on !XIP_KERNEL && MMU
depends on !ARCH_REALVIEW || !SPARSEMEM
help
Patch phys-to-virt and virt-to-phys translation functions at
boot and module load time according to the position of the
kernel in system memory.
This can only be used with non-XIP MMU kernels where the base
of physical memory is at a 16MB boundary.
Only disable this option if you know that you do not require
this feature (eg, building a kernel for a single machine) and
you need to shrink the kernel to the minimal size.
config NEED_MACH_GPIO_H
bool
help
Select this when mach/gpio.h is required to provide special
definitions for this platform. The need for mach/gpio.h should
be avoided when possible.
config NEED_MACH_IO_H
bool
help
Select this when mach/io.h is required to provide special
definitions for this platform. The need for mach/io.h should
be avoided when possible.
config NEED_MACH_MEMORY_H
bool
help
Select this when mach/memory.h is required to provide special
definitions for this platform. The need for mach/memory.h should
be avoided when possible.
config PHYS_OFFSET
hex "Physical address of main memory" if MMU
depends on !ARM_PATCH_PHYS_VIRT && !NEED_MACH_MEMORY_H
default DRAM_BASE if !MMU
help
Please provide the physical address corresponding to the
location of main memory in your system.
config GENERIC_BUG
def_bool y
depends on BUG
source "init/Kconfig"
source "kernel/Kconfig.freezer"
menu "System Type"
config MMU
bool "MMU-based Paged Memory Management Support"
default y
help
Select if you want MMU-based virtualised addressing space
support by paged memory management. If unsure, say 'Y'.
#
# The "ARM system type" choice list is ordered alphabetically by option
# text. Please add new entries in the option alphabetic order.
#
choice
prompt "ARM system type"
default ARCH_MULTIPLATFORM
config ARCH_MULTIPLATFORM
bool "Allow multiple platforms to be selected"
depends on MMU
select ARM_PATCH_PHYS_VIRT
select AUTO_ZRELADDR
select COMMON_CLK
select MULTI_IRQ_HANDLER
select SPARSE_IRQ
select USE_OF
config ARCH_INTEGRATOR
bool "ARM Ltd. Integrator family"
select ARCH_HAS_CPUFREQ
select ARM_AMBA
select COMMON_CLK
select COMMON_CLK_VERSATILE
select GENERIC_CLOCKEVENTS
select HAVE_TCM
select ICST
select MULTI_IRQ_HANDLER
select NEED_MACH_MEMORY_H
select PLAT_VERSATILE
select SPARSE_IRQ
select VERSATILE_FPGA_IRQ
help
Support for ARM's Integrator platform.
config ARCH_REALVIEW
bool "ARM Ltd. RealView family"
select ARCH_WANT_OPTIONAL_GPIOLIB
select ARM_AMBA
select ARM_TIMER_SP804
select COMMON_CLK
select COMMON_CLK_VERSATILE
select GENERIC_CLOCKEVENTS
select GPIO_PL061 if GPIOLIB
select ICST
select NEED_MACH_MEMORY_H
select PLAT_VERSATILE
select PLAT_VERSATILE_CLCD
help
This enables support for ARM Ltd RealView boards.
config ARCH_VERSATILE
bool "ARM Ltd. Versatile family"
select ARCH_WANT_OPTIONAL_GPIOLIB
select ARM_AMBA
select ARM_TIMER_SP804
select ARM_VIC
select CLKDEV_LOOKUP
select GENERIC_CLOCKEVENTS
select HAVE_MACH_CLKDEV
select ICST
select PLAT_VERSATILE
select PLAT_VERSATILE_CLCD
select PLAT_VERSATILE_CLOCK
select VERSATILE_FPGA_IRQ
help
This enables support for ARM Ltd Versatile board.
config ARCH_AT91
bool "Atmel AT91"
select ARCH_REQUIRE_GPIOLIB
select CLKDEV_LOOKUP
select HAVE_CLK
select IRQ_DOMAIN
select NEED_MACH_GPIO_H
select NEED_MACH_IO_H if PCCARD
select PINCTRL
select PINCTRL_AT91 if USE_OF
help
This enables support for systems based on Atmel
AT91RM9200 and AT91SAM9* processors.
config ARCH_BCM2835
bool "Broadcom BCM2835 family"
select ARCH_REQUIRE_GPIOLIB
select ARM_AMBA
select ARM_ERRATA_411920
select ARM_TIMER_SP804
select CLKDEV_LOOKUP
select COMMON_CLK
select CPU_V6
select GENERIC_CLOCKEVENTS
select GENERIC_GPIO
select MULTI_IRQ_HANDLER
select PINCTRL
select PINCTRL_BCM2835
select SPARSE_IRQ
select USE_OF
help
This enables support for the Broadcom BCM2835 SoC. This SoC is
use in the Raspberry Pi, and Roku 2 devices.
config ARCH_CNS3XXX
bool "Cavium Networks CNS3XXX family"
select ARM_GIC
select CPU_V6K
select GENERIC_CLOCKEVENTS
select MIGHT_HAVE_CACHE_L2X0
select MIGHT_HAVE_PCI
select PCI_DOMAINS if PCI
help
Support for Cavium Networks CNS3XXX platform.
config ARCH_CLPS711X
bool "Cirrus Logic CLPS711x/EP721x/EP731x-based"
select ARCH_REQUIRE_GPIOLIB
select AUTO_ZRELADDR
select CLKDEV_LOOKUP
select COMMON_CLK
select CPU_ARM720T
select GENERIC_CLOCKEVENTS
select MULTI_IRQ_HANDLER
select NEED_MACH_MEMORY_H
select SPARSE_IRQ
help
Support for Cirrus Logic 711x/721x/731x based boards.
config ARCH_GEMINI
bool "Cortina Systems Gemini"
select ARCH_REQUIRE_GPIOLIB
select ARCH_USES_GETTIMEOFFSET
select CPU_FA526
help
Support for the Cortina Systems Gemini family SoCs
config ARCH_SIRF
bool "CSR SiRF"
select ARCH_REQUIRE_GPIOLIB
select COMMON_CLK
select GENERIC_CLOCKEVENTS
select GENERIC_IRQ_CHIP
select MIGHT_HAVE_CACHE_L2X0
select NO_IOPORT
select PINCTRL
select PINCTRL_SIRF
select USE_OF
help
Support for CSR SiRFprimaII/Marco/Polo platforms
config ARCH_EBSA110
bool "EBSA-110"
select ARCH_USES_GETTIMEOFFSET
select CPU_SA110
select ISA
select NEED_MACH_IO_H
select NEED_MACH_MEMORY_H
select NO_IOPORT
help
This is an evaluation board for the StrongARM processor available
from Digital. It has limited hardware on-board, including an
Ethernet interface, two PCMCIA sockets, two serial ports and a
parallel port.
config ARCH_EP93XX
bool "EP93xx-based"
select ARCH_HAS_HOLES_MEMORYMODEL
select ARCH_REQUIRE_GPIOLIB
select ARCH_USES_GETTIMEOFFSET
select ARM_AMBA
select ARM_VIC
select CLKDEV_LOOKUP
select CPU_ARM920T
select NEED_MACH_MEMORY_H
help
This enables support for the Cirrus EP93xx series of CPUs.
config ARCH_FOOTBRIDGE
bool "FootBridge"
select CPU_SA110
select FOOTBRIDGE
select GENERIC_CLOCKEVENTS
select HAVE_IDE
select NEED_MACH_IO_H if !MMU
select NEED_MACH_MEMORY_H
help
Support for systems based on the DC21285 companion chip
("FootBridge"), such as the Simtec CATS and the Rebel NetWinder.
config ARCH_MXS
bool "Freescale MXS-based"
select ARCH_REQUIRE_GPIOLIB
select CLKDEV_LOOKUP
select CLKSRC_MMIO
select COMMON_CLK
select GENERIC_CLOCKEVENTS
select HAVE_CLK_PREPARE
select MULTI_IRQ_HANDLER
select PINCTRL
select SPARSE_IRQ
select USE_OF
help
Support for Freescale MXS-based family of processors
config ARCH_NETX
bool "Hilscher NetX based"
select ARM_VIC
select CLKSRC_MMIO
select CPU_ARM926T
select GENERIC_CLOCKEVENTS
help
This enables support for systems based on the Hilscher NetX Soc
config ARCH_H720X
bool "Hynix HMS720x-based"
select ARCH_USES_GETTIMEOFFSET
select CPU_ARM720T
select ISA_DMA_API
help
This enables support for systems based on the Hynix HMS720x
config ARCH_IOP13XX
bool "IOP13xx-based"
depends on MMU
select ARCH_SUPPORTS_MSI
select CPU_XSC3
select NEED_MACH_MEMORY_H
select NEED_RET_TO_USER
select PCI
select PLAT_IOP
select VMSPLIT_1G
help
Support for Intel's IOP13XX (XScale) family of processors.
config ARCH_IOP32X
bool "IOP32x-based"
depends on MMU
select ARCH_REQUIRE_GPIOLIB
select CPU_XSCALE
select NEED_MACH_GPIO_H
select NEED_RET_TO_USER
select PCI
select PLAT_IOP
help
Support for Intel's 80219 and IOP32X (XScale) family of
processors.
config ARCH_IOP33X
bool "IOP33x-based"
depends on MMU
select ARCH_REQUIRE_GPIOLIB
select CPU_XSCALE
select NEED_MACH_GPIO_H
select NEED_RET_TO_USER
select PCI
select PLAT_IOP
help
Support for Intel's IOP33X (XScale) family of processors.
config ARCH_IXP4XX
bool "IXP4xx-based"
depends on MMU
select ARCH_HAS_DMA_SET_COHERENT_MASK
select ARCH_REQUIRE_GPIOLIB
select CLKSRC_MMIO
select CPU_XSCALE
select DMABOUNCE if PCI
select GENERIC_CLOCKEVENTS
select MIGHT_HAVE_PCI
select NEED_MACH_IO_H
help
Support for Intel's IXP4XX (XScale) family of processors.
config ARCH_DOVE
bool "Marvell Dove"
select ARCH_REQUIRE_GPIOLIB
select COMMON_CLK_DOVE
select CPU_V7
select GENERIC_CLOCKEVENTS
select MIGHT_HAVE_PCI
select PINCTRL
select PINCTRL_DOVE
select PLAT_ORION_LEGACY
select USB_ARCH_HAS_EHCI
help
Support for the Marvell Dove SoC 88AP510
config ARCH_KIRKWOOD
bool "Marvell Kirkwood"
select ARCH_REQUIRE_GPIOLIB
select CPU_FEROCEON
select GENERIC_CLOCKEVENTS
select PCI
select PCI_QUIRKS
select PINCTRL
select PINCTRL_KIRKWOOD
select PLAT_ORION_LEGACY
help
Support for the following Marvell Kirkwood series SoCs:
88F6180, 88F6192 and 88F6281.
config ARCH_MV78XX0
bool "Marvell MV78xx0"
select ARCH_REQUIRE_GPIOLIB
select CPU_FEROCEON
select GENERIC_CLOCKEVENTS
select PCI
select PLAT_ORION_LEGACY
help
Support for the following Marvell MV78xx0 series SoCs:
MV781x0, MV782x0.
config ARCH_ORION5X
bool "Marvell Orion"
depends on MMU
select ARCH_REQUIRE_GPIOLIB
select CPU_FEROCEON
select GENERIC_CLOCKEVENTS
select PCI
select PLAT_ORION_LEGACY
help
Support for the following Marvell Orion 5x series SoCs:
Orion-1 (5181), Orion-VoIP (5181L), Orion-NAS (5182),
Orion-2 (5281), Orion-1-90 (6183).
config ARCH_MMP
bool "Marvell PXA168/910/MMP2"
depends on MMU
select ARCH_REQUIRE_GPIOLIB
select CLKDEV_LOOKUP
select GENERIC_ALLOCATOR
select GENERIC_CLOCKEVENTS
select GPIO_PXA
select IRQ_DOMAIN
select NEED_MACH_GPIO_H
select PINCTRL
select PLAT_PXA
select SPARSE_IRQ
help
Support for Marvell's PXA168/PXA910(MMP) and MMP2 processor line.
config ARCH_KS8695
bool "Micrel/Kendin KS8695"
select ARCH_REQUIRE_GPIOLIB
select CLKSRC_MMIO
select CPU_ARM922T
select GENERIC_CLOCKEVENTS
select NEED_MACH_MEMORY_H
help
Support for Micrel/Kendin KS8695 "Centaur" (ARM922T) based
System-on-Chip devices.
config ARCH_W90X900
bool "Nuvoton W90X900 CPU"
select ARCH_REQUIRE_GPIOLIB
select CLKDEV_LOOKUP
select CLKSRC_MMIO
select CPU_ARM926T
select GENERIC_CLOCKEVENTS
help
Support for Nuvoton (Winbond logic dept.) ARM9 processor,
At present, the w90x900 has been renamed nuc900, regarding
the ARM series product line, you can login the following
link address to know more.
config ARCH_LPC32XX
bool "NXP LPC32XX"
select ARCH_REQUIRE_GPIOLIB
select ARM_AMBA
select CLKDEV_LOOKUP
select CLKSRC_MMIO
select CPU_ARM926T
select GENERIC_CLOCKEVENTS
select HAVE_IDE
select HAVE_PWM
select USB_ARCH_HAS_OHCI
select USE_OF
help
Support for the NXP LPC32XX family of processors
config ARCH_TEGRA
bool "NVIDIA Tegra"
select ARCH_HAS_CPUFREQ
select CLKDEV_LOOKUP
select CLKSRC_MMIO
select COMMON_CLK
select GENERIC_CLOCKEVENTS
select GENERIC_GPIO
select HAVE_CLK
select HAVE_SMP
select MIGHT_HAVE_CACHE_L2X0
select SPARSE_IRQ
select USE_OF
help
This enables support for NVIDIA Tegra based systems (Tegra APX,
Tegra 6xx and Tegra 2 series).
config ARCH_PXA
bool "PXA2xx/PXA3xx-based"
depends on MMU
select ARCH_HAS_CPUFREQ
select ARCH_MTD_XIP
select ARCH_REQUIRE_GPIOLIB
select ARM_CPU_SUSPEND if PM
select AUTO_ZRELADDR
select CLKDEV_LOOKUP
select CLKSRC_MMIO
select GENERIC_CLOCKEVENTS
select GPIO_PXA
select HAVE_IDE
select MULTI_IRQ_HANDLER
select NEED_MACH_GPIO_H
select PLAT_PXA
select SPARSE_IRQ
help
Support for Intel/Marvell's PXA2xx/PXA3xx processor line.
config ARCH_MSM
bool "Qualcomm MSM"
select ARCH_REQUIRE_GPIOLIB
select CLKDEV_LOOKUP
select GENERIC_CLOCKEVENTS
select HAVE_CLK
help
Support for Qualcomm MSM/QSD based systems. This runs on the
apps processor of the MSM/QSD and depends on a shared memory
interface to the modem processor which runs the baseband
stack and controls some vital subsystems
(clock and power control, etc).
config ARCH_SHMOBILE
bool "Renesas SH-Mobile / R-Mobile"
select CLKDEV_LOOKUP
select GENERIC_CLOCKEVENTS
select HAVE_CLK
select HAVE_MACH_CLKDEV
select HAVE_SMP
select MIGHT_HAVE_CACHE_L2X0
select MULTI_IRQ_HANDLER
select NEED_MACH_MEMORY_H
select NO_IOPORT
select PM_GENERIC_DOMAINS if PM
select SPARSE_IRQ
help
Support for Renesas's SH-Mobile and R-Mobile ARM platforms.
config ARCH_RPC
bool "RiscPC"
select ARCH_ACORN
select ARCH_MAY_HAVE_PC_FDC
select ARCH_SPARSEMEM_ENABLE
select ARCH_USES_GETTIMEOFFSET
select FIQ
select HAVE_IDE
select HAVE_PATA_PLATFORM
select ISA_DMA_API
select NEED_MACH_IO_H
select NEED_MACH_MEMORY_H
select NO_IOPORT
help
On the Acorn Risc-PC, Linux can support the internal IDE disk and
CD-ROM interface, serial and parallel port, and the floppy drive.
config ARCH_SA1100
bool "SA1100-based"
select ARCH_HAS_CPUFREQ
select ARCH_MTD_XIP
select ARCH_REQUIRE_GPIOLIB
select ARCH_SPARSEMEM_ENABLE
select CLKDEV_LOOKUP
select CLKSRC_MMIO
select CPU_FREQ
select CPU_SA1100
select GENERIC_CLOCKEVENTS
select HAVE_IDE
select ISA
select NEED_MACH_GPIO_H
select NEED_MACH_MEMORY_H
select SPARSE_IRQ
help
Support for StrongARM 11x0 based boards.
config ARCH_S3C24XX
bool "Samsung S3C24XX SoCs"
select ARCH_HAS_CPUFREQ
select ARCH_USES_GETTIMEOFFSET
select CLKDEV_LOOKUP
select GENERIC_GPIO
select HAVE_CLK
select HAVE_S3C2410_I2C if I2C
select HAVE_S3C2410_WATCHDOG if WATCHDOG
select HAVE_S3C_RTC if RTC_CLASS
select NEED_MACH_GPIO_H
select NEED_MACH_IO_H
help
Samsung S3C2410, S3C2412, S3C2413, S3C2416, S3C2440, S3C2442, S3C2443
and S3C2450 SoCs based systems, such as the Simtec Electronics BAST
(), the IPAQ 1940 or the
Samsung SMDK2410 development board (and derivatives).
config ARCH_S3C64XX
bool "Samsung S3C64XX"
select ARCH_HAS_CPUFREQ
select ARCH_REQUIRE_GPIOLIB
select ARCH_USES_GETTIMEOFFSET
select ARM_VIC
select CLKDEV_LOOKUP
select CPU_V6
select HAVE_CLK
select HAVE_S3C2410_I2C if I2C
select HAVE_S3C2410_WATCHDOG if WATCHDOG
select HAVE_TCM
select NEED_MACH_GPIO_H
select NO_IOPORT
select PLAT_SAMSUNG
select S3C_DEV_NAND
select S3C_GPIO_TRACK
select SAMSUNG_CLKSRC
select SAMSUNG_GPIOLIB_4BIT
select SAMSUNG_IRQ_VIC_TIMER
select USB_ARCH_HAS_OHCI
help
Samsung S3C64XX series based systems
config ARCH_S5P64X0
bool "Samsung S5P6440 S5P6450"
select CLKDEV_LOOKUP
select CLKSRC_MMIO
select CPU_V6
select GENERIC_CLOCKEVENTS
select GENERIC_GPIO
select HAVE_CLK
select HAVE_S3C2410_I2C if I2C
select HAVE_S3C2410_WATCHDOG if WATCHDOG
select HAVE_S3C_RTC if RTC_CLASS
select NEED_MACH_GPIO_H
help
Samsung S5P64X0 CPU based systems, such as the Samsung SMDK6440,
SMDK6450.
config ARCH_S5PC100
bool "Samsung S5PC100"
select ARCH_USES_GETTIMEOFFSET
select CLKDEV_LOOKUP
select CPU_V7
select GENERIC_GPIO
select HAVE_CLK
select HAVE_S3C2410_I2C if I2C
select HAVE_S3C2410_WATCHDOG if WATCHDOG
select HAVE_S3C_RTC if RTC_CLASS
select NEED_MACH_GPIO_H
help
Samsung S5PC100 series based systems
config ARCH_S5PV210
bool "Samsung S5PV210/S5PC110"
select ARCH_HAS_CPUFREQ
select ARCH_HAS_HOLES_MEMORYMODEL
select ARCH_SPARSEMEM_ENABLE
select CLKDEV_LOOKUP
select CLKSRC_MMIO
select CPU_V7
select GENERIC_CLOCKEVENTS
select GENERIC_GPIO
select HAVE_CLK
select HAVE_S3C2410_I2C if I2C
select HAVE_S3C2410_WATCHDOG if WATCHDOG
select HAVE_S3C_RTC if RTC_CLASS
select NEED_MACH_GPIO_H
select NEED_MACH_MEMORY_H
help
Samsung S5PV210/S5PC110 series based systems
config ARCH_EXYNOS
bool "Samsung EXYNOS"
select ARCH_HAS_CPUFREQ
select ARCH_HAS_HOLES_MEMORYMODEL
select ARCH_SPARSEMEM_ENABLE
select CLKDEV_LOOKUP
select CPU_V7
select GENERIC_CLOCKEVENTS
select GENERIC_GPIO
select HAVE_CLK
select HAVE_S3C2410_I2C if I2C
select HAVE_S3C2410_WATCHDOG if WATCHDOG
select HAVE_S3C_RTC if RTC_CLASS
select NEED_MACH_GPIO_H
select NEED_MACH_MEMORY_H
help
Support for SAMSUNG's EXYNOS SoCs (EXYNOS4/5)
config ARCH_SHARK
bool "Shark"
select ARCH_USES_GETTIMEOFFSET
select CPU_SA110
select ISA
select ISA_DMA
select NEED_MACH_MEMORY_H
select PCI
select ZONE_DMA
help
Support for the StrongARM based Digital DNARD machine, also known
as "Shark" ().
config ARCH_U300
bool "ST-Ericsson U300 Series"
depends on MMU
select ARCH_REQUIRE_GPIOLIB
select ARM_AMBA
select ARM_PATCH_PHYS_VIRT
select ARM_VIC
select CLKDEV_LOOKUP
select CLKSRC_MMIO
select COMMON_CLK
select CPU_ARM926T
select GENERIC_CLOCKEVENTS
select GENERIC_GPIO
select HAVE_TCM
select SPARSE_IRQ
help
Support for ST-Ericsson U300 series mobile platforms.
config ARCH_U8500
bool "ST-Ericsson U8500 Series"
depends on MMU
select ARCH_HAS_CPUFREQ
select ARCH_REQUIRE_GPIOLIB
select ARM_AMBA
select CLKDEV_LOOKUP
select CPU_V7
select GENERIC_CLOCKEVENTS
select HAVE_SMP
select MIGHT_HAVE_CACHE_L2X0
select SPARSE_IRQ
help
Support for ST-Ericsson's Ux500 architecture
config ARCH_NOMADIK
bool "STMicroelectronics Nomadik"
select ARCH_REQUIRE_GPIOLIB
select ARM_AMBA
select ARM_VIC
select COMMON_CLK
select CPU_ARM926T
select GENERIC_CLOCKEVENTS
select MIGHT_HAVE_CACHE_L2X0
select PINCTRL
select PINCTRL_STN8815
select SPARSE_IRQ
help
Support for the Nomadik platform by ST-Ericsson
config PLAT_SPEAR
bool "ST SPEAr"
select ARCH_HAS_CPUFREQ
select ARCH_REQUIRE_GPIOLIB
select ARM_AMBA
select CLKDEV_LOOKUP
select CLKSRC_MMIO
select COMMON_CLK
select GENERIC_CLOCKEVENTS
select HAVE_CLK
help
Support for ST's SPEAr platform (SPEAr3xx, SPEAr6xx and SPEAr13xx).
config ARCH_DAVINCI
bool "TI DaVinci"
select ARCH_HAS_HOLES_MEMORYMODEL
select ARCH_REQUIRE_GPIOLIB
select CLKDEV_LOOKUP
select GENERIC_ALLOCATOR
select GENERIC_CLOCKEVENTS
select GENERIC_IRQ_CHIP
select HAVE_IDE
select NEED_MACH_GPIO_H
select TI_PRIV_EDMA
select USE_OF
select ZONE_DMA
help
Support for TI's DaVinci platform.
config ARCH_OMAP
bool "TI OMAP"
depends on MMU
select ARCH_HAS_CPUFREQ
select ARCH_HAS_HOLES_MEMORYMODEL
select ARCH_REQUIRE_GPIOLIB
select CLKSRC_MMIO
select GENERIC_CLOCKEVENTS
select HAVE_CLK
help
Support for TI's OMAP platform (OMAP1/2/3/4).
config ARCH_VT8500_SINGLE
bool "VIA/WonderMedia 85xx"
select ARCH_HAS_CPUFREQ
select ARCH_REQUIRE_GPIOLIB
select CLKDEV_LOOKUP
select COMMON_CLK
select CPU_ARM926T
select GENERIC_CLOCKEVENTS
select GENERIC_GPIO
select HAVE_CLK
select MULTI_IRQ_HANDLER
select SPARSE_IRQ
select USE_OF
help
Support for VIA/WonderMedia VT8500/WM85xx System-on-Chip.
endchoice
menu "Multiple platform selection"
depends on ARCH_MULTIPLATFORM
comment "CPU Core family selection"
config ARCH_MULTI_V4
bool "ARMv4 based platforms (FA526, StrongARM)"
depends on !ARCH_MULTI_V6_V7
select ARCH_MULTI_V4_V5
config ARCH_MULTI_V4T
bool "ARMv4T based platforms (ARM720T, ARM920T, ...)"
depends on !ARCH_MULTI_V6_V7
select ARCH_MULTI_V4_V5
config ARCH_MULTI_V5
bool "ARMv5 based platforms (ARM926T, XSCALE, PJ1, ...)"
depends on !ARCH_MULTI_V6_V7
select ARCH_MULTI_V4_V5
config ARCH_MULTI_V4_V5
bool
config ARCH_MULTI_V6
bool "ARMv6 based platforms (ARM11, Scorpion, ...)"
select ARCH_MULTI_V6_V7
select CPU_V6
config ARCH_MULTI_V7
bool "ARMv7 based platforms (Cortex-A, PJ4, Krait)"
default y
select ARCH_MULTI_V6_V7
select ARCH_VEXPRESS
select CPU_V7
config ARCH_MULTI_V6_V7
bool
config ARCH_MULTI_CPU_AUTO
def_bool !(ARCH_MULTI_V4 || ARCH_MULTI_V4T || ARCH_MULTI_V6_V7)
select ARCH_MULTI_V5
endmenu
#
# This is sorted alphabetically by mach-* pathname. However, plat-*
# Kconfigs may be included either alphabetically (according to the
# plat- suffix) or along side the corresponding mach-* source.
#
source "arch/arm/mach-mvebu/Kconfig"
source "arch/arm/mach-at91/Kconfig"
source "arch/arm/mach-bcm/Kconfig"
source "arch/arm/mach-clps711x/Kconfig"
source "arch/arm/mach-cns3xxx/Kconfig"
source "arch/arm/mach-davinci/Kconfig"
source "arch/arm/mach-dove/Kconfig"
source "arch/arm/mach-ep93xx/Kconfig"
source "arch/arm/mach-footbridge/Kconfig"
source "arch/arm/mach-gemini/Kconfig"
source "arch/arm/mach-h720x/Kconfig"
source "arch/arm/mach-highbank/Kconfig"
source "arch/arm/mach-integrator/Kconfig"
source "arch/arm/mach-iop32x/Kconfig"
source "arch/arm/mach-iop33x/Kconfig"
source "arch/arm/mach-iop13xx/Kconfig"
source "arch/arm/mach-ixp4xx/Kconfig"
source "arch/arm/mach-kirkwood/Kconfig"
source "arch/arm/mach-ks8695/Kconfig"
source "arch/arm/mach-msm/Kconfig"
source "arch/arm/mach-mv78xx0/Kconfig"
source "arch/arm/mach-imx/Kconfig"
source "arch/arm/mach-mxs/Kconfig"
source "arch/arm/mach-netx/Kconfig"
source "arch/arm/mach-nomadik/Kconfig"
source "arch/arm/plat-omap/Kconfig"
source "arch/arm/mach-omap1/Kconfig"
source "arch/arm/mach-omap2/Kconfig"
source "arch/arm/mach-orion5x/Kconfig"
source "arch/arm/mach-picoxcell/Kconfig"
source "arch/arm/mach-pxa/Kconfig"
source "arch/arm/plat-pxa/Kconfig"
source "arch/arm/mach-mmp/Kconfig"
source "arch/arm/mach-realview/Kconfig"
source "arch/arm/mach-sa1100/Kconfig"
source "arch/arm/plat-samsung/Kconfig"
source "arch/arm/plat-s3c24xx/Kconfig"
source "arch/arm/mach-socfpga/Kconfig"
source "arch/arm/plat-spear/Kconfig"
source "arch/arm/mach-s3c24xx/Kconfig"
if ARCH_S3C24XX
source "arch/arm/mach-s3c2412/Kconfig"
source "arch/arm/mach-s3c2440/Kconfig"
endif
if ARCH_S3C64XX
source "arch/arm/mach-s3c64xx/Kconfig"
endif
source "arch/arm/mach-s5p64x0/Kconfig"
source "arch/arm/mach-s5pc100/Kconfig"
source "arch/arm/mach-s5pv210/Kconfig"
source "arch/arm/mach-exynos/Kconfig"
source "arch/arm/mach-shmobile/Kconfig"
source "arch/arm/mach-sunxi/Kconfig"
source "arch/arm/mach-prima2/Kconfig"
source "arch/arm/mach-tegra/Kconfig"
source "arch/arm/mach-u300/Kconfig"
source "arch/arm/mach-ux500/Kconfig"
source "arch/arm/mach-versatile/Kconfig"
source "arch/arm/mach-vexpress/Kconfig"
source "arch/arm/plat-versatile/Kconfig"
source "arch/arm/mach-vt8500/Kconfig"
source "arch/arm/mach-w90x900/Kconfig"
source "arch/arm/mach-zynq/Kconfig"
# Definitions to make life easier
config ARCH_ACORN
bool
config PLAT_IOP
bool
select GENERIC_CLOCKEVENTS
config PLAT_ORION
bool
select CLKSRC_MMIO
select COMMON_CLK
select GENERIC_IRQ_CHIP
select IRQ_DOMAIN
config PLAT_ORION_LEGACY
bool
select PLAT_ORION
config PLAT_PXA
bool
config PLAT_VERSATILE
bool
config ARM_TIMER_SP804
bool
select CLKSRC_MMIO
select HAVE_SCHED_CLOCK
source arch/arm/mm/Kconfig
config ARM_NR_BANKS
int
default 16 if ARCH_EP93XX
default 8
config IWMMXT
bool "Enable iWMMXt support"
depends on CPU_XSCALE || CPU_XSC3 || CPU_MOHAWK || CPU_PJ4
default y if PXA27x || PXA3xx || ARCH_MMP
help
Enable support for iWMMXt context switching at run time if
running on a CPU that supports it.
config XSCALE_PMU
bool
depends on CPU_XSCALE
default y
config MULTI_IRQ_HANDLER
bool
help
Allow each machine to specify it's own IRQ handler at run time.
if !MMU
source "arch/arm/Kconfig-nommu"
endif
config ARM_ERRATA_326103
bool "ARM errata: FSR write bit incorrect on a SWP to read-only memory"
depends on CPU_V6
help
Executing a SWP instruction to read-only memory does not set bit 11
of the FSR on the ARM 1136 prior to r1p0. This causes the kernel to
treat the access as a read, preventing a COW from occurring and
causing the faulting task to livelock.
config ARM_ERRATA_411920
bool "ARM errata: Invalidation of the Instruction Cache operation can fail"
depends on CPU_V6 || CPU_V6K
help
Invalidation of the Instruction Cache operation can
fail. This erratum is present in 1136 (before r1p4), 1156 and 1176.
It does not affect the MPCore. This option enables the ARM Ltd.
recommended workaround.
config ARM_ERRATA_430973
bool "ARM errata: Stale prediction on replaced interworking branch"
depends on CPU_V7
help
This option enables the workaround for the 430973 Cortex-A8
(r1p0..r1p2) erratum. If a code sequence containing an ARM/Thumb
interworking branch is replaced with another code sequence at the
same virtual address, whether due to self-modifying code or virtual
to physical address re-mapping, Cortex-A8 does not recover from the
stale interworking branch prediction. This results in Cortex-A8
executing the new code sequence in the incorrect ARM or Thumb state.
The workaround enables the BTB/BTAC operations by setting ACTLR.IBE
and also flushes the branch target cache at every context switch.
Note that setting specific bits in the ACTLR register may not be
available in non-secure mode.
config ARM_ERRATA_458693
bool "ARM errata: Processor deadlock when a false hazard is created"
depends on CPU_V7
depends on !ARCH_MULTIPLATFORM
help
This option enables the workaround for the 458693 Cortex-A8 (r2p0)
erratum. For very specific sequences of memory operations, it is
possible for a hazard condition intended for a cache line to instead
be incorrectly associated with a different cache line. This false
hazard might then cause a processor deadlock. The workaround enables
the L1 caching of the NEON accesses and disables the PLD instruction
in the ACTLR register. Note that setting specific bits in the ACTLR
register may not be available in non-secure mode.
config ARM_ERRATA_460075
bool "ARM errata: Data written to the L2 cache can be overwritten with stale data"
depends on CPU_V7
depends on !ARCH_MULTIPLATFORM
help
This option enables the workaround for the 460075 Cortex-A8 (r2p0)
erratum. Any asynchronous access to the L2 cache may encounter a
situation in which recent store transactions to the L2 cache are lost
and overwritten with stale memory contents from external memory. The
workaround disables the write-allocate mode for the L2 cache via the
ACTLR register. Note that setting specific bits in the ACTLR register
may not be available in non-secure mode.
config ARM_ERRATA_742230
bool "ARM errata: DMB operation may be faulty"
depends on CPU_V7 && SMP
depends on !ARCH_MULTIPLATFORM
help
This option enables the workaround for the 742230 Cortex-A9
(r1p0..r2p2) erratum. Under rare circumstances, a DMB instruction
between two write operations may not ensure the correct visibility
ordering of the two writes. This workaround sets a specific bit in
the diagnostic register of the Cortex-A9 which causes the DMB
instruction to behave as a DSB, ensuring the correct behaviour of
the two writes.
config ARM_ERRATA_742231
bool "ARM errata: Incorrect hazard handling in the SCU may lead to data corruption"
depends on CPU_V7 && SMP
depends on !ARCH_MULTIPLATFORM
help
This option enables the workaround for the 742231 Cortex-A9
(r2p0..r2p2) erratum. Under certain conditions, specific to the
Cortex-A9 MPCore micro-architecture, two CPUs working in SMP mode,
accessing some data located in the same cache line, may get corrupted
data due to bad handling of the address hazard when the line gets
replaced from one of the CPUs at the same time as another CPU is
accessing it. This workaround sets specific bits in the diagnostic
register of the Cortex-A9 which reduces the linefill issuing
capabilities of the processor.
config PL310_ERRATA_588369
bool "PL310 errata: Clean & Invalidate maintenance operations do not invalidate clean lines"
depends on CACHE_L2X0
help
The PL310 L2 cache controller implements three types of Clean &
Invalidate maintenance operations: by Physical Address
(offset 0x7F0), by Index/Way (0x7F8) and by Way (0x7FC).
They are architecturally defined to behave as the execution of a
clean operation followed immediately by an invalidate operation,
both performing to the same memory location. This functionality
is not correctly implemented in PL310 as clean lines are not
invalidated as a result of these operations.
config ARM_ERRATA_720789
bool "ARM errata: TLBIASIDIS and TLBIMVAIS operations can broadcast a faulty ASID"
depends on CPU_V7
help
This option enables the workaround for the 720789 Cortex-A9 (prior to
r2p0) erratum. A faulty ASID can be sent to the other CPUs for the
broadcasted CP15 TLB maintenance operations TLBIASIDIS and TLBIMVAIS.
As a consequence of this erratum, some TLB entries which should be
invalidated are not, resulting in an incoherency in the system page
tables. The workaround changes the TLB flushing routines to invalidate
entries regardless of the ASID.
config PL310_ERRATA_727915
bool "PL310 errata: Background Clean & Invalidate by Way operation can cause data corruption"
depends on CACHE_L2X0
help
PL310 implements the Clean & Invalidate by Way L2 cache maintenance
operation (offset 0x7FC). This operation runs in background so that
PL310 can handle normal accesses while it is in progress. Under very
rare circumstances, due to this erratum, write data can be lost when
PL310 treats a cacheable write transaction during a Clean &
Invalidate by Way operation.
config ARM_ERRATA_743622
bool "ARM errata: Faulty hazard checking in the Store Buffer may lead to data corruption"
depends on CPU_V7
depends on !ARCH_MULTIPLATFORM
help
This option enables the workaround for the 743622 Cortex-A9
(r2p*) erratum. Under very rare conditions, a faulty
optimisation in the Cortex-A9 Store Buffer may lead to data
corruption. This workaround sets a specific bit in the diagnostic
register of the Cortex-A9 which disables the Store Buffer
optimisation, preventing the defect from occurring. This has no
visible impact on the overall performance or power consumption of the
processor.
config ARM_ERRATA_751472
bool "ARM errata: Interrupted ICIALLUIS may prevent completion of broadcasted operation"
depends on CPU_V7
depends on !ARCH_MULTIPLATFORM
help
This option enables the workaround for the 751472 Cortex-A9 (prior
to r3p0) erratum. An interrupted ICIALLUIS operation may prevent the
completion of a following broadcasted operation if the second
operation is received by a CPU before the ICIALLUIS has completed,
potentially leading to corrupted entries in the cache or TLB.
config PL310_ERRATA_753970
bool "PL310 errata: cache sync operation may be faulty"
depends on CACHE_PL310
help
This option enables the workaround for the 753970 PL310 (r3p0) erratum.
Under some condition the effect of cache sync operation on
the store buffer still remains when the operation completes.
This means that the store buffer is always asked to drain and
this prevents it from merging any further writes. The workaround
is to replace the normal offset of cache sync operation (0x730)
by another offset targeting an unmapped PL310 register 0x740.
This has the same effect as the cache sync operation: store buffer
drain and waiting for all buffers empty.
config ARM_ERRATA_754322
bool "ARM errata: possible faulty MMU translations following an ASID switch"
depends on CPU_V7
help
This option enables the workaround for the 754322 Cortex-A9 (r2p*,
r3p*) erratum. A speculative memory access may cause a page table walk
which starts prior to an ASID switch but completes afterwards. This
can populate the micro-TLB with a stale entry which may be hit with
the new ASID. This workaround places two dsb instructions in the mm
switching code so that no page table walks can cross the ASID switch.
config ARM_ERRATA_754327
bool "ARM errata: no automatic Store Buffer drain"
depends on CPU_V7 && SMP
help
This option enables the workaround for the 754327 Cortex-A9 (prior to
r2p0) erratum. The Store Buffer does not have any automatic draining
mechanism and therefore a livelock may occur if an external agent
continuously polls a memory location waiting to observe an update.
This workaround defines cpu_relax() as smp_mb(), preventing correctly
written polling loops from denying visibility of updates to memory.
config ARM_ERRATA_364296
bool "ARM errata: Possible cache data corruption with hit-under-miss enabled"
depends on CPU_V6 && !SMP
help
This options enables the workaround for the 364296 ARM1136
r0p2 erratum (possible cache data corruption with
hit-under-miss enabled). It sets the undocumented bit 31 in
the auxiliary control register and the FI bit in the control
register, thus disabling hit-under-miss without putting the
processor into full low interrupt latency mode. ARM11MPCore
is not affected.
config ARM_ERRATA_764369
bool "ARM errata: Data cache line maintenance operation by MVA may not succeed"
depends on CPU_V7 && SMP
help
This option enables the workaround for erratum 764369
affecting Cortex-A9 MPCore with two or more processors (all
current revisions). Under certain timing circumstances, a data
cache line maintenance operation by MVA targeting an Inner
Shareable memory region may fail to proceed up to either the
Point of Coherency or to the Point of Unification of the
system. This workaround adds a DSB instruction before the
relevant cache maintenance functions and sets a specific bit
in the diagnostic control register of the SCU.
config PL310_ERRATA_769419
bool "PL310 errata: no automatic Store Buffer drain"
depends on CACHE_L2X0
help
On revisions of the PL310 prior to r3p2, the Store Buffer does
not automatically drain. This can cause normal, non-cacheable
writes to be retained when the memory system is idle, leading
to suboptimal I/O performance for drivers using coherent DMA.
This option adds a write barrier to the cpu_idle loop so that,
on systems with an outer cache, the store buffer is drained
explicitly.
config ARM_ERRATA_775420
bool "ARM errata: A data cache maintenance operation which aborts, might lead to deadlock"
depends on CPU_V7
help
This option enables the workaround for the 775420 Cortex-A9 (r2p2,
r2p6,r2p8,r2p10,r3p0) erratum. In case a date cache maintenance
operation aborts with MMU exception, it might cause the processor
to deadlock. This workaround puts DSB before executing ISB if
an abort may occur on cache maintenance.
endmenu
source "arch/arm/common/Kconfig"
menu "Bus support"
config ARM_AMBA
bool
config ISA
bool
help
Find out whether you have ISA slots on your motherboard. ISA is the
name of a bus system, i.e. the way the CPU talks to the other stuff
inside your box. Other bus systems are PCI, EISA, MicroChannel
(MCA) or VESA. ISA is an older system, now being displaced by PCI;
newer boards don't support it. If you have ISA, say Y, otherwise N.
# Select ISA DMA controller support
config ISA_DMA
bool
select ISA_DMA_API
# Select ISA DMA interface
config ISA_DMA_API
bool
config PCI
bool "PCI support" if MIGHT_HAVE_PCI
help
Find out whether you have a PCI motherboard. PCI is the name of a
bus system, i.e. the way the CPU talks to the other stuff inside
your box. Other bus systems are ISA, EISA, MicroChannel (MCA) or
VESA. If you have PCI, say Y, otherwise N.
config PCI_DOMAINS
bool
depends on PCI
config PCI_NANOENGINE
bool "BSE nanoEngine PCI support"
depends on SA1100_NANOENGINE
help
Enable PCI on the BSE nanoEngine board.
config PCI_SYSCALL
def_bool PCI
# Select the host bridge type
config PCI_HOST_VIA82C505
bool
depends on PCI && ARCH_SHARK
default y
config PCI_HOST_ITE8152
bool
depends on PCI && MACH_ARMCORE
default y
select DMABOUNCE
source "drivers/pci/Kconfig"
source "drivers/pcmcia/Kconfig"
endmenu
menu "Kernel Features"
config HAVE_SMP
bool
help
This option should be selected by machines which have an SMP-
capable CPU.
The only effect of this option is to make the SMP-related
options available to the user for configuration.
config SMP
bool "Symmetric Multi-Processing"
depends on CPU_V6K || CPU_V7
depends on GENERIC_CLOCKEVENTS
depends on HAVE_SMP
depends on MMU
select HAVE_ARM_SCU if !ARCH_MSM_SCORPIONMP
select USE_GENERIC_SMP_HELPERS
help
This enables support for systems with more than one CPU. If you have
a system with only one CPU, like most personal computers, say N. If
you have a system with more than one CPU, say Y.
If you say N here, the kernel will run on single and multiprocessor
machines, but will use only one CPU of a multiprocessor machine. If
you say Y here, the kernel will run on many, but not all, single
processor machines. On a single processor machine, the kernel will
run faster if you say N here.
See also ,
and the SMP-HOWTO available at
.
If you don't know what to do here, say N.
config SMP_ON_UP
bool "Allow booting SMP kernel on uniprocessor systems (EXPERIMENTAL)"
depends on EXPERIMENTAL
depends on SMP && !XIP_KERNEL
default y
help
SMP kernels contain instructions which fail on non-SMP processors.
Enabling this option allows the kernel to modify itself to make
these instructions safe. Disabling it allows about 1K of space
savings.
If you don't know what to do here, say Y.
config ARM_CPU_TOPOLOGY
bool "Support cpu topology definition"
depends on SMP && CPU_V7
default y
help
Support ARM cpu topology definition. The MPIDR register defines
affinity between processors which is then used to describe the cpu
topology of an ARM System.
config SCHED_MC
bool "Multi-core scheduler support"
depends on ARM_CPU_TOPOLOGY
help
Multi-core scheduler support improves the CPU scheduler's decision
making when dealing with multi-core CPU chips at a cost of slightly
increased overhead in some places. If unsure say N here.
config SCHED_SMT
bool "SMT scheduler support"
depends on ARM_CPU_TOPOLOGY
help
Improves the CPU scheduler's decision making when dealing with
MultiThreading at a cost of slightly increased overhead in some
places. If unsure say N here.
config HAVE_ARM_SCU
bool
help
This option enables support for the ARM system coherency unit
config ARM_ARCH_TIMER
bool "Architected timer support"
depends on CPU_V7
help
This option enables support for the ARM architected timer
config HAVE_ARM_TWD
bool
depends on SMP
help
This options enables support for the ARM timer and watchdog unit
choice
prompt "Memory split"
default VMSPLIT_3G
help
Select the desired split between kernel and user memory.
If you are not absolutely sure what you are doing, leave this
option alone!
config VMSPLIT_3G
bool "3G/1G user/kernel split"
config VMSPLIT_2G
bool "2G/2G user/kernel split"
config VMSPLIT_1G
bool "1G/3G user/kernel split"
endchoice
config PAGE_OFFSET
hex
default 0x40000000 if VMSPLIT_1G
default 0x80000000 if VMSPLIT_2G
default 0xC0000000
config NR_CPUS
int "Maximum number of CPUs (2-32)"
range 2 32
depends on SMP
default "4"
config HOTPLUG_CPU
bool "Support for hot-pluggable CPUs"
depends on SMP && HOTPLUG
help
Say Y here to experiment with turning CPUs off and on. CPUs
can be controlled through /sys/devices/system/cpu.
config LOCAL_TIMERS
bool "Use local timer interrupts"
depends on SMP
default y
select HAVE_ARM_TWD if (!ARCH_MSM_SCORPIONMP && !EXYNOS4_MCT)
help
Enable support for local timers on SMP platforms, rather then the
legacy IPI broadcast method. Local timers allows the system
accounting to be spread across the timer interval, preventing a
"thundering herd" at every timer tick.
config ARCH_NR_GPIO
int
default 1024 if ARCH_SHMOBILE || ARCH_TEGRA
default 355 if ARCH_U8500
default 264 if MACH_H4700
default 512 if SOC_OMAP5
default 288 if ARCH_VT8500
default 0
help
Maximum number of GPIOs in the system.
If unsure, leave the default value.
source kernel/Kconfig.preempt
config HZ
int
default 200 if ARCH_EBSA110 || ARCH_S3C24XX || ARCH_S5P64X0 || \
ARCH_S5PV210 || ARCH_EXYNOS4
default OMAP_32K_TIMER_HZ if ARCH_OMAP && OMAP_32K_TIMER
default AT91_TIMER_HZ if ARCH_AT91
default SHMOBILE_TIMER_HZ if ARCH_SHMOBILE
default 100
config THUMB2_KERNEL
bool "Compile the kernel in Thumb-2 mode"
depends on CPU_V7 && !CPU_V6 && !CPU_V6K
select AEABI
select ARM_ASM_UNIFIED
select ARM_UNWIND
help
By enabling this option, the kernel will be compiled in
Thumb-2 mode. A compiler/assembler that understand the unified
ARM-Thumb syntax is needed.
If unsure, say N.
config THUMB2_AVOID_R_ARM_THM_JUMP11
bool "Work around buggy Thumb-2 short branch relocations in gas"
depends on THUMB2_KERNEL && MODULES
default y
help
Various binutils versions can resolve Thumb-2 branches to
locally-defined, preemptible global symbols as short-range "b.n"
branch instructions.
This is a problem, because there's no guarantee the final
destination of the symbol, or any candidate locations for a
trampoline, are within range of the branch. For this reason, the
kernel does not support fixing up the R_ARM_THM_JUMP11 (102)
relocation in modules at all, and it makes little sense to add
support.
The symptom is that the kernel fails with an "unsupported
relocation" error when loading some modules.
Until fixed tools are available, passing
-fno-optimize-sibling-calls to gcc should prevent gcc generating
code which hits this problem, at the cost of a bit of extra runtime
stack usage in some cases.
The problem is described in more detail at:
https://bugs.launchpad.net/binutils-linaro/+bug/725126
Only Thumb-2 kernels are affected.
Unless you are sure your tools don't have this problem, say Y.
config ARM_ASM_UNIFIED
bool
config AEABI
bool "Use the ARM EABI to compile the kernel"
help
This option allows for the kernel to be compiled using the latest
ARM ABI (aka EABI). This is only useful if you are using a user
space environment that is also compiled with EABI.
Since there are major incompatibilities between the legacy ABI and
EABI, especially with regard to structure member alignment, this
option also changes the kernel syscall calling convention to
disambiguate both ABIs and allow for backward compatibility support
(selected with CONFIG_OABI_COMPAT).
To use this you need GCC version 4.0.0 or later.
config OABI_COMPAT
bool "Allow old ABI binaries to run with this kernel (EXPERIMENTAL)"
depends on AEABI && EXPERIMENTAL && !THUMB2_KERNEL
default y
help
This option preserves the old syscall interface along with the
new (ARM EABI) one. It also provides a compatibility layer to
intercept syscalls that have structure arguments which layout
in memory differs between the legacy ABI and the new ARM EABI
(only for non "thumb" binaries). This option adds a tiny
overhead to all syscalls and produces a slightly larger kernel.
If you know you'll be using only pure EABI user space then you
can say N here. If this option is not selected and you attempt
to execute a legacy ABI binary then the result will be
UNPREDICTABLE (in fact it can be predicted that it won't work
at all). If in doubt say Y.
config ARCH_HAS_HOLES_MEMORYMODEL
bool
config ARCH_SPARSEMEM_ENABLE
bool
config ARCH_SPARSEMEM_DEFAULT
def_bool ARCH_SPARSEMEM_ENABLE
config ARCH_SELECT_MEMORY_MODEL
def_bool ARCH_SPARSEMEM_ENABLE
config HAVE_ARCH_PFN_VALID
def_bool ARCH_HAS_HOLES_MEMORYMODEL || !SPARSEMEM
config HIGHMEM
bool "High Memory Support"
depends on MMU
help
The address space of ARM processors is only 4 Gigabytes large
and it has to accommodate user address space, kernel address
space as well as some memory mapped IO. That means that, if you
have a large amount of physical memory and/or IO, not all of the
memory can be "permanently mapped" by the kernel. The physical
memory that is not permanently mapped is called "high memory".
Depending on the selected kernel/user memory split, minimum
vmalloc space and actual amount of RAM, you may not need this
option which should result in a slightly faster kernel.
If unsure, say n.
config HIGHPTE
bool "Allocate 2nd-level pagetables from highmem"
depends on HIGHMEM
config HW_PERF_EVENTS
bool "Enable hardware performance counter support for perf events"
depends on PERF_EVENTS
default y
help
Enable hardware performance counter support for perf events. If
disabled, perf events will use software events only.
source "mm/Kconfig"
config FORCE_MAX_ZONEORDER
int "Maximum zone order" if ARCH_SHMOBILE
range 11 64 if ARCH_SHMOBILE
default "12" if SOC_AM33XX
default "9" if SA1111
default "11"
help
The kernel memory allocator divides physically contiguous memory
blocks into "zones", where each zone is a power of two number of
pages. This option selects the largest power of two that the kernel
keeps in the memory allocator. If you need to allocate very large
blocks of physically contiguous memory, then you may need to
increase this value.
This config option is actually maximum order plus one. For example,
a value of 11 means that the largest free memory block is 2^10 pages.
config ALIGNMENT_TRAP
bool
depends on CPU_CP15_MMU
default y if !ARCH_EBSA110
select HAVE_PROC_CPU if PROC_FS
help
ARM processors cannot fetch/store information which is not
naturally aligned on the bus, i.e., a 4 byte fetch must start at an
address divisible by 4. On 32-bit ARM processors, these non-aligned
fetch/store instructions will be emulated in software if you say
here, which has a severe performance impact. This is necessary for
correct operation of some network protocols. With an IP-only
configuration it is safe to say N, otherwise say Y.
config UACCESS_WITH_MEMCPY
bool "Use kernel mem{cpy,set}() for {copy_to,clear}_user()"
depends on MMU
default y if CPU_FEROCEON
help
Implement faster copy_to_user and clear_user methods for CPU
cores where a 8-word STM instruction give significantly higher
memory write throughput than a sequence of individual 32bit stores.
A possible side effect is a slight increase in scheduling latency
between threads sharing the same address space if they invoke
such copy operations with large buffers.
However, if the CPU data cache is using a write-allocate mode,
this option is unlikely to provide any performance gain.
config SECCOMP
bool
prompt "Enable seccomp to safely compute untrusted bytecode"
---help---
This kernel feature is useful for number crunching applications
that may need to compute untrusted bytecode during their
execution. By using pipes or other transports made available to
the process as file descriptors supporting the read/write
syscalls, it's possible to isolate those applications in
their own address space using seccomp. Once seccomp is
enabled via prctl(PR_SET_SECCOMP), it cannot be disabled
and the task is only allowed to execute a few safe syscalls
defined by each seccomp mode.
config CC_STACKPROTECTOR
bool "Enable -fstack-protector buffer overflow detection (EXPERIMENTAL)"
depends on EXPERIMENTAL
help
This option turns on the -fstack-protector GCC feature. This
feature puts, at the beginning of functions, a canary value on
the stack just before the return address, and validates
the value just before actually returning. Stack based buffer
overflows (that need to overwrite this return address) now also
overwrite the canary, which gets detected and the attack is then
neutralized via a kernel panic.
This feature requires gcc version 4.2 or above.
config XEN_DOM0
def_bool y
depends on XEN
config XEN
bool "Xen guest support on ARM (EXPERIMENTAL)"
depends on EXPERIMENTAL && ARM && OF
depends on CPU_V7 && !CPU_V6
help
Say Y if you want to run Linux in a Virtual Machine on Xen on ARM.
endmenu
menu "Boot options"
config USE_OF
bool "Flattened Device Tree support"
select IRQ_DOMAIN
select OF
select OF_EARLY_FLATTREE
help
Include support for flattened device tree machine descriptions.
config ATAGS
bool "Support for the traditional ATAGS boot data passing" if USE_OF
default y
help
This is the traditional way of passing data to the kernel at boot
time. If you are solely relying on the flattened device tree (or
the ARM_ATAG_DTB_COMPAT option) then you may unselect this option
to remove ATAGS support from your kernel binary. If unsure,
leave this to y.
config DEPRECATED_PARAM_STRUCT
bool "Provide old way to pass kernel parameters"
depends on ATAGS
help
This was deprecated in 2001 and announced to live on for 5 years.
Some old boot loaders still use this way.
# Compressed boot loader in ROM. Yes, we really want to ask about
# TEXT and BSS so we preserve their values in the config files.
config ZBOOT_ROM_TEXT
hex "Compressed ROM boot loader base address"
default "0"
help
The physical address at which the ROM-able zImage is to be
placed in the target. Platforms which normally make use of
ROM-able zImage formats normally set this to a suitable
value in their defconfig file.
If ZBOOT_ROM is not enabled, this has no effect.
config ZBOOT_ROM_BSS
hex "Compressed ROM boot loader BSS address"
default "0"
help
The base address of an area of read/write memory in the target
for the ROM-able zImage which must be available while the
decompressor is running. It must be large enough to hold the
entire decompressed kernel plus an additional 128 KiB.
Platforms which normally make use of ROM-able zImage formats
normally set this to a suitable value in their defconfig file.
If ZBOOT_ROM is not enabled, this has no effect.
config ZBOOT_ROM
bool "Compressed boot loader in ROM/flash"
depends on ZBOOT_ROM_TEXT != ZBOOT_ROM_BSS
help
Say Y here if you intend to execute your compressed kernel image
(zImage) directly from ROM or flash. If unsure, say N.
choice
prompt "Include SD/MMC loader in zImage (EXPERIMENTAL)"
depends on ZBOOT_ROM && ARCH_SH7372 && EXPERIMENTAL
default ZBOOT_ROM_NONE
help
Include experimental SD/MMC loading code in the ROM-able zImage.
With this enabled it is possible to write the ROM-able zImage
kernel image to an MMC or SD card and boot the kernel straight
from the reset vector. At reset the processor Mask ROM will load
the first part of the ROM-able zImage which in turn loads the
rest the kernel image to RAM.
config ZBOOT_ROM_NONE
bool "No SD/MMC loader in zImage (EXPERIMENTAL)"
help
Do not load image from SD or MMC
config ZBOOT_ROM_MMCIF
bool "Include MMCIF loader in zImage (EXPERIMENTAL)"
help
Load image from MMCIF hardware block.
config ZBOOT_ROM_SH_MOBILE_SDHI
bool "Include SuperH Mobile SDHI loader in zImage (EXPERIMENTAL)"
help
Load image from SDHI hardware block
endchoice
config ARM_APPENDED_DTB
bool "Use appended device tree blob to zImage (EXPERIMENTAL)"
depends on OF && !ZBOOT_ROM && EXPERIMENTAL
help
With this option, the boot code will look for a device tree binary
(DTB) appended to zImage
(e.g. cat zImage .dtb > zImage_w_dtb).
This is meant as a backward compatibility convenience for those
systems with a bootloader that can't be upgraded to accommodate
the documented boot protocol using a device tree.
Beware that there is very little in terms of protection against
this option being confused by leftover garbage in memory that might
look like a DTB header after a reboot if no actual DTB is appended
to zImage. Do not leave this option active in a production kernel
if you don't intend to always append a DTB. Proper passing of the
location into r2 of a bootloader provided DTB is always preferable
to this option.
config ARM_ATAG_DTB_COMPAT
bool "Supplement the appended DTB with traditional ATAG information"
depends on ARM_APPENDED_DTB
help
Some old bootloaders can't be updated to a DTB capable one, yet
they provide ATAGs with memory configuration, the ramdisk address,
the kernel cmdline string, etc. Such information is dynamically
provided by the bootloader and can't always be stored in a static
DTB. To allow a device tree enabled kernel to be used with such
bootloaders, this option allows zImage to extract the information
from the ATAG list and store it at run time into the appended DTB.
choice
prompt "Kernel command line type" if ARM_ATAG_DTB_COMPAT
default ARM_ATAG_DTB_COMPAT_CMDLINE_FROM_BOOTLOADER
config ARM_ATAG_DTB_COMPAT_CMDLINE_FROM_BOOTLOADER
bool "Use bootloader kernel arguments if available"
help
Uses the command-line options passed by the boot loader instead of
the device tree bootargs property. If the boot loader doesn't provide
any, the device tree bootargs property will be used.
config ARM_ATAG_DTB_COMPAT_CMDLINE_EXTEND
bool "Extend with bootloader kernel arguments"
help
The command-line arguments provided by the boot loader will be
appended to the the device tree bootargs property.
endchoice
config CMDLINE
string "Default kernel command string"
default ""
help
On some architectures (EBSA110 and CATS), there is currently no way
for the boot loader to pass arguments to the kernel. For these
architectures, you should supply some command-line options at build
time by entering them here. As a minimum, you should specify the
memory size and the root device (e.g., mem=64M root=/dev/nfs).
choice
prompt "Kernel command line type" if CMDLINE != ""
default CMDLINE_FROM_BOOTLOADER
depends on ATAGS
config CMDLINE_FROM_BOOTLOADER
bool "Use bootloader kernel arguments if available"
help
Uses the command-line options passed by the boot loader. If
the boot loader doesn't provide any, the default kernel command
string provided in CMDLINE will be used.
config CMDLINE_EXTEND
bool "Extend bootloader kernel arguments"
help
The command-line arguments provided by the boot loader will be
appended to the default kernel command string.
config CMDLINE_FORCE
bool "Always use the default kernel command string"
help
Always use the default kernel command string, even if the boot
loader passes other arguments to the kernel.
This is useful if you cannot or don't want to change the
command-line options your boot loader passes to the kernel.
endchoice
config XIP_KERNEL
bool "Kernel Execute-In-Place from ROM"
depends on !ZBOOT_ROM && !ARM_LPAE && !ARCH_MULTIPLATFORM
help
Execute-In-Place allows the kernel to run from non-volatile storage
directly addressable by the CPU, such as NOR flash. This saves RAM
space since the text section of the kernel is not loaded from flash
to RAM. Read-write sections, such as the data section and stack,
are still copied to RAM. The XIP kernel is not compressed since
it has to run directly from flash, so it will take more space to
store it. The flash address used to link the kernel object files,
and for storing it, is configuration dependent. Therefore, if you
say Y here, you must know the proper physical address where to
store the kernel image depending on your own flash memory usage.
Also note that the make target becomes "make xipImage" rather than
"make zImage" or "make Image". The final kernel binary to put in
ROM memory will be arch/arm/boot/xipImage.
If unsure, say N.
config XIP_PHYS_ADDR
hex "XIP Kernel Physical Location"
depends on XIP_KERNEL
default "0x00080000"
help
This is the physical address in your flash memory the kernel will
be linked for and stored to. This address is dependent on your
own flash usage.
config KEXEC
bool "Kexec system call (EXPERIMENTAL)"
depends on EXPERIMENTAL && (!SMP || HOTPLUG_CPU)
help
kexec is a system call that implements the ability to shutdown your
current kernel, and to start another kernel. It is like a reboot
but it is independent of the system firmware. And like a reboot
you can start any kernel with it, not just Linux.
It is an ongoing process to be certain the hardware in a machine
is properly shutdown, so do not be surprised if this code does not
initially work for you. It may help to enable device hotplugging
support.
config ATAGS_PROC
bool "Export atags in procfs"
depends on ATAGS && KEXEC
default y
help
Should the atags used to boot the kernel be exported in an "atags"
file in procfs. Useful with kexec.
config CRASH_DUMP
bool "Build kdump crash kernel (EXPERIMENTAL)"
depends on EXPERIMENTAL
help
Generate crash dump after being started by kexec. This should
be normally only set in special crash dump kernels which are
loaded in the main kernel with kexec-tools into a specially
reserved region and then later executed after a crash by
kdump/kexec. The crash dump kernel must be compiled to a
memory address not used by the main kernel
For more details see Documentation/kdump/kdump.txt
config AUTO_ZRELADDR
bool "Auto calculation of the decompressed kernel image address"
depends on !ZBOOT_ROM && !ARCH_U300
help
ZRELADDR is the physical address where the decompressed kernel
image will be placed. If AUTO_ZRELADDR is selected, the address
will be determined at run-time by masking the current IP with
0xf8000000. This assumes the zImage being placed in the first 128MB
from start of memory.
endmenu
menu "CPU Power Management"
if ARCH_HAS_CPUFREQ
source "drivers/cpufreq/Kconfig"
config CPU_FREQ_IMX
tristate "CPUfreq driver for i.MX CPUs"
depends on ARCH_MXC && CPU_FREQ
select CPU_FREQ_TABLE
help
This enables the CPUfreq driver for i.MX CPUs.
config CPU_FREQ_SA1100
bool
config CPU_FREQ_SA1110
bool
config CPU_FREQ_INTEGRATOR
tristate "CPUfreq driver for ARM Integrator CPUs"
depends on ARCH_INTEGRATOR && CPU_FREQ
default y
help
This enables the CPUfreq driver for ARM Integrator CPUs.
For details, take a look at .
If in doubt, say Y.
config CPU_FREQ_PXA
bool
depends on CPU_FREQ && ARCH_PXA && PXA25x
default y
select CPU_FREQ_DEFAULT_GOV_USERSPACE
select CPU_FREQ_TABLE
config CPU_FREQ_S3C
bool
help
Internal configuration node for common cpufreq on Samsung SoC
config CPU_FREQ_S3C24XX
bool "CPUfreq driver for Samsung S3C24XX series CPUs (EXPERIMENTAL)"
depends on ARCH_S3C24XX && CPU_FREQ && EXPERIMENTAL
select CPU_FREQ_S3C
help
This enables the CPUfreq driver for the Samsung S3C24XX family
of CPUs.
For details, take a look at .
If in doubt, say N.
config CPU_FREQ_S3C24XX_PLL
bool "Support CPUfreq changing of PLL frequency (EXPERIMENTAL)"
depends on CPU_FREQ_S3C24XX && EXPERIMENTAL
help
Compile in support for changing the PLL frequency from the
S3C24XX series CPUfreq driver. The PLL takes time to settle
after a frequency change, so by default it is not enabled.
This also means that the PLL tables for the selected CPU(s) will
be built which may increase the size of the kernel image.
config CPU_FREQ_S3C24XX_DEBUG
bool "Debug CPUfreq Samsung driver core"
depends on CPU_FREQ_S3C24XX
help
Enable s3c_freq_dbg for the Samsung S3C CPUfreq core
config CPU_FREQ_S3C24XX_IODEBUG
bool "Debug CPUfreq Samsung driver IO timing"
depends on CPU_FREQ_S3C24XX
help
Enable s3c_freq_iodbg for the Samsung S3C CPUfreq core
config CPU_FREQ_S3C24XX_DEBUGFS
bool "Export debugfs for CPUFreq"
depends on CPU_FREQ_S3C24XX && DEBUG_FS
help
Export status information via debugfs.
endif
source "drivers/cpuidle/Kconfig"
endmenu
menu "Floating point emulation"
comment "At least one emulation must be selected"
config FPE_NWFPE
bool "NWFPE math emulation"
depends on (!AEABI || OABI_COMPAT) && !THUMB2_KERNEL
---help---
Say Y to include the NWFPE floating point emulator in the kernel.
This is necessary to run most binaries. Linux does not currently
support floating point hardware so you need to say Y here even if
your machine has an FPA or floating point co-processor podule.
You may say N here if you are going to load the Acorn FPEmulator
early in the bootup.
config FPE_NWFPE_XP
bool "Support extended precision"
depends on FPE_NWFPE
help
Say Y to include 80-bit support in the kernel floating-point
emulator. Otherwise, only 32 and 64-bit support is compiled in.
Note that gcc does not generate 80-bit operations by default,
so in most cases this option only enlarges the size of the
floating point emulator without any good reason.
You almost surely want to say N here.
config FPE_FASTFPE
bool "FastFPE math emulation (EXPERIMENTAL)"
depends on (!AEABI || OABI_COMPAT) && !CPU_32v3 && EXPERIMENTAL
---help---
Say Y here to include the FAST floating point emulator in the kernel.
This is an experimental much faster emulator which now also has full
precision for the mantissa. It does not support any exceptions.
It is very simple, and approximately 3-6 times faster than NWFPE.
It should be sufficient for most programs. It may be not suitable
for scientific calculations, but you have to check this for yourself.
If you do not feel you need a faster FP emulation you should better
choose NWFPE.
config VFP
bool "VFP-format floating point maths"
depends on CPU_V6 || CPU_V6K || CPU_ARM926T || CPU_V7 || CPU_FEROCEON
help
Say Y to include VFP support code in the kernel. This is needed
if your hardware includes a VFP unit.
Please see for
release notes and additional status information.
Say N if your target does not have VFP hardware.
config VFPv3
bool
depends on VFP
default y if CPU_V7
config NEON
bool "Advanced SIMD (NEON) Extension support"
depends on VFPv3 && CPU_V7
help
Say Y to include support code for NEON, the ARMv7 Advanced SIMD
Extension.
endmenu
menu "Userspace binary formats"
source "fs/Kconfig.binfmt"
config ARTHUR
tristate "RISC OS personality"
depends on !AEABI
help
Say Y here to include the kernel code necessary if you want to run
Acorn RISC OS/Arthur binaries under Linux. This code is still very
experimental; if this sounds frightening, say N and sleep in peace.
You can also say M here to compile this support as a module (which
will be called arthur).
endmenu
menu "Power management options"
source "kernel/power/Kconfig"
config ARCH_SUSPEND_POSSIBLE
depends on !ARCH_S5PC100
depends on CPU_ARM920T || CPU_ARM926T || CPU_SA1100 || \
CPU_V6 || CPU_V6K || CPU_V7 || CPU_XSC3 || CPU_XSCALE || CPU_MOHAWK
def_bool y
config ARM_CPU_SUSPEND
def_bool PM_SLEEP
endmenu
source "net/Kconfig"
source "drivers/Kconfig"
source "fs/Kconfig"
source "arch/arm/Kconfig.debug"
source "security/Kconfig"
source "crypto/Kconfig"
source "lib/Kconfig"