/* * omap2-restart.c - code common to all OMAP2xxx machines. * * Copyright (C) 2012 Texas Instruments * Paul Walmsley * * This program is free software; you can redistribute it and/or modify * it under the terms of the GNU General Public License version 2 as * published by the Free Software Foundation. */ #include #include #include #include #include "common.h" #include "prm2xxx.h" /* * reset_virt_prcm_set_ck, reset_sys_ck: pointers to the virt_prcm_set * clock and the sys_ck. Used during the reset process */ static struct clk *reset_virt_prcm_set_ck, *reset_sys_ck; /* Reboot handling */ /** * omap2xxx_restart - Set DPLL to bypass mode for reboot to work * * Set the DPLL to bypass so that reboot completes successfully. No * return value. */ void omap2xxx_restart(char mode, const char *cmd) { u32 rate; rate = clk_get_rate(reset_sys_ck); clk_set_rate(reset_virt_prcm_set_ck, rate); /* XXX Should save the cmd argument for use after the reboot */ omap2xxx_prm_dpll_reset(); /* never returns */ while (1); } /** * omap2xxx_common_look_up_clks_for_reset - look up clocks needed for restart * * Some clocks need to be looked up in advance for the SoC restart * operation to work - see omap2xxx_restart(). Returns -EINVAL upon * error or 0 upon success. */ static int __init omap2xxx_common_look_up_clks_for_reset(void) { reset_virt_prcm_set_ck = clk_get(NULL, "virt_prcm_set"); if (IS_ERR(reset_virt_prcm_set_ck)) return -EINVAL; reset_sys_ck = clk_get(NULL, "sys_ck"); if (IS_ERR(reset_sys_ck)) return -EINVAL; return 0; } core_initcall(omap2xxx_common_look_up_clks_for_reset);