/* * This file configures the internal USB PHY in OMAP4430. Used * with TWL6030 transceiver and MUSB on OMAP4430. * * Copyright (C) 2010 Texas Instruments Incorporated - http://www.ti.com * This program is free software; you can redistribute it and/or modify * it under the terms of the GNU General Public License as published by * the Free Software Foundation; either version 2 of the License, or * (at your option) any later version. * * Author: Hema HK * * This program is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the * GNU General Public License for more details. * * You should have received a copy of the GNU General Public License * along with this program; if not, write to the Free Software * Foundation, Inc., 675 Mass Ave, Cambridge, MA 02139, USA. * */ #include #include #include #include #include #include #include #include "soc.h" #include "control.h" #include "usb.h" #define CONTROL_DEV_CONF 0x300 #define PHY_PD 0x1 /** * omap4430_phy_power_down: disable MUSB PHY during early init * * OMAP4 MUSB PHY module is enabled by default on reset, but this will * prevent core retention if not disabled by SW. USB driver will * later on enable this, once and if the driver needs it. */ static int __init omap4430_phy_power_down(void) { void __iomem *ctrl_base; if (!cpu_is_omap44xx()) return 0; ctrl_base = ioremap(OMAP443X_SCM_BASE, SZ_1K); if (!ctrl_base) { pr_err("control module ioremap failed\n"); return -ENOMEM; } /* Power down the phy */ __raw_writel(PHY_PD, ctrl_base + CONTROL_DEV_CONF); iounmap(ctrl_base); return 0; } early_initcall(omap4430_phy_power_down); void am35x_musb_reset(void) { u32 regval; /* Reset the musb interface */ regval = omap_ctrl_readl(AM35XX_CONTROL_IP_SW_RESET); regval |= AM35XX_USBOTGSS_SW_RST; omap_ctrl_writel(regval, AM35XX_CONTROL_IP_SW_RESET); regval &= ~AM35XX_USBOTGSS_SW_RST; omap_ctrl_writel(regval, AM35XX_CONTROL_IP_SW_RESET); regval = omap_ctrl_readl(AM35XX_CONTROL_IP_SW_RESET); } void am35x_musb_phy_power(u8 on) { unsigned long timeout = jiffies + msecs_to_jiffies(100); u32 devconf2; if (on) { /* * Start the on-chip PHY and its PLL. */ devconf2 = omap_ctrl_readl(AM35XX_CONTROL_DEVCONF2); devconf2 &= ~(CONF2_RESET | CONF2_PHYPWRDN | CONF2_OTGPWRDN); devconf2 |= CONF2_PHY_PLLON; omap_ctrl_writel(devconf2, AM35XX_CONTROL_DEVCONF2); pr_info(KERN_INFO "Waiting for PHY clock good...\n"); while (!(omap_ctrl_readl(AM35XX_CONTROL_DEVCONF2) & CONF2_PHYCLKGD)) { cpu_relax(); if (time_after(jiffies, timeout)) { pr_err(KERN_ERR "musb PHY clock good timed out\n"); break; } } } else { /* * Power down the on-chip PHY. */ devconf2 = omap_ctrl_readl(AM35XX_CONTROL_DEVCONF2); devconf2 &= ~CONF2_PHY_PLLON; devconf2 |= CONF2_PHYPWRDN | CONF2_OTGPWRDN; omap_ctrl_writel(devconf2, AM35XX_CONTROL_DEVCONF2); } } void am35x_musb_clear_irq(void) { u32 regval; regval = omap_ctrl_readl(AM35XX_CONTROL_LVL_INTR_CLEAR); regval |= AM35XX_USBOTGSS_INT_CLR; omap_ctrl_writel(regval, AM35XX_CONTROL_LVL_INTR_CLEAR); regval = omap_ctrl_readl(AM35XX_CONTROL_LVL_INTR_CLEAR); } void am35x_set_mode(u8 musb_mode) { u32 devconf2 = omap_ctrl_readl(AM35XX_CONTROL_DEVCONF2); devconf2 &= ~CONF2_OTGMODE; switch (musb_mode) { case MUSB_HOST: /* Force VBUS valid, ID = 0 */ devconf2 |= CONF2_FORCE_HOST; break; case MUSB_PERIPHERAL: /* Force VBUS valid, ID = 1 */ devconf2 |= CONF2_FORCE_DEVICE; break; case MUSB_OTG: /* Don't override the VBUS/ID comparators */ devconf2 |= CONF2_NO_OVERRIDE; break; default: pr_info(KERN_INFO "Unsupported mode %u\n", musb_mode); } omap_ctrl_writel(devconf2, AM35XX_CONTROL_DEVCONF2); } void ti81xx_musb_phy_power(u8 on) { void __iomem *scm_base = NULL; u32 usbphycfg; scm_base = ioremap(TI81XX_SCM_BASE, SZ_2K); if (!scm_base) { pr_err("system control module ioremap failed\n"); return; } usbphycfg = __raw_readl(scm_base + USBCTRL0); if (on) { if (cpu_is_ti816x()) { usbphycfg |= TI816X_USBPHY0_NORMAL_MODE; usbphycfg &= ~TI816X_USBPHY_REFCLK_OSC; } else if (cpu_is_ti814x()) { usbphycfg &= ~(USBPHY_CM_PWRDN | USBPHY_OTG_PWRDN | USBPHY_DPINPUT | USBPHY_DMINPUT); usbphycfg |= (USBPHY_OTGVDET_EN | USBPHY_OTGSESSEND_EN | USBPHY_DPOPBUFCTL | USBPHY_DMOPBUFCTL); } } else { if (cpu_is_ti816x()) usbphycfg &= ~TI816X_USBPHY0_NORMAL_MODE; else if (cpu_is_ti814x()) usbphycfg |= USBPHY_CM_PWRDN | USBPHY_OTG_PWRDN; } __raw_writel(usbphycfg, scm_base + USBCTRL0); iounmap(scm_base); }