/* * Functions related to setting various queue properties from drivers */ #include #include #include #include #include #include #include "blk.h" /* * for max sense size */ #include /** * blk_end_sync_rq - executes a completion event on a request * @rq: request to complete * @error: end I/O status of the request */ static void blk_end_sync_rq(struct request *rq, int error) { struct completion *waiting = rq->end_io_data; rq->end_io_data = NULL; /* * complete last, if this is a stack request the process (and thus * the rq pointer) could be invalid right after this complete() */ complete(waiting); } /** * blk_execute_rq_nowait - insert a request into queue for execution * @q: queue to insert the request in * @bd_disk: matching gendisk * @rq: request to insert * @at_head: insert request at head or tail of queue * @done: I/O completion handler * * Description: * Insert a fully prepared request at the back of the I/O scheduler queue * for execution. Don't wait for completion. * * Note: * This function will invoke @done directly if the queue is dead. */ void blk_execute_rq_nowait(struct request_queue *q, struct gendisk *bd_disk, struct request *rq, int at_head, rq_end_io_fn *done) { int where = at_head ? ELEVATOR_INSERT_FRONT : ELEVATOR_INSERT_BACK; bool is_pm_resume; WARN_ON(irqs_disabled()); rq->rq_disk = bd_disk; rq->end_io = done; /* * don't check dying flag for MQ because the request won't * be resued after dying flag is set */ if (q->mq_ops) { blk_mq_insert_request(rq, at_head, true, false); return; } /* * need to check this before __blk_run_queue(), because rq can * be freed before that returns. */ is_pm_resume = rq->cmd_type == REQ_TYPE_PM_RESUME; spin_lock_irq(q->queue_lock); if (unlikely(blk_queue_dying(q))) { rq->cmd_flags |= REQ_QUIET; rq->errors = -ENXIO; __blk_end_request_all(rq, rq->errors); spin_unlock_irq(q->queue_lock); return; } __elv_add_request(q, rq, where); __blk_run_queue(q); /* the queue is stopped so it won't be run */ if (is_pm_resume) __blk_run_queue_uncond(q); spin_unlock_irq(q->queue_lock); } EXPORT_SYMBOL_GPL(blk_execute_rq_nowait); /** * blk_execute_rq - insert a request into queue for execution * @q: queue to insert the request in * @bd_disk: matching gendisk * @rq: request to insert * @at_head: insert request at head or tail of queue * * Description: * Insert a fully prepared request at the back of the I/O scheduler queue * for execution and wait for completion. */ int blk_execute_rq(struct request_queue *q, struct gendisk *bd_disk, struct request *rq, int at_head) { DECLARE_COMPLETION_ONSTACK(wait); char sense[SCSI_SENSE_BUFFERSIZE]; int err = 0; unsigned long hang_check; if (!rq->sense) { memset(sense, 0, sizeof(sense)); rq->sense = sense; rq->sense_len = 0; } rq->end_io_data = &wait; blk_execute_rq_nowait(q, bd_disk, rq, at_head, blk_end_sync_rq); /* Prevent hang_check timer from firing at us during very long I/O */ hang_check = sysctl_hung_task_timeout_secs; if (hang_check) while (!wait_for_completion_io_timeout(&wait, hang_check * (HZ/2))); else wait_for_completion_io(&wait); if (rq->errors) err = -EIO; return err; } EXPORT_SYMBOL(blk_execute_rq);