/* * Driver core for serial ports * * Based on drivers/char/serial.c, by Linus Torvalds, Theodore Ts'o. * * Copyright 1999 ARM Limited * Copyright (C) 2000-2001 Deep Blue Solutions Ltd. * * This program is free software; you can redistribute it and/or modify * it under the terms of the GNU General Public License as published by * the Free Software Foundation; either version 2 of the License, or * (at your option) any later version. * * This program is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the * GNU General Public License for more details. * * You should have received a copy of the GNU General Public License * along with this program; if not, write to the Free Software * Foundation, Inc., 59 Temple Place, Suite 330, Boston, MA 02111-1307 USA */ #include #include #include #include #include #include #include #include #include #include /* for serial_state and serial_icounter_struct */ #include #include #include #include #include /* * This is used to lock changes in serial line configuration. */ static DEFINE_MUTEX(port_mutex); /* * lockdep: port->lock is initialized in two places, but we * want only one lock-class: */ static struct lock_class_key port_lock_key; #define HIGH_BITS_OFFSET ((sizeof(long)-sizeof(int))*8) #ifdef CONFIG_SERIAL_CORE_CONSOLE #define uart_console(port) ((port)->cons && (port)->cons->index == (port)->line) #else #define uart_console(port) (0) #endif static void uart_change_speed(struct tty_struct *tty, struct uart_state *state, struct ktermios *old_termios); static void uart_wait_until_sent(struct tty_struct *tty, int timeout); static void uart_change_pm(struct uart_state *state, int pm_state); static void uart_port_shutdown(struct tty_port *port); /* * This routine is used by the interrupt handler to schedule processing in * the software interrupt portion of the driver. */ void uart_write_wakeup(struct uart_port *port) { struct uart_state *state = port->state; /* * This means you called this function _after_ the port was * closed. No cookie for you. */ BUG_ON(!state); tty_wakeup(state->port.tty); } static void uart_stop(struct tty_struct *tty) { struct uart_state *state = tty->driver_data; struct uart_port *port = state->uart_port; unsigned long flags; spin_lock_irqsave(&port->lock, flags); port->ops->stop_tx(port); spin_unlock_irqrestore(&port->lock, flags); } static void __uart_start(struct tty_struct *tty) { struct uart_state *state = tty->driver_data; struct uart_port *port = state->uart_port; if (!uart_circ_empty(&state->xmit) && state->xmit.buf && !tty->stopped && !tty->hw_stopped) port->ops->start_tx(port); } static void uart_start(struct tty_struct *tty) { struct uart_state *state = tty->driver_data; struct uart_port *port = state->uart_port; unsigned long flags; spin_lock_irqsave(&port->lock, flags); __uart_start(tty); spin_unlock_irqrestore(&port->lock, flags); } static inline void uart_update_mctrl(struct uart_port *port, unsigned int set, unsigned int clear) { unsigned long flags; unsigned int old; spin_lock_irqsave(&port->lock, flags); old = port->mctrl; port->mctrl = (old & ~clear) | set; if (old != port->mctrl) port->ops->set_mctrl(port, port->mctrl); spin_unlock_irqrestore(&port->lock, flags); } #define uart_set_mctrl(port, set) uart_update_mctrl(port, set, 0) #define uart_clear_mctrl(port, clear) uart_update_mctrl(port, 0, clear) /* * Startup the port. This will be called once per open. All calls * will be serialised by the per-port mutex. */ static int uart_port_startup(struct tty_struct *tty, struct uart_state *state, int init_hw) { struct uart_port *uport = state->uart_port; struct tty_port *port = &state->port; unsigned long page; int retval = 0; if (uport->type == PORT_UNKNOWN) return 1; /* * Initialise and allocate the transmit and temporary * buffer. */ if (!state->xmit.buf) { /* This is protected by the per port mutex */ page = get_zeroed_page(GFP_KERNEL); if (!page) return -ENOMEM; state->xmit.buf = (unsigned char *) page; uart_circ_clear(&state->xmit); } retval = uport->ops->startup(uport); if (retval == 0) { if (uart_console(uport) && uport->cons->cflag) { tty->termios.c_cflag = uport->cons->cflag; uport->cons->cflag = 0; } /* * Initialise the hardware port settings. */ uart_change_speed(tty, state, NULL); if (init_hw) { /* * Setup the RTS and DTR signals once the * port is open and ready to respond. */ if (tty->termios.c_cflag & CBAUD) uart_set_mctrl(uport, TIOCM_RTS | TIOCM_DTR); } if (tty_port_cts_enabled(port)) { spin_lock_irq(&uport->lock); if (!(uport->ops->get_mctrl(uport) & TIOCM_CTS)) tty->hw_stopped = 1; spin_unlock_irq(&uport->lock); } } /* * This is to allow setserial on this port. People may want to set * port/irq/type and then reconfigure the port properly if it failed * now. */ if (retval && capable(CAP_SYS_ADMIN)) return 1; return retval; } static int uart_startup(struct tty_struct *tty, struct uart_state *state, int init_hw) { struct tty_port *port = &state->port; int retval; if (port->flags & ASYNC_INITIALIZED) return 0; /* * Set the TTY IO error marker - we will only clear this * once we have successfully opened the port. */ set_bit(TTY_IO_ERROR, &tty->flags); retval = uart_port_startup(tty, state, init_hw); if (!retval) { set_bit(ASYNCB_INITIALIZED, &port->flags); clear_bit(TTY_IO_ERROR, &tty->flags); } else if (retval > 0) retval = 0; return retval; } /* * This routine will shutdown a serial port; interrupts are disabled, and * DTR is dropped if the hangup on close termio flag is on. Calls to * uart_shutdown are serialised by the per-port semaphore. */ static void uart_shutdown(struct tty_struct *tty, struct uart_state *state) { struct uart_port *uport = state->uart_port; struct tty_port *port = &state->port; /* * Set the TTY IO error marker */ if (tty) set_bit(TTY_IO_ERROR, &tty->flags); if (test_and_clear_bit(ASYNCB_INITIALIZED, &port->flags)) { /* * Turn off DTR and RTS early. */ if (!tty || (tty->termios.c_cflag & HUPCL)) uart_clear_mctrl(uport, TIOCM_DTR | TIOCM_RTS); uart_port_shutdown(port); } /* * It's possible for shutdown to be called after suspend if we get * a DCD drop (hangup) at just the right time. Clear suspended bit so * we don't try to resume a port that has been shutdown. */ clear_bit(ASYNCB_SUSPENDED, &port->flags); /* * Free the transmit buffer page. */ if (state->xmit.buf) { free_page((unsigned long)state->xmit.buf); state->xmit.buf = NULL; } } /** * uart_update_timeout - update per-port FIFO timeout. * @port: uart_port structure describing the port * @cflag: termios cflag value * @baud: speed of the port * * Set the port FIFO timeout value. The @cflag value should * reflect the actual hardware settings. */ void uart_update_timeout(struct uart_port *port, unsigned int cflag, unsigned int baud) { unsigned int bits; /* byte size and parity */ switch (cflag & CSIZE) { case CS5: bits = 7; break; case CS6: bits = 8; break; case CS7: bits = 9; break; default: bits = 10; break; /* CS8 */ } if (cflag & CSTOPB) bits++; if (cflag & PARENB) bits++; /* * The total number of bits to be transmitted in the fifo. */ bits = bits * port->fifosize; /* * Figure the timeout to send the above number of bits. * Add .02 seconds of slop */ port->timeout = (HZ * bits) / baud + HZ/50; } EXPORT_SYMBOL(uart_update_timeout); /** * uart_get_baud_rate - return baud rate for a particular port * @port: uart_port structure describing the port in question. * @termios: desired termios settings. * @old: old termios (or NULL) * @min: minimum acceptable baud rate * @max: maximum acceptable baud rate * * Decode the termios structure into a numeric baud rate, * taking account of the magic 38400 baud rate (with spd_* * flags), and mapping the %B0 rate to 9600 baud. * * If the new baud rate is invalid, try the old termios setting. * If it's still invalid, we try 9600 baud. * * Update the @termios structure to reflect the baud rate * we're actually going to be using. Don't do this for the case * where B0 is requested ("hang up"). */ unsigned int uart_get_baud_rate(struct uart_port *port, struct ktermios *termios, struct ktermios *old, unsigned int min, unsigned int max) { unsigned int try, baud, altbaud = 38400; int hung_up = 0; upf_t flags = port->flags & UPF_SPD_MASK; if (flags == UPF_SPD_HI) altbaud = 57600; else if (flags == UPF_SPD_VHI) altbaud = 115200; else if (flags == UPF_SPD_SHI) altbaud = 230400; else if (flags == UPF_SPD_WARP) altbaud = 460800; for (try = 0; try < 2; try++) { baud = tty_termios_baud_rate(termios); /* * The spd_hi, spd_vhi, spd_shi, spd_warp kludge... * Die! Die! Die! */ if (baud == 38400) baud = altbaud; /* * Special case: B0 rate. */ if (baud == 0) { hung_up = 1; baud = 9600; } if (baud >= min && baud <= max) return baud; /* * Oops, the quotient was zero. Try again with * the old baud rate if possible. */ termios->c_cflag &= ~CBAUD; if (old) { baud = tty_termios_baud_rate(old); if (!hung_up) tty_termios_encode_baud_rate(termios, baud, baud); old = NULL; continue; } /* * As a last resort, if the range cannot be met then clip to * the nearest chip supported rate. */ if (!hung_up) { if (baud <= min) tty_termios_encode_baud_rate(termios, min + 1, min + 1); else tty_termios_encode_baud_rate(termios, max - 1, max - 1); } } /* Should never happen */ WARN_ON(1); return 0; } EXPORT_SYMBOL(uart_get_baud_rate); /** * uart_get_divisor - return uart clock divisor * @port: uart_port structure describing the port. * @baud: desired baud rate * * Calculate the uart clock divisor for the port. */ unsigned int uart_get_divisor(struct uart_port *port, unsigned int baud) { unsigned int quot; /* * Old custom speed handling. */ if (baud == 38400 && (port->flags & UPF_SPD_MASK) == UPF_SPD_CUST) quot = port->custom_divisor; else quot = DIV_ROUND_CLOSEST(port->uartclk, 16 * baud); return quot; } EXPORT_SYMBOL(uart_get_divisor); /* FIXME: Consistent locking policy */ static void uart_change_speed(struct tty_struct *tty, struct uart_state *state, struct ktermios *old_termios) { struct tty_port *port = &state->port; struct uart_port *uport = state->uart_port; struct ktermios *termios; /* * If we have no tty, termios, or the port does not exist, * then we can't set the parameters for this port. */ if (!tty || uport->type == PORT_UNKNOWN) return; termios = &tty->termios; /* * Set flags based on termios cflag */ if (termios->c_cflag & CRTSCTS) set_bit(ASYNCB_CTS_FLOW, &port->flags); else clear_bit(ASYNCB_CTS_FLOW, &port->flags); if (termios->c_cflag & CLOCAL) clear_bit(ASYNCB_CHECK_CD, &port->flags); else set_bit(ASYNCB_CHECK_CD, &port->flags); uport->ops->set_termios(uport, termios, old_termios); } static inline int __uart_put_char(struct uart_port *port, struct circ_buf *circ, unsigned char c) { unsigned long flags; int ret = 0; if (!circ->buf) return 0; spin_lock_irqsave(&port->lock, flags); if (uart_circ_chars_free(circ) != 0) { circ->buf[circ->head] = c; circ->head = (circ->head + 1) & (UART_XMIT_SIZE - 1); ret = 1; } spin_unlock_irqrestore(&port->lock, flags); return ret; } static int uart_put_char(struct tty_struct *tty, unsigned char ch) { struct uart_state *state = tty->driver_data; return __uart_put_char(state->uart_port, &state->xmit, ch); } static void uart_flush_chars(struct tty_struct *tty) { uart_start(tty); } static int uart_write(struct tty_struct *tty, const unsigned char *buf, int count) { struct uart_state *state = tty->driver_data; struct uart_port *port; struct circ_buf *circ; unsigned long flags; int c, ret = 0; /* * This means you called this function _after_ the port was * closed. No cookie for you. */ if (!state) { WARN_ON(1); return -EL3HLT; } port = state->uart_port; circ = &state->xmit; if (!circ->buf) return 0; spin_lock_irqsave(&port->lock, flags); while (1) { c = CIRC_SPACE_TO_END(circ->head, circ->tail, UART_XMIT_SIZE); if (count < c) c = count; if (c <= 0) break; memcpy(circ->buf + circ->head, buf, c); circ->head = (circ->head + c) & (UART_XMIT_SIZE - 1); buf += c; count -= c; ret += c; } spin_unlock_irqrestore(&port->lock, flags); uart_start(tty); return ret; } static int uart_write_room(struct tty_struct *tty) { struct uart_state *state = tty->driver_data; unsigned long flags; int ret; spin_lock_irqsave(&state->uart_port->lock, flags); ret = uart_circ_chars_free(&state->xmit); spin_unlock_irqrestore(&state->uart_port->lock, flags); return ret; } static int uart_chars_in_buffer(struct tty_struct *tty) { struct uart_state *state = tty->driver_data; unsigned long flags; int ret; spin_lock_irqsave(&state->uart_port->lock, flags); ret = uart_circ_chars_pending(&state->xmit); spin_unlock_irqrestore(&state->uart_port->lock, flags); return ret; } static void uart_flush_buffer(struct tty_struct *tty) { struct uart_state *state = tty->driver_data; struct uart_port *port; unsigned long flags; /* * This means you called this function _after_ the port was * closed. No cookie for you. */ if (!state) { WARN_ON(1); return; } port = state->uart_port; pr_debug("uart_flush_buffer(%d) called\n", tty->index); spin_lock_irqsave(&port->lock, flags); uart_circ_clear(&state->xmit); if (port->ops->flush_buffer) port->ops->flush_buffer(port); spin_unlock_irqrestore(&port->lock, flags); tty_wakeup(tty); } /* * This function is used to send a high-priority XON/XOFF character to * the device */ static void uart_send_xchar(struct tty_struct *tty, char ch) { struct uart_state *state = tty->driver_data; struct uart_port *port = state->uart_port; unsigned long flags; if (port->ops->send_xchar) port->ops->send_xchar(port, ch); else { port->x_char = ch; if (ch) { spin_lock_irqsave(&port->lock, flags); port->ops->start_tx(port); spin_unlock_irqrestore(&port->lock, flags); } } } static void uart_throttle(struct tty_struct *tty) { struct uart_state *state = tty->driver_data; struct uart_port *port = state->uart_port; uint32_t mask = 0; if (I_IXOFF(tty)) mask |= UPF_SOFT_FLOW; if (tty->termios.c_cflag & CRTSCTS) mask |= UPF_HARD_FLOW; if (port->flags & mask) { port->ops->throttle(port); mask &= ~port->flags; } if (mask & UPF_SOFT_FLOW) uart_send_xchar(tty, STOP_CHAR(tty)); if (mask & UPF_HARD_FLOW) uart_clear_mctrl(port, TIOCM_RTS); } static void uart_unthrottle(struct tty_struct *tty) { struct uart_state *state = tty->driver_data; struct uart_port *port = state->uart_port; uint32_t mask = 0; if (I_IXOFF(tty)) mask |= UPF_SOFT_FLOW; if (tty->termios.c_cflag & CRTSCTS) mask |= UPF_HARD_FLOW; if (port->flags & mask) { port->ops->unthrottle(port); mask &= ~port->flags; } if (mask & UPF_SOFT_FLOW) { if (port->x_char) port->x_char = 0; else uart_send_xchar(tty, START_CHAR(tty)); } if (mask & UPF_HARD_FLOW) uart_set_mctrl(port, TIOCM_RTS); } static void do_uart_get_info(struct tty_port *port, struct serial_struct *retinfo) { struct uart_state *state = container_of(port, struct uart_state, port); struct uart_port *uport = state->uart_port; memset(retinfo, 0, sizeof(*retinfo)); retinfo->type = uport->type; retinfo->line = uport->line; retinfo->port = uport->iobase; if (HIGH_BITS_OFFSET) retinfo->port_high = (long) uport->iobase >> HIGH_BITS_OFFSET; retinfo->irq = uport->irq; retinfo->flags = uport->flags; retinfo->xmit_fifo_size = uport->fifosize; retinfo->baud_base = uport->uartclk / 16; retinfo->close_delay = jiffies_to_msecs(port->close_delay) / 10; retinfo->closing_wait = port->closing_wait == ASYNC_CLOSING_WAIT_NONE ? ASYNC_CLOSING_WAIT_NONE : jiffies_to_msecs(port->closing_wait) / 10; retinfo->custom_divisor = uport->custom_divisor; retinfo->hub6 = uport->hub6; retinfo->io_type = uport->iotype; retinfo->iomem_reg_shift = uport->regshift; retinfo->iomem_base = (void *)(unsigned long)uport->mapbase; } static void uart_get_info(struct tty_port *port, struct serial_struct *retinfo) { /* Ensure the state we copy is consistent and no hardware changes occur as we go */ mutex_lock(&port->mutex); do_uart_get_info(port, retinfo); mutex_unlock(&port->mutex); } static int uart_get_info_user(struct tty_port *port, struct serial_struct __user *retinfo) { struct serial_struct tmp; uart_get_info(port, &tmp); if (copy_to_user(retinfo, &tmp, sizeof(*retinfo))) return -EFAULT; return 0; } static int uart_set_info(struct tty_struct *tty, struct tty_port *port, struct uart_state *state, struct serial_struct *new_info) { struct uart_port *uport = state->uart_port; unsigned long new_port; unsigned int change_irq, change_port, closing_wait; unsigned int old_custom_divisor, close_delay; upf_t old_flags, new_flags; int retval = 0; new_port = new_info->port; if (HIGH_BITS_OFFSET) new_port += (unsigned long) new_info->port_high << HIGH_BITS_OFFSET; new_info->irq = irq_canonicalize(new_info->irq); close_delay = msecs_to_jiffies(new_info->close_delay * 10); closing_wait = new_info->closing_wait == ASYNC_CLOSING_WAIT_NONE ? ASYNC_CLOSING_WAIT_NONE : msecs_to_jiffies(new_info->closing_wait * 10); change_irq = !(uport->flags & UPF_FIXED_PORT) && new_info->irq != uport->irq; /* * Since changing the 'type' of the port changes its resource * allocations, we should treat type changes the same as * IO port changes. */ change_port = !(uport->flags & UPF_FIXED_PORT) && (new_port != uport->iobase || (unsigned long)new_info->iomem_base != uport->mapbase || new_info->hub6 != uport->hub6 || new_info->io_type != uport->iotype || new_info->iomem_reg_shift != uport->regshift || new_info->type != uport->type); old_flags = uport->flags; new_flags = new_info->flags; old_custom_divisor = uport->custom_divisor; if (!capable(CAP_SYS_ADMIN)) { retval = -EPERM; if (change_irq || change_port || (new_info->baud_base != uport->uartclk / 16) || (close_delay != port->close_delay) || (closing_wait != port->closing_wait) || (new_info->xmit_fifo_size && new_info->xmit_fifo_size != uport->fifosize) || (((new_flags ^ old_flags) & ~UPF_USR_MASK) != 0)) goto exit; uport->flags = ((uport->flags & ~UPF_USR_MASK) | (new_flags & UPF_USR_MASK)); uport->custom_divisor = new_info->custom_divisor; goto check_and_exit; } /* * Ask the low level driver to verify the settings. */ if (uport->ops->verify_port) retval = uport->ops->verify_port(uport, new_info); if ((new_info->irq >= nr_irqs) || (new_info->irq < 0) || (new_info->baud_base < 9600)) retval = -EINVAL; if (retval) goto exit; if (change_port || change_irq) { retval = -EBUSY; /* * Make sure that we are the sole user of this port. */ if (tty_port_users(port) > 1) goto exit; /* * We need to shutdown the serial port at the old * port/type/irq combination. */ uart_shutdown(tty, state); } if (change_port) { unsigned long old_iobase, old_mapbase; unsigned int old_type, old_iotype, old_hub6, old_shift; old_iobase = uport->iobase; old_mapbase = uport->mapbase; old_type = uport->type; old_hub6 = uport->hub6; old_iotype = uport->iotype; old_shift = uport->regshift; /* * Free and release old regions */ if (old_type != PORT_UNKNOWN) uport->ops->release_port(uport); uport->iobase = new_port; uport->type = new_info->type; uport->hub6 = new_info->hub6; uport->iotype = new_info->io_type; uport->regshift = new_info->iomem_reg_shift; uport->mapbase = (unsigned long)new_info->iomem_base; /* * Claim and map the new regions */ if (uport->type != PORT_UNKNOWN) { retval = uport->ops->request_port(uport); } else { /* Always success - Jean II */ retval = 0; } /* * If we fail to request resources for the * new port, try to restore the old settings. */ if (retval && old_type != PORT_UNKNOWN) { uport->iobase = old_iobase; uport->type = old_type; uport->hub6 = old_hub6; uport->iotype = old_iotype; uport->regshift = old_shift; uport->mapbase = old_mapbase; retval = uport->ops->request_port(uport); /* * If we failed to restore the old settings, * we fail like this. */ if (retval) uport->type = PORT_UNKNOWN; /* * We failed anyway. */ retval = -EBUSY; /* Added to return the correct error -Ram Gupta */ goto exit; } } if (change_irq) uport->irq = new_info->irq; if (!(uport->flags & UPF_FIXED_PORT)) uport->uartclk = new_info->baud_base * 16; uport->flags = (uport->flags & ~UPF_CHANGE_MASK) | (new_flags & UPF_CHANGE_MASK); uport->custom_divisor = new_info->custom_divisor; port->close_delay = close_delay; port->closing_wait = closing_wait; if (new_info->xmit_fifo_size) uport->fifosize = new_info->xmit_fifo_size; if (port->tty) port->tty->low_latency = (uport->flags & UPF_LOW_LATENCY) ? 1 : 0; check_and_exit: retval = 0; if (uport->type == PORT_UNKNOWN) goto exit; if (port->flags & ASYNC_INITIALIZED) { if (((old_flags ^ uport->flags) & UPF_SPD_MASK) || old_custom_divisor != uport->custom_divisor) { /* * If they're setting up a custom divisor or speed, * instead of clearing it, then bitch about it. No * need to rate-limit; it's CAP_SYS_ADMIN only. */ if (uport->flags & UPF_SPD_MASK) { char buf[64]; printk(KERN_NOTICE "%s sets custom speed on %s. This " "is deprecated.\n", current->comm, tty_name(port->tty, buf)); } uart_change_speed(tty, state, NULL); } } else retval = uart_startup(tty, state, 1); exit: return retval; } static int uart_set_info_user(struct tty_struct *tty, struct uart_state *state, struct serial_struct __user *newinfo) { struct serial_struct new_serial; struct tty_port *port = &state->port; int retval; if (copy_from_user(&new_serial, newinfo, sizeof(new_serial))) return -EFAULT; /* * This semaphore protects port->count. It is also * very useful to prevent opens. Also, take the * port configuration semaphore to make sure that a * module insertion/removal doesn't change anything * under us. */ mutex_lock(&port->mutex); retval = uart_set_info(tty, port, state, &new_serial); mutex_unlock(&port->mutex); return retval; } /** * uart_get_lsr_info - get line status register info * @tty: tty associated with the UART * @state: UART being queried * @value: returned modem value * * Note: uart_ioctl protects us against hangups. */ static int uart_get_lsr_info(struct tty_struct *tty, struct uart_state *state, unsigned int __user *value) { struct uart_port *uport = state->uart_port; unsigned int result; result = uport->ops->tx_empty(uport); /* * If we're about to load something into the transmit * register, we'll pretend the transmitter isn't empty to * avoid a race condition (depending on when the transmit * interrupt happens). */ if (uport->x_char || ((uart_circ_chars_pending(&state->xmit) > 0) && !tty->stopped && !tty->hw_stopped)) result &= ~TIOCSER_TEMT; return put_user(result, value); } static int uart_tiocmget(struct tty_struct *tty) { struct uart_state *state = tty->driver_data; struct tty_port *port = &state->port; struct uart_port *uport = state->uart_port; int result = -EIO; mutex_lock(&port->mutex); if (!(tty->flags & (1 << TTY_IO_ERROR))) { result = uport->mctrl; spin_lock_irq(&uport->lock); result |= uport->ops->get_mctrl(uport); spin_unlock_irq(&uport->lock); } mutex_unlock(&port->mutex); return result; } static int uart_tiocmset(struct tty_struct *tty, unsigned int set, unsigned int clear) { struct uart_state *state = tty->driver_data; struct uart_port *uport = state->uart_port; struct tty_port *port = &state->port; int ret = -EIO; mutex_lock(&port->mutex); if (!(tty->flags & (1 << TTY_IO_ERROR))) { uart_update_mctrl(uport, set, clear); ret = 0; } mutex_unlock(&port->mutex); return ret; } static int uart_break_ctl(struct tty_struct *tty, int break_state) { struct uart_state *state = tty->driver_data; struct tty_port *port = &state->port; struct uart_port *uport = state->uart_port; mutex_lock(&port->mutex); if (uport->type != PORT_UNKNOWN) uport->ops->break_ctl(uport, break_state); mutex_unlock(&port->mutex); return 0; } static int uart_do_autoconfig(struct tty_struct *tty,struct uart_state *state) { struct uart_port *uport = state->uart_port; struct tty_port *port = &state->port; int flags, ret; if (!capable(CAP_SYS_ADMIN)) return -EPERM; /* * Take the per-port semaphore. This prevents count from * changing, and hence any extra opens of the port while * we're auto-configuring. */ if (mutex_lock_interruptible(&port->mutex)) return -ERESTARTSYS; ret = -EBUSY; if (tty_port_users(port) == 1) { uart_shutdown(tty, state); /* * If we already have a port type configured, * we must release its resources. */ if (uport->type != PORT_UNKNOWN) uport->ops->release_port(uport); flags = UART_CONFIG_TYPE; if (uport->flags & UPF_AUTO_IRQ) flags |= UART_CONFIG_IRQ; /* * This will claim the ports resources if * a port is found. */ uport->ops->config_port(uport, flags); ret = uart_startup(tty, state, 1); } mutex_unlock(&port->mutex); return ret; } /* * Wait for any of the 4 modem inputs (DCD,RI,DSR,CTS) to change * - mask passed in arg for lines of interest * (use |'ed TIOCM_RNG/DSR/CD/CTS for masking) * Caller should use TIOCGICOUNT to see which one it was * * FIXME: This wants extracting into a common all driver implementation * of TIOCMWAIT using tty_port. */ static int uart_wait_modem_status(struct uart_state *state, unsigned long arg) { struct uart_port *uport = state->uart_port; struct tty_port *port = &state->port; DECLARE_WAITQUEUE(wait, current); struct uart_icount cprev, cnow; int ret; /* * note the counters on entry */ spin_lock_irq(&uport->lock); memcpy(&cprev, &uport->icount, sizeof(struct uart_icount)); /* * Force modem status interrupts on */ uport->ops->enable_ms(uport); spin_unlock_irq(&uport->lock); add_wait_queue(&port->delta_msr_wait, &wait); for (;;) { spin_lock_irq(&uport->lock); memcpy(&cnow, &uport->icount, sizeof(struct uart_icount)); spin_unlock_irq(&uport->lock); set_current_state(TASK_INTERRUPTIBLE); if (((arg & TIOCM_RNG) && (cnow.rng != cprev.rng)) || ((arg & TIOCM_DSR) && (cnow.dsr != cprev.dsr)) || ((arg & TIOCM_CD) && (cnow.dcd != cprev.dcd)) || ((arg & TIOCM_CTS) && (cnow.cts != cprev.cts))) { ret = 0; break; } schedule(); /* see if a signal did it */ if (signal_pending(current)) { ret = -ERESTARTSYS; break; } cprev = cnow; } current->state = TASK_RUNNING; remove_wait_queue(&port->delta_msr_wait, &wait); return ret; } /* * Get counter of input serial line interrupts (DCD,RI,DSR,CTS) * Return: write counters to the user passed counter struct * NB: both 1->0 and 0->1 transitions are counted except for * RI where only 0->1 is counted. */ static int uart_get_icount(struct tty_struct *tty, struct serial_icounter_struct *icount) { struct uart_state *state = tty->driver_data; struct uart_icount cnow; struct uart_port *uport = state->uart_port; spin_lock_irq(&uport->lock); memcpy(&cnow, &uport->icount, sizeof(struct uart_icount)); spin_unlock_irq(&uport->lock); icount->cts = cnow.cts; icount->dsr = cnow.dsr; icount->rng = cnow.rng; icount->dcd = cnow.dcd; icount->rx = cnow.rx; icount->tx = cnow.tx; icount->frame = cnow.frame; icount->overrun = cnow.overrun; icount->parity = cnow.parity; icount->brk = cnow.brk; icount->buf_overrun = cnow.buf_overrun; return 0; } /* * Called via sys_ioctl. We can use spin_lock_irq() here. */ static int uart_ioctl(struct tty_struct *tty, unsigned int cmd, unsigned long arg) { struct uart_state *state = tty->driver_data; struct tty_port *port = &state->port; void __user *uarg = (void __user *)arg; int ret = -ENOIOCTLCMD; /* * These ioctls don't rely on the hardware to be present. */ switch (cmd) { case TIOCGSERIAL: ret = uart_get_info_user(port, uarg); break; case TIOCSSERIAL: ret = uart_set_info_user(tty, state, uarg); break; case TIOCSERCONFIG: ret = uart_do_autoconfig(tty, state); break; case TIOCSERGWILD: /* obsolete */ case TIOCSERSWILD: /* obsolete */ ret = 0; break; } if (ret != -ENOIOCTLCMD) goto out; if (tty->flags & (1 << TTY_IO_ERROR)) { ret = -EIO; goto out; } /* * The following should only be used when hardware is present. */ switch (cmd) { case TIOCMIWAIT: ret = uart_wait_modem_status(state, arg); break; } if (ret != -ENOIOCTLCMD) goto out; mutex_lock(&port->mutex); if (tty->flags & (1 << TTY_IO_ERROR)) { ret = -EIO; goto out_up; } /* * All these rely on hardware being present and need to be * protected against the tty being hung up. */ switch (cmd) { case TIOCSERGETLSR: /* Get line status register */ ret = uart_get_lsr_info(tty, state, uarg); break; default: { struct uart_port *uport = state->uart_port; if (uport->ops->ioctl) ret = uport->ops->ioctl(uport, cmd, arg); break; } } out_up: mutex_unlock(&port->mutex); out: return ret; } static void uart_set_ldisc(struct tty_struct *tty) { struct uart_state *state = tty->driver_data; struct uart_port *uport = state->uart_port; if (uport->ops->set_ldisc) uport->ops->set_ldisc(uport, tty->termios.c_line); } static void uart_set_termios(struct tty_struct *tty, struct ktermios *old_termios) { struct uart_state *state = tty->driver_data; struct uart_port *uport = state->uart_port; unsigned long flags; unsigned int cflag = tty->termios.c_cflag; unsigned int iflag_mask = IGNBRK|BRKINT|IGNPAR|PARMRK|INPCK; bool sw_changed = false; /* * Drivers doing software flow control also need to know * about changes to these input settings. */ if (uport->flags & UPF_SOFT_FLOW) { iflag_mask |= IXANY|IXON|IXOFF; sw_changed = tty->termios.c_cc[VSTART] != old_termios->c_cc[VSTART] || tty->termios.c_cc[VSTOP] != old_termios->c_cc[VSTOP]; } /* * These are the bits that are used to setup various * flags in the low level driver. We can ignore the Bfoo * bits in c_cflag; c_[io]speed will always be set * appropriately by set_termios() in tty_ioctl.c */ if ((cflag ^ old_termios->c_cflag) == 0 && tty->termios.c_ospeed == old_termios->c_ospeed && tty->termios.c_ispeed == old_termios->c_ispeed && ((tty->termios.c_iflag ^ old_termios->c_iflag) & iflag_mask) == 0 && !sw_changed) { return; } uart_change_speed(tty, state, old_termios); /* Handle transition to B0 status */ if ((old_termios->c_cflag & CBAUD) && !(cflag & CBAUD)) uart_clear_mctrl(uport, TIOCM_RTS | TIOCM_DTR); /* Handle transition away from B0 status */ else if (!(old_termios->c_cflag & CBAUD) && (cflag & CBAUD)) { unsigned int mask = TIOCM_DTR; if (!(cflag & CRTSCTS) || !test_bit(TTY_THROTTLED, &tty->flags)) mask |= TIOCM_RTS; uart_set_mctrl(uport, mask); } /* * If the port is doing h/w assisted flow control, do nothing. * We assume that tty->hw_stopped has never been set. */ if (uport->flags & UPF_HARD_FLOW) return; /* Handle turning off CRTSCTS */ if ((old_termios->c_cflag & CRTSCTS) && !(cflag & CRTSCTS)) { spin_lock_irqsave(&uport->lock, flags); tty->hw_stopped = 0; __uart_start(tty); spin_unlock_irqrestore(&uport->lock, flags); } /* Handle turning on CRTSCTS */ else if (!(old_termios->c_cflag & CRTSCTS) && (cflag & CRTSCTS)) { spin_lock_irqsave(&uport->lock, flags); if (!(uport->ops->get_mctrl(uport) & TIOCM_CTS)) { tty->hw_stopped = 1; uport->ops->stop_tx(uport); } spin_unlock_irqrestore(&uport->lock, flags); } } /* * In 2.4.5, calls to this will be serialized via the BKL in * linux/drivers/char/tty_io.c:tty_release() * linux/drivers/char/tty_io.c:do_tty_handup() */ static void uart_close(struct tty_struct *tty, struct file *filp) { struct uart_state *state = tty->driver_data; struct tty_port *port; struct uart_port *uport; unsigned long flags; if (!state) return; uport = state->uart_port; port = &state->port; pr_debug("uart_close(%d) called\n", uport->line); if (tty_port_close_start(port, tty, filp) == 0) return; /* * At this point, we stop accepting input. To do this, we * disable the receive line status interrupts. */ if (port->flags & ASYNC_INITIALIZED) { unsigned long flags; spin_lock_irqsave(&uport->lock, flags); uport->ops->stop_rx(uport); spin_unlock_irqrestore(&uport->lock, flags); /* * Before we drop DTR, make sure the UART transmitter * has completely drained; this is especially * important if there is a transmit FIFO! */ uart_wait_until_sent(tty, uport->timeout); } mutex_lock(&port->mutex); uart_shutdown(tty, state); uart_flush_buffer(tty); tty_ldisc_flush(tty); tty_port_tty_set(port, NULL); spin_lock_irqsave(&port->lock, flags); tty->closing = 0; if (port->blocked_open) { spin_unlock_irqrestore(&port->lock, flags); if (port->close_delay) msleep_interruptible( jiffies_to_msecs(port->close_delay)); spin_lock_irqsave(&port->lock, flags); } else if (!uart_console(uport)) { spin_unlock_irqrestore(&port->lock, flags); uart_change_pm(state, 3); spin_lock_irqsave(&port->lock, flags); } /* * Wake up anyone trying to open this port. */ clear_bit(ASYNCB_NORMAL_ACTIVE, &port->flags); clear_bit(ASYNCB_CLOSING, &port->flags); spin_unlock_irqrestore(&port->lock, flags); wake_up_interruptible(&port->open_wait); wake_up_interruptible(&port->close_wait); mutex_unlock(&port->mutex); } static void uart_wait_until_sent(struct tty_struct *tty, int timeout) { struct uart_state *state = tty->driver_data; struct uart_port *port = state->uart_port; unsigned long char_time, expire; if (port->type == PORT_UNKNOWN || port->fifosize == 0) return; /* * Set the check interval to be 1/5 of the estimated time to * send a single character, and make it at least 1. The check * interval should also be less than the timeout. * * Note: we have to use pretty tight timings here to satisfy * the NIST-PCTS. */ char_time = (port->timeout - HZ/50) / port->fifosize; char_time = char_time / 5; if (char_time == 0) char_time = 1; if (timeout && timeout < char_time) char_time = timeout; /* * If the transmitter hasn't cleared in twice the approximate * amount of time to send the entire FIFO, it probably won't * ever clear. This assumes the UART isn't doing flow * control, which is currently the case. Hence, if it ever * takes longer than port->timeout, this is probably due to a * UART bug of some kind. So, we clamp the timeout parameter at * 2*port->timeout. */ if (timeout == 0 || timeout > 2 * port->timeout) timeout = 2 * port->timeout; expire = jiffies + timeout; pr_debug("uart_wait_until_sent(%d), jiffies=%lu, expire=%lu...\n", port->line, jiffies, expire); /* * Check whether the transmitter is empty every 'char_time'. * 'timeout' / 'expire' give us the maximum amount of time * we wait. */ while (!port->ops->tx_empty(port)) { msleep_interruptible(jiffies_to_msecs(char_time)); if (signal_pending(current)) break; if (time_after(jiffies, expire)) break; } } /* * This is called with the BKL held in * linux/drivers/char/tty_io.c:do_tty_hangup() * We're called from the eventd thread, so we can sleep for * a _short_ time only. */ static void uart_hangup(struct tty_struct *tty) { struct uart_state *state = tty->driver_data; struct tty_port *port = &state->port; unsigned long flags; pr_debug("uart_hangup(%d)\n", state->uart_port->line); mutex_lock(&port->mutex); if (port->flags & ASYNC_NORMAL_ACTIVE) { uart_flush_buffer(tty); uart_shutdown(tty, state); spin_lock_irqsave(&port->lock, flags); port->count = 0; clear_bit(ASYNCB_NORMAL_ACTIVE, &port->flags); spin_unlock_irqrestore(&port->lock, flags); tty_port_tty_set(port, NULL); wake_up_interruptible(&port->open_wait); wake_up_interruptible(&port->delta_msr_wait); } mutex_unlock(&port->mutex); } static int uart_port_activate(struct tty_port *port, struct tty_struct *tty) { return 0; } static void uart_port_shutdown(struct tty_port *port) { struct uart_state *state = container_of(port, struct uart_state, port); struct uart_port *uport = state->uart_port; /* * clear delta_msr_wait queue to avoid mem leaks: we may free * the irq here so the queue might never be woken up. Note * that we won't end up waiting on delta_msr_wait again since * any outstanding file descriptors should be pointing at * hung_up_tty_fops now. */ wake_up_interruptible(&port->delta_msr_wait); /* * Free the IRQ and disable the port. */ uport->ops->shutdown(uport); /* * Ensure that the IRQ handler isn't running on another CPU. */ synchronize_irq(uport->irq); } static int uart_carrier_raised(struct tty_port *port) { struct uart_state *state = container_of(port, struct uart_state, port); struct uart_port *uport = state->uart_port; int mctrl; spin_lock_irq(&uport->lock); uport->ops->enable_ms(uport); mctrl = uport->ops->get_mctrl(uport); spin_unlock_irq(&uport->lock); if (mctrl & TIOCM_CAR) return 1; return 0; } static void uart_dtr_rts(struct tty_port *port, int onoff) { struct uart_state *state = container_of(port, struct uart_state, port); struct uart_port *uport = state->uart_port; if (onoff) uart_set_mctrl(uport, TIOCM_DTR | TIOCM_RTS); else uart_clear_mctrl(uport, TIOCM_DTR | TIOCM_RTS); } /* * calls to uart_open are serialised by the BKL in * fs/char_dev.c:chrdev_open() * Note that if this fails, then uart_close() _will_ be called. * * In time, we want to scrap the "opening nonpresent ports" * behaviour and implement an alternative way for setserial * to set base addresses/ports/types. This will allow us to * get rid of a certain amount of extra tests. */ static int uart_open(struct tty_struct *tty, struct file *filp) { struct uart_driver *drv = (struct uart_driver *)tty->driver->driver_state; int retval, line = tty->index; struct uart_state *state = drv->state + line; struct tty_port *port = &state->port; pr_debug("uart_open(%d) called\n", line); /* * We take the semaphore here to guarantee that we won't be re-entered * while allocating the state structure, or while we request any IRQs * that the driver may need. This also has the nice side-effect that * it delays the action of uart_hangup, so we can guarantee that * state->port.tty will always contain something reasonable. */ if (mutex_lock_interruptible(&port->mutex)) { retval = -ERESTARTSYS; goto end; } port->count++; if (!state->uart_port || state->uart_port->flags & UPF_DEAD) { retval = -ENXIO; goto err_dec_count; } /* * Once we set tty->driver_data here, we are guaranteed that * uart_close() will decrement the driver module use count. * Any failures from here onwards should not touch the count. */ tty->driver_data = state; state->uart_port->state = state; tty->low_latency = (state->uart_port->flags & UPF_LOW_LATENCY) ? 1 : 0; tty_port_tty_set(port, tty); /* * If the port is in the middle of closing, bail out now. */ if (tty_hung_up_p(filp)) { retval = -EAGAIN; goto err_dec_count; } /* * Make sure the device is in D0 state. */ if (port->count == 1) uart_change_pm(state, 0); /* * Start up the serial port. */ retval = uart_startup(tty, state, 0); /* * If we succeeded, wait until the port is ready. */ mutex_unlock(&port->mutex); if (retval == 0) retval = tty_port_block_til_ready(port, tty, filp); end: return retval; err_dec_count: port->count--; mutex_unlock(&port->mutex); goto end; } static const char *uart_type(struct uart_port *port) { const char *str = NULL; if (port->ops->type) str = port->ops->type(port); if (!str) str = "unknown"; return str; } #ifdef CONFIG_PROC_FS static void uart_line_info(struct seq_file *m, struct uart_driver *drv, int i) { struct uart_state *state = drv->state + i; struct tty_port *port = &state->port; int pm_state; struct uart_port *uport = state->uart_port; char stat_buf[32]; unsigned int status; int mmio; if (!uport) return; mmio = uport->iotype >= UPIO_MEM; seq_printf(m, "%d: uart:%s %s%08llX irq:%d", uport->line, uart_type(uport), mmio ? "mmio:0x" : "port:", mmio ? (unsigned long long)uport->mapbase : (unsigned long long)uport->iobase, uport->irq); if (uport->type == PORT_UNKNOWN) { seq_putc(m, '\n'); return; } if (capable(CAP_SYS_ADMIN)) { mutex_lock(&port->mutex); pm_state = state->pm_state; if (pm_state) uart_change_pm(state, 0); spin_lock_irq(&uport->lock); status = uport->ops->get_mctrl(uport); spin_unlock_irq(&uport->lock); if (pm_state) uart_change_pm(state, pm_state); mutex_unlock(&port->mutex); seq_printf(m, " tx:%d rx:%d", uport->icount.tx, uport->icount.rx); if (uport->icount.frame) seq_printf(m, " fe:%d", uport->icount.frame); if (uport->icount.parity) seq_printf(m, " pe:%d", uport->icount.parity); if (uport->icount.brk) seq_printf(m, " brk:%d", uport->icount.brk); if (uport->icount.overrun) seq_printf(m, " oe:%d", uport->icount.overrun); #define INFOBIT(bit, str) \ if (uport->mctrl & (bit)) \ strncat(stat_buf, (str), sizeof(stat_buf) - \ strlen(stat_buf) - 2) #define STATBIT(bit, str) \ if (status & (bit)) \ strncat(stat_buf, (str), sizeof(stat_buf) - \ strlen(stat_buf) - 2) stat_buf[0] = '\0'; stat_buf[1] = '\0'; INFOBIT(TIOCM_RTS, "|RTS"); STATBIT(TIOCM_CTS, "|CTS"); INFOBIT(TIOCM_DTR, "|DTR"); STATBIT(TIOCM_DSR, "|DSR"); STATBIT(TIOCM_CAR, "|CD"); STATBIT(TIOCM_RNG, "|RI"); if (stat_buf[0]) stat_buf[0] = ' '; seq_puts(m, stat_buf); } seq_putc(m, '\n'); #undef STATBIT #undef INFOBIT } static int uart_proc_show(struct seq_file *m, void *v) { struct tty_driver *ttydrv = m->private; struct uart_driver *drv = ttydrv->driver_state; int i; seq_printf(m, "serinfo:1.0 driver%s%s revision:%s\n", "", "", ""); for (i = 0; i < drv->nr; i++) uart_line_info(m, drv, i); return 0; } static int uart_proc_open(struct inode *inode, struct file *file) { return single_open(file, uart_proc_show, PDE(inode)->data); } static const struct file_operations uart_proc_fops = { .owner = THIS_MODULE, .open = uart_proc_open, .read = seq_read, .llseek = seq_lseek, .release = single_release, }; #endif #if defined(CONFIG_SERIAL_CORE_CONSOLE) || defined(CONFIG_CONSOLE_POLL) /* * uart_console_write - write a console message to a serial port * @port: the port to write the message * @s: array of characters * @count: number of characters in string to write * @write: function to write character to port */ void uart_console_write(struct uart_port *port, const char *s, unsigned int count, void (*putchar)(struct uart_port *, int)) { unsigned int i; for (i = 0; i < count; i++, s++) { if (*s == '\n') putchar(port, '\r'); putchar(port, *s); } } EXPORT_SYMBOL_GPL(uart_console_write); /* * Check whether an invalid uart number has been specified, and * if so, search for the first available port that does have * console support. */ struct uart_port * __init uart_get_console(struct uart_port *ports, int nr, struct console *co) { int idx = co->index; if (idx < 0 || idx >= nr || (ports[idx].iobase == 0 && ports[idx].membase == NULL)) for (idx = 0; idx < nr; idx++) if (ports[idx].iobase != 0 || ports[idx].membase != NULL) break; co->index = idx; return ports + idx; } /** * uart_parse_options - Parse serial port baud/parity/bits/flow contro. * @options: pointer to option string * @baud: pointer to an 'int' variable for the baud rate. * @parity: pointer to an 'int' variable for the parity. * @bits: pointer to an 'int' variable for the number of data bits. * @flow: pointer to an 'int' variable for the flow control character. * * uart_parse_options decodes a string containing the serial console * options. The format of the string is , * eg: 115200n8r */ void uart_parse_options(char *options, int *baud, int *parity, int *bits, int *flow) { char *s = options; *baud = simple_strtoul(s, NULL, 10); while (*s >= '0' && *s <= '9') s++; if (*s) *parity = *s++; if (*s) *bits = *s++ - '0'; if (*s) *flow = *s; } EXPORT_SYMBOL_GPL(uart_parse_options); struct baud_rates { unsigned int rate; unsigned int cflag; }; static const struct baud_rates baud_rates[] = { { 921600, B921600 }, { 460800, B460800 }, { 230400, B230400 }, { 115200, B115200 }, { 57600, B57600 }, { 38400, B38400 }, { 19200, B19200 }, { 9600, B9600 }, { 4800, B4800 }, { 2400, B2400 }, { 1200, B1200 }, { 0, B38400 } }; /** * uart_set_options - setup the serial console parameters * @port: pointer to the serial ports uart_port structure * @co: console pointer * @baud: baud rate * @parity: parity character - 'n' (none), 'o' (odd), 'e' (even) * @bits: number of data bits * @flow: flow control character - 'r' (rts) */ int uart_set_options(struct uart_port *port, struct console *co, int baud, int parity, int bits, int flow) { struct ktermios termios; static struct ktermios dummy; int i; /* * Ensure that the serial console lock is initialised * early. */ spin_lock_init(&port->lock); lockdep_set_class(&port->lock, &port_lock_key); memset(&termios, 0, sizeof(struct ktermios)); termios.c_cflag = CREAD | HUPCL | CLOCAL; /* * Construct a cflag setting. */ for (i = 0; baud_rates[i].rate; i++) if (baud_rates[i].rate <= baud) break; termios.c_cflag |= baud_rates[i].cflag; if (bits == 7) termios.c_cflag |= CS7; else termios.c_cflag |= CS8; switch (parity) { case 'o': case 'O': termios.c_cflag |= PARODD; /*fall through*/ case 'e': case 'E': termios.c_cflag |= PARENB; break; } if (flow == 'r') termios.c_cflag |= CRTSCTS; /* * some uarts on other side don't support no flow control. * So we set * DTR in host uart to make them happy */ port->mctrl |= TIOCM_DTR; port->ops->set_termios(port, &termios, &dummy); /* * Allow the setting of the UART parameters with a NULL console * too: */ if (co) co->cflag = termios.c_cflag; return 0; } EXPORT_SYMBOL_GPL(uart_set_options); #endif /* CONFIG_SERIAL_CORE_CONSOLE */ /** * uart_change_pm - set power state of the port * * @state: port descriptor * @pm_state: new state * * Locking: port->mutex has to be held */ static void uart_change_pm(struct uart_state *state, int pm_state) { struct uart_port *port = state->uart_port; if (state->pm_state != pm_state) { if (port->ops->pm) port->ops->pm(port, pm_state, state->pm_state); state->pm_state = pm_state; } } struct uart_match { struct uart_port *port; struct uart_driver *driver; }; static int serial_match_port(struct device *dev, void *data) { struct uart_match *match = data; struct tty_driver *tty_drv = match->driver->tty_driver; dev_t devt = MKDEV(tty_drv->major, tty_drv->minor_start) + match->port->line; return dev->devt == devt; /* Actually, only one tty per port */ } int uart_suspend_port(struct uart_driver *drv, struct uart_port *uport) { struct uart_state *state = drv->state + uport->line; struct tty_port *port = &state->port; struct device *tty_dev; struct uart_match match = {uport, drv}; mutex_lock(&port->mutex); tty_dev = device_find_child(uport->dev, &match, serial_match_port); if (device_may_wakeup(tty_dev)) { if (!enable_irq_wake(uport->irq)) uport->irq_wake = 1; put_device(tty_dev); mutex_unlock(&port->mutex); return 0; } if (console_suspend_enabled || !uart_console(uport)) uport->suspended = 1; if (port->flags & ASYNC_INITIALIZED) { const struct uart_ops *ops = uport->ops; int tries; if (console_suspend_enabled || !uart_console(uport)) { set_bit(ASYNCB_SUSPENDED, &port->flags); clear_bit(ASYNCB_INITIALIZED, &port->flags); spin_lock_irq(&uport->lock); ops->stop_tx(uport); ops->set_mctrl(uport, 0); ops->stop_rx(uport); spin_unlock_irq(&uport->lock); } /* * Wait for the transmitter to empty. */ for (tries = 3; !ops->tx_empty(uport) && tries; tries--) msleep(10); if (!tries) printk(KERN_ERR "%s%s%s%d: Unable to drain " "transmitter\n", uport->dev ? dev_name(uport->dev) : "", uport->dev ? ": " : "", drv->dev_name, drv->tty_driver->name_base + uport->line); if (console_suspend_enabled || !uart_console(uport)) ops->shutdown(uport); } /* * Disable the console device before suspending. */ if (console_suspend_enabled && uart_console(uport)) console_stop(uport->cons); if (console_suspend_enabled || !uart_console(uport)) uart_change_pm(state, 3); mutex_unlock(&port->mutex); return 0; } int uart_resume_port(struct uart_driver *drv, struct uart_port *uport) { struct uart_state *state = drv->state + uport->line; struct tty_port *port = &state->port; struct device *tty_dev; struct uart_match match = {uport, drv}; struct ktermios termios; mutex_lock(&port->mutex); tty_dev = device_find_child(uport->dev, &match, serial_match_port); if (!uport->suspended && device_may_wakeup(tty_dev)) { if (uport->irq_wake) { disable_irq_wake(uport->irq); uport->irq_wake = 0; } mutex_unlock(&port->mutex); return 0; } uport->suspended = 0; /* * Re-enable the console device after suspending. */ if (uart_console(uport)) { /* * First try to use the console cflag setting. */ memset(&termios, 0, sizeof(struct ktermios)); termios.c_cflag = uport->cons->cflag; /* * If that's unset, use the tty termios setting. */ if (port->tty && termios.c_cflag == 0) termios = port->tty->termios; if (console_suspend_enabled) uart_change_pm(state, 0); uport->ops->set_termios(uport, &termios, NULL); if (console_suspend_enabled) console_start(uport->cons); } if (port->flags & ASYNC_SUSPENDED) { const struct uart_ops *ops = uport->ops; int ret; uart_change_pm(state, 0); spin_lock_irq(&uport->lock); ops->set_mctrl(uport, 0); spin_unlock_irq(&uport->lock); if (console_suspend_enabled || !uart_console(uport)) { /* Protected by port mutex for now */ struct tty_struct *tty = port->tty; ret = ops->startup(uport); if (ret == 0) { if (tty) uart_change_speed(tty, state, NULL); spin_lock_irq(&uport->lock); ops->set_mctrl(uport, uport->mctrl); ops->start_tx(uport); spin_unlock_irq(&uport->lock); set_bit(ASYNCB_INITIALIZED, &port->flags); } else { /* * Failed to resume - maybe hardware went away? * Clear the "initialized" flag so we won't try * to call the low level drivers shutdown method. */ uart_shutdown(tty, state); } } clear_bit(ASYNCB_SUSPENDED, &port->flags); } mutex_unlock(&port->mutex); return 0; } static inline void uart_report_port(struct uart_driver *drv, struct uart_port *port) { char address[64]; switch (port->iotype) { case UPIO_PORT: snprintf(address, sizeof(address), "I/O 0x%lx", port->iobase); break; case UPIO_HUB6: snprintf(address, sizeof(address), "I/O 0x%lx offset 0x%x", port->iobase, port->hub6); break; case UPIO_MEM: case UPIO_MEM32: case UPIO_AU: case UPIO_TSI: snprintf(address, sizeof(address), "MMIO 0x%llx", (unsigned long long)port->mapbase); break; default: strlcpy(address, "*unknown*", sizeof(address)); break; } printk(KERN_INFO "%s%s%s%d at %s (irq = %d) is a %s\n", port->dev ? dev_name(port->dev) : "", port->dev ? ": " : "", drv->dev_name, drv->tty_driver->name_base + port->line, address, port->irq, uart_type(port)); } static void uart_configure_port(struct uart_driver *drv, struct uart_state *state, struct uart_port *port) { unsigned int flags; /* * If there isn't a port here, don't do anything further. */ if (!port->iobase && !port->mapbase && !port->membase) return; /* * Now do the auto configuration stuff. Note that config_port * is expected to claim the resources and map the port for us. */ flags = 0; if (port->flags & UPF_AUTO_IRQ) flags |= UART_CONFIG_IRQ; if (port->flags & UPF_BOOT_AUTOCONF) { if (!(port->flags & UPF_FIXED_TYPE)) { port->type = PORT_UNKNOWN; flags |= UART_CONFIG_TYPE; } port->ops->config_port(port, flags); } if (port->type != PORT_UNKNOWN) { unsigned long flags; uart_report_port(drv, port); /* Power up port for set_mctrl() */ uart_change_pm(state, 0); /* * Ensure that the modem control lines are de-activated. * keep the DTR setting that is set in uart_set_options() * We probably don't need a spinlock around this, but */ spin_lock_irqsave(&port->lock, flags); port->ops->set_mctrl(port, port->mctrl & TIOCM_DTR); spin_unlock_irqrestore(&port->lock, flags); /* * If this driver supports console, and it hasn't been * successfully registered yet, try to re-register it. * It may be that the port was not available. */ if (port->cons && !(port->cons->flags & CON_ENABLED)) register_console(port->cons); /* * Power down all ports by default, except the * console if we have one. */ if (!uart_console(port)) uart_change_pm(state, 3); } } #ifdef CONFIG_CONSOLE_POLL static int uart_poll_init(struct tty_driver *driver, int line, char *options) { struct uart_driver *drv = driver->driver_state; struct uart_state *state = drv->state + line; struct uart_port *port; int baud = 9600; int bits = 8; int parity = 'n'; int flow = 'n'; int ret; if (!state || !state->uart_port) return -1; port = state->uart_port; if (!(port->ops->poll_get_char && port->ops->poll_put_char)) return -1; if (port->ops->poll_init) { struct tty_port *tport = &state->port; ret = 0; mutex_lock(&tport->mutex); /* * We don't set ASYNCB_INITIALIZED as we only initialized the * hw, e.g. state->xmit is still uninitialized. */ if (!test_bit(ASYNCB_INITIALIZED, &tport->flags)) ret = port->ops->poll_init(port); mutex_unlock(&tport->mutex); if (ret) return ret; } if (options) { uart_parse_options(options, &baud, &parity, &bits, &flow); return uart_set_options(port, NULL, baud, parity, bits, flow); } return 0; } static int uart_poll_get_char(struct tty_driver *driver, int line) { struct uart_driver *drv = driver->driver_state; struct uart_state *state = drv->state + line; struct uart_port *port; if (!state || !state->uart_port) return -1; port = state->uart_port; return port->ops->poll_get_char(port); } static void uart_poll_put_char(struct tty_driver *driver, int line, char ch) { struct uart_driver *drv = driver->driver_state; struct uart_state *state = drv->state + line; struct uart_port *port; if (!state || !state->uart_port) return; port = state->uart_port; port->ops->poll_put_char(port, ch); } #endif static const struct tty_operations uart_ops = { .open = uart_open, .close = uart_close, .write = uart_write, .put_char = uart_put_char, .flush_chars = uart_flush_chars, .write_room = uart_write_room, .chars_in_buffer= uart_chars_in_buffer, .flush_buffer = uart_flush_buffer, .ioctl = uart_ioctl, .throttle = uart_throttle, .unthrottle = uart_unthrottle, .send_xchar = uart_send_xchar, .set_termios = uart_set_termios, .set_ldisc = uart_set_ldisc, .stop = uart_stop, .start = uart_start, .hangup = uart_hangup, .break_ctl = uart_break_ctl, .wait_until_sent= uart_wait_until_sent, #ifdef CONFIG_PROC_FS .proc_fops = &uart_proc_fops, #endif .tiocmget = uart_tiocmget, .tiocmset = uart_tiocmset, .get_icount = uart_get_icount, #ifdef CONFIG_CONSOLE_POLL .poll_init = uart_poll_init, .poll_get_char = uart_poll_get_char, .poll_put_char = uart_poll_put_char, #endif }; static const struct tty_port_operations uart_port_ops = { .activate = uart_port_activate, .shutdown = uart_port_shutdown, .carrier_raised = uart_carrier_raised, .dtr_rts = uart_dtr_rts, }; /** * uart_register_driver - register a driver with the uart core layer * @drv: low level driver structure * * Register a uart driver with the core driver. We in turn register * with the tty layer, and initialise the core driver per-port state. * * We have a proc file in /proc/tty/driver which is named after the * normal driver. * * drv->port should be NULL, and the per-port structures should be * registered using uart_add_one_port after this call has succeeded. */ int uart_register_driver(struct uart_driver *drv) { struct tty_driver *normal; int i, retval; BUG_ON(drv->state); /* * Maybe we should be using a slab cache for this, especially if * we have a large number of ports to handle. */ drv->state = kzalloc(sizeof(struct uart_state) * drv->nr, GFP_KERNEL); if (!drv->state) goto out; normal = alloc_tty_driver(drv->nr); if (!normal) goto out_kfree; drv->tty_driver = normal; normal->driver_name = drv->driver_name; normal->name = drv->dev_name; normal->major = drv->major; normal->minor_start = drv->minor; normal->type = TTY_DRIVER_TYPE_SERIAL; normal->subtype = SERIAL_TYPE_NORMAL; normal->init_termios = tty_std_termios; normal->init_termios.c_cflag = B9600 | CS8 | CREAD | HUPCL | CLOCAL; normal->init_termios.c_ispeed = normal->init_termios.c_ospeed = 9600; normal->flags = TTY_DRIVER_REAL_RAW | TTY_DRIVER_DYNAMIC_DEV; normal->driver_state = drv; tty_set_operations(normal, &uart_ops); /* * Initialise the UART state(s). */ for (i = 0; i < drv->nr; i++) { struct uart_state *state = drv->state + i; struct tty_port *port = &state->port; tty_port_init(port); port->ops = &uart_port_ops; port->close_delay = HZ / 2; /* .5 seconds */ port->closing_wait = 30 * HZ;/* 30 seconds */ } retval = tty_register_driver(normal); if (retval >= 0) return retval; for (i = 0; i < drv->nr; i++) tty_port_destroy(&drv->state[i].port); put_tty_driver(normal); out_kfree: kfree(drv->state); out: return -ENOMEM; } /** * uart_unregister_driver - remove a driver from the uart core layer * @drv: low level driver structure * * Remove all references to a driver from the core driver. The low * level driver must have removed all its ports via the * uart_remove_one_port() if it registered them with uart_add_one_port(). * (ie, drv->port == NULL) */ void uart_unregister_driver(struct uart_driver *drv) { struct tty_driver *p = drv->tty_driver; unsigned int i; tty_unregister_driver(p); put_tty_driver(p); for (i = 0; i < drv->nr; i++) tty_port_destroy(&drv->state[i].port); kfree(drv->state); drv->state = NULL; drv->tty_driver = NULL; } struct tty_driver *uart_console_device(struct console *co, int *index) { struct uart_driver *p = co->data; *index = co->index; return p->tty_driver; } static ssize_t uart_get_attr_uartclk(struct device *dev, struct device_attribute *attr, char *buf) { struct serial_struct tmp; struct tty_port *port = dev_get_drvdata(dev); uart_get_info(port, &tmp); return snprintf(buf, PAGE_SIZE, "%d\n", tmp.baud_base * 16); } static ssize_t uart_get_attr_type(struct device *dev, struct device_attribute *attr, char *buf) { struct serial_struct tmp; struct tty_port *port = dev_get_drvdata(dev); uart_get_info(port, &tmp); return snprintf(buf, PAGE_SIZE, "%d\n", tmp.type); } static ssize_t uart_get_attr_line(struct device *dev, struct device_attribute *attr, char *buf) { struct serial_struct tmp; struct tty_port *port = dev_get_drvdata(dev); uart_get_info(port, &tmp); return snprintf(buf, PAGE_SIZE, "%d\n", tmp.line); } static ssize_t uart_get_attr_port(struct device *dev, struct device_attribute *attr, char *buf) { struct serial_struct tmp; struct tty_port *port = dev_get_drvdata(dev); unsigned long ioaddr; uart_get_info(port, &tmp); ioaddr = tmp.port; if (HIGH_BITS_OFFSET) ioaddr |= (unsigned long)tmp.port_high << HIGH_BITS_OFFSET; return snprintf(buf, PAGE_SIZE, "0x%lX\n", ioaddr); } static ssize_t uart_get_attr_irq(struct device *dev, struct device_attribute *attr, char *buf) { struct serial_struct tmp; struct tty_port *port = dev_get_drvdata(dev); uart_get_info(port, &tmp); return snprintf(buf, PAGE_SIZE, "%d\n", tmp.irq); } static ssize_t uart_get_attr_flags(struct device *dev, struct device_attribute *attr, char *buf) { struct serial_struct tmp; struct tty_port *port = dev_get_drvdata(dev); uart_get_info(port, &tmp); return snprintf(buf, PAGE_SIZE, "0x%X\n", tmp.flags); } static ssize_t uart_get_attr_xmit_fifo_size(struct device *dev, struct device_attribute *attr, char *buf) { struct serial_struct tmp; struct tty_port *port = dev_get_drvdata(dev); uart_get_info(port, &tmp); return snprintf(buf, PAGE_SIZE, "%d\n", tmp.xmit_fifo_size); } static ssize_t uart_get_attr_close_delay(struct device *dev, struct device_attribute *attr, char *buf) { struct serial_struct tmp; struct tty_port *port = dev_get_drvdata(dev); uart_get_info(port, &tmp); return snprintf(buf, PAGE_SIZE, "%d\n", tmp.close_delay); } static ssize_t uart_get_attr_closing_wait(struct device *dev, struct device_attribute *attr, char *buf) { struct serial_struct tmp; struct tty_port *port = dev_get_drvdata(dev); uart_get_info(port, &tmp); return snprintf(buf, PAGE_SIZE, "%d\n", tmp.closing_wait); } static ssize_t uart_get_attr_custom_divisor(struct device *dev, struct device_attribute *attr, char *buf) { struct serial_struct tmp; struct tty_port *port = dev_get_drvdata(dev); uart_get_info(port, &tmp); return snprintf(buf, PAGE_SIZE, "%d\n", tmp.custom_divisor); } static ssize_t uart_get_attr_io_type(struct device *dev, struct device_attribute *attr, char *buf) { struct serial_struct tmp; struct tty_port *port = dev_get_drvdata(dev); uart_get_info(port, &tmp); return snprintf(buf, PAGE_SIZE, "%d\n", tmp.io_type); } static ssize_t uart_get_attr_iomem_base(struct device *dev, struct device_attribute *attr, char *buf) { struct serial_struct tmp; struct tty_port *port = dev_get_drvdata(dev); uart_get_info(port, &tmp); return snprintf(buf, PAGE_SIZE, "0x%lX\n", (unsigned long)tmp.iomem_base); } static ssize_t uart_get_attr_iomem_reg_shift(struct device *dev, struct device_attribute *attr, char *buf) { struct serial_struct tmp; struct tty_port *port = dev_get_drvdata(dev); uart_get_info(port, &tmp); return snprintf(buf, PAGE_SIZE, "%d\n", tmp.iomem_reg_shift); } static DEVICE_ATTR(type, S_IRUSR | S_IRGRP, uart_get_attr_type, NULL); static DEVICE_ATTR(line, S_IRUSR | S_IRGRP, uart_get_attr_line, NULL); static DEVICE_ATTR(port, S_IRUSR | S_IRGRP, uart_get_attr_port, NULL); static DEVICE_ATTR(irq, S_IRUSR | S_IRGRP, uart_get_attr_irq, NULL); static DEVICE_ATTR(flags, S_IRUSR | S_IRGRP, uart_get_attr_flags, NULL); static DEVICE_ATTR(xmit_fifo_size, S_IRUSR | S_IRGRP, uart_get_attr_xmit_fifo_size, NULL); static DEVICE_ATTR(uartclk, S_IRUSR | S_IRGRP, uart_get_attr_uartclk, NULL); static DEVICE_ATTR(close_delay, S_IRUSR | S_IRGRP, uart_get_attr_close_delay, NULL); static DEVICE_ATTR(closing_wait, S_IRUSR | S_IRGRP, uart_get_attr_closing_wait, NULL); static DEVICE_ATTR(custom_divisor, S_IRUSR | S_IRGRP, uart_get_attr_custom_divisor, NULL); static DEVICE_ATTR(io_type, S_IRUSR | S_IRGRP, uart_get_attr_io_type, NULL); static DEVICE_ATTR(iomem_base, S_IRUSR | S_IRGRP, uart_get_attr_iomem_base, NULL); static DEVICE_ATTR(iomem_reg_shift, S_IRUSR | S_IRGRP, uart_get_attr_iomem_reg_shift, NULL); static struct attribute *tty_dev_attrs[] = { &dev_attr_type.attr, &dev_attr_line.attr, &dev_attr_port.attr, &dev_attr_irq.attr, &dev_attr_flags.attr, &dev_attr_xmit_fifo_size.attr, &dev_attr_uartclk.attr, &dev_attr_close_delay.attr, &dev_attr_closing_wait.attr, &dev_attr_custom_divisor.attr, &dev_attr_io_type.attr, &dev_attr_iomem_base.attr, &dev_attr_iomem_reg_shift.attr, NULL, }; static const struct attribute_group tty_dev_attr_group = { .attrs = tty_dev_attrs, }; static const struct attribute_group *tty_dev_attr_groups[] = { &tty_dev_attr_group, NULL }; /** * uart_add_one_port - attach a driver-defined port structure * @drv: pointer to the uart low level driver structure for this port * @uport: uart port structure to use for this port. * * This allows the driver to register its own uart_port structure * with the core driver. The main purpose is to allow the low * level uart drivers to expand uart_port, rather than having yet * more levels of structures. */ int uart_add_one_port(struct uart_driver *drv, struct uart_port *uport) { struct uart_state *state; struct tty_port *port; int ret = 0; struct device *tty_dev; BUG_ON(in_interrupt()); if (uport->line >= drv->nr) return -EINVAL; state = drv->state + uport->line; port = &state->port; mutex_lock(&port_mutex); mutex_lock(&port->mutex); if (state->uart_port) { ret = -EINVAL; goto out; } state->uart_port = uport; state->pm_state = -1; uport->cons = drv->cons; uport->state = state; /* * If this port is a console, then the spinlock is already * initialised. */ if (!(uart_console(uport) && (uport->cons->flags & CON_ENABLED))) { spin_lock_init(&uport->lock); lockdep_set_class(&uport->lock, &port_lock_key); } uart_configure_port(drv, state, uport); /* * Register the port whether it's detected or not. This allows * setserial to be used to alter this ports parameters. */ tty_dev = tty_port_register_device_attr(port, drv->tty_driver, uport->line, uport->dev, port, tty_dev_attr_groups); if (likely(!IS_ERR(tty_dev))) { device_set_wakeup_capable(tty_dev, 1); } else { printk(KERN_ERR "Cannot register tty device on line %d\n", uport->line); } /* * Ensure UPF_DEAD is not set. */ uport->flags &= ~UPF_DEAD; out: mutex_unlock(&port->mutex); mutex_unlock(&port_mutex); return ret; } /** * uart_remove_one_port - detach a driver defined port structure * @drv: pointer to the uart low level driver structure for this port * @uport: uart port structure for this port * * This unhooks (and hangs up) the specified port structure from the * core driver. No further calls will be made to the low-level code * for this port. */ int uart_remove_one_port(struct uart_driver *drv, struct uart_port *uport) { struct uart_state *state = drv->state + uport->line; struct tty_port *port = &state->port; BUG_ON(in_interrupt()); if (state->uart_port != uport) printk(KERN_ALERT "Removing wrong port: %p != %p\n", state->uart_port, uport); mutex_lock(&port_mutex); /* * Mark the port "dead" - this prevents any opens from * succeeding while we shut down the port. */ mutex_lock(&port->mutex); uport->flags |= UPF_DEAD; mutex_unlock(&port->mutex); /* * Remove the devices from the tty layer */ tty_unregister_device(drv->tty_driver, uport->line); if (port->tty) tty_vhangup(port->tty); /* * Free the port IO and memory resources, if any. */ if (uport->type != PORT_UNKNOWN) uport->ops->release_port(uport); /* * Indicate that there isn't a port here anymore. */ uport->type = PORT_UNKNOWN; state->uart_port = NULL; mutex_unlock(&port_mutex); return 0; } /* * Are the two ports equivalent? */ int uart_match_port(struct uart_port *port1, struct uart_port *port2) { if (port1->iotype != port2->iotype) return 0; switch (port1->iotype) { case UPIO_PORT: return (port1->iobase == port2->iobase); case UPIO_HUB6: return (port1->iobase == port2->iobase) && (port1->hub6 == port2->hub6); case UPIO_MEM: case UPIO_MEM32: case UPIO_AU: case UPIO_TSI: return (port1->mapbase == port2->mapbase); } return 0; } EXPORT_SYMBOL(uart_match_port); /** * uart_handle_dcd_change - handle a change of carrier detect state * @uport: uart_port structure for the open port * @status: new carrier detect status, nonzero if active */ void uart_handle_dcd_change(struct uart_port *uport, unsigned int status) { struct uart_state *state = uport->state; struct tty_port *port = &state->port; struct tty_ldisc *ld = NULL; struct pps_event_time ts; struct tty_struct *tty = port->tty; if (tty) ld = tty_ldisc_ref(tty); if (ld && ld->ops->dcd_change) pps_get_ts(&ts); uport->icount.dcd++; #ifdef CONFIG_HARD_PPS if ((uport->flags & UPF_HARDPPS_CD) && status) hardpps(); #endif if (port->flags & ASYNC_CHECK_CD) { if (status) wake_up_interruptible(&port->open_wait); else if (tty) tty_hangup(tty); } if (ld && ld->ops->dcd_change) ld->ops->dcd_change(tty, status, &ts); if (ld) tty_ldisc_deref(ld); } EXPORT_SYMBOL_GPL(uart_handle_dcd_change); /** * uart_handle_cts_change - handle a change of clear-to-send state * @uport: uart_port structure for the open port * @status: new clear to send status, nonzero if active */ void uart_handle_cts_change(struct uart_port *uport, unsigned int status) { struct tty_port *port = &uport->state->port; struct tty_struct *tty = port->tty; uport->icount.cts++; if (tty_port_cts_enabled(port)) { if (tty->hw_stopped) { if (status) { tty->hw_stopped = 0; uport->ops->start_tx(uport); uart_write_wakeup(uport); } } else { if (!status) { tty->hw_stopped = 1; uport->ops->stop_tx(uport); } } } } EXPORT_SYMBOL_GPL(uart_handle_cts_change); /** * uart_insert_char - push a char to the uart layer * * User is responsible to call tty_flip_buffer_push when they are done with * insertion. * * @port: corresponding port * @status: state of the serial port RX buffer (LSR for 8250) * @overrun: mask of overrun bits in @status * @ch: character to push * @flag: flag for the character (see TTY_NORMAL and friends) */ void uart_insert_char(struct uart_port *port, unsigned int status, unsigned int overrun, unsigned int ch, unsigned int flag) { struct tty_struct *tty = port->state->port.tty; if ((status & port->ignore_status_mask & ~overrun) == 0) if (tty_insert_flip_char(tty, ch, flag) == 0) ++port->icount.buf_overrun; /* * Overrun is special. Since it's reported immediately, * it doesn't affect the current character. */ if (status & ~port->ignore_status_mask & overrun) if (tty_insert_flip_char(tty, 0, TTY_OVERRUN) == 0) ++port->icount.buf_overrun; } EXPORT_SYMBOL_GPL(uart_insert_char); EXPORT_SYMBOL(uart_write_wakeup); EXPORT_SYMBOL(uart_register_driver); EXPORT_SYMBOL(uart_unregister_driver); EXPORT_SYMBOL(uart_suspend_port); EXPORT_SYMBOL(uart_resume_port); EXPORT_SYMBOL(uart_add_one_port); EXPORT_SYMBOL(uart_remove_one_port); MODULE_DESCRIPTION("Serial driver core"); MODULE_LICENSE("GPL");