/* * fs/eventpoll.c (Efficient event retrieval implementation) * Copyright (C) 2001,...,2009 Davide Libenzi * * This program is free software; you can redistribute it and/or modify * it under the terms of the GNU General Public License as published by * the Free Software Foundation; either version 2 of the License, or * (at your option) any later version. * * Davide Libenzi * */ #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include /* * LOCKING: * There are three level of locking required by epoll : * * 1) epmutex (mutex) * 2) ep->mtx (mutex) * 3) ep->lock (spinlock) * * The acquire order is the one listed above, from 1 to 3. * We need a spinlock (ep->lock) because we manipulate objects * from inside the poll callback, that might be triggered from * a wake_up() that in turn might be called from IRQ context. * So we can't sleep inside the poll callback and hence we need * a spinlock. During the event transfer loop (from kernel to * user space) we could end up sleeping due a copy_to_user(), so * we need a lock that will allow us to sleep. This lock is a * mutex (ep->mtx). It is acquired during the event transfer loop, * during epoll_ctl(EPOLL_CTL_DEL) and during eventpoll_release_file(). * Then we also need a global mutex to serialize eventpoll_release_file() * and ep_free(). * This mutex is acquired by ep_free() during the epoll file * cleanup path and it is also acquired by eventpoll_release_file() * if a file has been pushed inside an epoll set and it is then * close()d without a previous call to epoll_ctl(EPOLL_CTL_DEL). * It is also acquired when inserting an epoll fd onto another epoll * fd. We do this so that we walk the epoll tree and ensure that this * insertion does not create a cycle of epoll file descriptors, which * could lead to deadlock. We need a global mutex to prevent two * simultaneous inserts (A into B and B into A) from racing and * constructing a cycle without either insert observing that it is * going to. * It is necessary to acquire multiple "ep->mtx"es at once in the * case when one epoll fd is added to another. In this case, we * always acquire the locks in the order of nesting (i.e. after * epoll_ctl(e1, EPOLL_CTL_ADD, e2), e1->mtx will always be acquired * before e2->mtx). Since we disallow cycles of epoll file * descriptors, this ensures that the mutexes are well-ordered. In * order to communicate this nesting to lockdep, when walking a tree * of epoll file descriptors, we use the current recursion depth as * the lockdep subkey. * It is possible to drop the "ep->mtx" and to use the global * mutex "epmutex" (together with "ep->lock") to have it working, * but having "ep->mtx" will make the interface more scalable. * Events that require holding "epmutex" are very rare, while for * normal operations the epoll private "ep->mtx" will guarantee * a better scalability. */ /* Epoll private bits inside the event mask */ #define EP_PRIVATE_BITS (EPOLLWAKEUP | EPOLLONESHOT | EPOLLET) /* Maximum number of nesting allowed inside epoll sets */ #define EP_MAX_NESTS 4 #define EP_MAX_EVENTS (INT_MAX / sizeof(struct epoll_event)) #define EP_UNACTIVE_PTR ((void *) -1L) #define EP_ITEM_COST (sizeof(struct epitem) + sizeof(struct eppoll_entry)) struct epoll_filefd { struct file *file; int fd; }; /* * Structure used to track possible nested calls, for too deep recursions * and loop cycles. */ struct nested_call_node { struct list_head llink; void *cookie; void *ctx; }; /* * This structure is used as collector for nested calls, to check for * maximum recursion dept and loop cycles. */ struct nested_calls { struct list_head tasks_call_list; spinlock_t lock; }; /* * Each file descriptor added to the eventpoll interface will * have an entry of this type linked to the "rbr" RB tree. */ struct epitem { /* RB tree node used to link this structure to the eventpoll RB tree */ struct rb_node rbn; /* List header used to link this structure to the eventpoll ready list */ struct list_head rdllink; /* * Works together "struct eventpoll"->ovflist in keeping the * single linked chain of items. */ struct epitem *next; /* The file descriptor information this item refers to */ struct epoll_filefd ffd; /* Number of active wait queue attached to poll operations */ int nwait; /* List containing poll wait queues */ struct list_head pwqlist; /* The "container" of this item */ struct eventpoll *ep; /* List header used to link this item to the "struct file" items list */ struct list_head fllink; /* wakeup_source used when EPOLLWAKEUP is set */ struct wakeup_source *ws; /* The structure that describe the interested events and the source fd */ struct epoll_event event; }; /* * This structure is stored inside the "private_data" member of the file * structure and represents the main data structure for the eventpoll * interface. */ struct eventpoll { /* Protect the access to this structure */ spinlock_t lock; /* * This mutex is used to ensure that files are not removed * while epoll is using them. This is held during the event * collection loop, the file cleanup path, the epoll file exit * code and the ctl operations. */ struct mutex mtx; /* Wait queue used by sys_epoll_wait() */ wait_queue_head_t wq; /* Wait queue used by file->poll() */ wait_queue_head_t poll_wait; /* List of ready file descriptors */ struct list_head rdllist; /* RB tree root used to store monitored fd structs */ struct rb_root rbr; /* * This is a single linked list that chains all the "struct epitem" that * happened while transferring ready events to userspace w/out * holding ->lock. */ struct epitem *ovflist; /* wakeup_source used when ep_scan_ready_list is running */ struct wakeup_source *ws; /* The user that created the eventpoll descriptor */ struct user_struct *user; struct file *file; /* used to optimize loop detection check */ int visited; struct list_head visited_list_link; }; /* Wait structure used by the poll hooks */ struct eppoll_entry { /* List header used to link this structure to the "struct epitem" */ struct list_head llink; /* The "base" pointer is set to the container "struct epitem" */ struct epitem *base; /* * Wait queue item that will be linked to the target file wait * queue head. */ wait_queue_t wait; /* The wait queue head that linked the "wait" wait queue item */ wait_queue_head_t *whead; }; /* Wrapper struct used by poll queueing */ struct ep_pqueue { poll_table pt; struct epitem *epi; }; /* Used by the ep_send_events() function as callback private data */ struct ep_send_events_data { int maxevents; struct epoll_event __user *events; }; /* * Configuration options available inside /proc/sys/fs/epoll/ */ /* Maximum number of epoll watched descriptors, per user */ static long max_user_watches __read_mostly; /* * This mutex is used to serialize ep_free() and eventpoll_release_file(). */ static DEFINE_MUTEX(epmutex); /* Used to check for epoll file descriptor inclusion loops */ static struct nested_calls poll_loop_ncalls; /* Used for safe wake up implementation */ static struct nested_calls poll_safewake_ncalls; /* Used to call file's f_op->poll() under the nested calls boundaries */ static struct nested_calls poll_readywalk_ncalls; /* Slab cache used to allocate "struct epitem" */ static struct kmem_cache *epi_cache __read_mostly; /* Slab cache used to allocate "struct eppoll_entry" */ static struct kmem_cache *pwq_cache __read_mostly; /* Visited nodes during ep_loop_check(), so we can unset them when we finish */ static LIST_HEAD(visited_list); /* * List of files with newly added links, where we may need to limit the number * of emanating paths. Protected by the epmutex. */ static LIST_HEAD(tfile_check_list); #ifdef CONFIG_SYSCTL #include static long zero; static long long_max = LONG_MAX; ctl_table epoll_table[] = { { .procname = "max_user_watches", .data = &max_user_watches, .maxlen = sizeof(max_user_watches), .mode = 0644, .proc_handler = proc_doulongvec_minmax, .extra1 = &zero, .extra2 = &long_max, }, { } }; #endif /* CONFIG_SYSCTL */ static const struct file_operations eventpoll_fops; static inline int is_file_epoll(struct file *f) { return f->f_op == &eventpoll_fops; } /* Setup the structure that is used as key for the RB tree */ static inline void ep_set_ffd(struct epoll_filefd *ffd, struct file *file, int fd) { ffd->file = file; ffd->fd = fd; } /* Compare RB tree keys */ static inline int ep_cmp_ffd(struct epoll_filefd *p1, struct epoll_filefd *p2) { return (p1->file > p2->file ? +1: (p1->file < p2->file ? -1 : p1->fd - p2->fd)); } /* Tells us if the item is currently linked */ static inline int ep_is_linked(struct list_head *p) { return !list_empty(p); } static inline struct eppoll_entry *ep_pwq_from_wait(wait_queue_t *p) { return container_of(p, struct eppoll_entry, wait); } /* Get the "struct epitem" from a wait queue pointer */ static inline struct epitem *ep_item_from_wait(wait_queue_t *p) { return container_of(p, struct eppoll_entry, wait)->base; } /* Get the "struct epitem" from an epoll queue wrapper */ static inline struct epitem *ep_item_from_epqueue(poll_table *p) { return container_of(p, struct ep_pqueue, pt)->epi; } /* Tells if the epoll_ctl(2) operation needs an event copy from userspace */ static inline int ep_op_has_event(int op) { return op != EPOLL_CTL_DEL; } /* Initialize the poll safe wake up structure */ static void ep_nested_calls_init(struct nested_calls *ncalls) { INIT_LIST_HEAD(&ncalls->tasks_call_list); spin_lock_init(&ncalls->lock); } /** * ep_events_available - Checks if ready events might be available. * * @ep: Pointer to the eventpoll context. * * Returns: Returns a value different than zero if ready events are available, * or zero otherwise. */ static inline int ep_events_available(struct eventpoll *ep) { return !list_empty(&ep->rdllist) || ep->ovflist != EP_UNACTIVE_PTR; } /** * ep_call_nested - Perform a bound (possibly) nested call, by checking * that the recursion limit is not exceeded, and that * the same nested call (by the meaning of same cookie) is * no re-entered. * * @ncalls: Pointer to the nested_calls structure to be used for this call. * @max_nests: Maximum number of allowed nesting calls. * @nproc: Nested call core function pointer. * @priv: Opaque data to be passed to the @nproc callback. * @cookie: Cookie to be used to identify this nested call. * @ctx: This instance context. * * Returns: Returns the code returned by the @nproc callback, or -1 if * the maximum recursion limit has been exceeded. */ static int ep_call_nested(struct nested_calls *ncalls, int max_nests, int (*nproc)(void *, void *, int), void *priv, void *cookie, void *ctx) { int error, call_nests = 0; unsigned long flags; struct list_head *lsthead = &ncalls->tasks_call_list; struct nested_call_node *tncur; struct nested_call_node tnode; spin_lock_irqsave(&ncalls->lock, flags); /* * Try to see if the current task is already inside this wakeup call. * We use a list here, since the population inside this set is always * very much limited. */ list_for_each_entry(tncur, lsthead, llink) { if (tncur->ctx == ctx && (tncur->cookie == cookie || ++call_nests > max_nests)) { /* * Ops ... loop detected or maximum nest level reached. * We abort this wake by breaking the cycle itself. */ error = -1; goto out_unlock; } } /* Add the current task and cookie to the list */ tnode.ctx = ctx; tnode.cookie = cookie; list_add(&tnode.llink, lsthead); spin_unlock_irqrestore(&ncalls->lock, flags); /* Call the nested function */ error = (*nproc)(priv, cookie, call_nests); /* Remove the current task from the list */ spin_lock_irqsave(&ncalls->lock, flags); list_del(&tnode.llink); out_unlock: spin_unlock_irqrestore(&ncalls->lock, flags); return error; } /* * As described in commit 0ccf831cb lockdep: annotate epoll * the use of wait queues used by epoll is done in a very controlled * manner. Wake ups can nest inside each other, but are never done * with the same locking. For example: * * dfd = socket(...); * efd1 = epoll_create(); * efd2 = epoll_create(); * epoll_ctl(efd1, EPOLL_CTL_ADD, dfd, ...); * epoll_ctl(efd2, EPOLL_CTL_ADD, efd1, ...); * * When a packet arrives to the device underneath "dfd", the net code will * issue a wake_up() on its poll wake list. Epoll (efd1) has installed a * callback wakeup entry on that queue, and the wake_up() performed by the * "dfd" net code will end up in ep_poll_callback(). At this point epoll * (efd1) notices that it may have some event ready, so it needs to wake up * the waiters on its poll wait list (efd2). So it calls ep_poll_safewake() * that ends up in another wake_up(), after having checked about the * recursion constraints. That are, no more than EP_MAX_POLLWAKE_NESTS, to * avoid stack blasting. * * When CONFIG_DEBUG_LOCK_ALLOC is enabled, make sure lockdep can handle * this special case of epoll. */ #ifdef CONFIG_DEBUG_LOCK_ALLOC static inline void ep_wake_up_nested(wait_queue_head_t *wqueue, unsigned long events, int subclass) { unsigned long flags; spin_lock_irqsave_nested(&wqueue->lock, flags, subclass); wake_up_locked_poll(wqueue, events); spin_unlock_irqrestore(&wqueue->lock, flags); } #else static inline void ep_wake_up_nested(wait_queue_head_t *wqueue, unsigned long events, int subclass) { wake_up_poll(wqueue, events); } #endif static int ep_poll_wakeup_proc(void *priv, void *cookie, int call_nests) { ep_wake_up_nested((wait_queue_head_t *) cookie, POLLIN, 1 + call_nests); return 0; } /* * Perform a safe wake up of the poll wait list. The problem is that * with the new callback'd wake up system, it is possible that the * poll callback is reentered from inside the call to wake_up() done * on the poll wait queue head. The rule is that we cannot reenter the * wake up code from the same task more than EP_MAX_NESTS times, * and we cannot reenter the same wait queue head at all. This will * enable to have a hierarchy of epoll file descriptor of no more than * EP_MAX_NESTS deep. */ static void ep_poll_safewake(wait_queue_head_t *wq) { int this_cpu = get_cpu(); ep_call_nested(&poll_safewake_ncalls, EP_MAX_NESTS, ep_poll_wakeup_proc, NULL, wq, (void *) (long) this_cpu); put_cpu(); } static void ep_remove_wait_queue(struct eppoll_entry *pwq) { wait_queue_head_t *whead; rcu_read_lock(); /* If it is cleared by POLLFREE, it should be rcu-safe */ whead = rcu_dereference(pwq->whead); if (whead) remove_wait_queue(whead, &pwq->wait); rcu_read_unlock(); } /* * This function unregisters poll callbacks from the associated file * descriptor. Must be called with "mtx" held (or "epmutex" if called from * ep_free). */ static void ep_unregister_pollwait(struct eventpoll *ep, struct epitem *epi) { struct list_head *lsthead = &epi->pwqlist; struct eppoll_entry *pwq; while (!list_empty(lsthead)) { pwq = list_first_entry(lsthead, struct eppoll_entry, llink); list_del(&pwq->llink); ep_remove_wait_queue(pwq); kmem_cache_free(pwq_cache, pwq); } } /** * ep_scan_ready_list - Scans the ready list in a way that makes possible for * the scan code, to call f_op->poll(). Also allows for * O(NumReady) performance. * * @ep: Pointer to the epoll private data structure. * @sproc: Pointer to the scan callback. * @priv: Private opaque data passed to the @sproc callback. * @depth: The current depth of recursive f_op->poll calls. * * Returns: The same integer error code returned by the @sproc callback. */ static int ep_scan_ready_list(struct eventpoll *ep, int (*sproc)(struct eventpoll *, struct list_head *, void *), void *priv, int depth) { int error, pwake = 0; unsigned long flags; struct epitem *epi, *nepi; LIST_HEAD(txlist); /* * We need to lock this because we could be hit by * eventpoll_release_file() and epoll_ctl(). */ mutex_lock_nested(&ep->mtx, depth); /* * Steal the ready list, and re-init the original one to the * empty list. Also, set ep->ovflist to NULL so that events * happening while looping w/out locks, are not lost. We cannot * have the poll callback to queue directly on ep->rdllist, * because we want the "sproc" callback to be able to do it * in a lockless way. */ spin_lock_irqsave(&ep->lock, flags); list_splice_init(&ep->rdllist, &txlist); ep->ovflist = NULL; spin_unlock_irqrestore(&ep->lock, flags); /* * Now call the callback function. */ error = (*sproc)(ep, &txlist, priv); spin_lock_irqsave(&ep->lock, flags); /* * During the time we spent inside the "sproc" callback, some * other events might have been queued by the poll callback. * We re-insert them inside the main ready-list here. */ for (nepi = ep->ovflist; (epi = nepi) != NULL; nepi = epi->next, epi->next = EP_UNACTIVE_PTR) { /* * We need to check if the item is already in the list. * During the "sproc" callback execution time, items are * queued into ->ovflist but the "txlist" might already * contain them, and the list_splice() below takes care of them. */ if (!ep_is_linked(&epi->rdllink)) { list_add_tail(&epi->rdllink, &ep->rdllist); __pm_stay_awake(epi->ws); } } /* * We need to set back ep->ovflist to EP_UNACTIVE_PTR, so that after * releasing the lock, events will be queued in the normal way inside * ep->rdllist. */ ep->ovflist = EP_UNACTIVE_PTR; /* * Quickly re-inject items left on "txlist". */ list_splice(&txlist, &ep->rdllist); __pm_relax(ep->ws); if (!list_empty(&ep->rdllist)) { /* * Wake up (if active) both the eventpoll wait list and * the ->poll() wait list (delayed after we release the lock). */ if (waitqueue_active(&ep->wq)) wake_up_locked(&ep->wq); if (waitqueue_active(&ep->poll_wait)) pwake++; } spin_unlock_irqrestore(&ep->lock, flags); mutex_unlock(&ep->mtx); /* We have to call this outside the lock */ if (pwake) ep_poll_safewake(&ep->poll_wait); return error; } /* * Removes a "struct epitem" from the eventpoll RB tree and deallocates * all the associated resources. Must be called with "mtx" held. */ static int ep_remove(struct eventpoll *ep, struct epitem *epi) { unsigned long flags; struct file *file = epi->ffd.file; /* * Removes poll wait queue hooks. We _have_ to do this without holding * the "ep->lock" otherwise a deadlock might occur. This because of the * sequence of the lock acquisition. Here we do "ep->lock" then the wait * queue head lock when unregistering the wait queue. The wakeup callback * will run by holding the wait queue head lock and will call our callback * that will try to get "ep->lock". */ ep_unregister_pollwait(ep, epi); /* Remove the current item from the list of epoll hooks */ spin_lock(&file->f_lock); if (ep_is_linked(&epi->fllink)) list_del_init(&epi->fllink); spin_unlock(&file->f_lock); rb_erase(&epi->rbn, &ep->rbr); spin_lock_irqsave(&ep->lock, flags); if (ep_is_linked(&epi->rdllink)) list_del_init(&epi->rdllink); spin_unlock_irqrestore(&ep->lock, flags); wakeup_source_unregister(epi->ws); /* At this point it is safe to free the eventpoll item */ kmem_cache_free(epi_cache, epi); atomic_long_dec(&ep->user->epoll_watches); return 0; } static void ep_free(struct eventpoll *ep) { struct rb_node *rbp; struct epitem *epi; /* We need to release all tasks waiting for these file */ if (waitqueue_active(&ep->poll_wait)) ep_poll_safewake(&ep->poll_wait); /* * We need to lock this because we could be hit by * eventpoll_release_file() while we're freeing the "struct eventpoll". * We do not need to hold "ep->mtx" here because the epoll file * is on the way to be removed and no one has references to it * anymore. The only hit might come from eventpoll_release_file() but * holding "epmutex" is sufficient here. */ mutex_lock(&epmutex); /* * Walks through the whole tree by unregistering poll callbacks. */ for (rbp = rb_first(&ep->rbr); rbp; rbp = rb_next(rbp)) { epi = rb_entry(rbp, struct epitem, rbn); ep_unregister_pollwait(ep, epi); } /* * Walks through the whole tree by freeing each "struct epitem". At this * point we are sure no poll callbacks will be lingering around, and also by * holding "epmutex" we can be sure that no file cleanup code will hit * us during this operation. So we can avoid the lock on "ep->lock". */ while ((rbp = rb_first(&ep->rbr)) != NULL) { epi = rb_entry(rbp, struct epitem, rbn); ep_remove(ep, epi); } mutex_unlock(&epmutex); mutex_destroy(&ep->mtx); free_uid(ep->user); wakeup_source_unregister(ep->ws); kfree(ep); } static int ep_eventpoll_release(struct inode *inode, struct file *file) { struct eventpoll *ep = file->private_data; if (ep) ep_free(ep); return 0; } static int ep_read_events_proc(struct eventpoll *ep, struct list_head *head, void *priv) { struct epitem *epi, *tmp; poll_table pt; init_poll_funcptr(&pt, NULL); list_for_each_entry_safe(epi, tmp, head, rdllink) { pt._key = epi->event.events; if (epi->ffd.file->f_op->poll(epi->ffd.file, &pt) & epi->event.events) return POLLIN | POLLRDNORM; else { /* * Item has been dropped into the ready list by the poll * callback, but it's not actually ready, as far as * caller requested events goes. We can remove it here. */ __pm_relax(epi->ws); list_del_init(&epi->rdllink); } } return 0; } static int ep_poll_readyevents_proc(void *priv, void *cookie, int call_nests) { return ep_scan_ready_list(priv, ep_read_events_proc, NULL, call_nests + 1); } static unsigned int ep_eventpoll_poll(struct file *file, poll_table *wait) { int pollflags; struct eventpoll *ep = file->private_data; /* Insert inside our poll wait queue */ poll_wait(file, &ep->poll_wait, wait); /* * Proceed to find out if wanted events are really available inside * the ready list. This need to be done under ep_call_nested() * supervision, since the call to f_op->poll() done on listed files * could re-enter here. */ pollflags = ep_call_nested(&poll_readywalk_ncalls, EP_MAX_NESTS, ep_poll_readyevents_proc, ep, ep, current); return pollflags != -1 ? pollflags : 0; } #ifdef CONFIG_PROC_FS static int ep_show_fdinfo(struct seq_file *m, struct file *f) { struct eventpoll *ep = f->private_data; struct rb_node *rbp; int ret = 0; mutex_lock(&ep->mtx); for (rbp = rb_first(&ep->rbr); rbp; rbp = rb_next(rbp)) { struct epitem *epi = rb_entry(rbp, struct epitem, rbn); ret = seq_printf(m, "tfd: %8d events: %8x data: %16llx\n", epi->ffd.fd, epi->event.events, (long long)epi->event.data); if (ret) break; } mutex_unlock(&ep->mtx); return ret; } #endif /* File callbacks that implement the eventpoll file behaviour */ static const struct file_operations eventpoll_fops = { #ifdef CONFIG_PROC_FS .show_fdinfo = ep_show_fdinfo, #endif .release = ep_eventpoll_release, .poll = ep_eventpoll_poll, .llseek = noop_llseek, }; /* * This is called from eventpoll_release() to unlink files from the eventpoll * interface. We need to have this facility to cleanup correctly files that are * closed without being removed from the eventpoll interface. */ void eventpoll_release_file(struct file *file) { struct list_head *lsthead = &file->f_ep_links; struct eventpoll *ep; struct epitem *epi; /* * We don't want to get "file->f_lock" because it is not * necessary. It is not necessary because we're in the "struct file" * cleanup path, and this means that no one is using this file anymore. * So, for example, epoll_ctl() cannot hit here since if we reach this * point, the file counter already went to zero and fget() would fail. * The only hit might come from ep_free() but by holding the mutex * will correctly serialize the operation. We do need to acquire * "ep->mtx" after "epmutex" because ep_remove() requires it when called * from anywhere but ep_free(). * * Besides, ep_remove() acquires the lock, so we can't hold it here. */ mutex_lock(&epmutex); while (!list_empty(lsthead)) { epi = list_first_entry(lsthead, struct epitem, fllink); ep = epi->ep; list_del_init(&epi->fllink); mutex_lock_nested(&ep->mtx, 0); ep_remove(ep, epi); mutex_unlock(&ep->mtx); } mutex_unlock(&epmutex); } static int ep_alloc(struct eventpoll **pep) { int error; struct user_struct *user; struct eventpoll *ep; user = get_current_user(); error = -ENOMEM; ep = kzalloc(sizeof(*ep), GFP_KERNEL); if (unlikely(!ep)) goto free_uid; spin_lock_init(&ep->lock); mutex_init(&ep->mtx); init_waitqueue_head(&ep->wq); init_waitqueue_head(&ep->poll_wait); INIT_LIST_HEAD(&ep->rdllist); ep->rbr = RB_ROOT; ep->ovflist = EP_UNACTIVE_PTR; ep->user = user; *pep = ep; return 0; free_uid: free_uid(user); return error; } /* * Search the file inside the eventpoll tree. The RB tree operations * are protected by the "mtx" mutex, and ep_find() must be called with * "mtx" held. */ static struct epitem *ep_find(struct eventpoll *ep, struct file *file, int fd) { int kcmp; struct rb_node *rbp; struct epitem *epi, *epir = NULL; struct epoll_filefd ffd; ep_set_ffd(&ffd, file, fd); for (rbp = ep->rbr.rb_node; rbp; ) { epi = rb_entry(rbp, struct epitem, rbn); kcmp = ep_cmp_ffd(&ffd, &epi->ffd); if (kcmp > 0) rbp = rbp->rb_right; else if (kcmp < 0) rbp = rbp->rb_left; else { epir = epi; break; } } return epir; } /* * This is the callback that is passed to the wait queue wakeup * mechanism. It is called by the stored file descriptors when they * have events to report. */ static int ep_poll_callback(wait_queue_t *wait, unsigned mode, int sync, void *key) { int pwake = 0; unsigned long flags; struct epitem *epi = ep_item_from_wait(wait); struct eventpoll *ep = epi->ep; if ((unsigned long)key & POLLFREE) { ep_pwq_from_wait(wait)->whead = NULL; /* * whead = NULL above can race with ep_remove_wait_queue() * which can do another remove_wait_queue() after us, so we * can't use __remove_wait_queue(). whead->lock is held by * the caller. */ list_del_init(&wait->task_list); } spin_lock_irqsave(&ep->lock, flags); /* * If the event mask does not contain any poll(2) event, we consider the * descriptor to be disabled. This condition is likely the effect of the * EPOLLONESHOT bit that disables the descriptor when an event is received, * until the next EPOLL_CTL_MOD will be issued. */ if (!(epi->event.events & ~EP_PRIVATE_BITS)) goto out_unlock; /* * Check the events coming with the callback. At this stage, not * every device reports the events in the "key" parameter of the * callback. We need to be able to handle both cases here, hence the * test for "key" != NULL before the event match test. */ if (key && !((unsigned long) key & epi->event.events)) goto out_unlock; /* * If we are transferring events to userspace, we can hold no locks * (because we're accessing user memory, and because of linux f_op->poll() * semantics). All the events that happen during that period of time are * chained in ep->ovflist and requeued later on. */ if (unlikely(ep->ovflist != EP_UNACTIVE_PTR)) { if (epi->next == EP_UNACTIVE_PTR) { epi->next = ep->ovflist; ep->ovflist = epi; if (epi->ws) { /* * Activate ep->ws since epi->ws may get * deactivated at any time. */ __pm_stay_awake(ep->ws); } } goto out_unlock; } /* If this file is already in the ready list we exit soon */ if (!ep_is_linked(&epi->rdllink)) { list_add_tail(&epi->rdllink, &ep->rdllist); __pm_stay_awake(epi->ws); } /* * Wake up ( if active ) both the eventpoll wait list and the ->poll() * wait list. */ if (waitqueue_active(&ep->wq)) wake_up_locked(&ep->wq); if (waitqueue_active(&ep->poll_wait)) pwake++; out_unlock: spin_unlock_irqrestore(&ep->lock, flags); /* We have to call this outside the lock */ if (pwake) ep_poll_safewake(&ep->poll_wait); return 1; } /* * This is the callback that is used to add our wait queue to the * target file wakeup lists. */ static void ep_ptable_queue_proc(struct file *file, wait_queue_head_t *whead, poll_table *pt) { struct epitem *epi = ep_item_from_epqueue(pt); struct eppoll_entry *pwq; if (epi->nwait >= 0 && (pwq = kmem_cache_alloc(pwq_cache, GFP_KERNEL))) { init_waitqueue_func_entry(&pwq->wait, ep_poll_callback); pwq->whead = whead; pwq->base = epi; add_wait_queue(whead, &pwq->wait); list_add_tail(&pwq->llink, &epi->pwqlist); epi->nwait++; } else { /* We have to signal that an error occurred */ epi->nwait = -1; } } static void ep_rbtree_insert(struct eventpoll *ep, struct epitem *epi) { int kcmp; struct rb_node **p = &ep->rbr.rb_node, *parent = NULL; struct epitem *epic; while (*p) { parent = *p; epic = rb_entry(parent, struct epitem, rbn); kcmp = ep_cmp_ffd(&epi->ffd, &epic->ffd); if (kcmp > 0) p = &parent->rb_right; else p = &parent->rb_left; } rb_link_node(&epi->rbn, parent, p); rb_insert_color(&epi->rbn, &ep->rbr); } #define PATH_ARR_SIZE 5 /* * These are the number paths of length 1 to 5, that we are allowing to emanate * from a single file of interest. For example, we allow 1000 paths of length * 1, to emanate from each file of interest. This essentially represents the * potential wakeup paths, which need to be limited in order to avoid massive * uncontrolled wakeup storms. The common use case should be a single ep which * is connected to n file sources. In this case each file source has 1 path * of length 1. Thus, the numbers below should be more than sufficient. These * path limits are enforced during an EPOLL_CTL_ADD operation, since a modify * and delete can't add additional paths. Protected by the epmutex. */ static const int path_limits[PATH_ARR_SIZE] = { 1000, 500, 100, 50, 10 }; static int path_count[PATH_ARR_SIZE]; static int path_count_inc(int nests) { /* Allow an arbitrary number of depth 1 paths */ if (nests == 0) return 0; if (++path_count[nests] > path_limits[nests]) return -1; return 0; } static void path_count_init(void) { int i; for (i = 0; i < PATH_ARR_SIZE; i++) path_count[i] = 0; } static int reverse_path_check_proc(void *priv, void *cookie, int call_nests) { int error = 0; struct file *file = priv; struct file *child_file; struct epitem *epi; list_for_each_entry(epi, &file->f_ep_links, fllink) { child_file = epi->ep->file; if (is_file_epoll(child_file)) { if (list_empty(&child_file->f_ep_links)) { if (path_count_inc(call_nests)) { error = -1; break; } } else { error = ep_call_nested(&poll_loop_ncalls, EP_MAX_NESTS, reverse_path_check_proc, child_file, child_file, current); } if (error != 0) break; } else { printk(KERN_ERR "reverse_path_check_proc: " "file is not an ep!\n"); } } return error; } /** * reverse_path_check - The tfile_check_list is list of file *, which have * links that are proposed to be newly added. We need to * make sure that those added links don't add too many * paths such that we will spend all our time waking up * eventpoll objects. * * Returns: Returns zero if the proposed links don't create too many paths, * -1 otherwise. */ static int reverse_path_check(void) { int error = 0; struct file *current_file; /* let's call this for all tfiles */ list_for_each_entry(current_file, &tfile_check_list, f_tfile_llink) { path_count_init(); error = ep_call_nested(&poll_loop_ncalls, EP_MAX_NESTS, reverse_path_check_proc, current_file, current_file, current); if (error) break; } return error; } static int ep_create_wakeup_source(struct epitem *epi) { const char *name; if (!epi->ep->ws) { epi->ep->ws = wakeup_source_register("eventpoll"); if (!epi->ep->ws) return -ENOMEM; } name = epi->ffd.file->f_path.dentry->d_name.name; epi->ws = wakeup_source_register(name); if (!epi->ws) return -ENOMEM; return 0; } static void ep_destroy_wakeup_source(struct epitem *epi) { wakeup_source_unregister(epi->ws); epi->ws = NULL; } /* * Must be called with "mtx" held. */ static int ep_insert(struct eventpoll *ep, struct epoll_event *event, struct file *tfile, int fd) { int error, revents, pwake = 0; unsigned long flags; long user_watches; struct epitem *epi; struct ep_pqueue epq; user_watches = atomic_long_read(&ep->user->epoll_watches); if (unlikely(user_watches >= max_user_watches)) return -ENOSPC; if (!(epi = kmem_cache_alloc(epi_cache, GFP_KERNEL))) return -ENOMEM; /* Item initialization follow here ... */ INIT_LIST_HEAD(&epi->rdllink); INIT_LIST_HEAD(&epi->fllink); INIT_LIST_HEAD(&epi->pwqlist); epi->ep = ep; ep_set_ffd(&epi->ffd, tfile, fd); epi->event = *event; epi->nwait = 0; epi->next = EP_UNACTIVE_PTR; if (epi->event.events & EPOLLWAKEUP) { error = ep_create_wakeup_source(epi); if (error) goto error_create_wakeup_source; } else { epi->ws = NULL; } /* Initialize the poll table using the queue callback */ epq.epi = epi; init_poll_funcptr(&epq.pt, ep_ptable_queue_proc); epq.pt._key = event->events; /* * Attach the item to the poll hooks and get current event bits. * We can safely use the file* here because its usage count has * been increased by the caller of this function. Note that after * this operation completes, the poll callback can start hitting * the new item. */ revents = tfile->f_op->poll(tfile, &epq.pt); /* * We have to check if something went wrong during the poll wait queue * install process. Namely an allocation for a wait queue failed due * high memory pressure. */ error = -ENOMEM; if (epi->nwait < 0) goto error_unregister; /* Add the current item to the list of active epoll hook for this file */ spin_lock(&tfile->f_lock); list_add_tail(&epi->fllink, &tfile->f_ep_links); spin_unlock(&tfile->f_lock); /* * Add the current item to the RB tree. All RB tree operations are * protected by "mtx", and ep_insert() is called with "mtx" held. */ ep_rbtree_insert(ep, epi); /* now check if we've created too many backpaths */ error = -EINVAL; if (reverse_path_check()) goto error_remove_epi; /* We have to drop the new item inside our item list to keep track of it */ spin_lock_irqsave(&ep->lock, flags); /* If the file is already "ready" we drop it inside the ready list */ if ((revents & event->events) && !ep_is_linked(&epi->rdllink)) { list_add_tail(&epi->rdllink, &ep->rdllist); __pm_stay_awake(epi->ws); /* Notify waiting tasks that events are available */ if (waitqueue_active(&ep->wq)) wake_up_locked(&ep->wq); if (waitqueue_active(&ep->poll_wait)) pwake++; } spin_unlock_irqrestore(&ep->lock, flags); atomic_long_inc(&ep->user->epoll_watches); /* We have to call this outside the lock */ if (pwake) ep_poll_safewake(&ep->poll_wait); return 0; error_remove_epi: spin_lock(&tfile->f_lock); if (ep_is_linked(&epi->fllink)) list_del_init(&epi->fllink); spin_unlock(&tfile->f_lock); rb_erase(&epi->rbn, &ep->rbr); error_unregister: ep_unregister_pollwait(ep, epi); /* * We need to do this because an event could have been arrived on some * allocated wait queue. Note that we don't care about the ep->ovflist * list, since that is used/cleaned only inside a section bound by "mtx". * And ep_insert() is called with "mtx" held. */ spin_lock_irqsave(&ep->lock, flags); if (ep_is_linked(&epi->rdllink)) list_del_init(&epi->rdllink); spin_unlock_irqrestore(&ep->lock, flags); wakeup_source_unregister(epi->ws); error_create_wakeup_source: kmem_cache_free(epi_cache, epi); return error; } /* * Modify the interest event mask by dropping an event if the new mask * has a match in the current file status. Must be called with "mtx" held. */ static int ep_modify(struct eventpoll *ep, struct epitem *epi, struct epoll_event *event) { int pwake = 0; unsigned int revents; poll_table pt; init_poll_funcptr(&pt, NULL); /* * Set the new event interest mask before calling f_op->poll(); * otherwise we might miss an event that happens between the * f_op->poll() call and the new event set registering. */ epi->event.events = event->events; /* need barrier below */ pt._key = event->events; epi->event.data = event->data; /* protected by mtx */ if (epi->event.events & EPOLLWAKEUP) { if (!epi->ws) ep_create_wakeup_source(epi); } else if (epi->ws) { ep_destroy_wakeup_source(epi); } /* * The following barrier has two effects: * * 1) Flush epi changes above to other CPUs. This ensures * we do not miss events from ep_poll_callback if an * event occurs immediately after we call f_op->poll(). * We need this because we did not take ep->lock while * changing epi above (but ep_poll_callback does take * ep->lock). * * 2) We also need to ensure we do not miss _past_ events * when calling f_op->poll(). This barrier also * pairs with the barrier in wq_has_sleeper (see * comments for wq_has_sleeper). * * This barrier will now guarantee ep_poll_callback or f_op->poll * (or both) will notice the readiness of an item. */ smp_mb(); /* * Get current event bits. We can safely use the file* here because * its usage count has been increased by the caller of this function. */ revents = epi->ffd.file->f_op->poll(epi->ffd.file, &pt); /* * If the item is "hot" and it is not registered inside the ready * list, push it inside. */ if (revents & event->events) { spin_lock_irq(&ep->lock); if (!ep_is_linked(&epi->rdllink)) { list_add_tail(&epi->rdllink, &ep->rdllist); __pm_stay_awake(epi->ws); /* Notify waiting tasks that events are available */ if (waitqueue_active(&ep->wq)) wake_up_locked(&ep->wq); if (waitqueue_active(&ep->poll_wait)) pwake++; } spin_unlock_irq(&ep->lock); } /* We have to call this outside the lock */ if (pwake) ep_poll_safewake(&ep->poll_wait); return 0; } static int ep_send_events_proc(struct eventpoll *ep, struct list_head *head, void *priv) { struct ep_send_events_data *esed = priv; int eventcnt; unsigned int revents; struct epitem *epi; struct epoll_event __user *uevent; poll_table pt; init_poll_funcptr(&pt, NULL); /* * We can loop without lock because we are passed a task private list. * Items cannot vanish during the loop because ep_scan_ready_list() is * holding "mtx" during this call. */ for (eventcnt = 0, uevent = esed->events; !list_empty(head) && eventcnt < esed->maxevents;) { epi = list_first_entry(head, struct epitem, rdllink); /* * Activate ep->ws before deactivating epi->ws to prevent * triggering auto-suspend here (in case we reactive epi->ws * below). * * This could be rearranged to delay the deactivation of epi->ws * instead, but then epi->ws would temporarily be out of sync * with ep_is_linked(). */ if (epi->ws && epi->ws->active) __pm_stay_awake(ep->ws); __pm_relax(epi->ws); list_del_init(&epi->rdllink); pt._key = epi->event.events; revents = epi->ffd.file->f_op->poll(epi->ffd.file, &pt) & epi->event.events; /* * If the event mask intersect the caller-requested one, * deliver the event to userspace. Again, ep_scan_ready_list() * is holding "mtx", so no operations coming from userspace * can change the item. */ if (revents) { if (__put_user(revents, &uevent->events) || __put_user(epi->event.data, &uevent->data)) { list_add(&epi->rdllink, head); __pm_stay_awake(epi->ws); return eventcnt ? eventcnt : -EFAULT; } eventcnt++; uevent++; if (epi->event.events & EPOLLONESHOT) epi->event.events &= EP_PRIVATE_BITS; else if (!(epi->event.events & EPOLLET)) { /* * If this file has been added with Level * Trigger mode, we need to insert back inside * the ready list, so that the next call to * epoll_wait() will check again the events * availability. At this point, no one can insert * into ep->rdllist besides us. The epoll_ctl() * callers are locked out by * ep_scan_ready_list() holding "mtx" and the * poll callback will queue them in ep->ovflist. */ list_add_tail(&epi->rdllink, &ep->rdllist); __pm_stay_awake(epi->ws); } } } return eventcnt; } static int ep_send_events(struct eventpoll *ep, struct epoll_event __user *events, int maxevents) { struct ep_send_events_data esed; esed.maxevents = maxevents; esed.events = events; return ep_scan_ready_list(ep, ep_send_events_proc, &esed, 0); } static inline struct timespec ep_set_mstimeout(long ms) { struct timespec now, ts = { .tv_sec = ms / MSEC_PER_SEC, .tv_nsec = NSEC_PER_MSEC * (ms % MSEC_PER_SEC), }; ktime_get_ts(&now); return timespec_add_safe(now, ts); } /** * ep_poll - Retrieves ready events, and delivers them to the caller supplied * event buffer. * * @ep: Pointer to the eventpoll context. * @events: Pointer to the userspace buffer where the ready events should be * stored. * @maxevents: Size (in terms of number of events) of the caller event buffer. * @timeout: Maximum timeout for the ready events fetch operation, in * milliseconds. If the @timeout is zero, the function will not block, * while if the @timeout is less than zero, the function will block * until at least one event has been retrieved (or an error * occurred). * * Returns: Returns the number of ready events which have been fetched, or an * error code, in case of error. */ static int ep_poll(struct eventpoll *ep, struct epoll_event __user *events, int maxevents, long timeout) { int res = 0, eavail, timed_out = 0; unsigned long flags; long slack = 0; wait_queue_t wait; ktime_t expires, *to = NULL; if (timeout > 0) { struct timespec end_time = ep_set_mstimeout(timeout); slack = select_estimate_accuracy(&end_time); to = &expires; *to = timespec_to_ktime(end_time); } else if (timeout == 0) { /* * Avoid the unnecessary trip to the wait queue loop, if the * caller specified a non blocking operation. */ timed_out = 1; spin_lock_irqsave(&ep->lock, flags); goto check_events; } fetch_events: spin_lock_irqsave(&ep->lock, flags); if (!ep_events_available(ep)) { /* * We don't have any available event to return to the caller. * We need to sleep here, and we will be wake up by * ep_poll_callback() when events will become available. */ init_waitqueue_entry(&wait, current); __add_wait_queue_exclusive(&ep->wq, &wait); for (;;) { /* * We don't want to sleep if the ep_poll_callback() sends us * a wakeup in between. That's why we set the task state * to TASK_INTERRUPTIBLE before doing the checks. */ set_current_state(TASK_INTERRUPTIBLE); if (ep_events_available(ep) || timed_out) break; if (signal_pending(current)) { res = -EINTR; break; } spin_unlock_irqrestore(&ep->lock, flags); if (!schedule_hrtimeout_range(to, slack, HRTIMER_MODE_ABS)) timed_out = 1; spin_lock_irqsave(&ep->lock, flags); } __remove_wait_queue(&ep->wq, &wait); set_current_state(TASK_RUNNING); } check_events: /* Is it worth to try to dig for events ? */ eavail = ep_events_available(ep); spin_unlock_irqrestore(&ep->lock, flags); /* * Try to transfer events to user space. In case we get 0 events and * there's still timeout left over, we go trying again in search of * more luck. */ if (!res && eavail && !(res = ep_send_events(ep, events, maxevents)) && !timed_out) goto fetch_events; return res; } /** * ep_loop_check_proc - Callback function to be passed to the @ep_call_nested() * API, to verify that adding an epoll file inside another * epoll structure, does not violate the constraints, in * terms of closed loops, or too deep chains (which can * result in excessive stack usage). * * @priv: Pointer to the epoll file to be currently checked. * @cookie: Original cookie for this call. This is the top-of-the-chain epoll * data structure pointer. * @call_nests: Current dept of the @ep_call_nested() call stack. * * Returns: Returns zero if adding the epoll @file inside current epoll * structure @ep does not violate the constraints, or -1 otherwise. */ static int ep_loop_check_proc(void *priv, void *cookie, int call_nests) { int error = 0; struct file *file = priv; struct eventpoll *ep = file->private_data; struct eventpoll *ep_tovisit; struct rb_node *rbp; struct epitem *epi; mutex_lock_nested(&ep->mtx, call_nests + 1); ep->visited = 1; list_add(&ep->visited_list_link, &visited_list); for (rbp = rb_first(&ep->rbr); rbp; rbp = rb_next(rbp)) { epi = rb_entry(rbp, struct epitem, rbn); if (unlikely(is_file_epoll(epi->ffd.file))) { ep_tovisit = epi->ffd.file->private_data; if (ep_tovisit->visited) continue; error = ep_call_nested(&poll_loop_ncalls, EP_MAX_NESTS, ep_loop_check_proc, epi->ffd.file, ep_tovisit, current); if (error != 0) break; } else { /* * If we've reached a file that is not associated with * an ep, then we need to check if the newly added * links are going to add too many wakeup paths. We do * this by adding it to the tfile_check_list, if it's * not already there, and calling reverse_path_check() * during ep_insert(). */ if (list_empty(&epi->ffd.file->f_tfile_llink)) list_add(&epi->ffd.file->f_tfile_llink, &tfile_check_list); } } mutex_unlock(&ep->mtx); return error; } /** * ep_loop_check - Performs a check to verify that adding an epoll file (@file) * another epoll file (represented by @ep) does not create * closed loops or too deep chains. * * @ep: Pointer to the epoll private data structure. * @file: Pointer to the epoll file to be checked. * * Returns: Returns zero if adding the epoll @file inside current epoll * structure @ep does not violate the constraints, or -1 otherwise. */ static int ep_loop_check(struct eventpoll *ep, struct file *file) { int ret; struct eventpoll *ep_cur, *ep_next; ret = ep_call_nested(&poll_loop_ncalls, EP_MAX_NESTS, ep_loop_check_proc, file, ep, current); /* clear visited list */ list_for_each_entry_safe(ep_cur, ep_next, &visited_list, visited_list_link) { ep_cur->visited = 0; list_del(&ep_cur->visited_list_link); } return ret; } static void clear_tfile_check_list(void) { struct file *file; /* first clear the tfile_check_list */ while (!list_empty(&tfile_check_list)) { file = list_first_entry(&tfile_check_list, struct file, f_tfile_llink); list_del_init(&file->f_tfile_llink); } INIT_LIST_HEAD(&tfile_check_list); } /* * Open an eventpoll file descriptor. */ SYSCALL_DEFINE1(epoll_create1, int, flags) { int error, fd; struct eventpoll *ep = NULL; struct file *file; /* Check the EPOLL_* constant for consistency. */ BUILD_BUG_ON(EPOLL_CLOEXEC != O_CLOEXEC); if (flags & ~EPOLL_CLOEXEC) return -EINVAL; /* * Create the internal data structure ("struct eventpoll"). */ error = ep_alloc(&ep); if (error < 0) return error; /* * Creates all the items needed to setup an eventpoll file. That is, * a file structure and a free file descriptor. */ fd = get_unused_fd_flags(O_RDWR | (flags & O_CLOEXEC)); if (fd < 0) { error = fd; goto out_free_ep; } file = anon_inode_getfile("[eventpoll]", &eventpoll_fops, ep, O_RDWR | (flags & O_CLOEXEC)); if (IS_ERR(file)) { error = PTR_ERR(file); goto out_free_fd; } ep->file = file; fd_install(fd, file); return fd; out_free_fd: put_unused_fd(fd); out_free_ep: ep_free(ep); return error; } SYSCALL_DEFINE1(epoll_create, int, size) { if (size <= 0) return -EINVAL; return sys_epoll_create1(0); } /* * The following function implements the controller interface for * the eventpoll file that enables the insertion/removal/change of * file descriptors inside the interest set. */ SYSCALL_DEFINE4(epoll_ctl, int, epfd, int, op, int, fd, struct epoll_event __user *, event) { int error; int did_lock_epmutex = 0; struct file *file, *tfile; struct eventpoll *ep; struct epitem *epi; struct epoll_event epds; error = -EFAULT; if (ep_op_has_event(op) && copy_from_user(&epds, event, sizeof(struct epoll_event))) goto error_return; /* Get the "struct file *" for the eventpoll file */ error = -EBADF; file = fget(epfd); if (!file) goto error_return; /* Get the "struct file *" for the target file */ tfile = fget(fd); if (!tfile) goto error_fput; /* The target file descriptor must support poll */ error = -EPERM; if (!tfile->f_op || !tfile->f_op->poll) goto error_tgt_fput; /* Check if EPOLLWAKEUP is allowed */ if ((epds.events & EPOLLWAKEUP) && !capable(CAP_BLOCK_SUSPEND)) epds.events &= ~EPOLLWAKEUP; /* * We have to check that the file structure underneath the file descriptor * the user passed to us _is_ an eventpoll file. And also we do not permit * adding an epoll file descriptor inside itself. */ error = -EINVAL; if (file == tfile || !is_file_epoll(file)) goto error_tgt_fput; /* * At this point it is safe to assume that the "private_data" contains * our own data structure. */ ep = file->private_data; /* * When we insert an epoll file descriptor, inside another epoll file * descriptor, there is the change of creating closed loops, which are * better be handled here, than in more critical paths. While we are * checking for loops we also determine the list of files reachable * and hang them on the tfile_check_list, so we can check that we * haven't created too many possible wakeup paths. * * We need to hold the epmutex across both ep_insert and ep_remove * b/c we want to make sure we are looking at a coherent view of * epoll network. */ if (op == EPOLL_CTL_ADD || op == EPOLL_CTL_DEL) { mutex_lock(&epmutex); did_lock_epmutex = 1; } if (op == EPOLL_CTL_ADD) { if (is_file_epoll(tfile)) { error = -ELOOP; if (ep_loop_check(ep, tfile) != 0) { clear_tfile_check_list(); goto error_tgt_fput; } } else list_add(&tfile->f_tfile_llink, &tfile_check_list); } mutex_lock_nested(&ep->mtx, 0); /* * Try to lookup the file inside our RB tree, Since we grabbed "mtx" * above, we can be sure to be able to use the item looked up by * ep_find() till we release the mutex. */ epi = ep_find(ep, tfile, fd); error = -EINVAL; switch (op) { case EPOLL_CTL_ADD: if (!epi) { epds.events |= POLLERR | POLLHUP; error = ep_insert(ep, &epds, tfile, fd); } else error = -EEXIST; clear_tfile_check_list(); break; case EPOLL_CTL_DEL: if (epi) error = ep_remove(ep, epi); else error = -ENOENT; break; case EPOLL_CTL_MOD: if (epi) { epds.events |= POLLERR | POLLHUP; error = ep_modify(ep, epi, &epds); } else error = -ENOENT; break; } mutex_unlock(&ep->mtx); error_tgt_fput: if (did_lock_epmutex) mutex_unlock(&epmutex); fput(tfile); error_fput: fput(file); error_return: return error; } /* * Implement the event wait interface for the eventpoll file. It is the kernel * part of the user space epoll_wait(2). */ SYSCALL_DEFINE4(epoll_wait, int, epfd, struct epoll_event __user *, events, int, maxevents, int, timeout) { int error; struct fd f; struct eventpoll *ep; /* The maximum number of event must be greater than zero */ if (maxevents <= 0 || maxevents > EP_MAX_EVENTS) return -EINVAL; /* Verify that the area passed by the user is writeable */ if (!access_ok(VERIFY_WRITE, events, maxevents * sizeof(struct epoll_event))) return -EFAULT; /* Get the "struct file *" for the eventpoll file */ f = fdget(epfd); if (!f.file) return -EBADF; /* * We have to check that the file structure underneath the fd * the user passed to us _is_ an eventpoll file. */ error = -EINVAL; if (!is_file_epoll(f.file)) goto error_fput; /* * At this point it is safe to assume that the "private_data" contains * our own data structure. */ ep = f.file->private_data; /* Time to fish for events ... */ error = ep_poll(ep, events, maxevents, timeout); error_fput: fdput(f); return error; } /* * Implement the event wait interface for the eventpoll file. It is the kernel * part of the user space epoll_pwait(2). */ SYSCALL_DEFINE6(epoll_pwait, int, epfd, struct epoll_event __user *, events, int, maxevents, int, timeout, const sigset_t __user *, sigmask, size_t, sigsetsize) { int error; sigset_t ksigmask, sigsaved; /* * If the caller wants a certain signal mask to be set during the wait, * we apply it here. */ if (sigmask) { if (sigsetsize != sizeof(sigset_t)) return -EINVAL; if (copy_from_user(&ksigmask, sigmask, sizeof(ksigmask))) return -EFAULT; sigdelsetmask(&ksigmask, sigmask(SIGKILL) | sigmask(SIGSTOP)); sigprocmask(SIG_SETMASK, &ksigmask, &sigsaved); } error = sys_epoll_wait(epfd, events, maxevents, timeout); /* * If we changed the signal mask, we need to restore the original one. * In case we've got a signal while waiting, we do not restore the * signal mask yet, and we allow do_signal() to deliver the signal on * the way back to userspace, before the signal mask is restored. */ if (sigmask) { if (error == -EINTR) { memcpy(¤t->saved_sigmask, &sigsaved, sizeof(sigsaved)); set_restore_sigmask(); } else sigprocmask(SIG_SETMASK, &sigsaved, NULL); } return error; } static int __init eventpoll_init(void) { struct sysinfo si; si_meminfo(&si); /* * Allows top 4% of lomem to be allocated for epoll watches (per user). */ max_user_watches = (((si.totalram - si.totalhigh) / 25) << PAGE_SHIFT) / EP_ITEM_COST; BUG_ON(max_user_watches < 0); /* * Initialize the structure used to perform epoll file descriptor * inclusion loops checks. */ ep_nested_calls_init(&poll_loop_ncalls); /* Initialize the structure used to perform safe poll wait head wake ups */ ep_nested_calls_init(&poll_safewake_ncalls); /* Initialize the structure used to perform file's f_op->poll() calls */ ep_nested_calls_init(&poll_readywalk_ncalls); /* Allocates slab cache used to allocate "struct epitem" items */ epi_cache = kmem_cache_create("eventpoll_epi", sizeof(struct epitem), 0, SLAB_HWCACHE_ALIGN | SLAB_PANIC, NULL); /* Allocates slab cache used to allocate "struct eppoll_entry" */ pwq_cache = kmem_cache_create("eventpoll_pwq", sizeof(struct eppoll_entry), 0, SLAB_PANIC, NULL); return 0; } fs_initcall(eventpoll_init);