/* * linux/fs/fcntl.c * * Copyright (C) 1991, 1992 Linus Torvalds */ #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #define SETFL_MASK (O_APPEND | O_NONBLOCK | O_NDELAY | O_DIRECT | O_NOATIME) static int setfl(int fd, struct file * filp, unsigned long arg) { struct inode * inode = file_inode(filp); int error = 0; /* * O_APPEND cannot be cleared if the file is marked as append-only * and the file is open for write. */ if (((arg ^ filp->f_flags) & O_APPEND) && IS_APPEND(inode)) return -EPERM; /* O_NOATIME can only be set by the owner or superuser */ if ((arg & O_NOATIME) && !(filp->f_flags & O_NOATIME)) if (!inode_owner_or_capable(inode)) return -EPERM; /* required for strict SunOS emulation */ if (O_NONBLOCK != O_NDELAY) if (arg & O_NDELAY) arg |= O_NONBLOCK; if (arg & O_DIRECT) { if (!filp->f_mapping || !filp->f_mapping->a_ops || !filp->f_mapping->a_ops->direct_IO) return -EINVAL; } if (filp->f_op->check_flags) error = filp->f_op->check_flags(arg); if (error) return error; /* * ->fasync() is responsible for setting the FASYNC bit. */ if (((arg ^ filp->f_flags) & FASYNC) && filp->f_op->fasync) { error = filp->f_op->fasync(fd, filp, (arg & FASYNC) != 0); if (error < 0) goto out; if (error > 0) error = 0; } spin_lock(&filp->f_lock); filp->f_flags = (arg & SETFL_MASK) | (filp->f_flags & ~SETFL_MASK); spin_unlock(&filp->f_lock); out: return error; } static void f_modown(struct file *filp, struct pid *pid, enum pid_type type, int force) { write_lock_irq(&filp->f_owner.lock); if (force || !filp->f_owner.pid) { put_pid(filp->f_owner.pid); filp->f_owner.pid = get_pid(pid); filp->f_owner.pid_type = type; if (pid) { const struct cred *cred = current_cred(); filp->f_owner.uid = cred->uid; filp->f_owner.euid = cred->euid; } } write_unlock_irq(&filp->f_owner.lock); } int __f_setown(struct file *filp, struct pid *pid, enum pid_type type, int force) { int err; err = security_file_set_fowner(filp); if (err) return err; f_modown(filp, pid, type, force); return 0; } EXPORT_SYMBOL(__f_setown); int f_setown(struct file *filp, unsigned long arg, int force) { enum pid_type type; struct pid *pid; int who = arg; int result; type = PIDTYPE_PID; if (who < 0) { type = PIDTYPE_PGID; who = -who; } rcu_read_lock(); pid = find_vpid(who); result = __f_setown(filp, pid, type, force); rcu_read_unlock(); return result; } EXPORT_SYMBOL(f_setown); void f_delown(struct file *filp) { f_modown(filp, NULL, PIDTYPE_PID, 1); } pid_t f_getown(struct file *filp) { pid_t pid; read_lock(&filp->f_owner.lock); pid = pid_vnr(filp->f_owner.pid); if (filp->f_owner.pid_type == PIDTYPE_PGID) pid = -pid; read_unlock(&filp->f_owner.lock); return pid; } static int f_setown_ex(struct file *filp, unsigned long arg) { struct f_owner_ex __user *owner_p = (void __user *)arg; struct f_owner_ex owner; struct pid *pid; int type; int ret; ret = copy_from_user(&owner, owner_p, sizeof(owner)); if (ret) return -EFAULT; switch (owner.type) { case F_OWNER_TID: type = PIDTYPE_MAX; break; case F_OWNER_PID: type = PIDTYPE_PID; break; case F_OWNER_PGRP: type = PIDTYPE_PGID; break; default: return -EINVAL; } rcu_read_lock(); pid = find_vpid(owner.pid); if (owner.pid && !pid) ret = -ESRCH; else ret = __f_setown(filp, pid, type, 1); rcu_read_unlock(); return ret; } static int f_getown_ex(struct file *filp, unsigned long arg) { struct f_owner_ex __user *owner_p = (void __user *)arg; struct f_owner_ex owner; int ret = 0; read_lock(&filp->f_owner.lock); owner.pid = pid_vnr(filp->f_owner.pid); switch (filp->f_owner.pid_type) { case PIDTYPE_MAX: owner.type = F_OWNER_TID; break; case PIDTYPE_PID: owner.type = F_OWNER_PID; break; case PIDTYPE_PGID: owner.type = F_OWNER_PGRP; break; default: WARN_ON(1); ret = -EINVAL; break; } read_unlock(&filp->f_owner.lock); if (!ret) { ret = copy_to_user(owner_p, &owner, sizeof(owner)); if (ret) ret = -EFAULT; } return ret; } #ifdef CONFIG_CHECKPOINT_RESTORE static int f_getowner_uids(struct file *filp, unsigned long arg) { struct user_namespace *user_ns = current_user_ns(); uid_t __user *dst = (void __user *)arg; uid_t src[2]; int err; read_lock(&filp->f_owner.lock); src[0] = from_kuid(user_ns, filp->f_owner.uid); src[1] = from_kuid(user_ns, filp->f_owner.euid); read_unlock(&filp->f_owner.lock); err = put_user(src[0], &dst[0]); err |= put_user(src[1], &dst[1]); return err; } #else static int f_getowner_uids(struct file *filp, unsigned long arg) { return -EINVAL; } #endif static long do_fcntl(int fd, unsigned int cmd, unsigned long arg, struct file *filp) { long err = -EINVAL; switch (cmd) { case F_DUPFD: err = f_dupfd(arg, filp, 0); break; case F_DUPFD_CLOEXEC: err = f_dupfd(arg, filp, O_CLOEXEC); break; case F_GETFD: err = get_close_on_exec(fd) ? FD_CLOEXEC : 0; break; case F_SETFD: err = 0; set_close_on_exec(fd, arg & FD_CLOEXEC); break; case F_GETFL: err = filp->f_flags; break; case F_SETFL: err = setfl(fd, filp, arg); break; case F_GETLK: err = fcntl_getlk(filp, (struct flock __user *) arg); break; case F_SETLK: case F_SETLKW: err = fcntl_setlk(fd, filp, cmd, (struct flock __user *) arg); break; case F_GETOWN: /* * XXX If f_owner is a process group, the * negative return value will get converted * into an error. Oops. If we keep the * current syscall conventions, the only way * to fix this will be in libc. */ err = f_getown(filp); force_successful_syscall_return(); break; case F_SETOWN: err = f_setown(filp, arg, 1); break; case F_GETOWN_EX: err = f_getown_ex(filp, arg); break; case F_SETOWN_EX: err = f_setown_ex(filp, arg); break; case F_GETOWNER_UIDS: err = f_getowner_uids(filp, arg); break; case F_GETSIG: err = filp->f_owner.signum; break; case F_SETSIG: /* arg == 0 restores default behaviour. */ if (!valid_signal(arg)) { break; } err = 0; filp->f_owner.signum = arg; break; case F_GETLEASE: err = fcntl_getlease(filp); break; case F_SETLEASE: err = fcntl_setlease(fd, filp, arg); break; case F_NOTIFY: err = fcntl_dirnotify(fd, filp, arg); break; case F_SETPIPE_SZ: case F_GETPIPE_SZ: err = pipe_fcntl(filp, cmd, arg); break; default: break; } return err; } static int check_fcntl_cmd(unsigned cmd) { switch (cmd) { case F_DUPFD: case F_DUPFD_CLOEXEC: case F_GETFD: case F_SETFD: case F_GETFL: return 1; } return 0; } SYSCALL_DEFINE3(fcntl, unsigned int, fd, unsigned int, cmd, unsigned long, arg) { struct fd f = fdget_raw(fd); long err = -EBADF; if (!f.file) goto out; if (unlikely(f.file->f_mode & FMODE_PATH)) { if (!check_fcntl_cmd(cmd)) goto out1; } err = security_file_fcntl(f.file, cmd, arg); if (!err) err = do_fcntl(fd, cmd, arg, f.file); out1: fdput(f); out: return err; } #if BITS_PER_LONG == 32 SYSCALL_DEFINE3(fcntl64, unsigned int, fd, unsigned int, cmd, unsigned long, arg) { struct fd f = fdget_raw(fd); long err = -EBADF; if (!f.file) goto out; if (unlikely(f.file->f_mode & FMODE_PATH)) { if (!check_fcntl_cmd(cmd)) goto out1; } err = security_file_fcntl(f.file, cmd, arg); if (err) goto out1; switch (cmd) { case F_GETLK64: err = fcntl_getlk64(f.file, (struct flock64 __user *) arg); break; case F_SETLK64: case F_SETLKW64: err = fcntl_setlk64(fd, f.file, cmd, (struct flock64 __user *) arg); break; default: err = do_fcntl(fd, cmd, arg, f.file); break; } out1: fdput(f); out: return err; } #endif /* Table to convert sigio signal codes into poll band bitmaps */ static const long band_table[NSIGPOLL] = { POLLIN | POLLRDNORM, /* POLL_IN */ POLLOUT | POLLWRNORM | POLLWRBAND, /* POLL_OUT */ POLLIN | POLLRDNORM | POLLMSG, /* POLL_MSG */ POLLERR, /* POLL_ERR */ POLLPRI | POLLRDBAND, /* POLL_PRI */ POLLHUP | POLLERR /* POLL_HUP */ }; static inline int sigio_perm(struct task_struct *p, struct fown_struct *fown, int sig) { const struct cred *cred; int ret; rcu_read_lock(); cred = __task_cred(p); ret = ((uid_eq(fown->euid, GLOBAL_ROOT_UID) || uid_eq(fown->euid, cred->suid) || uid_eq(fown->euid, cred->uid) || uid_eq(fown->uid, cred->suid) || uid_eq(fown->uid, cred->uid)) && !security_file_send_sigiotask(p, fown, sig)); rcu_read_unlock(); return ret; } static void send_sigio_to_task(struct task_struct *p, struct fown_struct *fown, int fd, int reason, int group) { /* * F_SETSIG can change ->signum lockless in parallel, make * sure we read it once and use the same value throughout. */ int signum = ACCESS_ONCE(fown->signum); if (!sigio_perm(p, fown, signum)) return; switch (signum) { siginfo_t si; default: /* Queue a rt signal with the appropriate fd as its value. We use SI_SIGIO as the source, not SI_KERNEL, since kernel signals always get delivered even if we can't queue. Failure to queue in this case _should_ be reported; we fall back to SIGIO in that case. --sct */ si.si_signo = signum; si.si_errno = 0; si.si_code = reason; /* Make sure we are called with one of the POLL_* reasons, otherwise we could leak kernel stack into userspace. */ BUG_ON((reason & __SI_MASK) != __SI_POLL); if (reason - POLL_IN >= NSIGPOLL) si.si_band = ~0L; else si.si_band = band_table[reason - POLL_IN]; si.si_fd = fd; if (!do_send_sig_info(signum, &si, p, group)) break; /* fall-through: fall back on the old plain SIGIO signal */ case 0: do_send_sig_info(SIGIO, SEND_SIG_PRIV, p, group); } } void send_sigio(struct fown_struct *fown, int fd, int band) { struct task_struct *p; enum pid_type type; struct pid *pid; int group = 1; read_lock(&fown->lock); type = fown->pid_type; if (type == PIDTYPE_MAX) { group = 0; type = PIDTYPE_PID; } pid = fown->pid; if (!pid) goto out_unlock_fown; read_lock(&tasklist_lock); do_each_pid_task(pid, type, p) { send_sigio_to_task(p, fown, fd, band, group); } while_each_pid_task(pid, type, p); read_unlock(&tasklist_lock); out_unlock_fown: read_unlock(&fown->lock); } static void send_sigurg_to_task(struct task_struct *p, struct fown_struct *fown, int group) { if (sigio_perm(p, fown, SIGURG)) do_send_sig_info(SIGURG, SEND_SIG_PRIV, p, group); } int send_sigurg(struct fown_struct *fown) { struct task_struct *p; enum pid_type type; struct pid *pid; int group = 1; int ret = 0; read_lock(&fown->lock); type = fown->pid_type; if (type == PIDTYPE_MAX) { group = 0; type = PIDTYPE_PID; } pid = fown->pid; if (!pid) goto out_unlock_fown; ret = 1; read_lock(&tasklist_lock); do_each_pid_task(pid, type, p) { send_sigurg_to_task(p, fown, group); } while_each_pid_task(pid, type, p); read_unlock(&tasklist_lock); out_unlock_fown: read_unlock(&fown->lock); return ret; } static DEFINE_SPINLOCK(fasync_lock); static struct kmem_cache *fasync_cache __read_mostly; static void fasync_free_rcu(struct rcu_head *head) { kmem_cache_free(fasync_cache, container_of(head, struct fasync_struct, fa_rcu)); } /* * Remove a fasync entry. If successfully removed, return * positive and clear the FASYNC flag. If no entry exists, * do nothing and return 0. * * NOTE! It is very important that the FASYNC flag always * match the state "is the filp on a fasync list". * */ int fasync_remove_entry(struct file *filp, struct fasync_struct **fapp) { struct fasync_struct *fa, **fp; int result = 0; spin_lock(&filp->f_lock); spin_lock(&fasync_lock); for (fp = fapp; (fa = *fp) != NULL; fp = &fa->fa_next) { if (fa->fa_file != filp) continue; spin_lock_irq(&fa->fa_lock); fa->fa_file = NULL; spin_unlock_irq(&fa->fa_lock); *fp = fa->fa_next; call_rcu(&fa->fa_rcu, fasync_free_rcu); filp->f_flags &= ~FASYNC; result = 1; break; } spin_unlock(&fasync_lock); spin_unlock(&filp->f_lock); return result; } struct fasync_struct *fasync_alloc(void) { return kmem_cache_alloc(fasync_cache, GFP_KERNEL); } /* * NOTE! This can be used only for unused fasync entries: * entries that actually got inserted on the fasync list * need to be released by rcu - see fasync_remove_entry. */ void fasync_free(struct fasync_struct *new) { kmem_cache_free(fasync_cache, new); } /* * Insert a new entry into the fasync list. Return the pointer to the * old one if we didn't use the new one. * * NOTE! It is very important that the FASYNC flag always * match the state "is the filp on a fasync list". */ struct fasync_struct *fasync_insert_entry(int fd, struct file *filp, struct fasync_struct **fapp, struct fasync_struct *new) { struct fasync_struct *fa, **fp; spin_lock(&filp->f_lock); spin_lock(&fasync_lock); for (fp = fapp; (fa = *fp) != NULL; fp = &fa->fa_next) { if (fa->fa_file != filp) continue; spin_lock_irq(&fa->fa_lock); fa->fa_fd = fd; spin_unlock_irq(&fa->fa_lock); goto out; } spin_lock_init(&new->fa_lock); new->magic = FASYNC_MAGIC; new->fa_file = filp; new->fa_fd = fd; new->fa_next = *fapp; rcu_assign_pointer(*fapp, new); filp->f_flags |= FASYNC; out: spin_unlock(&fasync_lock); spin_unlock(&filp->f_lock); return fa; } /* * Add a fasync entry. Return negative on error, positive if * added, and zero if did nothing but change an existing one. */ static int fasync_add_entry(int fd, struct file *filp, struct fasync_struct **fapp) { struct fasync_struct *new; new = fasync_alloc(); if (!new) return -ENOMEM; /* * fasync_insert_entry() returns the old (update) entry if * it existed. * * So free the (unused) new entry and return 0 to let the * caller know that we didn't add any new fasync entries. */ if (fasync_insert_entry(fd, filp, fapp, new)) { fasync_free(new); return 0; } return 1; } /* * fasync_helper() is used by almost all character device drivers * to set up the fasync queue, and for regular files by the file * lease code. It returns negative on error, 0 if it did no changes * and positive if it added/deleted the entry. */ int fasync_helper(int fd, struct file * filp, int on, struct fasync_struct **fapp) { if (!on) return fasync_remove_entry(filp, fapp); return fasync_add_entry(fd, filp, fapp); } EXPORT_SYMBOL(fasync_helper); /* * rcu_read_lock() is held */ static void kill_fasync_rcu(struct fasync_struct *fa, int sig, int band) { while (fa) { struct fown_struct *fown; unsigned long flags; if (fa->magic != FASYNC_MAGIC) { printk(KERN_ERR "kill_fasync: bad magic number in " "fasync_struct!\n"); return; } spin_lock_irqsave(&fa->fa_lock, flags); if (fa->fa_file) { fown = &fa->fa_file->f_owner; /* Don't send SIGURG to processes which have not set a queued signum: SIGURG has its own default signalling mechanism. */ if (!(sig == SIGURG && fown->signum == 0)) send_sigio(fown, fa->fa_fd, band); } spin_unlock_irqrestore(&fa->fa_lock, flags); fa = rcu_dereference(fa->fa_next); } } void kill_fasync(struct fasync_struct **fp, int sig, int band) { /* First a quick test without locking: usually * the list is empty. */ if (*fp) { rcu_read_lock(); kill_fasync_rcu(rcu_dereference(*fp), sig, band); rcu_read_unlock(); } } EXPORT_SYMBOL(kill_fasync); static int __init fcntl_init(void) { /* * Please add new bits here to ensure allocation uniqueness. * Exceptions: O_NONBLOCK is a two bit define on parisc; O_NDELAY * is defined as O_NONBLOCK on some platforms and not on others. */ BUILD_BUG_ON(20 - 1 /* for O_RDONLY being 0 */ != HWEIGHT32( O_RDONLY | O_WRONLY | O_RDWR | O_CREAT | O_EXCL | O_NOCTTY | O_TRUNC | O_APPEND | /* O_NONBLOCK | */ __O_SYNC | O_DSYNC | FASYNC | O_DIRECT | O_LARGEFILE | O_DIRECTORY | O_NOFOLLOW | O_NOATIME | O_CLOEXEC | __FMODE_EXEC | O_PATH | __O_TMPFILE )); fasync_cache = kmem_cache_create("fasync_cache", sizeof(struct fasync_struct), 0, SLAB_PANIC, NULL); return 0; } module_init(fcntl_init)