#ifndef __LINUX_DCACHE_H #define __LINUX_DCACHE_H #include #include #include #include #include #include #include #include struct nameidata; struct path; struct vfsmount; /* * linux/include/linux/dcache.h * * Dirent cache data structures * * (C) Copyright 1997 Thomas Schoebel-Theuer, * with heavy changes by Linus Torvalds */ #define IS_ROOT(x) ((x) == (x)->d_parent) /* The hash is always the low bits of hash_len */ #ifdef __LITTLE_ENDIAN #define HASH_LEN_DECLARE u32 hash; u32 len; #else #define HASH_LEN_DECLARE u32 len; u32 hash; #endif /* * "quick string" -- eases parameter passing, but more importantly * saves "metadata" about the string (ie length and the hash). * * hash comes first so it snuggles against d_parent in the * dentry. */ struct qstr { union { struct { HASH_LEN_DECLARE; }; u64 hash_len; }; const unsigned char *name; }; #define QSTR_INIT(n,l) { { { .len = l } }, .name = n } #define hashlen_hash(hashlen) ((u32) (hashlen)) #define hashlen_len(hashlen) ((u32)((hashlen) >> 32)) struct dentry_stat_t { int nr_dentry; int nr_unused; int age_limit; /* age in seconds */ int want_pages; /* pages requested by system */ int dummy[2]; }; extern struct dentry_stat_t dentry_stat; /* Name hashing routines. Initial hash value */ /* Hash courtesy of the R5 hash in reiserfs modulo sign bits */ #define init_name_hash() 0 /* partial hash update function. Assume roughly 4 bits per character */ static inline unsigned long partial_name_hash(unsigned long c, unsigned long prevhash) { return (prevhash + (c << 4) + (c >> 4)) * 11; } /* * Finally: cut down the number of bits to a int value (and try to avoid * losing bits) */ static inline unsigned long end_name_hash(unsigned long hash) { return (unsigned int) hash; } /* Compute the hash for a name string. */ extern unsigned int full_name_hash(const unsigned char *, unsigned int); /* * Try to keep struct dentry aligned on 64 byte cachelines (this will * give reasonable cacheline footprint with larger lines without the * large memory footprint increase). */ #ifdef CONFIG_64BIT # define DNAME_INLINE_LEN 32 /* 192 bytes */ #else # ifdef CONFIG_SMP # define DNAME_INLINE_LEN 36 /* 128 bytes */ # else # define DNAME_INLINE_LEN 40 /* 128 bytes */ # endif #endif struct dentry { /* RCU lookup touched fields */ unsigned int d_flags; /* protected by d_lock */ seqcount_t d_seq; /* per dentry seqlock */ struct hlist_bl_node d_hash; /* lookup hash list */ struct dentry *d_parent; /* parent directory */ struct qstr d_name; struct inode *d_inode; /* Where the name belongs to - NULL is * negative */ unsigned char d_iname[DNAME_INLINE_LEN]; /* small names */ /* Ref lookup also touches following */ unsigned int d_count; /* protected by d_lock */ spinlock_t d_lock; /* per dentry lock */ const struct dentry_operations *d_op; struct super_block *d_sb; /* The root of the dentry tree */ unsigned long d_time; /* used by d_revalidate */ void *d_fsdata; /* fs-specific data */ struct list_head d_lru; /* LRU list */ /* * d_child and d_rcu can share memory */ union { struct list_head d_child; /* child of parent list */ struct rcu_head d_rcu; } d_u; struct list_head d_subdirs; /* our children */ struct hlist_node d_alias; /* inode alias list */ }; /* * dentry->d_lock spinlock nesting subclasses: * * 0: normal * 1: nested */ enum dentry_d_lock_class { DENTRY_D_LOCK_NORMAL, /* implicitly used by plain spin_lock() APIs. */ DENTRY_D_LOCK_NESTED }; struct dentry_operations { int (*d_revalidate)(struct dentry *, unsigned int); int (*d_hash)(const struct dentry *, const struct inode *, struct qstr *); int (*d_compare)(const struct dentry *, const struct inode *, const struct dentry *, const struct inode *, unsigned int, const char *, const struct qstr *); int (*d_delete)(const struct dentry *); void (*d_release)(struct dentry *); void (*d_prune)(struct dentry *); void (*d_iput)(struct dentry *, struct inode *); char *(*d_dname)(struct dentry *, char *, int); struct vfsmount *(*d_automount)(struct path *); int (*d_manage)(struct dentry *, bool); } ____cacheline_aligned; /* * Locking rules for dentry_operations callbacks are to be found in * Documentation/filesystems/Locking. Keep it updated! * * FUrther descriptions are found in Documentation/filesystems/vfs.txt. * Keep it updated too! */ /* d_flags entries */ #define DCACHE_OP_HASH 0x0001 #define DCACHE_OP_COMPARE 0x0002 #define DCACHE_OP_REVALIDATE 0x0004 #define DCACHE_OP_DELETE 0x0008 #define DCACHE_OP_PRUNE 0x0010 #define DCACHE_DISCONNECTED 0x0020 /* This dentry is possibly not currently connected to the dcache tree, in * which case its parent will either be itself, or will have this flag as * well. nfsd will not use a dentry with this bit set, but will first * endeavour to clear the bit either by discovering that it is connected, * or by performing lookup operations. Any filesystem which supports * nfsd_operations MUST have a lookup function which, if it finds a * directory inode with a DCACHE_DISCONNECTED dentry, will d_move that * dentry into place and return that dentry rather than the passed one, * typically using d_splice_alias. */ #define DCACHE_REFERENCED 0x0040 /* Recently used, don't discard. */ #define DCACHE_RCUACCESS 0x0080 /* Entry has ever been RCU-visible */ #define DCACHE_CANT_MOUNT 0x0100 #define DCACHE_GENOCIDE 0x0200 #define DCACHE_SHRINK_LIST 0x0400 #define DCACHE_NFSFS_RENAMED 0x1000 /* this dentry has been "silly renamed" and has to be deleted on the last * dput() */ #define DCACHE_COOKIE 0x2000 /* For use by dcookie subsystem */ #define DCACHE_FSNOTIFY_PARENT_WATCHED 0x4000 /* Parent inode is watched by some fsnotify listener */ #define DCACHE_MOUNTED 0x10000 /* is a mountpoint */ #define DCACHE_NEED_AUTOMOUNT 0x20000 /* handle automount on this dir */ #define DCACHE_MANAGE_TRANSIT 0x40000 /* manage transit from this dirent */ #define DCACHE_MANAGED_DENTRY \ (DCACHE_MOUNTED|DCACHE_NEED_AUTOMOUNT|DCACHE_MANAGE_TRANSIT) #define DCACHE_DENTRY_KILLED 0x100000 extern seqlock_t rename_lock; static inline int dname_external(struct dentry *dentry) { return dentry->d_name.name != dentry->d_iname; } /* * These are the low-level FS interfaces to the dcache.. */ extern void d_instantiate(struct dentry *, struct inode *); extern struct dentry * d_instantiate_unique(struct dentry *, struct inode *); extern struct dentry * d_materialise_unique(struct dentry *, struct inode *); extern void __d_drop(struct dentry *dentry); extern void d_drop(struct dentry *dentry); extern void d_delete(struct dentry *); extern void d_set_d_op(struct dentry *dentry, const struct dentry_operations *op); /* allocate/de-allocate */ extern struct dentry * d_alloc(struct dentry *, const struct qstr *); extern struct dentry * d_alloc_pseudo(struct super_block *, const struct qstr *); extern struct dentry * d_splice_alias(struct inode *, struct dentry *); extern struct dentry * d_add_ci(struct dentry *, struct inode *, struct qstr *); extern struct dentry *d_find_any_alias(struct inode *inode); extern struct dentry * d_obtain_alias(struct inode *); extern void shrink_dcache_sb(struct super_block *); extern void shrink_dcache_parent(struct dentry *); extern void shrink_dcache_for_umount(struct super_block *); extern int d_invalidate(struct dentry *); /* only used at mount-time */ extern struct dentry * d_make_root(struct inode *); /* - the ramfs-type tree */ extern void d_genocide(struct dentry *); extern struct dentry *d_find_alias(struct inode *); extern void d_prune_aliases(struct inode *); /* test whether we have any submounts in a subdir tree */ extern int have_submounts(struct dentry *); /* * This adds the entry to the hash queues. */ extern void d_rehash(struct dentry *); /** * d_add - add dentry to hash queues * @entry: dentry to add * @inode: The inode to attach to this dentry * * This adds the entry to the hash queues and initializes @inode. * The entry was actually filled in earlier during d_alloc(). */ static inline void d_add(struct dentry *entry, struct inode *inode) { d_instantiate(entry, inode); d_rehash(entry); } /** * d_add_unique - add dentry to hash queues without aliasing * @entry: dentry to add * @inode: The inode to attach to this dentry * * This adds the entry to the hash queues and initializes @inode. * The entry was actually filled in earlier during d_alloc(). */ static inline struct dentry *d_add_unique(struct dentry *entry, struct inode *inode) { struct dentry *res; res = d_instantiate_unique(entry, inode); d_rehash(res != NULL ? res : entry); return res; } extern void dentry_update_name_case(struct dentry *, struct qstr *); /* used for rename() and baskets */ extern void d_move(struct dentry *, struct dentry *); extern struct dentry *d_ancestor(struct dentry *, struct dentry *); /* appendix may either be NULL or be used for transname suffixes */ extern struct dentry *d_lookup(struct dentry *, struct qstr *); extern struct dentry *d_hash_and_lookup(struct dentry *, struct qstr *); extern struct dentry *__d_lookup(struct dentry *, struct qstr *); extern struct dentry *__d_lookup_rcu(const struct dentry *parent, const struct qstr *name, unsigned *seq, struct inode *inode); /** * __d_rcu_to_refcount - take a refcount on dentry if sequence check is ok * @dentry: dentry to take a ref on * @seq: seqcount to verify against * Returns: 0 on failure, else 1. * * __d_rcu_to_refcount operates on a dentry,seq pair that was returned * by __d_lookup_rcu, to get a reference on an rcu-walk dentry. */ static inline int __d_rcu_to_refcount(struct dentry *dentry, unsigned seq) { int ret = 0; assert_spin_locked(&dentry->d_lock); if (!read_seqcount_retry(&dentry->d_seq, seq)) { ret = 1; dentry->d_count++; } return ret; } /* validate "insecure" dentry pointer */ extern int d_validate(struct dentry *, struct dentry *); /* * helper function for dentry_operations.d_dname() members */ extern char *dynamic_dname(struct dentry *, char *, int, const char *, ...); extern char *__d_path(const struct path *, const struct path *, char *, int); extern char *d_absolute_path(const struct path *, char *, int); extern char *d_path(const struct path *, char *, int); extern char *d_path_with_unreachable(const struct path *, char *, int); extern char *dentry_path_raw(struct dentry *, char *, int); extern char *dentry_path(struct dentry *, char *, int); /* Allocation counts.. */ /** * dget, dget_dlock - get a reference to a dentry * @dentry: dentry to get a reference to * * Given a dentry or %NULL pointer increment the reference count * if appropriate and return the dentry. A dentry will not be * destroyed when it has references. */ static inline struct dentry *dget_dlock(struct dentry *dentry) { if (dentry) dentry->d_count++; return dentry; } static inline struct dentry *dget(struct dentry *dentry) { if (dentry) { spin_lock(&dentry->d_lock); dget_dlock(dentry); spin_unlock(&dentry->d_lock); } return dentry; } extern struct dentry *dget_parent(struct dentry *dentry); /** * d_unhashed - is dentry hashed * @dentry: entry to check * * Returns true if the dentry passed is not currently hashed. */ static inline int d_unhashed(struct dentry *dentry) { return hlist_bl_unhashed(&dentry->d_hash); } static inline int d_unlinked(struct dentry *dentry) { return d_unhashed(dentry) && !IS_ROOT(dentry); } static inline int cant_mount(struct dentry *dentry) { return (dentry->d_flags & DCACHE_CANT_MOUNT); } static inline void dont_mount(struct dentry *dentry) { spin_lock(&dentry->d_lock); dentry->d_flags |= DCACHE_CANT_MOUNT; spin_unlock(&dentry->d_lock); } extern void dput(struct dentry *); static inline bool d_managed(struct dentry *dentry) { return dentry->d_flags & DCACHE_MANAGED_DENTRY; } static inline bool d_mountpoint(struct dentry *dentry) { return dentry->d_flags & DCACHE_MOUNTED; } extern int sysctl_vfs_cache_pressure; #endif /* __LINUX_DCACHE_H */