#ifndef _LINUX_KERNEL_VTIME_H #define _LINUX_KERNEL_VTIME_H struct task_struct; #ifdef CONFIG_VIRT_CPU_ACCOUNTING extern void vtime_task_switch(struct task_struct *prev); extern void vtime_account_system(struct task_struct *tsk); extern void vtime_account_system_irqsafe(struct task_struct *tsk); extern void vtime_account_idle(struct task_struct *tsk); extern void vtime_account_user(struct task_struct *tsk); extern void vtime_account(struct task_struct *tsk); #else static inline void vtime_task_switch(struct task_struct *prev) { } static inline void vtime_account_system(struct task_struct *tsk) { } static inline void vtime_account_system_irqsafe(struct task_struct *tsk) { } static inline void vtime_account(struct task_struct *tsk) { } #endif #ifdef CONFIG_IRQ_TIME_ACCOUNTING extern void irqtime_account_irq(struct task_struct *tsk); #else static inline void irqtime_account_irq(struct task_struct *tsk) { } #endif static inline void vtime_account_irq_enter(struct task_struct *tsk) { /* * Hardirq can interrupt idle task anytime. So we need vtime_account() * that performs the idle check in CONFIG_VIRT_CPU_ACCOUNTING. * Softirq can also interrupt idle task directly if it calls * local_bh_enable(). Such case probably don't exist but we never know. * Ksoftirqd is not concerned because idle time is flushed on context * switch. Softirqs in the end of hardirqs are also not a problem because * the idle time is flushed on hardirq time already. */ vtime_account(tsk); irqtime_account_irq(tsk); } static inline void vtime_account_irq_exit(struct task_struct *tsk) { /* On hard|softirq exit we always account to hard|softirq cputime */ vtime_account_system(tsk); irqtime_account_irq(tsk); } #endif /* _LINUX_KERNEL_VTIME_H */