]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/blobdiff - arch/arm/Kconfig
Merge branch 'p-ti-linux-3.8.y' into p-ti-android-3.8.y
[android-sdk/kernel-video.git] / arch / arm / Kconfig
index 0e68a0b23280ac82fe74b903ef924e7d5be092d3..1def7c896b50902dc72b60cd61706fef9416bad1 100644 (file)
@@ -1647,7 +1647,7 @@ config ARCH_NR_GPIO
        default 1024 if ARCH_SHMOBILE || ARCH_TEGRA
        default 355 if ARCH_U8500
        default 264 if MACH_H4700
-       default 512 if SOC_OMAP5
+       default 512 if SOC_OMAP5 || SOC_DRA7XX
        default 288 if ARCH_VT8500
        default 0
        help
@@ -1876,6 +1876,15 @@ config XEN
        help
          Say Y if you want to run Linux in a Virtual Machine on Xen on ARM.
 
+config ARM_FLUSH_CONSOLE_ON_RESTART
+       bool "Force flush the console on restart"
+       help
+         If the console is locked while the system is rebooted, the messages
+         in the temporary logbuffer would not have propogated to all the
+         console drivers. This option forces the console lock to be
+         released if it failed to be acquired, which will cause all the
+         pending messages to be flushed.
+
 endmenu
 
 menu "Boot options"